NFCナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC Knowledge Base

ディスカッション

ソート順:
Hello NFC community:   NXP released the new PN7150 NFC Controller chip with enhanced power output, and there is also the new Arduino compatible demokit OM5578/PN7150ARD. See more information in the next pages:   PN7150: High performance full NFC Forum-compliant controlle|NXP OM5578/PN7150ARD: Demoboards for PN7150|NXP   There is also a new PN7120 SBC kit for arduino:   http://cache.nxp.com/documents/user_manual/UM11008.pdf http://cache.nxp.com/documents/user_manual/UM11008.pdf   Due to the Arduino interface pinout, these kits can also be used with Kinetis Freedom Boards. The target of this document is to create projects to use the NFC Controller lîbrary with the PN7120 or PN7150 together with a Kinetis host. Also you will find example projects created for the FRDM-K64F and FRDM-KL43Z.     Requirements:   - Kinetis Software Development Kit v1.3. -> Software Development Kit for Kinetis MCUs|NXP - KDS v3.x with KSDK v1.3 Eclipse Update Installed -> Kinetis Design Studio Integrated Development Enviro|NXP - Kinetis SDK project generator. Available from the "Downloads" tab of KSDK webpage -> Software Development Kit for Kinetis MCUs|NXP     CREATING NEW PROJECT   NOTE: In this step-by-step procedure the FRDM-K64F is used as reference. You can follow the guide according to your own Freedom board.   1) Open the KSDK project generator. 2) Enter the KSDK v1.3 installation path, give a name to the project, select your Freedom board and click on "Advanced":     3) In the advanced settings window enable the checkboxes for:   - Include BSP files - Generate standalone project - Kinetis Design Studio toolchain - Board (confirm that your board is shown in the drop-down menu)   NOTE: The path for the newly created project is set by default inside of the KSDK v1.3 installation. For a standalone project you can change the location, just remember such path to import the project to KDS workspace in a later step.   Leave the rest of configurations as default (New project, Platform library, no RTOS) and finally click on "Advanced Generate!".     4) From Kinetis Design Studio go to File -> Import.     5) Go to General -> Existing Projects into workspace and click "Next".     6) In "select root directory" browse to the location of the platform lib for the created project. By default this path would be:   C:\nxp\KSDK_1.3.0\examples\frdmk64f\user_apps\<project_name>\lib\ksdk_platform_lib\kds\<MCU>   <project_name>: The name given initially to the project. <MCU>: The corresponding device number (K64F12 in this case).   Make sure that the project check box is enabled and click on "Finish".     7) Select the KSDK platform library project and click on the "Hammer icon" to build it.     😎 Repeat steps 4 through 6, but this time browse to the location of the application project. In this example the path is:   C:\nxp\KSDK_1.3.0\examples\frdmk64f\user_apps\< project_name >\kds     INTEGRATING NFC CONTROLLER LIBRARY   The next steps describe how to integrate the NFC NCI library to your newly created project.   - The Arduino Interface Boards use the next pinout for communication between the OM5578/PN7150 or OM5577/PN7120 kits with the Freedom or Arduino boards:     As shown in the picture, the pinouts are similar except for the 5V connection. This leverages the enhanced output power feature of the PN7150 NFC Controller.   - We need to check the corresponding pins that will be used from the Freedom board. In this case, the connections to the FRDM-K64F board would be as next:   IMPORTANT: The pinout shown below corresponds to Rev E3 schematics of FRDM-K64F. For Rev D1 the pin used for IRQ (header location J2[2]) must be PTA0 instead of PTC12.     1) Open the file gpio_pins.c and add 2 pin configurations: 1 input pin called NFCCirqPin and 1 output pin called NFCCvenPin.   gpio_input_pin_user_config_t NFCCirqPin = {   .pinName = kGpioNFCCirq,   .config.isPullEnable = false,   .config.pullSelect = kPortPullUp,   .config.isPassiveFilterEnabled = false,   .config.interrupt = kPortIntDisabled, }; gpio_output_pin_user_config_t NFCCvenPin = {   .pinName = kGpioNFCCven,   .config.outputLogic = 1,   .config.slewRate = kPortSlowSlewRate,   .config.driveStrength = kPortLowDriveStrength, };   2) In the file gpio_pins.h add 2 extra elements to the gpio enumeration. Also add extern declarations for the 2 pins defined in the previous step.   NOTE: For FRDM-K64F the pins are PTC12 and PTC3. Select corresponding pins for your Freedom board.   extern gpio_input_pin_user_config_t NFCCirqPin; extern gpio_output_pin_user_config_t NFCCvenPin; /*! @brief Pin names */ enum _gpio_pins_pinNames {   kGpioSW2  = GPIO_MAKE_PIN(GPIOC_IDX, 6U),   kGpioSW3  = GPIO_MAKE_PIN(GPIOA_IDX, 4U),   kGpioSdhc0Cd  = GPIO_MAKE_PIN(GPIOE_IDX, 6U),   kGpioLED1     = GPIO_MAKE_PIN(GPIOE_IDX, 26U),   kGpioLED2     = GPIO_MAKE_PIN(GPIOB_IDX, 22U),   kGpioLED3     = GPIO_MAKE_PIN(GPIOB_IDX, 21U),   kGpioNFCCirq  = GPIO_MAKE_PIN(GPIOC_IDX,  12), /* GPIO for NFCC IRQ pin */   kGpioNFCCven  = GPIO_MAKE_PIN(GPIOC_IDX,  3),  /* GPIO for NFCC VEN pin */ }   3) In the file pin_mux.c define a function to configure the MUX setting of the required GPIO and I2C pins to interface with the NFC Controller.   void configure_nfcc_pins(void) {   /** I2C_SDA **/   PORT_HAL_SetMuxMode(PORTE,25u,kPortMuxAlt5);   PORT_HAL_SetOpenDrainCmd(PORTE,25u,true);   /** I2C_SCL **/   PORT_HAL_SetMuxMode(PORTE,24u,kPortMuxAlt5);   PORT_HAL_SetOpenDrainCmd(PORTE,24u,true);   /* NFCC IRQ */   PORT_HAL_SetMuxMode(PORTC,12u,kPortMuxAsGpio);   /* NFCC VEN */   PORT_HAL_SetMuxMode(PORTC,3u,kPortMuxAsGpio); }   NOTES: - Check the corresponding pins on your Freedom board. FRDM-K64F uses PTC12/PTC3 as GPIOs while PTE24/PTE25 are configured as I2C pins. For I2C pins also check the MUX number in the device's Reference Manual (e.g. PTE24/PTE25 in K64F have the I2C function in ALT5). - This function needs to be called from your project to configure the required pins. e.g. from hardware_init(). - Some Freedom boards share the I2C pins of the Arduino compatible header with an on-board I2C device (e.g. accelerometer), with SDA/SCL pull-up resistors populated already. If this is not the case for your board, make sure to place external pull-ups to  MCU VDD or enable the internal pull-ups as temporary workaround.   4) Add the prototype of the function to the header file pin_mux.h.   /* ** =================================================== **     Method :  configure_nfcc_pins */ /*! **     @brief **         Set mux configuration for I2C and GPIO pins **         to interface with the NFC Controller. */ /* ==================================================*/ void configure_nfcc_pins(void);   5) Copy the folders NfcLibrary and TML to the project folder. The file fsl_i2c_irq.c is also required. In this case the file is found in the next path:   C:\nxp\KSDK_1.3.0\examples\frdmk64f\user_apps\<project_name>\platform\drivers\src\i2c   NOTE: If the project was not created in standalone mode, just search the fsl_i2c_irq.c file from your KSDK installation.       6) Add the NfcLibrary and TML folders with all its subfolders and files to the project's tree, so the lilbrary is part of the build. Also add the file fsl_i2c_irq.c to the project. In KDS you can drag and drop folders and files to the project explorer view.       7) Add the compiler include paths for the inc folders.     😎 From the KDS preprocessor settings add or remove the next conditional compilation macros according to your functional requirements:   CARDEMU_SUPPORT: The NFC Controler host (MCU) can emulate a contactless card which can be accessed by an external Reader/Writer. P2P_SUPPORT: The host MCU can establish a 2-way communication accesing to or sending data to an external Reader/Writer. RW_SUPPORT: With this mode the host can access a remote contactless tag/card via the NFC Controller. NCI-DEBUG: If defined, all information transferred between the host MCU and the NFC Controller Interface (commands, responses, notifications, data) is echoed to console for debug purposes.     9) The file tml.h includes the macro NFCC_I2C_INSTANCE which defines the I2C module to use. For FRDM-K64F the module is I2C0. Set this macro according to your Freedom board.   /* NFC Controller I2C interface configuration */ #define NFCC_I2C_INSTANCE  0   At this point the project is ready to use the NFC Controller library and interface the Kinetis Freedom board with PN7120 or PN7150 NFC Controllers.     DEMO PROJECTS   At the end of this document you will find 2 example project packages for the FRDM-K64F and FRDM-KL43Z. Both of the projects can be used with either the OM5578/PN7150 or OM5577/PN7120 kits using the Arduino interface boards.   Each ZIP package includes 2 projects (example application and KSDK library). Unzip the package and import the projects from the resulting location.   Do not select "Copy projects into workspace" in KDS. If you do so the build will fail due to the linked source files not copied over.   The projects must be built in the next order:   1- Platform library project (FRDM-xxx_NFCNCI_Example\lib\ksdk_platform_lib\kds\<MCU>) 2- Demo project (FRDM-xxx_NFCNCI_Example\kds)   The OpenSDA virtual COM port is used to send data to a terminal at 115200 baud. Below an explanation on how to test the different project example features.   RW mode:   - Placing a tag with a single text, URI or vCard NDEF record next to the NFC reader antenna. Examples:         P2P mode:   - Bring an android phone with NFC enabled close to the NFC controller antenna and use the "beaming" feature. In the case below the NXP home page is "beamed" from the adroid phone's explorer. After this, the NFC enabled phone will receive the "Test" NDEF record.                     CARD EMULATION mode     For this mode it is required to remove the P2P_SUPPORT macro and rebuild/reprogram the project.   - Bringing an android phone set to read a NFC tag close to the NFC controller board. The NFC enabled phone will detecta T4T tag type with the "Test" NDEF record.     I hope you can find this document useful. Any questions or doubts please let me know in the comments.   Jorge Gonzalez NXP Technical Support
記事全体を表示
This is a step by step guide on setting up and running a simple NFC Demo App using the PN7150 NFC Controller SBC Kit for Arduino (OM5578/PN7150ARD) with a UDOO NEO board which uses an i.MX6SX and it's Arduino pin compatible. 1. Requirements - UDOO NEO board. This document refers to the UDOO NEO Full board, but the steps remain the same for all UDOO Neo boards as long as the appropriate Device Tree is used for each. For more information on this board please go to the official site (http://www.udoo.org/) UDOO Neo Full Board - PN7150 NFC Controller SBC Kit for Arduino (OM5578/PN7150ARD) which is shown on the image below. Alternatively you may use the PN7120 NFC Controller SBC Kit for Arduino (OM5577/PN7120ARD). PN7150 NFC Controller SBC Kit for Arduino mounted over the UDOO Neo You may find more details about the OM5578 board on the user manual (Doc ID UM10935) which is available on the following link. http://www.nxp.com/documents/user_manual/UM10935.pdf You may also find additional documentation and information of this and other PN7150 demoboards on the link below: Demoboards for PN7150|NXP​ You may find more details about the OM5577 board on the user manual (Doc ID UM10878) which is available on the following link. http://www.nxp.com/documents/user_manual/UM10878.pdf For additional resources for the OM5577 board please refer to the link below. PN7120 NFC Controller SBC Kit|NXP - Host computer with Ubuntu 12.04 or later (14.04 is preferred). - L3.14.28 BSP Release for the i.MX6SX installed on the host. You may find the documentation on how to download and setup this BSP on the following link. http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/embedded-linux-for-i.mx-applications-processors:IMXLINUX?code=IMXLINUX 2. Setting up NXP BSP Release and Toolchain Follow the instructions on the Yocto User’s Guide included on the L3.14.28 BSP Release to setup and build an image to for the i.MX6SX (MACHINE= imx6sxsabresd). We’ll be using the fsl-image-gui image with frame buffer (fb) backend. Other images may be used but please keep in mind that the core-image-minimal image does not include the libstdc++.so.6 library required by the NFC Demo App. It is also necessary to build and install the toolchain for cross compiling the kernel and bootloader. This can be done with the following command: $ bitbake meta-toolchain Once created you may install it by running the following script: <BSP_DIR>/<BUILD_DIR>/tmp/deploy/sdk/poky-glibc-x86_64-meta-toolchain-cortexa9hf-vfp-neon-toolchain-1.7.sh For more details on how to extract the toolchain please refer to the following Yocto Training Task: Task #7 - Create the toolchain 3. Editing the Device Tree In previous versions (3.0.35 backward) the Linux Kernel used to contain the entire description of the hardware so the bootloader just had to load the kernel image and execute it. In current Kernel versions the hardware description is located in the device tree blob (DTB), which allows for the same Kernel to be used in different Hardware by changing only the Device Tree. In this scenario the bootloader loads the Kernel image and also the Device Tree (DTB) binary. For more details on how to add a new Device Tree please look at the following Community Document that covers adding a new device tree: https://community.nxp.com/docs/DOC-329664 For this document we will change the current UDOO NEO Device Tree as we will only be adding support for the PN7150 NFC Controller Board. 3.1 Copying the original UDOO Neo Device Tree files Create a development folder in your home directory. mkdir udooneo-dev Download the kernel source into this folder. This also includes the device tree files. cd udooneo-dev git clone https://github.com/UDOOboard/linux_kernel The Device Tree files will be available at  udooneo-dev/linux_kernel/arch/arm/boot/dts 3.2. Editing the UDOO Neo Device Tree Files We will be using the UDOO Neo Full board, so we will be using the imx6sx-udoo-neo-full-hdmi-m4.dts. If we look into this file using a text editor we will see that it includes several include definition files which are also located in the same directory. #include "imx6sx-udoo-neo.dtsi" #include "imx6sx-udoo-neo-full.dtsi" #include "imx6sx-udoo-neo-m4.dtsi" #include "imx6sx-udoo-neo-hdmi.dtsi" #include "imx6sx-udoo-neo-externalpins.dtsi" We will need to copy these to the BSP Release dts directory (you may alternatively build the device tree from this directory, but we will cover how to add device trees to the BSP Release in this document): /<BSP_DIR>/<BUILD_DIR>/tmp/work/imx6sxsabresd-poky-linux-gnueabi/linux-imx/3.14.28-r0/git/arch/arm/boot/dts/ We will need to add the new dtb file to be compiled on the Makefile from the BSP Release.  This needs to be placed inside the precompiler directive $(CONFIG_ARCH_MXC) There are some additions that must be made to device tree in order to configure the pins used by the NFC controller Board which uses the Arduino Pinout. These can be done to the imx6sx-udoo-neo.dtsi so they are taken by any UDOO Neo Device Tree we compile. The I2C pins used are those of the I2C2 bus. The configuration for these pins should be already implemented on the imx6sx-udoo-neo.dtsi file. If not please add these lines inside the &iomuxc section. &iomuxc {                         pinctrl_i2c2_1: i2c2grp-1 {                                         fsl,pins = <                                                         MX6SX_PAD_GPIO1_IO03__I2C2_SDA          0x4001b8b1                                                         MX6SX_PAD_GPIO1_IO02__I2C2_SCL           0x4001b8b1                                         >;                       }; }; Then we need to add the pn547 entry into the &i2c2 section for the enable pin, interrupt pin, I2C address and buss speed for the PN7150. Put what is in bold below at the end of the “&i2c2” section as shown. &i2c2 { pn547: pn547@28 { compatible = "nxp,pn547";                 reg = <0x28>; clock-frequency = <400000>; interrupt-gpios = <&gpio4 9 0>; enable-gpios = <&gpio5 21 0>;         }; }; Important Note: Prior to adding either of these configurations it is critical that you ensure these pins and I2C addresses are not used anywhere else in this and other *udo*.dtsi files You may find the UDOO Neo Schematics on the UDDO website (link to the schematics below) to see the reason behind these settings. http://www.udoo.org/download/files/schematics/UDOO_NEO_schematics.pdf IR Signal – J4 Connector – Arduino 7 pin – i.MX6SX B13 pin VEN Signal - J6 Connector – Arduino 8 pin - i.MX6SX W5 pin SDA Signal – J6 Connector – Arduino SDA pin - i.MX6SX D20 pin SCL Signal – J6 Connector – Arduino SCL pin - i.MX6SX C20 pin If you want to review in more detail how to create a simple Device Tree from scratch please check the following very complete and easy to follow Community Document. Basic Device Tree for the Udoo Board To compile the device tree run the following command source /opt/poky/1.7/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi cd /<BSP_DIR>/<BUILD_DIR>/tmp/work/imx6sxsabresd-poky-linux-gnueabi/linux-imx/3.14.28-r0/git make ARCH=arm dtbs This will produce the Imx6sx-udoo-neo-full-hdmi-m4.dtb that will be used. 4. Compiling U-Boot We will be using the UDOO U-boot for the UDOO Neo Full board. The following steps describe how to download the source code and compiling it using our toolchain. Downloading the source code mkdir UDOOneo-dev cd UDOOneo-dev git clone -b 2015.04.imx-neo https://github.com/UDOOboard/uboot-imx cd uboot-imx Compiling u-boot source /opt/poky/1.7/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi ARCH=arm CROSS_COMPILE=arm-poky-linux-gnueabi- make udoo_neo_config ARCH=arm CROSS_COMPILE=arm-poky-linux-gnueabi- make This will generate a SLP file with the DCD (Device Configuration Data) table and the u-boot.img file. Note: By default this U-Boot configuration detects the UDOO Neo board and in our case it would look for the imx6sx-udoo-neo-full-hdmi-m4.dtb. You may need to use a different device tree depending on your board. 5. Flashing SD Card 5.1. Using the .sdcard file to load the BSP Release Image The easiest way to load the Root File System from our image is using the .sdcard file that is created after running bitbake. This image will be located on the following path: /<BSP_DIR>/<BUILD_DIR>/tmp/deploy/images/imx6sxsabresd This will also load the BSP Release U-boot and device tree files but we will then exchange for our own. To do this use the following command where sdx is your SD Card. $ sudo dd if=<image name>.sdcard of=/dev/sdx bs=1M && sync Alternatively we can manually create the two partitions needed. For more information on this please refer to the Yocto User’s Guide. 5.2. Writing U-boot To flash U-boot you need to flash both the SPL file and the u-boot.img file using the following commands assuming that your SD card is in /dev/sdx dd if=SPL of=/dev/sdx bs=1K seek=1 dd if=u-boot.img of=/dev/sdx bs=1K seek=69 5.3. Copying the Device Tree Blob Copy the imx6sx-udoo-neo-full-hdmi-m4.dtb device tree to a folder called dts on the FAT partition. 6. Adding Kernel Driver Download the driver source from the git repository from the Linux source directory cd /<BSP_DIR>/<BUILD_DIR>/tmp/work/imx6sxsabresd-poky-linux-gnueabi/linux-imx/3.14.28-r0/git/drivers/misc $ git clone https://github.com/NXPNFCLinux/nxp-pn5xx.git Add the line below to the Makefile of the current directory     obj-y += nxp-pn5xx/ Include the driver config by adding below line to the heading configuration file (drivers/misc/Kconfig). source "drivers/misc/nxp-pn5xx/Kconfig" Export the environment variables cd /<BSP_DIR>/<BUILD_DIR>/tmp/work/imx6sxsabresd-poky-linux-gnueabi/linux-imx/3.14.28-r0/git/     $ source /opt/poky/1.7/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi     $ export ARCH=arm     $ export CROSS_COMPILE=$TARGET_PREFIX     $ make imx_v7_defconfig make menuconfig Inside menu config include the driver as a module (<M>), which is on the path: Device Drivers --->       Misc devices --->     < M> NXP PN5XX based driver Save the changes and exit, and then compile the modules. $ make modules We will then install the modules to our image. Insert the SD card with the loaded image and mount it to access it from the command promt. sudo mount /dev/sdx ~/mountpoint/ Where sdx is your SD card. Then use the following command to install the modules. sudo ARCH=arm INSTALL_MOD_PATH=/home/user/mountpoint modules_install firmware_install Before unmounting our SD card we will install the NFC library. 7.Installing the NFC library. Install the necessary libraries on the host by running the following commands: sudo apt-get update sudo apt-get install automake sudo apt-get install autoconf sudo apt-get install libtool Note: In case you are using Ubuntu 12.04 the following commands will allow for autoconf 2.69 to be installed, which is the minimum version required by the NFC library. sudo add-apt-repository ppa:dns/gnu -y sudo apt-get update -q sudo apt-get install --only-upgrade autoconf Enter our directory and install the Linux libnfc-nci stack cd ~/UDOOneo-dev git clone https://github.com/NXPNFCLinux/linux_libnfc-nci.git Generate the configuration script by executing the bootstrap bash script cd ~/UDOOneo-dev/linux_libnfc-nci ./bootstrap Configure Make file. We are using the default toolchain sysroots path. To configure for the PN7150 please use the following settings: ./configure --enable-pn7150 --host=arm-none-linux --prefix=/opt/poky/1.7/sysroots/x86_64-pokysdk-linux/usr --sysconfdir=/home/user/mountpoint/etc To configure for the PN7120 please use the following settings: ./configure --enable-pn7120 --host=arm-none-linux --prefix=/opt/poky/1.7/sysroots/x86_64-pokysdk-linux/usr --sysconfdir=/home/user/mountpoint/etc We are ready to execute the make and install the stack. make sudo make install After a successful build the libraries and a application demo are built in .libs directory. Copy the libraries to “/usr/lib” directory of the target and nfcDemoApp to the targets “/usr/sbin” cd .libs sudo cp * /home/user/mountpoint/usr/lib sudo cp nfcDemoApp /home/user/mountpoint/usr/sbin cd ~/UDOOneo-dev/linux_libnfc-nci/conf/PN7150 sudo cp * /home/user/mountpoint/etc Now we can unmount our SD card. sudo umount /home/user/mountpoint 8. Testing the NFC Reader Insert the micro SD card into the slot of the UDOO Neo board and install the PN1750 NFC Controller board on top of the UDOO Neo board. We will be using the terminal console in order to access the board. You may use the official USB/Serial debug module for NEO or a similar adapter. For more information on setting up the Serial Debug Console on the UDOO Neo board please refer to the link below. http://www.udoo.org/docs-neo/Basic_Setup/Serial_Debug_Console.html Once it has booted, install the .ko file. insmod /lib/modules/3.14.28+g91cf351/kernel/drivers/misc/nxp-pn5xx/pn5xx_i2c.ko Then run the nfcDemoApp. We’ll test it in poll mode, where it looks for available tags and reads them. nfcDemoApp poll You should get a console output as shown below when placing a NFC tag next to the NFC reader. Appendix. References and useful documents http://www.nxp.com/documents/application_note/AN11697.pdf Demoboards for PN7150|NXP PN7120 NFC Controller SBC Kit|NXP NFC PN7120 on the  i.MX6Q | NXP Community Basic Device Tree for the Udoo Board Basic Device Tree for the Udoo Board U-Boot Migration Example http://www.nxp.com/documents/user_manual/UM10935.pdf
記事全体を表示
The video shows how to read the NDEF message under password protection. For more details , please kindly refer to https://community.nxp.com/docs/DOC-347622 
記事全体を表示
The demonstration aims at how to protect the NDEF messages in the NTAG, here we use OM5569-NT322ER | NTAG I2C plus Explorer Kit + reader | NXP  as this dev kit contains NTAG as well as the NFC reader. The NTAG I2C plus has the unprotected memory starting from page 04h of sector 0, and NDEF messages are stored there. Referring to 8.3.11 of the data sheet, AUTH0 specifies the starting page to be protected, ACCESS[NFC_PROT] enables read&write password protection from NFC interface, PWD and PACK are for password configuration, but before changing any of above , you have to do a password authentication as below: Then you may select sector 0 and read the contents starting from E3h. Here FFh is the default value for AUTH0.  Now you may change the AUTH0,ACCESS[NFC_PROT] , PWD and PACK as you wish, for example, something like below: read the data from E3h to E6h and change the corresponding bytes in one write. The video shows how to read the NDEF message under password protection.  
記事全体を表示
Example sends Wi-Fi credentials from phone to IoT device, so it can join the Wi-Fi network.  Using: iOS and Android phone with NXP's TagWriter app PN7462 NFC Reader device on PNEV7462B eval board, part of kit OM27462CDK Host Card Emulation mode example based on NfcrdlibEx8_HCE_T4T example from NFC Reader Library Example will also print out other NDEF messages received.  NDEF formats include: Contacts / Business Cards URL link Wi-Fi network and credentials Bluetooth MAC address for pairing Email address Phone number Geo location Launch application on host OS Plain text SMS (sorry the audio is horrible)
記事全体を表示
This post contains step by step guide of how to use NTAG 5 with LPC55S69. The goal of this post is to enable developers to use NTAG 5 and LPC55S69 together, quickly and easily.    Attached with this post are two ready to use packages:      'Simple_NDEF’ demonstrates how to read/write to NTAG 5 from the I 2 C  interface and field detection functionality.      'Passthrough’ demonstrates SRAM passthrough functionality, in which NTAG 5 acts as a fast bridge between the I 2 C interface device and RF interface device. NTAG 5 Overview NTAG 5 is a family of ISO/IEC 15693 and NFC Forum Type 5 Tag compliant tags with an EEPROM, SRAM, and I 2 C  host and slave interface. This ensures information exchange with all NFC Forum Devices with a tap. With this ability, the tag offers a long-reading range and privacy due to close proximity with mobile devices. NXP’s NTAG 5 boost shrinks the NFC footprint while adding AES security, so designers can deliver ultra-compact devices for use in IoT, consumer, and industrial applications. It is an NFC Forum-compliant contactless tag that delivers exceptional read range, giving tiny devices the ability to interact with the cloud, and other NFC-enabled devices, including smartphones. NXP’s NTAG 5 link lets designers of sensor-equipped systems add an NFC interface with a wired host interface that’s configurable as an I 2 C master/slave, a Pulse Width Modulator (PWM), or a General-Purpose I/O (GPIO). Operating at 13.56 MHz, it is an NFC Forum-compliant contactless tag that can be read and written by an NFC-enabled device at close range and by an ISO/IEC 15693-enabled industrial reader over a longer range. Hardware Requirements NTAG 5 Evaluation Board (OM23510ARD)                         OM23510ARD                                     2. LPCXpresso55S69 Board Hardware Connections Connecting the two boards is very easy since both have Arduino compatible headers, so simply plug the NTAG 5 EVK board on top of the LPCXpresso55S69 board.   1. Running 'Simple_NDEF' on LPC55S69 with NTAG 5 If this is the first time you’re using the LPCXpresso55S69 board, follow the getting started guide first LPC55S69-EVK. Make sure to install the SDK package for the LPC55S69 board which is required to run the project. Download the ‘Simple_NDEF’ package which you will find attached to this post. Drag and drop the downloaded package to the “Project Explorer” tab of your MCUXpresso IDE workspace (If you don’t have MCUXpresso, it can be downloaded for free from here:https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE Now that the package has been imported to the MCUXpresso IDE (via drag and drop), click on the Debug icon from the Quickstart panel to begin a debug session. Once the debug session has started, click on the run icon to run the code: 5. After step 3, the project should be running now. Here is how the output looks in the terminal: 2. Running 'Passthrough' on LPC55S69 with NTAG5 If this is the first time you’re using the LPCXpresso55S69 board, follow the getting started guide first an LPC55S69-EVK | NXP. Make sure to install the SDK package for the LPC55S69 board which is required to run the project. Download the ‘Passthrough’ package which you will find attached to this post. Drag and drop the downloaded package to the “Project Explorer” tab of your MCUXpresso IDE workspace (If you don’t have MCUXpresso, it can be downloaded for free from here:https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE  Now that the package has been imported to the MCUXpresso IDE (via drag and drop), click on the Debug icon from the Quickstart panel to begin a debug session. Once the debug session has started, click on the run icon to run the code: 5. After step 3, the project should be running now. To check the passthrough functionality, install the NTAG 5 App and then go into passthrough functionality. Available Resources LPC55S69-EVK: LPCXpresso55S69 Development Board https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc5500-cortex-m33/lpcxpresso55s69-development-board:LPC55S69-EVK NTAG 5 link: NFC Forum-compliant I²C bridge for IoT on-demand | NXP  NTAG 5 boost: NFC Forum-compliant I²C bridge for tiny devices | NXP 
記事全体を表示
This demonstration is based on RFIDDiscover full version and Pegoda EV710. You may refer to the following links for more details. RFIDDiscover | NXP  PEGODA Contactless Smart Card Reader | NXP  Before start the demonstration, please connect Pegoda with your PC via USB and place the MIFARE DESFire Light card on the reader. The history and log can be fetched from the attachment. Please refer to the video for more details.  
記事全体を表示
MIFARE DESFire Light read and write demonstration
記事全体を表示
This post contains a guide of how to use the NFC Reader Library with LPC845 using the Basic Discovery Loop example. The vanilla Basic Discovery Loop example is larger than the flash size of LPC845 (64KB), so the project needs to be reduced in size as well. How to reduce the size is explained in section “Porting the NFC Reader Library and reducing the size of project” A ready to use package “lpcxpresso845max_Basic_Discovery_Loop” example from the NFC Reader Library to be run on LPC845 and CLRC663 plus frontend is attached with this document. This document is structured as follows:   Overview of LPC845 The LPCXpresso-MAX family of boards provides a powerful and flexible development system for NXP's low-end Arm® Cortex®-M0+ based MCUs. They can be used with a range of development tools, including the MCUXpresso IDE toolchain. The LPCXpresso845-MAX board was created to enable evaluation of and prototyping with the LPC84x family of MCUs. Based on the Arm® Cortex®-M0+ core, LPC845 is a low-cost, 32-bit MCU family operating at frequencies of up to 30 MHz. The LPC845 MCU contains 64 KB of flash memory and 16 KB of SRAM.  Hardware Requirements Following hardware is required to run the project: LPCXpresso845-MAX development board. CLEV6630B board or BLE-NFC-V2 board. Both boards contain CLRC663 plus frontend. Here we use BLE-NFC-V2.   Connections Connect the two boards as follows: Porting the NFC Reader Library and reducing the size of Project: The porting of Basic Discovery Loop Example (NFC Reader Library) to LPC845 Max was done following the procedure mentioned in “NFC Reader Library Porting to i.MX RT1050” document. However, after completing the porting and building the project, the size of the binary, which is 134.264 KB, is greater than the size of Flash of LPC845 which is 64KB of flash. To reduce the size of the project, the following two steps were taken: 1. Apply compiler optimization for size. This can be done in the MCUXpresso by: Opening properties of project. Right Click project-   >Properties Go to Settings->Optimization. For Optimization Level choose “Optimize for Size” Building the project after this step results in a successful build but the project takes up 93% of all Flash, leaving very little space for adding more functionality. 2. The vanilla Basic discovery loop example detects all types of NFC tags. This increases our code size, so further size reduction can be achieved by limiting the number of protocols used. To limit our Basic Discovery loop to only look for Type A tags, do the following: Open the file “ph_NxpBuild_App.h” file which is inside in the “intfs” folder. This file defines the protocols (types) which are detected by the Basic Discovery Loop example. The type A cards uses the “ISO 14443-3A” protocol, so comment out all other protocol definitions except for “ISO 14443-3A” protocol as shown in Figure.   Building the project after this step takes up only 42.784KB of space consuming 65% of the Flash, leaving sufficient amount of space for adding application code.   Running Basic Discovery Loop on LPC845 If this is the first time you’re using the LPCXpresso845 Max board, follow the getting started guide first ->  LPC845Max | NXP . Make sure to install the SDK package LPCXpresso845 Max which is required for the project below to run. Download the “lpcxpresso845max_Basic_Discovery_Loop” package which you will find attached to this post. Drag and drop the downloaded package to the “Project Explorer” tab of your MCUXpresso IDE workspace (If you don’t have MCUXpresso, it can be downloaded for free from here: https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE ) Now that the package has been imported to the MCUXpresso IDE (via drag and drop), click on Debug icon from the Quickstart panel to begin a debug session. Once the debug session has started, click on the run icon to run the code: After step 4, the project should be running now. The output “BasicDiscoveryLoop Example” can be seen in the console. The project contains basic discovery loop functionality. Bring any NFC card near the frontend’s RF antenna and the output console will show the detection and type of the card. Running other examples from NFC Reader Library on LPC845: Once the “lpcxpresso845max_Basic_Discovery_Loop” project is running on the LPC845, running other examples from NFC Reader Library is simple. Here we use the “NfcrdlibEx9_NTagI2C” example from the reader library to describe the process. In “intfs” folder remove everything except the “phaApp_Init.h” file. Then go to the “intfs” folder of the NFC Reader Library example you want to run (“NfcrdlibEx9_NTagI2C” in this case), and copy all the files except “phaApp_Init.h” and paste them in the original “intfs” folder.  In line 57 of the “ph_NxpBuild_App.h” file in “intfs” folder, replace  Go to “source” folder and remove every file except “phApp_Init.c“ and “semihost_hardfault.c” files. Then go to “src” folder of the example you want to run (“NfcrdlibEx9_NTagI2C” in this case) and copy all the files except “phaApp_Init.c” and paste them into the “source” folder.  Finally, copy the main file of the example you want to run (NfcrdlibEx9_NTagI2C in this case) and paste it into the “source” folder as well. The project is ready to build and run on LPC845. Available Resources: Porting NFC Reader Library to i.MX RT1050. (Detailed Description of porting) https://community.nxp.com/docs/DOC-341843 NFC Reader Library  NFC Reader Library | NXP  LPC845 Max  LPCXpresso845-MAX Board for LPC84x Microcontrollers (MCUs) | NXP 
記事全体を表示
This post contains a guide of how to use the NFC Reader Library with LPC55S69. A ready to use package for using the “Basic Discovery Loop” example from the NFC Reader Library with LPC55S69 and CLRC663 plus frontend is attached with this document. This document is structured as follows: Overview of LPC55S69: The LPCXpresso55S69 development board provides the ideal platform for evaluation of and development with the LPC55S6x MCU based on the Arm® Cortex®-M33 architecture. The board includes a high performance onboard debug probe, audio subsystem and accelerometer, with several options for adding off-the-shelf add-on boards for networking, sensors, displays and other interfaces. The LPCXpresso55S69 is fully supported by the MCUXpresso suite of tools, which provides device drivers, middleware and examples to allow rapid development, plus configuration tools and an optional free IDE. MCUXpresso software is compatible with tools from popular tool vendors such as Arm and IAR, and the LPCXpresso55S69 may also be used with the popular debug probes available from SEGGER and P&E Micro. Hardware Requirements: Following hardware is required to run the project: LPC55S69-EVK development board. CLEV6630B board or BLE-NFC-V2 board. BLE-NFC-V2: It is easier to use the BLE-NFC-V2 board since it can be just plugged on top of the arduino interface available on the LPCXpresso55S69 board. The following figure shows the pin mapping between the two boards. CLEV6630B board: The CLEV6630B board consists of CLRC663 plus (NFC frontend) connected by default to an LPC1769 µC via SPI. However, the board is made in such a way that the LPC1769 MCU can be bypassed to connect to an external MCU (in our case the LPC55S69) easily. For doing so: Six resistors from the board need to be removed. These are highlighted in red in the Figure 1: Use the SPI pin connectors available on the left-hand side, on the board edge to connect to external MCU (LPC55S69 in this case) Solder jumper wires onto the following pins of CLEV6630B Board:  GND IRQ CLRC_NRST SSEL MOSI MISO SCK IF0 IF1      The CLEV6630B is shown in Figure 2 after the required changes have been made to it (Removal of resistors and soldering of wires).   Now connect the two boards as follows:   Running Basic Discovery Loop on LPC55S69:   If this is the first time you’re using LPC55S69-EVK board, follow the getting started guide first à  LPC55S69-EVK | NXP . Make sure to install the SDK package for LPC55S69-EVKboard which is required for the project below to run. Download either‘lpcxpresso55s69_BasicDiscoveryLoop_CLEV6630b' or 'lpcxpresso55s69_BasicDiscoveryLoop_BLE-NFC' package which you will find attached to this post. Drag and drop the downloaded package to the “Project Explorer” tab of your MCUXpresso IDE workspace (If you don’t have MCUXpresso, it can be downloaded for free from here: https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE Now that the package has been imported to the MCUXpresso IDE (via drag and drop), click on Debug icon from the Quickstart panel to begin a debug session. Once the debug session has started, click on the run icon to run the code: The project should be running now. The project contains basic discovery loop functionality. Here is how the output looks like in the terminal. Bring any NFC card near the frontend’s antenna and the output console will show the detection and type of the card. For example, in the picture below, we can see that type 4A card was detected:     Running other NFC Reader Library examples on LPC55S69: Once the “lpcxpresso55s69_BasicDiscoveryLoop” project is running on the LPC55S69. Running other examples from is simple. First step is to install the NFC Reader Library : Installing the NFC Reader Library: Go to www.nxp.com/pages/:NFC-READER-LIBRARY Go to the Downloads tab and click on the download button Click download on the NFC Reader Library for Kinetis K82F package. Import the library package in the workspace. The easiest way is to use the Quick Start Panel on the left-hand side: Click on Import project from file system Then, browse the library package in your file system. Click Finish to import it all to your workspace. After completing the import wizard, all projects are listed in the “Project Explorer” window. As can be seen in the screenshot, it contains different folders: API documentation folder Driver Abstraction Layer FreeRTOS support The platform support (in the screenshot, corresponding to the LPC support) The software examples  The Reader Library implementation And the OS abstraction layer   Running "NfcrdlibEx9_NTagI2C" on LPC55S69: Here we use the “NfcrdlibEx9_NTagI2C” example from the reader library to describe the method. The same method can be used to run other examples from the NFC Reader Library.  To run "NfcrdlibEx9_NTagI2C" on LPC55S69, we look at "lpcxpresso55s69_BasicDiscoveryLoop" project (available as a download below) and "NfcrdlibEx9_NTagI2C" project (from the Reader Library). We make changes to the following folders: In “intfs” folder remove everything except the “phaApp_Init.h” file. Then go to the “intfs” folder of the NFC Reader Library example you want to run (“NfcrdlibEx9_NTagI2C” in this case), and copy all the files except “phaApp_Init.h” and paste them in the original “intfs” folder. In line 57 of the “ph_NxpBuild_App.h” file in “intfs” folder, replace #if defined(PHDRIVER_LPC1769RC663_BOARD) \     || defined(PHDRIVER_FRDM_K82FRC663_BOARD)\ #   define NXPBUILD__PHHAL_HW_RC663 #endif with #if defined(PHDRIVER_LPC1769RC663_BOARD) \     || defined(PHDRIVER_FRDM_K82FRC663_BOARD)\     || defined(PHDRIVER_LPC55S69RC663_BOARD) #   define NXPBUILD__PHHAL_HW_RC663 #endif Go to “source” folder and remove every file except “phApp_Init.c“ and “semihost_hardfault.c” files. Then go to “src” folder of the example you want to run (“NfcrdlibEx9_NTagI2C” in this case) and copy all the files except “phaApp_Init.c” and paste them into the “source” folder. Finally, copy the main file of the example you want to run (NfcrdlibEx9_NTagI2C in this case) and paste it into the “source” folder as well. The project is ready to build and run on LPC55S69.       Available Resources: Porting NFC Reader Library to i.MX RT1050. (Detailed Description of porting) https://community.nxp.com/docs/DOC-341843 LPC55S69 https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/lpc-cortex-m-mcus/lpc5500-cortex-m33/lpcxpresso55s69-development-board:LPC55S69-EVK BLE-NFC-V2 https://www.nxp.com/products/identification-security/rfid/nfc-hf/nfc-readers/clrc663-iplus-i-and-qn902x-nfc-bluetooth-low-energy-solution-for-consumer-applications:BLE-NFC
記事全体を表示
This post contains a step by step guide of how to use PN7150 with LPC55S69.  This document is structured as follows: Overview of PN7150:  The PN7150 is a Plug-and-Play all-in-one NFC solution for easy integration into any OS environment like Linux and Android, reducing Bill of Material (BoM) size and cost. The embedded Arm® Cortex®-M0 microcontroller core is loaded with the integrated firmware, simplifying the implementation as all the NFC real-time constraints, protocols and the device discovery (polling loop) are processed internally. In few NCI commands, the host SW can configure the PN7150 to notify for card or peer detection and start communicating with them. It has the following salient features: Full NFC forum compliancy with small form factor antenna Embedded NFC firmware providing all NFC protocols as pre-integrated feature Direct connection to the main host or microcontroller, by I2C-bus physical and NCI protocol Ultra-low power consumption in polling loop mode Highly efficient integrated power management unit (PMU) allowing direct supply from a Battery Overview of LPC55S69:  The LPCXpresso55S69 development board provides the ideal platform for evaluation of and development with the LPC55S6x MCU based on the Arm® Cortex®-M33 architecture. The board includes a high performance onboard debug probe, audio subsystem and accelerometer, with several options for adding off-the-shelf add-on boards for networking, sensors, displays and other interfaces. The LPCXpresso55S69 is fully supported by the MCUXpresso suite of tools, which provides device drivers, middleware and examples to allow rapid development, plus configuration tools and an optional free IDE. MCUXpresso software is compatible with tools from popular tool vendors such as Arm and IAR, and the LPCXpresso55S69 may also be used with the popular debug probes available from SEGGER and P&E Micro. Hardware requirements: OM5578/PN7150ARD  LPCXpresso55S69 + usb  micro cable  Using PN7150 with LPC55S69-EVK: Hardware Connections: The hardware connections are simple. Both the LPC55S69-EVK board and OM5578/PN7150ARD board have an Arduino interface. So, mount the PN7150ARD board with male Arduino connector onto the female Arduino connector of the LPC55S69-EVK board. Running the demo: If this is the first time you’re using LPC55S69-EVK board, follow the getting started guide first à  LPC55S69-EVK | NXP . Make sure to install the SDK package for LPC55S69-EVKboard which is required for the project below to run. Download the ‘NXP-NCI_PN7150_LPC55xx_example’ package which you will find attached to this post. Drag and drop the downloaded package to the “Project Explorer” tab of your MCUXpresso IDE workspace (If you don’t have MCUXpresso, it can be downloaded for free by clicking here: Now that the package has been imported to the MCUXpresso IDE (via drag and drop), click on Debug icon from the Quickstart panel to begin a debug session. Once the debug session has started, click on the run icon to run the code: The project should be running now. The project contains basic discovery loop functionality. Here is how the output looks in the console tab on MCUXpresso: Bring any NFC card near the PN7150 board’s antenna and the output console will show the detection and type of the card. For example, in the picture below, we can see that type 4 card was detected: Available Resources: AN11990 NXP-NCI MCUXpresso example document. (https://www.nxp.com/docs/en/application-note/AN11990.pdf) The example project explained in this project was ported to LPC55S69 using section 5.3 and 6 of the above mentioned document. PN7150 datasheet (https://www.nxp.com/docs/en/data-sheet/PN7150.pdf) PN7150 User Manual (https://www.nxp.com/docs/en/user-guide/UM10936.pdf) PN7150 NFC Controller SBC Kit User Manual  (https://www.nxp.com/docs/en/user-guide/UM10935.pdf)
記事全体を表示
This post contains step by step guide of how to use the NTAG I²C plus with LPC55S69. This is easy and straightforward to do, since the MCUXpresso SDK Builder tool has an option to add NTAG I²C plus example directly to SDK of LPC55S69. Hardware Needed: LPC55S69-EVK NTAG I²C plus explorer kit Follow the following simple steps to use NTAG I²C plus with LPC55S69: Download and install MCUXpresso IDE (if you don’t have it already). It can be download for free by clicking here: Next step is to use the MCUXpresso SDK Builder tool to build and download the SDK for LPC55S69. For this: Go to  the MCUXpresso SDK Builder website: https://mcuxpresso.nxp.com/en/select Select the LPC55S69 board and then click on ‘Build MCUXpresso SDK’ button: Click on ‘Add Software component’, then select the NTAG I2C component, click ‘Save changes’ and then download the SDK. Drag and drop the downloaded SDK to the installed SDK’s tab in the MCUXpresso IDE to install it. Click on the ‘Import SDK example(s)’ in the Quickstart Panel in the MCUXpresso IDE. Then select LPC55S69, ‘check the ntag_i2c_plus_example’ box and hit ‘Finish’. Connect the LPC55S69 and NTAG I²C plus boards together. Details of these connections can be found in the “readme.txt” file in the “doc” folder of the project: Finally click on debug in the Quickstart Panel to build the project, flash it to the MCU, and start debugging. This is how the output looks like in the Console tab of IDE: Bring any active nfc device (e.g. an NFC phone with NFC enabled) near the ntagi2c board. The program will detect it and consequently blink the LED as well as display a message on the console: Read the “readme.txt” file for more details regarding the project. Available Resources: BLE pairing with NFC on KW41 and NTAG I²C plus source code www.nxp.com/downloads/en/snippets-boot-code-headers-monitors/SW4223.zip NTAG I²C plus kit for Arduino pinout www.nxp.com/demoboard/OM23221ARD
記事全体を表示
This post contains a step by step guide of how to use PN7150 with i.MX RT1060. This document is structured as follows: Overview of PN7150 PN7150 is a Plug-and-Play all-in-one NFC solution for easy integration into any OS environment like Linux and Android, reducing Bill of Material (BoM) size and cost. The embedded Arm® Cortex®-M0 microcontroller core is loaded with the integrated firmware, simplifying the implementation as all the NFC real-time constraints, protocols and the device discovery (polling loop) are processed internally. In few NCI commands, the host SW can configure the PN7150 to notify for card or peer detection and start communicating with them. It has the following salient features: Full NFC forum compliancy with small form factor antenna Embedded NFC firmware providing all NFC protocols as pre-integrated feature Direct connection to the main host or microcontroller, by I2C-bus physical and NCI protocol Ultra-low power consumption in polling loop mode Highly efficient integrated power management unit (PMU) allowing direct supply from a Battery Hardware Requirements      1. OM5578/PN7150ARD      2. i.MX RT1060 EVK Evaluation Board + usb micro cable        Using PN7150 with i.MX RT1060 Hardware Connections The hardware connections are simple. Both the EVKB-IMXRT1060 board and OM5578/PN7150ARD board have an Arduino interface. So, mount the PN7150ARD board with male Arduino connector onto the female Arduino connector of the EVKB-IMXRT1060 board.  Running the Demo If this is the first time you’re using EVK-MIMXRT1060 board, follow the getting started guide first: i.MX RT1060 Evaluation Kit | NXP . Make sure to install the SDK package for EVK-MIMXRT1060 board which is required for the project to run.   Download the ‘evkbimxrt1060_PN7150’ package which you will find attached to this post. Drag and drop the downloaded package to the “Project Explorer” tab of your MCUXpresso IDE workspace (If you don’t have MCUXpresso, it can be downloaded for free from here: https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE Now that the package has been imported to the MCUXpresso IDE (via drag and drop), click on Debug icon from the Quickstart panel to begin a debug session. Once the debug session has started, click on the run icon to run the code: After step 3, the project should be running now. The project contains basic discovery loop functionality. Here is how the output looks in the console tab on MCUXpresso: Bring any NFC card near the PN7150 board’s antenna and the output console will show the detection and type of the card. For example, in the picture below, we can see that type 4 card was detected: Available Resources AN11990 NXP-NCI MCUXpresso example document. (https://www.nxp.com/docs/en/application-note/AN11990.pdf) The example project explained in this project was ported to i.MX RT1060 using section 5.3 and 6 of the above mentioned document. PN7150 datasheet (https://www.nxp.com/docs/en/data-sheet/PN7150.pdf) PN7150 User Manual (https://www.nxp.com/docs/en/user-guide/UM10936.pdf) PN7150 NFC Controller SBC Kit User Manual  (https://www.nxp.com/docs/en/user-guide/UM10935.pdf)
記事全体を表示
SPIM module is one of the master interfaces provided by PN7462 , which is a 32-bit ARM Cortex-M0-based NFC microcontroller, and users may use this interface to connect with up to two SPI slave devices. The NFC reader library provides SPIM driver code in phHal/phhalSPIM, and users may directly use the following APIs in their application to implement simple SPI transaction, just like what is done  in the demo of "PN7462AU_ex_phExHif". While this demo has limitation with some SPI nor flash devices, which need a write-read operation in one NSS session, for example, the SPI nor flash device on OM27462 as below: Please note to solder R202 and connect it to 3V3 to make sure nHold pin has pull-up out of POR. The following is one of the command sets this device supports: This command contains 1 write(9F) followed by 3 read operations in one NSS session, but if you implement it with phhalSPIM_Transmit() and phhalSPIM_Receive() as below: status = phhalSPIM_Transmit(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_APPEND_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 2, cmd_buf, PH_EXHIF_HW_SPIM_CRC_OFFSET);    status = phhalSPIM_Receive(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, data_length, dst, PH_EXHIF_HW_SPIM_CRC_OFFSET);" You will have the following result: expected: NSS   \__________________________/ MOSI     CMD A7-A0 MISO                            DATA       actual:                         NSS   \____________||______________/ MOSI     CMD A7-A0 MISO                           DATA so the pulse between the write and read is the problem, and here we have to handle the NSS line manually, with the help of NSS_VAL and NSS_CONTROL bits in SPIM_CONFIG_REG. so the code should be like this:   Assert NSS   status = phhalSPIM_Transmit(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_APPEND_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 2, cmd_buf, PH_EXHIF_HW_SPIM_CRC_OFFSET);    status = phhalSPIM_Receive(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, data_length, dst, PH_EXHIF_HW_SPIM_CRC_OFFSET);"   De-assert NSS The NSS line assert and de-assert function can be implemented with register bit level APIs, just like below:             PH_REG_SET_BIT(SPIM_CONFIG_REG, NSS_VAL);//de-assert NSS             PH_REG_SET_BIT(SPIM_CONFIG_REG, NSS_CTRL);             PH_REG_CLEAR_BIT(SPIM_CONFIG_REG, NSS_VAL);//assert NSS Please also include the following header files in your application code. #include "ph_Reg.h" #include "PN7462AU/PN7462AU_spim.h" Please notice that phhalSPIM_Transmit() and phhalSPIM_Receive() are Rom based function, which clear NSS_CTRL bit by default. We can not change ROM API's behave but fortunately we have phhalSPIM_TransmitContinue() and phhalSPIM_ReceiveContinue() instead. so the final solution will be like below: Assert NSS   status = phhalSPIM_TransmitContinue(1, cmd_buf);    status = phhalSPIM_ReceiveContinue(3, dst);   De-assert NSS This doesn't mean phhalSPIM_Transmit() and phhalSPIM_Receive() are useless, because they can also help up to configure the SPI master interface, if you don't want to use register bit level API to initial the SPIM module manually. Please note to use 1 byte for write/read length to make these two functions work properly. so the whole pseudo code is like below: phhalSPIM_Init(PH_HW_SPIM_TIMEOUT) ; phhalSPIM_Configure(PH_HW_SPIM_SLAVE, PH_HW_SPIM_MSB_FIRST,                 \                                     PH_HW_SPIM_MODE, PH_HW_SPIM_BAUDRATE,  \                                     PH_HW_SPIM_NSSPULSE, PH_HW_SPIM_NSSPOL) ; status = phhalSPIM_Transmit(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_APPEND_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 1, cmd_buf, PH_EXHIF_HW_SPIM_CRC_OFFSET);    status = phhalSPIM_Receive(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 1, dst, PH_EXHIF_HW_SPIM_CRC_OFFSET);" Assert NSS   status = phhalSPIM_TransmitContinue(1, cmd_buf);    status = phhalSPIM_ReceiveContinue(3, dst);   De-assert NSS The following steps show how to create a new project based on NFC reader library, please refer to https://www.nxp.com/docs/en/user-guide/UM10883.pdf  on how to import the NFC reader library. 1. Create a new project after importing the NFC reader library. 2. if you installed PN7462 support package, you will see this: 3. add a link to NFC reader lib: 4. add path and enable NFC reader lib in the project: 5. delete cr_startup.c and create the main code as well as the header file: 6. Build result: 7.Debug result: To fetch the ready demo, please submit a private ticket via the guide of https://community.nxp.com/docs/DOC-329745 . Hope that helps, Best regards, Kan
記事全体を表示
This post contains step by step guide of how to use NTAG I²C plus with i.MX RT MCUs. The goal of this post is to enable developers to start developing their NFC Applications using NTAG I²C plus and i.MX RT MCUs quickly and easily. Attached with this post are two ready to use packages: ‘evkbimxrt1060_ntagI2C’ is to be used with MIMXRT1060-EVK and NTAG I²C plus kit for Arduino pinout. ‘evkbimxrt1050_ntagI2C’ is to be used with MIMXRT1050-EVK and NTAG I²C plus kit for Arduino pinout. Both packages contain the same example code but are configured for the two different boards. The example code demonstrates the following basic operations: Reading the EEPROM of NTAG I²C plus. Writing NTAG messages to NTAG I²C plus. Reading SRAM of NTAG I²C plus. Writing to SRAM of NTAG I²C plus. Using Field detect pin as interrupt to turn on an LED when an RF field is detected by the NTAG I²C board. The document has been structured as follows: NTAG I²C plus kit for Arduino pinout The NTAG I²C plus Arduino kit consist of two PCBs stacked together: The upper PCB is the antenna board with the connected tag The lower PCB is an interface adaptor board to the Arduino pinout This kit can be used to connect and evaluate the NTAG I²C plus  into many popular MCUs with Arduino compliant headers, for example:  Kinetis (e.g. KW41Z, i.MX (e.g. UDOO Neo, i.MX 6UL, i.MX 6 ULL, i.MX 7D), LPC MCUs (e.g. LPCXpresso MAX, V2 and V3 boards) and i.MX RT boards (e.g. i.MX RT1050, i.MX RT1060) The kit support package includes several software examples. The OM29110ARD is a generic interface board which offers support for connection to any PCB implementing Arduino connectors. It exposes: 3.3V and 5V power supply pins. I2C, SPI and UART host interfaces. Generic GPIOs (e.g. to be used for field detect, interrupts, reset pins or others) As such, it allows the NTAG I²C plus to be plugged into Arduino devices seamlessly. Hardware Requirements EVKB-IMXRT1050 board or EVKB-IMXRT1060 board. NTAG I²C plus kit for Arduino pinout (OM23221ARD) Cables: Micro USB cable 6 jumper wires Male to Female (Only required if using EVKB-IMXRT1050 board) Using NTAG I²C plus kit for Arduino pinout with EVKB-IMXRT1060 Hardware Connections The hardware connections are simple. Both the EVKB-IMXRT1060 board and OM23221ARD (NTAG I²C plus) board have Arduino interface. So simply connect both as shown in figure:  Running the Demo Follow the below mentioned steps to run the demo: Download the ‘evkbimxrt1060_ntagI2C’ package which you will find attached to this post.  Drag and drop the downloaded package to your MCUXpresso IDE workspace (If you don’t have MCUXpresso, it can be downloaded for free from here: https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE Now that the package has been imported to the MCUXpresso IDE, click on Debug icon from the Quickstart panel to begin a debug session. Once the debug session has started click on the run icon to run the code:                                 Note:  If this is your first time using IMXRT1060EVK board, it is recommended to follow the getting started guide first ( i.MX RT1060 Evaluation Kit | NXP  ) To see the output, you need to have a terminal application installed (like Tera term or PuTTY). The output looks like this:                                                    Using NTAG I²C plus kit for Arduino pinout with EVKB-IMXRT1050 Hardware Connections In case of EVKB-IMXRT1050, the I2C pins on the Arduino interface’s J24 pin 9 and 10 are only connected to the i.MX RT slave I²C port, not to a master I²C port. So, we cannot just plug in the NTAG I²C plus kit, instead we need to connect two boards with the help of jumper wires. The connections required are show in figure below.                                Running the Demo Download the ‘evkbimxrt1050_ntagI2C’ package which you will find attached to this post. Drag and drop the downloaded package to your MCUXpresso IDE workspace (If you don’t have MCUXpresso, it can be downloaded for free from here: https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE Now that the package has been imported to the MCUXpresso IDE, click on Debug icon from the Quickstart panel to begin a debug session. Once the debug session has started click on the run icon to run the code:                                Note:  If this is your first time using IMXRT1050EVK board, it is recommended to follow the getting started guide first ( i.MX RT1050 Evaluation Kit | NXP  ) To see the output, you need to have a terminal application installed (like Tera term or PuTTY). The output looks like this:                                            Porting the Package to any other i.MX RT Boards    If you want to use NTAG I²C plus with i.MX RT boards other than the i.MX RT1050 or the i.MX RT1060, then you’ve       to port the example package. This is fairly straightforward and the procedure is described below: Import the ‘hello world’ project from the SDK of the board to which you want to port the package. (SDKs for every board are freely available for download from the MCUXpresso SDK Builder website).We will modify this ‘hello world’ project adding code from attached packages, to make it work on the desired board.                                     Copy the following folders from the attached ‘evkbimxrt1060_ntagI2C’ or ‘evkbimxrt1050_ntagI2C’ package to the ‘hello world’ project imported in step 1:                               Copy the two files to the ‘drivers’ folder of ‘hello world’ project: Delete the ‘hello_world.c’ file from the source folder: Now copy the following preprocessor micros from ‘evkbimxrt1060_ntagI2C’ or ‘evkbimxrt1050_ntagI2C’ package to ‘hello world’ project:      Preprocessor settings can be found by right clicking Project-Properties>C++Build > Settings  Now we need to change the project configuration:        a.  Add the newly copied folders to source location; Right click on Project->Properties and add the following        folders:    b.  Include paths to the added libraries in the project. These can be copied from the from ‘evkbimxrt1060_ntagI2C’ or ‘evkbimxrt1050_ntagI2C’ package. Open project->properties and copy the following in the respective places as shown in the images:  Change pin configurations according to the board pins you are using:             a. For changing field detect pin, the code can be found in the source file:                   b. For I2C instance, the lines of code are in app_ntag->app_ntag.h:              c. These pins also need to be initialized which can be done through the pin initialization tool of MCUXpresso or code can be added to the ‘board.c’ file in ‘board’ folder. Once these changes are done, porting is complete. Build the project, it should build without any errors. Available resources BLE pairing with NFC on KW41 and NTAG I²C plus source code www.nxp.com/downloads/en/snippets-boot-code-headers-monitors/SW4223.zip NTAG I²C plus kit for Arduino pinout www.nxp.com/demoboard/OM23221ARD    
記事全体を表示
This document provides a step by step guide of how to use the CLRC663 plus with i.MX RT1050. For this purpose, we need to port the NFC Reader Library to i.MX RT1050.  There are two zip files attached to this document: 1. "NFCReaderLibrary_IMXRT1050_Porting Guide +DAL_IMXRT1050_BLE-NFC-V2.zip" : This folder is pre-configured for those who want to use BLE-NFC-v2 board with i.MX RT1050. 2. "NFCReaderLibrary_IMXRT1050_Porting Guide +DAL_IMXRT1050_CLEV6630B.zip" : This folder is pre-configured for those who want to use CLEV6630B board with i.MX RT1050. A video describing how to use i.MX RT1050 with CLRC663 Plus Family is available by clicking this link (Using i.MX RT 1050 with CLRC663 plus family |NXP ) as well. 
記事全体を表示
Hello NFC community, MIFARE® Ultralight-based tickets offer an ideal solution for low-cost, high-volume applications such as public transport, loyalty cards and event ticketing. They serve as a perfect contactless replacement for magnetic stripe, barcode, or QR-code systems. The introduction of the contactless MIFARE Ultralight® ICs for limited-use applications can lead to reduced system installation and maintenance costs. As you may know the MIFARE family has the Ultralight C tag which is a contactless IC supporting 3DES cryptography is mostly used in limited use applications such smart ticketing, this tag complies with ISO 14443-3 type A and it is defined as type 2 tag, in this document I want to show you the procedure to change the default key to a custom key also to protect certain areas in the tag so the authentication is needed to perform a read or write operation. --------------------------------------------------------------------------------------------------- For this document I used : MFEV710: PEGODA Contactless Smart Card Reader RFIDDiscover Software Lite version  Full Version Available in Docstore Mifare Ultralight c --------------------------------------------------------------------------------------------------- Information Old Key : 49454D4B41455242214E4143554F5946 New Key : 88776655443322117766554433221199 Data sheet ---------------------------------------------------------------------------------------------------- First we start with the procedure to activate the tag and the anticollision procedure explained in the ISO/IEC 14443-3. Command Direction    ">" this direction is command send from PCD (Reader) to PICC(Ultralight c)    "<" this direction is command send from PICC (Ultralight c) to PCD (Reader)    "=" Prepare this command before sending Command   Data message REQA =  Request Command, Type A >  26 ATQA = Answer To Request, Type A  <  4400 SEL + NVB = SEL (Select code for cascade level ) 93, NVB (Number of Valid bits) 20 >  9320 ANTICOLLISION START <  8804598356   >  93708804598356 SAK (Select Acknowledge) = indicates additional cascade level <  x04   >  9520   <  E1ED2580A9   >  9570E1ED2580A9   <  x00 UID = 045983E1ED2580  ** the following procedure is explained in section 7.5.5 from the datasheet** Command   Data message Authenticate Part 1  (command 1A) >  1A00   <  AFA1ED1D682E5101422CC7 Authenticate Part 2 (command AF) >  AF2970D895F186D0302970D895F186D030188AAF4DAF68C5B9   <  006BD027CEC3E04EBC6919 [AUTHENTICATED] Then according to  section 7.5.7 of the datasheet the sections  where the 3DES key are saved are the 2C (Page 44) to the 2F (Page 47). We proceed to  write our new key using the A2 (WRITE command) Command   Data message DATA = byte 07,06,05,04 = 11223344 WRITE to page 44 (2C) >  A22C11223344 Positive acknowledge (ACK) <  0A DATA = byte 03,02,01,00 = 55667788 WRITE to page 45 (2D) >  A22D55667788  Positive acknowledge (ACK) <  0A DATA = byte 0F,0E,0D,0C = 99112233 WRITE to page 46 (2E) >  A22E99112233  Positive acknowledge (ACK) <  0A DATA = byte 0B,0A,09,08 = 44556677 WRITE to page 47 (2F) >  A22F44556677  Positive acknowledge (ACK) <  0A [RESET FIELD] [Authenticate with new key] Command   Data message Authenticate Part 1  (command 1A >  1A00   <  AFFAE2EFF17FAAD69862E7 Authenticate Part 2 (command AF) >  AFFD5794F2D4EA1B19FD5794F2D4EA1B196CF420CD4D9E8104   <  0030922228601939B8FA18 [AUTENTICATED WITH NEW KEY] we proceed to define from which sector the authentication is needed in order to read or write, to do this we use a write command to the AUTH0 (AUTH0 defines the page address from which the authentication is required. Valid address values for byte AUTH0 are from 03h to 30h.) the AUTH0 is located on the section 2A please check table 5 from #datasheet. **for this example we will define that from page 6 (06) we will need authentication to perform a read or write operation** Command   Data message WRITE command (A2) to AUTH0 (2A) from page 6 (06) >  A22A06000000 Positive acknowledge (ACK) <  0A Now the Read capabilities from page 06  require an Authentication in order to be read or written. Hope you find this document useful to get a better understanding of the behavior of the Ultralight C and how its security features can help you in your applications. Have a great day! BR Jonathan
記事全体を表示
Environments & Devices --Hardware 1、PN7462 DEMO Board(PNEV7642B) --Software 1、Ubuntu 16.04 desktop 2、Test tools ---libusb ---pcsc-lite ---ccid driver ---opensc          Before testing, please install above test tools to Ubuntu 16.04 according to document on the link https://community.nxp.com/docs/DOC-334952 !          Then follow steps below to begin testing PN7462 DEMO board by above test tools. 1、Update firmware of PN7462 DEMO board          Please update firmware of PN7462 DEMO board according to UM10915.pdf, then test it on windows, ensuring PN7462 DEMO board can normally work at CCID protocol on window platform. 2、Connecting PN7462 DEMO Board to PC USB via USB OTG Cable.          On PENV7462B side, X3 connector should be used for USB OTG cable. 3、Using lsusb to list USB devices weidong@ubuntu:~$ lsusb Bus 002 Device 002: ID 0e0f:0003 VMware, Inc. Virtual Mouse Bus 002 Device 003: ID 0e0f:0002 VMware, Inc. Virtual USB Hub Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub Bus 002 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub Bus 002 Device 004: ID 0e0f:0008 VMware, Inc. Bus 002 Device 005: ID 1fc9:0117 NXP Semiconductors          Last line is PN7472 DEMO board. 4、Open 2 terminals at the same time on Ubuntu desktop (1) One terminal is used to run “pcsc” command weidong@ubuntu:~$ sudo /usr/local/sbin/pcscd -adf [sudo] password for weidong: 00000000 pcscdaemon.c:345:main() pcscd set to foreground with debug send to stdout 00012288 configfile.l:361:DBGetReaderList() Parsing conf file: /usr/local/etc/reader.conf.d 00000037 pcscdaemon.c:658:main() pcsc-lite 1.8.22 daemon ready. 00023126 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1D6B, PID: 0x0001, path: /dev/bus/usb/002/001 00000101 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1D6B, PID: 0x0001, path: /dev/bus/usb/002/001 00000113 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0003, path: /dev/bus/usb/002/002 00000112 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1D6B, PID: 0x0001, path: /dev/bus/usb/002/001 00000160 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0002, path: /dev/bus/usb/002/003 00000152 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0008, path: /dev/bus/usb/002/004 00000115 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0008, path: /dev/bus/usb/002/004 00000165 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0002, path: /dev/bus/usb/002/003 00000263 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1D6B, PID: 0x0002, path: /dev/bus/usb/001/001 ^V56546837 hotplug_libudev.c:651:HPEstablishUSBNotifications() USB Device add 00000101 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1FC9, PID: 0x0117, path: /dev/bus/usb/002/006 00000007 hotplug_libudev.c:436:HPAddDevice() Adding USB device: PN7462 USB Reader 00000045 readerfactory.c:1074:RFInitializeReader() Attempting startup of PN7462 USB Reader (1.00) 00 00 using /usr/local/lib/pcsc/drivers/ifd-ccid.bundle/Contents/Linux/libccid.so 00127887 readerfactory.c:949:RFBindFunctions() Loading IFD Handler 3.0 00000236 ifdhandler.c:1965:init_driver() Driver version: 1.4.27 00000477 ifdhandler.c:1982:init_driver() LogLevel: 0x0003 00000004 ifdhandler.c:1993:init_driver() DriverOptions: 0x0000 00000165 ifdhandler.c:111:CreateChannelByNameOrChannel() Lun: 0, device: usb:1fc9/0117:libudev:0:/dev/bus/usb/002/006 00000021 ccid_usb.c:302:OpenUSBByName() Using: /usr/local/lib/pcsc/drivers/ifd-ccid.bundle/Contents/Info.plist 00000727 ccid_usb.c:320:OpenUSBByName() ifdManufacturerString: Ludovic Rousseau (ludovic.rousseau@free.fr) 00000016 ccid_usb.c:321:OpenUSBByName() ifdProductString: Generic CCID driver 00000004 ccid_usb.c:322:OpenUSBByName() Copyright: This driver is protected by terms of the GNU Lesser General Public License version 2.1, or (at your option) any later version. 00000433 ccid_usb.c:656:OpenUSBByName() Found Vendor/Product: 1FC9/0117 (PN7462 USB Reader) 00000005 ccid_usb.c:658:OpenUSBByName() Using USB bus/device: 2/6 00000021 ccid_usb.c:717:OpenUSBByName() bNumDataRatesSupported is 0 00128471 ifdhandler.c:382:IFDHGetCapabilities() tag: 0xFB3, usb:1fc9/0117:libudev:0:/dev/bus/usb/002/006 (lun: 0) 00000027 readerfactory.c:396:RFAddReader() Using the reader polling thread 00004709 ifdhandler.c:382:IFDHGetCapabilities() tag: 0xFAE, usb:1fc9/0117:libudev:0:/dev/bus/usb/002/006 (lun: 0) 00000023 ifdhandler.c:477:IFDHGetCapabilities() Reader supports 1 slot(s) (2)The other terminal is used to run “"testpcsc " in pcsc-lite/src source code weidong@ubuntu:~/ccid/pcsc-lite-1.8.22/src$ ./testpcsc   MUSCLE PC/SC Lite unitary test Program   THIS PROGRAM IS NOT DESIGNED AS A TESTING TOOL FOR END USERS! Do NOT use it unless you really know what you do.   Testing SCardEstablishContext        : Command successful. Testing SCardIsValidContext   : Command successful. Testing SCardIsValidContext   : Invalid handle. (don't panic) Testing SCardListReaderGroups      : Command successful. Group 01: SCard$DefaultReaders Testing SCardFreeMemory               : Command successful. Testing SCardListReaders        : Command successful. Testing SCardListReaders        : Command successful. Reader 01: PN7462 USB Reader (1.00) 00 00 Waiting for card insertion        :          2 screenshots for above 2 terminals: 5、Test cards (All cards are contactless) (1) MIFARE Plus x 4K card Re move it: (2) MIFARE Nano card          Note: testpcsc should be run again. Remove it: (3) MIFARE EV1 card Remove it: 6、Using Opensc-tool to Test cards            Open a new terminal for running the command, please! (1)No cards (2) MIFARE Plus x 4K card (close to antenna , then run opensc-tool) (3) MIFARE Nano card (4) MIFARE EV1 card    TIC Weidong Sun 2018-07-09
記事全体を表示
As NFC reader library 5.12 also supports PN5180, switching the NFC frontend from CLRC663 to PN5180 is quite easy based on previous porting. The porting also includes the hardware settings and software modification. Hardware Setup for porting: a) Remove resistors on PNEV5180B to disconnect the onboard lpc1769 from PN5180, following steps on page 16 of https://www.nxp.com/docs/en/application-note/AN11908.pdf  b) Connect LPCXpresso board for LPC11U37 with PNEV5180 as below: Software Modification for porting: 1. Make a copy of Board_Lpc11u37Rc663.h , and change its name to "Board_Lpc11u37Pn5180.h", and import it into the DAL/boards folder. 2.Change the source code in the header file as below: 3. Add two more pins' definition and configuration for BUSY and DWL pins of PN5180, and new configuration for reset pin. and modify the reset logic: 4.Change the IRQ interrupt trigger type to rising edge. 5.Include this header file in BoardSelection.h 6.Add this new configuration in ph_NxpBuild_App.h 7.Add this new configuration in phApp_Init.h 8.Add this new configuration in ph_NxpBuild_Platform.h 9.Add this new configuration in Settings. 10.Building result: Testing result:
記事全体を表示
Hello NFC Community! This document demonstrates that multiple records can be also read from a Tag with TagXplorer. Please follow the steps below. Let's begin... Please make sure that you have written more than on record with NXP TagWriter app. For a more detailed explanation on this, please refer to the following document: Writing multiple NDEF text records with TagWrite app  The app can be found and downloaded from the Play Store: NFC TagWriter by NXP - Apps on Google Play  -> Connect the reader in TagXplorer -> Place the card on the reader and press Connect Tag -> Check for NDEF (1) and then, read NDEF (2). The Text Records can be visualized in the NDEF Payload Info below: I hope this is of great help! Ivan R.
記事全体を表示