Connects - 培训资料

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

讨论

排序依据:
As a major supplier to the world automotive market, NXP Standard Products continues to innovate new semiconductor packaging options for the unique needs of this market. This seminar will cover the latest in packaging technology including: Clip bonded LFPAK (focusing on LFPAK33, LFPAK88, flatpower diodes and BJT LFPAK56); SWF Side Wettable Flanks (focusing on logic DQFN and discrete devices); A comparison of leaded vs leadless MiniLogic packaging.
查看全文
This session will cover serial reprogramming capability (download, execute, etc.). Show the boot process from the ARM® Cortex®-M4 core including controlling A53 boot. Procedure for building and running baremetal code on Cortex-M4 and A53 using a debugger. Will discuss and demonstrate runtime communication between A53 and Cortex-M4 cores - with a discussion of options and examples.
查看全文
The automotive market is moving towards electrification and autonomous driving. This trend needs ADAS electronic systems capable of making decisions. To manage the risk of operations, the development of these systems follows the highest ISO26262 Automotive Safety Integrity Level (ASIL D). All safety electronic systems require a safety microcontroller and a reliable, safe source of power management connected to the car battery: this is the System Basis Chip (SBC). Safety microcontrollers and safety system basis chips are the backbone of embedded system architectures. In this presentation, you’ll review the latest functional safety innovations at the power management level (SBC), from the development phase to system design, underscoring the link to reliability and how to enable hardware that is safety ready. A short introduction to the fault tolerant system will be also presented.
查看全文
Introduction and review of the latest family of Functional Safety System Basis Chips with integrated CAN FD PHY. Power Management and flexible safety features will be discussed as well as the operation and interconnection with MCUs. Also in this presentation, you’ll identify how the robustness of our design are verified in a real application environment to achieve a common goal of an excellent system reliability performance. From the ADAS to the drive train market that requires reliability, power scalability and safety, learn how our system Basis Chip solution can enable and simplify your design.
查看全文
With a number of vehicles being connected to the internet, the need to have a secure environment inside the vehicle is increasing. This session will present secure use cases for edge nodes microcontroller in the vehicle and how the S32K can achieve them. Topics including what is security, NXP 4 layer of automotive security, and S32K CSEc.
查看全文
This session will present the advantages of H-bridge based window lifters against relay based ones, new functionalities that can be implemented and how NXP MagniV S12ZVMB64 microcontroller provides a well-integrated solution for a window lifter end node. With integrated functionalities like: internal regulator, GDU, PMF, ADC, current sensing, input capture and LIN physical layer.
查看全文
Ethernet adoption in new OEM platforms is accelerating, as a result of increased media, communication, and ADAS streams between different end points in vehicles. The required Quality of Service and synchronization is typically achieved through the implementation of Audio Video Bridging (AVB) specifications, or derivatives of AVB. NXP has a unique position in the market given our capability to offer a full solution for AVB in the car, from end points (MPUs as well as MCUs), PHYs, switches, plus the needed software stacks. In addition, the software stacks are full featured, including critical but often initially forgotten components such as Media Clock Recovery. Get an introduction to the basis of the AVB technology, and how NXP can help you deploy AVB in your products.
查看全文
Security is becoming a quintessential topic for any OEM, and possibly for the entire industry, as evolutions of Autonomous drive capabilities are inexorably tied to the ability to secure the car. A number of components in the security architecture of nodes in any vehicle are very close to the SoC, exploiting hardware capabilities to achieve intended functionality. Answering customer needs, NXP is providing a Trusted Execution Environment (TEE) stack, which provides a significant number of security features required by the Automotive needs. Get an introduction to the basis of NXP’s TEE stack, capabilities, and how does this integrates in the typical secure node architecture.
查看全文
Complexity is increasing abruptly in the IVI market, while TTM has decreased from 5 to 2-3 years over a few product generations. The entire ecosystem is moving from a close to an open system model, and from proprietary/close source to standard interfaces/open source components. NXP is committed to support you in this new reality, as well as providing help in leveraging the extensive BOM NXP typically has in IVI solutions. Through the IVI Platform, NXP offers a solid and complete base for fast product development, integrating productized and optimized BSP and middleware components, with out of the box security. Find out more during a one hour presentation, covering platform features, delivery mechanisms, roadmap and availability.
查看全文
Attendees will learn about modules on the S32K144 though brief tutorials and hands-on software examples. The lab will use NXP’s S32 Design Studio tools including Processor Expert and the S32K SDK. 
查看全文
Explain 3-phase motor control fundamentals with an overview of NXP’s hardware and software enablement solutions for motor control applications.
查看全文
In this class, participants will learn how to leverage model-based design technology (MATLAB/Simulink) to quickly develop motor control algorithms for BLDC, ACIM, and PMSM motors using NXP S32K MCUs on the S32K144 automotive reference platform. Learn the basics of the motor control toolbox to generate C-code from simulation models. The toolbox will be utilized demonstrating peripheral driver blocks, optimized automotive math/motor control blocks, software and processor in the loop techniques for algorithm verification, as well as other utilities for MCU profiling and algorithm development.
查看全文
Overview of NXP’s General Purpose and Integrated Solutions (GPIS) Portfolio with focus on the S32K and S32M (MagniV) products.  
查看全文
With the trend of frequent and remote software updates on the vehicle, the need of managing this properly at the microcontroller is critical. This session will present the challenges on reprogramming edge node microcontrollers inside the vehicle and show how our S32K144 microcontroller properly addresses it safe and efficiently.  
查看全文
This session will provide an overview of the feature set and intended capabilities of the S32V234 ADAS vision processor.  
查看全文
A guide to using the Manufacturing tool. Learn how to install and use the Manufacturing tool on NXP reference boards and modify the tool for use in your own application.  
查看全文
A guide to using the Vision SDK for S32V. Learn how to leverage S32V design tools to work with APEX and ISP on the S32V family.  
查看全文
A guide to developing with the Yocto Project for i.MX application processors. Learn how to leverage the Yocto Project in development by adding layers and recipes, customizing images, working with the kernel, and other essential Yocto development tasks. 
查看全文
The hottest topic in automotive design today is the concept of the eCockpit -- where all visual functions in the car are controlled across multiple screens and fully integrated for the driver’s convenience. The key technology that enables eCockpit to run on a single processor also offers new capabilities in industrial, embedded and consumer products such as drones, manufacturing HMI interfaces and smart displays. This class will cover the fundamental technologies and architectural techniques in the i.MX 8 processor which enables rich eCockpit functionality, how NXP has implemented the world’s most significant full chip virtualization capabilities in an ARM-based processor and breaks down the eCockpit demo from the Tech Lab.
查看全文
With the very public hacks of some major vehicle brands in 2015, there is a renewed focus on vehicle security. There is a large range of vehicle electrical architectures, with significant regional variations, but there is an acceleration towards a domain orientated secure network. This presentation will look at the growing importance of the central gateway in a world of increased connectivity and security. As Ethernet becomes more prevalent, the topic of IP routing & firewall will be introduced and its role in adding another security layer. Finally, the role of the central gateway in enabling OTA software updated beyond the telematics unit, to the entire network will be presented.  
查看全文