Connects - Training Material

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

Discussions

Sort by:
This course will provide an in-depth system analysis of High Voltage (HV) Electric We review how the MCU, GDIC and IGBTs function individually and as a system. We will discuss EV and HEV power systems and components for achieving a highly efficient and safe HV motor drive. Using system block diagrams and oscilloscope screen shots of NXP’s new HV IGBT GDIC, the GD3100, and Fuji GEN 7 IGBT modules as we will consider how to achieve smaller, more efficient and lower cost HV inverter designs. We will review SPI interface programmability that enables any IGBT to be tuned for maximum efficiency, thermal design considerations, layout considerations, power budget assessment, power up sequencing, managing short circuit faults, temperature monitoring and advanced features achieve system ASIL level D and ISO26262 certification.
View full article
Time-Sensitive Networking (TSN) makes deterministic Ethernet possible. TSN provides evolution for industrial real-time networks and is a set of IEEE® 802 Ethernet sub-standards defined by the IEEE TSN task group. In this session, learn about the key TSN standards and how they work together. Understand more about NXP solutions for both TSN endpoint and TSN switch with abundant software support based on Arm®v8 platforms.
View full article
This session will focus on tire localization: Dual axis sensors enable rotation rate detection and determination of drivers / passenger side in seconds. NogaroE: Enhanced features added to a proven volume production TPMS sensor. Gen 4x4: Next-generation of ultra-low power TPMS sensors in smallest package features increased accuracy and processing power.
View full article
During this session, we will discuss the new memories supported on the new i.MX8 processor family. For DRAM, this will include DDR4 and Low Power DDR4 (LPDDR4). For non-volatile memory this will include Octal SPI NOR (XccelaTM Flash) which offers up to 400MB/s as well as the latest eMMC 5.X devices that also support high speeds. These devices are offered with Commercial, Industrial or Automotive temperature and quality ratings. This year, we will provide additional information on LPDDR4X (X=lower power I/O) as well as eMMC 5.1 high performance features including command queueing, and several new Cache operations. This session will provide designers with the tools necessary to create state-of-the-art i.MX 8 systems.  
View full article
This session covers NXP virtualization offering on Arm based platforms. The following will be covered: KVM; DPAA2 direct assignment; PCI direct assignment; VIRTIO I/O virtualization; DPDK/ODP enablement in Virtual Machine; VIRTIO IOMMU support for enhanced isolation in Virtual Machine; Linux Containers, Dockers; Libvirt; Performance analysis and optimization; Debugging support; Future plans; Universal CPE devices and SD-WAN forwarders and branch routers.
View full article
Edge computing puts cloud-computing software infrastructure on embedded-class processing platforms to reduce latency and uplink bandwidth consumption. Ranging from 1-core to 16-core devices, integrating important I/O features and integrating a hardware root of trust, the Layerscape family is ideal for edge-computing platforms. Complementary software like EdgeScale increases these platforms ease of use and accelerates customers' time to market. This session provides an overview of running Edge compute applications on Layerscape family of processors. It covers the concept of Edge computing and why it is needed, and goes on to elaborate the various use-cases where it can be used. It explains how customers can use the Layerscape SDK to run container based Edge compute applications, and leverage popular Edge Compute frameworks from AWS, Azure, Alibaba amongst others.
View full article
In the last 10 years, Green Hills has observed carmaker and Tier 1 customers expand from the traditional segments of powertrain, airbags and braking ECUs into graphics-rich dashboards, open source operating sytems and the secure Connected Car. A leading requirement is ECU consolidation while keeping ASIL safety intact. This requires the run-time architecture to safety and securely run guest operating systems Linux or Android on the same single core (or across multiple cores as SMP) alongside safety or security-critical applications like instrument clusters, gateways, V2X and ADAS. Here, we'll take a closer look at the customer’s pain points and goals, and we’ll summarize various industry solutions, including the INTEGRITY Multivisor secure hypervisor.
View full article
ARM® mbed™ OS is an open source embedded operating system designed specifically for simplifying the development of scalable Internet of Things (IoT) devices. It includes all of the features you need to develop a connected-product based on ARM Cortex®-M microcontrollers such as Kinetis and LPC MCUs.  In this hands on workshop you will get familiar with the features of mbed OS and learn how to develop and debug mbed OS applications with a traditional IDE.
View full article
The number of ECUs in a car is increasing dramatically on a year by year basis. Modern cars are starting to introduce the concept of centralizing multiple domains (Infotainment, ADAS, etc.) in a single ECU and separate them using technologies like virtualization, multicore or multiple SOCs. Although separated, these entities need to communicate and implementing a software communication solution which is scalable, portable, open and easy to program is key to offering a complete software enablement to our customers. This session will present NXP software solution for communication within a domain and between domains controllers in an ECU.
View full article
See how to use the Trust Architecture Features of the LS1012A to securely connect to a cloud service.
View full article
Security has never been more critical than it is today. Learn how the QorIQ Trust Architecture can be leveraged to increase the security of your design. Different phases in a product's life cycle can expose different vulnerabilities for attackers to exploit. This session covers secure device life cycle management as a concept, while also providing specific examples of secure implementations using QorIQ Trust Architecture.
View full article
Overview of the S32x next-generation safety architecture spanning ASIL B to ASIL D. What’s new and how we better enable the customer with a full set of safety collateral including MCU HW, SW and SBC HW.
View full article
Show the importance of OTA updates and the requirements for a total system solution for FOTA.
View full article
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.  
View full article
Design, Software & Services LAT-DES-T2443 - An Update on i.MX Applications Processors Product Family: i.MX 6UltraLite, i.MX 6ULL, i.MX 6QuadPlus, i.MX 7 and i.MX 8  LAT-DES-T2441 - Demystifying Designs with MPUs: How the Available Documentation and Tools Can Ease the Process of a Complex i.MX Application Processor based Board  LAT-DES-T2445 - PCB Layout Tips and Tricks – A Journey to Robustness  Smart Home & Buildings LAT-HMB-T2459 - Future Electronics: Designing with Security in Mind  LAT-HMB-T2460 - Turing Computer: Hands-On Workshop: Adding Hotspot Features (3G/4G-Wi-Fi Router) to Your Multimedia Product  Insight & Innovation LAT-INS-T2442 - Analog Solutions for Multi-Market - Automotive and Industrial LAT-INS-T2438 - Learn About the Most Comprehensive Solutions based on ARM® Cortex®-M MCUs: Kinetis and LPC  LAT-INS-T2437 - Solutions Around the Core - Designing with NXP’s Interface and Power Solutions
View full article
S32K based soution for smart LED drivers from Inova Semiconductor. Introduction, protocol overview, hardware and software insights.
View full article
This hands-on workshop provides a detailed architecture description of Thread technology and wireless mesh networking. The main Thread concepts will be reviewed and analyzed thoroughly. The attendee will have a deep understanding of the main concepts and how these are mapped to the NXP software API. The session will close with hands-on training to enable the attendee to understand software usage and configuration, low-power features and security concepts.
View full article
The raison d'etre of edge computing is processing IoT sensor data, and machine learning techniques are increasingly being used for this analysis. Although general-purpose CPU cores can handle ML, specialized accelerators deliver 10x the performance in the same power envelope. Learn how Layerscape compute and acceleration is addressing the needs today - and see what the future holds.
View full article
Learn how to go from an IoT idea to a proof-of-concept as easy as 1-2-3 for a connected, secure, small-form factor IoT end node. The Rapid IoT kit integrates 30+ active components (11 NXP parts) with drivers, middleware, example applications and features an innovative web IDE with GUI-based programming, as well as mobile App and IoT cloud services.
View full article
In the past, auto HMI developers approached the instrument cluster, infotainment system and any other auxiliary driver displays as separate projects, each with their own unique challenges and requirements. With eCockpit HMI developers are tasked with approaching the cluster, IVI system, HUD, rear-seat entertainment and other screens in the vehicle as a single system of displays that have been fragmented within the vehicle and even run on a singular MPU. Examine the requirements for these new integrated cockpit systems. Discuss how design teams can deliver consistent language, look and feel across multiple displays with separate and varied purposes. Talk about the concerns related to safety and certification for system as it applies to a variety of auto standards and reveal how teams can successfully design these systems for a single processor family and reuse across low- high-end auto models.
View full article