コネクト - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

ディスカッション

ソート順:
Building on the classroom training presentation "Deploying eIQ Machine Learning on NXP MCU and Apps Processors", this hands-on session will allow attendees to take a trained neural network model and deploy it on a i.MX RT1060 crossover processor. Attendees will use MCUXpresso as the development environment and implement an end-to-end use case. See notes here.
記事全体を表示
i.MX RT has a flexible external SPI Flash interface, which supports all existing SPI protocols. However, Serial Flash products may vary in READ performance due to the number of I/O, command protocols and the maximum frequency. Serial Flash Read performance has a direct impact on the system bootup time as well as code execution efficiency. In an advanced system design where system code is shadowed from Flash to DRAM, the initial boot time depends on the data transfer time from Flash to DRAM. In a cost-efficient system design, DRAM is reduced or eliminated since the processor will be able to fetch execution instructions directly from the Flash to the internal cache. During code fetching, a fixed length of data (typically 32- or 64-Byte) is read out from the flash. Shortening the overall 32-Byte or 64-Byte Read time will greatly reduce processor’s wait cycle, leading to improvement on XiP efficiency.
記事全体を表示
No other company has the breadth and diversity of embedded solutions for addressing the challenge of IoT Security. From secure element ICs to advanced multimedia and networking processors, NXP delivers the technology needed for securing the entire Lifecycle of the end or edge node. In addition, with Edgescale Cloud services software, devices can be maintained from deployment until decomissioning. Join this class for an overview of NXP's security solution.
記事全体を表示
Hands-on starting with the i.MX 8M Mini EVK, we will cover the out-of-the-box enablement including software, tools, hardware design guides, and demonstration software. Attendees should leave this class with the confidence to start their own design using the i.MX 8M Mini.
記事全体を表示
Introduction to the MCU Alexa Voice solution describing the features, architecture, and presenting the cost and ease of use benefits. We will be also showing the Out-of-Box Experience of on-boarding Alexa using Wi-Fi as well as interacting with Alexa by using a cost effective far-field Implementation.  
記事全体を表示
People today face way too many options, especially when it comes to so called smart devices which can easily contain 50+ functional settings. With most people only using a few preferred settings, this session shows product managers, UI designers, and engineers how to leverage NXP’s out of the box Face Rec based Friction Free Interface production grade platform to rapidly add a truly seamless interface to devices such as appliances, home comfort systems, and alarm/safety/security panels, as well as many types of industrial equipment. By recognizing who you are and what you prefer based on past usage, today’s smart machines can tailor their interface to meet end consumer needs person by person (including controlling access) significantly improving customer satisfaction. Wi-Fi and/or connection to the cloud is NOT required to move your interface design to the next level!
記事全体を表示
The System Controller Firmware is an essential part of the i.MX 8 architecture. In this session you will learn what the System Controller Firmware is and how to use its API on your application.
記事全体を表示
Join this session to learn about the i.MX 8/8X application processors that offer a natural migration path from the successful i.MX 6 series for industrial and automotive markets. This class will highlight the feature enhancements in CPU performance, graphics, multimedia, audio and connectivity. And will cover the basics on security, machine learning, build and distribution of Linux and Android systems, management of storage devices, graphics and demo settings. You will leave the session with the knowledge on the features of the i.MX 8/8X and how to get up and running quickly on the development boards.
記事全体を表示
Hands-on starting with the i.MX 8M Mini EVK, we will cover the out-of-the-box enablement including software, tools, hardware design guides, and demonstration software. Attendees should leave this class with the confidence to start their own design using the i.MX 8M Mini.
記事全体を表示
Join this session to get a glimpse of where you will see i.MX 8/8X in the near future and why graphics, ML, AI, video, image processing, vision, connectivity, audio and voice functions make the i.MX 8 series ideal for Automotive and Industrial applications. Learn about the i.MX 8/8X families that are comprised of common subsystems establishing an unmatched range of performance scaling with pin-compatible options and the highest level of software reuse. In addition, learn more about the upcoming i.MX 8DualMax product line to help customers meet additional cost performance scaling across the i.MX 8 family.
記事全体を表示
NXP’s latest i.MX 8M processors require the latest memories to keep them running efficiently. As a system designer, your memory choices can impact the performance, size, cost, power reliability and longevity of your end product. We will discuss the latest memories supported on the new i.MX 8M processor family. This includes DDR3, DDR4 and LPDDR4. We will show designers how they can prioritize performance, power or price to develop the most optimum system. We will also provide details on eMMC 5.1 storage products. This includes high performance features including command queueing, and several new Cache operations. We will also highlight a new MCP that includes LPDDR4 and eMMC in a single space saving package. This session will provide designers with the tools necessary to create state-of-the-art i.MX 8M systems.
記事全体を表示
Learn how to get started with the Zephyr Project on i.MX RT. You will gain hands-on experience with the Zephyr build environment and program your first Zephyr application onto a board.
記事全体を表示
A guide to developing with the Yocto Project for i.MX application processors. Learn how to leverage the Yocto Project to get started working on NXP reference boards.
記事全体を表示
Start using UUU i.MX family. An overview of the new firmware download tool called Univeral Update Utility that has replaced the manufacturing tool.
記事全体を表示
This lecture provides an overview of the software and hardware enablement available to accelerate customer time-to-market and reduce development risks for an In-Vehicle Infotainment (IVI) system. Namely an application processor from i.MX 8 family, Ethernet Switch and PHY, Software Defined Radio and Audio processing, Audio Class-D amplifier, power management, supported by Genivi and AGL compliant BSP and integrated drivers and middleware components for these devices. In a second part, we will present the NXP eCockpit Proof of Concept, which leverages i.MX 8QM HW performances and partitioning capabilities and allows to run two concurrent and independent HLOS and a Safety Critical application (RVC, Display, Audio) on i.MX 8QM.
記事全体を表示
Learn how to create a secure / non-secure application and debug on a secure Cortex-M33 NXP device.
記事全体を表示
Course will provide an overview of the “Classical Machine Learning Toolbox” developed by the IoT Solutions team, along with an example integration with Microsoft Azure ML.
記事全体を表示
Hands-on starting with the i.MX 8M Mini EVK, we will cover the out-of-the-box enablement including software, tools, hardware design guides, and demonstration software. Attendees should leave this class with the confidence to start their own design using the i.MX 8M Mini.
記事全体を表示