i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
We are pleased to announce that Config Tools for i.MX v13 are now available.
記事全体を表示
BSP: L5.4.47-2.2.0-rc2 Board: imx8QM B0 HW:  LVDS2HDMI , MIPIDSI2HDMI. It is the porting of i.MX8QM dpu loopback to isi. to the 5.4.y, with the addition of the MIPI-DSI loopback and the HDMI loopback.  Overview of the DC capture configuration: For enabling the capture: only DC 0 Stream 0  and DC 1 Stream 1 can be captured The pixel link Master address should be set to 3 because the Receiver Address at ISI is 3 and can't be changed. To continue displaying the stream, the Receiver Address at LVDS and DSI or HDMI should be changed to 3. It is possible to change the RA by using GPIO of the modules.   Patches: Create V4L2 device enabling the capture of by the ISI of DC loop-backs. Enable ISI capture from DSI 0 / LVDS 1 in 1920x1080 (at the same time.) Enable ISI capture from HDMI in 2840x2160 (half with even pixel) in 1920x2160. While capturing with the ISI, the captured screen continue to be displayed. Remark: Ov5640 cameras are also enabled in the same dtb. So 4 stream in 1920x1080 can be captured at the same time. Installation and gstreamer command: See readme
記事全体を表示
The i.MX8QuadMax SMARC System On Module integrates Dual Cortex A72 + Quad Cortex A53 Cores, Dual GPU systems, 4K H.265 capable VPU dual failover-ready display controller based i.MX8 QuadMax SoC with on SOM Dual 10/100/1000 Mbps Ethernet PHY, USB 3.0 hub and IEEE 802.11a/b/g/n/ac Wi-Fi & Bluetooth 5.0 module.
記事全体を表示
current imx6 bsp, not only ltib but also yocto couldn't support subtitle. now we have two solution to support subtitle on yocto, 1)one is extract the subtitle, then draw the subtitle on the video by UI, which is supported by the imxplayer. this solution is using QT by imxplayer, so if you build yocto, should choose QT as target. basicly, aiurdemux send the text to the QT by appsink, then QT draw the text on the UI layer. when build the yocot, pls using the command as below: " bitbake fsl-image-qt5" copy the font libary to the /usr/lib/fonts, then when you play the imxplayer, choose the font you need. 2)another one is blending the subtitle on the video buffer by gstreamer, then output with video enable gst pango lib in gstreamer1.0-plugins-base change playbin flag to disable native video flag basetextoverlay apply patch http://cgit.freedesktop.org/gstreamer/gst-plugins-base/commit/ext/pango/gstbasetextoverlay.c?id=267a8c24af4f02ba6f3075bd589d3c5d1dc826e9 use following command line gst-launch-1.0 playbin flags=0x17 uri=file://$VIDEO_FILE suburi=file://$SUBTITLE_FILE
記事全体を表示
通常的音乐播放是这样一个流程: alsa将一段上层的应用空间和底层的物理空间通过mmap映射起来,然后DMA从被映射的物理空间往I2S的fifo传送数据。 现在有个客户想将FEC网络那边收到的数据中的audio数据分离出来,暂存到一段物理内存中,然后通过DMA传输到我们芯片的I2S fifo,从而节省掉数据在上层、底层之间来回调用的时间。 这就需要我们I2S这边支持通过DMA直接从一段物理内存拿数据。 为了较为方便的实现这一功能,通过对ALSA架构的分析,我保留了我们整个ASoC代码的架构,只是不让DMA从原来的mmap的地址拿数据,而是从我自己分配的DMA内存中拿数据。 258         uint8_t *wbuf; 259         uint8_t *index1; 261         wbuf = dma_alloc_coherent(NULL, 0x10000, &wpaddr, GFP_DMA); 265         for (i=0; i<0x10000; i++) { 269                         *(wbuf + i) = wav_data[i]; 273         } 333                 iprtd->desc = chan->device->device_prep_dma_cyclic( 334                         chan, wpaddr, 335 //                      chan, dma_addr, 336                         iprtd->period_bytes * iprtd->periods, 337                         iprtd->period_bytes, 338                         substream->stream == SNDRV_PCM_STREAM_PLAYBACK     ? 339                         DMA_TO_DEVICE : DMA_FROM_DEVICE); 代码实现上,实际上是比较简单的,可以套用以前做过的dma_m2m的部分代码。 现在我们要拿一些wav里面的audio数据。 linux可以用16进制的方法读wav里面的数据: hexdump -n 65700 -C audio44k16S.wav > wav_data_44100_s16_stereo.h将audio44k16S.wav 里面的audio数据用16进制的形式保存到wav_data_44100_s16_stereo.h这个文件里。 然后我们要编辑这个头文件里的audio数据,原数据是这种格式的: 00000000  52 49 46 46 12 63 0c 00  57 41 56 45 66 6d 74 20  |RIFF.c..WAVEfmt | 00000010  12 00 00 00 01 00 02 00  44 ac 00 00 10 b1 02 00  |........D.......| 00000020  04 00 10 00 00 00 66 61  63 74 04 00 00 00 b5 18  |......fact......| 00000030  03 00 64 61 74 61 d4 62  0c 00 58 01 f0 00 98 01  |..data.b..X.....| 00000040  56 01 3d 01 1e 01 d0 00  ae 00 81 00 35 00 40 00  |V.=.........5.@.| 00000050  dd ff f7 ff 90 ff 9f ff  1d ff 54 ff bb fe 18 ff  |..........T.....| 00000060  61 fe 1e ff e7 fd 5e ff  e4 fd 23 00 39 fe ee 00  |a.....^...#.9...| 我们要把它转换成符合我们要求的这种形式: ,0x63 ,0xf0 ,0x0f ,0xf0 ,0x7f ,0xf1 ,0x21 ,0xf1  ,0x89 ,0xf3 ,0xef ,0xf2 ,0x9d ,0xf5 ,0x8c ,0xf4 ,0x5f ,0xf7 ,0xd3 ,0xf5 ,0x8c ,0xf8 ,0x08 ,0xf7  ,0x4c ,0xf9 ,0x01 ,0xf8 ,0x74 ,0xf9 ,0x2e ,0xf8 ,0x1c ,0xf9 ,0x15 ,0xf8 ,0x09 ,0xf9 ,0x82 ,0xf7  ,0x45 ,0xf9 ,0xd1 ,0xf6 ,0x0b ,0xf9 ,0x1e ,0xf6 ,0xce ,0xf8 ,0xbe ,0xf5 ,0xd7 ,0xf8 ,0x9a ,0xf5  ,0xa8 ,0xf9 ,0xc7 ,0xf5 ,0xe0 ,0xfa ,0x3e ,0xf6 ,0x25 ,0xfc ,0x44 ,0xf7 ,0x44 ,0xfd ,0xa2 ,0xf8  ,0x9a ,0xfe ,0xea ,0xf9 ,0x25 ,0x00 ,0x94 ,0xfb ,0x16 ,0x02 ,0xec ,0xfc ,0xcb ,0x03 ,0xfe ,0xfd  ,0xef ,0x04 ,0xa5 ,0xfe ,0x45 ,0x05 ,0x0b ,0xff ,0x3b ,0x05 ,0x24 ,0xff ,0x34 ,0x05 ,0x94 ,0xff  ,0x06 ,0x05 ,0x13 ,0x00 ,0x6c ,0x04 ,0x82 ,0x00 这里有一个比较好的方法, 可以通过VIM 垂直编辑的方法较为轻松的实现。 vim垂直编辑: ctrl+v 然后上下左右移动选中,D删除选中的。 ctrl+v 选中, shift+i 可以在选中的地方加入想插入的字符。 将编辑过的数据放到uint8_t wav_data[],赋值给wbuf,wbuf对应的物理地址wpaddr中的数据,就是上面wav中的audio数据。 wbuf = dma_alloc_coherent(NULL, 0x10000, &wpaddr, GFP_DMA);中的0x10000=1024*64是我们分配的dma内纯的大小,我们sdma是根据以下大小传输数据的: iprtd->period_bytes = 21844, iprtd->periods = 3 //21844*3=65532= 0xfffc 这样实际上DMA是不停的刷我们分配的内存里的数据,因为我们没有更新DMA内存里的数据,所以听到的是不断重复播放的声音片段。 刚开始时,我听这个片段,发现片段之间有较为明显的pop音,这是由于我截取的是一首音乐开始的部分,包含了wav包头数据,这不是音乐数据,将这个去除就可以了。
記事全体を表示
Adding Support to USB Host High Speed on i.MX27ADS First, ensure these patches were applied: usbh2_cspi1_ss2.patch usbh2_set_ulpi_xcvr.patch Unselect SPI2: Device Drivers  --->              SPI support  --->                     [ ]   CSPI2 Select USB Host2: USB support  --->            <M>   EHCI HCD (USB 2.0) support                 [*]       Support for Host2 port on Freescale controller
記事全体を表示
The i.MX31 multimedia applications processors are designed for a broad range of industrial, consumer and automotive applications. Based on an ARM1136JF-S™ core, both the i.MX31 and the i.MX31L processors are engineered to deliver powerful performance while minimizing power consumption. The rich feature set of the i.MX31 processors make them an excellent choice for portable media players, portable navigation devices, medical/industrial monitoring systems, automotive infotainment systems and many general embedded applications. i.MX Family Comparison Product Information on Freescale.com i.MX31 Multimedia Applications Processor Evaluation/Development Boards and Systems IMX31PDK:  i.MX31 Product Development Kit Getting Started Getting Started with the i.MX31PDK Board Flashing i.MX31 PDK Board I.MX31 PDK Board using RedBoot Miscellaneous Tutorials Blinking iMX31PDK LEDs using U-Boot How to Test i.MX31 RNGA Hardware? How to Test i.MX31 TvOut on i.MX31PDK How to Use Clock Out on i.MX31 Issues when interfacing Micron's 78nm mDDRs IMX31ADS Getting Started Getting Started with the i.MX31ADS Board Flashing I.MX31 ADS Board Miscellaneous Tutorials Booting Linux from NAND Flash on the i.MX31ADS Compiling Linux kernel from mainline to i.MX31ADS Issues when interfacing Micron's 78nm mDDRs Embedded Software and Tools Android OS for i.MX Applications Processors Partners / 3rd-Party Development Tools Starterkit STKa31 (Technology in Quality) Additional Resources i.MX31 ADS i.MX31 PDK i.MX31 PDK Board Alpha Blending i.MX31 PDK Board DirectFB i.MX31 PDK Board V4L tests i.MX31 PDK Contents i.MX31 PDK Setting Buttons and Jumpers i.MX31 Lite Kit
記事全体を表示
///////////////////////////create device node /dev/galcore///////////////////////////// $home/myandroid/kernel_imx/drivers/mxc/gpu-viv/Kbuild MODULE_NAME ?= galcore /* define node name*/ $home/myandroid/kernel_imx/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_linux.h define DEVICE_NAME "galcore" $home/myandroid/kernel_imx/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_probe.c drv_init call ret = register_chrdev(major, DEVICE_NAME, &driver_fops); ///////////////////////////////opengles2 functios/////////////////////////////////////////// myandroid/device/fsl-proprietary/gpu-viv/lib/egl/libGLESv2_VIVANTE.so glActiveTexture glBindBuffer ... ... ... //those glxxxxxx call into sub_D40C int __fastcall sub_D40C(int a1, int a2, int a3) //address 0x0000D40C { int result; // r0@1 int v4; int v5; v4 = a2;   v5 = a3;   gcoOS_GetTLS(&v4);  //------------> goto libGAL.so   result = v4;   if ( v4 )     result = *(_DWORD *)(v4 + 36);   return result; } and $home/myandroid/device/fsl-proprietary/gpu-viv/lib/libGAL.so //export function signed int __fastcall gcoOS_GetTLS(void **a1) { ... ... gcoOS_GetTLS v4 = open("/dev/galcore", 2); ... ... } and device node /dev/galcore pass command into module galcore $home/myandroid/kernel_imx/drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel.c gckKERNEL_Dispatch This document was generated from the following discussion: Share Vivante 3d gc2000 work flow
記事全体を表示
Product Family Features Freescale's i.MX family of applications processors has demonstrated leadership in the portable handheld market. The i.MX21 multimedia applications processor is the latest addition to this family and builds on its low-power, high-performance heritage. Freescale has shipped more than 60 million chips of our industry-founding applications processors. That means you can start smart by picking products with a technology pedigree to handle all the creativity you can pump into them. The i.MX21 features the advanced and power-efficient ARM926EJ-S core operating at speeds starting at 266 MHz and is part of a growing family of Smart Speed products that offer high performance processing optimized for lowest power consumption. ARM926EJ-S™ core (16 KB I-Cache, 16 KB D-Cache) Smart Speed Switch 16/18-bit color LCD controller up to SVGA USB On-The-Go (two-host port) MPEG-4 and H.263 encode/decode acceleration up to CIF 30 fps Additional Resources IMX21-ADS I.MX21 ADS Board Flashing IMX21-and-iMXL-Lite-Kit
記事全体を表示
It is one mandatory patch if you are in the case: The chip you are using is imx6sx TO1.3 and newer, and use the kobs-ng to flash your image to the Nand memory chip. If you are using MFG, you also need rebuild the kobs-ng, and update the binary into your MFG tool.  The patch have been integrated into the default release yocto_4.1.15, but if you are using the older version release before yocto_4.1.15, please make sure you have integrated the modification when you need to use kobs-ng to flash the image to Nand memory chip. commit 5ecf08703da489a3bd317341f630870a3d07dab9 Author: Han Xu <[email protected]> Date:   Thu Jan 28 14:40:14 2016 -0600     MMT-105: change the i.mx6sx revision check change the i.mx6sx revision check since v1.3 uses v1.2 boot config as well.     Signed-off-by: Han Xu <[email protected]>     (cherry picked from commit 1dac0c14d1e2016c2fa804f6628543d8d238c680) diff --git a/src/plat_boot_config.c b/src/plat_boot_config.c index 461675a..e1ef6f3 100644 --- a/src/plat_boot_config.c +++ b/src/plat_boot_config.c @@ -1,5 +1,5 @@ /* -* Copyright (C) 2010-2015 Freescale Semiconductor, Inc. All Rights Reserved. +* Copyright (C) 2010-2016 Freescale Semiconductor, Inc. All Rights Reserved. */ /* @@ -256,10 +256,12 @@ int discover_boot_rom_version(void)                                         }                                         fgets(line_buffer, sizeof(line_buffer), revision);                                         if (!strncmp(line_buffer, "1.0", strlen("1.0")) || -                                                       !strncmp(line_buffer, "1.1", strlen("1.1"))) +                                                       !strncmp(line_buffer, "1.1", strlen("1.1"))) {                                                 plat_config_data = &mx6sx_boot_config; -                                       if (!strncmp(line_buffer, "1.2", strlen("1.2"))) +                                       /* all other revisions should use the latest boot config */ +                                       } else {                                                 plat_config_data = &mx6sx_to_1_2_boot_config; +                                       }                                 }                                 if (!strncmp(line_buffer, plat_imx6ul, strlen(plat_imx6ul))) How to apply it to older version quickly:  Apply the patch and rebuild the kobs-ng in yocto_3.14_x environment: bitbake -c compile -v -f imx-kobs cd tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/imx-kobs/5.0-r0/imx-kobs-5.0 git apply yocto_3_14_x.patch bitbake -c compile -v -f imx-kobs you can find the new binary “kobs-ng” under “tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/imx-kobs/5.0-r0/build/src” Apply the patch and rebuild the kobs-ng in yocto_3.10_53 environment: . ./setup-environment build bitbake -c compile -v -f imx-kobs cd tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/imx-kobs/3.10.53-1.1.0-r0/imx-kobs-3.10.53-1.1.0 git apply yocto_3_10_53patch bitbake -c compile -v -f imx-kobs you can find t he new binary “kobs-ng” under tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/imx-kobs/3.10.53-1.1.0-r0/imx-kobs-3.10.53-1.1.0/src As one alternation method, you also can download the whole imx-kobs-5.4 package which yocto_4.1.15 is using to build. wget http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-kobs-5.4.tar.gz
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343761 
記事全体を表示
For more information verify the U-Boot User Manual[1].   First all configure your board IP, your host IP and the gateway IP:   => setenv ipaddr 10.29.244.91   => setenv serverip 10.29.244.27   => setenv gatewayip 10.29.244.27 You don't need to set the gatewayip when using cross'cable! Save this configuration to flash: => saveenv   Download the file to board RAM: => tftp 0x80000000 zImage   Where:   400000 is the memory position where the file will be placed;   zImage is the file that will be downloaded from TFTP server.  
記事全体を表示
BSP version: 11.03 Multimedia Package version: 11.03 1. Install BSP and Multi Media package (11.03 release) 2. Avoid Display Timeout: append the following line to rootfs/etc/oprofile: echo -e -n '\033[9]' > /dev/tty0 3. Set VGA port as the primary display in the kernel command line: video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga 4. Connect a VGA monitor and WVGA display to the MX53 Quick Start 5. Boot Linux on MX53 Quick Start board (NFS is used in this example) 6. Unblank WVGA display (fb1): $ echo 0 > /sys/class/graphics/fb1/blank 7. On the target enter into /dev/shm directory. If the following files are present: vss_lock vss_shmem ,delete them. 8. On your host, edit the ltib/rootfs/usr/share/vssconfig as following: vss device definition Master=VGA, Slave=WVGA master display [VGA] type = framebuffer format = RGBP fb_num = 2 main_fb_num = 0 vs_max = 4 slave display [WVGA] type = framebuffer format = RGBP fb_num = 1 vs_max = 4 9. Run the Gstreamer pipeline below: gst-launch filesrc location=file.mp4 ! qtdemux ! mfw_vpudecoder ! mfw_isink display=VGA display-1=WVGA Video is played on the VGA and WVGA panels. A 720p file can be played at the same time.
記事全体を表示
Changing Freescale's BSP U-boot using LTIB This quick recipe demonstrates how to compile U-boot using Freescale BSP. 0. After installing i.MX51 BSP: 1. Extract u-boot source: ./ltib -m prep -p u-boot 2. (optional) If you wish to apply changes to the code, the source is located at: <ltib path>/rpm/BUILD/u-boot-2009.08 3. Compile u-boot for the i.MX51 EVK ./ltib -m scbuilb -p u-boot 4. Copy the compiled file to a SD card on your host machine, insert the SD card and: $ sudo dd if=rpm/BUILD/u-boot-2009.08/u-boot.bin of=/dev/mmcblk0 bs=512 /dev/mmcblk0 should replaced according to your host, use "dmesg" after inserting the SD to find out where is the SD on your host. Unmount it before issuing the dd command.   5. Insert the SD on the i.MX 51 EVK, set the switches for SD Card boot and power on the board.
記事全体を表示
Continental Yocto Training Author:           Leonardo Sandoval Material: PDF Tutorial: i.MX Yocto Project: Freescale Yocto Project Tutorial Provided Virtual Machine Wandboard Dual Wandboard - Freescale i.MX6 ARM Cortex-A9 Opensource Community Development Board - BLOG Tasks: Task 1: Build and Boot your board in N-steps     1.    Create a new folder ($ mkdir conti-fsl-community-bsp)     2.    Follow all N-steps (from the tutorial, page 2) EXCEPT the baking     3.     Baking has been done for you, so assume that the bake is done!     4.    Flash:         conti-fsl-community-bsp $ cd         $ cd fsl-community-bsp/build         build $ dd if=tmp/deploy/images/core-image-minimal-wandboard-dual.sdcard of=/dev/sdb bs=1M         build $ sync # NEVER FORGET THIS STEP, You have been warned!     5.    Boot         Task 2:    Folders     1. Tree structure & size         fsl-comunity-bsp $ tree -d -L 2         fsl-comunity-bsp $ du -h --max-depth=2 Task 3:    Architecture Task 4:    Metadata Task 5:    Config files         build $ cat conf/local.conf         build $ cat conf/bblayer.conf Task 6:     Layers build $ bitbake-layers show-layers sources $ cat meta-fsl-arm/conf/layer.conf Task 7:    Adding an existing layer     1. Clone the repo sources $ git clone https://github.com/lsandoval/meta-fsl-test.git     2. Add the layer to build/bblayers.conf sources $ cd ../build build $ vi conf/bblayers.conf     3. Browse the new layer files     4. Compile the kernel build $ bitbake -f -c compile linux-wandboard build $ bitbake -c deploy linux-wandboard     5. Flash    build $ sudo mkdir /media/boot         build $ sudo mount /dev/sdb1 /media/boot         build $ cp tmp/deploy/images/uImage /media/boot         build $ sudo umount /media/boot     6. Boot Task 8: (Optional) Check the core-image-minimal-test image, bake and flash it. Run the 'helloworld' app Task 9: Q&A
記事全体を表示
If Android device has Internet access, it can download and install TTS library automatically. However, sometimes in a developer environment, Internet may not be available. Download TTS library from Eyes-Free project, [1] Unzip all files into VFAT partition (of SDCard). It will create two directories: daiane@b19406:/media$ sudo ls disk-3/ -l total 231552 drwx------ 6 daiane root      4096 2010-05-24 15:46 espeak-data drwx------ 2 daiane root      4096 2010-05-24 15:46 svox daiane@b19406:/media$ mount /dev/sdd5 on /media/disk-1 type ext3 (rw,nosuid,nodev,uhelper=hal) /dev/sdd2 on /media/system type ext3 (rw,nosuid,nodev,uhelper=hal) /dev/sdd6 on /media/disk-2 type ext3 (rw,nosuid,nodev,uhelper=hal) /dev/sdd1 on /media/disk-3 type vfat (rw,nosuid,nodev,uhelper=hal,shortname=mixed,uid=1001,utf8,umask=077,flush) /dev/sdd4 on /media/recovery type ext3 (rw,nosuid,nodev,uhelper=hal)
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343059 
記事全体を表示
NFS After LTIB installation, follow the instructions below to configure and build Linux Image and Root File System. TIP: Type: $./ltib --help to get more information on ltib In the folder where LTIB were installed, execute the file: $./ltib It should take some minutes to complete the installation. Configure the ltib to select the options and packages to be defined and installed in Linux Image and Root File System. $./ltib -c     or     $./ltib -m config The menu configuration should appear: To configure for use the system with NFS, go to: Target Image Generation -> Target Image -> NFS Only For basic compilation, exit LTIB. It will compile and add some pre-built packages to make the target file system.
記事全体を表示
         Some customer enable AHAB function on i.MX8X board to realize security boot. So they have fused hab_closed bit on the board. While they want to change DDR type on this board so need to do DDR stress test. While If using NXP official released DDR stress test, it failed to run on such hab_closed board.         This article describe how to run command line version DDR stress test on such hab_closed board.        Thanks!
記事全体を表示
i.MX 51 EVK Board Bootloader i.MX 51 EVK Board Flashing i.MX 51 EVK U-boot i.MX 51 EVK Compiling U-boot i.MX 51 EVK Changing Env Linux i.MX 51 Flashing Linux Application Only with SD Card Reader Multimedia i.MX 51 EVK Board USB Camera i.MX 51 EVK Board OpenCV Android All Board Android Without Ramdisk All Board install TTS Library Manually i.MX 51 Android ADB over USB Ubuntu i.MX 51 Ubuntu USB TS i.MX 51 Ubuntu TS Lucid
記事全体を表示