i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Overview Resources Download Ubuntu 12.04.01 Download i.MX28EVK BSP and Documents Ubuntu Host Setup Host Package Update Ubuntu Configuration PDF Sudo Priviledges Default Shell CCACHE Directory Layout Extract SDK and Documents Install BSP Sources Ubuntu Software Packages for LTIB Patching LTIB Create SD Card Using Ubuntu Host Media Booting Selection Cable Connections   Overview Freescale's i.M28EVK development kit provides a platform for running software and evaluating features of the i.MX28 processor. This document provides the details for running the Linux Board Support Package (BSP) on the Ubuntu 12.04 64-bit Precise Pangolin Host on an Intel/AMD architecture computer. The 32-bit host is not covered in this document and does have different configuration steps than described here.   An Ubuntu Linux host is used to cross-compile the BSP creating ARM images. The BSP provides a build system named Linux Target Image Builder, (LTIB),  the GNU tool suite for compiling and debugging, U-Boot boot loader, Linux kernel, and a root file system. Resources i.M28EVK- i.MX28 Evaluation Kit Web Page MCIMX28EVKJ Product Summary Page- i.MX28 Download Collateral L2.6.36_MX28_SDK_10.12_Source- BSP Source Download Linux documentation - i.MX28EVK Documentation Ubuntu 12.04.1 LTS (Precise Pangolin)- Ubuntu 12.04 Release Download Ubuntu 12.04.01 A dedicated computer running Ubuntu or a Virtual Machine, (VMware or VirtualBox), can be used for running the Host Ubuntu software. The Ubuntu image is available for downloaded from the Ubuntu site: Ubuntu 12.04.1 LTS (Precise Pangolin).   This Ubuntu host ISO was used with the md5 checksum: ubuntu-12.04.1-desktop-amd64.iso  06472ddf11382c8da1f32e9487435c3d   One way to acquire the ISO is to use zsync to download: zsync http://releases.ubuntu.com/12.04/ubuntu-12.04.1-desktop-amd64.iso.zsync  Once downloaded, installing the ISO is user preference - either a dedicated Linux PC or in a Virtual Machine.   Download i.MX28EVK BSP and Documents The BSP download is from this site L2.6.36_MX28_SDK_10.12_Source and the documents from Linux documentation that requires a free registration to specify login credentials,   436e0b8e1c7976c657d530a45f9dbd0c L2.6.35_10.12.01_SDK_source_bundle.tar.gz de0274320a17c1e989d1ef5c088973e2 L2.6.35_10.12.01_SDK_docs.tar.gz   Ubuntu Host Setup Ubuntu login credentials of User: user Password: user are used for this documents. Host Package Update Once logged in to the Ubuntu host, the existing packages are brought up to date to the latest version before installing the BSP. The Ubuntu package manager used is apt-get. $ sudo apt-get update $ sudo apt-get upgrade  01. Check all installed packages for new revisions 02. all newer packages found are installed.   Addtional packages are required for the ltib build system. Ubuntu Configuration PDF evince is the default pdf reader, another option is zathura. $ sudo apt-get install zathura Sudo Priviledges LTIB requires super user priviledges for some operations. To enable a visudo entry is added to the sudo'ers file. For more information run 'man visudo'.   $ sudo visudo  The first word, user, is the login account 'user' This can be changed to whatever login you used, or if you have groups configured you can provide a group that developers are in - refer to the man page for sudo for details. Add this line:   user ALL =NOPASSWD: /usr/bin/rpm/ /opt/freescale/ltib/usr/bin/rpm   Default Shell Ubuntu uses the default shell 'dash'. This however causes failures on bash scripting which is part of the ltib system. Change the default shell from 'dash' to 'bash'   $ sudo update-alternatives --install /bin/sh sh /bin/bash 1  CCACHE ccache provides a fast C/C++ compiler cache which is supported in the ltib system. To configure once the ccache package has been installed: $ sudo apt-get install ccache $ ccache -M 50M $ ccache -c  02. Set the cache limit to 50 Meg 03. Clear the cache folder   Directory Layout The following directory structure is used: /home/user/freescale/imx28/ |-- archive |-- L2.6.35_10.12.01_ER_source |-- L2.6.35_10.12.01_SDK_docs |-- L2.6.35_10.12.01_SDK_scripts |-- ltib |-- ubuntu-imx28-ltib-patch   The archive directory is where the BSP and documents are stored; command to create the directory: $ mkdir -p ~/freescale/imx28/archive   Extract SDK and Documents The following instructions were used to extract the contents of the Software Development Kit:   $ cd ~/freescale/imx28/archive $ tar -zxf L2.6.35_10.12.01_SDK_source_bundle.tar.gz -C ..    01. Change into the directory containing the tar ball that is compressed. 02. Extract the contents into the directory above (-C ..) the current directory -z unzip -x extract -f L2.6.35_10.12.01_SDK_source_bundle.tar.gz   $ tar -zxf L2.6.35_10.12.01_SDK_docs.tar.gz  01. Extract the contents into the directory above (-C ..) the current directory     -z unzip     -x extract     -f L2.6.35_10.12.01_SDK_docs.tar.gz this file The contents of both tar files are now in the directory /home/user/freescale/imx28. Install BSP Sources After extracting the content from the L2.6.35_10.12.01_SDK_source_bundle.tar.gz the file L2.6.35_10.12.01_SDK.source.tar.gz contains all the sources and the build system. Extract the contents and install. This will create the ltib directory which is the build system. $ tar -zxf L2.6.35_10.12.01_SDK_source.tar.gz $ cd L2.6.35_10.12.01_ER_source $ ./install  Read the license information and accept by entering YES. An installation directory is then asked for, providing:  .. which is the parent directory. The installation script copies the packages and will inform you that 'Installation complete, your ltib installation has been placed in ../ltib, to complete the installation: cd .../ltib ./ltib  HOWEVER before doing this, there are packages and patches that need to be applied to run ltib on Ubuntu 12.04.01. Ubuntu Software Packages for LTIB The following packages are required. The script pkg-setup.sh attached below has these packages which can be downloaded and executed to install. $ sh pkg-setup.sh  sudo apt-get -y install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev sudo apt-get -y install libdbus-glib-1-dev liborbit2-dev intltool sudo apt-get -y install ccache zlib1g zlib1g-dev gcc g++ libtool sudo apt-get -y install uuid-dev liblzo2-dev tcl wget libncurses5-dev sudo apt-get -y install libncursesw5-dev lib32z1 libglib2.0-dev xsltproc sudo apt-get -y install ia32-libs libc6-dev-i386 The file pkg2-setup.sh contains optional packages for development. To install, download and execute: $ sh pkg2-setup.sh Please refer to the document ltib_build_host_setup.pdf for more information on host setup. Patching LTIB The location of files from the glibc-devel and zlib Ubuntu 12.04 packages has changed from 9.0.4 Ubuntu which the original ltib was released against. To update ltib operation the following patches are implemented from the directory ~/freescale/imx28/ltib 1. The file ltib is changed at line 2387 adding the '-v' option to the rpm call OLD:     system('rpm --force-debian 2>/dev/null') == 0? NEW:     system('rpm -v --force-debian 2>/dev/null') == 0? 2. The file bin/Ltibutils.pm is updated to support glibc-devel and zlib.   glibc-devel update: Line 563 add check for /usr/lib32/libm.so 'glibc-devel' => sub {-f 'usr/lib/libm.so' || -f '/usr/lib64/libz.so' || -f '/usr/lib32/libm.so'},   zlibc update: Line 584 add /lib/x86_64-linux-gnu/libz.so* zlib => sub{my @f = (glob('/usr/lib/libz.so*'),               glob('/lib/x86_64-linux-gnu/libz.so*'),               glob('/lib/libz.so*'),   The above patches are also in the attachment 0001-patches-for-12.04-ubuntu.patch.   LTIB packages also need adjustments to correctly build on Ubuntu. The tar file below, ubuntu-imx28-ltib-patch.tgz contains all the updates. Download and extract the contents at the same directory level as your ltib source directory. $ tar -zxf ubuntu-imx28-ltib-patch.tgz ├── ltib ├── ubuntu-imx28-ltib-patch └── ubuntu-imx28-ltib-patch.tgz Change directories to ubuntu-imx28-ltib-patch and then run the install-patches.sh script. $ cd ubuntu-imx28-ltib-patch $ ./install-patches.sh   The following packages are updated: lkc mtd-utils mux_server sparse Create SD Card Using Ubuntu Host The tar file L2.6.35_10.12.01_SDK_scripts.tar.gz contains scripts for writing the images from the ltib build to a SD card. Extract the content, copy the scripts to the ltib directory, and update the mk_mx28_sd script to work with the updated fdisk command.   $ tar -zxf L2.6.35_10.12.01_SDK_scripts.tar.gz $ cd L2.6.35_10.12.01_SDK_scripts $ cp mk_hdr.sh ~/freescale/imx28/ltib $ cp mk_mx28_sd ~/freescale/imx28/ltib $ cd ~/freescale/imx28/ltib  Edit mk_mx28_sd script and add the 'u' at line 177 then the o command after. This changes cylinders to sectors.   OLD: echo "o n   NEW: echo "u o n   Once updated to create the SD card which is at /dev/sdb: $ ./mk_mx28_sd /dev/sdb  NOTE: if mounted automatically, you need to unmount for the script to work $ sudo umount /dev/sdb*      Media Booting Selection The i.MX28EVK has a boot option to execute from the SD Card in Slot 0 which is located on the bottom of the EVK. On the top of the EVK there are switches that are read during the start up process to determine what boot media to use. The SD Card in slot 0 is used for this example which requires the settings: B3/DIP1 B2/DIP2 B1/DIP3 B0/DIP4 1 0 0 1 Refer to the user guide, i.MX28_Linux_BSP_UG.pdf section 3.2.1. Boot Modes for all options. The user guide is found in the Linux documentation bundle documentation.  Refer to the next section for a picture showing the boot switch location and the SD Card Slot 0 location. Cable Connections A computer serial port is connected to the i.MX28EVK serial port. The communication setting is 115200 baud, 8 data bits, No parity, and 1 stop bit. There is NO flow control set for this port. This is typically shown as 115200, 8N1. The power supply is connected  
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-345644 
View full article
The doc gives an introduction about how to get and run the watch-face APK on i.MX.8ULP watch board based on Android 14.0.0_1.0.0. 1. Get source code Get the shell script and related patches from the attachment at the end of the article. Run Watchface_setup.sh. Watchface_setup.sh will download all the needed gits codes. combine with them and apply patches automatically. You need to clone the gits manually if network access is not good. 2. Build the project The project is in the sub-directory named "KWART_Kid_Launcher". Then you can build it either in Android studio or Android SDK. Android studio Open the project in Android studio and build it like regular. Android SDK Copy KWART_Kid_Launcher/ into vendor/nxp-opensource/fsl_imx_demo/ Add the following into the end of device/nxp/imx8ulp/watch_8ulp/watch_8ulp.mk. PRODUCT_PACKAGES += \ KWARTLauncher Rebuild the SDK. Please refer to Android User's Guide for more details about SDK building. make -j4 2>&1 | tee make.log 3. Install the APK Install the APK Android studio Run the app like regular. Android SDK Reflash the SDK images and the app will occur after boot finishes. Then you will find the following APP.  
View full article
Overview The purpose of this document is to provide a guide on how to enable UART 4 on i.MX8M Mini on Cortex A53. By default on i.MX-ATF is set on Cortex M4 Domain, i.MX-ATF helps ensure that i.MX processors boot securely. Reference: imx-atf. Requirements: Arm Toolchain: sudo apt-get install gcc-aarch64-linux-gnu 1. Build imx-boot image For a better reference how to build imx-boot image, go to Section 4.5.13 How to build imx-boot image by using imx-mkimage available on i.MX Linux User's Guide.   $ cd ~ $ git clone https://github.com/nxp-imx/uboot-imx -b lf_v2023.04 $ cd uboot-imx/ $ git checkout lf-6.6.23-2.0.0 $ make -j $(nproc --all) ARCH=arm CROSS_COMPILE=aarch64-linux-gnu- imx8mm_evk_defconfig $ export ARCH=arm64 $ cd ~ $ git clone https://github.com/nxp-imx/imx-mkimage.git $ cd imx-mkimage/ $ git checkout lf-6.6.23-2.0.0 $ cd ~ $ git clone https://github.com/nxp-imx/imx-atf.git $ cd imx-atf/ $ git checkout lf-6.6.23-2.0.0   The master domain for the UART4 is assigned to the Cortex M4, so, make the following changes to assign it to the A53 processor instead: diff --git a/plat/imx/imx8m/imx8mm/imx8mm_bl31_setup.c b/plat/imx/imx8m/imx8mm/imx8mm_bl31_setup.c index 179b6226f..b0427afff 100644 --- a/plat/imx/imx8m/imx8mm/imx8mm_bl31_setup.c +++ b/plat/imx/imx8m/imx8mm/imx8mm_bl31_setup.c @@ -114,10 +114,11 @@ static const struct imx_csu_cfg csu_cfg[] = { #else static const struct imx_rdc_cfg rdc[] = { /* Master domain assignment */ - RDC_MDAn(RDC_MDA_M4, DID1), + RDC_MDAn(RDC_MDA_A53, DID0), /* peripherals domain permission */ - RDC_PDAPn(RDC_PDAP_UART4, D1R | D1W), + RDC_PDAPn(RDC_PDAP_UART4, D0R | D0W), RDC_PDAPn(RDC_PDAP_UART2, D0R | D0W), RDC_PDAPn(RDC_PDAP_UART1, D0R | D0W),   After applying the changes, set your toolchain and then, compile with the following command: $ make PLAT=imx8mm bl31   In case you have the following error: Use this command to unset the flags and compile again: $ unset LDFLAGS   Then, copy the corresponding files to imx-mkimage/iMX8M. For more information, please check section 4.5.13 on i.MX Linux User's Guide. *NOTE: Some of this files are located on a link which you can access with the following command, for more information check the Release Notes, in this case for version 6.6.23-2.0.0 on Embedded Linux for i.MX Applications Processors. $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.24-fbe0a4c.bin $ chmod +x firmware-imx-8.24-fbe0a4c.bin $ ./firmware-imx-8.24-fbe0a4c.bin   Finally, copy flash.bin located on: imx-mkimage/iMX8M to a folder to flash your board as follows: You can download the uuu.exe from mfgtools and the .wic file from the prebuild images from: Embeded Linux for i.MX Applications Processors uuu.exe -b emmc_all flash.bin imx-image-full-imx8mmevk.wic   2. Change DTB to enable UART4 First, copy and rename the imx8mm-evk.dts to identify there is a change for enabling UART4: $ cd linux-imx $ cp arch/arm64/boot/dts/freescale/imx8mm-evk.dts arch/arm64/boot/dts/freescale/imx8mm-evk-uart4.dts $ vi arch/arm64/boot/dts/freescale/imx8mm-evk-uart4.dts And make the following changes: &ecspi2 { status = "disabled"; }; &uart4 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_uart4>; assigned-clocks = <&clk IMX8MM_CLK_UART4>; assigned-clock-parents = <&clk IMX8MM_SYS_PLL1_80M>; fsl,uart-has-rtscts; status = "okay"; }; &iomuxc { pinctrl_uart4: uart4grp { fsl,pins = < MX8MM_IOMUXC_ECSPI2_SCLK_UART4_DCE_RX 0x140 MX8MM_IOMUXC_ECSPI2_MOSI_UART4_DCE_TX 0x140 MX8MM_IOMUXC_ECSPI2_SS0_UART4_DCE_RTS_B 0x140 MX8MM_IOMUXC_ECSPI2_MISO_UART4_DCE_CTS_B 0x140 >; }; }   After applying the changes, set your toolchain and then, compile with the following commands: $ make imx_v8_defconfig $ make freescale/imx8mm-evk-uart4.dtb Finally, copy the DTB to your board, reboot it and change the DTB in the u-boot environment, boot your board and take a look to see if the UART4 is correctly enabled.    
View full article
Hello, on this post I will explain how to record separated audio channels using an 8MIC-RPI-MX8 Board. As background about how to setup the board to record and play audio using i.MX boards, I suggest you take a look on the next post: How to configure, record and play audio using an 8MIC-RPI-MX8 Board. Requirements: I.MX 8M Mini EVK. Linux Binary Demo Files - i.MX 8MMini EVK. 8MIC-RPI-MX8 Board. Serial console emulator (Tera Term, Putty, etc.). Headphones/speakers. Waveform Audio Format WAV, known for WAVE (Waveform Audio File Format), is a subset of Microsoft’s Resource Interchange File Format (RIFF) specification for storing digital audio files. This format does not apply compression to the information and stores the audio with different sampling rates and bitrates. WAV files are larger in size compared to other formats such as MP3 which uses compression to reduce the file size while maintaining a good audio quality but, there is always some lose on quality since audio information is too random to be compressed with conventional methods, the main advantage of this format is provide an audio file without losses that is also widely used on studio. This files starts with a file header with data chunks. A WAV file consists of two sub-chunks: fmt chunk: data format. data chunk: sample data. So, is structured by a metadata that is called WAV file header and the actual audio information. The header of a WAV (RIFF) file is 44 bytes long and has the following format: How to separate the channels? To separate each audio channel from the recording we need to use the next command that will record raw data of each channel. arecord -D plughw:<audio device> -c<number of chanels> -f <format> -r <sample rate> -d <duration of the recording> --separate-channels <output file name>.wav arecord -D plughw:2,0 -c8 -f s16_le -r 48000 -d 10 --separate-channels sample.wav This command will output raw data of recorded channels as is showed below. This raw data cannot be used as a “normal” .wav file because the header information is missing. It is possible to confirm it if import raw data to a DAW and play recorded samples: So, to use this information we need to create the header for each file using WAVE library on python. Here the script that I used: import wave import os name = input("Enter the name of the audio file: ") os.system("arecord -D plughw:2,0 -c8 -f s16_le -r 48000 -d 10 --separate-channels " + name + ".wav") for i in range (0,8): with open(name + ".wav." + str(i), "rb") as in_file: data = in_file.read() with wave.open(name + "_channel_" + str(i) +".wav", "wb") as out_file: out_file.setnchannels(1) out_file.setsampwidth(2) out_file.setframerate(48000) out_file.writeframesraw(data) os.system("mkdir output_files") os.system("mv " + name + "_channel_" + "* " + "output_files") os.system("rm " + name + ".wav.*") If we run the script, will generate a directory with the eight audio channels in .wav format. Now, we will be able to play each channel individually using an audio player. References IBM, Microsoft Corporation. (1991). Multimedia Programming Interface and Data Specifications 1.0. Microsoft Corporation. (1994). New Multimedia Data Types and Data Techniques. Standford University. (2024, January 30). Retrieved from WAVE PCM sound file format: http://hummer.stanford.edu/sig/doc/classes/SoundHeader/WaveFormat/
View full article
PCIE IP on i.MX8MM and i.MX8MP is same, customer can follow PCIE test Application note to do compliance test, if eye diagram failed, they can fine turn corresponding regs below: iMX8MMRM.pdf IMX8MPRM.pdf GEN1:             GEN2:                 Related code in kernel Phy-fsl-imx8-pcie.c (kernel-source\drivers\phy\freescale)    3794      2020/11/4 static int imx8_pcie_phy_init(struct phy *phy) { ……          /* Configure TX drive level  */        writel(0x2d, imx8_phy->base + 0x404);          return 0; }   Thanks Lambert
View full article
[中文翻译版] 见附件   原文链接: Enable GmSSL which supports OSCCA Algorithm Toolbox on i.MX 
View full article
If you are a Windows user and don't want to install Linux on your machine, VMware is a virtual machine used to install Linux under Windows. It's a good way to start with Linux (if you're unfamiliar with it) and also start your i.MX development. Installing VMWare - VMWare Workstation [VMWare Workstation (Click here to go to Download page)] VMWare Workstation is available in commercial and trial versions. With Workstation is possible to create your own installation image—installing a new operating system as you would install it in a new machine. - VMWare Player [VMWare Player (Click here to go to Download page)] VMWare Player is available in a free version. With Player is only possible to run images previously made. - VMWare Images at ThoughtPolice site [ThoughtPolice site (Click here to go to Download page)] This site has many ready VMWare images from many Linux distributions. It just needs to be downloaded, unziped and it's ready to be used with VMware. Workstation or Player.
View full article
This document mainly introduces how to use gpio usb id. This can provide more options to avoid pin conflicts.   iMX93 11x11 evk uses a peripheral circuit built with a typeC chip to perform USB role switch. However, in many cases, the hardware design does not have the same typeC circuit as the evk, and the USB ID is needed to do switch. The two USB IDs of the current iMX93 are muxed with the eQOS pins. The probability of this conflict is very high. So we need to use an alternative solution “gpio usb id”  to avoid this pin allocation conflict. MX93_PAD_ENET1_MDC__HSIOMIX_OTG_ID1 MX93_PAD_ENET1_MDC__ENET_QOS_MDC MX93_PAD_ENET1_TD3__HSIOMIX_OTG_ID2 MX93_PAD_ENET1_TD3__ENET_QOS_RGMII_TD3   Based on lf-6.6.52-2.2.0  
View full article
The user interface has limited the use of the tool GUI Guider. Getting an interaction only through a mouse or touchscreen can be enough for some use cases. However, sometimes the use case requires to go beyond its limitations. This video/appnote explores the possibility of integrating voice by creating a bridge between a speech recognition technology, such as VIT, and the interface creator GUI Guider. It uses a universal way to link all the voice recognition commands and a wakeword to any interaction created by GUI Guider. The following video shows the steps necessary to create that connection by creating the voice recognition using VIT voice commands and wakewords, create an interface of GUI Guider using a template, how to connect between them using the board i.MX 93 evk and testing it. For more information consult the following links AppNote HTML: https://docs.nxp.com/bundle/AN14270/page/topics/abstract.html?_gl=1*1glzg9k*_ga*NDczMzk4MDYuMTcxNjkyMDI0OA..*_ga_WM5LE0KMSH*MTcxNjkyMDI0OC4xLjEuMTcxNjkyMDcyMy4wLjAuMA AppNote PDF: https://www.nxp.com/docs/en/application-note/AN14270.pdf Associated File: AN14270SW  
View full article
P3T1755DP is a ±0.5°C accurate temperature-to-digital converter with a -40 °C to +125 °C range. It uses an on-chip band gap temperature sensor and an A-to-D conversion technique with overtemperature detection. The temperature register always stores a 12-bit two's complement data, giving a temperature resolution of 0.0625 °C P3T1755DP which can be configured for different operation conditions: continuous conversion, one-shot mode, or shutdown mode.   The device has very good features but, unfortunately, is not supported by Linux yet!   The P31755 works very similarly to LM75, pct2075, and other compatibles.   We can add support to P3T1755 in the LM75.c program due to the process to communicate with the device is the same as LM75 and equivalents.   https://github.com/nxp-imx/linux-imx/blob/lf-6.1.55-2.2.0/drivers/hwmon/lm75.c route: drivers/hwmon/lm75.c   The modifications that we have to do are the next:    1. We have to add the configurations to the kernel on the imx_v8_defconfig file CONFIG_SENSORS_ARM_SCMI=y CONFIG_SENSORS_ARM_SCPI=y CONFIG_SENSORS_FP9931=y +CONFIG_SENSORS_LM75=m +CONFIG_HWMON=y +CONFIG_I2C=y +CONFIG_REGMAP_I2C=y CONFIG_SENSORS_LM90=m CONFIG_SENSORS_PWM_FAN=m CONFIG_SENSORS_SL28CPLD=m    2. Add the part on the list of parts compatible with the driver LM75.c enum lm75_type { /* keep sorted in alphabetical order */ max6626, max31725, mcp980x, + p3t1755, pct2075, stds75, stlm75,   3. Add the configuration in the structure lm75_params device_params[]. .default_resolution = 9, .default_sample_time = MSEC_PER_SEC / 18, }, + [p3t1755] = { + .default_resolution = 12, + .default_sample_time = MSEC_PER_SEC / 10, + }, [pct2075] = { .default_resolution = 11, .default_sample_time = MSEC_PER_SEC / 10,   Notes: You can change the configuration of the device using .set_mask and .clear_mask, see more details on LM75.c lines 57 to 78   4. Add the ID to the list in the structure i2c_device_id lm75_ids and of_device_id __maybe_unused lm75_of_match    { "max31725", max31725, }, { "max31726", max31725, }, { "mcp980x", mcp980x, }, + { "p3t1755", p3t1755, }, { "pct2075", pct2075, }, { "stds75", stds75, }, { "stlm75", stlm75, },   + { + .compatible = "nxp,p3t1755", + .data = (void *)p3t1755 + },   5. In addition to all modifications, I modify the device tree of my iMX8MP-EVK to connect the Sensor in I2C3 of the board.  https://github.com/nxp-imx/linux-imx/blob/lf-6.1.55-2.2.0/arch/arm64/boot/dts/freescale/imx8mp-evk.dts   }; }; + + p3t1755: p3t1755@48 { + compatible = "nxp,p3t1755"; + reg = <0x48>; + }; + };   Connections: We will use the expansion connector of the iMX8MP-EVK and J9 of the P3T1755DP-ARD board.   P3T1755DP-ARD board   iMX8MP-EVK   P3T1755DP-ARD ----> iMX8MP-EVK J9              ---------->            J21 +3v3 (Pin 9) ---> +3v3 (Pin 1) GND(Pin 7) ---> GND (PIN 9) SCL (Pin 4) ---> SCL (Pin 5) SDA (Pin 3) ---> SDA (Pin 3)     Reading the Sensor We can read the sensor using the next commands:   Read Temperature: $ cat /sys/class/hwmon/hwmon1/temp1_input Reading maximum temperature: $ cat /sys/class/hwmon/hwmon1/temp1_max Reading hysteresis: $ cat /sys/class/hwmon/hwmon1/temp1_max_hyst   https://www.nxp.com/design/design-center/development-boards-and-designs/analog-toolbox/arduino-shields-solutions/p3t1755dp-arduino-shield-evaluation-board:P3T1755DP-ARD    
View full article
We are pleased to announce that Config Tools for i.MX v14.0 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) The product is based on Eclipse 2022-12 Open JDK 17 is updated. Batch processing on command line is supported. Support for SDK 2.14 in Project cloner and Detect toolchain project is added. Quick fix for errors allows setting the "Called by the default initialization function" flag when it would fix an error. Search functionality to Code Preview is added. TEE Export TEE registers via wizard or command line is available. Boot ROM hiding feature is supported. Tier mode for TRDC is supported. Domain ambivalence for RDC masters is added. Master-specific memory alias Validation for A28 bit of MPU region address is added. Memory map filters are aligned with Arm terminology. Status bar is united with other tools. Pins Labels defined for Expansion header pins can be set as identifiers of the routed pin. Expansion headers can be locked for editing. Expansion headers and boards are added to the HTML and CSV reports. Pins filtering is added into the expansion header pin routing dialogs. Columns from Routing Details can be added to the External User Signals view. New External User Signals can be created for all routed pins that are missing in the signals table. Clocks Support for the same frequencies settings from different source for internal clocks is added.
View full article
This demo for all(bootloader, device tree, Linux kernel, rootfs) in spi. It uses raw read(sf read)/raw write(sf write in uuu script) to achieve that. sf probe 0; sf read ${fdt_addr} 0x500000 0x100000; sf read ${loadaddr} 0x600000 0x1E00000; sf read ${initrd_addr} 0x2400000 0x600000; setenv bootargs console=${console},${baudrate} earlycon=${earlycon},${baudrate} rdinit=/linuxrc; booti ${loadaddr} ${initrd_addr} ${fdt_addr} |-- 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch --- patch for this demo |-- demo_binary | |-- flash.b0.bin --- b0 bootloader | |-- flash.bin --- c0 bootloader | |-- Image-imx8qxpc0mek.bin --- Linux kernel | |-- imx8qxp-mek.dtb --- device tree | |-- uramdisk_boot.rootfs.aarch64.img --- ram disk | |-- uuu.qspi.all.b0.uuu --- uuu script for b0 | `-- uuu.qspi.all.uuu --- uuu script for c0 `-- readme.txt --- this file # The spi layout used is: # - --------- -------------------------------------------- # | | flash.bin | env | dtb | Image |rootfs| # - --------------- -------------------------------------- # ^ ^ ^ ^ ^ ^ ^ # | | | | | | | # 0 4kiB 4MiB 5MiB 6MiB 36MiB 42MiB 0x1000 0x400000 0x500000 0x600000 0x2400000 Test: HW: i.MX8QXP MEK SW: lf-5.10.72-2.2.0 + 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch Test log: SF: Detected mt35xu512aba with page size 256 Bytes, erase size 128 KiB, total 64 MiB device 0 offset 0x500000, size 0x100000 SF: 1048576 bytes @ 0x500000 Read: OK device 0 offset 0x600000, size 0x1e00000 SF: 31457280 bytes @ 0x600000 Read: OK device 0 offset 0x2400000, size 0x600000 SF: 6291456 bytes @ 0x2400000 Read: OK [ 4.787552] imx6q-pcie 5f010000.pcie: unable to add pcie port. [ 4.797467] Freeing unused kernel memory: 2944K [ 4.807379] Run /linuxrc as init process Starting syslogd: OK Starting klogd: OK Running sysctl: OK Starting network: OK /bin/sh: can't access tty; job control turned off / #  
View full article
Customer can force PCIE to work at GEN1/GEN2 mode if PCB layout is not good. Pls refer to: linux/Documentation/devicetree/bindings/pci/fsl,imx6q-pcie.txt:40:- fsl,max-link-speed: Specify PCI gen for link capability. Must be '2' for i.MX8M: diff --git a/arch/arm64/boot/dts/freescale/fsl-imx8mq.dtsi b/arch/arm64/boot/dts/freescale/fsl-imx8mq.dtsi index f4dcf7ac3c98..262db6f93cb2 100755 --- a/arch/arm64/boot/dts/freescale/fsl-imx8mq.dtsi +++ b/arch/arm64/boot/dts/freescale/fsl-imx8mq.dtsi @@ -1314,7 +1314,7 @@                     <&clk IMX8MQ_CLK_PCIE1_AUX>,                     <&clk IMX8MQ_CLK_PCIE1_PHY>;              clock-names = "pcie", "pcie_bus", "pcie_phy"; -            fsl,max-link-speed = <2>; +            fsl,max-link-speed = <1>;              ctrl-id = <0>;              power-domains = <&pcie0_pd>;              status = "disabled"; @@ -1344,7 +1344,7 @@                     <&clk IMX8MQ_CLK_PCIE2_AUX>,                     <&clk IMX8MQ_CLK_PCIE2_PHY>;              clock-names = "pcie", "pcie_bus", "pcie_phy"; -            fsl,max-link-speed = <2>; +            fsl,max-link-speed = <1>;              ctrl-id = <1>;              power-domains = <&pcie1_pd>;              status = "disabled"; diff --git a/drivers/pci/dwc/pci-imx6.c b/drivers/pci/dwc/pci-imx6.c index 54459b52f526..a63de7e7bae0 100644 --- a/drivers/pci/dwc/pci-imx6.c +++ b/drivers/pci/dwc/pci-imx6.c @@ -1548,6 +1548,7 @@ static int imx_pcie_establish_link(struct imx_pcie *imx_pcie)       u32 tmp;       int ret;   +    dw_pcie_dbi_ro_wr_en(pci);       /*        * Force Gen1 operation when starting the link.  In case the link is        * started in Gen2 mode, there is a possibility the devices on the   i.MX8/8x: fsl-imx8dx.dtsi pcieb: pcie@0x5f010000 {               /*               * pcieb phyx1 lane1 in default, adjust it refer to the               * exact hw design.               */ . . . . .               power-domains = <&pd_pcie>;               fsl,max-link-speed = <1>;         /* 3=gen3, 1=gen1 */               hsio-cfg = <PCIEAX2PCIEBX1>;               hsio = <&hsio>;               ctrl-id = <1>; /* pcieb */               cpu-base-addr = <0x80000000>;               status = "disabled";        };   pci-imx6.c @@ -1799,6 +1799,7 @@ static int imx_pcie_establish_link(struct imx6_pcie *imx6_pcie)      u32 tmp;      int ret;   +    dw_pcie_dbi_ro_wr_en(pci);      /*       * Force Gen1 operation when starting the link.  In case the link is       * started in Gen2 mode, there is a possibility the devices on the @@ -1870,11 +1871,13 @@ static int imx_pcie_establish_link(struct imx6_pcie *imx6_pcie)             dev_info(dev, "Link: Gen2 disabled\n");      }   +    dw_pcie_dbi_ro_wr_dis(pci);      tmp = dw_pcie_readl_dbi(pci, PCIE_RC_LCSR);      dev_info(dev, "Link up, Gen%i\n", (tmp >> 16) & 0xf);      return 0;    err_reset_phy: +    dw_pcie_dbi_ro_wr_dis(pci);      dev_dbg(dev, "PHY DEBUG_R0=0x%08x DEBUG_R1=0x%08x\n",             dw_pcie_readl_dbi(pci, PCIE_PORT_DEBUG0),             dw_pcie_readl_dbi(pci, PCIE_PORT_DEBUG1));
View full article
This is a quick article focused on how to add the support of SFTP on the i.MX devices using Yocto to add that packages.   Refer to the pdf attached.
View full article
Here is the docment about arm64 kernel booting process, which is helpful for us to port kernel. It include the bootloader protocol, virtual memory layout, dtb, memory init, irq init, timer init and so on, please take the attachment for details. vmlinux ELF vmlinux.lds.S head.S __create_page_tables __cpu_setup __primary_switch init_task IRQ Vectors Start_kernel setup_arch paging_init bootmem_init psci_dt_init mm_init sched_init init_IRQ time_init rest_init You can refer the diagram show as below:  
View full article
The i.MX 8QuadXPlus Multisensory Enablement Kit (MEK) is a NXP development platform based on Cortex A-35 + Cortex-M4 cores. Built with high-level integration to support graphics, video, image processing, audio, and voice functions, the i.MX 8X processor family is ideal for safety-certifiable and efficient performance requirements. This tutorial shows how to enable the Cortex-M4 using the MCUXpresso SDK package and loading the binary from the network. NOTE: It is also possible to load the Cortex-M4 image from the SCFW using the imx-mkimage utility. But now we are going to focus on MCUXpresso. Setting up the machine   Install cmake on the host machine: $ sudo apt-get install cmake Download the armgcc toolchain and export the location as ARMGCC_DIR: $ export ARMGCC_DIR=<your_path_to_arm_gcc>/gcc-arm-none-eabi-9-2020q2/ NOTE: The ARMGCC_DIR variable needs to be exported on the terminal used for compilation. To setup the TFTP server on the host machine: Configuring your Host PC for TFTPPermalink   The first step is to install all the prerequisite packages for TFTP: $ sudo apt-get install xinetd tftpd tftp Create a TFTP folder in your desired location with root owner and the “rwx” permission for all users: $ sudo mkdir /tftpboot $ sudo chmod –R 777 /tftpboot $ sudo chown –R root /tftpboot Create a configuration file for the TFTP with the following content. (The server_args parameter must match with the folder created above) $ cat /etc/xinetd.d/tftp service tftp { protocol = udp port = 69 socket_type = dgram wait = yes user = root server = /usr/sbin/in.tftpd server_args = -s /tftpboot disable = no } Restart the xinetd service: $ sudo /etc/init.d/xinetd restart You can place any file at the TFTP folder and load it through U-Boot, you can also create symbolic links from your building directory avoiding to copy and paste your zImage and dtb files every time. Configuring your Host PC for NFSPermalink   Install all the needed packages for NFS: $ sudo apt-get install nfs-kernel-server Create a folder for placing your rootfs: $ mkdir /tftpboot/rfs Add the following line in the end of your /etc/exports file: /tftpboot/rfs *(rw,no_root_squash,no_subtree_check) Restart the NFS service: $ sudo service nfs-kernel-server restart Place your rootfs or create a symbolic link for the NFS folder.    Downloading the SDK Download the MCUXpresso following these steps: Click on “Select Development Board”; Select MEK-MIMX8QX under “Select a Device, Board, or Kit” and click on “Build MCUXpresso SDK” on the right; Select “Host OS” as Linux and “Toolchain/IDE” as GCC ARM Embedded; Add “FreeRTOS” and all the wanted Middleware and hit “Request Build”; Wait for the SDK to build and download the package. Building the image All demos and code examples available on the SDK package are located in the directory <<SDK_dir>>/boards/mekmimx8qx/. This tutorial shows how to build and flash the hello_world demo but similar procedures can be applied for any example (demo, driver, multicore, etc) on the SDK. To build the demo, enter the armgcc folder under the demo directory and make sure that the ARMGCC_DIR variable is set correctly. $ cd ~/SDK_2.3.0_MEK-MIMX8QX/boards/mekmimx8qx/demo_apps/hello_world/armgcc $ export ARMGCC_DIR=<your_path_to_arm_gcc>/gcc-arm-none-eabi-9-2020q2/ Run the build_release.sh script to build the code. $ ./build_release.sh NOTE: If needed, give the script execution permission by running chmod +x build_release.sh. This generates the M4 binary (hello_world.bin) under the release folder. Copy this image to the /tftpboot/ directory on the host PC. NOTE: This procedure shows how to build the M4 image that runs on TCM. To run the image from DDR, use the build_ddr_release.sh script to build the binary under the ddr_release folder. Flashing the image Open two serial consoles, one for /dev/ttyUSB0 for Cortex-A35 to boot Linux, and one for /dev/ttyUSB1 for Cortex-M4 to boot the SDK image. On the A35 console, with a SD Card with U-Boot, stop the booting process and enter the following commands to load the M4 binary to TCM: => dhcp => setenv serverip <ip_from_host_pc> => tftp 0x88000000 hello_world.bin => dcache flush => bootaux 0x88000000 Then the M4 core will load the image to the /dev/ttyUSB1 console.    
View full article
Software environment: L5.4.47_2.2.0 Hardware i.MX8QXPC0 EVK board In the uuu script we can see the bootloader imx-boot-imx8qxpc0mek-sd.bin-flash is necessary. The default BSP build generate in the yocto project is with the spl, some customers are confused about the how to build the imx-boot-imx8qxpc0mek-sd.bin-flash. Here I give the manually compile way and generate it in yocto. In the yocto generate it is more convenient than the manually compile way. Hope this can do help for you.
View full article