i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
The i.MX 6 D/Q/DL/S/SL Linux 3.10.17_1.0.1 patch release is now available in the Freescale git. The issue fixed is a GPU issue, for 2D GPU cores there is a potential need to manage the maximum number of outstanding return requests from the memory subsystem. The proper way to manage these for 2D cores with this configuration is to use a FLUSH. The patch does a FLUSH after every DRAW, the pipe will not overfill and the scenario which may lead to a stall will not occur. The instruction to get the patch are in the Readme on the git, under this link: http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/tree/README?h=imx-3.10.17-1.0.1_ga
記事全体を表示
Introduction to Linux In 1989, a Finnish student called Linus Torvalds started an improvement work of Minix's Kernel, an operational system like Unix wrote by Andrew Tannenbaum, calling his own Kernel as Linux, a mix of Linus and Minix. The main idea about this new Kernel is that it's free. Anyone can develop to improve the Kernel, share the software, change it specific application and distribute without any fee or restriction. All the code is open. Finally, in 1991, Linus launched the first official Linux version, later joining Richard Stallman's GNU project in 1992 with the objective to produce the complete operational system that we know today. Linux had fast success on the x86 architecture and soon it had ported for various processor architectures and became very popular on embedded devices in many different applications like automotive, industrial, telecommunications, consumer and internet appliances. The use of Linux in embedded devices has many advantages: Supports many devices, file systems, networking protocols High portability, since it has been ported for many CPU architectures Large number of ready applications Mature source code with constant actualization Large community of programmers and users over the world testing and adding new features Which Linux distribution should I install on my PC? There are many distributions of Linux available for free. Below are a list of some of them: Ubuntu (IPA: [uːˈbuːntuː] in English,[3][ùbúntú] in Zulu) is an operating system for desktops, laptops, and servers. It has consistently been rated among the most popular of the many Linux distributions. Ubuntu's goals include providing an up-to-date yet stable Linux distribution for the average user and having a strong focus on usability and ease of installation. It is a derivative of Debian, another popular distribution. Ubuntu is sponsored by Canonical Ltd, owned by South African entrepreneur Mark Shuttleworth. The name of the distribution comes from the African concept of ubuntu which may be rendered roughly as "humanity toward others", "we are people because of other people", or "I am who I am because of who we all are", though other meanings have been suggested. This Linux distribution is named as such to bring the spirit of the philosophy to the software world. Ubuntu is free software and can be shared by any number of users. Kubuntu and Xubuntu are official subprojects of the Ubuntu project, aiming to bring the KDE and Xfce desktop environments, respectively, to the Ubuntu core (by default Ubuntu uses GNOME for its desktop environment). Edubuntu is an official subproject designed for school environments, and should be equally suitable for children to use at home. Gobuntu is an official subproject that is aimed at adhering strictly to the Free Software Foundation's Four Freedoms. The newest official subproject is JeOS. Ubuntu JeOS (pronounced "Juice") is a concept for what an operating system should look like in the context of a virtual appliance. Ubuntu releases new versions every six months, and supports those releases for 18 months with daily security fixes and patches to critical bugs. LTS (Long Term Support) releases, which occur every two years, are supported for 3 years for desktops and 5 years for servers. The most recent LTS version, Ubuntu 10.04 LTS (Lucid Lynx), was released on 29 April 2010. The current non-LTS version is 10.10 (Maverick Meerkat) released on 10/10/10 (10 October 2010). Click here for official site Mandriva Linux (formerly Mandrakelinux or Mandrake Linux) is a Linux distribution created by Mandriva (formerly Mandrakesoft). It uses the RPM Package Manager. The product lifetime of Mandriva Linux releases is 18 months for base updates and 12 months for desktop updates. Click here for official site openSUSE, (pronounced /ˌoʊpɛnˈsuːzə/), is a community project, sponsored by Novell and AMD, to develop and maintain a general purpose Linux distribution. After acquiring SUSE Linux in January 2004, Novell decided to release the SUSE Linux Professional product as a 100% open source project, involving the community in the development process. The initial release was a beta version of SUSE Linux 10.0, and as of October 2007 the current stable release is openSUSE 10.3. Beyond the distribution, openSUSE provides a web portal for community involvement. The community assists in developing openSUSE collaboratively with representatives from Novell by contributing code through the open Build Service, writing documentation, designing artwork, fostering discussion on open mailing lists and in Internet Relay Chat channels, and improving the openSUSE site through its wiki interface. Novell markets openSUSE as the best, easiest distribution for all users. Like most distributions it includes both a default graphical user interface (GUI) and a command line interface option; it allows the user (during installation) to select which GUI they are comfortable with (either KDE, GNOME or XFCE), and supports thousands of software packages across the full range of open source development. Click here for official site Fedora is an RPM-based, general purpose Linux distribution, developed by the community-supported Fedora Project and sponsored by Red Hat. Fedora's mission statement is: "Fedora is about the rapid progress of Free and Open Source software." One of Fedora's main objectives is not only to contain free and open source software, but also to be on the leading edge of such technologies. Also, developers in Fedora prefer to make upstream changes instead of applying fixes specifically for Fedora – this ensures that updates are available to all Linux distributions. Click here for official site Debian (pronounced [ˈdɛbiən]) is a computer operating system (OS) composed entirely of software which is both free and open source (FOSS). Its primary form, Debian GNU/Linux, is a popular and influential Linux distribution. It is a multipurpose OS; it can be used as a desktop or server operating system. Debian is known for strict adherence to the Unix and free software philosophies. Debian is also known for its abundance of options — the current release includes over twenty-six thousand software packages for eleven computer architectures. These architectures range from the Intel/AMD 32-bit/64-bit architectures commonly found in personal computers to the ARM architecture commonly found in embedded systems and the IBM eServer zSeries mainframes. Throughout Debian's lifetime, other distributions have taken it as a basis to develop their own, including: Ubuntu, MEPIS, Dreamlinux, Damn Small Linux, Xandros, Knoppix, Linspire, sidux, Kanotix, and LinEx among others. A university's study concluded that Debian's 283 million source code lines would cost 10 billion USA Dollars to develop by proprietary means. Prominent features of Debian are its APT package management system, its strict policies regarding its packages and the quality of its releases. These practices afford easy upgrades between releases and easy automated installation and removal of packages. Debian uses an open development and testing process. It is developed by volunteers from around the world and supported by donations through SPI, a non-profit umbrella organization for various free software projects. The default install provides popular programs such as: OpenOffice, Iceweasel (a rebranding of Firefox), Evolution mail, CD/DVD writing programs, music and video players, image viewers and editors, and PDF viewers. Only the first CD/DVD is necessary for the default install; the remaining discs contain all 26,000+ extra programs and packages currently available. If a user does not wish to download the CDs/DVDs, these extras can be downloaded and installed separately using the package manager. Debian can also be configured to download and install updates automatically. Click here for official site Slackware is a Linux distribution created by Patrick Volkerding of Slackware Linux, Inc. Slackware was one of the earliest distributions, and is the oldest currently being maintained. Slackware aims for design stability and simplicity, and to be the most Unix-like GNU/Linux distribution. Click here for official site
記事全体を表示
Two IPUs are supported in i.MX6Q SoC, each IPU supports 1920x1080 resolution, and 4 kinds of interfaces on i.MX6Q PADs can be used to connect display devices: HDMI, Digital RGB24, LVDS1+LVDS2, MIPI DSI. In the documents, we will discuss how to expand VGA port with digital RGB and realize dual-display via HDMI & VGA, The solution has been validated on Android4.2.2 and Android4.4.2 BSP released by NXP. 1.  Expanding VGA port based on digital RGB24 interface with ADV7125 Schematic is in attachments. 2. Configurations of envionment variables in u-boot The following settings are for booting via NFS, users can adjust them to boot via Flash on board. setenv ipaddr 192.168.1.103 setenv serverip 192.168.1.102 setenv gateway 192.168.1.1 setenv ethaddr 00:04:9f:00:ea:d3 setenv bootargs_base 'setenv bootargs console=ttymxc0,115200' setenv bootargs_android 'setenv bootargs ${bootargs} init=/init androidboot.console=ttymxc0 androidboot.hardware=freescale' setenv bootargs_nfs 'setenv bootargs ${bootargs} ip=${ipaddr}:${serverip}:${gateway}:${netmask}::eth0 off root=/dev/nfs nfsroot=${serverip}:${nfsroot}' setenv bootargs_disp 'setenv bootargs ${bootargs} video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb1:dev=lcd,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off fbmem=32M vmalloc=400M' setenv bootcmd_net 'run bootargs_base bootargs_android bootargs_nfs bootargs_disp;tftpboot ${loadaddr} uImage;bootm' 3. Configurations in BSP file (1)IOMUX of DISP0 port (in header file)     MX6Q_PAD_DI0_DISP_CLK__IPU1_DI0_DISP_CLK,     MX6Q_PAD_DI0_PIN15__IPU1_DI0_PIN15,        /* DE */     MX6Q_PAD_DI0_PIN2__IPU1_DI0_PIN2,        /* HSync */     MX6Q_PAD_DI0_PIN3__IPU1_DI0_PIN3,        /* VSync */     MX6Q_PAD_DISP0_DAT0__IPU1_DISP0_DAT_0,     MX6Q_PAD_DISP0_DAT1__IPU1_DISP0_DAT_1,     MX6Q_PAD_DISP0_DAT2__IPU1_DISP0_DAT_2,     MX6Q_PAD_DISP0_DAT3__IPU1_DISP0_DAT_3,     MX6Q_PAD_DISP0_DAT4__IPU1_DISP0_DAT_4,     MX6Q_PAD_DISP0_DAT5__IPU1_DISP0_DAT_5,     MX6Q_PAD_DISP0_DAT6__IPU1_DISP0_DAT_6,     MX6Q_PAD_DISP0_DAT7__IPU1_DISP0_DAT_7,     MX6Q_PAD_DISP0_DAT8__IPU1_DISP0_DAT_8,     MX6Q_PAD_DISP0_DAT9__IPU1_DISP0_DAT_9,     MX6Q_PAD_DISP0_DAT10__IPU1_DISP0_DAT_10,     MX6Q_PAD_DISP0_DAT11__IPU1_DISP0_DAT_11,     MX6Q_PAD_DISP0_DAT12__IPU1_DISP0_DAT_12,     MX6Q_PAD_DISP0_DAT13__IPU1_DISP0_DAT_13,     MX6Q_PAD_DISP0_DAT14__IPU1_DISP0_DAT_14,     MX6Q_PAD_DISP0_DAT15__IPU1_DISP0_DAT_15,     MX6Q_PAD_DISP0_DAT16__IPU1_DISP0_DAT_16,     MX6Q_PAD_DISP0_DAT17__IPU1_DISP0_DAT_17,     MX6Q_PAD_DISP0_DAT18__IPU1_DISP0_DAT_18,     MX6Q_PAD_DISP0_DAT19__IPU1_DISP0_DAT_19,     MX6Q_PAD_DISP0_DAT20__IPU1_DISP0_DAT_20,     MX6Q_PAD_DISP0_DAT21__IPU1_DISP0_DAT_21,     MX6Q_PAD_DISP0_DAT22__IPU1_DISP0_DAT_22,     MX6Q_PAD_DISP0_DAT23__IPU1_DISP0_DAT_23,     MX6Q_PAD_NANDF_D4__GPIO_2_4,        /* ADV7125 Power on / off (2) Frame buffer static struct ipuv3_fb_platform_data qcorein_fb_data[] = { /*    {     .disp_dev = "ldb",     .interface_pix_fmt = IPU_PIX_FMT_RGB666,     .mode_str = "LDB-WXGA",     .default_bpp = 16,     .int_clk = false,     .late_init = false,     }, */     {     .disp_dev = "hdmi",     .interface_pix_fmt = IPU_PIX_FMT_RGB24,     .mode_str = "1920x1080M@60",     .default_bpp = 32,     .int_clk = false,     .late_init = false,     },     {     .disp_dev = "lcd",     .interface_pix_fmt = IPU_PIX_FMT_RGB24,     .mode_str = "1920x1080",     .default_bpp = 32,     .int_clk = false,     }, }; (3) Settings about IPUs /* HDMI -- IPU1_DI0 */ static struct fsl_mxc_hdmi_core_platform_data hdmi_core_data = {     .ipu_id = 1,     .disp_id = 1, }; /* RGB24 DISP0 LCD(Here is RGB24-->VGA via ADV7125 -- IPU0_DI0 */ static struct fsl_mxc_lcd_platform_data lcdif_data = {     .ipu_id = 0,     .disp_id = 0,     .default_ifmt = IPU_PIX_FMT_RGB24, }; (4) Adding LCD data in board_init() funtion static void __init mx6_qcorein_board_init(void) { .... imx6q_add_lcdif(&lcdif_data); ... } (5) Adding mxc_lcd.c driver to linux kernel When using make menuconfig to configure kernel, don't forget to add LCD driver to kernel.  Note: If users are using other version of android BSP, she can do porting according to above thinking. Weidong Sun NXP TIC team
記事全体を表示
  This document shows how to use the open source gstreamer1.0-rtsp-server package on i.MX6QDS and i.MX8x to stream video files and camera using RTP protocol.  The i.MX 6ULL and i.MX 7 doesn't have Video Processing Unit (VPU). Real time protocol (RTP) is a very common network protocol for delivering media over IP networks. On the board, you will need a GStreamer pipeline that encodes the raw video, adds the RTP payload, and sends over a network sink. A generic pipeline would look as follows: video source ! video encoder ! RTP payload ! network sink Video source: often it is a camera, but it can be a video from a file or a test pattern, for example. Video encoder: a video encoder as H.264, H.265, VP8, JPEG and others. RTP payload: an RTP payload that matches the video encoder. Network sink: a video sync that streams over the network, often via UDP. Pre-Requisites: MX6x o MX8x board with the L6.6.52 BSP installed. A host PC with either Gstreamer or VLC player installed.   Receiving h264 / h.265 Encoded RTP Video Stream on a Host Using GStreamer: GStreamer is a low-latency method for receiving RTP video. On your host machine, install Gstreamer and send the following command: $ gst-launch-1.0 -v udpsrc port=5000 caps = "application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96" ! rtph264depay ! decodebin ! videoconvert ! autovideosink sync=false   Using HOST PC: VLC Player Optionally, you can use VLC player to receive RTP video on a PC. First, in your PC, create a sdp file with the following content:  stream.sdpv=0m=video 5000 RTP/AVP 96c=IN IP4 127.0.0.1a=rtpmap:96 H264/90000 After this, with the GStreamer pipepline on the device running, open this .sdp file with VLC Player on the host PC.   Sending h.264 and h.265 Encoded RTP video stream GStreamer provides an h.264 encoding element by software named x264enc. Use this plugin if your board does not support h.264 encoding by hardware or if you want to use the same pipeline on different modules. Note that the video performance will be lower compared with the plugins with encoding accelerated by hardware. # gst-launch-1.0 videotestsrc ! videoconvert ! x264enc ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 Note: Replace <host-machine-ip> by the IP of the host machine. In all examples you can replace videotestsrc by v4l2src element to collect a stream from a camera   i.MX8X # gst-launch-1.0 videotestsrc ! videoconvert ! v4l2h264enc ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000   i.MX8M Mini Quad / 8M Plus # gst-launch-1.0 videotestsrc ! videoconvert ! vpuenc_h264 ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 i.MX6X The i.MX6QDS does not support h.265 so the h.264 can work: # gst-launch-1.0 videotestsrc ! videoconvert ! vpuenc_h264 ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 Using other video Encoders While examples of streaming video with other encoders are not provided, you may try it yourself. Use the gst-inspect tool to find available encoders and RTP payloaders on the board: # gst-inspect-1.0 | grep -e "encoder"# gst-inspect-1.0 | grep -e "rtp" -e " payloader" Then browse the results and replace the elements in the original pipelines. On the receiving end, you will have to use a corresponding payload. Inspect the payloader element to find the corresponding values. For example: # gst-inspect-1.0 rtph264pay   Install rtp in your yocto different form L6.6.52 BSP, to install gstreamer1.0-rtsp-server in any Yocto Project image, please follow the steps below: Enable meta-multimedia layer: Add the following on your build/conf/bblayers.conf: BBLAYERS += "$"${BSPDIR}/sources/meta-openembedded/meta-multimedia" Include gstreamer1.0-rtsp-server into the image: Add the following on your build/conf/local.conf: IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server" Run bitbake and mount your sdcard. Copy the binaries: Access the gstreamer1.0-rtsp-server examples folder: $ cd /build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0-rtsp-server/$version/build/examples/.libs Copy the test-uri and test-launch to the rootfs /usr/bin folder. $ sudo cp test-uri test-launch /media/USER/ROOTFS_PATH/usr/bin Be sure that the IPs are correctly set: SERVER: => ifconfig eth0 $SERVERIP CLIENT: => ifconfig eth0 $CLIENTIP Video file example SERVER: => test-uri file:///home/root/video_file.mp4 CLIENT: => gst-launch-1.0 playbin uri=rtsp://$SERVERIP:8554/test You can try to improve the framerate performance using manual pipelines in the CLIENT with the rtspsrc plugin instead of playbin. Follow an example: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test caps = 'application/x-rtp'  ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! queue max-size-buffers=0 ! imxv4l2sink sync=false   Camera example SERVER: => test-launch "( imxv4l2src device=/dev/video0 ! capsfilter caps='video/x-raw, width=1280, height=720, framerate=30/1, mapping=/test' ! vpuenc_h264 ! rtph264pay name=pay0 pt=96 )" CLIENT: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test ! decodebin ! autovideosink sync=false The rtspsrc has two properties very useful for RTSP streaming: Latency: Useful for low-latency RTSP stream playback (default 200 ms); Buffer-mode: Used to control buffer mode. The slave mode is recommended for low-latency communications. Using these properties, the example below gets 29 FPS without a sync=false property in the sink plugin. The key achievement here is the fact that there is no dropped frame: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test latency=100 buffer-mode=slave ! queue max-size-buffers=0 ! rtph264depay ! vpudec ! imxv4l2sink    
記事全体を表示
Hello, this post describes how you can add Japanese Language to the Yocto BSP. There are just a few steps to achieve. It was tested on the i.MX93-FRDM board, i.MX93-EVK and i.MX8M (Family). And Linux kernel 6.6.36.   The first step before to start your board building according to the Yocto Project User's Guide, is adding the below lines to the local.conf file: GLIBC_GENERATE_LOCALES = "en_US.UTF-8 ja_JP.UTF-8" IMAGE_LINGUAS = "en-us ja-jp" IMAGE_INSTALL:append = " \ glibc-gconv-euc-jp \ glibc-gconv-sjis \ glibc-gconv-utf-16 \ glibc-utils \ fontconfig \ ttf-bitstream-vera \ ttf-dejavu-sans \ "   Where:  glibc-gconv-*: Adds Japanese encoding conversions.   After building, flash the Image to the board and boot it. You can check if the Japanese font was installed successfully with: root@imx93frdm:~# locale -a C POSIX en_US en_US.utf8 ja_JP ja_JP.utf8   We can see it was installed successfully: ja_JP ja_JP.utf8   Then, we can change the Language at Runtime with: root@imx93frdm:~# export LANG=ja_JP.UTF-8 root@imx93frdm:~# export LC_ALL=ja_JP.UTF-8   Finally, probe with a command that supports Japanese outputs like "date": root@imx93frdm:~# date 2024年 2月 27日 火曜日 17:29:11 UTC     I hope this information can helps to you.   Best regards, Salas.
記事全体を表示
Hello everyone! In this document you'll find an example on how to build your own flash.bin for i.MX93 low power mode where only the Cortex-M33 rom is running after Power-On Reset, the following table provides the boot devices supported for LP boot: In LP boot, up to three containers (NXP and OEM containers) are expected to be handled by CM33 ROM code. • NXP container (optional): EdgeLock Enclave FW only (must-have in case NXP container present) • OEM container (mandatory), contains: — CM33 FW (must-have) — FCB Region Copy Image (optional) Requirements: Ubuntu 20.04 or later host PC i.MX93 EVK UUU Tool ARM GNU Toolchain (arm-gnu-toolchain-12.3.rel1-x86_64-aarch64-none-linux-gnu) SDK package (SDK_2_16_000_MCIMX93-EVK) Build procedure: Clone imx-mkimage, it is better to use the same SW version for each source we are working with, please refer to i.MX Linux Release Notes document, table 3. BSP and multimedia standard packages for this information. $ git clone https://github.com/nxp-imx/imx-mkimage -b lf-6.6.52-2.2.0 Decompress the GNU toolchain into a path in local disk, in this guide would be /opt $ sudo tar -xvJf arm-gnu-toolchain-12.3.rel1-x86_64-aarch64-none-linux-gnu.tar.xz -C /opt Clone and build Uboot $ git clone https://github.com/nxp-imx/uboot-imx -b lf-6.6.52-2.2.0 $ cd uboot-imx $ make -j $(nproc --all) clean $ make -j$(nproc --all) ARCH=arm CROSS_COMPILE=/opt/arm-gnu-toolchain-12.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- imx93_11x11_evk_defconfig $ make -j $(nproc --all) ARCH=arm CROSS_COMPILE=/opt/arm-gnu-toolchain-12.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- Download and extract i.MX firmware $ cd .. $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-ele-imx-1.3.0-17945fc.bin $ chmod +x firmware-ele-imx-1.3.0-17945fc.bin $ ./firmware-ele-imx-1.3.0-17945fc.bin --auto-accept Optional if using AHAB FW $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.26-d4c33ab.bin $ chmod +x firmware-imx-8.26-d4c33ab.bin $ ./firmware-imx-8.26-d4c33ab.bin --auto-accept Clone and build ATF $ git clone https://github.com/nxp-imx/imx-atf -b lf-6.6.52-2.2.0 $ cd imx-atf $ make -j $(nproc --all) PLAT=imx93 bl31 CROSS_COMPILE=/opt/arm-gnu-toolchain-12.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- Build M33 code, in this example we are using hello world from the i.MX SDK package. $ cd .. $ tar -xvzf SDK_2_16_000_MCIMX93-EVK.tar.gz $ cd SDK_2_16_000_MCIMX93-EVK/boards/mcimx93evk/demo_apps/hello_world/armgcc $ export ARMGCC_DIR=~/gcc-arm-none-eabi-10.3-2021.10 $ export PATH=$PATH:~/gcc-arm-none-eabi-10.3-2021.10 $ ./build_release.sh Copy the resulting binaries to imx-mkimage $ cp ~/imx-atf/build/imx93/release/bl31.bin ~/imx-mkimage/iMX93 $ cp ~/uboot-imx/u-boot.bin ~/imx-mkimage/iMX93 $ cp ~/uboot-imx/spl/u-boot-spl.bin ~/imx-mkimage/iMX93 $ cp release/sdk20-app.bin ~/imx-mkimage/iMX93/m33_image.bin Copy i.MX firmware to imx-mkimage $ cd .. $ cp firmware-imx-8.26-d4c33ab/firmware/ddr/synopsys/lpddr4_imem_1d_v202201.bin ~/imx-mkimage/iMX93 $ cp firmware-imx-8.26-d4c33ab/firmware/ddr/synopsys/lpddr4_dmem_1d_v202201.bin ~/imx-mkimage/iMX93 $ cp firmware-imx-8.26-d4c33ab/firmware/ddr/synopsys/lpddr4_dmem_2d_v202201.bin ~/imx-mkimage/iMX93 $ cp firmware-imx-8.26-d4c33ab/firmware/ddr/synopsys/lpddr4_imem_2d_v202201.bin ~/imx-mkimage/iMX93 $ cp firmware-ele-imx-1.3.0-17945fc/mx93a1-ahab-container.img ~/imx-mkimage/iMX93 Build the flash.bin using mkimage, we have different target memory options for lpboot $ cd imx-mkimage eMMC/SD $ make SOC=iMX9 REV=A1 flash_lpboot eMMC/SD no AHAB $ make SOC=iMX9 REV=A1 flash_lpboot_no_ahabfw Flexspi $ make SOC=iMX9 REV=A1 flash_lpboot_flexspi Flexspi no AHAB $ make SOC=iMX9 REV=A1 flash_lpboot_flexspi_no_ahabfw Flexspi XiP $ make SOC=iMX9 REV=A1 flash_lpboot_flexspi_xip Change the binary name so we can identify and it is easier when flashing $ mv flash.bin flash_m33_lpboot.bin Also, build singleboot flashbin so we can use it to run UUU and flash the lpboot binary $ make SOC=iMX9 REV=A1 flash_singleboot $ mv flash.bin flash_UUU.bin Set SW1301 for serial download on the EVK (0011), connect debug, download and power cables and turn on the EVK. Flash the resulting binary into the EVK for the respective target (SD/eMMC/FSPI) $ uuu -b sd flash_UUU.bin flash_m33_lpboot.bin $ uuu -b emmc flash_UUU.bin flash_m33_lpboot.bin $ uuu -b qspi flash_UUU.bin lash_m33_lpboot.bin Once it is done change SW1301 to the respective bootmedia SD Low power boot (1010) eMMC Low power boot (1000) FlexSPI NOR Low power boot* (1101) *Note M.2 QSPI card is required for FlexSPI Boot option, since QSPI memory is not populated into the EVK Power on the board, and the example should be running on the Cortex-M33 terminal only. Hope everyone finds this useful! For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
記事全体を表示
Test environment: i.MX93FRDM LF6.6.36. With Yocto training.
記事全体を表示
i.MX93 eMMC Secondary Boot          i.MX93 eMMC Secondary Boot.zip   i.MX8MP eMMC Secondary Boot           i.MX8MP eMMC Secondary Boot.zip i.MX8MM SDCARD Secondary Boot Demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-SDCARD-Secondary-Boot-Demo/ta-p/1500011   i.MX8QXP eMMC Secondary Boot https://community.nxp.com/t5/i-MX-Community-Articles/i-MX8QXP-eMMC-Secondary-Boot/ba-p/1257704#M45    i.MX6 SDCARD Secondary Boot Demo           i.MX6_SDCARD_Secondary_Boot_Demo.pdf      
記事全体を表示
Hello, here Jorge. On this post I will explain how to enable MQS1 on i.MX8ULP. As background about how to setup the environment to build the image using Yocto, please take a look on our i.MX Yocto Project User's Guide: Requirements: i.MX 8ULP EVK. Serial console emulator (Tera Term, Putty, etc.). USB Type-C cable. Micro USB cable. Headphones/speakers. Linux PC. Build done in Linux 6.6.23_2.0.0. i.MX8ULP audio subsystem. i.MX 8ULP extends audio capabilities on i.MX 7ULP by adding dedicated DSP cores for voice trigger and audio processing, enabling lower latency and power efficiency to support variety of audio applications. Some of hardware blocks implemented on 8ULP to support audio use cases are the next: Cadence Fusion F1 DSP processor. Cadence HiFi4 DSP processor. PowerQuad hardware accelerator with fixed and floating + FFT. Digital Microphone interface with support of up-to 8 PDM channels. Up-to 8 independent SAI instances. Up-to 2 Medium Quality Sound (MQS). Sony/Philips Digital interface (SPDIF). As is described before, MQS0 and MQS1 are part of real time domain and application domain respectively. I’m going to focus this post on how to enable MQS1 on application domain. Medium Quality Sound (MQS)  This module is basically generates a PWM from PCM audio data. For the major part of typical audio applications will require an external CODEC to deliver the audio quality but, sometimes where the application does not demand this quality, MQS can provide a medium quality audio via GPIO pin that can directly drive the audio output to a speaker or headphone via inexpensive external amplifier/buffer instead of CODEC. The design of the MQS can be described as follows: Input the PCM audio data (from SAI) into a 16-bit register. Up-sample data to match PWM switching frequency. Perform a simple 2nd order Sigma-Delta smooth on the current data versus previous data. Convert the PCM register into a 6-bit PWM width register and output through a GPIO pin.   How to enable it? By default, our BSP does not enable clock for MQS1. This clock is controlled on CGC1 (AD), specifically on MQS1CLK (Multiplexer to select the audio clock connected to the MQS clock input). So, it is needed to modify imx8ulp-clock.h and clk-imx8ulp.c. Please take a look on patch attached at the end of this post to see the modification in drivers easily. These drivers have the definition/configuration for MQS1_SEL in CGC1 and needs to be added as follows: MQS1_SEL definition needs to be added in imx8ulp-clock.h: #define IMX8ULP_CLK_MQS1_SEL 56 #define IMX8ULP_CLK_CGC1_END 57 MQS1_SEL configuration needs to be added in imx8ulp_clk_cgc1_init of clk-imx8ulp.c: clks[IMX8ULP_CLK_MQS1_SEL] = imx_clk_hw_mux2("mqs1_sel", base + 0x90c, 0, 2, sai45_sels, ARRAY_SIZE(sai45_sels)); Also, it is necessary to configure MQS1 on device tree of i.MX8ULP. Add this in soc: soc@0 of imx8ulp.dtsi: mqs1: mqs@0x29290064 { reg = <0x29290064 0x4>; compatible = "fsl,imx8qm-mqs"; assigned-clocks = <&cgc1 IMX8ULP_CLK_MQS1_SEL>; assigned-clock-parents = <&cgc1 IMX8ULP_CLK_SPLL3_PFD1_DIV1>; clocks = <&cgc1 IMX8ULP_CLK_MQS1_SEL>, <&cgc1 IMX8ULP_CLK_MQS1_SEL>; clock-names = "core", "mclk"; status = "disabled"; }; And create a new device tree, in this case is going to be named imx8ulp-evk-mqs.dts and is as follows: #include "imx8ulp-evk.dts" / { sound-simple-mqs { compatible = "simple-audio-card"; simple-audio-card,name = "imx-simple-mqs"; simple-audio-card,frame-master = <&sndcpu>; simple-audio-card,bitclock-master = <&sndcpu>; simple-audio-card,dai-link@0 { format = "left_j"; sndcpu: cpu { sound-dai = <&sai4>; }; codec { sound-dai = <&mqs1>; }; }; }; }; &cgc1 { assigned-clock-rates = <24576000>; }; &iomuxc1 { pinctrl_mqs1: mqs1grp { fsl,pins = < MX8ULP_PAD_PTF7__MQS1_LEFT 0x43 >; }; }; &mqs1 { #sound-dai-cells = <0>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_mqs1>; status = "okay"; }; &sai4 { #sound-dai-cells = <0>; assigned-clocks = <&cgc1 IMX8ULP_CLK_SAI4_SEL>; assigned-clock-parents = <&cgc1 IMX8ULP_CLK_SPLL3_PFD1_DIV1>; status = "okay"; }; Let’s apply these changes on our BSP, in my case I’m going to create a new layer in Yocto to add these modifications with a patch that can be found at the end on this post, here the steps: Install essential Yocto Project host packages: $ sudo apt install gawk wget git diffstat unzip texinfo gcc build-essential chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping python3-git python3-jinja2 python3-subunit zstd liblz4-tool file locales libacl1 Install the “repo” utility: $ mkdir ~/bin $ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo $ chmod a+x ~/bin/repo $ export PATH=~/bin:$PATH Set up Git: $ git config --global user.name "Your Name" $ git config --global user.email "Your Email" $ git config –list Download the i.MX Yocto Project Community BSP recipe layers and create build folder: $ mkdir imx-yocto-bsp $ cd imx-yocto-bsp $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.23-2.0.0.xml $ repo sync $ DISTRO=fsl-imx-wayland MACHINE=imx8ulp-lpddr4-evk source imx-setup-release.sh -b 8ulp_build Create the new layer: $ cd ~/imx-yocto-bsp/sources $ bibake-layers create-layer meta-mqs $ cd meta-mqs conf/layer.conf should be as follows: BBPATH .= ":${LAYERDIR}" BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \ ${LAYERDIR}/recipes-*/*/*.bbappend" BBFILE_COLLECTIONS += "meta-mqs" BBFILE_PATTERN_meta-mqs = "^${LAYERDIR}/" BBFILE_PRIORITY_meta-mqs = "6" LAYERSERIES_COMPAT_meta-mqs = "nanbield" Let’s change the recipe: $ sudo rm -r recipes-example $ mkdir -p recipes-kernel/linux/files 0001-8ULP-MQS-Enable.patch should be copied to ~/imx-yocto-bsp/sources/meta-mqs/recipes-kernel/linux/files Add an append (on this case is called “linux-imx_%.bbappend”)to change the recipe with next content: FILESEXTRAPATHS:prepend := "${THISDIR}/files:" SRC_URI += "file:// 0001-8ULP-MQS-Enable.patch " addtask copy_dts after do_unpack before do_prepare_recipe_sysroot do_copy_dts () { if [ -n "${DTS_FILE}" ]; then if [ -f ${DTS_FILE} ]; then echo "do_copy_dts: copying ${DTS_FILE} in ${S}/arch/arm64/boot/dts/freescale" cp ${DTS_FILE} ${S}/arch/arm64/boot/dts/freescale/ fi fi } The next step is add the layer and build the image: $ cd ~/imx-yocto-bsp/8ulp_build $ bitbake-layers add-layer ~/imx-yocto-bsp/sources/meta-mqs Confirm that the layer has been added: $ bitbake-layers show-layers Build the image: $ bitbake imx-image-multimedia i.MX8ULP EVK limitations The i.MX8ULP has the next MQS1 pins available: But, in the EVK board, the mayor part of these pins are used for other functions such as: - Push button: - MIPI DSI:  - Etc… So, take the output signal of MQS1 pins of EVK board is difficult, in this article, I’m going to configure PTF7 only (MQS1_left) for practicality. If you are working with this board and you need to use these pins for MQS function you will need to manipulate the traces and take the required signals. If you are designing a custom board, planning is essential to avoid this issue. Flash the board. One the build has been finished, we will have the necessary files to flash the board and test it. If you are not too familiarized with this process I suggest you take a look on this post. First, put the board in serial download mode changing the boot configuration switches on the board:   The next step is connecting the power cable, micro-USB cable on the debug port and USB-C type cable to USB0 connector on the board. Then, turn-on the board and run the next command in terminal of build directory: uuu -b emmc_all imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 imx-image-multimedia-imx8ulpevk.wic Now, power-off the board, change the boot mode to single boot-eMMC and power it on to test it. Test MQS1 in i.MX8ULP. To test MQS1 it is needed to change the device tree we created, we can do it with the next commands in U-boot: u-boot=> setenv fdtfile imx8ulp-evk-mqs.dtb u-boot=> saveenv u-boot=> boot Now we can test MQS1 on i.MX8ULP EVK, let's confirm that the clock is active in MQS module with the next command: $ cat /sys/kernel/debug/clk/clk_summary -n As you can see mqs1_sel is active and running at 24576000 Hz: And the card appears if we run the next command: $ aplay -l To play audio through MQS we can do it as any sound card: $ speaker-test -D sysdefault:CARD=imxsimplemqs -c 2 -f 48000 -F S16_LE -t pink -P 3 The signal should look like this in the pin output: And like this after a filter, for example the filter used in i.MX93 EVK.   With this post we have been able check the general operation of MQS, configure and compile the image with the required changes to enable MQS1 on EVK board and measure the output on the board. There is a considerable limitation on EVK board since we cannot test left and right outputs without intervene the base board, but this can be helpful as a reference to who would like to use this audio output on i.MX8ULP processor. Best regards. References. Yocto Project customization guide - NXP Community How to add a new layer and a new recipe in Yocto - NXP Community Flashing Linux BSP using UUU - NXP.  i.MX8ULP reference manual. Embedded Linux Projects Using Yocto Project Cookbook.
記事全体を表示
this is tested with MX93(A1) EVK running 6.1.55_2.2.0 pre-build image.   USB can output test patterns with either one of the setup below: 1. through device node: root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# cat role gadget root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo host > role [ 2672.864083] ci_hdrc ci_hdrc.0: EHCI Host Controller [ 2672.868996] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1 [ 2672.893320] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00 [ 2672.899314] hub 1-0:1.0: USB hub found [ 2672.909235] hub 1-0:1.0: 1 port detected root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# cat role host root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo 4 > port_test root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo 3 > port_test root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo 2 > port_test root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo 1 > port_test   2. use memtool to program registers for i in $(find /sys -name control | grep usb);do echo on > $i;echo "echo on > $i";done; echo host > /sys/kernel/debug/usb/ci_hdrc.0/role #Offset:184h USB_OTG1 base address: 4C10_0000h base address USB_OTG2 base address: 4C20_0000h Register address Register address:base address+offset $ /unit_tests/memtool 0x4c100184 1 # Force to output Test Packet for Eye Diagram Test $ /unit_tests/memtool 0x4c100184=0x18041215 #Force to output J_STATE $ /unit_tests/memtool 0x4c100184=0x18011215 #Force to output K_STATE $ /unit_tests/memtool 0x4c100184=0x18021215 #Force to output SE0 (host) / NAK (device) $ /unit_tests/memtool 0x4c100184=0x18031215
記事全体を表示
Hardware i.MX 93 EVK​ TFT LCD 480x272 RGB888 (NV3047E, parallel)​ Condition A55 off​ DDR self-refresh​ OCRAM for framebuffer, TCM for code/data​ LCDIF on with parallel interface​ M33 update panel content each second​ 255KB single frame buffer(RGB565) (fit in OCRAM: 0x20480000 ~ 0x204DFFFF)​ Code Bitbucket:ssh://[email protected]/mpucnse/imx93-cm33-usecase.git​ Branch: imx93_sdk_2.14.1-lcd_on_ocram​ Demo code: imx93-cm33-usecase/boards/mcimx93evk/demo_apps/lcd_on_ocram​ DTS: imx93-cm33-usecase/boards/mcimx93evk/demo_apps/lcd_on_ocram/dts​ Working Flow   ​Test Flow In uboot console,​ setenv mmcargs $mmcargs clk-imx93.mcore_booted​ setenv fdtfile imx93-11x11-evk-lcd_panel.dtb​ fatload mmc 1:1 0x80000000 sdk20-app.bin;cp.b 0x80000000 0x201e0000 0x10000;bootaux 0x1ffe0000 0​ boot​ In kernel console,​ echo mem > /sys/power/state​ start the power test Power Consumption SoC power: 94.4mW​ [email protected]​ CM33@100MHz​ CM33@100MHz​ A55 suspend​ DDR retention​ WAKEUPMIX off​ NICMIX and MEDIAMIX on​  ​  
記事全体を表示
Dynamic debug is designed to allow you to dynamically at runtime  enable/disable  kernel code to obtain additional kernel information. Currently, if ``CONFIG_DYNAMIC_DEBUG`` is set, then all ``pr_debug()``/``dev_dbg()`` and ``print_hex_dump_debug()``/``print_hex_dump_bytes()`` calls can be dynamically enabled per-callsite.    
記事全体を表示
This is the procedure and patch to set up Ubuntu 12.04 64bit Linux Host PC and building i.MX28 L2.6.35_1.1.0_130130.  It has been tested to build GNOME profile and with FSL Standard MM codec. A) Basic Requirement: Set up the Linux Host PC using ubuntu-12.04.3-desktop-amd64.iso Make sure the previous LTIB installation and the /opt/freescale have been removed B) Installed the needed packages to the Linux Host PC $ sudo apt-get update $ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev $ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool $ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool $ sudo apt-get install uuid-dev liblzo2-dev $ sudo apt-get install tcl dpkg $ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev $ sudo apt-get install texlive texinfo $ sudo apt-get install ia32-libs libc6-dev-i386 lib32z1 $ sudo apt-get install uboot-mkimage $ sudo apt-get install scrollkeeper $ sudo apt-get install gparted $ sudo apt-get install nfs-common nfs-kernel-server $ sudo apt-get install git-core git-doc git-email git-gui gitk $ sudo apt-get install meld atftpd C) Unpack and install the LTIB source package and assume done on the home directory: $ cd ~ $ tar -zxvf L2.6.35_1.1.0_130130_source.tar.gz $ ./L2.6.35_1.1.0_130130_source/install After that, you will find ~/ltib directory created D) Apply the patch to make L2.6.35_1.1.0 could be installed and compiled on Ubuntu 12.04 64bit OS $ cd ~/ltib $ git apply 0001_make_L2.6.35_1.1.0_130130_compile_on_ubuntu_12.04_64bit_OS.patch a) The patch modifies the following files:    dist/lfs-5.1/base_libs/base_libs.spec    dist/lfs-5.1/lkc/lkc.spec    dist/lfs-5.1/mux_server/mux_server.spec    dist/lfs-5.1/ncurses/ncurses.spec b) Add the following files to the pkgs directory:    pkgs/lkc-1.4-lib.patch    pkgs/lkc-1.4-lib.patch.md5 E) Then, it is ready to proceed the rest of the LTIB env setup process: $ cd ~/ltib $ ./ltib -m config $ ./ltib Reference: L2.6.35_1.1.0_130130_docs/doc/mx28/Setting_Up_LTIB_Host_on_Ubuntu_9_04.pdf https://community.freescale.com/docs/DOC-93394 https://community.freescale.com/message/332385#332385 https://community.freescale.com/thread/271675 https://community.freescale.com/message/360556#360556 scrollkeeper is for the gnome-desktop compilation NOTE: When compiling gstreamer, this warning was pop up.  Just ignore it seems okay.
記事全体を表示
The SNVS LDO output (VDD_SNVS_CAP) requires an external capacitor. Freescale's updated recommendation is that this should be a single 0.22 uF capacitor. Freescale is working to get documents in alignment. As of Feb 2013, some documents (such as schematics or user guides) show a single 0.22 uF capacitor, others do not.
記事全体を表示
Two year ago we have developed a 16 bit ETM adaptor to connect our PowerTrace II module with our AUTOFOCUS II preprocessor : TRACE32® Chip Support and Configurations for IMX6QUAD This adaptor is connected on the EDGE connector of the SABRE Automotive Industry board from Freescale and provide a MICTOR 38 connector compatible with 16 bit maximum ETM size. This is the maximum ETM size supported by iMX6. The maximum Trace clock frequency riched is 132 Mhz, which provide enough bandwidth to trace a full ANDROID running on Quad Core iMX6 !!! and it works perfectly. with Lauterbach tools you can debug completely Linux kernel and driver and full ANDROID support using our dalvik awareness that show you the complete call stack from low level system linux call to high level JAVA code. this adaptor is already in use on several customer from us, with perfect result. TRACE32 can now display all the code executed by the iMX6 Quad for each core, with no limitation on time recording. Linux task switch timing, profiling function, MIPS information, Detailed Tree function etc ... more detail here : TRACE32® Trace-based Profiling here below a small example of what you can see : here below the board, and schematic. in case you want the full schematic for this adaptor, please contact me, i can then provide it for free ... if you buy some Lauterbach tools 😉 Jean-Pierre Paradiso Sales Manager http://www.lauterbach.com/frames.html?tutorials.html PS : we are also developping a new ETM adapter compatible with our partner DAVE (DAVE Embedded Systems ) that develop very nice eval board on iMX6 called AXEL EVB will be available soon through the official DAVE  distributor in France : Cynetis
記事全体を表示
Hi everybody, The attached document walks you through to build a Linux image for UDOO Quad board with QT5 support by using a Yocto Project build environment. The Kernel used in this process is 3.14.52. I hope you find it useful. Best regards, Carlos
記事全体を表示
Customers are experiencing significant and unexpected performance issues in their applications running on Android 14 relative to the performance that they saw on older versions of the OS (such as A12 or A13). This is a known issue on Android Community and is note related to NXP implementation of AOSP (Android Open Source Project). The information Android 14 can recollect from any debuggable application is a lot. With the help of Perfetto you can get and incredible analysis of all processes running on Android OS or an analysis of the memory usages. All this features have a side effect on debuggable applications, where debuggable application can experiment low performance. The degradation on the performance is around 1.5x and 2.0x the time taken on a previous Android version. In order to take really measurements on the application performance it is necessary to disable those features when building the apk . Quick Workaround There are two ways of disabling debug features: Build a release variant by adding a dummy key to Android-Studio. Read the following link to get further details on how to do it. Set debuggable feature to false on build.gradle (Module :app) . Here an example: android { buildTypes { debug { applicationIdSuffix '.debug' debuggable false // The important line! } } } Rebuild the apk and installed to the target with adb install <my-apk> . The application should now have the same performances it was having with A13 or older. References: Debuggable APP lag after updating to Android14
記事全体を表示
Hello! In this time, we will look how the i.MX93 GPIOs IRQs works, also I will focus on Cortex M33 side with SDK 2_16_0 but also tested on 2_15.   We can see in this other post, how the i.MX8M family works, but for i.MX93 this is a little different because there are a Secure/Non-Secure options and Privilege/Non-Privilege.   According to reference Manual and SDK LED example, we must to set the PCNS and ICNS registers to 0x00 to set in Secure access.    Materials Used: i.MX93EVK Jumper cable to connect GPIO2_IO02 with GPIO2_IO03 SDK 2_16_0 from MCUXpresso SDK Builder Source power for i.MX93EVK USB C Cable for serial debug USB C Cable to transfer .bin ro EVK   The Cortex-M33 processor supports Secure and Non-secure security states, Thread and Handler operating modes, and can run in either Thumb or Debug operating states. In addition, the processor can limit or exclude access to some resources by executing code in privileged or unprivileged mode. Code can execute as privileged or unprivileged. Unprivileged execution limits or excludes access to some resources appropriate to the current security state. Privileged execution has access to all resources available to the security state. Handler mode is always privileged. Thread mode can be privileged or unprivileged. You can find this information in the ARM documentation.   To resume this post, we will focus just in the necessary registers to configure properly a GPIO as IRQ input.   On this example, we will take the i.MX93EVK board. The GPIO2_IO02 will be configured as an output and the GPIO2_IO03 will be configured as an input with Rising edge IRQ. On each GPIO2_IO02 Rising edge, the software will detect an IRQ.     At first, we need to configure our IOMUX: void BOARD_InitPins(void) { IOMUXC_SetPinMux(IOMUXC_PAD_GPIO_IO02__GPIO2_IO02, 0U); IOMUXC_SetPinMux(IOMUXC_PAD_GPIO_IO03__GPIO2_IO03, 0U); IOMUXC_SetPinMux(IOMUXC_PAD_UART2_RXD__LPUART2_RX, 0U); IOMUXC_SetPinMux(IOMUXC_PAD_UART2_TXD__LPUART2_TX, 0U); IOMUXC_SetPinConfig(IOMUXC_PAD_GPIO_IO02__GPIO2_IO02, IOMUXC_PAD_DSE(15U) | IOMUXC_PAD_FSEL1(2U) | IOMUXC_PAD_PD_MASK); IOMUXC_SetPinConfig(IOMUXC_PAD_GPIO_IO03__GPIO2_IO03, IOMUXC_PAD_PD_MASK); IOMUXC_SetPinConfig(IOMUXC_PAD_UART2_RXD__LPUART2_RX, IOMUXC_PAD_PD_MASK); IOMUXC_SetPinConfig(IOMUXC_PAD_UART2_TXD__LPUART2_TX, IOMUXC_PAD_DSE(15U)); }   Then, we can start to code. Using as an starting point we can use the SDK/boards/mcimx93evk/driver_examples/rgpio/led_output example. Our definitions (PIN_OUT_RGPIO and PIN_IN_RGPIO are the same GPIO2 but it is just for good practice):😞 /******************************************************************************* * Definitions ******************************************************************************/ #define PIN_OUT_RGPIO GPIO2 #define PIN_IN_RGPIO GPIO2 #define PIN_OUT_RGPIO_PIN 2U #define PIN_IN_RGPIO_PIN 3U   Then, our IRQ handler: void Reserved73_IRQHandler(void) { RGPIO_ClearPinsInterruptFlags(PIN_IN_RGPIO, kRGPIO_InterruptOutput0, 1U << PIN_IN_RGPIO_PIN); PRINTF("\r\n IRQ.........\r\n"); SDK_ISR_EXIT_BARRIER; }   Why Reserved73_IRQHandler? That is the correspondent for GPIO2, you can look this on SDK/devices/MIMX9352/gcc in the file called startup_MIMX9352_cm33.S:   Basically, the interruption will clear the IRQ flag and print a little message.   Now, here we have the complete main function, we will break down the most important points. int main(void) { /* Define the init structure for the output pin*/ rgpio_pin_config_t pin_out_config = { kRGPIO_DigitalOutput, 0, }; rgpio_pin_config_t pin_in_config = { kRGPIO_DigitalInput, 0, }; /* Board pin, clock, debug console init */ /* clang-format off */ const clock_root_config_t rgpioClkCfg = { .clockOff = false, .mux = 0, // 24Mhz Mcore root buswake clock .div = 1 }; /* clang-format on */ BOARD_InitBootPins(); BOARD_BootClockRUN(); BOARD_InitDebugConsole(); CLOCK_SetRootClock(EXAMPLE_RGPIO_CLOCK_ROOT, &rgpioClkCfg); CLOCK_EnableClock(EXAMPLE_RGPIO_CLOCK_GATE); CLOCK_EnableClock(kCLOCK_Gpio2); /* Set PCNS register value to 0x0 to prepare the RGPIO initialization */ PIN_OUT_RGPIO->PCNS = 0x0; PIN_IN_RGPIO->ICNS = 0x0; /* Print a note to terminal. */ PRINTF("\r\n RGPIO Driver example\r\n"); PRINTF("\r\n An IRQ will happen each GPIO2_IO02 Rising edge\r\n"); /* Init output PIN GPIO. */ RGPIO_PinInit(PIN_OUT_RGPIO, PIN_OUT_RGPIO_PIN, &pin_out_config); /* Init Input with IRQ Pin GPIO*/ RGPIO_SetPinInterruptConfig(PIN_IN_RGPIO, PIN_IN_RGPIO_PIN, kRGPIO_InterruptOutput0, kRGPIO_InterruptRisingEdge); EnableIRQ(GPIO2_0_IRQn); RGPIO_PinInit(PIN_IN_RGPIO, PIN_IN_RGPIO_PIN, &pin_in_config); while (1) { SDK_DelayAtLeastUs(1000000U, SystemCoreClock); RGPIO_PortToggle(PIN_OUT_RGPIO, 1u << PIN_OUT_RGPIO_PIN); } }   As we can see, we need set the GPIO2 PCNS register to 0x00:   Pin Control Nonsecure (PCNS) Configures secure or nonsecure access protection for each pin. You can write to this register only in the Secure-Privilege state if it is not locked (LOCK[PCNS] = 0).   Also the ICNS register to 0x00.   Interrupt Control Nonsecure (ICNS) Configures secure and nonsecure access protection for each interrupt, or DMA request. You can update this register only in the Secure-Privilege state if it is not locked (LOCK[ICNS] = 0).   Now, we can compile and run the example. On each GPIO2_IO02 Rising edge, the CM33 will detect an IRQ in GPIO2_IO03 (short those pads as showed in the image at first of the post).     I will attach the full .c file.   I hope this information can helps to everyone.   Best regards, --... ...-- Salas.
記事全体を表示
In some cases, such as OTA, need a complete reset/reboot of the i.MX8/i.MX8X. Current BSP default design for  i.MX8/i.MX8X is partition reset/reboot. So even using spl bootloader(flash.bin). The scfw is still running old version. Not the upgrade version as expected. Because the reset/reboot by the u-boot or Linux, Only reset/reboot the A Core partition. SCU is not reset. Need to change to the board reset, which will launch entire reset/reboot of the i.MX8/i.MX8X including SCU.
記事全体を表示