i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
GUI Guider version:  1.9.x LVGL version: v8.x.x , v9.x.x Host software requirements: Ubuntu 20.04, Ubuntu 22.04 or Debian 12 Hardware requirements: FRDM i.MX 93 Development Board i.MX 93 Evaluation Kit   Steps: 1. Export your project from the folder GUI-Guider-Projects to your Linux PC.            Screenshot 2025-03-25 073449.png 2. Build an image for iMX93 using The Yocto Project.    a. Based on iMX Yocto Porject Users Guide set directories and download the repo $ mkdir imx-bsp-6.6 $ cd imx-bsp-6.6 $: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.52-2.2.0.xml $ repo sync Use distro fsl-imx-xwayland and select machine imx93evk and use this commnad with a build folder name: $ MACHINE=imx93evk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh - b bld-imx93evk b. Use bitbake command to start the build process. Also, add the -c populate_sdk to get the toolchain. $ bitbake imx-image-full -c populate_sdk  c. Install the Yocto toolchain located on <build-folder>/tmp/deploy/sdk/.  $ sudo sh ./fsl-imx-xwayland-glibc-x86_64-imx-image-full-armv8a-imx93evk-toolchain-6.6-scarthgap.sh d. Install ninja utility on the build host $ sudo apt update $ sudo apt upgrade -y $ sudo apt install ninja-build e. Unzip the gui guider and lvgl sources $ cd meta-gui-guider/recipes-graphics/gui-guider/gui-guider/ $ unzip gui-guider.zip $ cd ../../lvgl/lvgl/ $ unzip lvgl.zip $ cd ../../gui-guider/gui-guider/ $ mv ../../lvgl/lvgl/ . $ cd ports/linux/ f. Change the interpreter on build.sh from #!/bin/sh to #!/bin/bash. $ nano build.sh -- #!/bin/sh ++ #!/bin/bash g. use the following commands to make build.sh executable $ dos2unix build.sh $ chmod +x build.sh h. Execute the build.sh $ ./build.sh i. Copy the binary to the iMX93 using a USB or SCP.    RESULTS:   Chavira_1-1742846257590.jpeg   I hope this article will be helpful
查看全文
i.MX28 GPIO pins only support the following IRQ types: IRQ_TYPE_EDGE_RISING, IRQ_TYPE_EDGE_FALLING, IRQ_TYPE_LEVEL_HIGH and IRQ_TYPE_LEVEL_LOW. IRQ_TYPE_EDGE_BOTH is not supported. It application requires interrupt on both rising and falling edges, software can set the IRQ type to level trigger and set the polarity in reverse to the current GPIO input level. Below is the example. value = gpio_get_value(pdata->id_gpio) ? 1 : 0; if (value)     set_irq_type(gpio_to_irq(pdata->id_gpio), IRQ_TYPE_LEVEL_LOW); else     set_irq_type(gpio_to_irq(pdata->id_gpio), IRQ_TYPE_LEVEL_HIGH); ... When GPIO input value is low, set the IRQ type to IRQ_TYPE_LEVEL_HIGH. When the GPIO input value is high, set the IRQ type to IRQ_TYPE_LEVEL_LOW. Do the same checking in the GPIO IRQ handler. In this way, interrupts on both edges can be captured. This document was generated from the following discussion: i.MX28: GPIO interrupt on both rising and falling edges
查看全文
Attached package includes BSP patch for AI Robot Platform Based on i.MX 8M Plus  Version 6.1.55 : Rel_imx_6.1.55-2.2.0_8mp_airobot.tar.gz
查看全文
vpuwraper can fulfill VPU decoder/encoder, if customer’s user case is simple, for example they just need to encode yuv stream to H264, or decode H264 stream to yuv, There is no need to use gstreamer or V4L2 complex framework, you can use vpuwraper. Platform: i.MX8MP + L5.4.70.2.3.0 Build Procedure: mkdir vpu cd vpu git clone https://github.com/nxp-imx/imx-vpuwrap   cd imx-vpuwrap/ git tag -l   git switch -c rel_imx_5.4.70_2.3.0   source ../../.././5.4.70.2.3.0/sdk/environment-setup-aarch64-poky-linux   make -f Makefile_8mp   Test on i.MX8MP EVK board Pls find attached test log for decode and encode If busChromaU in YUV file is null, you will failed to encode it, pls apply vpuwraper patch for L5.4.70.2.3.0.patch to fix it If YUV file is interleave format, you need to add interleave parameter : -interleave 1 ./test_enc_arm_elinux -i test.yuv -o aaa.h264 -f 2 -w 176 -h 96 -interleave 1   Thanks, Lambert
查看全文
  Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is a detailed programming aid for the registers associated with i.MX 8/8X DDR initialization.  For more details, refer to the i.MX 8/8X main DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/...  
查看全文
Environment: openjdk-8 with L5.4.24-2.1.0 and GCC-9 1. Clone meta-java with dedicated branch name: git clone git://git.yoctoproject.org/meta-java -b zeus 2. Update .bb file for compile error in meta-java: diff --git a/recipes-core/icedtea/icedtea7-native.inc b/recipes-core/icedtea/icedtea7-native.inc index 8d0dc71..153a604 100644 --- a/recipes-core/icedtea/icedtea7-native.inc +++ b/recipes-core/icedtea/icedtea7-native.inc @@ -26,7 +26,7 @@ CXXFLAGS_append = " -fno-tree-dse" CXX_append = " -std=gnu++98" # WORKAROUND: ignore errors from new compilers -CFLAGS_append = " -Wno-error=stringop-overflow -Wno-error=return-type" +CFLAGS_append = " -Wno-error=stringop-overflow -Wno-error=return-type -Wno-error=format-overflow" inherit native java autotools pkgconfig inherit openjdk-build-helper 3. Add meta-java layer into bblayers.conf: BBLAYERS += "${BSPDIR}/sources/meta-java" 4. Edit the conf/local.conf to add openjdk variables # Possible provider: cacao-initial-native and jamvm-initial-native PREFERRED_PROVIDER_virtual/java-initial-native = "cacao-initial-native" # Possible provider: cacao-native and jamvm-native PREFERRED_PROVIDER_virtual/java-native = "jamvm-native" # Optional since there is only one provider for now PREFERRED_PROVIDER_virtual/javac-native = "ecj-bootstrap-native" PREFERRED_PROVIDER_java2-runtime = " openjdk-7-jre" IMAGE_INSTALL_append = " openjdk-7-jdk " diff --git a/recipes-core/openjdk/openjdk-8-common.inc b/recipes-core/openjdk/openjdk-8-common.inc index d8b30b8..ed03d60 100644 --- a/recipes-core/openjdk/openjdk-8-common.inc +++ b/recipes-core/openjdk/openjdk-8-common.inc @@ -181,5 +181,5 @@ FLAGS_GCC9 = "-fno-lifetime-dse -fno-delete-null-pointer-checks" BUILD_CFLAGS_append = " ${@openjdk_build_helper_get_build_cflags(d)}" BUILD_CXXFLAGS_append = " ${@openjdk_build_helper_get_build_cflags(d)}" # flags for -cross -TARGET_CFLAGS_append = " ${@openjdk_build_helper_get_target_cflags(d)}" +TARGET_CFLAGS_append = " ${@openjdk_build_helper_get_target_cflags(d)} -Wno-error=format-overflow" TARGET_CXXFLAGS_append = " ${@openjdk_build_helper_get_target_cflags(d)}" diff --git a/recipes-core/openjdk/openjdk-8-native.inc b/recipes-core/openjdk/openjdk-8-native.inc index 321a43d..97ff03f 100644 5. Switch the host GCC to gcc-8 and g++-8: sudo apt-get install gcc-8 g++-8 sudo update-alternatives --install /usr/bin/gcc gcc /usr/bin/gcc-8 --slave /usr/bin/g++ g++ /usr/bin/g++-8 --slave /usr/bin/gcov gcov /usr/bin/gcov-8 --slave /usr/bin/gcov-tool gcov-tool /usr/bin/gcov-tool-8 --slave /usr/bin/gcc-ar gcc-ar /usr/bin/gcc-ar-8 --slave /usr/bin/gcc-nm gcc-nm /usr/bin/gcc-nm-8 --slave /usr/bin/gcc-ranlib gcc-ranlib /usr/bin/gcc-ranlib-8 sudo update-alternatives --config gcc  6. And change the conf/local.conf from openjdk-7 -> openjdk-8: PREFERRED_PROVIDER_java2-runtime = " openjdk-8-jre" IMAGE_INSTALL_append = " openjdk-8 " 
查看全文
FAQ Question: I receive the following error message when compiling GTK2 using LTIB" Making all in demos make[2]: Entering directory `/home/ltib/rpm/BUILD/gtk+-2.14.3/demos' no --raw --build-list \         apple_red  ./apple-red.png \                 gnome_foot ./gnome-foot.png \         > test-inline-pixbufs.h \ || (rm -f test-inline-pixbufs.h && false) /bin/sh: no: command not found make[2]: *** [test-inline-pixbufs.h] Error 1 make[2]: Leaving directory `/home/ltib/rpm/BUILD/gtk+-2.14.3/demos' make[1]: *** [all-recursive] Error 1 make[1]: Leaving directory `/home/ltib/rpm/BUILD/gtk+-2.14.3' make: *** [all] Error 2 error: Bad exit status from /home/ltib/tmp/rpm-tmp.69212 (%build) Answer: Some packages on your host are missing, install the following packages: For deb distributions: sudo apt-get install libgtk2.0-dev or For Fedora distributions: sudo yum install gtk2-devel IMPORTANT: After install the package above, be sure to remove the installed GTK package on your ltib: On your LTIB directory: rm -rf rpm/BUILD/gtk+-2.14.3/ Question: I receive the following error message when booting through NFS: "Root-NFS: Server returned error -13 while mounting /tftpboot/ltib" Answer: Probabilty you remake your rootfs and forgot to restart NFS server. To solve this issue the command: "service nfs restart" Question: I am receiving "error: cannot open Name index using db3" when installing LTIB on new Ubuntu 9.10 Answer: Edit the file "ltib" and modify line 2428 to: $cf->{rpm}           = "rpm --force-debian"; Question: I receive the error message "Cannot create lockfile. Sorry." when I try to open minicom. Answer: This error message is generated because your user doesn't have permission to create a lock file in /var/lock. Change /var/lock permission: # chmod 777 /var/lock Question: I receive the error message "cannot open /dev/ttyS0: Permission denied" when I try to open minicom. Answer: This error message is generated because your user doesn't have permission to open /dev/ttyUSB0. Change /dev/ttyUSB0 permission: # chmod 777 /dev/ttyS0 Question: Compilation of e2fsprogs package or others packages with dependencies like Qtopia using LTIB in Debian derived linux system like Ubuntu makes an error like: make[1]: Leaving directory `/home/daiane/LTIB/L2.6.24_1.2.1_SDK_042008/rpm/BUILD/e2fsprogs-1.34/tests/progs' making all in po make[1]: Entering directory `/home/daiane/LTIB/L2.6.24_1.2.1_SDK_042008/rpm/BUILD/e2fsprogs-1.34/po' : --update cs.po e2fsprogs.pot rm -f cs.gmo && : -c --statistics -o cs.gmo cs.po mv: cannot stat `t-cs.gmo': No such file or directory make[1]: *** [cs.gmo] Error 1 make[1]: Leaving directory `/home/daiane/LTIB/L2.6.24_1.2.1_SDK_042008/rpm/BUILD/e2fsprogs-1.34/po' make: *** [all-progs-recursive] Error 1 error: Bad exit status from /home/daiane/LTIB/L2.6.24_1.2.1_SDK_042008/tmp/rpm-tmp.66904 (%build) Answer: This error is caused by lack of the new version of package gettext. Install the gettext. For Ubuntu, the command line is: sudo apt-get install gettext But LTIB just recognize the existence of this package if it was installed before the LTIB installation. So, reinstall the LTIB. Question Compiling LTIB I got this error message: checking for glib-genmarshal... no configure: error: Could not find a glib-genmarshal in your PATH error: Bad exit status from /home/alan/ltib/tmp/rpm-tmp.48168 (%build) Answer: This error happen when you don't have glib2.0-dev in your system. To Ubuntu execute: sudo apt-get install libglib2.0-dev Question: How to convert an ELF binary to raw ARM binary? Answer: arm-none-linux-gnueabi-objcopy -O binary test.elf test.bin Question: How to inform to kernel to print all message on screen? Answer: echo 8 > /proc/sys/kernel/printk Question: How to disassembly an ARM binary? Answer: arm-none-linux-gnueabi-objdump -b binary -m arm -D test.bin Question: RedBoot returns invalid parameter: RedBoot> load -r -b 0x100000 zImage Using default protocol (TFTP) Can't load 'zImage': invalid parameter Answer: Verify if your tftp server is running correctly. If so, then verify if RedBoot network is configured correctly. You can use ping command to verify if communication with computer is working. Insert non-formatted text here Configure RedBoot to not use script and configure network: RedBoot> ^C RedBoot> fc Run script at boot: false Use BOOTP for network configuration: true. Update RedBoot non-volatile configuration - continue (y/n)? y ... Read from 0x07ee0000-0x07eff000 at 0xa1fe0000: . ... Erase from 0xa1fe0000-0xa2000000: . ... Program from 0x07ee0000-0x07f00000 at 0xa1fe0000: . RedBoot> Reset the board and then load the image Question: How can I test GPIO using a very simple test? Answer: You can find a very simple test here
查看全文
We will cross compile L5.4.3_1.0.0 on ubuntu18.04 LTS platform in three steps. 1. Installing Ubuntu 18.04 to vmplayer14 & Configuring Ubuntu 18.04 LTS 2. Compiling L5.4.3_1.0.0 BSP According to Steps in i.MX_Yocto_Project_User's_Guide.pdf 3. Handling tensorflow-lite compilation errors. --BEGIN No.1 Installing Ubuntu 18.04 to vmplayer14 & Configuring Ubuntu 18.04 LTS 1. Install 18.04 on vmplayer After installation is done, root user should be set at first. # sudo passwd root Then follow these steps to configuration ubuntu 18.04 for environment of compiliation --Changing sources of ubuntu 18.04 mirror If you are Chinese users, you can do the step, which can improve your system performance. # sudo cp /etc/apt/sources.list /etc/apt/sources.list.bak # sudo geit /etc/apt/source.list Comment I.MX customers outside China do not need to modify Ubuntu source list, or can modify it to local mirror site of Ubuntu 18.04, which can improve the speed of software upgrade. Delet all sources and copy following lines here, Then save it and exit Update ubuntu source deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-updates main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-updates main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-backports main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-backports main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-security main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-security main restricted universe multiverse # deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-proposed main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-proposed main restricted universe multiverse Then running these 2 commands to update sources and packages # sudo apt-get update # sudo apt-get upgrade 2. Installing packages for compiliation Packages For Compiling BSP # sudo apt-get install flex bison gperf build-essential zlib1g-dev lib32ncurses5-dev x11proto-core-dev libx11-dev lib32z1-dev libgl1-mesa-dev tofrodos python-markdown libxml2-utils xsltproc # sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 gcc-multilib g++-multilib subversion openssh-server openssh-client uuid uuid-dev zlib1g-dev liblz-dev lzop  liblzo2-2 liblzo2-dev git-core curl # sudo apt-get install u-boot-tools mtd-utils android-tools-fsutils openjdk-8-jdk device-tree-compiler aptitude libcurl4-openssl-dev nss-updatedb # sudo apt-get install chrpath texinfo gawk cpio diffstat No.2 Compiling L5.4.3_1.0.0 BSP According to Steps in i.MX_Yocto_Project_User's_Guide.pdf          The detailed BSP compilation steps are given in i.MX_Yocto_Project_User's_Guide.pdf. Here are just some tips and simple steps. For Chinese customers, the system may not respond when the repo init or repo sync command is executed after obtaining the repo script. Detailed description is below: (1)Getting repo script # mkdir ~/bin (this step may not be needed if the bin folder already exists) # curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo # chmod a+x ~/bin/repo # export PATH=~/bin:$PATH (2)Getting Yocto source # mkdir imx-yocto-bsp # cd imx-yocto-bsp # repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.3-1.0.0.xml # repo sync          After running repo init or repo sync, you may encounter a situation where there is no progress for a long time, and repo sync stops there without any prompt. This may be caused by googlesource site being inaccessible.          At this time, you can modify the googlesource URL to the URL of Tsinghua University. # gedit ./repo          Changing REPO_URL = 'https://gerrit.googlesource.com/git-repo'          To be:                    REPO_URL = 'https://mirrors.tuna.tsinghua.edu.cn/git/git-repo'          Save and exit. Then run “repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.3-1.0.0.xml”. or repo sync No.3 Handling tensorflow-lite compilation errors       If you encounter a tensorflow-lite compilation error during the compilation process, the following processing methods may be helpful to you. Cause Analysis:          Compiling tensorflow-lite requires three steps: fetching packages, configuring environment, and compiling code.          During the configuring environment, the following 8 software packages need to be downloaded. If any of the 8 files are not successfully downloaded, an error will be reported and compilation will be terminated.          ①9f48e814419e.tar.gz          ②38ebac7b059e84692f53e5938f97a9943c120d98.zip          ③release-1.8.0.tar.gz          ④389ec3f906f018661a5308458d623d01f96d7b23.tar.gz          ⑤master.zip          ⑥816a4ae622e964763ca0862d9dbd19324a1eaf45.tar.gz          ⑦1f5eae5d6a135ff6811724f6c57f911d1f46bb15.tar.gz          ⑧fft.tgz          If you encounter this problem, you can refer to the following methods to solve it. Open the file with editor: ~/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow-lite/1.13.2-r0/git/tensorflow/lite/tools/make/download_dependencies.sh URLs EIGEN_URL="https://bitbucket.org/eigen/eigen/get/9f48e814419e.tar.gz" GEMMLOWP_URL="https://github.com/google/gemmlowp/archive/38ebac7b059e84692f53e5938f97a9943c120d98.zip" GOOGLETEST_URL="https://github.com/google/googletest/archive/release-1.8.0.tar.gz" ABSL_URL="https://github.com/abseil/abseil-cpp/archive/389ec3f906f018661a5308458d623d01f96d7b23.tar.gz" NEON_2_SSE_URL="https://github.com/intel/ARM_NEON_2_x86_SSE/archive/master.zip" FARMHASH_URL="https://github.com/google/farmhash/archive/816a4ae622e964763ca0862d9dbd19324a1eaf45.tar.gz" FLATBUFFERS_URL="https://github.com/google/flatbuffers/archive/1f5eae5d6a135ff6811724f6c57f911d1f46bb15.tar.gz" FFT2D_URL="http://www.kurims.kyoto-u.ac.jp/~ooura/fft.tgz" Save and exit. [comment]     Don’t run “bitbake tensorflow-lite -c cleanall before you modify it”, otherwise files will be deleted.  Then try to compile tensorflow-lite like below: # bitbake tensorflow-lite -c compile   At the same time, we can open this directory and check if the following directories are created. If these 8 directories are successfully created, it means that links we modified are no problem.          After tensorflow-lite is successfully built, we can continue to compile full images. # bitbake imx-image-full --END NXP TIC team Weidong Sun 2020/3/30
查看全文
L5.4.3_1.0.0 release is now available on IMX_SW landing page: BSP Updates and Releases -> Linux ->Linux L5.4.3_1.0.0. Documentation -> Linux -> Linux 5.4.3_1.0.0 Documentation Files available: # Name Description 1 imx-yocto-LF_L5.4.3_1.0.0.zip i.MX L5.4.3_1.0.0 for Linux BSP Documentation. Includes Release Notes, User Guide. 2 LF_v5.4.y-1.0.0_images_MX6QPDLSOLOX.zip i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualLite, i.MX 6Solox Linux Binary Demo Files 3 LF_v5.4.y-1.0.0_images_MX6SLLEVK.zip i.MX 6SLL EVK Linux Binary Demo Files 4 LF_v5.4.y-1.0.0_images_MX6UL7D.zip i.MX 6UltraLite EVK, 7Dual SABRESD, 6ULL EVK Linux Binary Demo Files 5 LF_v5.4.y-1.0.0_images_MX7ULPEVK.zip i.MX 7ULP EVK Linux Binary Demo Files  6 LF_v5.4.y-1.0.0_images_MX8MMEVK.zip i.MX 8M Mini EVK Linux Binary Demo Files  7 LF_v5.4.y-1.0.0_images_MX8MNEVK.zip i.MX 8M Nano EVK Linux Binary Demo Files  8 LF_v5.4.y-1.0.0_images_MX8MQEVK.zip i.MX 8M Quad EVK Linux Binary Demo files 9 LF_v5.4.y-1.0.0_images_MX8QMMEK.zip i.MX 8QMax MEK Linux Binary Demo files 10 LF_v5.4.y-1.0.0_images_MX8QXPMEK.zip i.MX 8QXPlus MEK Linux Binary Demo files 11 imx-scfw-porting-kit-1.2.10.1.tar.gz System Controller Firmware (SCFW) porting kit v1.2.10.1 for L5.4.3_1.0.0   Target board: MX 8 Series MX 8QuadXPlus MEK Board MX 8QuadMax MEK Board MX 8M Quad EVK Board MX 8M Mini EVK Board MX 8M Nano EVK Board MX 7 Series MX 7Dual SABRE-SD Board MX 7ULP EVK Board MX 6 Series MX 6QuadPlus SABRE-SD and SABRE-AI Boards MX 6Quad SABRE-SD and SABRE-AI Boards MX 6DualLite SDP SABRE-SD and SABRE-AI Boards MX 6SoloX SABRE-SD MX 6UltraLite EVK Board MX 6ULL EVK Board MX 6ULZ EVK Board MX 6SLL EVK Board   What’s New/Features: Please consult the Release Notes.   Known Issues: For known issues and more details please consult the Release Notes.   More information on changes of Yocto, see: README: https://source.codeaurora.org/external/imx/imx-manifest/tree/README?h=imx-linux-zeus ChangeLog: https://source.codeaurora.org/external/imx/imx-manifest/tree/ChangeLog?h=imx-linux-zeus      
查看全文
Some customer need to test ENET IEEE1588 1pps ouput signal. This article describe all i.MX8 serials test procedure, including normal ENET port and EQOS port(i.MX8MP & i.MX8DXL support EQOS).
查看全文
ATK (Advanced Toolkit) ATK (Advanced Toolkit) is a Windows software for programming the flash memory of i.MX boards. It can be downloaded here. Using ATK This section will describe the procedure to erase the flash memory and program the bootloader. 1 - Connect a serial cable between PC and i.MX board. 2 - Some hardware configurations (switches) must be done to flash the board. Set red and cream switches as below: Switch SW5 -> 000000 Switch SW4 -> 1000000 {{Note|On SW5 and SW4, "1" means the keys selected towards the edge of the board.} 3 - Run ATK (1.6 or above) going to Start -> Programs -> AdvancedToolKit -> AdvancedToolKit Set the options: i.MX CPU -> i.MX35_TO2 Device memory -> DDR2; Custom Initial File -> (keep it unmarked) Communication Channel -> Serial Port (Usually COM1) If you are using TO1, Device Memory -> MDDR 4 - Click on Flash Tools to erase, program or dump the the flash memory and click GO NAND Flash Erasing 1- Configure the Dip Switch of Personality Board: Switch 1 2 3 4 5 6 7 8 SW1 OFF OFF OFF OFF N/A N/A N/A N/A SW2 ON OFF OFF ON ON OFF OFF OFF 2- Choose NAND model K9LAG08U8M 3- Continue the steps Remember to select the checkbutton BBT (Back Block Table)
查看全文
The system controller timer service is responsible for: Watchdog - The watchdog resource is managed by the SCU. The SCFW exposes a "virtual" watchdog to all CPUs. This virtual watchdog is managed by software and it is based on a low power timer, the SCU also features a physical watchdog timer that is used to ensure the correct operation of the device. Some of the features implemented by this watchdog service are: - Update of the watchdog timeout - Start/stop of the watchdog - Refresh of the watchdog - Return of the watchdog status such as maximum watchdog timeout that can be set, watchdog timeout interval, and watchdog timeout interval remaining. Since this is usually handled by the OS itself no examples are provided in this guide. Real Time Clock (RTC) - The SCFW is responsible for providing access to the RTC. The features supported by the API are: - Set/get time - Setting alarms Only the partition that owns the SC_R_SYSTEM resource is allowed to set the time, alarms and calibration values for the RTC. All other partitions are able to read the RTC time.  Here is an example on setting the RTC from the M4 side: struct time_date{ uint16_t year; uint8_t month; uint8_t day; uint8_t hour; uint8_t min; uint8_t sec; } rtc_time; sc_err_t sc_status; sc_ipc_t ipc; /* Open IPC channel */ sc_status = sc_ipc_open(&ipc, SC_IPC_AP_CH0); if(sc_status != SC_ERR_NONE) printf("Error opening Inter Processor Channel\n"); /* Initialize RTC */ /* Hard code RTC time to January 5th 2018 at 12:00 hours */ sc_status = sc_timer_set_rtc_time(ipcHandle, 2018, 1, 5, 12, 0, 0); if(sc_status != SC_ERR_NONE) printf("Error initializing RTC. \r\n"); /* Return time */ sc_status = sc_timer_get_rtc_time(ipcHandle, &(rtc_time.year), &(rtc_time.month), &(rtc_time.day), &(rtc_time.hour), &(rtc_time.min), &(rtc_time.sec)); printf("Year: %d, Month: %d, Day: %d, Hour: %d, Minutes: %d, Seconds: %d. \r\n", rtc_time.year, rtc_time.month, rtc_time.day, rtc_time.hour, rtc_time.min, rtc_time.sec);‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ https://community.nxp.com/docs/DOC-342654 
查看全文
Question: How do I add the opencore amrnb plugin to be the default for amrnb for use with playbin2? With a .3gp file to play and audio amrnb encoded, amr plugins do not work ( i.e. are not even part of the build and when configured to build, they do not even build ). Opencore had been added and got it to build and install with our ltib BSP and it plays the audio from the .3gp file in question fine ( but with an explicit pipeline ). But, the opencore amrnb plugin is not selected by gstreamer playbin2 when it does a typefind on the amrnb audio type. Answer: There are three options: 1. Fix the aiurdemux to allow correct demuxing 2. Lower the aiurdemux rank 3. Remove the /usr/lib/gstreamer-0.10/libmfw_gst_aiur_demux.so Obviously, 3 is a ugly hack but it can be just enough for customer. If option 1 or is selected, patches may be required from MM team. On this system, the aiurdemux does not have any issue, and audio playback works as expected. These are the VPU firmware and GST-FSL versions on YOCTO: VPU Version: firmware 1.4.50; libvpu: 5.3.2 MFW_GST_VPU_DECODER_PLUGIN 3.0.8 build on Sep 30 2013 16:36:27. where in LTIB: VPU Version: firmware 1.4.48; libvpu: 5.3.2 MFW_GST_VPU_DECODER_PLUGIN 2.0.3 build on Jul 23 2013 11:20:21. So the next moved would be to try upgrading versions on LTIB if they want to use this system; in case switching to Yocto is viable, then the upgrade is already done.
查看全文
This article is rather short that only mentions the script that is needed to make an iMX93EVK act as a USB mass storage device so that whenever you connect your iMX device to a windows/linux system via USB, it should get enumerated something like a usb drive.  The storage that is used in this example is mmc so the expectation is that you have inserted a mmc card in the slot. Below is the script:- #!/bin/sh   # This composite gadget include function: # - MASS STORAGE     # # Exit status is 0 for PASS, nonzero for FAIL # STATUS=0   # Check if there is udc available, if not, return fail UDC_DIR=/sys/class/udc if test "$(ls -A "$UDC_DIR")"; then echo "The available udc:" for entry in "$UDC_DIR"/* do echo "$entry" done else STATUS=1 echo "No udc available!" exit $STATUS; fi   id=1; udc_name=ci_hdrc.0 #back_file=/dev/mmcblk1 back_file=/tmp/lun0.img   mkdir /sys/kernel/config/usb_gadget/g$id cd /sys/kernel/config/usb_gadget/g$id   # Use NXP VID, i.MX8QXP PID echo 0x1fc9 > idVendor echo 0x12cf > idProduct   mkdir strings/0x409 echo 123456ABCDEF > strings/0x409/serialnumber echo NXP > strings/0x409/manufacturer echo "NXP iMX USB Composite Gadget" > strings/0x409/product   mkdir configs/c.1 mkdir configs/c.1/strings/0x409   echo 5 > configs/c.1/MaxPower echo 0xc0 > configs/c.1/bmAttributes   mkdir functions/mass_storage.1 echo $back_file > functions/mass_storage.1/lun.0/file ln -s functions/mass_storage.1 configs/c.1/   echo $udc_name > UDC First execute the script. After that insert the g_mass_storage module in the kernel by executing :- modprobe g_mass_storage file=/dev/mmcblk1 removable=1 In the dmesg output, you will see something like below:-   gauravsharma7_0-1714041731840.png After that you can connect a C type USB cable to the USB1 port of imx93evk and the other end to any USB ports of a laptop. The moment it is connected, you would be able to see a USB drive similar to what you get when we connect a pen-drive. 
查看全文
In some cases, such as mass production or preparing a demo. We need u-boot environment stored in demo sdcard mirror image.  Here is a way: HW:  i.MX8MP evk SW:  LF_v5.15.52-2.1.0_images_IMX8MPEVK.zip The idea is to use fw_setenv to set the sdcard mirror as the operation on a real emmc/sdcard. Add test=ABCD in u-boot-initial-env for test purpose. And use fw_printenv to check and use hexdump to double confirm it. The uboot env is already written into sdcard mirror(imx-image-multimedia-imx8mpevk.wic). All those operations are on the host x86/x64 PC. ./fw_setenv -c fw_env.config -f u-boot-initial-env Environment WRONG, copy 0 Cannot read environment, using default ./fw_printenv -c fw_env.config Environment OK, copy 0 jh_root_dtb=imx8mp-evk-root.dtb loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${bsp_script}; mmc_boot=if mmc dev ${devnum}; then devtype=mmc; run scan_dev_for_boot_part; fi arch=arm baudrate=115200 ...... ...... ...... splashimage=0x50000000 test=ABCD usb_boot=usb start; if usb dev ${devnum}; then devtype=usb; run scan_dev_for_boot_part; fi vendor=freescale hexdump -s 0x400000 -n 2000 -C imx-image-multimedia-imx8mpevk.wic 00400000 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................| hexdump -s 0x400000 -n 10000 -C imx-image-multimedia-imx8mpevk.wic 00400000 5f a4 9b 97 20 6a 68 5f 72 6f 6f 74 5f 64 74 62 |_... jh_root_dtb| 00400010 3d 69 6d 78 38 6d 70 2d 65 76 6b 2d 72 6f 6f 74 |=imx8mp-evk-root| 00400020 2e 64 74 62 00 20 6c 6f 61 64 62 6f 6f 74 73 63 |.dtb. loadbootsc| 00400030 72 69 70 74 3d 66 61 74 6c 6f 61 64 20 6d 6d 63 |ript=fatload mmc| 00400040 20 24 7b 6d 6d 63 64 65 76 7d 3a 24 7b 6d 6d 63 | ${mmcdev}:${mmc| 00400050 70 61 72 74 7d 20 24 7b 6c 6f 61 64 61 64 64 72 |part} ${loadaddr| 00400060 7d 20 24 7b 62 73 70 5f 73 63 72 69 70 74 7d 3b |} ${bsp_script};| 00400070 00 20 6d 6d 63 5f 62 6f 6f 74 3d 69 66 20 6d 6d |. mmc_boot=if mm| ...... ...... ...... 00401390 76 3d 31 00 73 6f 63 3d 69 6d 78 38 6d 00 73 70 |v=1.soc=imx8m.sp| 004013a0 6c 61 73 68 69 6d 61 67 65 3d 30 78 35 30 30 30 |lashimage=0x5000| 004013b0 30 30 30 30 00 74 65 73 74 3d 41 42 43 44 00 75 |0000.test=ABCD.u| 004013c0 73 62 5f 62 6f 6f 74 3d 75 73 62 20 73 74 61 72 |sb_boot=usb star| 004013d0 74 3b 20 69 66 20 75 73 62 20 64 65 76 20 24 7b |t; if usb dev ${| 004013e0 64 65 76 6e 75 6d 7d 3b 20 74 68 65 6e 20 64 65 |devnum}; then de| flash the sdcard mirror into i.MX8MP evk board emmc to check uuu -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-image-multimedia-imx8mpevk.wic  The first time boot, the enviroment is already there. Untitled.png  How to achieve that: a. fw_setenv/fw_printenv: https://github.com/sbabic/libubootenv.git Note: Please do not use uboot fw_setenv/fw_printenv Compile it on the host x86/x64 PC. It is used on host. b. u-boot-initial-env Under uboot, make u-boot-initial-env Note: Yocto deploys u-boot-initial-env by default c. fw_env.config  imx-image-multimedia-imx8mpevk.wic 0x400000 0x4000 0x400000 0x4000 are from uboot-imx\configs\imx8mp_evk_defconfig CONFIG_ENV_SIZE=0x4000 CONFIG_ENV_OFFSET=0x400000 Now, you can run  ./fw_setenv -c fw_env.config -f u-boot-initial-env
查看全文
  Introduction   Platform: i.MX93 EVK Uboot: origin/lf_v2022.04(lf-6.1.1-1.0.0) The LVDS design and media block control in i.MX93 is very similiar with i.MX8MPlus.This article implements the LVDS driver in uboot. You need apply 0001-Add-fake-adp5585-pwm-driver.patch which implements the adp5585 pwm driver in uboot. This is a fake pwm driver only implement the pwm driver framework. You can't use pwm value to adjust brightness for the moment, but this is enough to enable the backlight. Then please apply 0002-Add-imx93-lvds-and-panel-driver.patch, you will see nxp logo with this panel: https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/dy1212w-4856:DY1212W-4856   Porting suggestions   1. Modify panel timing in drivers/video/simple_panel.c /* define your panel timing here and * copy it in simple_panel_get_display_timing */ static const struct display_timing boe_ev121wxm_n10_1850_timing = { .pixelclock.typ = 71143000, .hactive.typ = 1280, .hfront_porch.typ = 32, .hback_porch.typ = 80, .hsync_len.typ = 48, .vactive.typ = 800, .vfront_porch.typ = 6, .vback_porch.typ = 14, .vsync_len.typ = 3, }; static int simple_panel_get_display_timing(struct udevice *dev, struct display_timing *timings) { memcpy(timings, &boe_ev121wxm_n10_1850_timing, sizeof(*timings)); return 0; }   2.Modify VIDEO_PLL The VIDEO_PLL = pixel clock * 7. For default panel, the pixel clock is 71.143MHz and VIDEO_PLL  is 498MHz. static struct imx_fracpll_rate_table imx9_fracpll_tbl[] = { FRAC_PLL_RATE(1000000000U, 1, 166, 4, 2, 3), /* 1000Mhz */ FRAC_PLL_RATE(933000000U, 1, 155, 4, 1, 2), /* 933Mhz */ FRAC_PLL_RATE(700000000U, 1, 145, 5, 5, 6), /* 700Mhz */ FRAC_PLL_RATE(498000000U, 1, 166, 8, 0, 1),/* rate, rdiv, mfi, odiv, mfn, mfd */ FRAC_PLL_RATE(484000000U, 1, 121, 6, 0, 1), FRAC_PLL_RATE(445333333U, 1, 167, 9, 0, 1), FRAC_PLL_RATE(466000000U, 1, 155, 8, 1, 3), /* 466Mhz */ FRAC_PLL_RATE(400000000U, 1, 200, 12, 0, 1), /* 400Mhz */ FRAC_PLL_RATE(300000000U, 1, 150, 12, 0, 1), }; 3. Modify lcdif node in dts <498000000>, <71142857>, <400000000>, <133333333>; <VIDEO PLL>,<PIX CLK>, <MEDIA_AXI>,<MEDIA_APB> &lcdif { status = "okay"; - assigned-clock-rates = <484000000>, <121000000>, <400000000>, <133333333>; + assigned-clock-rates = <498000000>, <71142857>, <400000000>, <133333333>; };  
查看全文
The miscellaneous service is in charge of providing access to all features not handled by the other services some examples include the following features: Subsystems controls - Some subsystems have settings that can be configured through the SCFW. For instance it is possible to set thresholds for a temperature alarm and get the temperature value of the sensor in different resources. For a complete list of resources and its controls please refer to the sc_fw_api document Chapter 5 Control List. DMA configurations - The SCFW provides access to DMA grouping and priority functions. Security functions - The SCFW provides some security functions such as: Image loading and authentication Fuse writing Life cycle management. Debug features - The SCFW provides some debug functionality through its miscellaneous service, some examples include:  Output a character through the SCU UART port Obtain SCFW build information (SCFW version) Obtain device Unique ID For a complete list of functions supported by your device please refer to the (SVC) Miscellaneous Service chapter of the sc_fw_api document.  This guide will cover the most common functions,  Getting and setting a control The process to get and set a control on a resource is the same for all available controls. Refer to the Control list chapter of your SoC SCFW API document for a complete list of the available controls. The following example will be based on an i.MX8QM.  The control list looks as follows: The table lists the controls available per resource as well as the width of the data to get/set, the 'Set' column describes whether a control is 'settable' or not, for instance the temperature sensor on the A53 resource can only be read/retrieved it cannot be 'written' (set) therefore the 'Y' (yes) in this column is missing, a brief description of the control is also provided. To get a control sc_misc_get_control must be called: uint32_t val; sc_misc_get_control(ipc, SC_R_A53, SC_C_TEMP, &val)‍;‍‍‍‍‍‍ By default all calls to get_control need a pointer to a 32 bit unsigned integer, the width field on the control list table defines the span of meaningful data. In the example above the data from the temperature sensor in the A53 resource is retrieved. This call returns SC_ERR_NONE whenever it succeeds. If the parameters are invalid it returns SC_PARM and if the caller does not have access to that resource it returns SC_ERR_NOACCESS. To set a control sc_misc_set_control must be called: uint32_t val = high_alarm_temperature_value; sc_misc_set_control(ipc, SC_R_A53, SC_C_TEMP_HI, val);‍‍‍‍‍‍‍‍ As in the get example sc_misc_set_control expects a 32 bit unsigned integer, it is the responsibility of the user to pass a value within the width limits defined in the control list table. In the example above the upper threshold for the A53 resource is being set/configured. The return values are the same as in sc_misc_get_control. Other functions There is a different method for getting/setting temperatures in a friendly human readable format, the method above uses a 'raw' format to interact with the temperature sensors in the resources, an easier way is to use the sc_misc_get_temp and sc_misc_set_temp functions. This functions return the temperature value in degrees Celsius as well as it's fractional part. To define whether to get/set the value for the temperature sensor itself or one of it's alarm the sc_misc_temp_t has been defined. SC_MISC_TEMP      -> Temperature sensor SC_MISC_TEMP_HIGH -> Upper threshold temperature sensor alarm SC_MISC_TEMP_LOW  -> Lower threshold temperature sensor alarm‍‍‍‍‍‍‍‍‍ For instance to get the temperature reading from the A53 resource the following call can be made: int16_t celsius; int8_t tenths; sc_misc_get_temp(ipc, SC_R_A53, SC_MISC_TEMP, &celsius, &tenths);‍‍‍‍‍‍‍‍‍ And to set the upper threshold alarm: int16_t celsius = 80; int8_t tenths = 0; /* Set High temperature alarm to 80 degrees Celsius */ sc_misc_set_temp(ipc, SC_R_A53, SC_MISC_TEMP_HIGH, celsius, tenths);‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Unique ID of the chip as well as the build info of the SCFW can also be obtained through the miscellaneous service, the following example queries for this information: /* Getting SCFW version information */ uint32_t build_version; uint32_t commit_hash; sc_misc_build_info(ipc, &build_version, &commit_hash);‍‍‍ /* Getting Device Unique ID */ uint32_t ID_L; uint32_t ID_H; /* The ID is a 64-bit number ID_L stores the lower 32-bit portion and ID_H the 32-bit upper portion */ sc_misc_unique_id(ipc, &ID_L, &ID_H);‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Refer to the sc_fw_api document for a definition of the remaining miscellaneous functions. https://community.nxp.com/docs/DOC-342654 
查看全文
As we haven't provided a guide with steps that implement the Linux OS encryption and signature for i.MX9x products so far. So, the document provides the steps for that. For details related to how to encrypt and sign a bootloader image, please have a reference to This Guide 
查看全文