i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Question: Clarify if the delay units, mentioned in  i.MX6 RM in two places are the same : 1. There are delay units for data strobes, that are considered in calibration procedures. 2. There are delay units for clocks SDCLK, mentioned in section 44.12.54 “MMDC PHY CK Control Register (MMDCx_MPSDCTRL)” of the RM. General delay units description states : “ The delay issued by the delay-line (according to the configured value) is absolute and takes into account the operating and temperature conditions. The delay-line has a resolution that may vary from device to device; an increment of 1 delay unit may vary between 20 pSec to 50 pSec.” It may be guessed that the same relates to SDCLK delays, but preliminary i.MX6 specs mention that bit fields SDCLKx_DEL (x=0,1) control SDCLK delay, that can be up to 1 cycle.  This means SDCLKx_DEL step is 1/4  of the SDCLK. Please clarify SDCLK delays (SDCLKx_DEL) in more details. Answer: "The delay elements in the SDCLK path are similar to those in the data strobes but they are not exactly the same. The delay is on the order of picoseconds, though, not a full SDCLK cycle as might have been interpreted from the older document."
View full article
I have imx53 quick sort board i downloaded u-boot-mx53.bin and uImage to loade that into the board and dowloaded rootfs.ext2.gz in the L2.6.35_11.09.01_ERimages and i did partitions on 1GB memory card and loaded that u-boot-mx53.bin,uImage images on to the 500mb of NTFS filesystem and loaded and rootfs.ext2.gz on to the othe 500mb of ext4 file system the i inserted memorycard in to the board but u-boot logs are not comming what will be the solution
View full article
1. User Case: Demo Architecture: Demo Description: A, B, C and Speaker all are i.MX6DQ SabreSD board and running Ubuntu system. A is media server which send out broadcast 30Mbps h264 video and audio stream and running iperf to send out tcp packets via best efforts lane to PC. B and C are clients to get video data only and play in screen.  Speaker is a client to receive audio data only and play to speaker. PC which install ubuntu system is used to received best efforts data from A. Demo Goal: Use Gstreamer playback 30Mbps streaming  "H264_AVC_1080p_30fps_27Mbps_mp3.avi", while running iperf TCP streaming under the following two case: 1. Running the non-CBS kernel 2. Enable the FIQ kernel Validate the Qav (Queue and Forwarding Protocol) which is developed by SW. 2. Resource: FIQ Patch: 0001-GIC-FIQ-EPIT-implement.patch 0002-set-EPIT-priority-to-highest.patch 0003-GIC-support-SMP-4-cores-of-FIQ.patch CBS &Shaper Patch: 0004-Implement-credit-base-shaper-alogrithim-to-schdule-A.patch 0005-enet-avb-CBS-SIRQ-rum-mode-pass-performance-stress-t.patch Others Patch: 0006-Fix-the-61883-sub-type-protocol-check.patch 0007-Add-hrtimer-for-the-sirq.-Talker-transmit-packets-nu.patch 0008-1.-Fix-memory-map-size-issue.patch 0009-Increase-BD-entries-to-reduce-the-full-times.patch 0010-Add-sys-interface-to-log-out-the-video-packet-number.patch 0011-Add-AVB-timestamp-support.patch 0012-GIC-support-SMP-4-cores-of-FIQ.patch Gstreamer UDPAVB Plug-in Library and Source: Library: udp/output/libgstudp.so Source: udp/* 3. Setup the Patch:       - Low level:  kernel enet driver implement CBS and traffic shaper:              1. Apply all the patches in the patch_whole.tar.gz in the attachment               2. Rebuild kernel 3.0.35: Enable "CONFIG_ENET_IMX6_AVB" to support AVB.                        Enable "CONFIG_RUN_IN_FIQ"  in kernel:            let CBS run in FIQ mode.                3. make uImage.                You can also use the uImage-avb-fig in the attachment directly.  Flash to the SD card use dd command, the user gudie refer to the  i.MX_6Dual6Quad SABRE_SD_Linux_User_Guide.pdf.                Note: the uImage_org_nonavb in the attachment is the kernel image without QAV and FIQ. - High level: use Gstreamer as the media input/output interface, encapsulation with IEEE1722 format:         Before the below action, you should already have seutp the Ubuntu Rootfs,  copied all the Freescale *.deb files that come alone with the Release BSP demo image package and copied all the MM codec *.deb files (IMX_MMCODEC_3.0.7.tar) that from Freescale offical website, the user gudie refer to the  i.MX_6Dual6Quad SABRE_SD_Linux_User_Guide.pdf. 1. Add gstreamer setup version as following: - gstreamer core version: 0.10.35 - gst-plugins-good version: 0.10.30 - gst-plugins-bad version: 0.10.11 2. Setup: - tar xvzf udp.tar.gz - cd gst-plugins-good-0.10.30 - ./configure - make - make install - cp ~/udp/* gst/udp/ - cd gst/udp - make - cp  libgstudp.so /usr/lib/gstreamer-0.10/ - gst-inspect | grep avb         //Check whether the avb plugin is installed successfully. If the three avb plugin is printed out in the terminal, the avb plugins are proved to install properly. 4. Run the Demo:       1.  Start the iperf server in PC linux machine by inputting " iperf -s -i 1&".              2.  Power on the A board, ensure the board can get the DHCP IP address, Start the iperf client on the demo board which sends outgoing Audio-Video streaming in the background. Input "iperf -c <iperf server ip> - t 6000&". If the connection is  successful, the iperf log should be able to be seen in the linux machine terminal.              3.  Power on the B and C board, inputting the following command to receive video data:            Run "./startRxVideoAVB.sh"  to start gstreamer video receive process on video display board       4.  Power on the speaker board, inputting the following command to receive audio data:             Run "./startRxAudioAVB.sh" to start gstream audio receive process on audio  playback board 5.  Inputting the following command to send video/audio data to client at the A board terminal windowns:                              Run "./startTxAVB.sh" to start the 1722 streaming traffic                                      (note: H264_AVC_1080p_30fps_27Mbps_mp3.avi located at current directory)               6.  Change to the kernel with QAV and follow the steps 1~5 above 5. Result: Without FIQ Qav,  video play at client B and C serious freeze. It takes 3 minutes to play 1min 40s h264 stream.  iperf speed over 80Mbps. With FIQ Qav, video play at client B and  C is smooth and same as without iperf in background. Iperf show speed is less than 70Mbps.  FIQ Qav correctly reserve necessary bandwidth to AV stream 6. Know issues Failed to request the IP from DHCP         [Solution]  For FIQ, after kernel up, you must run the command: echo 1 > /sys/devices/platform/imx_wfi_issue.0/enable   2.   Kernel is halted or crashed [Solution] In bootloader parameter, add 'nosmp' in bootargs_mmc.
View full article
In traditional file system, the WinCE image is a signal file “NK.NB0”/”NK.BIN”. And when using NAND flash for storage, since it can’t support XIP, the total “NK.NB0” need be copied into RAM before running. The EBOOT will do this copy. In this way, there are two main shortages: Long boot time and big size RAM requirement. If the WinCE image is big (Included more features), these issues will be critical. The BINFS can fix those two issues fine. It gave the chance to use 32MB RAM run 64MB WinCE image, this can cost down the final products. In BINFS file system, the final WinCE image will be divided into multi-BIN files, and only the XIPKERNEL BIN (Less than 7 MB) need be copied into RAM by EBOOT. The files in other BIN will work with demand paging mode. These files will be loaded into RAM only when they need run.
View full article
Current the SSI is set to I2S slave mode in FSL default release BSP. attached the code for how to set it to master mode.
View full article
I've recently done some digging into fstrim feature on sabresd-6q. Here list it below detailed: Background:      When Nexus 7 first came out, many users felt it was speedy and high-performance. But after months of installing applications and using the tablet, things began slowing down.This was a friction point that many hoped would be fixed in the new Nexus 7 (2013) model, which it was. There’s even more to the story though, it turns out Google has fixed that storage I/O aging problem on all Nexus devices with the Android 4.3 update which comes with a little-hyped feature that could be huge for performance in the future – TRIM support via fstrim. Why slowing down?      Remember that deleting a file in software isn't actually communicated to solid state storage (whether SSD or eMMC). The space is freed up from the user's perspective, but the eMMC controller in this case still treats the pages in NAND as having valid data. Let's say you copy a 3GB movie to your internal storage, watch the movie and later delete it. You'd have 3GB free to re-use, but until you re-write those blocks the eMMC controller would treat all 3GB as valid data. There's a data structure used by the eMMC controller that tracks mapping logical locations to physical locations in NAND. I won't go into great detail here but the more complex that mapping becomes, and the more locations that have to be tracked, the slower internal NAND management works. Why SSD has such issue? Root cause is "Flash memory is divided into blocks, which is further divided in pages. The minimum write unit is a page, but the smallest erase unit is a block" which will cause fragments as time goes. Why fstrim?      Fstrim is one mechanism of linux filesystem which derives from TRIM. TRIM is already introduced since linux2.6.33. It is the name of a command that the operating system can send to tell the SSD which blocks are free in the filesystem.The SSD uses this information to internally defragment the blocks and keep free pages available to be written quickly and efficiently. How framework triggers fstrim in android4.3?      Android4.3 introduces a new service IdleMaintenanceService to manage when and how trigger fstrim in right time. Once system satisfies the following conditions, it will send out one "ACTION_IDLE_MAINTENANCE_START" intent which the MountService listens for. Last time  "ACTION_IDLE_MAINTENANCE_START" intent has been sent before 24 hours. The device is either off-charger with 80% battery or on-charger with 30% battery The device can go idle state. User don't use it for 71 minutes. Test fstrim on Imx.6      In order to wait little time to trigger fstrim, I tried to change the following variables not to wait 71 minutes and 24 hours. After changing, it will trigger one time fstrim two minutes after system goes into idle state every 30 minutes. --- a/services/java/com/android/server/IdleMaintenanceService.java +++ b/services/java/com/android/server/IdleMaintenanceService.java -    private static final long MIN_IDLE_MAINTENANCE_INTERVAL_MILLIS = 24 * 60 * 60 * 1000; // 1 day +    private static final long MIN_IDLE_MAINTENANCE_INTERVAL_MILLIS = 30 * 60 * 1000; // 30 minute -    private static final long MIN_USER_INACTIVITY_IDLE_MAINTENANCE_START = 71 * 60 * 1000; // 71 min +    private static final long MIN_USER_INACTIVITY_IDLE_MAINTENANCE_START = 2 * 60 * 1000; // 2 min -    private static final long MAX_IDLE_MAINTENANCE_DURATION = 71 * 60 * 1000; // 71 min +    private static final long MAX_IDLE_MAINTENANCE_DURATION = 2 * 60 * 1000; // 2 min Firstly I  run Quadrant apk to see my I/O performance at beginning, Its score is 3544. During this 30 minutes, you can try to mess your system. Try your best to install most apks. Run monkey test in background. Then I  run Quadrant again to check my I/O performance, its score is only a little decline 3538. After that I run "logcat | busybox grep -i fstrim" in console to wait for the action of fstrim, here is my logcat: 130|root@sabresd_6dq:/ # logcat -d | busybox grep -i fstrim I/fstrim  ( 2344): Starting fstrim work... I/fstrim  ( 2344): Invoking FITRIM ioctl on /data I/fstrim  ( 2344): Trimmed 6367305728 bytes on /data I/fstrim  ( 2344): Invoking FITRIM ioctl on /cache I/fstrim  ( 2344): Trimmed 526355456 bytes on /cache I/fstrim  ( 2344): Finished fstrim work. OK, I checked the I/O information again, its score is restored to 3546: Conclusion      Good, fstrim takes effect. So on imx.6 using android4.3, fstrim will also work automatically. We will also enjoy good performance in I/O memory.Great!
View full article
This document provide an overall guide how to get started with i.MX6 development. There are several chapters: 1. how to get necessary docs from freescale website; 2. how to setup environment and build your own images;3. Hardware design consideration;4. How to get help. I hope the doc will bring you in i.MX world more easily, and hope you all have a fun in it.
View full article
Q: how to do PCIe compliance measurement on the Sabre SDB? Phase Jitter on the PCIe reference clock had been see problem. Pin C7  "CLK1_N" and Pin D7 "CLK1_P"  were used like on the Sabre SD. During Compliance meassurments  margin of -80% and more.... was seen. Is there a known issue? Has someone done a similar compliance measurement on the Sabre SDB? A: The PCIe TX compliance tests on i.MX6 SD boards in TK's Open Lab.  Based on the internal PLL clock, i.MX6 SD boards pass the PCIe TX compliance tests. 1, please check the capacitor on NVCC_PLL_OUT, it should no less than 10uF, 22uF is better. 2, please check if the 24MHz input crystal is good enough. 50ppm is required. 3, please check the test step: 1.1     TX Test Configuration and Procedures Overview of Test Steps 1.      Integrate the patch for PCIE test to mainline, recompile the Kernel , and replace the old image of the board under test. ·         Make sure the following configuration has been set, when re-compiling the kernel image. # MX6 Options: # CONFIG_IMX_PCIE=y 2.      Correctly set up the test environment: ·         Connect the compliance load board (CLB x1/x16) revision 2.0 into the slot of DUT, and change the switch and jumpers to select x1 . ·         Connect the lane under test to oscilloscope via differential probe and matched coaxial , do remember that cable calibration should be done before test. ·         Connect the clock signal to the oscilloscope. The clock must have SSC enabled or disabled to be consistent with settings for the system during normal operation. ·         Power on the system. 3.      After I.MX6x enters Polling.Compliance , press the Toggle Button on CLB to select the output , make sure the data waveform is compliance pattern, 5.0GT/s for GEN2, 2.5GT/s for GEN1. 4.      Follow the Oscilloscope operation instruction, set it to the right mode. 5.      Capture and save at least 1 million * 200 ps of data and clock simultaneously at the sample rate of 50GS/s for GEN2, or 250,000 UI * 400 ps of data at the sample rate of 25GS/s for GEN1. 6.      Run free software Sigtest to analyze the PCIE TX signal. 7.      Customer could adjust the parameters of the PCIE_PHY by changing IOMUXC_GPR8 register settings to get the test past. a.       The default of this Register is configured as: imx_pcie_clrset(IOMUXC_GPR8_TX_DEEMPH_GEN1, 0 << 0, IOMUXC_GPR8); imx_pcie_clrset(IOMUXC_GPR8_TX_DEEMPH_GEN2_3P5DB, 0 << 6, IOMUXC_GPR8); imx_pcie_clrset(IOMUXC_GPR8_TX_DEEMPH_GEN2_6DB, 20 << 12, IOMUXC_GPR8); imx_pcie_clrset(IOMUXC_GPR8_TX_SWING_FULL, 127 << 18, IOMUXC_GPR8); imx_pcie_clrset(IOMUXC_GPR8_TX_SWING_LOW, 127 << 25, IOMUXC_GPR8); b.      write the Register, Address: 20E_0000h base + 20h offset = 20E_0020h; command: /unit_tests/memtool -32 0x020e0020= FFFD4000 This document was generated from the following discussion: i.Mx6 PCIe compliance
View full article
Q:Is there an issue using odd DIV_SELECT values? When setting the CPU clock (maybe others also) in uboot, the code will only use even valuesfor the DIV_SELECT field. There is nothing in the Reference Manual or Errata that indicates only even values can be used for this field. There were 2 SR's that had conflicting answers and we are trying to determine what can be used. The CPU freq setting trying to be achieved is 996MHz. With a 24MHz source, you need 24MHz x 41.5 = 996MHz. Since the DIV_SELECT is x2, a value of 83 would be needed. A: Below is the DIV_SELECT description of ARM PLL, since the Fin is 24MHz, so there is no odd issue of DVI_SELECT, as 24 / 2 = 12MHz. Such as for 996M, this value is 83, that is fine. "This field controls the pll loop divider. Valid range for divider value: 54-108. Fout = Fin * div_select/2.0." This document was generated from the following discussion: mx6Q PLL Setting
View full article
Q: Does anyone have the Lauterbach script files for connecting to the mx53?  Also,  does anyone know of a converter to convert RealView scripts to Lauterbach? A: Please see below attach.cmm and load_simbols.cmm for i.MX53. attach.cmm ; ; Script to attach to a running system, halt the CPU, ; and display the ASM code ; screen.on ; Debugger Reset winpage.reset area.reset WINPOS 0. 26. 75. 8. 0. 0. W000 area print "resetting ICD..." System.Down Break.Delete MAP.RESet TASK.RESet sYmbol.RESet Data.PROLOG.RESet Data.EPILOG.RESet sYmbol.AutoLoad.CHECK OFF      ; disable dynamic autoloader sYmbol.AutoLoad.RESet          ; reset autoloader list MMU.RESet ; setup of ICD JTAG print "initializing JTAG..." SYStem.CPU CORTEXA8 SYStem.MultiCore IRPOST 0x0 SYStem.MultiCore IRPRE 0x0 SYStem.MultiCore DRPOST 0x0 SYStem.MultiCore DRPRE 0x0 SYStem.MultiCore DAPIRPOST 0x09 SYStem.MultiCore DAPIRPRE 0x0 SYStem.MultiCore DAPDRPOST 0x02 SYStem.MultiCore DAPDRPRE 0x0 SYStem.MultiCore MEMORYACCESSPORT 0 SYStem.MultiCore DEBUGACCESSPORT 1 SYStem.MultiCore COREBASE APB:0xC0008000 SYStem.Option DACR ON          ; give Debugger global write permissions TrOnchip.Set DABORT OFF        ; used by Linux OS for page miss! TrOnchip.Set PABORT OFF        ; used by Linux OS for page miss! TrOnchip.Set UNDEF OFF         ; let UNDEF be handled by Linux OS SYStem.Option MMU ON           ; enable space ids to virtual addresses SYStem.JtagClock 20.0MHz SETUP.IMASKASM ON              ; lock interrupts while single stepping ; Use on-chip breakpoints Break.SELect PROGRAM ONCHIP Break.SELect READ ONCHIP Break.SELect WRITE ONCHIP Break.SELect ALPHA ONCHIP Break.SELect BETA ONCHIP Break.SELect CHARLY ONCHIP Break.SELect DELTA ONCHIP Break.SELect ECHO ONCHIP SYStem.Option EnReset OFF SYS.m attach ; wait until reset is complete wait 2.s if run()     Break ; Open a Code Window -- we like to see something WINPOS 0. 0. 75. 20. Data.List enddo load.symbols.cmm ; ; Script to load the Linux kernel symbols into the debugger ; print "loading Linux kernel symbols..." &linuxpath="S:\git\kernel\linux-2.6-imx-0" &kbuildpath="build" sYmbol.SourcePATH.SET &linuxpath Data.LOAD.Elf &linuxpath\&kbuildpath\imx5\vmlinux /StripPART 3 /gnu /nocode ; Map the virtual kernel symbols to physical addresses ; to give the debugger access to it before CPU MMU is ; initialized print "setting system MMU..." MMU.FORMAT Linux swapper_pg_dir 0xc0000000--0xc1ffffff 0x70000000 MMU.Create 0xc0000000--0xc1ffffff 0x70000000 ; map kernel pages at RAM start MMU.COMMON 0xc0000000--0xffffffff            ; common area for kernel and processes ;MMU.TableWalk OFF   ; debugger uses a table walk to decode virtual addresses MMU.ON             ; switch on debugger(!) address translation ; Initialize Mutitasking Support print "initializing multitask support..." TASK.CONFIG ../linux       ; loads Linux awareness (linux.t32) MENU.ReProgram ../linux    ; loads Linux menu (linux.men) HELP.FILTER.Add rtoslinux  ; add linux awareness manual to help filter enddo This document was generated from the following discussion: Lauterbach CMM scripts for mx53
View full article
Q: Looking at the datasheet, why a 14.7KOhm pulldown and a 4.7KOhm pullup must be used? When useing 4.7KOhm resistors in series from an MCU to control the boot pins, pull up is ok, but pull down is not. The EIM boot pins only see 4.7KOhm and not 14.7KOhm as recommended in the design guide. How did we determine those resistor values? at boot there is a pull-up of 100KOhm in the pad if I understand well, 4.7KOhm would do the job as well as 14.7K. right? A: 4.7k will work fine for pull-up or pull-down. 10k pull-downs is to limit current drain while allowing use of simple SPST switches to configure boot-up. There are on-chip 100k pull resistors, so this limits max resistor size. This document was generated from the following discussion: EIM boot resistor value
View full article
Q: Does VIN have to be valid before we can talk to the PMIC over i2c? Can a valid voltage on LICELL and VDDIO work instead? The PF0100 datasheet says: ---------------------------------------------- To communicate with I2C, VIN must be valid and VDDIO, to which SDA and SCL are pulled up, must be powered by a 1.7 to 3.6V supply. VIN, or the coin cell voltage must be valid to maintain the contents of the registers. -------------------------------- A: VIN and VDDIO must be valid for communicating to the I2C block. Having LICELL and VDDIO will not work since a portion of the digital circuitry needed for accessing the registers is powered through VIN. This document was generated from the following discussion: Programming PMIC over i2c
View full article
Q: What is quality level of IBIS file? In chapter 8.6 in IMX6DQ6SDLHDG (Rev.0). It says the following about quality assurance. ===== All models (GPIO, DDR, LVDS, MLB) have passed the following checks: • IBISCHK without errors or unexplained warnings • Data for basic simulation checked • Data for timing analysis checked • Data for power analysis checked • Correlated against Spice simulations Validation reports can be provided upon demand. ==== A: In addition, please see http://www.vhdl.org/pub/ibis/quality_wip/checklist/Using_IQ_2.0_checklist.pdf. This document says about quality level. According to these information, the IBIS quality level is IQ4 (IQ3 + data for power  analysis checked) + "Correlated against Spice simulations". This document was generated from the following discussion: IBIS QUALITIY LEVEL
View full article
Q: What is latency figures for the VPU to decode Device: i.MX6Q OS: Linux Resolution:                         1920x1080(HD) Frame rate:                        30 FPS Function:                             Overlay messages. Input/Output:                   8 bit / YUV 4:2:0 / NAL stream Profile level:                      4.1. Constrained Baseline. I and P frames support. A: It depend on the syntax in H.264, includes num_reorder_frames,max_dec_frame_buffering,num_ref_frames,MaxDpbSize,etc. for start latency: it cover vpu driver loading, allocate buffers, init, decoding the first frame less than 100ms on iMX6/Linux. This document was generated from the following discussion: VPU Latency i.MX6
View full article
Computer On Module • Processor Freescale i.MX535,1GHz/i.MX536, 800MHz • RAM 512MB/1GB DDR3 SDRAM • ROM 4GB EMMC,up to 32GB • Power supply Single 3.1V to 5.5V • Size 54mm SO-DIMM • Temp.-Range -20°C..70°C   -40°C..120°C Key Features • 10/100Mbps Ethernet • Two High Speed USB 2.0 ports • LCD controller up to 1600 x 1200, 24bpp • OpenGL ES 2.0 and OpenVG 1.1 hardware accelerators • Multi-format HD 1080p video decoder and 720p video encoder hardware engine • Two Camera Interfaces • NEON SIMD media accelerator • Unified 256KB L2 cache • Vector Floating Point Unit • Several interfaces: 3x UART, 2x SDIO, 2x SSI/AC97/I2S, I2C, CSPI, Keypad, Ext. Memory I/F • 3.3V I/O OS Support     • Linux     • Android Application:Smart mobile devices,Smart Display,Automotive Infotainment,Digital Signage, Telemedicine,Retail POS Terminal,Security,Barcode Scanner,Visual IP Phone,Patient Monitors,Surveillance Cameras,building control, factory / home automation, HMI For more information, please see Attachment We can provide a complete solution
View full article
Computer On Module • Processor i.MX25, 400 MHz • RAM 64/128 MB mDDR • ROM up to 2 GB NAND Flash • Power supply Single 3.0V to 5.5V • Size 42.2mm SO-DIMM200 • Temp.-Range -40°C..85°C Key Features • 10/100Mbps Ethernet • High-Speed USB 2.0 OTG • Full-Speed USB 2.0 Host • LCD controller • Still-picture camera interface • Several peripheral interfaces: UART, SD-CARD, I2C, PWM, 1-wire, Keypad, Digital Audio (AC97/I2S), Configurable serial peripheral interface, 4 wire Touchscreen, CAN OS Support • Windows Embedded CE 6.0 • Linux 2.6.35 Application:POS, handheld terminals, building security, anti-theft devices for e-commerce, smart meters and access control For more information, please see Attachment We can provide a complete solution
View full article
Computer On Module • Processor Freescale i.MX287, 454 MHz • RAM 128MB DDR2-400 SDRAM • ROM 128MB NAND Flash • Power supply Single 3.1V to 5.5V • Size 40mmX35mm • Temp.-Range -40°C..85°C Key Features • Two 10/100Mbps Ethernet ports with IEEE1588 support • Two High-Speed USB 2.0 ports • One colour LCD controller • Two CAN interfaces • 4 wire Touchscreen interface • Several peripheral interfaces: UART, SD-CARD, I2C, PWM, Serial Audio, SPI • Power management optimized for long battery life • 3.3V I/O OS Support • Windows Embedded CE 6.0 • Linux 2.6.35 Application:Building control, factory automation, printers and security panels, HMI, industrial control media gateways / accessories, portable medical devices, energy-saving Energy Gateway / Meter For more information, please see Attachment We can provide a complete solution
View full article
Computer On Module • Processor Freescale i.MX 6Quad, 1GHz • RAM 1GB DDR3 SDRAM 64-bit • ROM 4GB NAND Flash UP to 16GB • ROM 2M SPI Nor Flash ! • Power supply Single 5V • Size 40mm SO-DIMM • Temp.-Range          0 to + 95C (Consumer)         -20 to + 105C (Extended Consumer)         -40 to +105C (Industrial)         -40 to + 125C (Automotive) Key Features • 10/100Mbps Ethernet • One High Speed USB 2.0 ports • Full HD LCD controller, 24bpp • OpenGL ES 2.0 and OpenVG 1.1 hardware accelerators • Multi-format HD 1080p60 video decoder and 1080p30 encoder hardware engine • Two Camera Interfaces • NEON MPE coprocessor — SIMD Media Processing Architecture — dual, single-precision floating point execute pipeline • Unified 1MB L2 cache • Several interfaces: 5x UART, 2x SDIO, 1x SSI/AC97/I2S, 3x I2C, 2xCSPI • 3.3V I/O • 2x Controller Area Network (FlexCAN) • PCIe 2.0 (1-lane) OS Support     • Linux 3.0     • Android 4.2 Application:Media Tablet,Education Tablet PC,EBook,Automotive Infotainment,Aviation Infotainment,HMI,Portable Medical Instruments,IPTV,IP Phone,Smart Energy Systems,Intelligent industrial control systems For more information, please see Attachment We can provide a complete solution
View full article
In Chinese Twitter: Sino Weibo, one famous distributor mentioned “i.MX28 is the best choice in ARM9 core-based processor, no ‘one of’”. With high integration of analog module and digital module, i.MX28 is attracting more and more engineers in various applications. Despite its advantage, there are some mistakes one may commit or issues they may meet. The note records a number of issues/mistakes. Each case in the note comes from a real story. I hope the note will help you in your development work. And It is definitely welcomed for everyone to add your own content to the note.The more you share, the more you get.
View full article
Q: When trying to mount his SDIO WiFi module (an Azurewave module containing a Marvel 88W8790)  in 4 bit mode, and got error wifi module on iMX6 Smart SD dev board using the alpha kernel (3.5.7+3285970). mwifiex_sdio mmc0:0001:1: WLAN FW is active mwifiex_sdio mmc0:0001:1: mwifiex_cmd_timeout_func: Timeout cmd id (2004.239824) = 0xa9, act = 0x0 mwifiex_sdio mmc0:0001:1: num_data_h2c_failure = 0 mwifiex_sdio mmc0:0001:1: num_cmd_h2c_failure = 0 mwifiex_sdio mmc0:0001:1: num_cmd_timeout = 1 mwifiex_sdio mmc0:0001:1: num_tx_timeout = 0 mwifiex_sdio mmc0:0001:1: last_cmd_index = 1 mwifiex_sdio mmc0:0001:1: last_cmd_resp_index = 0 mwifiex_sdio mmc0:0001:1: last_event_index = 0 mwifiex_sdio mmc0:0001:1: data_sent=1 cmd_sent=1 mwifiex_sdio mmc0:0001:1: ps_mode=1 ps_state=0 +++++++++++++++++++++++ There are only two known issues with the SDHC driver as noted in the release notes and these don't seem to match.  The Linux Reference Manual states the operation of the SDIO was veriifed usign the AR6003.  My assumption is that this is the Silex module we have standardized on.  Was 4 bit mode verified using this module? Does anyone have any idea what could be happening here? A: L3.5.7 is an alpha release, and WiFi function is not stable. The test report shows that open WiFi issue exists. Wifi module sometime can't work on mx6q_smd. After insmod ath, ath6kl_core and ath6kl_sdio. Insert the wifi card, sometime(50%) will display -------------------------- ath6kl: unable to read RX_LOOKAHEAD_VALID                                      ath6kl: Unable to recv target info: -84                                        ath6kl: Failed to init ath6kl core                                             ath6kl_sdio: probe of mmc0:0001:1 failed with error -84    -------------------------- reinsert the wifi card may solve the problem. when execute "udhcpc -i wlan0", sometime (30%) will cause program exception. Sometime can't get the wlan0 ip(program hang). Environment(OS,Platform,Driver, etc): HW: MX6Q_SMD Num014 and Num017 MX6Q_ARD don't have this problem SW: Kernel 3.5.7-1.0.0 GNU/Linux Case ID: TGE-LV-WIFI-0043 Reproduce Steps: #modprobe ath #modprobe ath6kl_core #modprobe ath6kl_sdio insert the wifi card # iwconfig wlan0 mode managed # iwlist wlan0 scanning | grep MAD-wifi #iwconfig wlan0 key 00112233445566778899123456 #iwconfig wlan0 essid MAD-wifi #udhcpc -i wlan0 Attached MX6 ARD WiFi issue also. [Kernel3.5.7_MX6QARD]Wifi:wifi card can't work during suspend and resume. 100% -- Bug detailed description: With wifi card inserted in the board. doing system suspend and resume test. wifi card can't work well after the system suspend and resume. Always report : ath6kl: Unable to decrement the command credit count register: -84             ath6kl: Unable to write to the device: -84                                     ath6kl: bmi_write_memory for uart debug failed                                 ath6kl: Failed to boot hw in resume: -5          Environment(OS,Platform,Driver, etc): HW: MX6QARD -023 Only tried on this platform SW: root@imx6qsabreauto:~# uname -a                                                Linux imx6qsabreauto 3.5.7-1.0.0+3285970 #1 SMP PREEMPT Sat Jun 29 10:20:45 CDT 2013 armv7l GNU/Linux Case ID:  TGE-LV-WIFI-1060 and TGE-LV-WIFI-1062 Reproduce Steps: 1. boot the kernel with wif card inserted 2. doing wifi stress test 3. doing suspend and resume
View full article