i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
LTIB Creating Uimage Uboot Configuration file for fw_(printenv/saveenv) utility Add new i.MX5x board on LTIB LTIB Creating Uimage Uboot U-boot expects uImage format for the kernel image. In order to LTIB generate a uImage file: $ export SYSCFG_KTARG=uImage $ ./ltib -p kernel Setup in U-Boot the kernel bootargs: u-boot> setenv bootargs noinitrd console=ttymxc0,115200 init=/linuxrc root=/dev/nfs nfsroot=10.29.244.27:/tftpboot/rootfs ip=dhcp Change 10.29.244.27 to your host IP. The procedure above is needed when default bootloader used by ltib was redboot. In some ltib releases (before 2010) default bootloader is u-boot. In this case, ltib will create uImage by default Configuration file for fw_(printenv/saveenv) utility # Configuration file for fw_(printenv/saveenv) utility. # Up to two entries are valid, in this case the redundant # environment sector is assumed present. # Notice, that the "Number of sectors" is ignored on NOR.               # MTD device name Device offset Env. size Flash sector size Number of sectors #/dev/mtd1 0x0000 0x4000 0x4000 #/dev/mtd2 0x0000 0x4000 0x4000 # NAND example /dev/mtd0 0x80000 0x40000 0x20000 2 Add new i.MX5x board on LTIB After porting u-boot to your i.MX5x board you might want add it on LTIB menu, "Choose your board for u-boot" section. For this, edit ltib/config/platform/imx/main.lkc to add your board: Enter board on menu: comment "Choose your board for u-boot" choice prompt "board" default BOARD_MX51_BBG depends on PLATFORM = "imx51" help This menu will let you choose the board you use. ... + config BOARD_MX53_MYBOARD + bool "mx53_myboard" ... endchoice Add the "mx53_myboard_config" that matches your board configuration on the u-boot Makefile to PKG_U_BOOT_CONFIG_TYPE: config PKG_U_BOOT_CONFIG_TYPE   string   ... + default "mx53_myboard_config" if ( PLATFORM = "imx51" && BOARD_MX53_MYBOARD && !PKG_KERNEL_UPDATER )   ...
記事全体を表示
This patch implements (or exposes) routines to poll the imx uarts. The KGDB drivers need these methods to be implemented or the ttymxc driver is not sufficient. The synthetic CONFIG_CONSOLE_POLL value activates these routines (or CONFIG_SERIAL_MXC_CONSOLE for the polled write). There is still no poll routines in -855-ge067785, which is the September 2010 Linux release from Freescale. Also not in Linux 2.6.36 drivers/serial/imx.c either. $ git diff drivers/serial/mxc_uart.c diff --git a/drivers/serial/mxc_uart.c b/drivers/serial/mxc_uart.c index ae6d2e1..728b607 100644 --- a/drivers/serial/mxc_uart.c +++ b/drivers/serial/mxc_uart.c @@ -1551,6 +1551,28 @@ mxcuart_pm(struct uart_port *port, unsigned int state, unsigned int oldstate)                             clk_enable(umxc->clk);    }  +#ifdef CONFIG_CONSOLE_POLL +/* + * Read a character from the UART. + */ +static inline int mxcuart_console_read_char(struct uart_port *port) +{ +       volatile unsigned int status; +    int ch; + +       do { +               status = readl(port->membase + MXC_UARTUSR2); +       } while ((status & MXC_UARTUSR2_RDR) == 0); +       ch = readl(port->membase + MXC_UARTURXD); +/* Ignore parity errors, etc. */ +/*  status = ch | UART_CREAD_BIT; */ +    ch &= 0xff; + +    return ch; +} +static void mxcuart_console_write_char(struct uart_port *port, char ch); +#endif +    /*!     * This structure contains the pointers to the control functions that are     * invoked by the core serial driver to access the UART hardware. The @@ -1575,14 +1597,18 @@ static struct uart_ops mxc_ops = {                 .config_port = mxcuart_config_port,                 .verify_port = mxcuart_verify_port,                 .send_xchar = mxcuart_send_xchar, +#ifdef CONFIG_CONSOLE_POLL +              .poll_put_char = mxcuart_console_write_char, +              .poll_get_char = mxcuart_console_read_char, +#endif };  -#ifdef CONFIG_SERIAL_MXC_CONSOLE +#if defined(CONFIG_SERIAL_MXC_CONSOLE) || defined (CONFIG_CONSOLE_POLL)     /*     * Write out a character once the UART is ready     */ -static inline void mxcuart_console_write_char(struct uart_port *port, char ch) +static void mxcuart_console_write_char(struct uart_port *port, char ch)    {            volatile unsigned int status;  @@ -1592,6 +1618,10 @@ static inline void mxcuart_console_write_char(struct uart_port *port, char ch)                writel(ch, port->membase + MXC_UARTUTXD);     }  +#endif + +#ifdef CONFIG_SERIAL_MXC_CONSOLE +    /*!     * This function is called to write the console messages through the UART port.     *
記事全体を表示
Question: How much control of the bitrate does the i.MX6's VPU provide? VPU API includes a bitrate setting in the EcnOpenParam, is this a maximum, minimum, or something else? To encode two 1280x1080 streams at 30fps with a bit rate of at least 20Mbps, from the information in the following thread, it looks like this isn't supported due to VPU bandwitdh, Is there any limit on bitrate due to the VPU's processing bandwidth?  I.e., if the stream is limited to one 1280x1080 channel, can we choose a maximum bit rate and if so, how do we determine what it is? Answer: The bitRate field in the EncOpenParam structure is the desired target bit rate in kbps. If 0, there is no rate control and frames are encoded based on the quantization parameter specified by the quantParam field in EncParam.structure. It seems upper limit is 20Mbps for 1280x1080@30fps. So you should specified bitrate=2000 in your use case. In general, the maximum bitrate is about 30Mbps. Vpu driver will return invalid parameter if the appointed bitrate reach out of the range (0, 32767kbps). Please refer to Q&A: MX6 VPU H.264 Dual Stream Encode Limits.
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343242 
記事全体を表示
I have imx53 quick sort board i downloaded u-boot-mx53.bin and uImage to loade that into the board and dowloaded rootfs.ext2.gz in the L2.6.35_11.09.01_ERimages and i did partitions on 1GB memory card and loaded that u-boot-mx53.bin,uImage images on to the 500mb of NTFS filesystem and loaded and rootfs.ext2.gz on to the othe 500mb of ext4 file system the i inserted memorycard in to the board but u-boot logs are not comming what will be the solution
記事全体を表示
DEVREGS - Is a tool to display and modify a device's registers at runtime. Under Linux, you can access registers, or any area of physical memory through the /dev/mem pseudo-device and the wonders of the mmap system call. To use it, you open the /dev/mem device, mmap the page in which a register is located, then use the pointer returned to read and/or write the data. Boundary Devices, developed a tool known as " devregs  " that allows you to put a little structure around this facility. It allows you to give names to particular physical memory areas and to describe the bits within a register in the text file /etc/devregs.dat. How to read from register : To read one or more registers, use devregs with a single parameter that’s either an address or a register name. Ex : $  devregs 0x73f88000 :0x73f88000    =0x803dffaf If a register address matches a register in /etc/devregs.dat , you’ll see the register name: Ex : $ devregs 0x73f88000 GPIO2_DR:0x73f88000    =0x803dffaf If used with a register name, any bitfields defined will be shown: Ex: devregs UART1_UFCR UART1_UFCR: 0x73fc0090   =0x0801 UART1_UFCR:0x73fc0090    =0x0801       TXTL                      10-15     =0x2       RFDIV                    7 - 9      =0x0       DCEDTE                 6 - 6     = 0x0       RXTL                       0 - 5     = 0x1 How to write to register : Ex : $ devregs GPIO2_GDIR GPIO2_GDIR:0x73f88004    =0x0002c0a4 Ex: $ devregs GPIO2_GDIR 0x2c0a0 GPIO2_GDIR:0x73f88004    =0x0002c0a4 GPIO2_GDIR:0x73f88004 == 0x0002c0a4...0x0002c0a0 Ex: $ devregs GPIO2_GDIR GPIO2_GDIR:0x73f88004    =0x0002c0a0 For more detailed information please go through the following below links : http://boundarydevices.com/i-mx5x-device-register-access/ http://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/
記事全体を表示
Video in Host Side Converting images (png, jpg, etc) to YUV format ffmpeg -f image2 -i test.png -pix_fmt yuv420p test.yuv Converting AVI files to YUV format To convert AVI to YUV you can use the lav2yuv program. In Ubuntu Linux this program is in mjpegtools package. This is the way to convert: lav2yuv myfile.avi > myfile.yuv Converting YUV video files to AVI (DivX) Use the ffmpeg tool: ffmpeg -s 176x144 -i kuuba_maisema_25fps_qcif.yuv -vcodec mpeg4 -sameq -aspect 4:3 ~/kuuba.avi You need to specify the video dimensions (176 × 144), the video codec (mpeg4), and the aspect ratio (4:3). Converting MP4 to AVI Use the mencoder tool: mencoder Bike1.mp4 -ovc lavc -oac lavc -o NewBike1.avi
記事全体を表示
Attached is a chunk of the filesystem for the Linux Image https://community.freescale.com/docs/DOC-93887
記事全体を表示
Overview The purpose of this document is to describe how to enable 3G modem in i.MX sabresx board for Android software. Hardware Changes Unlike other boards of I.mx series, in sabresx board  3G modem doesn't share to use PCIE slot any longer. It is not connected with PCIE slot by default. So if you still want to use 3G modem like in sabresd board. You need to do a tiny hardware rework. Like the below, R177 and R178 is DNP. Just add a zero resistor here. Software patches After you have do hardware rework above, then you should git am the attached patch to add software support which will add the dts config of 3G power. In our official release version, we don't include this patch.
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342833 
記事全体を表示
Quick notes on testing audio on the i.MX 8QuadMax MEK board with 4.19.35-1.1.0 BSP. Hardware:   - Connect the MCIMX8QM-CPU to the MCIMX8-8X-BB.  - Connect the IMX-AUD-IO to the Audio Slot 1 on the MCIMX8-8X-BB.  - Short 2 and 3 on J47 on the MCIMX8-8X-BB  - Connect an external powered speaker to RCA connectors Audio OUT FR and/or Audio OUT FL on the IMX-AUD-IO  - Optionally, connect a headphone on J15 on the MCIMX8QM-CPU   Test: Power on the board. aplay -l shows the audio interface available. root@imx8qmmek:~# aplay -l **** List of PLAYBACK Hardware Devices **** card 0: cs42888audio [cs42888-audio], device 0: HiFi cs42888-0 [] Subdevices: 1/1 Subdevice #0: subdevice #0 card 0: cs42888audio [cs42888-audio], device 1: HiFi-ASRC-FE (*) [] Subdevices: 1/1 Subdevice #0: subdevice #0 card 1: wm8960audio [wm8960-audio], device 0: HiFi wm8960-hifi-0 [] Subdevices: 1/1 Subdevice #0: subdevice #0 card 2: imxaudmix [imx-audmix], device 0: HiFi-AUDMIX-FE (*) [] Subdevices: 1/1 Subdevice #0: subdevice #0 card 2: imxaudmix [imx-audmix], device 1: HiFi-AUDMIX-FE (*) [] Subdevices: 1/1 Subdevice #0: subdevice #0 Play file on powered speaker via cs42888: root@imx8qmmek:~# aplay -Dhw:0,0 test.wav Playing WAVE 'test.wav' : Signed 16 bit Little Endian, Rate 48000 Hz, Stereo Play file on headphone via wm8960: root@imx8qmmek:~# aplay -Dhw:1,0 test.wav
記事全体を表示
This tutorial teaches how to flash bootloader using ATK. ATK (Advanced Toolkit) ATK (Advanced Toolkit) is a Windows software for programming the flash memory of i.MX boards. Using ATK This section will describe the procedure to erase the flash memory and program the bootloader. 1 - Connect a serial cable between PC and i.MX board. 2 - Some hardware configurations (switches) must be done to flash the board.    Set S18 switch as below: Switch S18 -> 111100 3 - Run ATK by clicking Start -> Programs -> AdvancedToolKit -> AdvancedToolKit      Set the options:    Device memory -> DDR; Custom Initial File -> (keep it unmarked)    Communication Channel -> Serial Port (Usually COM1) 4 - Click Flash Tools to erase, program or dump the the flash memory and click GO Flash Programming The next step is to program the bootloader image into the board's Flash following the steps below. 1 - Select the parameters as shown in the figure below and press Program.    The bootloader binary image file can be found into your Board Support PackageSet Program, NOR Spansion, Bi Swap 2 - Add it on Image File field and press Program. 3 - Close ATK, turn off the board and set switch back as shown in the picture below. Installing ATK on Linux Download ATK: Download. Extract ATK: # unzip ATK_1_41_STD_installer.zip Execute the default install process: # wine SETUP.EXE Get mfc42.dll and msvcp60.dll from a Windows Machine (C:\Windows\System32) and copy to wine system32 (/root/.wine/drive_c/windows/system32) Run ATK: # wine ADSToolkit_std.exe
記事全体を表示
Question: Two boards are used and practically identical - one using the i.MX6Solo, the other is using a Dual. The sw settings in both cases are identical (except IOMUX addresses). On the i.MX6Solo they do not see any packet loss, on the i.MX6Dual they do. I recommended modifying the MTU size, but this also did not help. So here my two questions: 1)      is there still some hw difference between the Ethernet block on the Solo and the Dual/Quad? 2)      They run the AHB at only 100MHz. Could that be a problem? If not, why do the two chips behave so differently? To increase the AHB clock to 133 MHz.appears to solve the packet corruption issue. Is the 100 MHz AHB clock really the root cause. Answer: The DualLite/Solo and SoloLite contain different ethernet controllers. The DL/S has a 1000M controller which requires the AHB bus to be greater than 125MHz, while the SL has a 100M controller. As the question was about the Solo and the Dual and both use the Gigabit Ethernet block I assume that both will require a minimum AHB clock of 125MHz.
記事全体を表示
The patches are based on iMX53 L2.6.35_ER1109 BSP. In default linux BSP, the followed two pathes were supported in kernel driver mxc_v4l2_capture.c: CSI->IC->MEM CSI->MEM After appied these two patches, it can support the followed path: CSI->VDI->IC->MEM In this mode, the VDI de-interlace will be handled on the fly, so the whole system bandwidth will be reduced. Limitations: 1. Since the IC can only output resolution up to 1024*1024, so this is the limation on output. 2. Only VDI motion mode 2 was supported. mxc_v4l2_tvin_vdi_ic.zip: It is the test aplication, test command: "./mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 800 -oh 480 -i 2" "-i 2" means CSI->VDI->IC->MEM path.
記事全体を表示
U-boot expects uImage format for the kernel image. In order for LTIB to generate a uImage file: $ export SYSCFG_KTARG=uImage $ ./ltib -p kernel Setup in U-Boot the kernel bootargs: u-boot> setenv bootargs noinitrd console=ttymxc0,115200 init=/linuxrc root=/dev/nfs nfsroot=10.29.244.27:/tftpboot/rootfs ip=dhcp Change 10.29.244.27 to your host IP. The procedure above is needed when default bootloader used by ltib was redboot. In some ltib releases (before 2010) default bootloader is u-boot. In this case, ltib will create uImage by default
記事全体を表示
Audio transcoding # Transcode the input file into MP3 gst-launch filesrc location=media_file typefind=true ! beepdec ! mfw_mp3encoder ! matroskamux ! filesink location=output_audio_file.mk Audio transcoding + streaming # Transcode the input file into MP3 and stream it # On host, get the transcoded audio data gst-launch udpsrc port=8880 ! <CAPS_FROM_THE_TARGET> ! queue ! ffdec_mp3 ! alsasink # where <CAPS_FROM_THE_TARGET> can be something like 'audio/mpeg, mpegversion=(int)1, layer=(int)3, rate=(int)44100, channels=(int)2' # run the pipeline and check the caps gst-launch filesrc location=media_file typefind=true ! queue ! beepdec ! mfw_mp3encoder ! udpsink host=10.112.103.77 port=8880 -v Video Transcoding* # Transcode the input file into AVC (H-264) gst-launch filesrc location=media_file typefind=true ! aiurdemux name=demux ! queue ! vpudec ! vpuenc codec=avc ! matroskamux name=mux ! filesink location=output_media_file.mk Video Transcoding + scaling* # Transcode the input file into AVC (H264) and rescale video to 480p gst-launch filesrc location=media_file typefind=true ! aiurdemux name=demux ! queue ! vpudec ! mfw_ipucsc ! 'video/x-raw-yuv, width=(int)720, height=(int)480' ! vpuenc codec=avc ! matroskamux name=mux ! filesink location=output_media_file.mk Video transcoding + scaling + streaming* # NOTE: Run the pipelines in the presented order # On host, get the transcoded+scaled video data $ gst-launch udpsrc port=8888 ! <CAPS_FROM_THE_TARGET> ! queue ! ffdec_h264 ! xvimagesink # On target, run the pipeline and check the caps gst-launch filesrc location=media_file typefind=true ! aiurdemux name=demux ! queue ! vpudec ! mfw_ipucsc ! 'video/x-raw-yuv, width=(int)720, height=(int)480' ! vpuenc codec=avc ! udpsink host=$HOST_IP port=8888 -v * There is a limit for the number of pipelines which can be run simultaneously, for high resolution input files, at most two for 1080p and four for 720p.
記事全体を表示
This is a copy of the currently posted i.MX25 reference manual to be used to enter community comments.  Please feel free to add inline comments in this reference manual. You can point out where more information is needed or where existing information is incorrect.  You can also enter information in your comment that expands on existing information in the document, based on your experience with the device.  If you are pointing out that more information is needed in a paragraph or a section, please be very specific, not “needs more information”.  Your comments in this manual may help other members and will drive improvements in this and future documentation. Note: The doc viewer does not support going directly to a specified page.  Instead of manually paging through one page at a time, you can do a search on a string on a page such as "types of resets", or you can go to chapter links listed in the inline comments.  To do this, page down to the comments below the doc view, select "Inline Comments", sort the comments by "page", and then select the chapter you want to view.
記事全体を表示
You can power on/off i.MX31 PDK LEDs using U-Boot: u-boot> mw.b B6020000 FF Where B6020000 is the CPLD LED address and FF is the 8 bits hexadecimal value which will be displayed on LEDs.
記事全体を表示
Creating Deployment System          Configuring Bootloader       Running Linux     
記事全体を表示