i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
ATK (Advanced Toolkit) ATK (Advanced Toolkit) is a Windows software for programming the flash memory of i.MX boards. Using ATK This section will describe the procedure to erase the flash memory and program the bootloader. 1 - Connect a serial cable between PC and i.MX board. 2 - Some hardware configurations (switches) must be done to flash the board.   Set SW2 switch as below: Switch SW2 -> 11111 3 - Run ATK going to Start -> Programs -> AdvancedToolKit -> AdvancedToolKit   Set the options:   Device memory -> DDR; Custom Initial File -> (keep it unmarked)   Communication Channel -> Serial Port (Usually COM1) 4 - Click on Flash Tools to erase, program or dump the the flash memory and click GO h4> Flash Programming The next step is to program the bootloader image into the board's Flash following the steps below. 1 - Select the parameters as shown in the figure below and press Program. The bootloader binary image file can be found into your Board Support Package Set Program, NOR Spansion 2 - Add it on Image File field and press Program. 3 - Close ATK, turn off the board and set switch back as shown in the picture below. Set SW2 switch as below: Switch SW2 -> 11010 Installing ATK on Linux Download ATK: Download. Extract ATK: # unzip ATK_1_41_STD_installer.zip Execute the default install process: # wine SETUP.EXE Get mfc42.dll and msvcp60.dll from a Windows Machine (C:\Windows\System32) and copy to wine system32 (/root/.wine/drive_c/windows/system32) Run ATK: # wine ADSToolkit_std.exe
View full article
i.MX25 for Industrial and General Embedded The i.MX25 family of multimedia applications processors extends the Freescale ARM9™ portfolio and makes the industrial and general embedded market a key focus of i.MX with the integration of many new features. Speed up to 400 MHz, low power consumption and multiple connectivity options support the growing needs of industrial and general embedded products, while allowing customers to reduce their overall system bill of materials cost. The i.MX258 processor provides additional security features making it the ideal solution for payment terminal (POS), or any other type of product needing secure system boot and tamper detection. i.MX25 for Automotive Today's drivers expect more connectivity in more places from more things—phones, media players and, increasingly, cars. Bluetooth™ connectivity is becoming the norm as more people keep their hands on the wheel instead of on the phone. Connectivity and compatibility with media players is becoming a requirement as consumers' media investment goes digital. The challenge: how can designers support high-end features such as connectivity and media playback without charging high-end prices? The i.MX25 family of processors offers integration that tailors itself to the connectivity requirements of today's automobile but eliminates expensive parts not needed for a cost-conscious infotainment system. The i.MX25 applications processor is a Freescale Energy-Efficient Solutions product. Product Information on Freescale.com i.MX257: Multimedia Applications Processor i.MX251: Multimedia Applications Processor i.MX253: Multimedia Applications Processor i.MX255: Multimedia Applications Processor i.MX258: Multimedia Applications Processor Additional Resources i.MX25 PDK Board I.MX25 PDK Board Get Started i.MX25 PDK Board Flashing NAND i.MX25 PDK Board Flashing SPI NOR i.MX25 PDK Board Flashing SD Card i.MX25 PDK Board Running Linux I.MX25 PDK U-boot SplashScreen I.MX25 PDK U-boot SDCard I.MX25 PDK Using FEC i.MX25: When using 120MHz UPLL as clock source, GPT counter returns unexpected results Limitations of the i.MX SIM Controller to Pass the EMV Certification
View full article
Question: What is minimum requirement for VDDSNVS_IN voltage to keep RTC timing info in SNVS block? In the datasheet, there is requirement for VDDSNVS_IN input and it is 2.9V to 3.3V. Is it recommended requirement for RTC operation? Other security function is not used in SNVS and just interested in basic RTC fuction after power off. Answer: The finall answer is tha to folow our datasheet saying for no matter if you are only RTC keeping application. "The SNVS regulator takes the SNVS_IN supply and generates the SNVS_CAP supply which powers the real time clock and SNVS blocks. If  VDDHIGH_IN is present, then the SNVS_IN supply is internally shorted to the VDDHIGH_IN supply to allow coin cell recharging if necessary. The output voltage is roughly one third(1/3) of SNVS_IN. -- in the SNVS_CAP powered on-chip logics, need min 0.9v for normal operation, we can only guarantee the operation in this condition, whih means min SNVS_IN = 3*SNVS_CAP = around 2.7. with some margin, so min 2.8v is the requireent. Again, we can only guarantee the operation in this condition(VDD_SNVS_CAP >0.9v). The datasheet is correct : VDDSNVS_IN must not be less than 2.8 V (Table 6. Operating Ranges, of IMX6DQCEC,  Rev. 2.2, 07/2013 )  I guess you talked about operating condition in ON mode. In case of OFF mode, VSNVS output of PFUZE depends on LICELL input power and usually coincell can supply under 2.5V output. According to PFUZE spec, VSNVS output in OFF mode is under 1.8V. And as I know, LP (low power) part of SNVS is only operation al in OFF mode so I don't think VDDSNVS_IN requires over 3V in that condition. In my assumption, SNVS can maintain itis data and RTC if VDDSNVS_IN is over 1.1 ~ 1.3V in OFF mode but I just want to know what is our spec for it. If we consider low power modes of the i.MX6, then - according to Table 10 (Stop Mode Current and Power Consumption) of IMX6DQCEC, Rev. 2.3, 07/2013 (for example) - in "SNVS Only" mode VDD_SNVS_IN of 2.8V is considered. Here 2.8 V is taken as minimal value. At least, as we can see, there are no other specifications.
View full article
ATK (Advanced Toolkit) ATK is a Windows tool for programming the flash memory of i.MX boards. It can be downloaded here. Using ATK This section will describe the procedure to erase the flash memory and program the bootloader. 1. Assemble the PDK using the CPU board, the Personality board, and the Debug board. 2. Connect a USB cable between the PC and the i.MX25 PDK Personality board. 3. Some hardware configurations (switches) must be set for booting from UART/USB:   On the debug board:   Switch SW5 -> Off   Switch SW6 -> Off   Switch SW7 -> Off   Switch SW8 -> Off   Switch SW9 -> On   Switch SW10 -> On   On the personality board:   Switch SW21 -> 11000000   Switch SW22 -> 00000000 {{Note|On SW5 thourgh SW10, "1" means the keys selected towards the edge of the board.} 4. Run ATK (1.6 or above) going to Start -> Programs -> AdvancedToolKit -> AdvancedToolKit   Set the options:   i.MX CPU -> i.MX25_TO1.1   Device memory -> DDR2;   Custom Initial File -> (keep it unmarked)   Communication Channel -> USB 5. Power up the i.MX25 PDK 6. Click on "Next" 7. Click on Flash Tools to erase, program or dump the the flash memory and click GO. NAND Flash Erasing 1. Configure the Dip Switch of Personality Board:                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                      Switch 1 2 3 4 5 6 7 8 SW1 OFF OFF OFF OFF N/A N/A N/A N/A SW2 ON OFF OFF ON ON OFF OFF OFF 2. Choose NAND model K9LAG08U8M 3. Continue the steps Remember to select the checkbutton BBT (Back Block Table) Commands to flash kernel and rootfs fis init -f load -r -b 0x100000 zImage -h <host IP address> fis create -f 0x300000 kernel load -r -b 0x100000 rootfs.jffs2 -h <host IP address> fis create -f 0x800000 root fis load kernel exec -c "noinitrd console=ttymxc0 115200 root=/dev/mtdblock2 rw ip=dhcp rootfstype=jffs2" Command to create rootfs.jffs2 mkfs.jffs2 -r rootfs -e 0x80000 -s 0x1000 -n -o rootfs.jffs2
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344462 
View full article
I have a few questions about the various reference designs for the i.mx6UL. Please see the attachment for specifics.
View full article
Qtopia Qt Extended, formerly known as Qtopia until September 30, 2008, is an application platform for Embedded Linux-based mobile computing devices such as personal digital assistants, mobile phones, and web pads. It is being developed by Qt Software, a subsidiary of Nokia. [Source: http://en.wikipedia.org] Qt Software discontinues Qt Extended March 3, 2009 — Oslo, Norway — Qt Software today announced that the product, Qt Extended, will be discontinued as a stand-alone product. Instead, selected features will be migrated into the Qt framework which will result in Qt becoming an even richer, cross-platform application framework. The final release of Qt Extended will be version 4.4.3, which will is planned for release on March 5, 2009. Qt Extended will be maintained for one year from that date. Qt Software will honor all existing support agreements, and for customers who need continued access to support beyond the term of their current agreement, Qt Software is offering the possibility of purchasing supplemental support. [Source: http://www.qtsoftware.com/about/news/qt-software-discontinues-qt-extended] Compiling Qtopia Crosscompiling Qtopia for i.MX processors requires some packages to be installed on host (PC). For more details click on your host PC Linux distribution below: All Boards Qtopia All Boards Qtopia on Ubuntu It's possible to compile Qtopia (version 2 or 4) by selecting Qtopia on package list or simply selecting Qtopia profile on Ltib configuration. Starting Qtopia Touchscreen setup When the system starts up, TSLIB_TSDEVICE environment variable must be set and ts_calibration application must be called to calibrate the touchscreen. $export TSLIB_TSDEVICE=/dev/input/event1 /dev/input/event1 is the usual touchscreen device. Some systems can address the touchscreen device to other names. It's possible to check what's the touchscreen device by typing: $cat /dev/input/<supposed device> After the command above, when touchscreen is pressed, some characters will be showed indicating that the <supposed device> device is the touchscreen device and it's working properly. $ts_calibrate Calibrate screen will appear. After touchscreen calibration, Qtopia can be executed by calling the following script: $/etc/rc.d/init.d/qtopia start Qtopia will be started.
View full article
This doc show: on i.MX6Q SabreSD board, configure ov5640 sensor(parallel or MIPI) output 5MP(2592x1944) RAW(Bayer) data at 15fps,and i.MX6Q IPU capture RAW RGB data, and i.MX6Q GPU debayer RAW data then display image. HW: i.MX6Q-SabreSD board, ov5640 sensor. SW: Linux 4.14.98_2.0.0 BSP, and patches in this doc. Configure at camera sensor side A Bayer filter is a color filter array (CFA) for arranging RGB color filters on a square grid of photosensors. The filter pattern is 50% green, 25% red and 25% blue, hence is also called BGGR, RGBG ,GRGB, or RGGB. The ov5640 has an image array capable of operating at up to 15 fps in 5 megapixel (2592x1944) resolution. OV5640 support output formats: RAW(Bayer), RGB565/555/444,CCIR656, YUV422/420, YCbCr422, and compression. To make ov5640 output 5MP RAW data at 15fps, check my patch imx6_ov5640_dvp_mipi_raw_capture_driver-4.14.98_2.0.0.diff which apply on i.MX Linux 4.14.98_2.0.0 BSP kernel code: Parallel interface ov5640, use ov5640_raw_setting[] array of drivers/media/platform/mxc/capture/ov5640.c. This register setting is come from ov5640 software application note and data sheet. MIPI interface ov5640, use ov5640_mipi_raw_setting[] array of drivers/media/platform/mxc/capture/ov5640_mipi.c. This register setting is combine setting of original code (remove ISP register setting), plus PLL register setting for MIPI interface, plus some data format register setting. Configure at i.MX6Q side The i.MX6Q IPU camera port(CSI-2 module) support data format include Raw(Bayer), RGB, YUV 4:4:4, YUV 4:2:2 and grayscale, up to 16 bits per value. Below is camera data routing for i.MX6Q:    Below is i.MX6Q IPU block daigram: The CSI-2 of IPU which is responsible for synchronizing and packing the video (or generic data) and sending it to other blocks. The video data received by CSI-2, could be sent to three other blocks: SMFC, VDI, IC. For RAW (Bayer) data capture, should go through path like this: CSI-2-->SMFC-->IDMAC-->DDR memory It means RAW data is received as generic data, see IPU_PIX_FMT_GENERIC in my patch, and IPU cannot process this kind data, it is just received to DDR memory. For MIPI interface camera, need note is i.MX6 side MIPI D-PHY clock must be calibrated to the actual clock range of the camera sensor’s D-PHY clock and the calibrated value must be equal to or greater than the camera sensor clock, detail see  AN5305. Take MIPI ov5640 as example: Pixel clock = 2592x1944x15fpsx(1/2 cycle/pixel)x1.35 blank interval = 51MHZ MIPI data rate = 51MHZ x 16 bit = 816Mb/s so 816/2/2*2 is 408MHZ is i.MX6 side D-PHY clock. Here due to one bayer pixel is 8bit, and i.MX6 MIPI data bus is 16 bit, so above use 1/2 cycle/pixel. And check ov5640_mipi_raw_setting[], you will got the sensor side D-PHY clock is about 672/2 = 336MHZ. And check AN5305, register MIPI_CSI2_PHY_TST_CTRL1 of i.MX6 need set as 0xC, but here i still keep it as default BSP value 0x14.   3.Capture test code I changed unit test mxc_v4l2_capture.c to capture the RAW data and save it to file. Check my patch imx6_ov5640_raw_captupre_test_4.14.98_2.0.0_ga.diff which apply on i.MX  Linux 4.14.98_2.0.0 BSP unit test code. Note the usage is: ./cap.out -c 1 -i 1 -fr 15 -m 6 -iw 2592 -ih 1944 -ow 2592 -oh 1944 -f BA81 -d /dev/video1 savefile.dmp parameter -i 1 means use CSI to MEM mode /dev/video1 is MIPI ov5640, /dev/video0 is parallel ov5640   4.Display RAW data The RAW data cannot be displayed directly, debayer process is needed to get complete red, green, blue color for each pixel. The debayer process if run on CPU, will cost much CPU time. To save CPU time, debayer could done by GPU. The method is, captured RAW data upload to GPU as texture , then GPU will do the debayer, then full color of each pixel will be got, then display it. To upload RAW camera data to GPU with zero memory copy, i will use i.MX6Q GPU extension GL_VIV_direct_texture. It create a texture with direct access support. API glTexDirectVIVMap,  which support mapping a user space memory or a physical address into the texture surface. The API glTexDirectVIVMap need logic and physical address of data buffer, so i will allocate data buffer from /dev/mxc_ipu, it is dma-buffer also get logic/physical address of buffer, then queue it as USERPTR to ipu v4l2 capture driver, after dequeue got RAW camera data, pass it to GPU for debayer. GPU side, I will use OpenGL shader code from "Efficient, High-Quality Bayer Demosaic Filtering on GPUs". Check my patch imx6-5640-debayer-testcode-gpusdk-5.2.0.diff which apply on i.MX GPU SDK 5.2.0 code. Note, here i only do is debayer, no extra process.   Known issue One thing is ov5640 output 5MP at 15fps, compare with output 5MP at 5fps, there are more noise of camera data at 15fps case. My debug found is , this noise seems come from ov5640 itself.   Reference: a>https://www.nxp.com/webapp/Download?colCode=IMX6DQRM b>https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.0.0_MX6QDLSOLOX&appType=license c>https://github.com/NXPmicro/gtec-demo-framework d>https://www.nxp.com/docs/en/application-note/AN5305.pdf e>ov5640 data sheet f>ov5640 software application note g>Efficient, High-Quality Bayer Demosaic Filtering on GPUs https://www.semanticscholar.org/paper/Efficient%2C-High-Quality-Bayer-Demosaic-Filtering-on-McGuire/088a2f47b7ab99c78d41623bdfaf4acdb02358fb
View full article
The i.MX 6 Linux L3.10.17_1.0.3 Patch release is now available. Patch Release Notes can be found on  www.freescale.com . This release supports the following i.MX 6 reference boards: ·        i.MX 6 Quad/DualLite/Solo SABRE SD ·        i.MX 6 Quad/DualLite/Solo SABRE Auto ·        i.MX 6 SoloLite This patch release is based on the i.MX 6 Linux L3.10.17_1.0.0 GA release. Release changes the following components: ·        Kernel branch: imx_v2013.04_3.10.17_1.0.0_ga ·        U-Boot branch: imx_3.10.17_1.0.0_ga ·        Graphics: gpu-viv-bin-mx6q, 3.10.17_1.0.3 ·        Graphics: gpu-viv-g2d, 3.10.17_1.0.3 ·        Graphics: Xorg-driver, 3.10.17_1.0.3 More detailed patch description: Please consult the release notes document.
View full article
The i.MX Android L5.0.0_1.0.0 GA release is now available on http://www.freescale.com . ·        Files available # Name Description 1 android_L5.0.0_1.0.0-ga_doc.tar.gz i.MX6 Android L5.0.0_1.0.0 BSP Documentation 2 android_L5.0.0_1.0.0-ga_core_source.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo  i.MX 6Sololite and i.MX6SX Android L5.0.0_1.0.0 BSP, Source Code for BSP and Codecs. 3 android_L5.0.0_1.0.0-ga_images_6qsabreauto.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, and i.MX 6Solo Android L5.0.0_1.0.0 BSP Binary Demo Files for the SABRE for Automotive Infotainment. 4 android_L5.0.0_1.0.0-ga_images_6qsabresd.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, and i.MX 6Solo Android L5.0.0_1.0.0 BSP Binary Demo Files for the SABRE Platform and SABRE Board for Smart Devices. 5 android_L5.0.0_1.0.0-ga_images_6slevk.tar.gz i.MX 6Sololite Android L5.0.0_1.0.0 BSP Binary Demo Files for the SoloLite evaluation kit. 6 android_L5.0.0_1.0.0-ga_images_6sx.tar.gz i.MX 6SoloX Android L5.0.0_1.0.0 BSP Binary Demo Files. 7 fsl_aacp_dec_L5.0.0_1.0.0-ga.tar.gz AAC Plus Codec for i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo i.MX 6Sololite and i.MX 6SX Android L5.0.0_1.0.0 BSP. 8 android_L5.0.0_1.0.0-ga_tools.tar.gz i.MX 6Family Manufacturing Toolkit for L5.0.0_1.0.0 ·        Supported Hardware SoC/Boards: o  i.MX 6Quad SABRE-SD board and platform o  i.MX 6DualLite SABRE-SD board and platform o  i.MX 6Quad SABRE-AI board and platform o  i.MX 6DualLite SABRE-AI board and platform o  i.MX6SoloLite EVK platform o  i.MX6SoloX SABRE-SD board o  i.MX6SoloX SABRE-AI board and platform ·        Change List Compared to the L5.0.0_1.0.0-alpha release, this release has the following major changes: o  Applies Cortex-A9 Errata 845369, which will cause performance drop in memcpy. o  Prefetches offset change for PL310 to improve the memcpy performance. o    Disables shell as Android CTS requirement. o  Switches the default NAND chip from MT29F8G08ABACA to MT29F64G08AFAAA. o    Includes several fixes to pass CTS android-cts-5.0_r2. ·        Features For features please consult the release notes. ·        Known issues For known issues and more details please consult the release notes.
View full article
Dumping the pipeline elements into a image file # On target, run the pipeline $ export GST_DEBUG_DUMP_DOT_DIR=<folder where dot files are created> $ gst-launch playbin2 uri=file://${avi} $ # Move the .dot files to a host machine (scp, etc) # On Host dot <dot file> -Tpng -o out.png # dot command is part the the graphviz package Querying which elements are being used on a gst-launch command GST_DEBUG=GST_ELEMENT_FACTORY:3 gst-launch playbin2 uri=file://`pwd`/<media file> Interrupting a gst-launch process running in the background kill -INT $PID # where $PID is the process ID Using only SW codecs # Backup and remove $ find /usr/lib/gstreamer-0.10 -name "libmfw*" | grep -v sink | xargs tar cvf /libmfw_gst.tar $ find /usr/lib/gstreamer-0.10 -name "libmfw*" | grep -v sink | xargs rm # Run your pipeline. This time SW codecs are used $ gst-launch playbin2 uri=file://`pwd`/media_file # To 'install' FSL plugins again, just untar the file $ cd / && tar xvf libmfw_gst.tar && cd - # then run your pipeline. This time HW codecs are used $ gst-launch playbin2 uri=file://`pwd`/media_file
View full article
If someone wants to use the OpenGL ES 2.0 extension "GL_OES_vertex_array_object", the macro "GL_GLEXT_PROTOTYPES" must be defined in his program first. Then he can get the extension program location by calling the API eglGetProcAddress.  Here is an example to use this extension. #define GL_GLEXT_PROTOTYPES PFNGLGENVERTEXARRAYSOESPROC glGenVertexArraysOESv; PFNGLBINDVERTEXARRAYOESPROC glBindVertexArrayOESv; PFNGLDELETEVERTEXARRAYSOESPROC glDeleteVertexArraysOESv; glGenVertexArraysOESv = (PFNGLGENVERTEXARRAYSOESPROC)eglGetProcAddress ( "glGenVertexArraysOES" ); glBindVertexArrayOESv = (PFNGLBINDVERTEXARRAYOESPROC)eglGetProcAddress ( "glBindVertexArrayOES" ); glDeleteVertexArraysOESv = (PFNGLDELETEVERTEXARRAYSOESPROC)eglGetProcAddress ( "glDeleteVertexArraysOES" ); After these steps, the new alias glGenVertexArraysOESv, glBindVertexArrayOESv, glDeleteVertexArraysOESv can be use to call the VAO operation function in OpenGL ES 2.0 extensions.
View full article
We are very proud to announce that Element14's SabreLite i.MX6Q board is now officially supported by Adeneo Embedded's i.MX6 WEC7 BSP. As a consequence, our customers are able to use the SabreLite board from Element14 as well as the one from Boundary Devices. Follow this link for Adeneo Embedded's i.MX6 WEC7 BSP Follow this link for Element 14's SabreLite board Ce document a été généré à partir de la discussion suivante : Element14's SabreLite board officially supported by Adeneo Embedded's i.MX6 WEC7 BSP
View full article
Step 1: Build r13.4.1         make         /* Store images file for MFGTool use */         make dist    /* Get ota_1.zip, and target_files_1.zip at out/dist, store them in a dedicated directory, for example .../release-1 */ Step 2: Modify any files in source code base; Step 3: make dist    /* Get ota_2.zip, and target_files_2.zip at out/dist, store them in a dedicated directory, for example .../release-2 */ Step 4: MFGTool flash release-1 images; Step 5: cp ota_2.zip to SD; Step 6: start board, then execute following commands under serial terminal;         cp /sdcard/ota_2.zip /cache/ota_2.zip         mkdir /cache/recovery         echo --update_package=/cache/ota_2.zip > /cache/recovery/command         sync         reboot recovery         Then you can see the upgrade successful. Step 7: MFGTool flash release-1 images; Step 8: ./build/tools/releasetools/ota_from_target_files -i .../release-1/target_files_1.zip .../release-2/target_files_2.zip ./diff_from_1_to_2.zip Step 9: cp diff_from_1_to_2.zip to SD; Step10: start board, then execute following commands under serial terminal;         cp /sdcard/diff_from_1_to_2.zip /cache/diff.zip         mkdir /cache/recovery         echo --update_package=/cache/diff.zip > /cache/recovery/command         sync         reboot recovery
View full article
To use Android GDB for native code, take mediaserver as an example. Setup on board. adb push prebuilt/android-arm/gdbserver/gdbserver system/bin/ adb shell ps adb shell /system/bin/gdbserver :5039 --attach <PID> & Setup on host. source build/env.sh adb forward tcp:5039 tcp:5039 gdbclient mediaserver b createPlayer c
View full article
Issue Description When running Android R10.4 on MX51 BBG, the system can not resume sometimes by following the test steps: 1) Enable CLAA-WVGA lcd panel - single display. 2) Play a video in Gallery. 3) Press power key to suspend the system. 4) Press power key to resume the system. 5) Do 3) and 4) continuously. Debug Details When adding the following debug information into vpu_resume function in file drivers/mxc/vpu/mxc_vpu.c, the system gets hang into while loop with the log "VPU Blocking 1**************": static int vpu_resume(struct platform_device *pdev) {         int i;                 WRITE_REG(BITVAL_PIC_RUN, BIT_INT_ENABLE);                 WRITE_REG(0x1, BIT_BUSY_FLAG);                 WRITE_REG(0x1, BIT_CODE_RUN);                 while (READ_REG(BIT_BUSY_FLAG)) {                           printk("VPU Blocking 1**************\r\n");                }; } Root Cause In some use cases,  VPU power gating didn't happen after vpu_suspend() returned successfully because some other devices refused to suspend or other reasons. So vpu_resume() ran FW init code when VPU was idle instead of power off, which could keep BIT_BUSY_FLAG always be 1. Solution In vpu_resume(), if VPU PC is not 0, which means VPU is still running, skip running FW init code. See attached patch based on R10.4.
View full article
A simple Linux kernel module to react on GPIO-generated interrupts
View full article
MX6X_Uboot_V1-20130910.doc: 3.0.35: 3.0.35
View full article
imx53 DDR stress tester V0.042
View full article
HI, I want to build an Ubuntu Linux operating system with LTIB, but from the user guide the host system is Ubuntu 9.04, but we can't use 'apt-get install' any package due to there are no source lists. What should we do next? Thank you!
View full article