i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-341566 
記事全体を表示
The i.MX Android L5.1.1_2.1.0 GA release is now available on the Web Site.  (i.MX6 BSP Updates and Releases à Android) ·        Files available android_L5.1.1_2.1.0-ga_doc.tar.gz​​​ i.MX6 Android L5.1.1_2.1.0 BSP Documentation android_L5.1.1_2.1.0-ga_core_source.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo  i.MX 6Sololite and i.MX6SX Android L5.1.1_2.1.0 BSP, Source Code for BSP and Codecs. android_L5.1.1_2.1.0-ga_images_6qsabreauto.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, and i.MX 6Solo Android L5.1.1_2.1.0 BSP Binary Demo Files for the SABRE for Automotive Infotainment. android_L5.1.1_2.1.0-ga_images_6dqsabresd.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, and i.MX 6Solo Android L5.1.1_2.1.0 BSP Binary Demo Files for the SABRE Platform and SABRE Board for Smart Devices. android_L5.1.1_2.1.0-ga_images_6slevk.tar.gz i.MX 6Sololite Android L5.1.1_2.1.0 BSP Binary Demo Files for the SoloLite evaluation kit. android_L5.1.1_2.1.0-ga_images_6sx.tar.gz i.MX 6SoloX Android L5.1.1_2.1.0 BSP Binary Demo Files. android_L5.1.1_2.1.0-ga_tools.tar.gz i.MX 6 Family Manufacturing Toolkit for L5.1.1_2.1.0 ·        Supported Hardware SoC/Boards: o  i.MX 6Quad SABRE-SD board and platform o  i.MX 6DualLite SABRE-SD platform o  i.MX 6Quad SABRE-AI board and platform o  i.MX 6QuadPlus SABRE-AI board and platform o  i.MX 6DualLite SABRE-AI board and platform o  i.MX 6SoloLite EVK platform o  i.MX 6SoloX SABRE-SD board o  i.MX 6SoloX SABRE-AI board and platform o  i.MX 7Dual SABRE-SD board and platform ·        Change List Compared to the L5.1.1_2.0.0_6qp-ga release, this release has the following major changes: o  Upgraded the Linux kernel version from the L3.14.38_6qp-ga release to the L3.14.52-ga release. o  Added i.MX 6QuadPlus SABRE-SD board support. o  Enabled Broadcom BCM4339 Wi-Fi and Bluetooth module. o  Fixed screen tearing in recovery mode during factory resetting and OTA upgrading. o  Fixed system hang-up issue when playing some short videos for a long time. o  Moved all Freescale extended API to freescale-extended.jar. o  Enabled the ZRAM function for Android platform to enlarge the memory size. o  Integrated 2015-11 AOSP Security patches. ·        Features For features please consult the release notes. ·        Known issues For known issues and more details please consult the release notes.
記事全体を表示
Before reading: only a personal works and sharing, not any form of "release". I didn't find any confidential information from the packages. So, I'm publishing it here. This is only for testing purpose. Do NOT use it for building a product. Use it at your own risk!! Yocto is flexible and powerful, and also, big and slow (when building). Sometimes we only need to build uboot or kernel or some piece of testing code. It's really a waste of time to build-up the whole Yocto environment which may cost over 50GB disk space and over 3 hours of building. I've made some scripts and sum them up to form a toolset for building uboot, kernel and some testing code out of Yocto environment. It's only a simple container and expect to use with uboot and kernel source code from formal Freescale release and a SDK built from Yocto project. GitHub source repo:       https://github.com/gopise/gopbuild What’s made off (a full package, not only the container): 1.    Some scripts and configurations files. 2.    SDK built from Yocto. 3.    Uboot/kernel from specific version. 4.    A hello-world to demonstrate how to build app in this environment. 5.    A slimmed rootfs binary from specific BSP pre-built as base. Will customize base on the source under “rootfs” folder. Only a placeholder in the container-only version. How to use it: Several common used board configurations have been included in the script: 6qsabresd/6qsabreai/6qpsabreai. You can add more into the “gopbuild” script easily. The “sabresd” has been set as default.      If you want to build all for sabresd (First of all, de-compress the package): cd <de-compressed-folder> source envsetup [It will prompt for selecting board configuration to be built. Choose one by input corresponding number or click <ENTER> for default board.] gmk ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍      If you want to build specific module for default board, such as uboot: gmk uboot ‍‍‍‍‍‍‍‍‍      Build kernel for sabreai board instead of default device: gmk kernel sabreai ‍‍‍‍‍‍‍‍‍      Clean everything? gmk all clean ‍‍‍‍‍‍‍‍‍ After a successfully full build, you will get everything under “output” folder, including a log folder contains full build log:      “u-boot.imx/zImage/rootfs.tar.bz2/*.dtb”, can be used with MFG or uuu.      “fsl-image.sdcard”, can be burn into SD card directly. "Ready-for-building" Package: The "gopbuild" itself is a "container-only" package which doesn't contain any source or SDK. I've also made some packages based on latest BSP release for i.MX6/i.MX7/i.MX8. These packages are "ready-for-build" package which you can de-compress and build it directly. -------------------------------------------------------------------------------------------------- URL:https://pan.baidu.com/s/1Xlh1OBGsTRXez_NQw-Rjxg Password: gdc9 -------------------------------------------------------------------------------------------------- Note: 1. To build for i.MX8 (8QM/8MQ/8QXP), you need L4.14.* or above. 2. To build for i.MX8, please download the SCFW from i.MX software page       i.MX Software and Development Tools | NXP      After download, decompress corresponding package for specific chip and put it under "/platform/scfw/". Take i.MX8QXP for example:             /platform/scfw/scfw_export_mx8qx/ All material (uboot/kernel/test code and SDK) are from official Yocto release. Thanks!
記事全体を表示
THE CONTENTS •Background Knowledge −Bootloader Introduction −U-boot Directory Structure of the Source Code •Bootloader Boot Procedure(e.g. U-boot) −i.MX6Q Introduction −Linux OS Boot Process −First Stage of Boot Sequence(Assembly Language) −Second Stage of Boot Sequence(Assembly + C Language)
記事全体を表示
For long I looked for a working tutorial to build Qt5 with YOCTO (Yocto Training - HOME) both the libraries for the board image and also a toolchain to build Qt5 applications for the board. See the full tutorial here: Building Qt5 using yocto on Wandboard - Wandboard Wiki The Tutorial is written for the Wandboard that also uses an i.MX6 CPU but you can adapt the tutorial for most of the boards of the i.MX6 family I think - in my case it worked with the i.MX6 SABRE AI without problems. You only have to adjust the sysroot and maybe also the toolchain-path because the wiki entry is a little bit older Ask your questions for this topic - maybe I can help.
記事全体を表示
Introduction This is a sharing of my experience about porting the audio codec WM8960 in Linux BSP. I know this driver is not the perfect one.  If you find any place is not good in the driver, please let me know. This driver is modified base on the wm8960.c in L3.0.35 Linux BSP. This document is talking about how to modify the codec driver. The Audio Codec driver is located in linux/sound/soc/codec/wm8960.c. ALSA The Audio Codec driver is based on ALSA to setup up all the things. For details, please see : AlsaProject Advanced Linux Sound Architecture - Wikipedia, the free encyclopedia. kcontrols are defined in linux/include/sound/soc.h and soc-dapm.h. Audio controls and path in WM8960 Left and Right Input signal path Output signal path Base on the input and output signal diagrams, we can setup all the controls that we want in the driver. Such as switches, volume controls, PGA controls and so on. All the controls below can be used in the alsamixer. static const struct snd_kcontrol_new wm8960_snd_controls[] = { SOC_DOUBLE_R_TLV("PCM DAC Playback Volume", WM8960_LDAC, WM8960_RDAC, 0, 255, 0, dac_tlv), //LDACVOL , RDACVOL SOC_DOUBLE_R_TLV("PCM ADC Capture Volume", WM8960_LADC, WM8960_RADC, 0, 255, 0, adc_tlv), //LADCVOL, RADCVOL SOC_DOUBLE_R_TLV("Headphone Volume", WM8960_LOUT1, WM8960_ROUT1, 0, 127, 0, out_tlv), SOC_DOUBLE_R("Headphone ZC Switch", WM8960_LOUT1, WM8960_ROUT1,    7, 1, 0), SOC_DOUBLE_R_TLV("Speaker Volume", WM8960_LOUT2, WM8960_ROUT2, 0, 127, 0, out_tlv), SOC_DOUBLE_R("Speaker ZC Switch", WM8960_LOUT2, WM8960_ROUT2, 7, 1, 0), SOC_DOUBLE_R("Capture Volume ZC Switch", WM8960_LINVOL, WM8960_RINVOL, 6, 1, 0), SOC_SINGLE_TLV("Input Volume of LINPUT1", WM8960_LINVOL, 0, 63, 0, in_tlv),  //LINVOL SOC_SINGLE_TLV("Input Volume of RINPUT1", WM8960_RINVOL, 0, 63, 0, in_tlv),  //RINVOL SOC_SINGLE_TLV("Input Boost Volume LINPUT3", WM8960_INBMIX1, 4, 7, 0, boost_tlv),    //RIN3BOOST SOC_SINGLE_TLV("Input Boost Volume LINPUT2", WM8960_INBMIX1, 1, 7, 0, boost_tlv),    //RIN2BOOST SOC_SINGLE_TLV("Input Boost Volume RINPUT3", WM8960_INBMIX2, 4, 7, 0, boost_tlv),    //LIN3BOOST SOC_SINGLE_TLV("Input Boost Volume RINPUT2", WM8960_INBMIX2, 1, 7, 0, boost_tlv),    //LIN2BOOST SOC_SINGLE_TLV("PGA LB2LOVOL-Bypass from Left Boost", WM8960_BYPASS1, 4, 7, 1, bypass_tlv),    //LB2LOVOL SOC_SINGLE_TLV("PGA LI2LOVOL-Bypass from LINPUT3", WM8960_LOUTMIX, 4, 7, 1, bypass_tlv),    //LI2LOVOL SOC_SINGLE_TLV("PGA RB2ROVOL-Bypass from Right Boost", WM8960_BYPASS2, 4, 7, 1, bypass_tlv),    //RB2ROVOL SOC_SINGLE_TLV("PGA RI2ROVOL-Bypass from RINPUT3", WM8960_ROUTMIX, 4, 7, 1, bypass_tlv),    //RI2ROVOL SOC_SINGLE("Capture Mute (Left)", WM8960_LINVOL, 7, 1, 0), // LINMUTE SOC_SINGLE("Capture Mute (Right)", WM8960_RINVOL, 7, 1, 0), // RINMUTE SOC_SINGLE("PCM Playback -6dB Switch", WM8960_DACCTL1, 7, 1, 0), SOC_SINGLE("Speaker DC gain", WM8960_CLASSD3, 3, 5, 0), SOC_SINGLE("Speaker AC gain", WM8960_CLASSD3, 0, 5, 0), SOC_ENUM("ADC Polarity", wm8960_enum[0]), SOC_SINGLE("ADC High Pass Filter Switch", WM8960_DACCTL1, 0, 1, 0), SOC_ENUM("DAC Polarity", wm8960_enum[2]), SOC_SINGLE_BOOL_EXT("DAC Deemphasis Switch", 0, wm8960_get_deemph, wm8960_put_deemph), SOC_ENUM("3D Filter Upper Cut-Off", wm8960_enum[2]), SOC_ENUM("3D Filter Lower Cut-Off", wm8960_enum[3]), SOC_SINGLE("3D Depth", WM8960_3D, 1, 15, 0), SOC_SINGLE("3D", WM8960_3D, 0, 1, 0), SOC_ENUM("ALC Function", wm8960_enum[4]), SOC_SINGLE("ALC Max Gain", WM8960_ALC1, 4, 7, 0), SOC_SINGLE("ALC Target", WM8960_ALC1, 0, 15, 1), SOC_SINGLE("ALC Min Gain", WM8960_ALC2, 4, 7, 0), SOC_SINGLE("ALC Hold Time", WM8960_ALC2, 0, 15, 0), SOC_ENUM("ALC Mode", wm8960_enum[5]), SOC_SINGLE("ALC Decay", WM8960_ALC3, 4, 15, 0), SOC_SINGLE("ALC Attack", WM8960_ALC3, 0, 15, 0), SOC_SINGLE("Noise Gate Threshold", WM8960_NOISEG, 3, 31, 0), SOC_SINGLE("Noise Gate Switch", WM8960_NOISEG, 0, 1, 0), SOC_ENUM("Capture Left Boost", wm8960_enum[6]), //LMICBOOST SOC_ENUM("Capture Right Boost", wm8960_enum[7]), //RMICBOOT }; 1. SOC_SINGLE(xname, reg, shift, max, invert) To setup a simple switch, we can use SOC_SINGLE. e.g SOC_SINGLE("PCM Playback -6dB Switch", WM8960_DACCTL1, 7, 1, 0), - The name of this control is “PCM Playback -6dB Switch”. - The register in WM8960 is WM8960_DACCTL1 . (the register address is 0x5, defined in wm8960.h) - ‘7’ : The 7th bit in DACCTL1 register is used to enable/disable the DAC 6dB Attenuate. - ‘1’ : Only one enable or disable option. - ‘0’ : the value you set is not inverted. 2. SOC_SINGLE_TLV(xname, reg, shift, max, invert, tlv_array) To setup a switch with levels, we can use SOC_SINGLE_TLV. e.g. In this example, the left input volume control is from 000000(-17.25dB) to 111111(+30dB). Each step is 0.75dB. Total is 63 steps. SOC_SINGLE_TLV("Input Volume of LINPUT1", WM8960_LINVOL, 0, 63, 0, in_tlv), The scale of in_tlv declare like this: static const DECLARE_TLV_DB_SCALE(in_tlv, -1725, 75, 0); in_tlv : the name of the scale. -1725 : start from -17.25dB 75: each step is 0.75dB 0: the step is start from 0. For some volume control case the first step is "mute", then the step is start from 1 so change this number to 1. for example: The 0000 0000 of the DAC volume control is digital mute. static const DECLARE_TLV_DB_SCALE(dac_tlv, -12700, 50, 1); 3. SOC_DOUBLE_R(xname, reg_left, reg_right, xshift, xmax, xinvert) SOC_DOUBLE_R is a stereo version of SOC_SINGLE. You can control the left and right channel at the same time. e.g. SOC_DOUBLE_R("Headphone ZC Switch", WM8960_LOUT1, WM8960_ROUT1, 7, 1, 0), 4. SOC_DOUBLE_R_TLV(xname, reg_left, reg_right, xshift, xmax, xinvert, tlv_array) SOC_DOUBLE_R_TLV is the stereo version of SOC_SINGLE_TLV. e.g. SOC_DOUBLE_R_TLV("PCM DAC Playback Volume", WM8960_LDAC, WM8960_RDAC, 0, 255, 0, dac_tlv), 5. SOC_ENUM_SINGLE(xreg, xshift, xmax, xtexts) When the control option are some texts, we can use SOC_ENUM to enum the options. e.g. MIC boost 5.1. setup the array for the texts. static const char *wm8960_micboost[] = {"0dB","+13dB","+20dB","+29dB"}; 5.2. use the SOC_ENUM_SINGLE. static const struct soc_enum wm8960_enum[] = {      SOC_ENUM_SINGLE(WM8960_DACCTL1, 5, 4, wm8960_polarity),      SOC_ENUM_SINGLE(WM8960_DACCTL2, 5, 4, wm8960_polarity),      SOC_ENUM_SINGLE(WM8960_3D, 6, 2, wm8960_3d_upper_cutoff),      SOC_ENUM_SINGLE(WM8960_3D, 5, 2, wm8960_3d_lower_cutoff),      SOC_ENUM_SINGLE(WM8960_ALC1, 7, 4, wm8960_alcfunc),      SOC_ENUM_SINGLE(WM8960_ALC3, 8, 2, wm8960_alcmode),      SOC_ENUM_SINGLE(WM8960_LINPATH, 4, 4, wm8960_micboost),      SOC_ENUM_SINGLE(WM8960_RINPATH, 4, 4, wm8960_micboost), }; 5.3.  use SOC_ENUM to add the controls for MIC boost. SOC_ENUM("Capture Left Boost", wm8960_enum[6]), SOC_ENUM("Capture Right Boost", wm8960_enum[7]), After created all the controls, we can start to create the switches. The following switches created base on the input and output diagrams. I used the same name from datasheet of each switch. It will more easy to find out the proper switch in alsamixer. static const struct snd_kcontrol_new wm8960_lin[] = { SOC_DAPM_SINGLE("<- LMP2", WM8960_LINPATH, 6, 1, 0), //LMP2 SOC_DAPM_SINGLE("<- LMP3", WM8960_LINPATH, 7, 1, 0), //LMP3 SOC_DAPM_SINGLE("<- LMN1", WM8960_LINPATH, 8, 1, 0), //LMN1 }; static const struct snd_kcontrol_new wm8960_lin_boost[] = { SOC_DAPM_SINGLE("<- LMIC2B", WM8960_LINPATH, 3, 1, 0), //LMIC2B }; static const struct snd_kcontrol_new wm8960_rin[] = { SOC_DAPM_SINGLE("<- RMP2", WM8960_RINPATH, 6, 1, 0), //RMP2 SOC_DAPM_SINGLE("<- RMP3", WM8960_RINPATH, 7, 1, 0), //RMP3 SOC_DAPM_SINGLE("<- RMN1", WM8960_RINPATH, 8, 1, 0), //RMN1 }; static const struct snd_kcontrol_new wm8960_rin_boost[] = { SOC_DAPM_SINGLE("<- RMIC2B", WM8960_RINPATH, 3, 1, 0), //RMIC2B }; static const struct snd_kcontrol_new wm8960_loutput_mixer[] = { SOC_DAPM_SINGLE("<- LD2LO", WM8960_LOUTMIX, 8, 1, 0), //LD2LO SOC_DAPM_SINGLE("<- LI2LO", WM8960_LOUTMIX, 7, 1, 0), //LI2LO SOC_DAPM_SINGLE("<- LB2LO", WM8960_BYPASS1, 7, 1, 0), //LB2LO }; static const struct snd_kcontrol_new wm8960_routput_mixer[] = { SOC_DAPM_SINGLE("<- RD2RO", WM8960_ROUTMIX, 8, 1, 0), //RD2RO SOC_DAPM_SINGLE("<- RI2RO", WM8960_ROUTMIX, 7, 1, 0), //RI2RO SOC_DAPM_SINGLE("<- RB2RO", WM8960_BYPASS2, 7, 1, 0), //RB2RO }; static const struct snd_kcontrol_new wm8960_mono_out[] = { SOC_DAPM_SINGLE("<- L2MO", WM8960_MONOMIX1, 7, 1, 0), //L2MO SOC_DAPM_SINGLE("<- R2MO", WM8960_MONOMIX2, 7, 1, 0), //R2MO }; Then, create the inputs, ADC, DAC, mixers, PGA and outputs. static const struct snd_soc_dapm_widget wm8960_dapm_widgets[] = { SND_SOC_DAPM_INPUT("LINPUT1"), SND_SOC_DAPM_INPUT("RINPUT1"), SND_SOC_DAPM_INPUT("LINPUT2"), SND_SOC_DAPM_INPUT("RINPUT2"), SND_SOC_DAPM_INPUT("LINPUT3"), SND_SOC_DAPM_INPUT("RINPUT3"), SND_SOC_DAPM_MICBIAS("MICB", WM8960_POWER1, 1, 0), SND_SOC_DAPM_MIXER("Left Boost Mixer", WM8960_POWER1, 5, 0, wm8960_lin_boost, ARRAY_SIZE(wm8960_lin_boost)), SND_SOC_DAPM_MIXER("Right Boost Mixer", WM8960_POWER1, 4, 0, wm8960_rin_boost, ARRAY_SIZE(wm8960_rin_boost)), SND_SOC_DAPM_MIXER("Left Input PGA", WM8960_POWER3, 5, 0, wm8960_lin, ARRAY_SIZE(wm8960_lin)), SND_SOC_DAPM_MIXER("Right Input PGA", WM8960_POWER3, 4, 0, wm8960_rin, ARRAY_SIZE(wm8960_rin)), SND_SOC_DAPM_ADC("Left ADC", "Capture", WM8960_POWER1, 3, 0), SND_SOC_DAPM_ADC("Right ADC", "Capture", WM8960_POWER1, 2, 0), SND_SOC_DAPM_DAC("Left DAC", "Playback", WM8960_POWER2, 8, 0), SND_SOC_DAPM_DAC("Right DAC", "Playback", WM8960_POWER2, 7, 0), SND_SOC_DAPM_MIXER("Left Output Mixer", WM8960_POWER3, 3, 0, wm8960_loutput_mixer, ARRAY_SIZE(wm8960_loutput_mixer)), SND_SOC_DAPM_MIXER("Right Output Mixer", WM8960_POWER3, 2, 0, wm8960_routput_mixer, ARRAY_SIZE(wm8960_routput_mixer)), SND_SOC_DAPM_PGA("Left HP PGA", WM8960_POWER2, 6, 0, NULL, 0), SND_SOC_DAPM_PGA("Right HP PGA", WM8960_POWER2, 5, 0, NULL, 0), SND_SOC_DAPM_PGA("Left Speaker PGA", WM8960_POWER2, 4, 0, NULL, 0), SND_SOC_DAPM_PGA("Right Speaker PGA", WM8960_POWER2, 3, 0, NULL, 0), SND_SOC_DAPM_PGA("Right Speaker Output", WM8960_CLASSD1, 7, 0, NULL, 0), //SPK_OP_EN SND_SOC_DAPM_PGA("Left Speaker Output", WM8960_CLASSD1, 6, 0, NULL, 0), SND_SOC_DAPM_OUTPUT("SPK_LP"), SND_SOC_DAPM_OUTPUT("SPK_LN"), SND_SOC_DAPM_OUTPUT("HP_L"), SND_SOC_DAPM_OUTPUT("HP_R"), SND_SOC_DAPM_OUTPUT("SPK_RP"), SND_SOC_DAPM_OUTPUT("SPK_RN"), SND_SOC_DAPM_OUTPUT("OUT3"), }; Now, we can start to route the audio path. The path is from right to left , like : { “destination”, “switch”, “source” } So, lets take the LINPUT1 to ADC as an example: { "Left Input PGA", "<- LMN1", "LINPUT1" }, { "Left Boost Mixer", "<- LMIC2B", "Left Input PGA" }, { "Left ADC", NULL, "Left Boost Mixer" }, Another example is DAC to Headphone.                 { "Left Output Mixer", "<- LD2LO", "Left DAC" },                 { "Right Output Mixer", "<- RD2RO", "Right DAC" },                 { "Left HP PGA", NULL, "Left Output Mixer" },                 { "Right HP PGA", NULL, "Right Output Mixer" },                 { "HP_L", NULL, "Left HP PGA" },                 { "HP_R", NULL, "Right HP PGA" }, In linux, you can run "alsamixer" to turn on/off the switches and adjust the volumes. (this picture is an example of alsamixer of other codec, not for wm8960) In alsamixer, use 'M' to turn the switch on/off,  use arrow keys to control the volumes. wm8960_dai_ops is another important part in the driver. Here is the ops of the wm8960_dai. static struct snd_soc_dai_ops wm8960_dai_ops = {                 .hw_params = wm8960_hw_params,                 .digital_mute = wm8960_mute,                 .set_fmt = wm8960_set_dai_fmt,                 .set_clkdiv = wm8960_set_dai_clkdiv,                 .set_pll = wm8960_set_dai_pll, }; wm8960_hw_params : used to set the PCM format (16bit/24bit), set the deemph, alc_rates and etc. wm8960_mute:  used to mute the output wm8960_set_dai_fmt : used to set the Master/Slave mode, set the interface format (I2S, DSP, Left justified and Right justified) and set the clock inversion. wm8960_set_dai_clkdiv: used to set the CLK divider such as DACDIV, ADCDIV, BCLKDIV and so on. wm8960_set_dai_pll: used to calculate the proper PLL values. In the wm8960_set_dai_pll, we need to calculate the proper PLL values. Base on the table, if the MCLK >14.4, the sysclk prescale divider is 2. So, set the sysclk pre-divider to 2 before finding pll_factors. if (freq_in > 15000000 ) {                                 /* update sysclk div */                                 reg = snd_soc_read(codec, WM8960_CLOCK1) & 0x1f9;                                 snd_soc_write(codec, WM8960_CLOCK1, reg | 0x4);                                 clk_in = clk_in/2;                                 }                 if (freq_in && freq_out) {                                 ret = pll_factors(clk_in, freq_out, &pll_div);                                 if (ret != 0)                                                 return ret;                 } In the driver, there are two names are important. One is the name of codec dai. The name is “wm8960”. Make sure this codec dai name is the same codec dai name used in the imx-wm8960.c. static struct snd_soc_dai_driver wm8960_dai = {                 .name = "wm8960",                 .playback = {                                 .stream_name = "Playback",                                 .channels_min = 1,                                 .channels_max = 2,                                 .rates = WM8960_RATES,                                 .formats = WM8960_FORMATS,},                 .capture = {                                 .stream_name = "Capture",                                 .channels_min = 1,                                 .channels_max = 2,                                 .rates = WM8960_RATES,                                 .formats = WM8960_FORMATS,},                 .ops = &wm8960_dai_ops,                 .symmetric_rates = 1, }; Another name is the I2C device id. Make sure the I2C name is same as the name used in your_board.c file. static const struct i2c_device_id wm8960_i2c_id[] = {                 { "wm8960", 0 },                 { } }; MODULE_DEVICE_TABLE(i2c, wm8960_i2c_id); static struct i2c_driver wm8960_i2c_driver = {                 .driver = {                                 .name = "wm8960",                                 .owner = THIS_MODULE,                 },                 .probe =    wm8960_i2c_probe,                 .remove =   __devexit_p(wm8960_i2c_remove),                 .id_table = wm8960_i2c_id, }; Here is the name used in your_board.c static struct i2c_board_info mxc_i2c0_board_info[] __initdata = {     {         I2C_BOARD_INFO("wm8960", 0x1a),     }, } Machine driver imx-wm8960.c Basically, the machine driver is the connection between wm8960.c and the i.MX. It is modified base on the imx-wm8962.c. I didn't add the HP and MIC detection in this driver. If you need the HP and MIC detection, please take the imx-wm8962.c for reference. Here is an example of my_board.c. The following platform data pass to the machine driver from my board. static struct platform_device audio_wm8960_device = {     .name = "imx-wm8960", }; static struct mxc_audio_platform_data wm8960_pdata; static int wm8960_clk_enable(int enable) {     if (enable)         clk_enable(clko);     else         clk_disable(clko);     return 0; } static int mxc_wm8960_init(void) {     int rate;     clko = clk_get(NULL, "clko_clk");     if (IS_ERR(clko)) {         pr_err("can't get CLKO clock.\n");         return PTR_ERR(clko);     }     /* both audio codec and comera use CLKO clk*/     rate = clk_round_rate(clko, 24000000);     clk_set_rate(clko, rate);     wm8960_pdata.sysclk = rate;     return 0; } static struct mxc_audio_platform_data wm8960_pdata = {     .ssi_num = 1,     .src_port = 2,     .ext_port = 3,     .init = mxc_wm8960_init,     .clock_enable = wm8960_clk_enable, }; I attach the driver and the machine driver here. I hope this document is useful for you.
記事全体を表示
Attached is the U-boot binary needed to construct the following image: i.MX 6Dual/6Quad Power Consumption Measurement Linux Image
記事全体を表示
In our reference design board the eMMC IC is Sandisk SDIN5C2-8 (4.41), and in i.MX6 Reference manual and datasheet we can known that it compatible with the MMC System Specification version 4.2/4.3/4.4, and details in datasheet declare that the uSDHC module is "fully compliant with the MMC command/response sets and Physical Layer as defined in the Multimedia Card System Specification, v4.2/4.3/4.4/4.41, including high-capacity (> 2 GB) HC MMC cards." EMMC4.4/4.41 of cause can work in our released BSP. But eMMC 4.4 has been discontinued and there is a possibility eMMC 4.41 will be discontinued.  And many of our customers will choose the eMMC 4.5 or high verison EMMC 5.0 and EMMC 5.1. And how to make the eMMC 4.5 , EMMC 5.0 and EMMC 5.1 work on i.MX6 ? The EMMC 4.5 or EMMC 5.0 /5.1 is backward-compatible with eMMC4.4, we can use it in eMMC4.4 mode to enable eMMC4.4 functionality and performance on the i.MX6 platform. Booting from a eMMC 4.5 device or high version is not supported,  boot ROM will fall back to the eMMC4.4 standard when a eMMC4.5 or high version capable device is detected. In BSP it is possible to bypass eMMC version checking, so that eMMC v4.5 or high version can work as eMMC v4.4 cards, no specific v4.5 feature supported. Only basic read/write operations are supported. In the source code we can change check value of card->ext_csd.rev. Take the eMMC 4.5 work as example, the current i.MX6 Linux BSP (L3.0.35_4.1.0) has added code to interface with an eMMC4.5 card to operate as an eMMC4.4 card. Change the value of card->ext_csd.rev 5 to 6, now eMMC 5.0 can work as an eMMC 4.4. The code drivers/mmc/core/mmc.c: And for the EMMC 5.0 and EMMC5.1, modify the kernel to support eMMC 5.0 and 5.1 extended CSD revisions, as shown below: /drivers/mmc/core/mmc.c : if (card->ext_csd.rev > 6) {              // The '6' has to be replaced with '7' For EMMC5.0                                                         //  The '6' has to be replaced with '8'  For EMMC5.1 pr_err("%s: unrecognised EXT_CSD revision %d\n", mmc_hostname(card->host), card->ext_csd.rev); err = -EINVAL; goto out;          } After modifying the code we need to rebuild the the firmware uImage used for MfgTool . Update the uImage in Mfgtool , and it can flash successful. Then the eMMC version 5.0 and 5.1 can be used with IMX6 based boards.
記事全体を表示
Getting started with Linux on the i.MX53QSB
記事全体を表示
Hi All, The new Android JB4.3_1.1.0-GA release is now available on www.freescale.com ·         Files available           Name Description IMX6_JB43_110_ANDROID_DOCS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Android   jb4.3_1.1.0 BSP Documentation. Includes Release Notes, User's Guide, QSG and   FAQ Sheet. IMX6_JB43_110_ANDROID_SOURCE_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Android   jb4.3_1.1.0 BSP, Documentation and Source Code for BSP and Codecs. IMX6_JB43_110_ANDROID_DEMO_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Android   jb4.3_1.1.0  BSP Binary Demo Files IMX6_JB43_110_AACP_CODEC_CODA AAC   Plus Codec for i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX   6Sololite Android jb4.3_1.1.0 ·         Target HW boards o   i.MX6DL  SABRE SD board o   i.MX6Q  SABRE SD board o   i.MX6DQ SABRE AI board o   i.MX6DL SABRE AI board o   i.MX6SL EVK board ·         Release Description i.MX Android jb4.3_1.1.0 release includes all necessary codes, documents and tools to assist users in building and running Android 4.3 on the i.MX 6Quad, i.MX 6DualLite and i.MX6SoloLite hardware board from the scratch. The prebuilt images are also included for a quick trial on Freescale i.MX 6Quad and i.MX 6DualLite SABRE-SD Board and Platform, i.MX 6Quad and i.MX 6DualLite SABRE-AI Board and Platforms and i.MX6SoloLite EVK Board and Platforms. This release includes all Freescale porting and enhancements based on Android open source code. Most of deliveries in this release are provided in source code with the exception of some proprietary modules/libraries from third parties. ·         What's in this release         Android Source Code Patch All   Freescale i.MX specific patches (apply to Google Android repo)   to enable Android on i.MX based boards. For example Hardware   Abstraction Layer implementation, hardware codec acceleration,   etc. Packed in   android_jb4.3_1.1.0-ga_source.tar.gz Documents The   following documents are included in android_jb4.3_1.1.0-ga_docs.tar.gz: ●   i.MX Android jb4.3_1.1.0-ga Quick Start: A   manual explains how to run android on i.MX board by using prebuilt images. ●   i.MX Android jb4.3_1.1.0-ga User Guide: A   detailed manual for this release package. ●   i.MX Android jb4.3_1.1.0-ga FAQ: A document lists   “Frequently Asked Questions”. ●   i.MX Android Codec Release Notes: A   document to describes the Freescale Codec Package ●   i.MX Android Wi-FI Display Sink API Introduction A   document to describes how to use i.MX Android Wi-Fi Display Sink API ●   i.MX6 G2D API User Guide document to introduce how to use i.MX6 G2D API for   2D BLT usage ●   i.MX Android jb4.3_1.1.0-ga Release Note A   document to introduce the key updates and known issues in this release. Tools Tools   in android_jb4.3_1.1.0-ga_tools.tar.gz ●  MFGTool. Manufacturing tools for i.MX platform ●  USB tethering windows .inf driver configure file.tool/tetherxp.inf Prebuilt Images You   can test Android on i.MX with prebuilt image on i.MX board before building   any code. ● android_jb4.3_1.1.0-ga_image_6qsabresd.tar.gz: Prebuilt   images for the SABRE-SD board. ●  android_jb4.3_1.1.0-ga_image_6qsabreauto.tar.gz: Prebuilt   images for the SABRE-AI board. ●  android_jb4.3_1.1.0-ga_image_6slevk.tar.gz: Prebuilt images for the 6SL   SABRE-AI board. All   prebuilt images are in another package. See "i.MX Android jb4.3_1.1.0-ga   Quick Start" and "i.MX Android jb4.3_1.1.0-ga User Guide" to   understand which image should be used in which case. ·         Known issues For known issues and limitations please consult the release notes
記事全体を表示
Q:Is there an issue using odd DIV_SELECT values? When setting the CPU clock (maybe others also) in uboot, the code will only use even valuesfor the DIV_SELECT field. There is nothing in the Reference Manual or Errata that indicates only even values can be used for this field. There were 2 SR's that had conflicting answers and we are trying to determine what can be used. The CPU freq setting trying to be achieved is 996MHz. With a 24MHz source, you need 24MHz x 41.5 = 996MHz. Since the DIV_SELECT is x2, a value of 83 would be needed. A: Below is the DIV_SELECT description of ARM PLL, since the Fin is 24MHz, so there is no odd issue of DVI_SELECT, as 24 / 2 = 12MHz. Such as for 996M, this value is 83, that is fine. "This field controls the pll loop divider. Valid range for divider value: 54-108. Fout = Fin * div_select/2.0." This document was generated from the following discussion: mx6Q PLL Setting
記事全体を表示
SABRE-AI Development Platform bulletin on Touch Interrupt
記事全体を表示
Overview The purpose of this document is to collect general information about PCIe certificaton (Tx only) on i.MX 7Dual SabreSD board. Test Procedure Please refer to "PCIe Certification Guide for i.MX 7Dual" for more details about test procedure. Software Configuration PCIe certificaiton requires PCIe module to keep clocks always on. So software needs to enable "CONFIG_PCI_IMX6_COMPLIANCE_TEST" by default for the certification. Appropriative PCIe reference clock generator is recommended for certification. i.MX differential clock is not compliant with PCIe standard. So external reference clock is recommended for PCIe certification. i.MX 7Dual SabreSD board enables external reference clock by default and  and i.MX 7Dual default BSP has also adopted external reference clock as PCIe clock source by default. Test Report Please see attachment for i.MX 7Dual PCIe certification test report for Tx based on the following configuration: Software Image: L4.1.15_1.2.0_ga internal candidate image with enabling CONFIG_PCI_IMX6_COMPLIANCE_TEST configuration for Kernel image. Hardware: i.MX 7Dual SabreSD board.
記事全体を表示
The attched package includes mbedTLS and CAAM driver based on SDK2.2, you can apply it on Windows Installer: MCUXpresso SDK2.2 for i.MX 6UltraLite 1. fsl_caam.c and fsl_caam.h under devices\MCIMX6G3\drivers is CAAM driver. 2. Some files under middleware\mbedtls-2.4.0\port\sdk are porting code for mbedTLS 3. Example codes are under folder boards\evkmcimx6ul which have driver example and mbedTLS example. 4, The patch package only support IAR toolchain. 5, Due to SDK don't support allocation of non-cachable memory dynamically, so some static non-cachable bufferes in sdk_mbedtls.c is used for shared memory with hareware. So mbedTLS don't be used for multi-thread concurrently.
記事全体を表示
[中文翻译版] 见附件   原文链接: Enable GmSSL which supports OSCCA Algorithm Toolbox on i.MX 
記事全体を表示
Installing OpenOCD and GDB i.MX27 This tutorial was tested on i.MX27ADS REV. 2.6 and may not work on other board revision. Step 0: Installing the FTDI library The libFTDI is necessary when using JTAG based on FT2232 or others FTDI chips. LibFTDI need libusb, then install it first: $ sudo apt-get install libusb-dev Download libftdi from http://www.intra2net.com/en/developer/libftdi: $ wget http://www.intra2net.com/en/developer/libftdi/download/libftdi-0.18.tar.gz Now decompress and install it: $ tar zxvf libftdi-0.18.tar.gz $ ./configure $ make $ sudo make install Step 1: Compiling OpenOCD To compile OpenOCD you need to have GCC, Autoconf and automake installed. Get the OpenOCD source code (we are using rev. 1083): svn checkout http://svn.berlios.de/svnroot/repos/openocd/trunk openocd --revision 1399 Create the configure file and Makefile.in: $ ./bootstrap Run configure: $ ./configure --enable-ft2232_libftdi Compile: $ make Install it: $ sudo make install Step 2: Initializing OpenOCD Connect your JTAG interface on computer and i.MX27ADS board. Run OpenOCD passing as parameter the processor config and JTAG interface config: $ sudo openocd -f interface/myinterface.cfg -f board/imx27ads.cfg Replace myinterface.cfg by jtag interface you are using. In our case we are using Signalyzer Jtag Interface: $ sudo openocd -f interface/signalyzer.cfg -f board/imx27ads.cfg Note: We need to add "jtag_speed 5" on signalyzer.cfg in order to it works on i.MX27ADS. You will see this init message: # openocd -f interface/signalyzer.cfg -f board/imx27ads.cfg Open On-Chip Debugger 1.0 (2009-03-06-08:47) svn:1399 BUGS? Read http://svn.berlios.de/svnroot/repos/openocd/trunk/BUGS $URL: http://svn.berlios.de/svnroot/repos/openocd/trunk/src/openocd.c $ jtag_speed: 5 dcc downloads are enabled Info : JTAG tap: imx27.bs tap/device found: 0x1b900f0f (Manufacturer: 0x787, Part: 0xb900, Version: 0x1) Info : JTAG Tap/device matched Info : JTAG tap: imx27.cpu tap/device found: 0x07926121 (Manufacturer: 0x090, Part: 0x7926, Version: 0x0) Info : JTAG Tap/device matched Warn : no telnet port specified, using default port 4444 Warn : no gdb port specified, using default port 3333 Warn : no tcl port specified, using default port 6666 Step 3: Creating an ARM GDB tool If you already have an arm-elf-gdb then skip this step, otherwise go on. To create an arm GDB enter on LTIB -> Package List and select this: [*] gdb [ ]   gdb to run natively on the target [*]   cross gdb (runs on build machine) It will create the ARM GDB file at ~/ltib-dir/bin/gdb $ cd /home/alan/ltib-imx27ads-20071219/bin Copy this gdb binary to /usr/bin renaming it to arm-elf-gdb: $ sudo cp gdb /usr/bin/arm-elf-gdb Step 4: Debugging an application You can test the ledtest application to i.MX27ADS supplied by OpenOCD: Enter in ledtest directory: $ cd openocd/testing/examples/ledtest-imx27ads Run arm-elf-gdb passing as argument the gdbinit_imx27ads file: $ arm-elf-gdb --command=gdbinit-imx27ads You will see this gdb message: $ arm-elf-gdb --command=gdbinit_imx27ads GNU gdb 6.6 Copyright (C) 2006 Free Software Foundation, Inc. GDB is free software, covered by the GNU General Public License, and you are welcome to change it and/or distribute copies of it under certain conditions. Type "show copying" to see the conditions. There is absolutely no warranty for GDB.  Type "show warranty" for details. This GDB was configured as "--host=i686-pc-linux-gnu --target=arm-linux". Setting up for the Freescale iMX27 ADS Board. The target endianness is set automatically (currently little endian) The target may not be able to correctly handle a memory-write-packet-size of 1024 bytes. Change the packet size? (y or n) [answered Y; input not from terminal] 0xc0000260 in ?? () JTAG device found: 0x1b900f0f (Manufacturer: 0x787, Part: 0xb900, Version: 0x1) JTAG device found: 0x07926121 (Manufacturer: 0x090, Part: 0x7926, Version: 0x0) target state: halted target halted in ARM state due to debug-request, current mode: Supervisor cpsr: 0x200000d3 pc: 0xc0000264 MMU: disabled, D-Cache: disabled, I-Cache: disabled Loading section .text, size 0x13c lma 0xa0000000 Start address 0xa0000000, load size 316 Transfer rate: 45963 bits/sec, 316 bytes/write. Warning: the current language does not match this frame. Breakpoint 1 at 0xa000008c: file test.c, line 12.  Breakpoint 1, main () at test.c:12 12                    volatile unsigned char *ledoff = ((volatile unsigned char *)0xD4000008); (arm-gdb) Now issue continue (or just c) command and you will see D30 LED blinking! (arm-gdb) c Continuing. You can repeat this test and issue next (or just n) to debugging line by line then you can see the LED turning on and off. Using step (or just s) is not a good option because it will spend much time on for loop.
記事全体を表示
The i.MX 6 D/Q L3.035_1.1.3 patch release is now available on the www.freescale.com ·         Files available # Name Description 1 L3.0.35_1.1.3_TEMP_PATCH This patch release is based on the i.MX 6Dual/6Quad Linux   L3.0.35_1.1.0 release. The purpose of this patch release is fix the   miscalibration issue for the thermal sensor.
記事全体を表示
Product Family Features The i.MX6 series unleashes the industry’s first truly scalable multicore platform that includes single-, dual- and quad-core families based on the ARM® Cortex™-A9 architecture. Together with a robust ecosystem, i.MX6 series provides the ideal platform to develop a portfolio of end devices based on a single hardware design. With high-performance multimedia processing, pin*- and software- compatible product families and integrated power management, i.MX6 series is purpose built for the new era of smart devices. *4 of 5 families are pin-compatible The i.MX6 applications processor is a Energy-Efficient Solutions products. Automotive As drivers adopt personal and home-based smart devices, automotive manufacturers are bringing a similar experience in-vehicle. Able to meet demands of connectivity, real time data delivery, digital instrumentation, audio and multi-stream video, i.MX 6 series enables auto infotainment and instrument cluster designers to re-create today’s consumer technology experience in the car. Smart Devices The market for intelligent, multimedia centric, touch based devices is increasing exponentially. Not just for tablets or smartphones anymore, tomorrow's battery powered Smart Devices, Aero Infotainment systems, medical systems, enterprise-class intelligent control and data systems all must present data and user interface choices to the end user primarily through rich sound, video, voice, pictures and touch, rather than keyboards and mice. i.MX 6 series enables developers to deliver a more seamless natural user interface (NUI) experience, plus save time and costs by leveraging one design across a portfolio of devices. i.MX 6 Series Portfolio View the complete i.MX 6 Series; compare features and performance   Product Information i.MX6DL: i.MX 6DualLite Family of Applications Processors i.MX6S: i.MX 6Solo Family of Applications Processors i.MX6D: i.MX 6Dual Family of Applications Processors i.MX6Q: i.MX 6Quad Family of Applications Processors i.MX6SL: i.MX 6SoloLite Family of Applications Processors Design Resources i.MX 6 Series Software and Development Tools i.MX 6SoloLite Evaluation Kit SABRE Platform for Smart Devices SABRE Board for Smart Devices SABRE for Automotive Infotainment i.MX 6 Family Ecosystem Partners Partners / 3rd-Party Development Tools Development platform for i.MX 6Quad - Built to SABRE Lite design from Element 14 Element14's SabreLite Board Officially Supported by Adeneo Embedded's i.MX6 WEC7 BSP Emtrion's i.MX6 DIMM Modules and Kits i.Core M6 : i.Mx6 based SOM Industry-First Pico-ITX SBC based on i.MX6 from iWave Systems i.MX6 Q7 Development Kit by iWave Systems New PMIC to Support the i.MX6 Processor Family NovPek i.MX6Q/D by NovTech Video- iWave Launches Industry's first i.MX6 Solo/Dual Lite Based Pico-ITX Single Board Computer i.MX6 Q7 Development Kit by iWave Systems The Wandboard - ultra lowcost development board with i.MX6 Cortex-A9 processor SABRE Lite by Boundary Devices Nitrogen6X by Boundary Devices Additional Resources i.MX6 (All) Tips & Tricks Android data partition encryption on i.MX6 Android Graphic UI with GPU Hardware Acceleration Auto Insmod Kernel Modules Through Modprobe with Extra Parameter A Patch to Fix i.MX6 GPU Startup Issue Due to Memory Connection Qt Landing page De-interlace Capture Device Enabling MMU and Caches on i.MX6 Series Platform SDK Errata_ERR006282_Description_IMX_Community.pdf Fast GPU Image Processing in the i.MX 6x Freescale Yocto Project main page Gstreamer HW Design Checklist for i.MX6 How to Add Ethernet UI Support in ICS How to Support New WiFi Card in Android How to Support Recovery Mode for POR Reboot Based on i.MX6 Android R13.4.1 How to Trace the Low-Level Malloc i.MX6 Crystal Drive Level (24 MHz) EB830 i.MX6 Android 13.4.1.03 Patch Release i.MX6 Dual/6 Quad Power Consumption Measurement Scripts i.MX6 IPU Output Timing Generation Counters and Interrupts i.MX6 Platform SDK 1.1 Release i.MX6 VDD_SNVS_CAP Component Recommendation Linux Fast Boot on i.MX6 Sabresd Board LMbench Benchmarks on i.MX New PMIC to Support the i.MX6 Processor Family Memory Management on i.MX6 Android Patch to Support BT656 and BT1120 Output For i.MX6 BSP Prevent PMIC PF0100 Backfeed on i.MX6 Designs Using a USB Camera with GStreamer VAR-SOM-MX6, $52 i.MX6 System on Module i.MX6D/6Q (Dual/Quad) Tips & Tricks De-interlace Capture Device Android Power Management on i.MX6DQ/DL Android Graphic UI with GPU Hardware Acceleration Memory Management on i.MX6 Android iMX6QD How to add 24-bit LVDS support in Android i.MX6 D/Q L3.035_1.0.2 Patch Release i.MX6 D/Q L3.0.35_1.0.3 patch release i.MX6 D/Q L3.035_1.1.3 patch release i.MX6Q Ubuntu Fluxbox Multimedia with VPU &amp; IPU HW Acceleration in Android Let Ubuntu NetworkManager Recognize BCM4330 Wireless Interface Auto Insmod Kernel Modules Through Modprobe with Extra Parameter Video Playback Performance Evaluation on i.MX6DQ Board Linux Fast Boot on i.MX6 Sabresd Board Linux Fast Boot on i.MX6Q Board: Building Steps New Ubuntu SD Card Demo Image for the i.MX6Q SABRE AI SDMA ap_to_ap Fixed Scripts (i.MX6DQ) Surround View Demo With Linux Fast Boot Review Surround View (D1) Demo on i.MX6 Test Digital Zoom of Camera Preview Using i.MX6Q to Build a Palm-Sized Heterogeneous Mini-HPC i.MX6DL (DualLite)  Tips & Tricks Android Power Management on i.MX6DQ/DL i.MX6 DL/S L3.035_3.0.4 patch release i.MX6SL (SoloLite)  Tips & Tricks Dithering Implementation for Eink Display Panel
記事全体を表示
i.MX6UL Hardware design checklist v0.1
記事全体を表示
Multiple-Overlay (or Multi-Overlay) means several video playbacks on a single screen. In case multiple screens are needed, check the dual-display case GStreamer i.MX6 Multi-Display $ export VSALPHA=1 $ SAMPLE1=sample1.avi; SAMPLE2=sample2.avi; SAMPLE3=sample3.avi; SAMPLE4=sample4.avi; $ WIDTH=320; HEIGHT=240; SEP=20 Four displays (2x2) $gst-launch \ playbin2 uri=file://`pwd`/$SAMPLE1 video-sink="mfw_isink axis-top=0 axis-left=0   disp-width=$WIDTH disp-height=$HEIGHT" \ playbin2 uri=file://`pwd`/$SAMPLE2 video-sink="mfw_isink axis-top=0 axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT" \ playbin2 uri=file://`pwd`/$SAMPLE3 video-sink="mfw_isink axis-top=`expr $HEIGHT + $SEP` axis-left=0   disp-width=$WIDTH disp-height=$HEIGHT" \ playbin2 uri=file://`pwd`/$SAMPLE4 video-sink="mfw_isink axis-top=`expr $HEIGHT + $SEP` axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT" Basic rotation, (2 x 1, normal and inverted) gst-launch \ playbin2 uri=file://`pwd`/$SAMPLE1 video-sink="mfw_isink axis-top=0 axis-left=0   disp-width=$WIDTH disp-height=$HEIGHT rotation=0" \ playbin2 uri=file://`pwd`/$SAMPLE2 video-sink="mfw_isink axis-top=`expr $HEIGHT + $SEP` axis-left=0 disp-width=$WIDTH disp-height=$HEIGHT rotation=3"
記事全体を表示