i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Question: In a single uImage to contain the compressed kernel and rootfs, if the uImage is greater than 16MB, the system will not boot and reports errors. Is there a size limitation on uImage?  If so, is there a work around? Answer: uImage should only contains kernel compressed. rootfs should be read through a linux partition after the kernel boots up. Regarding the uImage's size, there is no limitation. In the other hand, a single uImage with kernel and filesystem is needed; in other words, kernel (alias uImage) needs a filesystem to work, and these are two independent systems in that sense. If u-boot, kernel and filesystem are in a single device (SD Card), the filesystem must be mounted in the first partition (SD, eMMC, etc) starting somewhere > 16M/512 sectors. But in cases where: * A fast boot is needed with  very small rootfs * As a intermediate (temporal) rootfs  before switching  to the real rootfs. The usage (actually used when flashing with the MFG tool) of this intermediate system is to load heavy modules, keeping the uImage small. This mechanism is called initramfs and the uImage will contain the kernel and the this mini rootfs compressed as cpio archive. But there appears to be a 16MB limitation. See here:  http://www.isysop.com/unpacking-and-repacking-u-boot-uimage-files/ It seems to be related to alignment suggesting that 24-bit addressing is used instead of 32-bit.  I did notice Thumb mode is used, which seems odd to me.
View full article
THE CONTENTS •Background Knowledge −Kernel Introduction −Linux Kernel Directory Structure of the Source Code •Kernel Loading Procedure −Linux OS Boot Process −First Stage of Loading Sequence(Assembly Language) −Second Stage of Loading Sequence(C Language)
View full article
RedBoot is a bootloader, which contains support for some i.MX SoCs. Compiling RedBoot All Boards Compiling RedBoot Configuring RedBoot Configuring RedBoot All Boards Configuring RedBoot Loading Redboot Binary Directly to RAM Minicom Updating RedBoot Updating RedBoot Through RedBoot All Boards Updating RedBoot Through RedBoot IMX27 PDK NAND Flashing RedBoot i.MX31 PDK NAND Flashing RedBoot i.MX35 PDK NAND Flashing Kernel and Root File System Using RedBoot RedBoot Utilities All Boards Transfer Serial RedBoot Fixing Redboot RAM Bug Fixing Redboot RAM bug (CSD1 not activated)
View full article
Product Family Features Freescale's i.MX family of applications processors has demonstrated leadership in the portable handheld market. The i.MX21 multimedia applications processor is the latest addition to this family and builds on its low-power, high-performance heritage. Freescale has shipped more than 60 million chips of our industry-founding applications processors. That means you can start smart by picking products with a technology pedigree to handle all the creativity you can pump into them. The i.MX21 features the advanced and power-efficient ARM926EJ-S core operating at speeds starting at 266 MHz and is part of a growing family of Smart Speed products that offer high performance processing optimized for lowest power consumption. ARM926EJ-S™ core (16 KB I-Cache, 16 KB D-Cache) Smart Speed Switch 16/18-bit color LCD controller up to SVGA USB On-The-Go (two-host port) MPEG-4 and H.263 encode/decode acceleration up to CIF 30 fps Additional Resources IMX21-ADS I.MX21 ADS Board Flashing IMX21-and-iMXL-Lite-Kit
View full article
Flash a full SD Card Android Image (4GB) using Linux on VMWare Flash a full SD card image (4GB) using Flashnul in Windows Flash a full SD Card Android Image (4GB) using Linux on VMWare Note: It is preferred that SanDisk 4G SD card be used rather then Kingston. Kingston seemed to enumerate slightly smaller then SanDisk which actually inhibited us from flashing the image onto Kingston.    Within VMWare player, go to places/filesystems/dev to see what the SD card is called. When plugging in or removing the SD card from an external reader, you should see within the dev folder files called sdx…etc. [x= some letter]. That will help you specify which card to program with your image. Make note of the file [which is really a drive] name. For example in my VMWare player, it turns out that my SD card that I want to program was sdb. Also, if windows asks to format the drive, allow it and use Fat32. And, if you notice the drive is only 1GB instead of 3-4GB its because you only formatted the windows structure of the disk, the Linux portion that might reside on it does not show up in Windows. For distribution, the entire image which includes the *.bin file {this is the one you are trying to get onto the SD card} can be downloadable from a Freescale FTP site or some other media. It is a large file which is between 1-2GB. In this Android example, the file is called MasterA.gz. GZ is a linux based zip application which runs circles around winzip or 7-zip. The Android image, MasterA.gz, was 1.08 GB. The file you want to see in this example is MasterA.bin. Open a terminal window in VMWare. Within VMWare, unzip the file. If you select the file, then right mouse click it it will give you the option to uncompress using GZ. Before moving forward, make sure the SD card is unmounted. To do this type sudo umount /dev/sdX {note: sdb was the SD card we previously found enumerated}.           If you don’t know if it is mounted, in places/filesystems/dev on the left side of the screen you will see names with shown next to it. That means it’s          mounted. To copy Android image to sd card, type sudo dd if=masterA.bin of=/dev/sdX bs=10M X is the sd card (like /sdb, /sdc etc.) This will take some time, so if you have to stop this process hit <ctrl C> or close the terminal window. This will take some time but that’s all that it takes. Use the bottom task bar of the VMware screen, to attach the USB removable drive to Linux. Flash a full SD card image (4GB) using Flashnul in Windows  The tool you will use to flash the content is FlashNul in windows. This is available at http://shounen.ru/soft/flashnul/flashnul-1rc1.zip Steps Insert your flash media Run flashnul -p (from the dir that has flashnul) Note the physical device number for flash media Run flashnul <number obtained in prior step> -L \path\to\downloaded.img Answer "yes" if the selected destination device is correct Remove your flash media when the command completes Be careful what drive you erase. There are warnings presented before you commit: Disk PhysicalDrive2 (UNC name: \\.\PhysicalDrive2)         ------------------------------------------------------------[Drive geometry]--         Cylinders/heads/sectors = 482/255/63         Bytes per sector = 512         CHS size = 3964584960 (3780 Mb)         ---------------------------------------------------------------[Device size]--         Device size = 3965190144 (3781 Mb)         delta to near power of 2 = 329777152 (314 Mb), 8%         Surplus size = 605184 (591 kb)         -----------------------------------------------[Adapter & Device properties]--         Bus type = (7) USB         Removable device = Yes         Command Queue = Unsupported         Device vendor = Generic         Device name = USB SD Reader         Revision = 0.00         --------------------------------------------------------------[Hotplug info]--         Device hotplug = Yes         Media hotplug = No Selected operation: load file content Selected drive: PhysicalDrive2, 3965190144b (3781 Mb)</pre>         THIS OPERATION IS DESTRUCTIVE!!!         Type 'yes' to confirm operation. All other text will stop it. Really destroy data on drive PhysicalDrive2? :yes         -----------------------------------------------------------------------[Log]-- Runing operation [load file content] for drive PhysicalDrive2 Writing 0x36110000 (865 Mb), 3362893 b/s      
View full article
i.MX6UL/ULL extend uart port and integrate SIP I2C device. Contents 1 硬件设计说明 ............................................................. 2 硬件框图 ........................................................................ 2 硬件模块设计 ................................................................. 4 IOMUX 表 ....................................................................... 8 2 编译环境搭建 ............................................................. 8 编译环境文档及镜像下载。 ............................................ 8 编译环境搭建 ............................................................... 11 3 移植BSP 到扩展串口板 ........................................... 15 Uboot 中支持新的DTB ................................................ 15 Uboot 中调试串口改成UART6 ..................................... 16 去除掉无用的驱动及其IOMUX .................................... 18 增加i.MX6UL/ULL 本身串口支持 ................................. 18 增加GPIO 输出支持(GPIO_LED) ............................ 26 增加GPIO 输入支持(GPIO_KEY) ........................... 30 增加PWM支持 ............................................................ 34 增加i.MX6UL 本身ADC 支持 ....................................... 38 修改网口驱动仅支持一个网口 ...................................... 41 增加NXP PCF8591 I2C 转ADC 芯片支持 ................... 44 增加NXP PCA9555A I2C 转GPIO 芯片支持(rework 支持) 47 增加NXP PCT2075 I2C 温度传感器芯片支持(rework 支持) 55 增加NXP PCF8563 I2C RTC 支持(rework 支持) ......... 58 增加NXP PCA9632 I2C LED控制器芯片支持(rework 支持) 65 增加CH438 EIM 转串口芯片支持(delay) ..................... 70
View full article
MIPI can support video streaming over 1, 2, 3 and 4 lanes. On i.MX6 Sabre boards, the OV5640 camera supports 1 or 2 lanes and the NXP Linux Kernel uses 2 lanes as default. In order to use only one lane, follow the steps below: 1 - Change the board Device Tree on Linux Kernel. On file <linux kernel folder>/arch/arm/boot/dts/imx6qdl-sabresd.dtsi, find the entry "&mipi_csi" and change lanes from 2 to 1. 2 - Configure OV5640 to use only one lane instead of two. On file <linux kernel folder>/drivers/media/platform/mxc/capture/ov5640_mipi.c, change the register 0x300e value from 0x45 to 0x05. This register setup is located at struct ov5640_init_setting_30fps_VGA. 3 - Build the kernel and device tree files. 4 - Test the camera. Unit test can be used to test the video capture: /unit_tests/mxc_v4l2_overlay.out -di /dev/video1 -ow 1024 -oh 768 -m 1 5 - Checking if it's really using one lane. MIPI_CSI_PHY_STATE resgister (address 0x021D_C014) provides the status of all data and clock lanes. During video streaming using 2 lanes, the register value constantly changes its value between 0x0000_0300 and 0x0000_0330. When using only one lane, this register value constantly changes its value between 0x0000_0300 and 0x0000_0310. To read the register value during the stream, run the video test with &: /unit_tests/mxc_v4l2_overlay.out -di /dev/video1 -ow 1024 -oh 768 -m 1 & Now, run the memtool: /unit_tests/memtool -32 0x021dc014 1 i.MX6DL running mxc_v4l2_overlay.out with only one lane:
View full article
All Boards Creating App MP3 OpenEmbedded
View full article
ADB is very well known as the tool to manually install APK’s, but there are some other useful commands. ADB is a command line tool that acts as the bridge between you and your android device. I want to show you some of them, but first, let’s make sure we have everything needed to use ADB. Requirements First, you need to have Java and the Android SDK installed on your PC, you can download it from here: Java SDK: Java SE - Downloads | Oracle Technology Network | Oracle Android SDK: http://developer.android.com/sdk/index.html Once it is installed, it is recommended to update the SDK Manager Once you have done this, flash the Freescale Android BSP onto your board… Once you have installed it, you need to enable USB Debugging in the Developer Options of your board.        Here's the steps to enable USB debugging: Go to Settings. Click on "about tablet" Scroll down to the last row (Build Number) and tap that row 7 times. Return to the previous screen and click on "developer options" Confirm that "usb debugging" is checked. Once you enable it, your OS (assuming you are using Windows) will look for the Android ADB Interface driver. Windows systems are the only ones that need this ADB driver. After this procedure, you can now start using ADB. Open a terminal window and go to the platform-tools directory of your SDK installation to find the ADB program. The usual path to find it would be: adt-bundle-windows-x86 >> sdk >>platform-tools adb start-server                              ::  Starts the ADB server in case it is not running already adb kill-server                   :: Terminates de ADB server adb devices                        :: Checks  and prints the status of each device plugged to your PC  (If you don’t see your device, make sure USB debugging is enabled in your tablet.) adb install  'apk file'       :: It will install an apk to the tablet.   This apk must be located in the same folder where the adb is. adb uninstall 'apk file' :: It will uninstall an apk adb pull 'file'                                               :: It copies a file or directory (and sub-directories) from your device to the PC. adb push 'file'                          :: It copies a file of directory (and sub-directories) from your PC to the device. adb logcat                        :: Prints the logdata to the screen adb logcat –c                  :: Clears the buffer to remove any old log data. adb bugreport               :: Prints dumpsys, dumpstate and logcat. adb shell pm list packages –f    ::  List all installed packages adb shell input keyevent 26     :: Send the power button event to turn on/off the device adb shell screencap –p /sdcard/screen.png      :: Takes a screenshot of the android display adb shell screenrecord /sdcard/demo.mp4      :: Records any activity on the android display Using the window manager There is also a very useful tool to manage the display. This can be ran through a terminal connection to your board. You run this command from the following path /system/bin of your android BSP These are some of the commands available: wm density 'density number'              :: Changes the display density wm size 'display size'                                :: Changes your display’s resolution Using the activity manager In the same path is the activity manager which has several other commands for use: am start 'package'   :: Starts an activity am monitor                     :: Monitors activities am bug-report               :: Requests a bug report am restart                        :: Restarts the OS
View full article
This section for all Freescale i.MX users ranging from customers to designers to help provide the best solution to the most frequently encountered questions related to Freescale i.MX products. Products Below are links to pages containing links to documentation related to that product. i.MX Family i.MX6 Multimedia Applications Processors i.MX53 Multimedia Applications Processors i.MX51 Multimedia Applications Processors i.MX35 Multimedia Applications Processors i.MX31 Multimedia Applications Processors i.MX28 Multimedia Applications Processors i.MX27 Multimedia Applications Processors i.MX25 Multimedia Applications Processors i.MX21 Multimedia Applications Processors Topics Below are links to pages containing links to documentation related to that topic. 19-iMX_Serial_Download_Protocol.py All Boards 2D/3D Graphics All Boards Accessing Registers All Boards Audio All Boards Bluetooth Dongle All Boards Compiling RedBoot All Boards Configuring RedBoot All Boards Creating App Video All Boards Deploy NFS All Boards DirectFB All Boards FlexCAN All Boards Hardware Software All Boards How To Convert RVICE CP15 To OpenOCD All Boards How To Understand JTAG BSDL All Boards I2C-tools All Boards Java All Boards JTAG All Boards LTIB All Boards LTIB Config Ubuntu All Boards LTIB Creating Uimage Uboot All Boards NFS on Fedora All Boards NFS on Slackware All Boards NFS on Ubuntu All Boards OpenEmbedded All Boards Pdfreader All Boards PMIC Registers All Boards Qtopia All Boards Qtopia on Ubuntu All Boards Qt v2 All Boards RedBoot All Boards Serial Console All Boards TCP All Boards Tethering All Boards TFTP All Boards TFTP Fedora All Boards TFTP on OpenSuse All Boards TFTP on Ubuntu All Boards Theora Encoder All Boards Transfer Serial RedBoot All Boards U-boot All Boards Updating RedBoot Through RedBoot All Boards Video All Boards Video Host All Boards VMWare All Boards Wi-Fi All Boards X11 Android Demonstration Platform Exercising the i.MX Serial Download Protocol with a Python Script Gstreamer GTK How to Enable Second Display Showing Different Things on JB4.2.2 SabreSD How to Measure Signal Frequency by Using the Camera Sensor Interface of an i.MX i.MX as a USB Playback/Capture Device on One OTG Port i.MX Bootlets (i.MX233 EVK) i.MX USB Loader i.MXS Development Kit InternalI2C Linux Kernel Mxuart patch New Release of the i.MX OTP Tools V1.3.3 NFS OpenEmbedded Redboot Running ATK on Linux Script to Flash a Linux System into a SD card U-Boot Yoctoproject
View full article
Support SSI Master function based on 0001_SSI_ASRC_P2P.patch
View full article
Configuring U-Boot LTIB Creating Uimage Uboot U-boot FW Printenv FW Env File Add New i.MX5x Board on LTIB i.MX25 PDK I.MX25 PDK U-boot SplashScreen I.MX25 PDK U-boot SDCard i.MX27 ADS Board Compiling U-Boot for i.MX27ADS Installing U-Boot on iMX27ADS i.MX31 ADS Board i.MX31ADS Compiling Uboot I.MX31ADS Installing Uboot i.MX31 PDK Board i.MX 31 PDK Board Screenshot I.MX31 PDK Board Flashing i.MX31 PDK Board DirectFB i.MX51 EVK Board i.MX51 EVK U-boot I.MX51EVK Install U-Boot i.MX51 EVK Compiling U-boot i.MX51 EVK Changing Env
View full article
Attached is the Kernel needed to construct the following image: i.MX 6Dual/6Quad Power Consumption Measurement Linux Image
View full article
Hi All, The i.MX6 Android R13.4-GA.03 patch release is now available on www.freescale.com ·         Files available # Name Description 1 IMX6_R13.4.03_ANDROID_PATCH This patch release is based on the i.MX 6 Android R13.4   release. The purpose of this patch release is correct the PFD workflow in   U-Boot, fix the miscalibration issue for the thermal sensor and corrects   ramp-up time of the internal LDOs
View full article
Development environment: i.MX6Q SabreSD w/ L3.0.35_1.1.0_121218 release. Quoting from Wikipedia about exFAT (exFAT - Wikipedia, the free encyclopedia) as following: exFAT (Extended File Allocation Table) is a Microsoft file system optimized for flash drives. [3] It is proprietary and patent-pending. [1] It is supported in Windows XP and Windows Server 2003 with update KB955704, [2] Windows Embedded CE 6.0, Windows Vista with Service Pack 1, [4] Windows Server 2008, [5] Windows 7, Windows 8, Windows Server 2008 R2 (except Windows Server 2008 Server Core), Mac OS X Snow Leopard starting from 10.6.5, [6] Mac OS X Lion and OS X Mountain Lion. The history of support exFAT in Linux was since from 2.6.x, it involves several parts that will be described followingly. Part 1: Linux Kernel            Enable FUSE (Filesystem in userspace) feature in Kernel Config, then build a new uImage and module if set it to be "M"; Part 2: fuse-2.9.2.tar.gz            Download fuse-2.9.2.tar.gz from http://sourceforge.net/projects/fuse/files/fuse-2.X/, untar it, then build it with following commands: ./configure --prefix=/home/alanz/i.MX6_L3.0.35_121218/ltib/rootfs/usr --host=`/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc -dumpmachine` --enable-lib --enable-util --enable-example --exec-prefix=/home/alanz/i.MX6_L3.0.35_121218/ltib/rootfs/usr make sudo make install Part 3: exfat-utils-1.0.1.tar.gz            Download exfat-utils-1.0.1.tar.gz from http://code.google.com/p/exfat/downloads/list, untar it, then build it with following command: sudo scons SYSROOT=/home/alanz/i.MX6_L3.0.35_121218/ltib/rootfs DESTDIR=/home/alanz/i.MX6_L3.0.35_121218/ltib/rootfs/sbin CC=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc AR=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-ar RANLIB=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-ranlib STRIP=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-strip install Part 4: fuse-exfat.git git clone git://sources.progress-linux.org/git/releases/baureo-backports/packages/fuse-exfat.git  fuse-exfat.git cd fuse-exfat.git Replace the root SConstruct with the attached one, then execute command: sudo scons SYSROOT=/home/alanz/i.MX6_L3.0.35_121218/ltib/rootfs DESTDIR=/home/alanz/i.MX6_L3.0.35_121218/ltib/rootfs/sbin CC=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc AR=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-ar RANLIB=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-ranlib STRIP=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-strip install After all above steps done, you can check whether the necessary files under your rootfs like I did as following: http://en.wikipedia.org/wiki/ExFAT#cite_note-uspatent-2alanz@alanz-VirtualBox:~/i.MX6_L3.0.35_121218/ltib$ find ./rootfs/ -name *exfat*./rootfs/sbin/exfatlabel ./rootfs/sbin/mount.exfat ./rootfs/sbin/fsck.exfat ./rootfs/sbin/dumpexfat ./rootfs/sbin/exfatfsck ./rootfs/sbin/mount.exfat-fuse ./rootfs/sbin/mkexfatfs ./rootfs/sbin/mkfs.exfat alanz@alanz-VirtualBox:~/i.MX6_L3.0.35_121218/ltib$ find ./rootfs/ -name *fuse*./rootfs/usr/include/fuse ./rootfs/usr/include/fuse/fuse_common_compat.h ./rootfs/usr/include/fuse/fuse_compat.h ./rootfs/usr/include/fuse/fuse_lowlevel_compat.h ./rootfs/usr/include/fuse/fuse_opt.h ./rootfs/usr/include/fuse/fuse_lowlevel.h ./rootfs/usr/include/fuse/fuse.h ./rootfs/usr/include/fuse/fuse_common.h ./rootfs/usr/include/fuse.h ./rootfs/usr/src/linux/include/linux/fuse.h ./rootfs/usr/lib/libfuse.so ./rootfs/usr/lib/libfuse.a ./rootfs/usr/lib/libfuse.so.2.9.2 ./rootfs/usr/lib/libfuse.la ./rootfs/usr/lib/libfuse.so.2 ./rootfs/sbin/mount.exfat-fuse Check Steps can be referenced by the steps presented on internet. NOTE: The directory name "/home/alanz/i.MX..." should be revised per your self development environment.
View full article
Issue: kernel panic when repeating plug/unplug USB device(e.g. USB flash disk) in Linux 4.1.15 The issue is in kernel BLOCK DEVICE, this is not a hardware related issue(happens to all devices running L4.1.15 or L4.4.x), please refer to following link on kernel.org for more details and fixes: blockdev kernel regression (bugzilla 173031) - Patchwork 
View full article
NOTE: Always de-power the target board and the aggregator when plugging or unplugging smart sensors from the aggregator. NOTE: See this link to instrument a board with a Smart Sensor. Overview The i.MX Power Profiler system consists of one to fourteen "smart" current sensors, an aggregator shield, and a Kinetis FRDM board (the FRDM-KL25 has been used in prototyping but the FRDM-K64F and FRDM-K66F should also be fully compatible). One of the biggest improvements of this system over its preceeding dual-range measurement system is that the microcontroller on each sensor board allows near-simultaneous measurement of all instrumented rails on a board. The dual range profiler has only a single MCU for all sensors, so only one measurement can be made at a time.  It is intended to be used to instrument one to fourteen rails of a target i.MX appliation board. Ideally, the target board will have been designed with a matching/mating power sense footprint for each rail to be measured.  Each smart sensor can sense current in three ranges with three current sense amplifiers. They are "smart" because each sensor board has a Kinetis KL05Z on it to control the switching FETs and to digitize the analog signals (the sense amplifier outputs and the target's power supply rail voltage). A 1% voltage regulator on each smart sensor provides a good voltage reference right next to the KL05Z to ensure better ADC accuracy. Each smart sensor board communicates via I2C. The aggregator shield has three I2C bus extenders (PCA9518) which essentially provide a dedicated I2C bus for each of the connected smart sensors. The FRDM board's I2C is also connected to one of the bus extenders ports. Individual GPIO lines are routed to each smart sensor's connected along with a ganged reset and trigger line for all of the connected smart sensors. A boost regulator generates almost 12V from the FRDM board's 5V supply, which is used for all the switching FETs on the smart sensor boards. The FRDM board's 5V rail is also routed to each smart sensor, which is regulated down to 3.3V locally on each connected smart sensor. Here is a photo of the very first prototypes after moving to 10-pin 0.05" spaced headers and ribbon cables instead of FFC: The smart sensor is intended to mate with through-hole current sense tap points on the target i.MX application board. Three holes spaced at 0.05" each. When not instrumented with sensor, a short needs to be placed across the outer two pins so that the board will function normally. The through hole connections provide physical protection to the target board, keeping traces from getting ripped off. The ground connection in the center provides a reference for meauring the rail voltage on the target board. A partial layout example of the implementation of the current sense footprint is below, where two 0805 shorting resistors in parallel are placed on each side of the holes. The top trace connects to the regulator output and the bottom to the load, usually an i.MX power supply rail. To include the current sense footprint into a board during the design phase, it should be configured as in the following partial schematic:  Every effort should be made to place the feedback on the i.MX side of the sense points so that the regulator compensates for the additional series resistance of the smart sensor, which effectively eliminates the additional series resistance the smart sensor adds. The Feedback should be before the smart sensor if the switching supply won't tolerate the additional series resistance (i.e., output becomes unstable).
View full article
Summary of the Issue: We have had customers reporting failure to run MC and SC production parts at 1GHz or higher frequencies. The signature of the fail is that the system will hang once it tries to ramp from the boot frequency of 800MHz to 1GHz or higher. The root cause was tracked to the setting of the LDO_VOLT_CHANGE_EN fuse in production parts. The LDO_VOLT_CHANGE_EN fuse sets the LDO boot voltage to either 1.15V (indicated by a fuse setting of “1”) or 1.1V  (indicated by a fuse setting of “0”). In production parts the fuse is set to “1”, i.e. 1.15V, since this is the optimal setting based on characterization data. On pre-production units the LDO voltage was set to the lower setting of 1.1V (i.e. fuse set to “0”). The reason this is a problem with MC/SC parts is because the fuse is read by the ROM during boot and overwrites the LDO ramp rate bits in the PMU_MISC2 register based on the setting of the fuse. When the LDO_VOLT_CHANG_EN fuse is set to “1” then the LDO ramp up time to spec voltage is set (in PMU_MISC2) to 500uS instead of the 50uS assumed by the CPUFreq driver. This will cause the system to hang when transitioning from the boot frequency to a higher frequency/voltage point since the required voltage to support the higher frequency is not yet present. In real terms, customers who have production i.MX 6Quad/6Dual/6DualLite and 6 Solo parts have seen failures to ramp their products to 1GHz or higher frequencies. This is completely fixed by a software patch that corrects the LDO ramp setting in the PMU_MISC_2 register by setting it back to the fastest ramp time. Note that the LDO_VOLT_CHANGE_EN fuse is not in the reference manual since it is not a customer visible fuse. It is programmed and locked at final test. This is a mandatory fix for all customers. Affected Parts: i.MX 6Quad – all SC and MC parts, consumer and automotive. Industrial MC parts not yet shipping. i.MX 6Dual – all SC and MC parts, consumer and automotive. Industrial MC parts not yet shipping. i.MX 6DualLite – all MC parts consumer parts. Automotive and industrial MC parts not yet shipping. i.MX 6Solo – all MC consumer parts. Automotive and industrial MC parts not yet shipping. Patch Availability and Location: Patches exist for both Linux and Android. They are available on freescale.com. See below for more details. i.MX 6Quad – www.freescale.com/imx6q i.MX 6Dual – www.freescale.com/imx6d i.MX 6DualLite – www.freescale.com/imx6dl  i.MX 6Solo – www.freescale.com/imx6s Select the “Software and Tools” tab and then expand the section “Updates and Patches”.  The relevant patches are: Linux – L3.0.35_1.1.1_LDO_PATCH (i.MX 6Quad/6Dual) Linux – L3.0.35_3.0.3_LDO_PATCH (i.MX 6DualLite/6Solo) Android – IMX6_R13.4103_ANDROID_LDO_PATCH (i.MX 6Quad/6Dual/6DualLite/6Solo) Communication Roll-out: i.MX FAE’s: done (via maillist). Will post copy of this email to i.MX support space by end of day 1 st March. i.MX DFAE’s: 8 th March. Customer notification: 8 th March. i.MX community: 8 th March (to coincide with customer notification). We are also working on an engineering bulletin that describes the change for customers who are not using our provided Linux and Android BSP’s. Target date: TBD. But goal is to make this available on/around mid-March. Best regards, Amanda and Kyle This document was generated from the following discussion: i.MX 6 Series LDO Ramp Issue: Linux and Android Patches Now Available
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343113 
View full article