i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Here is a quick summary at building a bootloader, a kernel and a root filesystem for the i.MX 6 sabre sd platform, using buildroot. This assumes you have a "working" Linux development environment at hand (e.g. Debian). Buildroot is a fine build system, which makes deploying Linux on embedded platforms really easy. It is comparable to Yocto in spirit, but much simpler. Thanks to my colleague gillestalis, buildroot now has builtin support for the i.MX6 sabre sd platform. Get buildroot sources We will use git to fetch buildroot sources: $ git clone git://git.busybox.net/buildroot This should create a buildroot directory with all the latest sources (after a while). Note that for more stability you might want to checkout a release instead of the latest version; to do so, list the available release tags with e.g. git tag -l '201*', and git checkout <the-desired-tag>. Compile The beauty of buildroot is that it will take care of everything for you, including preparing a cross compiler. You can download and build everything by doing: $ cd buildroot $ make freescale_imx6sabresd_defconfig $ make This should download and build everything, so it will take a while. buildroot detects the number of CPUs you have in your machine and builds with parallel jobs automatically; no need to specify any -j argument to make here. All build results fall under the output/images folder: output/images/ +- rootfs.ext2 +- rootfs.tar +- u-boot.bin `- uImage Format the SD card As for Debian, we need to format the SD card with two partitions; one small FAT partition to contain the Linux kernel, and one large ext4 partition, which will contain the root filesystem with the buildroot generated userspace. Also, we need to make sure we leave some space for u-boot starting from offset 1024B. Here is an example SD card layout: +-----+------+--------+-----+---------------+----------------- | MBR |  ... | u-boot | ... | FAT partition | Linux partition ... +-----+------+--------+-----+---------------+----------------- 0     512    1024           1M              ~257M (offsets in bytes) Here is an example SD card layout, as displayed by fdisk: Device    Boot      Start         End      Blocks   Id  System /dev/sdc1            2048      526335      262144    c  W95 FAT32 (LBA) /dev/sdc2          526336     8054783     3764224   83  Linux (units: 512B sectors) You can format the FAT boot partition with: # mkfs.vfat /dev/<your-sd-card-first-partition> Your SD card first partition is typically something in /dev/sd<X>1 or/dev/mmcblk<X>p1. You can format the Linux partition with: # mkfs.ext4 /dev/<your-sd-card-second-partition> Your SD card second partition is typically something in /dev/sd<X>2 or/dev/mmcblk<X>p2. Put on SD As explained here, u-boot should reside at offset 1024B of your SD card. Also, as buildroot generates an u-boot.bin (and not an u-boot.imx) we should skip its first KB, too. In summary, to put u-boot on your SD, do:   # dd if=output/images/u-boot.bin of=/dev/<your-sd-card> bs=1k seek=1 skip=1   # sync Your SD card device is typically something in /dev/sd<X> or /dev/mmcblk<X>. Note that you need write permissions on the SD card for the command to succeed, so you might need to su - as root, or use sudo, or do a chmod a+w as root on the SD card device node to grant permissions to users. Similarly to what this post describes, you can copy the kernel to the FAT boot partition with: # mount /dev/<your-sd-card-second-partition> /mnt # cp output/images/uImage /mnt/ # umount /mnt Your SD card first partition is typically something in /dev/sd<X>1 or/dev/mmcblk<X>p1. And not unlike what is done in this post, You can install your generated root filesystem to the Linux partition with: # mount /dev/<your-sd-card-second-partition> /mnt # tar -C /mnt -xvf output/images/rootfs.tar # umount /mnt Your SD card second partition is typically something in /dev/sd<X>2 or/dev/mmcblk<X>p2. Boot! Your SD card is ready for booting. Insert it in the SD card slot of your i.MX6 sabre sd platform, connect to the USB to UART port with a serial terminal set to 115200 baud, no parity, 8bit data and power up the platform. Like with Debian, u-boot default settings will not allow it to boot from the SD card, so we need to interrupt it by pressing enter at u-boot prompt for the first boot and setup u-boot environment to fix this: MX6Q SABRESD U-Boot > setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p2 rootwait' MX6Q SABRESD U-Boot > setenv bootcmd_mmc 'run bootargs_base bootargs_mmc; mmc dev 2; fatload mmc 2:1 ${loadaddr} ${kernel}; bootm' MX6Q SABRESD U-Boot > setenv bootcmd 'run bootcmd_mmc' MX6Q SABRESD U-Boot > saveenv Saving Environment to MMC... Writing to MMC(2)... done As this is saved in the SD card it need only to be done once at first boot. You can reboot your board or type boot; your buildroot system should boot to a prompt: (...) Welcome to Buildroot buildroot login: From there you may login as root. Enjoy! Tweak buildroot uses Linux kernel kconfig to handle its configuration. So, as for the Linux kernel, changes to the configuration can be done with e.g.: $ make menuconfig Most of the options can be tuned from there, including (most importantly) which packages get installed into the generated root filesystem. This is configuration section 'Filesystem images'. Further details are documented in buildroot manual. Tips ccache is natively supported by buildroot and can be easily enabled with configuration option BR2_CCACHE. If you only use the generated rootfs.tar as described in this post and do not care about the rootfs.ext2, you might as well save a few seconds of build by disabling its generation. This is done with configuration option BR2_TARGET_ROOTFS_EXT2. It is recommended to install an ssh server inside the target for further development. This is conveniently done with configuration option BR2_PACKAGE_OPENSSH. See also... Other root filesystems may make more sense for you; see this post for a Debian root filesystem, and this post for a minimal busybox filesystem. Freescale Yocto Project main page
View full article
Overview This document provides some solutions for building i.MX 6 series LTIB on an Ubuntu 14.04 Trusty Tahr host. A Virtualbox virtual machine was created for the Ubuntu computer which is used for the build host.   Linux Target Image Builder (LTIB) is a perl script used for creating images (Bootloader u-boot, Linux uImage, and root file system). The build example shown here was for the i.MX 6Q and minimum root file system.   Software Versions L3.0.35_4.1.0_ER_SOURCE_BSP L3.0.35 : Linux version 3.0.35 4.1.0 :  Freescale release number ER_SOURCE_BSP : Engineering Release source Board support package File download URL:  L3.0.35_4.1.0_130816_source.tar.gz. Note this requires a free account registration at freescale.com. md5sum L3.0.35_4.1.0_130816_source.tar.gz dec08bb266134b94af0f54356e2e9de9  L3.0.35_4.1.0_130816_source.tar.gz L3.0.35_4.1.0_docs.tar.gz Documentation bundle. File download URL: L3.0.35_4.1.0_docs.tar.gz md5sum L3.0.35_4.1.0_docs.tar.gz 85f122c72735f3d162a99ae42554e886  L3.0.35_4.1.0_docs.tar.gz Ubuntu 14.04 LTS Trusty Tahr LTS : Long Term Supported 64-bit version File download URL: http://www.ubuntu.com/download/desktop md5sum ubuntu-14.04-desktop-amd64.iso dccff28314d9ae4ed262cfc6f35e5153  ubuntu-14.04-desktop-amd64.iso Virtualbox Version 4.3.10 File download URL: Oracle VM VirtualBox Machine Setup 4 CPU 4 GB RAM 64 GB Hard disk from USB 3.0 connected drive Host Computer Dell M4600, 8GB RAM,  8 CPU Ubuntu Linux 12.04.02 LTS   Ubuntu Host 14.04 Host Packages Various packages are required to meet build requirements of LTIB. Please refer to "Setting_Up_LTIB_host.pdf" document found in the L3.0.35_4.1.0_docs.tar.gz download. See below for the trustyPkgs.txt attachment that shows all the packages that were installed. This was created using the command: dpkg --list   On your host you can run the command "dpkg --list" and compare with the trustyPkgs.txt using your favorite diff tool. (examples, meld, diff). Any package missing can be added using your favorite package manager.  For example to install mkimage which is found in the u-boot-tools package:  sudo apt-get install u-boot-tools   Build LTIB Host Package M4 Failure The package m4 fails to build. Paste of the error messages:   gcc -std=gnu99  -I.     -g -O2 -MT clean-temp.o -MD -MP -MF .deps/clean-temp.Tpo -c -o clean-temp.o clean-temp.c In file included from clean-temp.h:22:0,                  from clean-temp.c:23: ./stdio.h:477:1: error: 'gets' undeclared here (not in a function) make[3]: *** [clean-temp.o] Error 1 make[3]: Leaving directory `/opt/freescale/ltib/usr/src/rpm/BUILD/m4-1.4.16/lib' make[2]: *** [all] Error 2 make[2]: Leaving directory `/opt/freescale/ltib/usr/src/rpm/BUILD/m4-1.4.16/lib'   Solution Replace the m4 package with a newer version. The m4 package bundled with LTIB is version 1.4.16. A newer version 1.4.17 is available and does not have build failures. File download URL: http://ftp.gnu.org/gnu/m4/m4-1.4.17.tar.gz Create a md5 file:           md5sum m4-1.4.17.tar.gz > m4-1.4.17.tar.gz.md5 Move both files to /opt/freescale/pkgs which is where ltib searches for packages.           mv m4* /opt/freescale/pkgs Edit the m4.spec file that specifies the version           cd <ltib>/dist/lfs5.1/m4/           Edit m4.spec using your favorite editor.  Line 5 is the Version number to change from 16 to 17:   Original: 1 %define pfx /opt/freescale/rootfs/%{_target_cpu} 2 3 Summary : The GNU macro processor 4 Name  : m4 5 Version : 1.4.16 6 Release : 1 7 License : GPL   Updated: 1 %define pfx /opt/freescale/rootfs/%{_target_cpu} 2 3 Summary : The GNU macro processor 4 Name  : m4 5 Version : 1.4.17 6 Release : 1 7 License : GPL       busybox   Failure   /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find /lib/libc.so.6 /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find /usr/lib/libc_nonshared.a /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find /lib/ld-linux.so.3 collect2: ld returned 1 exit status make: *** [busybox_unstripped] Error 1 error: Bad exit status from /home/user/imx6/ltib/tmp/rpm-tmp.60711 (%build)     RPM build errors:     Bad exit status from /home/user/imx6/ltib/tmp/rpm-tmp.60711 (%build) Build time for busybox: 93 seconds   Failed building busybox   Solution:   Go into ltib/dist/lfs-5.1/base_libs/base_libs.spec and find these lines:      # remove absolute paths from text search files (if they exist)      perl -w -e '          @ARGV = grep { `file $_` =~ m,ASCII C program text, } @ARGV;          exit(0) unless @ARGV; Remove the last two (the lines beginning with "@ARGV" and "exit(0)"   Adding the # character removes the lines 299 and 300 297 # remove absolute paths from text search files (if they exist) 298 perl -w -e ' 299 #@ARGV = grep { `file $_` =~ m,ASCII C program text, } @ARGV; 300 #exit(0) unless @ARGV; 301$^I = ".bak";     Success When the build completes, u-boot.bin and uImage are found in <ltib>/rootfs/boot   [user@trusty ltib]$ tree rootfs/boot rootfs/boot ├── bootable_kernel -> uImage ├── linux.config ├── System.map ├── u-boot ├── u-boot.bin ├── uImage ├── vmlinux └── zImage Original Attachment has been moved to: trustyPkgs.txt.zip Original Attachment has been moved to: lkc-1.4.tar.gz
View full article
                                                                                         Watch the Freescale i.MX team boot up Android 5.0 Lollipop in i.mx6 application processors—在线播放—优酷网,视频高清在线观看 The Freescale i.MX Android team has booted up Android 5.0 Lollipop in the SABRE platform for i.mx6 series. Google pushed all of the latest source for its Android release to AOSP on Nov. 5, and the Freescale Android Team started their work. With the previous 6 days to boot Android Lollipop up, the Freescale i.MX Android team enabled the basic features like connectivity, audio/video playback, sensors, inputs and display on day 7! You can see the some changes in the demo video at the beginning of the post. The Freescale i.MX Android team has closely followed almost every version of Android since it is released by AOSP and has good experience on it. Below are some snapshots and pictures for the Android Lollipop.
View full article
Here is a quick summary at booting Linux on the i.MX 6 sabre sd platform. This assumes you already have u-boot working on your platform as described here. This implies you already have a "working" Linux development environment with some ARM cross-compilers at hand (e.g. Debian + Emdebian). Get Linux sources We will use git to fetch Linux sources:   $ git clone git://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git This should create a linux directory with all the latest sources (after a while). Note that for more stability you might want to checkout a release instead of the latest version; to do so, list the available release tags with e.g. git tag -l 'v*', and git checkout <the-desired-tag>. Compile Assuming your cross compiler is called e.g. arm-linux-gnueabihf-gcc, you can compile by doing:   $ cd linux   $ export ARCH=arm   $ export CROSS_COMPILE=arm-linux-gnueabihf-   $ make imx_v6_v7_defconfig   $ make You then need to supply a LOADADDR (as joowonkim pointed out); do:   $ make uImage LOADADDR=0x10008000 This should create a number of files, including arch/arm/boot/uImage and arch/arm/boot/dts/imx6q-sabresd.dtb. Put on SD We need a proper FAT partition on the SD card, from which u-boot will be able to load the kernel and dtb. Also, we need to make sure we leave some space for u-boot starting from offset 1024B. Here is an example SD card layout:   +-----+------+--------+-----+----------------   | MBR |  ... | u-boot | ... | FAT partition ...   +-----+------+--------+-----+----------------   0     512    1024           1M (offsets in bytes) Here is an example SD card layout, as displayed by fdisk:   Device    Boot      Start         End      Blocks   Id  System   /dev/sdc1            2048     8054783     4026368    c  W95 FAT32 (LBA) (units: 512B sectors) You can format the FAT partition, mount, copy and unmount with:   $ mkfs.vfat /dev/<your-sd-card-first-partition>   $ mount /dev/<your-sd-card-first-partition> /mnt   $ cp arch/arm/boot/uImage arch/arm/boot/dts/imx6q-sabresd.dtb /mnt/   $ umount /mnt Your SD card first partition is typically something in /dev/sd<X>1 or /dev/mmcblk<X>p1. Note that you need write permissions on the SD card for the command to succeed, so you might need to su - as root, or use sudo, or do a chmod a+w as root on the SD card device node to grant permissions to users. Also, be sure to have u-boot on the SD card as explained in this post. Boot! That's it; u-boot already knows how to deal with your kernel by default so you are good to go. Insert the SD card into the SD card slot of your i.MX6 sabre sd platform, connect to the USB to UART port with a serial terminal set to 115200 baud, no parity, 8bit data and power up the platform. You should see u-boot messages:   U-Boot 2013.07-rc1-00014-g74771f4 (Jun 21 2013 - 16:27:39) u-boot should load the uImage and dtb from SD card and boot the kernel:   (...)   reading uImage   4215344 bytes read in 449 ms (9 MiB/s)   Booting from mmc ...   reading imx6q-sabresd.dtb   22818 bytes read in 22 ms (1012.7 KiB/s)   ## Booting kernel from Legacy Image at 12000000 ...      Image Name:   Linux-3.10.0-rc6      Image Type:   ARM Linux Kernel Image (uncompressed)      Data Size:    4215280 Bytes = 4 MiB      Load Address: 10008000      Entry Point:  10008000      Verifying Checksum ... OK   ## Flattened Device Tree blob at 11000000      Booting using the fdt blob at 0x11000000      Loading Kernel Image ... OK   OK      Using Device Tree in place at 11000000, end 11008921   Starting kernel ... The kernel should boot:   Booting Linux on physical CPU 0x0   Linux version 3.10.0-rc6 (vstehle@debian) (gcc version 4.7.2 (Debian 4.7.2-5) ) #1 SMP Fri Jun 21 18:09:26 CEST 2013 By default, the kernel will try to mount a root filesystem from the SD card second partition, as can be read in the default kernel command line:   (...)   Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw ...but we did not prepare a root filesystem partition, so after a number of boot messages the kernel will wait indefinitely:   (...)   mmc1: new SDHC card at address b368   (...)    mmcblk0: p1   (...)   Waiting for root device /dev/mmcblk1p2... We will see in another post how to prepare this root filesystem on the second SD card partition. Enjoy! See also... If you plan to compile Linux often, you might want to use a C compiler cache; see this post. Once you have Linux booting on your platform the next step is to give it a root filesystem. See this post for a Debian root filesystem, this post for a minimal busybox filesystem and this post for generating a root filesystem with buildroot.
View full article
The edit-compile-test loop is the quickest way so can test your changes. 1. Go to the package's source code folder and edit your files. 2. Compile that particular package, e.g. bitbake linux-imx -c compile -f 3. Deploy, e.g. bitbake linux-imx -c deploy 4. Insert the SD card into your host, and copy the Linux kernel into the the first partition sudo cp tmp/deploy/images/uImage /media/Boot 5. Insert the SD card into your board, boot and test your changes 6. In case you are satisfied with the results, you need to create a patch and add into the package's recipe. Check this document to execute this step.
View full article
The i.MX Android O8.0.0_1.0.0 GA release is now available from IMX_SW page. Overview -> BSP Updates and Releases -> Android 8.0.0 Oreo (O8.0.0_1.0.0, 4.9 kernel)   Files available: # Name Description 1 android_O8.0.0_1.0.0_docs.tar.gz i.MX Android O8.0.0_1.0.0 BSP Documentation 2 imx-o8.0.0_1.0.0_ga.tar.gz i.MX Android O8.0.0_1.0.0 proprietary surce code for i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo  i.MX 6Sololite, i.MX6SX and i.MX7D 3 android_O8.0.0_1.0.0_image_6dqpsabreauto.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE for Automotive Infotainment based on i.MX 6QuadPlus, i.MX 6Quad, and i.MX 6DualLite 4 android_O8.0.0_1.0.0_image_6dqpsabresd.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Platform and SABRE Board based on i.MX 6QuadPlus, i.MX 6Quad and i.MX 6DualLite. 5 android_O8.0.0_1.0.0_image_6slevk.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - i.MX 6Sololite evaluation kit. 6 android_O8.0.0_1.0.0_image_6sxsabresd.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Board based on i.MX 6SoloX 7 android_O8.0.0_1.0.0_image_6sxsabreauto.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE for Automotive infotainment based on i.MX 6SoloX 8 android_O8.0.0_1.0.0_image_7dsabresd.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Board based on i.MX 7Dual 9 fsl_aacp_dec_O8.0.0_1.0.0.tar.gz AAC Plus Codec for O8.0.0_1.0.0 10 android_O8.0.0_1.0.0_tools.tar.gz Manufacturing Toolkit and VivanteVTK for O8.0.0_1.0.0   Supported Hardware SoC/Boards: i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-SD board and platform i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI board and platform i.MX 6SoloLite EVK platform i.MX 6SoloX SABRE-SD board and platforms i.MX 6SoloX SABRE-AI board and platforms i.MX 7Dual SABRE-SD board and platform   Changes: Compared to the N7.1.2_2.0.0 release, this release has the following major changes: Upgraded the Android code base from android-7.1.2_r9 to android-8.0.0_r25. Removed the device partition and added the vendor partition. Enabled ION-based gralloc and EGL. Feature: For features please consult the release notes.   Known issues For known issues and more details please consult the Release Notes.
View full article
1. Enable QtMultimedia 1) In “source/meta-qt5/recipes-qt/qt5/qtmultimedia_git.bb”, add “gstreamer” at the end of “PACKAGECONFIG ??=” .      For example on  L3.14.52  bsp, build  x11  backend: PACKAGECONFIG ??= "${@bb.utils.contains('DISTRO_FEATURES', 'alsa', 'alsa', '', d)} \                    ${@bb.utils.contains('DISTRO_FEATURES', 'pulseaudio', 'pulseaudio', '', d)} \                    gstreamer" 2) Build qtmultimedia:  bitbake qtmultimedia 3) Copy the built package to target file system.      For example : cp  -a ./build-x11/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtmultimedia/5.5.0+gitAUTOINC+46a83d5b86-r0/image/usr/   /usr   export  DISPLAY=:0 Video example application located at : /usr/share/qt5/examples/multimedia/video/qmlvideo 2. Enable Qt Logging Info export  QT_LOGGING_RULES=<category>[.type]=ture|false      For example: Turn on all debug logging:      export QT_LOGGING_RULES=*.debug=true Turn on all logging level of all multimedia module:      export QT_LOGGING_RULES=qt.multimedia.*=true 3. Performance Checking Gstreamer: overlaysink fps=51.585      gst-launch-1.0 playbin uri=file:///H264_AVC_1080p_30fps_27Mbps_mp3.avi  video-sink=”overlaysink sync=false” Gstreamer: glimagesink fps=43.850      gst-launch-1.0 playbin uri=file:///H264_AVC_1080p_30fps_27Mbps_mp3.avi video-sink="glimagesink sync=false" Qtmultimedia: fps=45.201      ./qmlvideo  -url file:///H264_AVC_1080p_30fps_27Mbps_mp3.avi -hide-perf Current qt5 multimedia has a special video node for imx6 at     "/src/plugins/videonode/imx6" which uses GPU DirectVIV to accelerate the video rendering. So  the rendering performance is almost same as the glimagesink. For check the free run frame rate, the qt multimedia source need change a little bit to set sink sync as false and calculate the real video rendering rate. Set sync as false: In "/src/plugins/gstreamer/mediaplayer/qgstreamerplayersession.cpp" QGstreamerPlayerSession::playbinNotifySource(): -       g_object_set(G_OBJECT(self->m_videoSink), "sync", !self->m_isLiveSource, NULL); +       g_object_set(G_OBJECT(self->m_videoSink), "sync", false/!self->m_isLiveSource/, NULL); Get fps: In "/src/gsttools/qgstvideorenderersink.cpp" +#include <QTime> +gint g_frame_showed; +QTime g_time; + bool QVideoSurfaceGstDelegate::start(GstCaps *caps) … +   g_frame_showed = 0; +   g_time.restart(); … void QVideoSurfaceGstDelegate::stop() … +   printf(">>>>> fps=%f:\n", (gdouble)g_frame_showed*1000/g_time.elapsed()); … bool  QVideoSurfaceGstDelegate::handleEvent(QMutexLocker *locker) …             const bool rendered = m_activeRenderer->present(m_surface, buffer); +   g_frame_showed++; … Or use the attached patch: qtmultimedia_fps_check.diff 4. Streaming Playing:  HTTP RTP RTSP HTTP: ./qmlvideo -url http://10.192.225.205/streaming/http/H264_HP13_1280x720_29_2850_AAC_LC_44_64_NobodyMTV.mp4 RTSP: ./qmlvideo -url rtsp://10.192.225.205/MPEG4_SP1_720x576_30fps_282_AMRNB_TVC.mp4 RTP: QT mediaplayer use gstreamer playbin as the backend, playbin don’t support rtp address as uri. So QT mediaplayer can’t support RTP playing directly. 5. Audio Recording /usr/share/qt5/examples/multimedia/audiorecorder/audiorecorder This is a widget application, not a QML application. It use QAudioRecorder as its background worker. By default it will use pulsesrc and lamemp3enc to recorder audio as mkv file at user home folder with name of clip_0001.mkv, clip_0002.mkv, and so on. If need special pipeline for recording, example use imxmp3enc to record mp3 files, we need change the function GstElement *QGstreamerCaptureSession::buildEncodeBin in  “src/plugins/gstreamer/mediacapture/qgstreamercapturesession.cpp” as well as QGstreamerMediaContainerControl(QObject *parent) in “src/plugins/gstreamer/mediacapture/qgstreamermediacontainercontrol.cpp” 6. Camera Widgets Application: “/usr/share/qt5/examples/multimediawidgets/camera/camera” QML Application: “/usr/share/qt5/examples/multimedia/declarative-camera/declarative-camera” Qt Multimedia has some bugs on L3.14.52 with QCamera for recording. Use the attached patches: 0001-gstreamer-fix-camerabin-not-negotiated-error.patch 0001-QCamera-can-t-set-recording-container-format-video-a.patch 0002-QtCamera-change-default-encoding-parameters-to-use-N.patch If you want use overlaysink as the preview sink, then use following patch: 0003-use-overlaysink-as-the-preview-sink.patch Both applications need to set environment variable QT_GSTREAMER_CAMERABIN_VIDEOSRC to use imxv4l2src If camera device is other than /dev/video0, set environment variable QT_GSTREAMER_CAMERABIN_VIDEOSRC_DEVICE to the right camera device, such as "/dev/video1" ,  for example: export QT_GSTREAMER_CAMERABIN_VIDEOSRC=imxv4l2src export DISPLAY=:0 export QT_GSTREAMER_CAMERABIN_VIDEOSRC_DEVICE="/dev/video1" By default, the “post-preview” feature of camerabin was disabled by the patches provided, since the imxv4l2src can’t work with “post-preview” internal “videoconvert” element. To enable “post-preview”  feature, one need uncomment following line //g_object_set(G_OBJECT(m_camerabin), POST_PREVIEWS_PROPERTY, TRUE, NULL); in “/qtmultimedia/src/plugins/gstreamer/camerabin/camerabinsession.cpp”, Function: CameraBinSession::CameraBinSession(GstElementFactory *sourceFactory, QObject *parent) And Change “videoconvert” to “imxvideoconvert_g2d” or “imxvideoconvert_ipu” or “imxvideoconvert_pxp” in line : csp = gst_element_factory_make ("videoconvert", "preview-vconv"); of  file “/gstreamer1.0-plugins-bad/gst-libs/gst/basecamerabinsrc/gstcamerabinpreview.c”  function: GstCameraBinPreviewPipelineData *gst_camerabin_create_preview_pipeline (GstElement * element,   GstElement * filter)
View full article
i.MX6 Series - Crystal Drive Level guidance; includes calculator.  
View full article
This example makes use of a U-Boot image as a bootloader. U-Boot is commonly used as a bootloader for Linux devices and is provide by the Freescale Linux BSP. The default memory layout of the Freescale U-Boot port can be modified to meet the encrypted boot requirements. This is shown in figure 5. As it can be seen, this layout is similar to any other U-Boot port, with the addition of the security mechanisms appended at the end of the image.                          Figure  Chosen memory layout of the encrypted u-boot 1)Assumptions In designing a U-Boot image as an encrypted boot solution, there are three assumptions which accelerate and simplify the construction process. . The U-boot image can be build for multiple board configuration, but for demonstration purposes this example uses i.MX6 Solo X . The user is familiar with the secure configuration for U-Boot and is able to properly sign and boot a U-Boot image. . The encrypted image will be constructed by an individual party, and there is no need to worry about provisioning the DEK. 2)Requirements The components required to build an encrypted image are shown below. Note that the majority of these components are the product of following the signing U-Boot image procedure.    a)Code Signing Tool in encryption mode o To build the CST in encryption mode, run the following command make OSTYPE=linux ENCRYPTION=yes HAB_RELEASE=~/hab/hab_release release o Note: that CST is not in encryption mode by default. This feature needs to be enabled before encrypting the bootloader image. The performance of the CST might be affected, due to its dependency on the host entropy. Refer to the CST User Guide for more details.   b) iMX6 Solo X device in secure mode   c) U-Boot image with secure boot support enabled. o To configure U-Boot to be built with secure boot support, CONFIG_SECURE_BOOT will need to be defined in the board header file (i.e. at include/configs/mx6q_arm2.h)   d) Signed U-Boot image o A U-Boot image with a CSF and digital signature attached. 3) Implementation Many different implementations for constructing a encrypted U-boot image are possible. The right implementation depends on the solution’s requirement. The presented implementation is intended to provide the foundation principles; it can be modified to meet different needs.
View full article
1. Set up HDMI Set up your kernel to use HDMI adding the following code to bootargs on u-boot: video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 2. Test raw audio In order to test only raw audio, use the following command: aplay -D hw:1,0 Kaleidoscope.wav 3. Make HDMI audio the default output In order to configure audio output over HDMI, please, replace content of file ~/.asoundrc to the following one pcm.dmix_48000{      type dmix      ipc_key 5678293      ipc_key_add_uid yes      slave{           pcm "hw:1,0"           period_time 0           period_size 2048           buffer_size 24576           format S16_LE           rate 48000      } } pcm.!dsnoop_44100{      type dsnoop      ipc_key 5778293      ipc_key_add_uid yes      slave{           pcm "hw:0,0"           period_time 0           period_size 2048           buffer_size 24576           format S16_LE           rate 44100      } } pcm.!dsnoop_48000{      type dsnoop      ipc_key 5778293      ipc_key_add_uid yes      slave{           pcm "hw:1,0"           period_time 0           period_size 2048           buffer_size 24576           format S16_LE           rate 48000      } } pcm.asymed{      type asym      playback.pcm "dmix_48000"      capture.pcm "dsnoop_44100" } pcm.dsp0{      type plug      slave.pcm "asymed" } pcm.!default{      type plug      route_policy "average"      slave.pcm "asymed" } ctl.mixer0{      type hw      card 0 } This will configure alsa to use sound card hw:1,0. Please, pay attention to use the proper audio card name for your device. In order to see available sound cards on board: root@imx53qsb:~# aplay -l **** List of PLAYBACK Hardware Devices **** card 0: imx3stack [imx-3stack], device 0: SGTL5000 SGTL5000-0 []   Subdevices: 1/1   Subdevice #0: subdevice #0 card 1: imx3stackspdif [imx-3stack-spdif], device 0: IMX SPDIF mxc spdif-0 []   Subdevices: 1/1   Subdevice #0: subdevice #0 For detail on how to create asound.conf, please see alsa-lib configuration introduction. 4. Encoded audio For encoded (i.e. AC3, DTS) audio, you can use, for example, ac3dec, an utility provided by alsa-tools with the following command line: ac3dec -D hw:1,0 -C test.ac3 This would work for both HDMI audio and SPDIF audio. Double check your hardware and/or schematic in order to know which one to use.
View full article
Splash Screen on U-boot for i.MX25 PDK Having a bitmap on the LCD a few seconds after boot is a requirement on several embedded systems, u-Boot supports this feature. However, currently, the code provided on Freescale's BSP only implements support for the LCD controller on Linux. This page provides instructions to add support for the LCDC on the u-boot. 1 - Install Freescale i.MX25 BSP, SDK 1.7 It is available on www.freescale.com. If needed follow the getting started section instructions. 2 - Update u-boot source After installing the BSP and running LTIB for the first time, it's time to update u-boot: - Download u-Boot patch and spec file. - Replace the file "u-boot.spec.in" located at <ltib_path>/config/platform/imx by the one downloaded - Copy the "u-boot-2009.08-1273860148.patch" downloaded to /opt/freescale/pkgs 3 - Extract and rebuild u-boot - To extract the source and aply the patch run: <Ltib_path>$ ./ltib -p u-boot -m prep - Now Build:     <Ltib_path>$ ./ltib -p u-boot -m scbuild    After completing this step an u-Boot binary (u-boot.bin) will be saved at <ltib_path>/rpm/BUILD/u-boot-2009.08 4 - Program the SD card Program a SD card with the new u-Boot binary and a bitmap image to be displayed. Insert the SD and run:      $sudo dd if=<ltib_path>/rpm/BUILD/u-boot-2009.08/u-boot.bin of=/dev/mmcblk0 bs=512 "/dev/mmcblk0" should replaced according to your host, use "dmesg" after inserting the SD to find out where is the SD on your host. Unmount it before issuing the dd command. $sudo dd if="your_image".bmp of=/dev/mmcblk0 bs=512 seek=608 Argument seek 608, skips the first 608 blocks of the SD (608x512) where the uboot is stored. If you need to relocate the image, update also the environment variable "splashimage_mmc_init_block", see step 6. 5 - Boot Boot the image from the SD. Personality Board settings:   12345678 SW22 -> 00000000 SW21 -> 11000000    Debug Board settings: SW5,6,7,8,9,10 -> OFF      12345678 SW4 -> 10000001 Turn on the board and stop at u-boot prompt: MX25 U-Boot > 6 - u-Boot environment variables Update u-Boot environment variables for the splash screen to work: The address in memory to load the splash screen from: MX25 U-Boot > setenv splashimage 0x80800000 The SD device on the board: MX25 U-Boot > setenv splashimage_mmc_dev 0 The block on the SD where the bitmap is stored, this must match the block on step 4. MX25 U-Boot > setenv splashimage_mmc_init_block 0x260  The amount in blocks to be read from the SD card, this depends on the bitmap size, i.e. for a 308278 bytes bitmap, 0x2B5 blocks are enough on a 512 bytes per block SD, (308278 / 512). MX25 U-Boot > setenv splashimage_mmc_blkcnt 0x2b5 The SD card block size in bytes: MX25 U-Boot > setenv splashimage_mmc_blksize 512 Save the environment variables: MX25 U-Boot > saveenv Now reboot the board and you should see the splash screen on the LCD. 7 - Booting Linux When Linux takes control of the board it initializes the LCD controller and Framebuffer again. To maintain the splash screen on the LCD you can replace the Linux Logo with the figure used for the splash screen, the side effect is a blink when Linux takes over the LCDC. To achieve this, create a new image in Gimp and save it as ".ppm". Copy it to Linux "logo" folder <ltib_path>/rpm/BUILD/linux-2.6.31/drivers/video/logo Run: $ ppmquant -mapfile clut_vga16.ppm "my_image.ppm" | pnmnoraw > logo_linux_vga16.ppm where: logo_linux_vga16.ppm is the current logo being used by Linux. Recompile the kernel and boot it.
View full article
     This documents shows how to secure and encrypt boot loader image for i.MX6 processor. Secure boot is necessary to be sure that CPU is allowed to run genuine and authentic images. Encrypted image secures your intellectual property from theft. Both methods secure/encryption can be extended to cover whole software on board. Boot loader image encryption is easy to do with CST tools and HAB feature build in Freescale processor. Encrypted image preparation is consist of three parts: Encrypt u-boot.imx plain image by CST utility; Wrap DEK to get DEK blob by specific board; Append DEK blob key to the u-boot image. In this document as reference board we used SABRESD iMX6q. But it's easily to adjust it for any other board based on i.MX6 CPU with HAB4.1 feature. Encrypted u-boot image consist of: IVT, DCD, u-boot.bin, CSF, dek_blob.bin. In our example finished u-boot_encrypted.imx image looks like: Address in file Data 0x000000 IVT 0x000020 DCD + pad to address 0xC00 0x000C00 u-boot.bin + pad to address* 0x7BC000 0x07DBB8 CSF bin data + pad to address** 0x07DBB8 + Wrapped DEK (dek_blob.bin)** * (IVT + DCD + u-boot.bin) has to be padded to align 0x1000. ** (CSF bin data + padding + dek_blob.bin) has to have size 0x2000 Step-by-step instruction: Clone u-boot git repository. $ mkdir ~/imx6encryption $ cd ~/imx6encryption $ git clone git://git.denx.de/u-boot.git $ cd u-boot $ git checkout v2016.03 -b tmp To enable secure features in u-boot modify the following files: Add function usec2ticks to the end of file timer.c. $ nano arch/arm/imx-common/timer.c unsigned long usec2ticks(unsigned long usec) {         ulong ticks;         if (usec < 1000)                 ticks = ((usec * (get_tbclk()/1000)) + 500) / 1000;         else                 ticks = ((usec / 10) * (get_tbclk() / 100000));         return ticks; } Press Ctrl+X and Y and Enter to save changes. In file mx6q_4x_mt41j128.cfg add string CSF 0x2000 after string BOOT_FROM sd $ nano board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg Press Ctrl+X and Y and Enter to save changes. Add defines in file mx6sabresd.h before string #define CONFIG_MACH_TYPE 3980. $ nano include/configs/mx6sabresd.h #define CONFIG_SECURE_BOOT #define CONFIG_SYS_FSL_SEC_COMPAT    4 /* HAB version */ #define CONFIG_FSL_CAAM #define CONFIG_CMD_DEKBLOB #define CONFIG_SYS_FSL_SEC_LE #define CONFIG_FAT_WRITE Press Ctrl+X and Y and Enter to save changes. Delete the following strings: gpimage.0 \ gpimage-common.o \ omapimage.o \ in Makefile. $ nano tools/Makefile Press Ctrl+X and Y and Enter to save changes Download Linaro GCC compiler. $ cd ~/imx6encryption $ wget -c https://releases.linaro.org/components/toolchain/binaries/5.3-2016.02/arm-linux-gnueabihf/gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf.tar.xz $ tar xf gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf.tar.xz $ export CC=`pwd`/gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf- Check compiler version. $ ${CC}gcc --version Output: arm-linux-gnueabihf-gcc (Linaro GCC 5.3-2016.02) 5.3.1 20160113 Copyright (C) 2015 Free Software Foundation, Inc. This is free software; see the source for copying conditions.  There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. Build u-boot image with mx6qsabresd_defconfig. $ cd u-boot $ make ARCH=arm CROSS_COMPILE=${CC} distclean $ make ARCH=arm CROSS_COMPILE=${CC} mx6qsabresd_defconfig $ make ARCH=arm CROSS_COMPILE=${CC} Using mkimage utility build and get information of u-boot.imx image. $ ./tools/mkimage -T imximage -n board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg.cfgtmp -e 0x17800000 -d u-boot.bin u-boot.imx Output: Image Type:   Freescale IMX Boot Image Image Ver:    2 (i.MX53/6/7 compatible) Data Size:    516096 Bytes = 504.00 kB = 0.49 MB Load Address: 177ff420 Entry Point:  17800000 HAB Blocks:   177ff400 00000000 0007bc00 Register an account on NXP website to have access to download NXP Code Signing Tool for the High Assurance Boot library. Copy downloaded archive into “imx6encryption” folder. $ cd ~/imx6encryption $ tar xf cst-2.3.1.tar.gz $ cd cst-2.3.1 $ chmod u+x linux64/* keys/* Compile back end sources of CST utility $ sudo apt-get install libssl-dev $ cd ~/imx6encryption/cst-2.3.1/code/back_end/src $ gcc -o cst -I ../hdr -L ../../../linux64/lib *.c -lfrontend -lcrypto $ mv cst ../../../linux64 Generate keys and certificates which will be used to sign boot loader image. $ cd ~/imx6encryption/cst-2.3.1/keys Create file serial. $ nano serial Enter 8 random digits, for example: 12345678 Press Ctrl+X and Y and Enter to save changes. Create key_pass.txt $ nano key_pass.txt Enter two lines of identical text: HelloWorld HelloWorld Press Ctrl+X and Y and Enter to save changes. Execute hab4_pki_tree.sh. $ ./hab4_pki_tree.sh Do you want to use an existing CA key (y/n)?: n Enter key length in bits for PKI tree: 2048 Enter PKI tree duration (years): 10 How many Super Root Keys should be generated? 4 Do you want the SRK certificates to have the CA flag set? (y/n)?: y Generate SRK table. $ cd ~/imx6encryption/cst-2.3.1/crts $ ../linux64/srktool -h 4 -t SRK_1_2_3_4_table.bin -e SRK_1_2_3_4_fuse.bin -d sha256 -c ./SRK1_sha256_2048_65537_v3_ca_crt.pem,./SRK2_sha256_2048_65537_v3_ca_crt.pem,./SRK3_sha256_2048_65537_v3_ca_crt.pem,./SRK4_sha256_2048_65537_v3_ca_crt.pem -f 1 CST utility requires CSF script. This file describes certificates, keys and the data ranges used in sign and encryption functions. Create u-boot.csf file. $ cd ~/imx6encryption/cst-2.3.1/linux64 $ nano u-boot.csf And put the following text: [Header] Version = 4.1 Hash Algorithm = SHA256 Engine Configuration = 0 Certificate Format = X509 Signature Format = CMS Engine = CAAM [Install SRK] File = "../crts/SRK_1_2_3_4_table.bin" # Index of the key location in the SRK table to be installed Source index = 0 [Install CSFK] # Key used to authenticate the CSF data File = "../crts/CSF1_1_sha256_2048_65537_v3_usr_crt.pem" [Authenticate CSF] [Unlock] Engine = CAAM Features = RNG [Install Key] # Key slot index used to authenticate the key to be installed Verification Index = 0 # Key to install Target Index = 2 File = "../crts/IMG1_1_sha256_2048_65537_v3_usr_crt.pem" [Authenticate Data] # Key slot index used to authenticate the image data Verification Index = 2 #       Address   Offset        Length      Data File Path Blocks = 0x177ff400 0x00000000 0x00000C10 "./u-boot.imx" #Encrypt the boot image and create a DEK [Install Secret Key] Verification Index = 0 Target Index = 0 Key = "./dek.bin" Key Length = 128 Blob Address = 0x1787CFB8 #Provide DEK blob location to decrypt [Decrypt Data] Verification Index = 0 Mac Bytes = 16 Blocks = 0x17800010 0x00000C10 0x0007AFF0 "./u-boot.imx" Press Ctrl+X and Y and Enter to save changes. Execute CST utility to encrypt image. Note that after execution u-boot.imx file will be encrypted. $ cp ~/imx6encryption/u-boot/u-boot.imx . $ ./cst --o u-boot_csf.bin < u-boot.csf $ objcopy -I binary -O binary --pad-to=0x1FB8 --gap-fill=0x00 u-boot_csf.bin u-boot_csf.bin Prepare SD card partition table. Check SD card name in system ($dmesg | tail), for example used /dev/sdb. $ echo -e "o""\n""n""\n""p""\n""1""\n""2048""\n""+256M""\n""w" | sudo fdisk /dev/sdb $ sudo mkfs.vfat /dev/sdb1 $ cd ~/imx6encryption/u-boot $ sudo dd if=u-boot.imx of=/dev/sdb bs=512 seek=2 $ sync Wrap DEK to get DEK blob from i.MX6 CPU. Mount partition 1 and copy dek.bin file to the 1st FAT partition on SD card. $ cd ~/imx6encryption/cst-2.3.1/linux64 $ mkdir /tmp/partition0 $ sudo mount /dev/sdb1 /tmp/partition0 $ sudo cp dek.bin /tmp/partition0 $ sudo umount /tmp/partition0 Insert SD card into the board. And press any key to enter into u-boot prompt. Firstly load dek.bin to the RAM memory. Use dek_blob command to wrap dek.bin. Write file from RAM memory to SD card. => fatload mmc 1:1 0x10800000 dek.bin => dek_blob 0x10800000 0x10801000 128 => fatwrite mmc 1:1 0x10801000 dek_blob.bin 0x48 Append DEK blob key to the u-boot image. Mount SD card partition 1 and copy dek_blob.bin file to the linux64 folder. $ mkdir -p /tmp/partition0 $ sudo mount /dev/sdb1 /tmp/partition0 $ cd /tmp/partition0 $ cp dek_blob.bin ~/imx6encryption/cst-2.3.1/linux64/ $ cd ~/imx6encryption/cst-2.3.1/linux64/ $ sudo umount /tmp/partition0 $ cat u-boot_csf.bin >> u-boot.imx $ cat dek_blob.bin >> u-boot.imx Install encrypted u-boot.imx into SD card. $ sudo dd if=u-boot.imx of=/dev/sdb bs=512 seek=2 $ sync Insert SD card into the board. Press any key to enter into u-boot prompt. And check if hab_status command executes without HAB Event errors. => hab_status Attention, OTP fuses can be programmed once, double check everything before burning. If everything is fine, burn required fuses SRK_HASH, SEC_CONFIG as described in AN4581. As a result we have encrypted boot image which can be loaded and executed by only current board. Because dek_blob.bin is unique per i.MX6 CPU. Vitaliy Vasinovich April 2016
View full article
Design Check Lists: HW Design Checking List for i.MX6DQSDL HW Design Checking List for i.Mx53 Hardware Design Checklist for i.MX28 HW_Design_Checking_List_for_i.MX6SoloX i.MX6UL Hardware design checklist   DDR Design Tool: I.MX53 DDR3 Script Aid imx53 DDR stress tester V0.042 i.Mx6DQSDL DDR3 Script Aid MX6DQP DDR3 Script Aid i.Mx6DQSDL LPDDR2 Script Aid i.Mx6SL LPDDR2 Script Aid i.MX6SX DDR3 Script Aid I.MX6UL DDR3 Script Aid i.MX6UL_LPDDR2_Script_Aid i.MX6ULL_DDR3_Script_Aid  i.MX6ULL_LPDDR2_Script_Aid  MX6SLL_LPDDR2_Script_Aid  MX6SLL_LPDDR3_Script_Aid  i.MX6 DDR Stress Test Tool V1.0.3 i.MX6/7 DDR Stress Test Tool V3.00 i.MX8MSCALE DDR Tool Release  i.MX8M DDR3L register programming aid  i.MX 8/8X Family DDR Tools Release   Application Notes: MX_Design_Validation_Guide I.MX6 series USB Certification Guides
View full article
The i.MX Android N7.1.2_2.0.0 GA release is now available on IMX_SW page.   Files available: # Name Description 1 android_N7.1.2_2.0.0_docs.tar.gz i.MX Android N7.1.2_2.0.0 BSP Documentation 2 android_N7.1.2_2.0.0_source.tar.gz Source Code of Android N7.1.2_2.0.0 BSP (4.1 kernel) for i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo i.MX 6Sololite, i.MX6SX and i.MX7D 3 android_N7.1.2_2.0.0_image_6dqpsabreauto.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE for Automotive Infotainment based on i.MX 6QuadPlus, i.MX 6Quad, and i.MX 6DualLite 4 android_N7.1.2_2.0.0_image_6dqpsabresd.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE Platform and SABRE Board based on i.MX 6QuadPlus, i.MX 6Quad and i.MX 6DualLite. 5 android_N7.1.2_2.0.0_image_6slevk.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - i.MX 6Sololite evaluation kit. 6 android_N7.1.2_2.0.0_image_6sxsabresd.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE Board based on i.MX 6SoloX 7 android_N7.1.2_2.0.0_image_6sxsabreauto.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE for Automotive infotainment based on i.MX 6SoloX 8 android_N7.1.2_2.0.0_image_7dsabresd.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE Board based on i.MX 7Dual 9 fsl_aacp_dec.tar.gz AAC Plus Codec for N7.1.2_2.0.0 10 android_N7.1.2_2.0.0_tools.tar.gz Manufacturing Toolkit and VivanteVTK for N7.1.2_2.0.0   Supported Hardware SoC/Boards: i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-SD board and platform i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI board and platform i.MX 6SoloLite EVK platform i.MX 6SoloX SABRE-SD board and platforms i.MX 6SoloX SABRE-AI board and platforms i.MX 7Dual SABRE-SD board and platform   Changes: Compared to the N7.1.1_1.0.0 release, this release has the following major changes: Upgraded the Android code base from android-7.1.1_r13 to android-7.1.2_r9. Upgraded U-Boot from v2015.04 to v2017.03. Upgraded the kernel from v4.1.15 to v4.9.17. Upgraded the GPU driver from 6.2.0.p2 to 6.2.2.p1. Upgraded the Wi-Fi BCMDHD release version to 1.141.100.6. Refine the Gralloc and HWC HAL. Enable the GPT partition to replace the MBR partition.   Feature: For features please consult the release notes.   Known issues For known issues and more details please consult the Release Notes.
View full article
According to EHSET_v1.01.pdf description (http://testusb.com/EHHS.html), the USB physical certification test are from 2 sides. One test case is PC running USB-IF HSET utility as being USB host to test the target board being USB device; the other case is target board acting as USB host to initate test signals to a test fixture. The principle of test modes supported are based on Vid/Pid pair  during enumration by host whoever takes. Apply the attached patch (I use r13.4.1 kernel_imx tree), then enable "FSL_USB_TEST_MODE" in kernel config, rebuild uImage to get the test modes support kernel.
View full article
In this article, some experiments are done to verify the capability of i.MX6DQ on video playback under different VPU clocks. 1. Preparation Board: i.MX6DQ SD Bitstream: 1080p sunflower with 40Mbps, it is considered as the toughest H264 clip. The original clip is copied 20 times to generate a new raw video (repeat 20 times of sun-flower clip) and then encapsulate into a mp4 container. This is to remove and minimize the influence of startup workload of gstreamer compared to vpu unit test. Kernels: Generate different kernel with different VPU clock setting: 270MHz, 298MHz, 329MHz, 352MHz, 382MHz. test setting: 1080p content decoding and display with 1080p device. (no resize) 2. Test command for VPU unit test and Gstreamer The tiled format video playback is faster than NV12 format, so in below experiment, we choose tiled format during video playback. Unit test command: (we set the frame rate -a 70, higher than 1080p 60fps HDMI refresh rate)     /unit_tests/mxc_vpu_test.out -D "-i /media/65a78bbd-1608-4d49-bca8-4e009cafac5e/sunflower_2B_2ref_WP_40Mbps.264 -f 2 -y 1 -a 70" Gstreamer command: (free run to get the highest playback speed)     gst-launch filesrc location=/media/65a78bbd-1608-4d49-bca8-4e009cafac5e/sunflower_2B_2ref_WP_40Mbps.mp4 typefind=true ! aiurdemux ! vpudec framedrop=false ! queue max-size-buffers=3 ! mfw_v4lsink sync=false 3. Video playback framerate measurement During test, we enter command "echo performance > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor" to make sure the CPU always work at highest frequency, so that it can respond to any interrupt quickly. For each testing point with different VPU clock, we do 5 rounds of tests. The max and min values are removed, and the remaining 3 data are averaged to get the final playback framerate. #1 #2 #3 #4 #5 Min Max Avg Dec Playback Dec Playback Dec Playback Dec Playback Dec Playback Playback Playback Playback 270M unit test 57.8 57.3 57.81 57.04 57.78 57.3 57.87 56.15 57.91 55.4 55.4 57.3 56.83 GST 53.76 54.163 54.136 54.273 53.659 53.659 54.273 54.01967 298M unit test 60.97 58.37 60.98 58.55 60.97 57.8 60.94 58.07 60.98 58.65 57.8 58.65 58.33 GST 56.755 49.144 53.271 56.159 56.665 49.144 56.755 55.365 329M unit test 63.8 59.52 63.92 52.63 63.8 58.1 63.82 58.26 63.78 59.34 52.63 59.52 58.56667 GST 57.815 55.857 56.862 58.637 56.703 55.857 58.637 57.12667 352M unit test 65.79 59.63 65.78 59.68 65.78 59.65 66.16 49.21 65.93 57.67 49.21 59.68 58.98333 GST 58.668 59.103 56.419 58.08 58.312 56.419 59.103 58.35333 382M unit test 64.34 56.58 67.8 58.73 67.75 59.68 67.81 59.36 67.77 59.76 56.58 59.76 59.25667 GST 59.753 58.893 58.972 58.273 59.238 58.273 59.753 59.03433 Note: Dec column means the vpu decoding fps, while Playback column means overall playback fps. Some explanation: Why does the Gstreamer performance data still improve while unit test is more flat? On Gstreamer, there is a vpu wrapper which is used to make the vpu api more intuitive to be called. So at first, the overall GST playback performance is constrained by vpu (vpu dec 57.8 fps). And finally, as vpu decoding performance goes to higher than 60fps when vpu clock increases, the constraint becomes the display refresh rate 60fps. The video display overhead of Gstreamer is only about 1 fps, similar to unit test. Based on the test result, we can see that for 352MHz, the overall 1080p video playback on 1080p display can reach ~60fps. Or if time sharing by two pipelines with two displays, we can do 2 x 1080p @ 30fps video playback. However, this experiment is valid for 1080p video playback on 1080p display. If for interlaced clip and display with size not same as 1080p, the overall playback performance is limited by some postprocessing like de-interlacing and resize.
View full article
Overview The purpose of this doument is to introduce how to enable PCIe WiFi into i.MX6 Android release. Environment Setup Hardware: i.MX6 SABRE-SD board Software: Android Jelly Bean 4.2 Software Configurations The source codes of Intel PCIe WiFi have been integrated for i.MX6 SABRE-SD board into i.MX6 Android release. However it's disabled by default. To enable it for i.MX6 SABRE-SD board, you can do the following: Change BOARD_WLAN_VENDOR to INTEL in device/fsl board configuration files. For example, diff --git a/sabresd_6dq/BoardConfig.mk b/sabresd_6dq/BoardConfig.mk index 9c8a32d..912e752 100755 --- a/sabresd_6dq/BoardConfig.mk +++ b/sabresd_6dq/BoardConfig.mk @@ -11,7 +11,7 @@ TARGET_BOOTLOADER_BOARD_NAME := SABRESD PRODUCT_MODEL := SABRESD-MX6DQ # Wifi -BOARD_WLAN_VENDOR                       := ATHEROS +BOARD_WLAN_VENDOR                       := INTEL # for atheros vendor ifeq ($(BOARD_WLAN_VENDOR),ATHEROS) BOARD_WLAN_DEVICE                       := ar6003 @@ -30,6 +30,7 @@ WIFI_COMPAT_MODULE_ARG                         := "" endif #for intel vendor ifeq ($(BOARD_WLAN_VENDOR),INTEL) +BOARD_WLAN_DEVICE                       := INTEL BOARD_HOSTAPD_PRIVATE_LIB               ?= private_lib_driver_cmd BOARD_WPA_SUPPLICANT_PRIVATE_LIB        ?= private_lib_driver_cmd WPA_SUPPLICANT_VERSION                  := VER_0_8_X After changing BOARD_WLAN_VENDOR as "INTEL", the following files will be compiled for intel WiFi: device/fsl-proprietary/pcie-wifi/ external/wpa_supplicant_8 hardware/imx/wlan/intel/ hardware/libhardware_legacy/wifi/wifi_intel.c Enable PCIe WiFi driver in kernel_imx by running "make menuconfig" command: Select "System Type -> Freescale MXC Implementations -> PCI Express support" as "*" Select "Networking support -> Wireless ->  cfg80211 - wireless configuration API" as "*". Then select "Networking support -> Wireless -> Generic IEEE 802.11 Networking Stack (mac80211)" as "*" Select "Device Drivers ->  Network device support -> Wireless LAN -> Intel Wireless WiFi 4965AGN (iwl4965)" as "*" Then run "make" command to build kernel. The followings are the dependencies files to enable above configuration: Kernel configuration: * -> System Type -> Freescale MXC Implementations Select the PCI Express support. Then config intel WIFI driver: Generic IEEE 802.11 Networking Stack (mac80211) used by WIFI devices Symbol: MAC80211 [=y] Type : tristate Prompt: Generic IEEE 802.11 Networking Stack (mac80211) Defined at net/mac80211/Kconfig:1 Depends on: NET [=y] && WIRELESS [=y] && CFG80211 [=y] Location: -> Networking support (NET [=y]) -> Wireless (WIRELESS [=y]) Intel iwl4965 or iwl6300 card driver Symbol: IWL4965 [=y] Type : tristate Prompt: Intel Wireless WiFi 4965AGN (iwl4965) Defined at drivers/net/wireless/iwlegacy/Kconfig:65 Depends on: NETDEVICES [=y] && WLAN [=y] && PCI [=y] && MAC80211 [=y] Location: -> Device Drivers -> Network device support (NETDEVICES [=y]) Then you can follow up the instructions into Android User guide to build Android image. Known Limitation PCIe low power mode is not supported according to BSP release note. So when building in PCIe, the system suspend/resume should be disabled now.
View full article
   The purpose of this article is to describe how to join together the Processor Expert and ARM GCC toolchain under Eclipse environment.    Freescale provides the Processor Expert, which contains the Pin Settings Tool to support an easy way to configure pin signals, from multiplexing to the electrical properties of pins. With such Tool all the pins can be configured with a graphical user interface, and then generate C code, in order to use it as an example in applications. Please refer to the following Web for more details. http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PROCESSOR-EXPERT-IMX   The Processor Expert Software for i.MX Processors (Version 1.0) does not include a compiler or linker. Customers should merge the generated code into a build system.   However, it is possible to use common Eclipse-based IDE for the Processor Expert (V 1.0) and GNU ARM “C” toolchains. In particular, the following sequence may be implemented for both Linux and Windows hosts. 1. Install Eclipse (Kepler release) IDE for C/C++ Developers. https://eclipse.org/downloads/packages/eclipse-ide-cc-developers/keplersr2 2. Add Eclipse Processor Expert plug-in, as recommended in the documentation. http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PROCESSOR-EXPERT-IMX https://community.freescale.com/docs/DOC-101470 3.  Add GNU ARM Eclipse, which contains configurations for different toolchains, including Linux ones. http://gnuarmeclipse.livius.net/blog/plugins-install/ 4. Install appropriate toolchain. For bare-metal applications Sourcery CodeBench Lite for ARM is sutable one. Sourcery CodeBench Lite Edition including ARM GCC IDE - Mentor Graphics Please use Getting Started Guide document from the CodeBench Lite package, that explains how to install and build applications with the CodeBench Lite.    As an example, let’s consider minimal startup code for i.MX6Q (LED flickering project on i.MX6Q SDB / SDP). Assuming Eclipse IDE with the Processor Expert and GNU ARM tools is installed, we should create new “C” project under Eclipse : New -> C Project. Select “Empty Project” and “Cross ARM GCC”, enter “Project name”. Then : select “Advanced settings” -> C/C++ Build -> Settings Tab “Target Processor” : ARM Family : cortex – a9 Architecture : armv7-a Instruction set : ARM (-marm) Endianness : Little endian (-mlittle-endian) FloatABI : Library with FP (softfp) FPU Type : neon Unaligned access : Disabled (-mno-unaligned-access) “Cross ARM GNU Create Flash Image” : General : Raw binary. TAB “Toolchains” : Name : Sourcery CodeBench Lite for ARM EABI (arm-none-eabi-gcc) (If needed customers can select appropriate toolchain) Architecture : ARM (AArch32) Prefix : arm-none-eabi Check “Use global toolchain path” or select the required path directly.  Source codes may added via Eclipse : File -> Import -> File System -> From directory Example source is enclosed. After sources as included in the project, let’s configure linker options via project properties, C/C++ Build -> Settings -> Tool Settings -> Cross ARM C Linker -> General. Add script file “mx6dq.ld”, uncheck “Remove unused section”, check “Do not use standard start files”.   Note, the article of Miro Samek is very helpful in clarifying of startup code and linker script. Please refer to “Building Bare-Metal ARM Systems with GNU”. Article Published online at www.Embedded.com,  July/August 2007. So, now we can build the project : Project -> Build Project. Two executable file will be generated : test.elf (for JTAG debugger) and test.bin, which may be used to create bootable SD card, using cfimager-imx.exe utility : CMD> cfimager-imx -o 0 -f test.bin -d g: Please use readme files in the enclosed for more details.
View full article
Build the tool chain image. It generates the toolchain that will be installed on your host machine and used to build any source code: $ bitbake meta-toolchain It does take some time to build. Why to create a toolchain? Yocto is not intended to be used to package development. Yocto is a linux distribution creator. It´s intended to be a image builder, a rootfs creator. (please, see more about "what is yocto" here and here) So, yocto itself should not be used to "develop" a new package. Although, Yocto can help creating a environment for development like meta-toolchain or Eclipse ADT. Go HOME Go Task #6 - Customize the image
View full article
Here we show how to bootstrap the Debian Linux distribution from a PC to the i.MX6 sabre sd platform. While bootstrapping Debian on any architecture "natively" is pretty straightforward, "cross-bootstrapping" requires some techniques that we will explain. This document assumes you are able to boot a Linux kernel on your platform already. See this post for details on how to do it. Also, this document assumes you are using a Debian PC for preparing your SD card. You will require the following packages to be installed: binfmt-support qemu-user-static debootstrap Note: all the commands found in the following steps need to be run as root. Formatting the SD card We need to format the SD card with two partitions; one small FAT partition to contain the Linux kernel and its dtb, and one large ext4 partition, which will contain the root filesystem with the Debian userspace. Also, we need to make sure we leave some space for u-boot starting from offset 1024B. Here is an example SD card layout:   +-----+------+--------+-----+---------------+-----------------   | MBR |  ... | u-boot | ... | FAT partition | Linux partition ...   +-----+------+--------+-----+---------------+-----------------   0     512    1024           1M              ~257M (offsets in bytes) Here is an example SD card layout, as displayed by fdisk:   Device    Boot      Start         End      Blocks   Id  System   /dev/sdc1            2048      526335      262144    c  W95 FAT32 (LBA)   /dev/sdc2          526336     8054783     3764224   83  Linux (units: 512B sectors) You can format and mount the Linux partition with:   # mkfs.ext4 /dev/<your-sd-card-second-partition>   # mount /dev/<your-sd-card-second-partition> /mnt Your SD card second partition is typically something in /dev/sd<X>2 or /dev/mmcblk<X>p2. Do not forget to install u-boot and a Linux kernel as explained in those posts. Bootstrapping Debian First stage The first stage of Debian bootstrapping is done with:   # debootstrap --foreign --arch=armhf testing /mnt This will retrieve the base Debian packages from the internet, and perform a first stage of installation:   I: Retrieving Release   I: Retrieving Release.gpg   I: Checking Release signature   I: Valid Release signature (key id A1BD8E9D78F7FE5C3E65D8AF8B48AD6246925553)   I: Validating Packages   I: Resolving dependencies of required packages...   I: Resolving dependencies of base packages...   I: Found additional required dependencies: insserv libbz2-1.0 libcap2 libdb5.1 libsemanage-common libsemanage1 libslang2 libustr-1.0-1   I: Found additional base dependencies: libee0 libept1.4.12 libestr0 libgcrypt11 libgnutls-openssl27 libgnutls26 libgpg-error0 libidn11 libjson-c2 liblognorm0 libmnl0 libnetfilter-acct1 libnfnetlink0 libp11-kit0 libsqlite3-0 libtasn1-3 libxapian22   I: Checking component main on http://ftp.us.debian.org/debian...   (...)   I: Extracting util-linux...   I: Extracting liblzma5...   I: Extracting zlib1g... At this point, the necessary tools for second stage of installation are under /mnt/debootstrap/. Second stage The second stage needs to run natively; on an arm platform, that is. But we can use the combination of two techniques to perform this stage on the PC anyway:   # cp /usr/bin/qemu-arm-static /mnt/usr/bin/   # chroot /mnt /debootstrap/debootstrap --second-stage Those commands copy an arm emulator on the target filesystem, and use the chroot command to execute the second stage of the installation into the SD card, on the PC, with transparent emulation:   I: Installing core packages...   I: Unpacking required packages...   I: Unpacking libacl1:armhf...   I: Unpacking libattr1:armhf...   I: Unpacking base-files...   (...)   I: Configuring tasksel...   I: Configuring tasksel-data...   I: Configuring libc-bin...   I: Base system installed successfully. You can now remove /mnt/usr/bin/qemu-arm-static, or keep it for later, subsequent chroot under emulation. Finetuning the root filesystem For development it is handy to remove the root password on the target by removing the '*' from /mnt/etc/shadow on the SD card:   root::15880:0:99999:7::: Also, we can add the following line in /mnt/etc/inittab to obtain a login prompt on the UART:   T0:23:respawn:/sbin/getty -L ttymxc0 115200 vt100 You can now unmount the filesystem with:   # umount /mnt Boot! Your SD card is ready for booting. Insert it in the SD card slot of your i.MX6 sabre sd platform, connect to the USB to UART port with a serial terminal set to 115200 baud, no parity, 8bit data and power up the platform. At the time of writing u-boot tells the kernel to boot from the wrong partition by default, so we need to interrupt by pressing enter at u-boot prompt for the first boot and setup u-boot environment to fix this:   U-Boot > setenv mmcroot /dev/mmcblk0p2 rootwait rw   U-Boot > saveenv   Saving Environment to MMC...   Writing to MMC(1)... done As this is saved in the SD card it need only to be done once at first boot. You can reboot your board or type boot; your Debian system should boot to a prompt:   (...)   [ ok ] Starting periodic command scheduler: cron.   [ ok ] Running local boot scripts (/etc/rc.local).   Debian GNU/Linux jessie/sid debian ttymxc0   debian login: From there you may login as root. It is recommended to setup the network connection and install an ssh server inside the target for further development. Enjoy! See also... With the amounts of memory we have today in the systems, it is even possible to boot Debian in a ramdisk. See this post about busybox for the ramdisk generation. Another way of generating a root filesystem is by building it with buildroot. See and this post for details.
View full article