i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
       
View full article
A new version of the Pins Tool for i.MX Application Processors has been released and is available for download as desktop tool from Pins Tool for i.MX Application Processors|NXP. The pins Tool for i.MX Application Processors is used for pin routing configuration, validation and code generation, including pin functional/electrical properties, power rails, run-time configurations, with the following main features: Desktop application Muxing and pin configuration with consistency checking Multicore support ANSI-C initialization code Graphical processor package view Multiple configuration blocks/functions Easy-to-use device configuration Selection of Pins and Peripherals Package with IP blocks Routed pins with electrical characteristics Registers with configured and reset values Power Groups with assigned voltage levels Source code for C/C++ applications Documented and easy to understand source code CSV Report and Device Tree File Localized for English and Simplified Chinese Mostly Connected: On-Demand device data download Integrates with any compiler and IDE What's New Added Label support to give signals a name Added ‘Log’ and ‘Problems’ view to report conflicts between settings Added support for templates to store user configurations as starting point for new configurations Added ability to download and share data for devices, especially for off-network host machines i.MX header files are now automatically part of the device data Import of legacy Processor Expert .pe files Export of register defines Various bug fixes and documentation improvements The release notes of the desktop application are attached to this article. Import Processor Expert Files A new importer has been added to import legacy Processor Expert for i.MX files: Labels Signals can now have user defined labels: Templates, Kits, Boards and Processors When creating a new configuration, it offers Templates, Boards and Processors. Custom configurations can be stored as templates and then used for new configurations. Board Specific Functions With the provided board and kit configurations, there are now pre-configured initialization functions for major blocks on the board: Export Data To simplify downloading the device specific data for the desktop tool, the 'Export' function can be used to download and export the data. The data can be copied that way to another machine or all data for a set of devices can be loaded. Export Registers With the Export command the registers can be exported as text/source: This is used to store the register values: /*FUNCTION********************************************************************** * * Function Name : init_audmux_pins * Description   : Configures pin routing and optionally pin electrical features. * *END**************************************************************************/ #define INIT_AUDMUX_PINS_IOMUXC_AUD5_INPUT_DA_AMX_SELECT_INPUT_VALUE            0x00000000   /*!< Register name: IOMUXC_AUD5_INPUT_DA_AMX_SELECT_INPUT */ #define INIT_AUDMUX_PINS_IOMUXC_AUD5_INPUT_TXCLK_AMX_SELECT_INPUT_VALUE         0x00000000   /*!< Register name: IOMUXC_AUD5_INPUT_TXCLK_AMX_SELECT_INPUT */ #define INIT_AUDMUX_PINS_IOMUXC_AUD5_INPUT_TXFS_AMX_SELECT_INPUT_VALUE          0x00000000   /*!< Register name: IOMUXC_AUD5_INPUT_TXFS_AMX_SELECT_INPUT */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DI0_PIN02_VALUE                  0x00000002   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DI0_PIN02 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DI0_PIN03_VALUE                  0x00000002   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DI0_PIN03 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DI0_PIN04_VALUE                  0x00000002   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DI0_PIN04 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DI0_PIN15_VALUE                  0x00000002   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DI0_PIN15 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA16_VALUE               0x00000003   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA16 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA18_VALUE               0x00000003   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA18 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA19_VALUE               0x00000003   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA19 */ ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ We hope you will find this new release useful. Thanks for designing with NXP! 
View full article
Overview Measuring the power consumed an i.MX application processor can be a challenging undertaking. This document describes several boards designed to instrument i.MX application boards for current measurements. While this system does not offer many digits of accuracy, it can be used to quantify power consumed by application use cases as well as while in low power modes. The system can be used to instrument up to four power supply rails and measure current in two ranges. Range switching on the sensor boards is controlled via software running on the Kinetis K20 at the heard of the profiler board. Measured data is sent to a host computer over a virtual serial link over USB. Power for the profiler system is obtained from the USB connection although a external 5V supply may be used. Dual-Range Current Sensors INA250 + INA21x Sensor Circuit Description: The INA250 + INA21x Sensor board can measure two ranges using the INA250 and INA21x current sense amplifiers. The high range is measured with an INA250, which has an integrated 0.002 Ohm shunt, and is available in four output gains. The low range is measured with shunt R1 and the INA21x sense amp. The low range shunt is taken out of the circuit (by shorting it) with two paralleled, very low-Rds(on) FETs, Q1 and Q1. VCC_SENSE powers the two sense amplifiers. VCC_FET supplies the gate voltage on Q1 and Q2. The DMN1019 device has a Vgs max of 8V. The sources of both FETs are tied to the i.MX side of the current sense loop, so the gate voltage Q1 and Q2 see is VCC_FET-(rail voltage). The signal /LOW_EN controls the state of both Q1 and Q2. The sense amplifier outputs (HIGH_OUT1 and LOW_OUT1) and rail voltage (V_RAIL_MEASURE) are sent down the ribbon cable (X2) to the profiler board for measurement. When not used for a wire loop for a Hall-effect current probe, resistor R3 should be shorted with a solder bridge, a piece of wire, or a 0.001 Ohm resistor. Schematic: Board Layout: The two large vias by the current sense connection points are provided for use with a 0.1" header and jumper to short the low range shunt, allowing normal operation of the target board when the profiler is not powered. It should be noted a jumper will not be as effective for relatively large currents. BOM: Part   Device C1,C2  0.1uF 0805 Q1,Q2  DMN1019USN-13 SOT23 R1     2 1% 0805 (resize to change low range) R2     10k 0805 R3     Solder bridge/wire loop (see schematic) U1     INA250 TSSOP16 (choose gain, A3 [0.8V/A] or A4 [2.0V/A]) U2     INA21X SC70 (choose desired gain) X2     WM6769CT/0527460871 (bottom contacts) Dual INA21x Sensor Circuit Description: The Dual INA21x Sensor board can measure two ranges using two INA21x current sense amplifiers and two different shunts. The high range shunt (R1) is always in place. The low range shunt is taken out of the circuit (by shorting it) with two paralleled, very low-Rds(on) FETs, Q1 and Q1. VCC_SENSE powers the two sense amplifiers. VCC_FET supplies the gate voltage on Q1 and Q2. The DMN1019 device has a Vgs max of 8V. The sources of both FETs are tied to the i.MX side of the current sense loop, so the gate voltage Q1 and Q2 see is VCC_FET-(rail voltage). The signal /LOW_EN controls the state of both Q1 and Q2. The sense amplifier outputs (HIGH_OUT1 and LOW_OUT1) and rail voltage (V_RAIL_MEASURE) are sent down the ribbon cable (X2) to the profiler board for measurement. Schematic: Board Layout: The two large vias by the current sense connection points are provided for use with a 0.1" header and jumper to short the low range shunt, allowing normal operation of the target board when the profiler is not powered. It should be noted a jumper will not be as effective for relatively large currents. BOM: Part   Device C1,C2  0.1uF 0805 Q1,Q2  DMN1019USN-13 SOT23 R1     0.002 1% 0805 (resize to change high range) R2     0.05 1% 0805 (resize to change low range) R3     10k 0805 U1,U2  INA21X SC70 (choose desired gain) X2     WM6769CT/0527460871  (bottom contacts) Four-Channel Power Profiler Circuit Description: The Four-Channel Power Profiler board has at its heart a Kinetis K20 on a Teensy3.2 board. The ADCs of the K20 measure all the current sense amplifier's outputs, the voltage of each instrumented rail. There is provision for measuring temperature using up to three thermistors. GPIO provide control each sensor board's current range, and optionally, a hardware wake-up signal for the instrumented target board. Up to four dual-range sensor boards can be connected (either sensor board mentioned above). A micro-SD card socket is included for storing measured data (the SD card functionality has been tested but not implemented for use with measurements). Measured data is sent to the host computer over a virtual serial port using the Teensy's USB. Charge pump U1 boosts the 5V supply to 12V. The output is regulated down to 8V on VCC_FET via regulator U2. R2 and C5 provide filtering for the 3.3V supply from the Teensy that feeds the sensor boards through VCC_SENSE. FETs Q1 through Q4 provide voltage level translation which protect the Teensy's GPIO pins from the 8V that's placed on the gates of the shorting FETs on the sensor boards. Regulator IC2 provides power for the micro-SD socket, since the 3.3V regulator on the Teensy does not provide enough capacity. Since there are not "smarts" on the sensor boards, the Teensy has no way of knowing what kind of sensor board is connected or what shunt values and sense amplifier gains are in use. As currently implemented, current and voltage calculations are hard coded in the Teensy application code. Schematic: Board Layout: BOM: Part    Device C1,C2   0.22uF 0805 C3-C7   1uF 0805 C10,C12 1uF 0805 C11     0.1uF 0805 IC2     MCP1825ST-3302 SOT223 Q1-Q4   DMN1019USN SOT23 R2-R4   20k 1% 0805 R5-R8   10k 0805 R9      Ferrite bead 0805 S1-S4   WM6769CT/0527460871 (bottom contacts) U$1     101-00660-68-6-1-ND MICROSD U1      MAX662CPASO8 SO08 U2      78L08SMD SO08 Use mating Molex cables: 8in: 0150200087 or 10in: 0151660091 Using the Power Profiler Obtaining Sensor and Profiler Boards: Bare boards may be ordered directly from OSH Park using these links: INA250 + INA21x Sensor board (order with 2oz copper option selected) Dual INA21x Sensor board (order with 2oz copper option selected) Power Profiler board The sensor boards should be ordered with the 2oz copper option selected to reduce the trace resistance of the target board's current path. No special option is needed for the profiler board. Teensy3.2 boards may be ordered from OSH Park as well, and at a slightly lower price than the manufacturer (PJRC) sells them. Choosing Current Ranges: To choose the value of a shunt resistor, use the following equation: Rsh = Vfs / (Ifs * gain) where: Rsh is the shunt resistance Vfs is the full scale sense amplifier output voltage (3.3V here) Ifs is the full scale current to be measured gain is the gain of the sense amp to be used For example, to measure a 66mA full scale current with a sense amp of gain 1000, Rsh = 3.3V / (0.066A * 1000) = 0.050 Ohms. For sleep/leakage current, say 1mA full scale: Rsh = 3.3V / (0.001 * 1000) = 3.3 Ohms. The pads on both sensor boards for the shunt resistors have been laid out for 0805 SMT resistors. Precision resistors should be used, 1% or better. The highest power dissipation resistor available should be used to minimize resistance change from the shunt resistor heating up; 0805 resistors are typically available with 1/8, 1/4, 1/2 and 1 Watt dissipation. Building and Testing: These boards were designed to be assembled by hand in small quantities. The most difficult components to solder are the ribbon connectors and the SC70 packaged sense amplifiers. A fine tip soldering iron and a microscope are required. Solder wick is helpful for removing solder bridges from between pins (typically the ribbon connector and the sense amplifiers).  Early versions of the profiler board were assembled with header pins soldered to the Teensy and mating female recepticles soldered to the profiler board. Later versions (like in the example below) were assembled with male header pins between the Teensy and the profiler board.  To test the boards after assembly, check for the presence of 8V on the pull-up resistors R5-R8 when a USB cable is plugged into the Teensy. Program the Teensy with suitable application code. Connect the sensor boards to the profiler. Connect all the sensor boards together in series, positive of one to negative of the next and connect to a calibrated current source. (The image below shows an early prototype of the profiler with the sensor boards connected in series. Current is forced through them via the Kelvin contact clips.) Open a terminal window on the host computer. Force known currents and toggle the ranges of each sensor to verify that each sensor operates correctly in both ranges. To check that the profiler measures rail voltage correctly, disconnect the current source and apply the positive side of a voltage source to either side of the sensors still connected in series and connect the ground of the voltage source to a ground point on the profiler. The rail voltage measured by each sensor should match the supplied voltage (0 to 3.3V max). Accuracy/Calibration: After building in excess of 20 sensor boards and 6 profiler boards and checking their measurements against a Keysight B2902 SMU forcing known currents, the profiler system is fairly accurate. Measurements are good down to about 2% of any range's full scale; lower than that gets into the input offset range of the sense amplifier. Individual readings within 1% of that range's full scale when compared against forced current values. No calibration or tuning has been necessary. Measured values should only be considered good to at most 3 significant figures. Limitations: The maximum current through any sensor should be limited to a maximum of 4A. The current limit when using the low range needs to avoid exceeding the power dissipation of the low range shunt resistor. Particularly, the dissipation in the low range shunt resistor can cause resistance changes that would affect measurement accuracy. The voltage of any instrumented rail cannot be greater than 3.3V, the maximum input voltage of the K20's ADC inputs. Minimum resistance the sensor introduces is in high range is about 0.012 to 0.015 Ohms with a 0.002 Ohm shunt. At least 0.005 Ohms comes from the two shorting FETs on the sensor board. The rest comes from the traces on the board as well as the interconnect wires. The bottom line is: the sensor board has to be mounted as closely as possible to the current sense point on the target board. The maximum resistance the sensor introduces depends on the low range shunt. With a 0.020 Ohm low range shunt, the resistance is about 0.025 to 0.030 Ohms. With a 0.050 Ohm low range shunt, the resistance is about 0.065 to 0.075 Ohms. The sensor board needs to be rigidly mounted to prevent ripping up the current sense points on the target board. This can be a challenge when many rails are instrumented. Instrumenting Target Board: When instrumenting a target board, the on-board current sense resistor should be removed. The sensor board should be attached to the target board placed as close as possible to the sense resistor pads. Connection wires to the sensor board should be as short as possible to minimize series resistance. Great care should be taken to prevent movement of the sensor boards that could in turn lift the sense resistor pads off the target board. Foam double sticky tape should be used over clear areas of the target board to avoid dislodging components when the tape is removed. In the photos below, seven power supplies are instrumented on an interposer card. In this example, the sensor boards were affixed to perf board held in place by the headers. Because of the physical constraints of the target board and its power supply card, mounting the sensor boards directly to the interposer was not possible. Four sensors were mounted on one side and three on the other. Notches were cut in the perf board for the sensor's connection wires on the opposite side. Two profiler boards are required for simultaneous use. (Two were also required because the 0.1" headers and jumpers were not installed on the sensor boards to passively short the low-range shunts; all the sensor boards need to be powered to actively short the low-range shunts.)  The positive input of the sensor board (the center of the three connection points) goes to the regulator side of the current sense resistor. The negative input (either of the two outside connections) goes to the i.MX side of the sense resistor. [NOTE: In this example, the power profiler boards have not been fully populated: the thermistor-related components and the micro-SD card socket. The sensor boards were fully populated with the exception of the passive shorting jumper.] Here is another example of a board with six instrumented rails. The sensors in this case are mounted directly on the target board. In this example, the 12V rail is instrumented, which required modding to add a voltage divider to V_RAIL_LOWSIDE on that sensor board.  And here's yet another example of an instrumented i.MX6Q SDB (which still has wires on it from measuring it the old way...). Although it's difficult to see in this photo, all of the sensor boards have a jumper across the low range shunt which permits normal operation of the board without the profiler board attached to provide power to the shorting FETs. Profiler Application Code for Kinetis/Teensy: Below is sample application code for the Teensy for use with four INA250 + INA21x sensor boards populated with the INA250A3 (0.8V/A gain) for the high range and 0.05 Ohm shunts and INA212 (gain 1000). The current range of each channel can be independently changed. This code is also attached below as a file. Data is sent to the host computer over a USB virtual serial port. To reflash/update Teensy code, follow the instructions from PJRC. Download Windows virtual com port driver. /* MIT License (https://spdx.org/licenses/MIT.html) Copyright 2017 NXP Teensy Power Profiler v.2 (revised main board with individual Hi/Lo GPIO, fixed voltage levels, and on-board uSD card socket. Very basic code for the Teensy Power Profiler that sets up the ADCs and controls the GPIO with very basic, single-character serial commands... This version for all INA250A3 on high range, and 0.05Ohms+INA212 (1000 gain) on low range. */ // These constants won't change.  They're used to give names to the pins used: const int LoHiEn1 = 0; const int LoHiEn2 = 1; const int LoHiEn3 = 2; const int LoHiEn4 = 3; const int WakeUp = 5; const int Lo_1 = A0; const int Vrail_1 = A1; const int Hi_1 = A2; const int Lo_2 = A3; const int Vrail_2 = A4;  const int Hi_2 = A5; const int Lo_3 = A6; const int Vrail_3 = A7; const int Hi_3 = A8; const int Lo_4 = A9; const int Vrail_4 = A11; const int Hi_4 = A10; const int Therm1 = A14; #include <math.h> // thermistor temperature calculation stuff... int sensorValue = 0;        // value read from the pot float sensorValuef = 0.0; int B = 4334; // B25/100 value for thermistor NXRT15WF104FA1B040 // other stuff... int delayintvl = 20; int incomingByte; float vrefL = 3.3; float vrefH = 3.3; float vrefV = 3.3; bool one=true;   bool dispone=true; bool two=true;   bool disptwo=true; bool three=true; bool dispthree=true; bool four=true;  bool dispfour=true; int i,j; int num=100; float v1, v2, v3, v4, i1, i2, i3, i4; float il1, il2, il3, il4; void setup() {   // initialize serial communications at 115200 bps:   Serial.begin(115200);   // set analog resolution to 12 bits... (we want more than the 8 default bits...)   analogReadResolution(12);   // set up low/high range wakeup GPIO signals...   pinMode(LoHiEn1, OUTPUT); digitalWrite(LoHiEn1, HIGH);   pinMode(LoHiEn2, OUTPUT); digitalWrite(LoHiEn2, HIGH);   pinMode(LoHiEn3, OUTPUT); digitalWrite(LoHiEn3, HIGH);   pinMode(LoHiEn4, OUTPUT); digitalWrite(LoHiEn4, HIGH);   pinMode(WakeUp, OUTPUT); digitalWrite(WakeUp, HIGH); } void loop() {   // average voltages and currents...   v1=0; v2=0; v3=0; v4=0;   i1=0; i2=0; i3=0; i4=0;   il1=0; il2=0; il3=0; il4=0;   for (i=0; i<num; i++){     v1 = v1+ analogRead(Vrail_1)/4095.*vrefV;     i1 = i1+ analogRead(Hi_1)/4095.*vrefH/0.8*1000;     il1 = il1+ analogRead(Lo_1)/4095.*vrefH/0.05;     v2 = v2+ analogRead(Vrail_2)/4095.*vrefV;     i2 = i2+ analogRead(Hi_2)/4095.*vrefH/0.8*1000;     il2 = il2+ analogRead(Lo_2)/4095.*vrefH/0.05;     v3 = v3+ analogRead(Vrail_3)/4095.*vrefV;     i3 = i3+ analogRead(Hi_3)/4095.*vrefH/0.8*1000;     il3 = il3+ analogRead(Lo_3)/4095.*vrefH/0.05;     v4 = v4+ analogRead(Vrail_4)/4095.*vrefV;     i4 = i4+ analogRead(Hi_4)/4095.*vrefH/0.8*1000;     il4 = il4+ analogRead(Lo_4)/4095.*vrefH/0.05;   }   v1 = v1/num; v2 = v2/num; v3 = v3/num; v4 = v4/num;   i1 = i1/num; i2 = i2/num; i3 = i3/num; i4 = i4/num;   il1 = il1/num; il2 = il2/num; il3 = il3/num; il4 = il4/num;   // print the results to the serial monitor:   if (dispone) {   Serial.print(" RAIL1 (V)= ");  Serial.print(v1);  //Serial.print("\r\n");   if (!one) {Serial.print("    L1 (mA)= ");  Serial.print(il1, 1);}  //Serial.print("\r\n");   if (1==1) {Serial.print("    H1 (mA)= ");  Serial.print(i1, 1); }   Serial.print("\r\n");   }   if (disptwo) {   Serial.print(" RAIL2 (V)= ");  Serial.print(v2);  //Serial.print("\r\n");   if (!two) {Serial.print("    L2 (mA)= ");  Serial.print(il2, 1);}  //Serial.print("\r\n");   if (1==1) {Serial.print("    H2 (mA)= ");  Serial.print(i2, 1);}    Serial.print("\r\n");   }   if (dispthree) {   Serial.print(" RAIL3 (V)= ");  Serial.print(v3);  //Serial.print("\r\n");   if (!three) {Serial.print("    L3 (mA)= ");  Serial.print(il3, 1);}  //Serial.print("\r\n");   if (1==1) {Serial.print("    H3 (mA)= ");  Serial.print(i3, 1);}    Serial.print("\r\n");   }   if (dispfour) {   Serial.print(" RAIL4 (V)= ");  Serial.print(v4);  //Serial.print("\r\n");   if (!four) {Serial.print("    L4 (mA)= ");  Serial.print(il4, 1);}  //Serial.print("\r\n");   if (1==1) {Serial.print("    H4 (mA)= ");  Serial.print(i4, 1);}    Serial.print("\r\n");   }   Serial.print("\r\n");   Serial.print("\r\n");   while (Serial.available()) {  // while there are characters in the buffer, grab them all...     incomingByte = Serial.read();  // will not be -1     Serial.print("Incoming byte: "); Serial.print(incomingByte);     // Serial.print("    Delay interval:"); Serial.print(delayintvl);  Serial.print("\r\n");     if (incomingByte == 'h' || incomingByte == 'H'){       Serial.print("\r\n\r\nHelp:\r\n\r\n");       Serial.print("  +/= delay interval +/- 10mS\r\n");       Serial.print("  /- delay interval 20msec/1sec\r\n");       Serial.print("  l/L all rails low/high range in unison\r\n");       Serial.print("  q/w/e/r toggle display of rail 1/2/3/4\r\n");       Serial.print("  1/2/3/4 high range of rail 1/2/3/4\r\n");       Serial.print("  !/@/#/$ low range of rail 1/2/3/4\r\n");       Serial.print("  h print this help...\r\n");       Serial.print("\r\n");       delay(2000);       }     // change delay interval...     if (incomingByte == '+') delayintvl = delayintvl + 10;     if (incomingByte == '=') delayintvl = delayintvl - 10;     if (incomingByte == '_') delayintvl = 20;     if (incomingByte == '-') delayintvl = 1000;     if (delayintvl<1) delayintvl = 20;     // toggle low/high range of all rails in unison...     if (incomingByte == 'L') {       digitalWrite(LoHiEn1, LOW);       digitalWrite(LoHiEn2, LOW);       digitalWrite(LoHiEn3, LOW);       digitalWrite(LoHiEn4, LOW);       one = true; two = true; three = true; four = true;     }     if (incomingByte == 'l') {       digitalWrite(LoHiEn1, HIGH);       digitalWrite(LoHiEn2, HIGH);       digitalWrite(LoHiEn3, HIGH);       digitalWrite(LoHiEn4, HIGH);       one = false; two = false; three = false; four = false;     }     // still unimplemented, but for wakeup of target board...     if (incomingByte == 'w') digitalWrite(WakeUp, LOW);     if (incomingByte == 'W') digitalWrite(WakeUp, HIGH);     // toggle display of rail...     if (incomingByte == 'q') dispone = !dispone;     if (incomingByte == 'w') disptwo = !disptwo;     if (incomingByte == 'e') dispthree = !dispthree;     if (incomingByte == 'r') dispfour = !dispfour;     // change between high/low range..     if (incomingByte == '1') { digitalWrite(LoHiEn1, LOW);  one = true; }     if (incomingByte == '!') { digitalWrite(LoHiEn1, HIGH); one = false;}     if (incomingByte == '2') { digitalWrite(LoHiEn2, LOW);  two = true;}     if (incomingByte == '@') { digitalWrite(LoHiEn2, HIGH); two = false;}     if (incomingByte == '3') { digitalWrite(LoHiEn3, LOW);  three = true;}     if (incomingByte == '#') { digitalWrite(LoHiEn3, HIGH); three = false;}     if (incomingByte == '4') { digitalWrite(LoHiEn4, LOW);  four = true;}     if (incomingByte == '$') { digitalWrite(LoHiEn4, HIGH); four = false;}     }   // wait delayintvl mS after the last reading:   delay(delayintvl); }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Future Work and Improvements Work on a "smart" sensor with a local Kinetis device (KL02Z or KL05Z) on the sensor board itself that has three separate sense amplifiers (one run/high current and two low) has begun. There are several advantages to having a microcontroller on each sensor board: All instrumented rails can be measured simultaneously The sampling rate can be increase over current generation's round robin Measured data is sent over I2C or UART, allowing arbitrary number of rails to be instrumented Each sensor board can provide all its shunt and gain info Sensor board can be used in isolation, i.e., without a master profiler board A GUI interface for the serial data output by the profiler would be really nice... Addditional Information For more information on current measurements in general, see this tutorial series: A Current Sensing Tutorial--Part 1: Fundamentals | EE Times  A Current Sensing Tutorial-Part II: Devices | EE Times  A Current Sensing Tutorial--Part III: Accuracy | EE Times  A Current Sensing Tutorial-Part IV: Layout and Troubleshooting Guidelines | EE Times 
View full article
Before reading: only a personal works and sharing, not any form of "release". I didn't find any confidential information from the packages. So, I'm publishing it here. This is only for testing purpose. Do NOT use it for building a product. Use it at your own risk!! Yocto is flexible and powerful, and also, big and slow (when building). Sometimes we only need to build uboot or kernel or some piece of testing code. It's really a waste of time to build-up the whole Yocto environment which may cost over 50GB disk space and over 3 hours of building. I've made some scripts and sum them up to form a toolset for building uboot, kernel and some testing code out of Yocto environment. It's only a simple container and expect to use with uboot and kernel source code from formal Freescale release and a SDK built from Yocto project. GitHub source repo:       https://github.com/gopise/gopbuild What’s made off (a full package, not only the container): 1.    Some scripts and configurations files. 2.    SDK built from Yocto. 3.    Uboot/kernel from specific version. 4.    A hello-world to demonstrate how to build app in this environment. 5.    A slimmed rootfs binary from specific BSP pre-built as base. Will customize base on the source under “rootfs” folder. Only a placeholder in the container-only version. How to use it: Several common used board configurations have been included in the script: 6qsabresd/6qsabreai/6qpsabreai. You can add more into the “gopbuild” script easily. The “sabresd” has been set as default.      If you want to build all for sabresd (First of all, de-compress the package): cd <de-compressed-folder> source envsetup [It will prompt for selecting board configuration to be built. Choose one by input corresponding number or click <ENTER> for default board.] gmk ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍      If you want to build specific module for default board, such as uboot: gmk uboot ‍‍‍‍‍‍‍‍‍      Build kernel for sabreai board instead of default device: gmk kernel sabreai ‍‍‍‍‍‍‍‍‍      Clean everything? gmk all clean ‍‍‍‍‍‍‍‍‍ After a successfully full build, you will get everything under “output” folder, including a log folder contains full build log:      “u-boot.imx/zImage/rootfs.tar.bz2/*.dtb”, can be used with MFG or uuu.      “fsl-image.sdcard”, can be burn into SD card directly. "Ready-for-building" Package: The "gopbuild" itself is a "container-only" package which doesn't contain any source or SDK. I've also made some packages based on latest BSP release for i.MX6/i.MX7/i.MX8. These packages are "ready-for-build" package which you can de-compress and build it directly. -------------------------------------------------------------------------------------------------- URL:https://pan.baidu.com/s/1Xlh1OBGsTRXez_NQw-Rjxg Password: gdc9 -------------------------------------------------------------------------------------------------- Note: 1. To build for i.MX8 (8QM/8MQ/8QXP), you need L4.14.* or above. 2. To build for i.MX8, please download the SCFW from i.MX software page       i.MX Software and Development Tools | NXP      After download, decompress corresponding package for specific chip and put it under "/platform/scfw/". Take i.MX8QXP for example:             /platform/scfw/scfw_export_mx8qx/ All material (uboot/kernel/test code and SDK) are from official Yocto release. Thanks!
View full article
 This article uses i.MX Linux® User's Guide, Rev. L4.1.15_2.1.0-ga, 05/2017 as an example (it may be found as attachment), please refer to section 4.5.12 (How to build U-Boot and Kernel in standalone environment).   First, generate a development SDK, which includes the tools, toolchain, and small rootfs to compile against to put on the host machine.     • Generate an SDK from the Yocto Project build environment with the following command. To set up the Yocto Project build environment, follow the steps in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG). In the following command, set <Target-Machine> to the machine you are building for.   <Target-Machine> may be one of the following :   • imx6qpsabreauto • imx6qpsabresd • imx6ulevk • imx6ull14x14evk • imx6ull9x9evk • imx6dlsabreauto • imx6dlsabresd • imx6qsabreauto • imx6qsabresd • imx6slevk • imx6sllevk • imx6solosabreauto • imx6solosabresd • imx6sxsabresd • imx6sxsabreauto • imx7dsabresd  The «populate_sdk» generates an script file that sets up environment without Yocto Project. This SDK should be updated for each release to pick up the latest headers, toolchain, and tools from the current release.   $ DISTRO=fsl-imx-fb MACHINE=<Target-Machine> source fsl-setup-release.sh -b build-fb   $ DISTRO=fsl-imx-fb MACHINE=<Target-Machine> bitbake core-image-minimal -c populate_sdk   or   $ bitbake meta-toolchain       • From the build directory, the bitbake was run in, copy the sh file in tmp/deploy/sdk to the host machine to build on and execute the script to install the SDK. The default location is in /opt but can be placed anywhere on the host machine.     Note. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.    $ . /opt/fsl-imx-fb/4.1.15-2.0.0/environment-setup-cortexa9hf-neon-poky-linux-gnueabi   or    $ source /opt/fsl-imx-fb/4.1.15-2.0.0/environment-setup-cortexa9hf-neon-poky-linux-gnueabi   From  Yocto Project Mega-Manual  Note By default, this toolchain does not build static binaries. If you want to use the toolchain to build these types of libraries, you need to be sure your image has the appropriate static development libraries. Use the  IMAGE_INSTALL  variable inside your  local.conf  file to install the appropriate library packages. Following is an example using  glibc  static development libraries:      IMAGE_INSTALL_append = " glibc-staticdev"   On the host machine, these are the steps to build U-Boot and Kernel:  • On the host machine, set the environment with the following command before building.   $ export CROSS_COMPILE=/opt/fsl-imx-fb/4.1.15/environment-setup-cortexa9hf-vfp-neon-pokylinux-gnueabi   $ export ARCH=arm • To build U-Boot, find the configuration for the target boot. In the following example, i.MX 6ULL is the target.     Download source by cloning with   $ git clone http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git -b imx_v2016.03_4.1.15_2.0.0_ga   $ cd uboot-imx $ make clean $ make mx6ull_14x14_evk_defconfig $ make u-boot.imx   • To build the kernel, execute the following commands:   Download source by cloning with   $ git clone http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git -b imx_4.1.15_2.0.0_ga   $ cd linux-imx $ make defconfig $ make   • To build an application (Hello World) as test.c:   $ source /opt/fsl-imx-fb/4.1.15-2.0.0/environment-setup-cortexa9hf-neon-poky-linux-gnueabi $ cd ~/test/ $ arm-poky-linux-gnueabi-gcc --sysroot=/opt/fsl-imx-fb/4.1.15-2.0.0/sysroots/cortexa9hf-neon-poky-linux-gnueabi -mfloat-abi=hard test.c To check if the the compiled code (a.out) is ARM executable   $ file ./a.out   ./a.out: ELF 32-bit LSB executable, ARM, EABI5 version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-armhf.so.3, for GNU/Linux 2.6.32, BuildID[sha1]=0e5c22dcf021748ead2c0bd51a4553cb7d38f6f2, not stripped   Copy file a.out to target Linux filesystem and before run it check again :   root@imx6ul7d:/unit_tests/1# file a.out   a.out: ELF 32-bit LSB executable, ARM, EABI5 version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-armhf.so.3, for GNU/Linux 2.6.32, BuildID[sha1]=0e5c22dcf021748ead2c0bd51a4553cb7d38f6f2, not stripped   To define what Linux libs are needed to run our application :   root@imx6ul7d:/unit_tests/1# ldd a.out     linux-vdso.so.1 (0x7ee93000)   libc.so.6 => /lib/libc.so.6 (0x76e64000)   /lib/ld-linux-armhf.so.3 (0x76f9d000)   If some libs are not located in the filesystem you can observe the following message :   -sh: root@imx6ul7d:/unit_tests/1#./a.out: No such file or directory   Finally - run a.out:   root@imx6ul7d:/unit_tests/1# ./a.out Hello World root@imx6ul7d:/unit_tests/1#
View full article
NOTE: Always de-power the target board and the aggregator when plugging or unplugging smart sensors from the aggregator. NOTE: See this link to instrument a board with a Smart Sensor. This page documents the triple-range "smart" current sensor that's part of a larger system for profiling power on application boards. The smart sensor features a Kinetis KL05Z with three current sense amplifiers. It allows measurement currents in three ranges. Four assembly options allow measurement of rail voltages 0-3.3V (two overall current ranges), 0-6.6V, and 12V. It connects to an aggregator, which powers, controls and aggregates data from a number of smart sensor boards. One of the biggest improvements over the older dual-range measurement system is that the on-sensor microcontroller allows near-simultaneous measurement of all instrumented rails on a board. The dual range profiler can only make one measurement at a time.  These are intended to be used with a microncontroller board to act as a trigger and data aggregator. This aggregator could also be used to reprogram the sensors.  The series resistance added by the smart sensor when in run mode (highest current range) is under 11 milliOhms as measured with 4-point probes and a Keysight B2902B SMU.  A "power oscilloscope" can be made by triggering measurements at regular intervals and presenting the results graphically.... Schematic: Board Layout, Top: Board Layout, Bottom: Here's a photo of two with a nickel is included to show scale. The board measures about 0.5 by 1.3 inches. Connections: The smart sensor header connections are: 5V: powers the 3.3V regulator, which in turn powers everything else on the sensor board 12V: all the gates of all the switching FETs are pulled pulled up to 12V GND: ground connection SCL/TX: I2C clock line  SDA/RX: I2C data line  SWD_CLK:  line for triggering smart sensors to make measurements RESET_B:  line for resetting the smart sensor board SWD_IO: select line for the smart sensor Theory of operation: Three shunts and current sense amplifiers are used to measure current in three ranges. One shunt/sense amp pair has a 0.002Ω shunt integrated into the IC package (U1, INA250). The other two sense amps (U2 and U3, INA212) require an external shunt.  FETs Q1, Q2,  and Q3 are used to switch the two lower range shunt/sense amp pairs in and out of circuit. In normal run operation (highest current range), Q1 (FDMC012N03, with Rds(on) under 1.5mΩ) is turned on, which shorts leaves only U1 in circuit. FETs Q4, Q5 and Q6 translate the voltages to 3.3V so that GPIO on U4 (MCU KL05Z) can control them.  Rail voltage measurement is facilitated via resistors R3, R4, and R12 and Q7. Not all of these are populated in every assembly option. For measuring rail voltages 0-3.3V, R12 is populated. To measure 0-6.6V, R3, R4,and Q7 are populated. When turned on Q7 enables the voltage divider. All of the assembly option population info can be found in the schematic (attached). Regulator U5 (AP2210N) provides the 3.3V supply for all of the components on the board. This 1% tolerance regulator is used to provide a good reference for the ADC in U4.  Microcontroller U4 detects the assembly population option of the board via resistors R9, R10, and R11 so that the same application code can be used across all variations of the sensor boards. GPIO control the FETs and four ADC channels are used to measure the sense amplifier outputs and the rail voltage. Having a microcontroller on the sensor board allows the user to do extra credit things like count coulombs as well as allowing all similarly instrumented rails to measure at the same time via trigger line SWD_CLK. Data communication can be via I2C or UART, since these two pins can do both.  But if multiple sensor boards are to be used with an aggregator, communication needs to be over I2C. Application Code: The latest application code for the KL05Z on the smart sensor resides here: https://os.mbed.com/users/r14793/code/30847-SMRTSNSR-KL05Z/. The latest binary is attached below. In order to re-flash a smart sensor, the modification detailed in the aggregator page needs to be made. Once the modification is completed, leave the aggregator unpowered while pluging the SWD debugger into J5 and the smart sensor to be programmed into JP15. Very old UART-based application code for the KL05Z, built in the on-line MBED compiler (note that it requires the modified mbed library for internal oscillator). This code was used while testing the first smart sensor prototypes. It has since been abandoned. It's published here in the event that a user wants to use a single sensor plugged into JP15 with UART breakout connector J6. /****************************************************************************** * * MIT License (https://spdx.org/licenses/MIT.html) * Copyright 2017-2018 NXP * * MBED code for KL05Z-based "smart" current sensor board, basic testing * of functions via UART (connected via FRDM board and OpenSDA USB virtual * COM port). * * Eventual goal is to have each smart sensor communicate over I2C to an * aggregator board (FRDM board with a custom shield), allowing 1-10 power * supply rails to be instrumented. Extra credit effort is to support * sensors and aggregator with sigrok... * * Because there is no crystal on the board, need to edit source mbed-dev library * to use internal oscillator with pound-define: * change to "#define CLOCK_SETUP 0" in file: * mbed-dev/targets/TARGET_Freescale/TARGET_KLXX/TARGET_KL05Z/device/system_MKL05Z4.c * ******************************************************************************/ #include "mbed.h" // These will be GPIO for programming I2C address... // not yet implemented, using as test pins... DigitalOut addr0(PTA3); DigitalOut addr1(PTA4); DigitalOut addr2(PTA5); DigitalOut addr3(PTA6); // configure pins for measurements... // analog inputs from sense amps and rail voltage divider... AnalogIn HIGH_ADC(PTB10); AnalogIn VRAIL_ADC(PTB11); AnalogIn LOW1_ADC(PTA9); AnalogIn LOW2_ADC(PTA8); // outputs which control switching FETs... DigitalOut VRAIL_MEAS(PTA7); // turns on Q7, connecting voltage divider DigitalOut LOW_ENABLE(PTB0); // turns on Q4, turning off Q1, enabling low measurement DigitalOut LOW1(PTB2); // turns on Q5, turning off Q2, disconnecting shunt R1 DigitalOut LOW2(PTB1); // turns on Q6, turning off Q3, disconnecting shunt R2 // input used for triggering measurement... // will eventually need to be set up as an interrupt so it minimizes delay before measurement InterruptIn trigger(PTA0); // use as a trigger to make measurement... // PTB3/4 can be used as UART or I2C... // For easier development with one smart sensor, we are using UART here... Serial uart(PTB3, PTB4); // tx, rx long int count=0; int n=25; // global number of averages for each measurement int i, temp; bool repeat=true; // flag indicating whether measurements should repeat or not const float vref = 3.3; // set vref for use in calculations... float delay=0.25; // default delay between measurement bool gui = false; // flag for controlling human vs machine readable output bool statistics = false;// flag for outputting min and max along with average (GUI mode only) void enableHighRange(){ LOW_ENABLE = 0; // short both low current shunts, close Q1 wait_us(5); // delay for FET to settle... (make before break) LOW1 = 0; LOW2 = 0; // connect both shunts to make lower series resistance VRAIL_MEAS = 0; // disconnect rail voltage divider wait_us(250); // wait for B2902A settling... } void enableLow1Range(){ LOW1 = 0; LOW2 = 1; // disconnect LOW2 shunt so LOW1 can measure wait_us(5); // delay for FET to settle... (make before break) LOW_ENABLE = 1; // unshort low current shunts, open Q1 VRAIL_MEAS = 0; // disconnect rail voltage divider wait_us(250); // wait for B2902A settling... } void enableLow2Range(){ LOW1 = 1; LOW2 = 0; // disconnect LOW1 shunt so LOW2 can measure wait_us(5); // delay for FET to settle... (make before break) LOW_ENABLE = 1; // unshort low current shunts, open Q1 VRAIL_MEAS = 0; // disconnect rail voltage divider wait_us(500); // wait for B2902A settling... } void enableRailV(){ VRAIL_MEAS = 1; // turn on Q7, to enable R3-R4 voltage divider wait_us(125); // wait for divider to settle... // Compensation cap can be used to make // voltage at ADC a "square wave" but it is // rail voltage and FET dependent. Cap will // need tuning if this wait time is to be // removed/reduced. // // So, as it turns out, this settling time and // compensation capacitance are voltage dependent // because of the depletion region changes in the // FET. Reminiscent of grad school and DLTS. // Gotta love device physics... } void disableRailV(){ VRAIL_MEAS = 0; // turn off Q7, disabling R3-R4 voltage divider } // this function measures current, autoranging as necessary // to get the best measurement... void measureAuto(){ Timer t; float itemp; float tempI=0; float imin = 1.0; // used to keep track of the minimum... float imax = 0; // used to keep track of the maximum... t.start(); // use timer to see how long things take... enableHighRange(); // this should already be the case, but do it anyway... for (i = 0; i < n; i++){ itemp = HIGH_ADC; // read HIGH range sense amp output if (statistics && itemp>imax) imax = itemp; // update max if necessary if (statistics && itemp<imin) imin = itemp; // update min if necessary tempI += itemp; // add current sample to running sum } tempI = tempI/n *vref/0.8; // compute average we just took... if (gui) uart.printf("=> %5.3f ", tempI); if (statistics && gui) uart.printf("[%5.3f/%5.3f] ", imin*vref/0.8, imax*vref/0.8); // if current is below this threshold, use LOW1 to measure... if (tempI < 0.060) { if (!gui) uart.printf("... too Low: %f A, switching to low1 ==>\r\n", tempI); tempI=0; enableLow1Range(); // change FETs to enable LOW1 measurement... imin = 1.0; imax = 0; for (i = 0; i < n; i++){ itemp = LOW1_ADC; // read LOW1 sense amp output if (statistics && itemp>imax) imax = itemp; // update max if necessary if (statistics && itemp<imin) imin = itemp; // update min if necessary tempI += itemp; // add current sample to running sum } tempI = tempI/n *vref/0.05/1000; // compute average we just took... if (gui) uart.printf("%6.4f ", tempI); if (statistics && gui) uart.printf("[%6.4f/%6.4f] ", imin*vref/0.05/1000, imax*vref/0.05/1000); // if current is below this threshold, use LOW2 to measure... if (tempI < 0.0009){ if (!gui) uart.printf("... too Low: %f A, switching to low2 ==>\r\n", tempI); tempI=0; enableLow2Range(); // change FETs to enable LOW1 measurement... imin = 1.0; imax = 0; for (i = 0; i < n; i++){ itemp = LOW2_ADC; // read LOW2 sense amp output if (statistics && itemp>imax) imax = itemp; // update max if necessary if (statistics && itemp<imin) imin = itemp; // update min if necessary tempI += itemp; // add current sample to running sum } tempI = tempI/n *vref/2/1000; // compute average we just took... if (gui) uart.printf("%8.6f ", tempI); if (statistics && gui) uart.printf("[%8.6f/%8.6f] ", imin*vref/2/1000, imax*vref/2/1000); } } t.stop(); // stop the timer to see how long it took do do this... enableHighRange(); if (!gui) uart.printf("\r\nCurrent = %f A Current Measure Time = %f sec\r\n", tempI, t.read()); } // the autoranging should really be done with functions that return values, as should the // functions below... This would make for shorter and more elegant code, but the author // is a bit of a pasta programmer... void measureHigh(){ float highI=0; enableHighRange(); for (i = 0; i < n; i++){ highI += HIGH_ADC; } highI = highI/n; uart.printf("HIghI = %f A\r\n", vref*highI/0.8); } void measureLow1(){ float low1I=0; enableLow1Range(); for (i = 0; i < n; i++){ low1I += LOW1_ADC; } enableHighRange(); low1I = low1I/n; uart.printf("low1I = %f A\r\n", vref*low1I/0.05/1000); } void measureLow2(){ float low2I=0; enableLow2Range(); for (i = 0; i < n; i++){ low2I += LOW2_ADC; } enableHighRange(); low2I = low2I/n; uart.printf("low2I = %f A\r\n", vref*low2I/2/1000); } // measure the rail voltage, default being with // a divide by 2 resistor divider // It has to be switched out when not in use or it will // add to the measured current, at least in the low ranges... void measureRailV(){ float railv=0; float mult = vref*2; // since divide by 2, we can measure up to 6.6V... float vmin = 5; float vmax = 0; float vtemp; enableRailV(); // switch FETs so divider is connected... for (i = 0; i < n; i++){ vtemp = VRAIL_ADC; // read voltage at divider output... if (statistics && vtemp>vmax) vmax = vtemp; // update max if necessary if (statistics && vtemp<vmin) vmin = vtemp; // update min if necessary railv += vtemp; // add current sample to running sum } disableRailV(); // now disconnect the voltage divider railv = railv/n; // compute average (note this is in normalized ADC [0..1]) // Convert to voltage by multiplying by "mult" if (!gui) uart.printf("RailV = %5.3f V ", mult*railv); if (gui) uart.printf("%5.3f ", mult*railv); if (statistics && gui) uart.printf("[%5.3f/%5.3f] ", mult*vmin, mult*vmax); uart.printf("\r\n"); } // not sure how useful this function is... void measureAll(){ measureHigh(); measureLow1(); measureLow2(); measureRailV(); } // test function to see if trigger pin is being hit... // intended for use later to do timed triggering of measurements... void triggerIn(){ uart.printf("You're triggering me! \r\n"); measureAll(); } // main... int main() { // set up basic conditions... Timer m; uart.baud(115200); enableHighRange(); // default state - only HIGH sense amp in circuit, no divider // signal that we're alive... uart.printf("Hello World!\r\n"); // configure the trigger interrupt... trigger.rise(&triggerIn); while (true) { count++; wait(delay); if (repeat){ // if repeat flag is set, keep making measurements... m.reset(); // reset and start timer... m.start(); measureAuto(); // measuring current using auto-ranging... measureRailV(); // measure rail voltage... m.stop(); // stop the timer. if (!gui) uart.printf(" Total Measure Time = %f sec", m.read()); if (!gui) uart.printf("\r\n\r\n"); } // see if there are any characters in the receive buffer... // this is how we change things on the fly... // Commands (single keystroke... it's easier) // t = one shot automeasure // v = measure volt // h = one shot high measure // k = one shot LOW1 measure // l = one shot LOW2 measure (letter l) // r = toggle repeat // R = turn off repeat // + = faster repeat rate // - = slower repeat rate // = = set repeat rate to 0.25 sec // g = use human readable text output // G = use compressed text format for GUI // s = turn statistics output off // S = turn statistics output on (only in GUI mode) // n = decrease number of averages for each measurement // N = increase number of averages for each measurement // // these were for testing FET switching... // 1 = LOW_ENABLE = 0 (the number 1) // 2 = LOW1 = 0 // 3 = LOW2 = 0 // 4 = VRAIL_MEAS = 0 // ! = LOW_ENABLE = 1 // @ = LOW1 = 1 // # = LOW2 = 1 // $ = VRAIL_MEAS = 1 if (uart.readable()){ temp = uart.getc(); if (temp==(int) 't') { if (!gui) uart.printf("Keyboard trigger: "); measureAuto(); measureRailV(); //measureAll(); } if (temp==(int) 'v') { uart.printf("Keyboard trigger: "); measureRailV(); } if (temp==(int) 'h') { uart.printf("Keyboard trigger: "); measureHigh(); } if (temp==(int) 'k') { uart.printf("Keyboard trigger: "); measureLow1(); } if (temp==(int) 'l') { uart.printf("Keyboard trigger: "); measureLow2(); } if (temp==(int) '1') { LOW_ENABLE = 0; uart.printf("Keyboard trigger: LowEnable = %d\r\n", 0); } if (temp==(int) '2') { LOW1 = 0; uart.printf("Keyboard trigger: LOW1 = %d\r\n", 0); } if (temp==(int) '3') { LOW2 = 0; uart.printf("Keyboard trigger: LOW2 = %d\r\n", 0); } if (temp==(int) '4') { VRAIL_MEAS = 0; uart.printf("Keyboard trigger: VRAILMEAS = %d\r\n", 0); } if (temp==(int) '!') { LOW_ENABLE = 1; uart.printf("Keyboard trigger: LowEnable = %d\r\n", 1); } if (temp==(int) '@') { LOW1 = 1; uart.printf("Keyboard trigger: LOW1 = %d\r\n", 1); } if (temp==(int) '#') { LOW2 = 1; uart.printf("Keyboard trigger: LOW2 = %d\r\n", 1); } if (temp==(int) '$') { VRAIL_MEAS = 1; uart.printf("Keyboard trigger: VRAILMEAS = %d\r\n", 1); } if (temp==(int) 'r') { repeat = !repeat; uart.printf("Keyboard trigger: repeat toggle: %s \r\n", repeat ? "true" : "false"); } if (temp==(int) 'R') repeat = false; if (temp==(int) '+') { delay -= 0.05; if (delay<0.05) delay = 0.05; } if (temp==(int) '-') { delay += 0.05; if (delay>1) delay = 1; } if (temp==(int) '=') delay = 0.25; if (temp==(int) 'g') gui = false; if (temp==(int) 'G') gui = true; if (temp==(int) 's') statistics = false; if (temp==(int) 'S') statistics = true; if (temp==(int) 'n') { n -= 25; if (n<25) n = 25; } if (temp==(int) 'N') { n += 25; if (n>1000) n = 1000; } if (temp==(int) 'N' || temp==(int) 'n') uart.printf("/r/n/r/n Averages = %d \r\n\r\b", n); } } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
View full article
Check new updated version for with Morty here Step 1 : Get iMX Yocto AVS setup environment Review the steps under Chapter 3 of the i.MX_Yocto_Project_User'sGuide.pdf on the L4.X LINUX_DOCS to prepare your host machine. Including at least the following essential Yocto packages $ sudo apt-get install gawk wget git-core diffstat unzip texinfo \   gcc-multilib build-essential chrpath socat libsdl1.2-dev u-boot-tools Install the i.MX NXP AVS repo Create/Move to a directory where you want to install the AVS yocto build enviroment. Let's call this as <yocto_dir> $ cd <yocto_dir> $ repo init -u https://source.codeaurora.org/external/imxsupport/meta-avs-demos -b master -m imx7d-pico-avs-sdk_4.1.15-1.0.0.xml Download the AVS BSP build environment: $ repo sync Step 2: Setup yocto for Alexa_SDK image with AVS-SETUP-DEMO script: Run the avs-setup-demo script as follows to setup your environment for the imx7d-pico board: $ MACHINE=imx7d-pico DISTRO=fsl-imx-x11 source avs-setup-demo.sh -b <build_sdk> Where <build_sdk> is the name you will give to your build folder. After acepting the EULA the script will prompt if you want to enable: Sound Card selection The following Sound Cards are supported on the build: SGTL (In-board Audio Codec for PicoPi) 2-Mic Conexant The script will prompt if you are going to use the Conexant Card. If not then SGTL will be assumed as your selection Are you going to use Conexant Sound Card [Y/N]? Install Alexa SDK Next option is to select if you want to pre-install the AVS SDK software on the image. Do you want to build/include the AVS_SDK package on this image(Y/N)? If you select YES, then your image will contain the AVS SDK ready to use (after authentication). Note this AVS_SDK will not have WakeWord detection support, but it can be added on runtime. If your selection was NO, then you can always manually fetch and build the AVS_SDK on runtime. All the packages dependencies will be already there, so only fetching the AVS_SDK source code and building it is required. Finish avs-image configuration At the end you will see a text according with the configuration you select for your image build. Next is an example for a Preinstalled AVS_SDK with Conxant Sound Card support and WiFi/BT not enabled. ==========================================================   AVS configuration is now ready at conf/local.conf             - Sound Card = Conexant                                     - AVS_SDK pre-installed                                       You are ready to bitbake your AVS demo image now:               bitbake avs-image                                        ========================================================== Step 3: Build the AVS image Go to your <build_sdk> directory and start the build of the avs-image There are 2 options Regular Build: $ cd <yocto_dir>/<build_sdk> $ bitbake avs-image With QT5 support included: $ cd <yocto_dir>/<build_sdk> $ bitbake avs-image-qt5 The image with QT5 is useful if you want to add some GUI for example to render DisplayCards. Step 4 : Deploying the built images to SD/MMC card to boot on target board. After a build has succesfully completed, the created image resides at <build_sdk>/tmp/deploy/images/imx7d-pico/ In this directory, you will find the imx7d-pico-avs.sdcard image or imx7d-pico-avs-qt5.sdcard, depending on the build you chose on Step3. To Flash the .sdcard image into the eMMC device of your PicoPi board follow the next steps: Download the bootbomb flasher Follow the instruction on Section 4. Board Reflashing of the Quick Start Guide for AVS kit to setup your board on flashing mode. Copy the built SDCARD file $ sudo dd if=imx7d-pico-avs.sdcard of=/dev/sd bs=1M && sync $ sync Properly eject the pico-imx7d board: $ sudo eject /dev/sd NXP Documentation Refer to the Quick Start Quide for AVS SDK to fully setup your PicoPi board with Synaptics 2Mic and PicoPi i.mx7D For a more comprehensive understanding of Yocto, its features and setup; more image build and deployment options and customization, please take a look at the i.MX_Yocto_Project_User's_Guide.pdf document from the Linux documents bundle mentioned at the beginning of this document. For a more detailed description of the Linux BSP, u-boot use and configuration, please take a look at the i.MX_Linux_User's_Guide.pdf document from the Linux documents bundle mentioned at the beginning of this document.
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344336 
View full article
The document to descript change the u-boot environment variables under the Linux rootfs.  Also provide a demo on i.MX6ull evk of sdcard mirror.  Linux fw_printenv fw_setenv to access U-Boot's environment variables.pdf  --- the document fw_printenv_fw_setenv_demo_iMX6ullevk_L4.14.98_2.0.0_ga.sdcard  --- demo sdcard mirror
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342877 
View full article
L5.4.3_1.0.0 release is now available on IMX_SW landing page: BSP Updates and Releases -> Linux ->Linux L5.4.3_1.0.0. Documentation -> Linux -> Linux 5.4.3_1.0.0 Documentation Files available: # Name Description 1 imx-yocto-LF_L5.4.3_1.0.0.zip i.MX L5.4.3_1.0.0 for Linux BSP Documentation. Includes Release Notes, User Guide. 2 LF_v5.4.y-1.0.0_images_MX6QPDLSOLOX.zip i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualLite, i.MX 6Solox Linux Binary Demo Files 3 LF_v5.4.y-1.0.0_images_MX6SLLEVK.zip i.MX 6SLL EVK Linux Binary Demo Files 4 LF_v5.4.y-1.0.0_images_MX6UL7D.zip i.MX 6UltraLite EVK, 7Dual SABRESD, 6ULL EVK Linux Binary Demo Files 5 LF_v5.4.y-1.0.0_images_MX7ULPEVK.zip i.MX 7ULP EVK Linux Binary Demo Files  6 LF_v5.4.y-1.0.0_images_MX8MMEVK.zip i.MX 8M Mini EVK Linux Binary Demo Files  7 LF_v5.4.y-1.0.0_images_MX8MNEVK.zip i.MX 8M Nano EVK Linux Binary Demo Files  8 LF_v5.4.y-1.0.0_images_MX8MQEVK.zip i.MX 8M Quad EVK Linux Binary Demo files 9 LF_v5.4.y-1.0.0_images_MX8QMMEK.zip i.MX 8QMax MEK Linux Binary Demo files 10 LF_v5.4.y-1.0.0_images_MX8QXPMEK.zip i.MX 8QXPlus MEK Linux Binary Demo files 11 imx-scfw-porting-kit-1.2.10.1.tar.gz System Controller Firmware (SCFW) porting kit v1.2.10.1 for L5.4.3_1.0.0   Target board: MX 8 Series MX 8QuadXPlus MEK Board MX 8QuadMax MEK Board MX 8M Quad EVK Board MX 8M Mini EVK Board MX 8M Nano EVK Board MX 7 Series MX 7Dual SABRE-SD Board MX 7ULP EVK Board MX 6 Series MX 6QuadPlus SABRE-SD and SABRE-AI Boards MX 6Quad SABRE-SD and SABRE-AI Boards MX 6DualLite SDP SABRE-SD and SABRE-AI Boards MX 6SoloX SABRE-SD MX 6UltraLite EVK Board MX 6ULL EVK Board MX 6ULZ EVK Board MX 6SLL EVK Board   What’s New/Features: Please consult the Release Notes.   Known Issues: For known issues and more details please consult the Release Notes.   More information on changes of Yocto, see: README: https://source.codeaurora.org/external/imx/imx-manifest/tree/README?h=imx-linux-zeus ChangeLog: https://source.codeaurora.org/external/imx/imx-manifest/tree/ChangeLog?h=imx-linux-zeus      
View full article
[中文翻译版] 见附件   原文链接: i.MX Create Android SDCard Mirror 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343079 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343046 
View full article
Hardware : i.MX8MNLPDDR4EVK Build Yocto Image [Linux 4.14.98_2.3.1] Yocto Project Setup          $: mkdir imx-yocto-bsp          $: cd imx-yocto-bsp                $: repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.3.1.xml          $: repo sync  copy marvell bb.file into yocto source         $: cp  0001-Porting-mrvl-8987-wifi.patch   imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp         $: git apply 0001-Porting-mrvl-8987-wifi.patch Image Build         $: DISTRO=fsl-imx-xwayland MACHINE=imx8mnlpddr4evk source fsl-setup-release.sh -b build-xwayland         $:bitbake fsl-image-qt5-validation-imx Enable wifi and BT (These operations is on EVK) WiFi $:insmod /lib/modules/4.14.98-2.3.1+g860ec89/extra/sd8xxx.ko fw_name=/mrvl/sduart8987_combo.bin cal_data_cfg=none cfg80211_wext=0xf BT $:hciattach /dev/ttymxc0 any -s 115200 115200 flow dtron $:hciconfig hci0 reset $:hcitool -ihci0 cmd 0x3f 0x0009 0xc0 0xc6 0x2d 0x00 & $:killall hcitool $:killall hciattach $:hciattach /dev/ttymxc0 any -s 3000000 3000000 flow dtron Build  Android Image[Android P9_2.3.4] These patches in  Android-2.3.4-patch. Getting i.MX Android release source code        $: cd ~ (or any other directory you like)        $: tar xzvf imx-p9.0.0_2.3.4.tar.gz        $: mkdir ~/bin        $: curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo        $: chmod a+x ~/bin/repo        $: export PATH=${PATH}:~/bin        $: source ~/imx-p9.0.0_2.3.0/imx_android_setup.sh        # By default, the imx_android_setup.sh script will create the source code build environemnt        in the folder ~/android_build        # ${MY_ANDROID} will be refered as the i.MX Android source code root directory in all i.MX        Andorid release documentation.        $ : export MY_ANDROID=~/android_build Copy 88W8987 firmware and driver into  Android release code        $:copy -r Android-2.3.4-patch/mrvl    android_build/vendor/nxp/fsl-proprietary  Apply these patches.The name of these patches is the patche installation path.            example:  0001-android_build-hardware-marvell-wlan.patch         $: cp 0001-android_build-hardware-marvell-wlan.patch   android_build/hardware/marvell/wlan            (if not exist android_build/hardware/marvell/wlan, mkdir -p android_build/hardware/marvell/wlan)         $: git apply 0001-android_build-hardware-marvell-wlan.patch  Building Android images          $: cd  android_build          $: source build/envsetup.sh          $: lunch evk_8mn-userdebug          $: make 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343344 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343372 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343273 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343518 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343576 
View full article