テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
EUF-NET-T1744 - Overview on QorIQ roadmap and processing solution for addressing new technical challenge in virtualized network. We will introduce latest new product derivatives based on Power Architecture® and ARM® while highlighting key NXP differentiators for packet acceleration, security features connectivity, power dissipation and scalability. You will learn on new reference design for smart network based on LS1021, T1024, LS1043, T4240, and LS208X.
記事全体を表示
Understand the value, benefits and features  of Arm's latest Cortex-M33 core through a LPC5500-based product training and hand-on session.
記事全体を表示
Learn how to solve your I2C system challenges by deploying I3C. Our experts will provide a comprehensive introduction into the new MIPI I3C interface and its advantages compared to the well-known, I2C interface. This session gives an overview of how to develop I3C-based systems as well as provide a view of NXP’s MIPI I3C slave RTL, which is the first verified, freely available RTL source code available for download.
記事全体を表示
Design, Software & Services APF-DES-T2274 - Kinetis KW and Thread  APF-DES-T2229 - Kinetis New Products, KE+, Security with K8x & KL8x  APF-DES-T2226 - Improve the RF Performance for the Connectivity  Secure Mobile, Healthcare & Wearables APF-MHW-T2232 - LPC541xx for Wearable  Smart Machinery & Industrial Automation APF-SMI-T2225 - Motion Sensors for Industry and Medical
記事全体を表示
The biggest challenge in embedded GUI development is managing changes in design (iterations) that nearly all projects encounter. Historically, changes at the design level resulted in teams needing to hunt for and replace all changed assets manually within the project. This would result in development delays, changes being missed, coded behavior being lost, and ultimately, poor UX. Join this session to learn how customers from medical to automotive have leveraged Storyboard’s Rapid Design Import and Iteration Technology to streamline design changes and develop embedded GUI applications that provided outstanding user experiences while getting to market on a tight deadline. Presenters: Garry Clarkson, FAE, Crank Software Shelby Unger, MCU Ecosystem Product Marketer, NXP
記事全体を表示
This class provides an introduction on the S32 Design Studio for Vision IDE with the new S32 Debugger and S32 Debug Probe. The lecture will provide an overview of the S32 Design Studio for Vision IDE with S32 Debugger and S32 Debug Probe along with a demonstration. Also, there will be a preview of the S32 Configuration Tool coming in the next generation S32 Design Studio.
記事全体を表示
Introduce the BLDC and PMSM motor control theory, including the trapezoidal control, FOC control and sensor-less algorithm. The session will also introduce MagniV family products and the hardware design guide.
記事全体を表示
Evolving IoT Needs of Brands Protect and Enhance Product Experiences through Advances in NFC Technology
記事全体を表示
A guide to developing with the Yocto Project for i.MX application processors. Learn how to leverage the Yocto Project in development by adding layers and recipes, customizing images, working with the kernel, and other essential Yocto development tasks.
記事全体を表示
Automotive instrument clusters and in-vehicle infotainment rely more and more on complex application processors. They also require large software components to function properly. This complexity also increases risks of failures. There is also a growing need of safety, to detect and handle system faults in a timely manner. This is traditionally achieved by adding external parts dedicated to this purpose, increasing the system cost. We introduce the SafeAssure Rear View Camera and SafeAssure Display solutions, with which we show how a system design can be simplified, and cost reduce during the unique safety features integrated in the NXP i.MX 8 application processor.
記事全体を表示
EUF-NET-T1756 - This session will go over the RF solutions for the industrial and military market.
記事全体を表示
Learn how to create a custom SDK for your specific hardware board featuring MCUXpresso SDK and config tools.
記事全体を表示
Bluetooth speakers and headsets, printers, cameras, projectors, set-top-boxes, TVs, Wi-Fi routers, fridges and washing machines, they all have one thing in common: Near-field-communication (NFC) which allows new features and easier handling. Just bringing two NFC-enabled devices close together is all it takes to create a connection. Accessories and consumables can be identified and authenticated without any user interaction. And commissioning an IoT node into a wireless network has never been as easy as it is now with NFC.
記事全体を表示
In this class, you will learn to use NXP’s FreeMASTER debug tool to aid in system development and debug. Although it is has many uses in various applications, we will demonstrate the features and use of FreeMASTER to simplify the development process with a motor control example based on our MagniV MC9S12ZVMRM microcontroller. Participants will see how useful and easy it is to use and configure so that system variables can be adjusted on the fly or watch system parameters real time.
記事全体を表示
The MQX Application Builder is the most recent addition to the MCUXpresso Config Tools. In this session you will use this powerful tool to rapidly create a sophisticated IoT application without requiring detailed knowledge of the protocols used, or how to configure them. By the end of the session you will have created an application that serves up customized web pages, uses the REST and MQTT protocols to remotely access key application parameters, interfaces with a cloud server, synchronize with a time server, remotely control your application with Lua Scripting Language, and more. Learn the power of using the MQX platform over other operating system such as FreeRTOS.
記事全体を表示
Automotive Automotive Safety and HEV Offering for Vehicle Dynamics and Safety (VDS)  i.MX 8/8X Overview  S32K Complete Portfolio Update  S32 Radar Processor, Product Revolution  Understanding the Autonomous System  Artificial Intelligence, Enabling Technologies, Security & Solutions A Vision for Machine Learning (ML) and Artificial Intelligence (AI) in Low-cost Edge-computing Nodes  Hands-On Workshop: Advanced Debugging with MCUXpresso IDE  Hands-On Workshop: Crossover MCU Memory Expansion Advantage: Designing with Execute in Place Serial Flash   i.MX RT Execute in Place Serial Flash Lab Guide.pdf  Hands-On Workshop: Develop Managed IoT Deployments with Arm® Mbed™ OS and NXP Platforms  Hands-On Workshop: Learn to Get Up and Running Fast with MCUXpresso Software and Tools  AMF-ENT-T3024 - Lab 2 - Getting Started with MCUXpresso.pdf  Hands-On Workshop: Leveraging MCUXpresso SDK Examples within Your Designs  AMF-ENT-T3025 - SDK Examples - Labs 1-5.pdf  Hands-On Workshop: Optimizing and Tuning FreeRTOS Applications with MCUXpresso Software and Tools  Optimizing FreeRTOS Lab Guide  Hands-On Workshop: Using MCUXpresso Software and Tools with Amazon Web Services (AWS)  AMF-ENT-T3026 - AWS Shadow - Labs 1-2.pdf  AMF-ENT-T3026 - AWS Greengrass - Labs 3-4.pdf  Using OpenWRT, Yocto, Ubuntu or Your Own Custom Linux® Distribution? Learn How NXP is Making it Easy to Leverage a Multi-Distribution Approach to Software Development  Smart Machinery & Industrial Automation A71CH Plug and Trust Solution for IoT Security  NFC in Industrial and Healthcare - More Use Cases Than You Imagine  Securing My Connected Device - Where are the Threats and What Solutions Does NXP Offer You?  Time Sensitive Networking (TSN) and Precision Time Protocol (PTP): Challenges, Opportunities and Solutions  Smarter World Solutions & Multimode Connectivity Amazon Alexa Voice Services  Hands-On Workshop: Get Started with LPC54018 Based IoT Module to Develop a Cloud-Connected End Node  AMF-SMC-T3148 - AWS Shadow - Labs 1-2 Hands-On Workshop: i.MX RT Overview and Training  i.MX 8M - Next-Generation of Applications Processors for High Performance, Smart Design and Advanced Multimedia  Introduction of NXP Wireless Charging  IoT Sensor Applications—Industrial and Automotive Use Cases  NXP BLE Low-Power Solutions for Consumer, Medical, Industrial IoT and Automotive Markets  NXP Connectivity Solutions for Smart Home, Building and Lighting  Rapid IoT Prototyping Kit
記事全体を表示
If you find yourself in need of using a low cost co-processor to act as a communications hub, why not consider a GPIO expander?  With the features in our latest GPIO expanders, this device can almost mimic a low cost MCU while being more cost-effective and reducing the complexity of your system. Come learn about the features and benefits, and actually see the GPIO expander in action on a simple PCB you’ll experiment with in this class.
記事全体を表示
Solutions from NXP provide the right hardware, modular software, certifications, partners and documentation to accelerate time-to-market for our customers. Join this class to experience a deep dive on what is delivered from the newly launched SLN-POS-RDR Card Reader Solution.
記事全体を表示
Security is critical to the growing market for IoT-enabled devices: There were already more than 5 billion connected devices in the world last year, and use is expected to grow to 12 billion by 2020. To support this rapid expansion, prominent internet players, including Alibaba, AWS, Google, IBM and Microsoft are establishing their own cloud services and industrial suppliers are moving quickly to broaden their private cloud offerings. At NXP, we believe strong security doesn't have to be hard to work with. Our "Plug & Trust" approach simplifies the implementation of strong security mechanisms in today's IoT devices. NXP's latest A71CH provides just this level of Plug & Trust IoT Security and delivers proven, chip-to-cloud security right out of the box, enabling every customer to secure IoT devices and safely connect to IoT clouds and services without writing security codes or exposing keys.
記事全体を表示
This session will go over the evolution of the eID documents and regulations in Europe.
記事全体を表示