技术日 - 培训资料

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

讨论

排序依据:
S32V234 vision product family introduction.
查看全文
A guide to developing with the Yocto Project for i.MX application processors. Learn how to leverage the Yocto Project in development by adding layers and recipes, customizing images, working with the kernel, and other essential Yocto development tasks.
查看全文
In this class, you will learn to use NXP’s FreeMASTER debug tool to aid in system development and debug. Although it is has many uses in various applications, we will demonstrate the features and use of FreeMASTER to simplify the development process with a motor control example based on our MagniV MC9S12ZVMRM microcontroller. Participants will see how useful and easy it is to use and configure so that system variables can be adjusted on the fly or watch system parameters real time.
查看全文
Secure designs begin with a security model consisting of policies, an understanding of the threat landscape and the methods used to enforce physical and logical security. To protect firmware execution given today’s threat landscape, there must be a policy to only allow execution of authenticated firmware. The methods used to enforce this policy rely on MCU security technology to create a protected boot flow. The boot firmware can contain public key cryptography to authenticate application code. In addition to these components integrated in the end device, there are tools and steps that must be taken in the manufacturing environment using manufacturing hardware for code signing and host programs for provisioning. Join this session to explore the design and implementation of a secure boot with i.MX RT.
查看全文
Learn how to create a custom SDK for your specific hardware board featuring MCUXpresso SDK and config tools.
查看全文
Hands-on getting started with MagniV. Participants will work with bare metal application code and Processor Expert, working with an S12ZVC development kit and CodeWarrior IDE. Short presentations followed by hands-on labs. Learn coding secrets for fast application startup!
查看全文
Evolving IoT Needs of Brands Protect and Enhance Product Experiences through Advances in NFC Technology
查看全文
Do you plan to secure your data transmission keeping high data throughput, low power and CPU load? Layerscape family is your best choice.
查看全文
This session will go over the evolution of the eID documents and regulations in Europe.
查看全文
Solutions from NXP provide the right hardware, modular software, certifications, partners and documentation to accelerate time-to-market for our customers. Join this class to experience a deep dive on what is delivered from the newly launched SLN-POS-RDR Card Reader Solution.
查看全文
Automotive engine control, HEV and safety roadmaps, value proposition, current and future plans for tools and reference designs.
查看全文
Bluetooth speakers and headsets, printers, cameras, projectors, set-top-boxes, TVs, Wi-Fi routers, fridges and washing machines, they all have one thing in common: Near-field-communication (NFC) which allows new features and easier handling. Just bringing two NFC-enabled devices close together is all it takes to create a connection. Accessories and consumables can be identified and authenticated without any user interaction. And commissioning an IoT node into a wireless network has never been as easy as it is now with NFC.
查看全文
If you find yourself in need of using a low cost co-processor to act as a communications hub, why not consider a GPIO expander?  With the features in our latest GPIO expanders, this device can almost mimic a low cost MCU while being more cost-effective and reducing the complexity of your system. Come learn about the features and benefits, and actually see the GPIO expander in action on a simple PCB you’ll experiment with in this class.
查看全文
The MQX Application Builder is the most recent addition to the MCUXpresso Config Tools. In this session you will use this powerful tool to rapidly create a sophisticated IoT application without requiring detailed knowledge of the protocols used, or how to configure them. By the end of the session you will have created an application that serves up customized web pages, uses the REST and MQTT protocols to remotely access key application parameters, interfaces with a cloud server, synchronize with a time server, remotely control your application with Lua Scripting Language, and more. Learn the power of using the MQX platform over other operating system such as FreeRTOS.
查看全文
Hands-on workshop introducing LCP55xx.
查看全文
Getting started with MCUXpresso SDK, IDE, and Config tools.
查看全文
This hands-on session will show users how to get to market faster by leveraging MCUXpresso SDK examples within their end product designs. Attendees will get hands-on with key SDK demo applications and driver examples.
查看全文
This class provides an introduction on the S32 Design Studio for Vision IDE with the new S32 Debugger and S32 Debug Probe. The lecture will provide an overview of the S32 Design Studio for Vision IDE with S32 Debugger and S32 Debug Probe along with a demonstration. Also, there will be a preview of the S32 Configuration Tool coming in the next generation S32 Design Studio.
查看全文
This training will take a user from “out of box” to a functioning IoT system including edge devices, gateway/border router, smart phone app and cloud connectivity, then run the system through its paces to highlight a subset of common IoT capabilities. The training will leverage the NXP Modular IoT Framework using a currently shipping, fully documented, Integrated Development Experience for the exercises. Southbound connectivity between gateway and the edge devices will be Thread and ZigBee®. Device commissioning will be via NFC and BLE. Northbound connectivity from gateway to cloud will be Wi-Fi. Cloud support will be via a major cloud provider. Note: Users will be able to use their own Android or iPhone with a recent OS version.
查看全文