Bluetooth® LE Advanced Session on Localization

File uploaded by Renee Fortenberry Employee on Oct 22, 2018Last modified by Renee Fortenberry Employee on Nov 29, 2018
Version 2Show Document
  • View in full screen mode

The presenter explains the key principles for localizing objects and gives a description of the silicon IP that is included in the KW devices and supports localization. Algorithms such as RSSI, Time-of-Flight and AoA/AoD are clearly described and examples of implementation are provided through the delivery of test results obtained on devices such as the KW35 and KW36. Partnership with external companies is also mentioned so that support can be obtained companies having a long experience in his technical domain.

Attachments

Outcomes