テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
Business Line Smart Antenna Solution delivers a broad range of RF products for many different applications ranging from mobile phones to wireless infrastructure. All these applications require high performance RF products to deliver reliable, high data rate connections. This training will show how our RF products can be successfully used in IoT applications to improve the RF connection: range extension by using LNAs in the receive chain or by adding a PA at the transmit side. Our wide product portfolio ensures that  the different needs of IoT (frequency range, power consumption and performance gain) can be met.
記事全体を表示
This session will highlight the features and design advantages of the QN9080 BLE SoC portfolio for small form factor products with rich feature sets that can operate for multiple years on small coin cell batteries.
記事全体を表示
Level 3 -5 Autonomous vehicle systems are complex systems where algorithms for perception, localization, planning and control needs to run on real time hardware platform; all algorithm are developed considering off line data storage, simulation, high-definition (HD) mapping, and deep learning model training. This session will go through an overview of autonomous vehicle systems design trying to highlight the major state of the art technologies, mostly referring to algorithms implementation to meet real-time and reliability requirements. A NXP system partition solution will be discussed.
記事全体を表示
Hands-on getting started with MagniV. Participants will work with bare metal application code and Processor Expert, working with an S12ZVC development kit and CodeWarrior IDE. Short presentations followed by hands-on labs. Learn coding secrets for fast application startup!
記事全体を表示
Mbed OS and Mbed Cloud overview. Builiding device apps with NXP MCUXpresso IDE building device apps that connect to Mbed cloud.
記事全体を表示
When choosing the NFC device for a new design, the system architect must consider many parameters. Usually a strong focus is put on hardware specific aspects like the environment, possible antenna size, performance and interface. To avoid unpleasant surprises during software implementation phase, software has to be taken into account as well from the beginning. Different NFC IC categories (NFC Frontends, NFC Controller, Connected Tag) have different strengths, depending on the software environment. The way how highly integrated operating systems like Linux are structured brings both new challenges and advantages. This session examines the considerations necessary when designing in NFC in different operating systems or "bare metal" systems. It also discusses the advantages and disadvantages of the different device categories in dependence of the designated environment.
記事全体を表示
NXP security solutions and use cases. The fast, easy way to deploy secure IoT connections.
記事全体を表示
MCUupdate_public version.pdf Next generation of NFC_Tech Days Lyon & Strasbourg_May 2016-02.pdf  NXP - i.MX Latest NPI Introduction_non NDA .pdf Sensors_Multimarkets_may16.pdf Thread tech days.pdf USB_TypeC_Portfolio Presentation (Tech Days Lyon & Strasboug - May 2016)....pdf
記事全体を表示
Expect your platform to boot in less than one second...do your customer's demand it? Even if that is not fast enough for some cases...we will discuss what can be done to improve the booting performance. Learn from the experts on how to architect and optimize the boot process from boot ROM, boot loader through to OS and applications.
記事全体を表示
Introduction to working with NXP's Automotive NFC NCI library and demo software.
記事全体を表示
Join this session to understand all the security features integrated in the recently launched LPC5500 MCU Family and learn how to implement these features to design a low-power system with robust security using the MCUXpresso Software & Tools.
記事全体を表示
This training will take a user from “out of box” to a functioning IoT system including edge devices, gateway/border router, smart phone app and cloud connectivity, then run the system through its paces to highlight a subset of common IoT capabilities. The training will leverage the NXP Modular IoT Framework using a currently shipping, fully documented, Integrated Development Experience for the exercises. Southbound connectivity between gateway and the edge devices will be Thread and ZigBee®. Device commissioning will be via NFC and BLE. Northbound connectivity from gateway to cloud will be Wi-Fi. Cloud support will be via a major cloud provider. Note: Users will be able to use their own Android or iPhone with a recent OS version.
記事全体を表示
In electronic systems, it is typical to have a central processing unit that interfaces with other peripheral devices, other sub-systems or the user. Often, the signals from these interconnects may be incompatible on both ends. Therefore, various semiconductor devices such as analog switches, voltage level translators and GPIO expanders are often used to bridge between the interconnects on the board. In this session, we will explore the application of these interface devices from NXP and discuss their applications in various customer systems.
記事全体を表示
Presentation of the high-performance packet processing solutions being developed on i.MX processors and expected performance gains compared to a standard software stack.
記事全体を表示
Industrial OEMs have been hampered by the large array of networking protocols that they need to support in their devices. The new IEEE Time Sensitive Networking (TSN) standard offers to consolidate multiple proprietary protocols with a common IEEE based standard. Come learn what you can achieve with TSN.
記事全体を表示
Do you plan to secure your data transmission keeping high data throughput, low power and CPU load? Layerscape family is your best choice.
記事全体を表示
Enabling Design, Technologies & Solutions Hands-On Workshop: MCUXpresso Software and Tools  Hands-On Workshop: MCUXpresso Software and Tools_Lab Guide.pdf  Hands-On Workshop: Using MCUXpresso SDK  Introduction to the Next-Generation USB Type-C Connector and NXP’s End-to-End Solution  Irvine: Boost Your Productivity with CodeWarrior® Development Tools for ARM®v8 Architecture  Irvine: LPC800 MCUs Technical Overview: NXP®’s Fastest Growing Portfolio for the Broad, 8-bit Alternative Market  Irvine: Overview of the I3C Interface, Successor of the Well-Known I2C Interface  NXP’s Next-Generation Layerscape Linux® SDK  Payment, Banking & Retail Hands-On Workshop: Solution Card Reader Training: The Purpose and Value of a Solution  Hands-On Workshop: Solution Card Reader Training: The Purpose and Value of a Solution_Lab Guide 1  Hands-On Workshop: Solution Card Reader Training: The Purpose and Value of a Solution_Lab Guide 2  Secure Connected & Automated Vehicles i.MX 8 and 8X Applications Processor Overview  Introduction to Wireless Charging Solutions  Smart Buildings & Consumer Goods Google™ Home and NXP®: Android Things, Google Assistant and Chromecast™ Built-in  Identification and Authentication of Consumables and Accessories via NFC  i.MX 8M Processor Overview and the Road Ahead  Irvine: Modular IoT Framework  Irvine: NFC in Consumer Electronics and Home Appliances  Low-Power i.MX Applications Processors Overview  Secure Authentication for Anti-Counterfeit Applications  Voice Control Solutions: Creating Amazon® Alexa® Devices with i.MX  Smart Networks & Computing How Far Can You Go with NXP's Flexible Layerscape Portfolio?  Learn from Our Experience! Hints, Tips and Tricks to Speed your QorIQ® LS1012A, LS1043A and LS1046A Design Cycle using NXP Support  NXP RF Solutions for IoT to Deliver Reliable, High-Performance Wireless Connections What Can You Build with a 1W 64-bit ARM®v8 SoC? 
記事全体を表示
The i.MX RT10xx MCU family leverages high performance, extensive memory options, and security features aimed at protecting your IP. IP protection is a key concern for companies developing products based on embedded devices and these concerns may seem particularly troubling when working with external memories and board level programming facilities. This webinar explores how to utilize key security features during the production process to alleviate these concerns when developing with the i.MX RT10xx MCUs. The session will showcase the Cyclone production programmers available from PEmicro, the development workflow enabling the creation of an encrypted stand-alone programming (eSAP) image with the Secure Boot Utility, and establishing a secure connection to the device for provision and programming. Presenters: Clark Jarvis, Ecosystem Product Marketer, NXP Kevin Perreault, President, PEmicro
記事全体を表示
Overview of the S32x next-generation safety architecture spanning ASIL B to ASIL D. What’s new and how we better enable the customer with a full set of safety collateral including MCU HW, SW and SBC HW.
記事全体を表示
Cyber Physical Systems are networked computer controlled machines capable of generating effects in the physical world. As humans who live in the physical world, we have more than a passing interest in making sure these systems can be trusted to do what they are supposed to be doing. This session describes the hardware and software associated with NXP’s Layerscape processors that provide the basis of trustworthy operation.
記事全体を表示