Technology Days - Training Material

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

Discussions

Sort by:
Learn about using NXP’s high-performance line of Arm® microprocessors for real-time industrial control applications. The Open Industrial Linux® SDK provides multiple levels of real-time performance, and provides support for Ethernet Time-Sensitive Networking (TSN).
View full article
Review of NXP’s current CAN portfolio and CAN functions, our support for CAN FD and an overview of the breakthrough products keeping CAN highly relevant for the new generation of vehicles.
View full article
NXP's Essential Audio Processing (EAP) software library is available on several NXP platforms to help enhance the audio playback of your product. With support for several audio algorithms such as static equalizer, dynamic bass boost, limiter, 3D effect and more, EAP provides a great audio experience for users. To permit easy and fast enablement, NXP's EAP library is available in the MCUXpresso SDK with integrated examples, and an associated Audio Tuning Tool that enables you to easily tune and simulate EAP behavior without any hardware. Join this session for an overview of EAP and its features. Presenters: Christophe Boulant, Voice & Audio TEC Team, NXP Shelby Unger, MCU Ecosystem Product Marketer, NXP
View full article
2019 is forecasted to be the year that voice will move beyond smart speakers to all segments of the IoT/industrial market. In this class we will give an overview of different architectures and solutions that can be implemented based on NXP processors.
View full article
Along with industry leading performance and integration, the i.MX RT crossover processor family integrates strong security protections. With the latest NXP software and tools, every design can integrate boot authentication and encrypted execution. Join this session to use the MCUXpresso Tools to protect your design. Learn about the threats and attacks that can be mitigated for every embedded design.
View full article
This session introduces new low cost S32V system-on-module (SOM) board from MicroSys for vision processing. Class also walks through complete hardware and software ecosystem with hands-on approach. These boards include support with QNX, LDW demo and many other demos.
View full article
AWS Shadow - Labs 1-2
View full article
This presentation provides an overview of the new toolchain to support the S32 platform of MCUs and application processors, this includes an IDE with new project generation, extensive collateral for ease of use and getting started as well as the next-generation Debugger tools, a new Flash tool specifically design for the S32 platform, the S32 configuration tool plus numerous software products integrated into the toolchain for ease of customer use.
View full article
With its broad portfolio, NXP is uniquely positioned to propose a full system allowing a scalability from NCAP to L4/L5 autonomous driving. To address such scalability, NXP has faced some challenging decisions about the system partitioning, performance, safety decomposition, AI Acceleration and Programming language. All these challenges will be addressed during the session.
View full article
NXP recently announced its first Azure Sphere-certified crossover applications processor chip, the i.MX 8ULP-CS SoloLite with Azure Sphere, and plans to build additional Azure Sphere-certified chips as part of the NXP i.MX 9 series. Join this tech talk to learn about Azure Sphere and what it means to have a highly secured solution from the hardware to the cloud. We’ll discuss the specific challenges of building and securing connected devices and what sets the i.MX 8ULP-CS apart. We’ll dig into the four components of Azure Sphere, all of which are included with the i.MX 8ULP-CS: Microsoft Pluton on NXP EdgeLock™ secure enclave for a secured hardware root of trust, the secured Azure Sphere OS, the cloud-based Azure Sphere Security Service, and the ongoing OS updates and security improvements supported by Microsoft experts for the lifetime of the device. Presenters: Sudhanva Huruli, Program Manager, Azure Sphere Naama Bak, Business Development and IoT Security, NXP Semiconductors
View full article
This class will teach you how to spin a BLDC, PMSM or ACIM motor with KMS. You do not need prior motor control experience. You will use the KMS GUI to do motor tuning and MCUXpresso IDE to develop a stand-alone motor control project. Bring your own motor and we will test it with KMS. With your registration please indicate the voltage and max current of your motor.
View full article
Introduction to A100x secure authenticator, authentication protocols, what to look for in security IC, and potential use cases.
View full article
Introduction to i.MX RT products and automotive qualified variants for multimedia applications requiring real time processing and low bill of materials.
View full article
In-vehicle wireless charging solutions portfolio overview, automotive grade hardware and software offerings, market success stories, technical description of charging deliver and control, foreign object detection, NFC and AUTOSAR integration, and special considerations for in-vehicle operation.
View full article
Go deep on the Industry's broadest and most scalable Cortex-M portfolio.
View full article
DDR4 (and beyond) dramatically increased the complexity of DDR configuration - even after simulation. More importantly, knowing the right parameters for DDR can make or break the performance of your product. Learn how to configure, optimize and validate DDR functionality directly on your board. Understand the tools and techniquest to obtain the data eye margins, reduce the time for DDR board bring-up and functional validation from weeks to hours.
View full article
Explores the fast-growing Automotive Gateway market, identifying key use cases and requirements, and how gateways will evolve over the next decade.
View full article