Technology Days - Training Material

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

Discussions

Sort by:
No other company has the breadth and diversity of embedded solutions for addressing the challenge of IoT security. From secure element ICs to advanced multimedia and networking microprocessors, NXP delivers the technology needed for securing the entire Lifecycle of the end or edge node. In addition, with Edgescale Cloud services software, devices can be maintained from deployment until decomissioning. Join this class for an overview of NXP's security solution.
View full article
Understand difference between consumer and automotive Ethernet and evolution of automotive communication architecture with the new CAN technologies and higher-speed Ethernet.
View full article
Understand the value, benefits and features  of Arm's latest Cortex-M33 core through a LPC5500-based product training and hand-on session.
View full article
Learn more about the innovative new industry standard USB Type-C connector offering seamless connectivity of data, video, power and security over a single connector. Usage spans multiple applications from computing and mobile to peripherals and accessories. You will learn about the compelling applications and NXP’s leadership in AC-DC, TC-PC PHY, high-speed switching signal integrity, authentication and power switches product portfolio offering differentiated end-to end Type-C solutions.
View full article
This session will provide an overview of the NXP wireless charging solutions portfolio with integrated NFC communication in wireless charging transmitters. Attendees will receive a clear understanding about NXP’s state of the art transmit and receive reference designs available for automotive, consumer, appliance and infrastructure markets.
View full article
This session will feature the LPC54114 MCU, the latest release of the LPC54000 low-power series, to demonstrate how to take advantage of dual-core architecture in always-on applications. Optimize product design for extended battery life and bring them to market quickly with this hands-on session. Topics will range from system architecture, software design and debugging, to power optimization, sound detection, and voice triggering.
View full article
This hands-on session introduces the MCUXpresso suite of tools (IDE, SDK, Config Tools) and shows users how to rapidly start development with thousands of Kinetis and LPC MCUs based on the Arm® Cortex®-M core. Using either Kinetis, LPC or i.MX RT development hardware, attendees will build a custom SDK, configure pins and clocks settings, generate a project, import and debug an application.
View full article
This session will provide an introduction to automotive cybersecurity. Amongst others, we will outline: NXP's automotive security product portfolio; industry standards and best practices; and NXP's global security organization, cybersecurity design and business practices.
View full article
The session will introduce an upcoming xEV traction motor power inverter platform system-play solution featuring a new MCU, new IGBT gate driver, and new safe SBC bound together with system enablement software and ASIL-D compliant safety support. A fully functional traction motor reference design being designed by partner Vepco will also be introduced based on a Power IGBT Module from Fuji Electric. The session will describe the platform’s components, software structure, value proposition, enablement support and go-to-market approach to help enhance understanding of the application and NXP solution as well as how to sell the system platform.
View full article
Discover NXP’s Layerscape multicore 64-bit ARM®-based solutions and learn how this scalable family leverages line-rate networking and production grade software to accelerate your time-to-market in industrial, networking and consumer applications.
View full article
Hands-on class diving into advanced debugging and trace features featured in MCUXpresso IDE.
View full article
This class will provide an overview of the i.MX RT series, key peripheral, including a demo using the i.MX RT EVK.
View full article
This presentation will first highlights some basic training techniques, such as data augmentation, but the primary focus will be on various ways to deploy neural network frameworks and classical machine learning algorithms, and most importantly, utilizing a variety of open source tools and techniques. We will show how these techniques fit in with some real use cases such as object recognition and anomaly detection. The hands-on session portion of the class will allow attendees to take a trained neural network model and deploy it on a i.MX 8M. Attendees will utilize the Linux development environment and implement an end-to-end use case.
View full article
Learn about NXP's secured IoT Gateway platform with sensor fusion, local and cloud analytic. IoT data aggregation, sensor fusion and analytic processes are run in VMs providing VM isolation advantage. IoT processes can also run in Virtualized Network Functions (VnF) that can run as service chains across end-to-end virtualized network equipment.
View full article
Near-field-communication (NFC) is the better, safer way to protect brands while ensuring ease of use for accessories and consumables. With NFC, the device itself can verify the authenticity and can configure operating modes or change settings based on the type of accessory or consumable. With a standard NFC phone, a user can check the originality or trigger a reorder through a simple tap. Based on the brand new NFC Nutshell Kit we will show which options exist on NFC tag and reader side, and how to implement a solution into even space constraint environments.
View full article
Secure designs begin with a security model consisting of policies, an understanding of the threat landscape and the methods used to enforce physical and logical security. To protect firmware execution given today’s threat landscape, there must be a policy to only allow execution of authenticated firmware. The methods used to enforce this policy rely on MCU security technology to create a protected boot flow. The boot firmware can contain public key cryptography to authenticate application code. In addition to these components integrated in the end device, there are tools and steps that must be taken in the manufacturing environment using manufacturing hardware for code signing and host programs for provisioning. Join this session to explore the design and implementation of a secure boot by making use of the Arm mbed TLS open source software and protect against firmware attacks.
View full article
Full power helm! A new way to design your power system, focused on the “Plumbing”! A simple EM physics and geometry based approach to designing power distribution networks on PCBs. From input power connection to the IC die, the simple rules discussed can be used to reduce power supply noise and improve EMC. Examples with results will be discussed.
View full article
Show the importance of OTA updates and the requirements for a total system solution for FOTA.
View full article
Amazon Alexa has changed voice control forever. Come learn about our i.MX based solutions for Amazon Alexa. Learn about our reference platforms, Solutions with AVS certified system Integraots what are the key factors to consider when designing a voice control solution and see how easily you can add Alexa into your next-generation devices.
View full article
Learn how to create a secure / non-secure application and debug on a secure Cortex-M33 NXP device.
View full article