NXP Tech Blog - 6ページ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Tech Blog - 6ページ

Eli_H
NXP Pro Support
NXP Pro Support

I was quite impressed with how quickly I could get LVGL up and running on the Mini-Monkey.     If you are looking at implementing embedded graphics on the LPC55S69 or another NXP part, LVGL should be on your short list for evaluation.    

詳細を読む...

件数が多いもの
1 0 6,113
brendonslade
NXP TechSupport
NXP TechSupport

On November 2nd, 2020 we introduced our latest debug tool - the new MCU-Link debug probe, initially supporting our general purpose Arm(R) Cortex(R)-M based MCUs, priced at just $10.99 from the nxp.com website.

詳細を読む...

件数が多いもの
2 0 3,936
brendonslade
NXP TechSupport
NXP TechSupport

Ázure RTOS ThreadX and other middleware components have now been released for i.MX RT1050/1060/1064 families. This highly optimized, safety-certified software can now be use for free in your projects.

詳細を読む...

件数が多いもの
1 0 4,310
petrstruzka
NXP Employee
NXP Employee

MCUXpresso Config Tools v8.1 release announcement.

詳細を読む...

件数が多いもの
0 0 2,104
yosoytono
Fresh Out Contributor

Dive into different aspects to optimize your software design with the NXP MBDT: a comprehensive collection of tools that plug into the MATLAB® and Simulink® model-based design environment to support fast prototyping, verification, and validation on NXP microcontroller

詳細を読む...

件数が多いもの
4 0 3,135
Eli_H
NXP Pro Support
NXP Pro Support

There is often confusion that "Edge Processing" and "Cloud" solutions are distinct offerings.   In my opinion, they should be combined to enable truly remarkable offerings.

詳細を読む...

件数が多いもの
0 0 6,790
petrstruzka
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso Secure Provisioning Tool v2 is now available.

MCUXpresso Secure Provisioning Tool is a graphical user interface (GUI) tool covering the secure boot
process, aimed primarily at microcontroller customers. It provides unified GUI front-end over existing
command-line tools - FlashLoader, elftosb, blhost, cst.

詳細を読む...

件数が多いもの
0 0 2,440
CJarvis
NXP Employee
NXP Employee

Interested in a basic overview of the MCUXpresso Secure Provisioning Tool and seeing a live demonstration of the tool?

A new training module for the MCUXpresso Secure Provisioning Tool is posted at the https://nxp.com/training site.

詳細を読む...

件数が多いもの
0 0 2,287
Eli_H
NXP Pro Support
NXP Pro Support

In some of my past articles on the PowerQuad,  we examined some common signal processing operations (IIR BiQuad and the Fast Fourier Transform) and then showed  how to use the PowerQuad  DSP engine to accelerate the computations.        The matrix engine in the PowerQuad can be used to perform common matrix and vector operations to free the M33 CPU(s) to perform other tasks in parallel.     In general, the matrix engine is limited to a maximum size of 16x16 size (or 256 operations).

詳細を読む...

件数が多いもの
0 0 3,670
nxf64478
NXP Employee
NXP Employee

The i.MX RT series bridges the simplicity of MCUs with the complexity of applications processors into a hybrid portfolio offering ease-of-use designed to address the growing consumer demand for enhanced user experiences. Offering high-performance – up to 1Ghz – modernized HMI capabilities, expanded memory options, and advanced security, the i.MX RT series can help you push the boundaries of what is possible in the IoT – even on price-conscious designs.  The possibilities are endless: Imagine using the i.MX RT in clothing technology to help manage airflow; and maybe that device interacts with others such as smartwatches to actively cool the body. Similarly, imagine adding IoT capabilities to gaming devices for an enhanced gaming experience.

詳細を読む...

件数が多いもの
0 0 1,965
PetrKraus
NXP Employee
NXP Employee

There is a wiki page describing the way hot create the SCR entry for the SDK component here.

It is referenced from the MCUX SDK wiki space.

Feel free to put your comments and questions directly on the wiki page. 

詳細を読む...

件数が多いもの
0 0 2,157
Eli_H
NXP Pro Support
NXP Pro Support

I wanted to take a quick break from some of the PowerQuad articles to show off a neat library that works well with the LPC55S69.      One of the design features of the Mini-Monkey experiment was a 240x240 Pixel IPS display.     I feel that the LPC55S69 is a good fit for small, low active power embedded graphics applications.  It has quite a bit of internal SRAM to store a framebuffer and has lots of processing power to composite a scene on a small display.  In some of my previous articles,  we use this display to show static images as well as displaying time series data from a built in MEMs microphone.   I ran across a twitter user “The Performance Whisper” who had recently released a lightweight and efficient  animated GIF decoder.

詳細を読む...

件数が多いもの
1 0 4,832
devonna_dorton
NXP Employee
NXP Employee

NXP has released the newest versions of MCUXpresso SDK, IDE, Configuration Tools, and Secure Provisioning Tool. In addition to new product support, you will find these updates and enhanced features in the new releases.

詳細を読む...

件数が多いもの
0 0 2,469
MeganHansen
NXP Employee
NXP Employee

Today, NXP announced an update to the eIQ™ Machine Learning Software Development Environment, becoming the first semiconductor vendor to implement the Glow neural network compiler for vision-, sensor- and voice-based ML applications. This new neural network compiler technology delivers unprecedented inferencing performance for NXP’s i.MX RT series of crossover MCUs.

詳細を読む...

件数が多いもの
2 0 2,430
Eli_H
NXP Pro Support
NXP Pro Support

I had some design updates for “Rev B” of my Mini-Monkey design that I wanted to get in the "queue" for testing.  For the next revision, I wanted to try PCB:NG for the board fabrication and assembly.  PCB:NG is an “on-demand” PCB assembly service focused on turnkey prototypes via simple a web interface.    The pricing looked attractive and it appeared that the Mini-Monkey fit within their standard design rules.    The Mini-Monkey design uses an NXP LPC55S69 microcontroller that is in a 0.5mm pitch VFBGA98 package.   NXP offers guidance on how to use this device with low-cost design rules and I thought this would be a great test for PCB:NG.   I had success with Rev A at Macrofab and thought I would give PCB:NG a shot.

詳細を読む...

件数が多いもの
0 0 3,799
petrstruzka
NXP Employee
NXP Employee

We are pleased to announce that Config Tools for i.MX Application Processors v8 are now available.

The Config Tools for i.MX is a set of configuration tools that provide an efficient method
for evaluation and configuration of pins routing and DDR memory settings when designing
with NXP's application processors based on Arm® Cortex®-A cores, including i.MX MPUs.

詳細を読む...

件数が多いもの
0 0 2,824
petrstruzka
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso Config Tools v8 are now available.

MCUXpresso Configuration Tools is a product with set of tools that help users of all levels with a Cortex-M-based MCU solution.

詳細を読む...

件数が多いもの
1 0 3,066
lpcxpresso_supp
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso IDE v11.2.0 (build 4120) is now available. This is a major new version of the IDE, and contains new features, enhancements and bug fixes over the previous versions, including latest announced MCUXpresso IDE v11.1.1 .

詳細を読む...

件数が多いもの
0 0 4,822
ioana_maria_cul
Contributor I

This project was implemented by Ioana CULIC (ioana_maria.culic@upb.ro), PhD candidate at the Politehnica University of Bucharest, and Alexandru VOCHESCU (alexandru.vochescu@stud.acs.upb.ro) as part of his bachelor thesis at the Politehnica University of Bucharest. All the contributions are open source and are part of the Tock project, available on github.

詳細を読む...

件数が多いもの
0 0 3,092
Eli_H
NXP Pro Support
NXP Pro Support

In my last article, we examined a common time domain filter called the Biquad and how it could be computed using the LPC55S69 PowerQuad engine.        We will now turn our attention to another powerful component of the PowerQuad, the “Transform Engine”.      The PowerQuad transform engine can compute a Fast Fourier Transform (FFT) in both a power and time efficient manner leaving your main CPU cores to handle other tasks.  

詳細を読む...

件数が多いもの
1 0 5,148
Eli_H
NXP Pro Support
NXP Pro Support

In my last article,   we starting discussing the PowerQuad engine in the LPC55S69 as well as the concept of data in the “time domain”.    Using the Mini-Monkey board, we showed the function of collecting a bucket of data over time.     I chose to use a microphone as a data source as it is easy to visualize and understand.      You can now easily imagine replacing the microphone with *anything* that changes over time.     In this article we are going to look at some common algorithms for processing data in the time domain.  In particular, we will look at the “Dual Biquad IIR” engine in the LPC55S69 PowerQuad. An IIR biquad is a commonly used building block as it is possible to configure the filter for many common filtering use cases.   This article is not intended to review all of the DSP theory behind IIR filter implementations but I do want to highlight some key points and the PowerQuad implementation.

詳細を読む...

件数が多いもの
1 0 5,905
diego_dorta
NXP Employee
NXP Employee

PyeIQ is written on top of eIQ ML Software Development Environment and provides a set of Python classes allowing the user to run Machine Learning applications in a simplified and efficient way without spending time on cross-compilations, deployments, or reading extensive guides.

詳細を読む...

件数が多いもの
11 0 13K
andrewmeyerbti
Contributor III

The internal clock frequency of Kinetis chips varies due to manufacturing tolerances. A trim value is programmed into the chips to compensate for this variance and make the slow bus frequency uniform between chips.

For some inexplicable reason, this trim value is not active during debug mode. This makes developing serial and CAN applications very difficult, as the baud rates which are set are not the baud rates which are achieved. To make matters worse, if I understand the documentation correctly, the baud rate in debug mode is different from the baud rate in normal mode.

詳細を読む...

件数が多いもの
0 0 2,522
Eli_H
NXP Pro Support
NXP Pro Support

Built into the LPC55S69 is a powerful coprocessor called the “PowerQuad”.   In this article we are going to introduce the PowerQuad and some interesting use cases.   Over the next several weeks we will look at using some of the different processing elements in the PowerQuad using the “Mini-Monkey” board.   

詳細を読む...

件数が多いもの
2 2 8,573
ashokfair
Contributor IV

Hi All,

This is Mini Drum Pad build in with IMXRT1015. Also it has AFE shield board which is used for capsense buttons.

IMX RT is, using SAI to play the audio file at 16KHZ. I have created 12 samples (.wav file) and the raw data is stored in the music file. Based on the capsense button press triggering the sound effect.

Speaker I used is from Boat, it has internal battery so only thing required is to feed the Aux input from IMXRT EVK.

I felt that, button sense over I2C bit slow due to that having the limitation of playing the music as faster. Anyway its just demonstration of my concept.

詳細を読む...

件数が多いもの
0 0 2,140
iWave
Contributor V

Have you recently been sceptical of using a contact-based access system in your office or a public place? This trait is a major concern in most places for a valid reason. An access surface in a public place is used by many individuals, which makes it a potential source for contracting the deadly Covid 19 virus. Taking this into account, iWave Systems, a leading embedded solutions provider, has successfully demonstrated an alternative solution using facial recognition technology. The solution helps customers with a zero-contact access application by using individuals' faces to authorize access to a commercial/industrial space, home/office, transportation, banking, and Government sites.

詳細を読む...

件数が多いもの
0 0 2,504
brendonslade
NXP TechSupport
NXP TechSupport

Thanks to all of you that joined the MCUXpresso training we've been providing over the last few weeks and months via our webinars. We've also been adding more training videos covering some of the items from the webinars but also some more in-depth tips and tricks - check them out, and let us know what other videos you'd like to see!

詳細を読む...

件数が多いもの
0 0 3,182
monicavelez
NXP Employee
NXP Employee

In this blog, Mark Dunnett of embeddedpro puts the LPC55S16-EVK to the test ... How fast does it go? How much current does it take?

 

詳細を読む...

件数が多いもの
1 0 2,324
monicavelez
NXP Employee
NXP Employee

Mark Dunnett of embeddedpro shares his first impressions about the new LPC551x/S1x MCU family - our latest addition to the LPC5500 MCU series - complete with an unboxing experience. 

詳細を読む...

件数が多いもの
1 0 2,270
brendonslade
NXP TechSupport
NXP TechSupport

Share your FreeMASTER dashboard designs, get a board!

 

Calling all FreeMASTER fans!

 

Are you an experienced FreeMASTER user who has already created custom dashboards, or are you an HTML/Javascript coder who is new to this great tool and keen to share your creative ideas? With all the possibilities that resources such as jqWidgets, Google, PrimeUI, Plotly.js combined with FreeMASTER offer for creating engaging dashboards to control and/or demo your application, we'd love you to share your creations with the NXP Community. We are giving away* 50 NXP evaluation boards (20 each of the i.MX RT1020 and LPC55S28 EVKs, and 10 of the S32K144EVB) as a thank you to those of you who are willing to share your dashboards with our community.

詳細を読む...

件数が多いもの
2 13 12.4K