NXP Tech Blog - 11ページ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Tech Blog - 11ページ

CJarvis
NXP Employee
NXP Employee

In March of 2017, NXP released the debut version of the MCUXpresso SDK along with an IDE and set of Config Tools under the same MCUXpresso name.  Since that time we have seen an amazing response from developers downloading and using this suite of software and tools.  The number of MCUXpresso SDK downloads recently surpassed 100,000 unique downloads.

As the NXP and former Freescale microcontrollers were unified under one company, we knew we needed to provide a consistent and efficient software development platform – one that would allow you  the flexibility to develop on a wide range on NXP microcontrollers without the need to relearn a new software architecture or re-invent basic enablement functionality.

詳細を読む...

件数が多いもの
0 0 2,868
Ragan_Dunham
NXP Employee
NXP Employee

Machine Learning at the Edge:

eIQ Software for i.MX Applications Processors

Developing machine learning (ML) applications for embedded devices can be a daunting task. For the traditional embedded developer, the learning curve can be quite steep, as there are numerous decisions that must be made and new jargon that must be learned. Which framework should I choose? Which model best meets the requirements of my application and how do I know when it’s good enough? What “size” microcontroller or application processor do I need? The questions are many and figuring out how to get started can prove to be a challenge.

詳細を読む...

件数が多いもの
2 7 24.8K
brendonslade
NXP TechSupport
NXP TechSupport

LPC845 Breakout Board now has an SDK package available! We are working on updating our getting started information to show how to use this rather than starting from the LPC845 chip SDK. The board is called LPC845BREAKOUT in the SDK builder.

詳細を読む...

件数が多いもの
1 0 1,746
nxf39066
NXP Employee
NXP Employee

If you need to create you own SuperSet, following steps should help you.

First of all you need mcu-sdk-2.0 repository with current submodules. Then you need to create some release config e.g. release_config.yml on you disk. Release config format can be found here. Devices, boards or kits names referenced in release config are case sensitive!

詳細を読む...

件数が多いもの
2 1 3,195
nxf47831
NXP Employee
NXP Employee

New features update:

  •  SDKGEN-982Support adding all folder content recursively

        Generator now supports adding all files and all files of its subfolders under some directory recursively with wildcard.

詳細を読む...

件数が多いもの
1 0 2,091
petrstruzka
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso Config Tools v6 are now available.

MCUXpresso Configuration Tools is a product with set of tools that help users of all levels with a Cortex-M-based MCU solution.

詳細を読む...

件数が多いもの
1 0 3,203
nxf46154
NXP Employee
NXP Employee

New versions of MCUXpresso SDK, IDE, and Configuration Tools are now available. In addition to new product support, you will find these updates and enhanced features in the new releases

詳細を読む...

件数が多いもの
0 2 4,248
nxa18344
NXP Employee
NXP Employee

SPDK (Storage Performance Development Kit) is an optimized storage reference architecture. It is initiated and developed by Intel.

SPDK provides a set of tools and libraries for writing high performance, scalable, user-mode storage applications. It achieves high performance by moving all of the necessary drivers into userspace and operating in a polled mode, like DPDK.

詳細を読む...

件数が多いもの
0 0 4,633
lpcxpresso_supp
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso IDE v11.0.0 (build 2516) is now available.

This is a major new version of the IDE, and contains many new features and enhancements over the previous MCUXpresso IDE v10.3.1 and earlier releases. The attached presentation, recommended viewing for all users (new or experienced), provides an overview of many of the major changes, as well as things to be aware of when upgrading from an earlier release

詳細を読む...

件数が多いもの
5 0 7,542
lpcxpresso_supp
NXP Employee
NXP Employee

This article discusses the use of SDK Trustzone example (Hello World) for the LPC55S69 MCU within MCUXpresso IDE.

The following are required to follow this blog post:

  1. MCUXpresso IDE Version 11.0.x
  2. LPCXpresso 55S69 EVK development board
  3. LPCXpresso 55S69 EVK version 2.6 SDK
詳細を読む...

件数が多いもの
0 0 6,317
lpcxpresso_supp
NXP Employee
NXP Employee

When using the QN9080 with SDK v2.2 2019-01-29, or earlier, there is an issue in the SDK internal data which can lead to MCUXpresso IDE v11.0.0 failing to set consistent floating point options when importing multiple examples.

詳細を読む...

件数が多いもの
1 0 2,415
hemantagrawal
NXP Employee
NXP Employee

  • Disable hw_prefetch (u-boot):

setenv hwconfig 'fsl_ddr:bank_intlv=auto;core_prefetch:disable=0xFE'

qixis reset altbank (reset the board - in case using bank 0 run 'qixis reset' only)

 

  • bootargs or othbootargs - add below parameters to bootargs (u-boot).

                  Make sure you see the same in ‘cat /proc/cmdline’ once kernel is booted:

- use 1G hugepages:

default_hugepagesz=1024m hugepagesz=1024m hugepages=6 (or any number)

- isolate cpu's for user space (for the CPUs running DPDK without kernel interference):

isolcpus=1-7

- make sure no rcu stalls and watchdog prints:

nmi_watchdog=0 rcupdate.rcu_cpu_stall_suppress=1

詳細を読む...

件数が多いもの
0 0 3,751
BlackNight
NXP Employee
NXP Employee

With the cost of an single pin, many ARM Cortex-M boards including the NXP i.MX RT1064 can produde SWO data: think about a pin able to stream data out of the chip in realtime.

詳細を読む...

件数が多いもの
3 0 4,688
xiaodong_zhang
NXP Employee
NXP Employee

GmSSL is an open source cryptographic toolbox that supports SM2 / SM3 / SM4 / SM9 and other national secret (national commercial password) algorithm, SM2 digital certificate and SM2 certificate based on SSL / TLS secure communication protocol to support the national security hardware password device , To provide in line with the national standard programming interface and command line tools, can be used to build PKI / CA, secure communication, data encryption and other standards in line with national security applications. For more information, please access GmSSL official website http://gmssl.org/english.html.

詳細を読む...

件数が多いもの
1 0 3,475
nxf47831
NXP Employee
NXP Employee

New features update:

  •  SDKGEN-967Support to automatically hide doc files in Xtensa workspace

         Previously for Xtensa toolchain, developers need to use "hidden: true" in yml to hide documentation files in the                 workspace.
         Now generator can filter files by type attribute to bypass doc type file for Xtensa, which means files with .txt .rtf                 .html .htm .readme .pdf .Doxyfile .xls .css extensions will not be added into the Xtensa workspace.

詳細を読む...

件数が多いもの
1 0 2,191
BlackNight
NXP Employee
NXP Employee

In my previous articles I have used the command line on Linux to build and debug NXP MCUXpresso SDK applications. In this article I'm running code on NXP i.MX RT1064 in RAM or FLASH.

詳細を読む...

件数が多いもの
1 0 5,295
PetrKraus
NXP Employee
NXP Employee

Hi Team,

I would like to share python script for yml verification. It compares yml record with content of physical component folder. Provided information is:

  • Print list of components in yml.
  • Show which files are in yml, but not on disk.
  • Show which files are on disk, but not in yml.
詳細を読む...

件数が多いもの
1 0 1,987
BlackNight
NXP Employee
NXP Employee

Amazon Web Services has released a preconfigured FreeRTOS example for Armv8-M and the NXP LPCXpresso55S69 board. With the addition of board- and device-specific examples, it is even easier to start and use the Arm® TrustZone® features combined with MPU (Memory Protection Unit) on the NXP LPC55xx MCU.

詳細を読む...

件数が多いもの
1 0 3,916
xiaodong_zhang
NXP Employee
NXP Employee

GmSSL是一个开源的密码工具箱,支持SM2/SM3/SM4/SM9/ZUC等国密(国家商用密码)算法、SM2国密数字证书及基于SM2证书的SSL/TLS安全通信协议,提供符合国密规范的编程接口与命令行工具,可以用于构建PKI/CA、安全通信、数据加密等符合国密标准的安全应用。GmSSL项目是OpenSSL项目的分支,并与OpenSSL保持接口兼容。因此GmSSL可以替代应用中的OpenSSL组件,并使应用自动具备基于国密的安全能力。GmSSL项目采用对商业应用友好的类BSD开源许可证,开源且可以用于闭源的商业应用。

詳細を読む...

件数が多いもの
1 1 6,999
BlackNight
NXP Employee
NXP Employee

The ARM TrustZone is an optional secu=rity feature for Cortex-M33 which shall improve the security for embedded applications running on microcontroller as the NXP LPC55S69 (dual-core M33) on the LPC55S69-EVK.

詳細を読む...

件数が多いもの
1 1 10.6K
BlackNight
NXP Employee
NXP Employee

This article covers the NXP LPC55S69-EVK board: a dual ARM Cortex-M33 running at 100 MHz with ARM TrustZone

詳細を読む...

件数が多いもの
1 0 6,733
PetrKraus
NXP Employee
NXP Employee

Comprehensive information about SDK SW components and SDK release describing YML can be found in the Yml data record guide here:

http://10.193.108.154:4000/mcu-sdk-generator/doc/Yml%20data%20record%20guide.html#add-a-middleware-y...

Example

We need to build a dependency from the eIQ component to the CMSIS DSK Library component.

詳細を読む...

件数が多いもの
2 0 2,269
nxf47831
NXP Employee
NXP Employee

New features update:

  •  SDKGEN-924Support to automatically link secure and non-secure projects in Mcuxpresso IDE

        This feature supports to link trustzone projects. In MCUXpresso IDE, if you select a secure project or non-secure         project, the other trustzone paired project will be selected automatically.
        In order to enable the feature, "linked_project" need to be set for both projects.

詳細を読む...

件数が多いもの
1 0 2,319
BlackNight
NXP Employee
NXP Employee

In “Tutorial: MCUXpresso SDK with Linux, Part 1: Installation and Build with Maked” I used cmake and make to build the SDK application. In this part I’m going to use the command line gdb to debug the application on the board.

詳細を読む...

件数が多いもの
0 0 6,095
BlackNight
NXP Employee
NXP Employee

I admit: my work laptop machine is running a Windows 10 OS by default. But this does not prevent me running Linux in a Virtual Machine (VM). Each host platform has its benefits, and I don’t feel biased to one or the other, but I have started using Ubuntu more and more, simply because I have worked more on Embedded Linux projects. While I have used mostly Windows with Eclipse for NXP LPC, Kinetis and i.MX platforms in the past, I started using Ubuntu too from last year with the NXP MCUXpresso SDK. I did not find much documentation about this on the web, so I thought it might be a good idea to write a tutorial about it. So here we go…

詳細を読む...

件数が多いもの
3 0 14.2K
Kathleen
NXP Employee
NXP Employee

The way in which people digest information is changing, as more distractions lead way to shorter attention spans and multi-tasking becomes even more important.  The new training series from NXP, i.MX RT Tech Minute, is intended to address this.  The need for technical information present in things like webinars, applications notes, white papers, etc. is important.  But what if you do not even know which topic you are interested in?  How do you know where to get started?

詳細を読む...

件数が多いもの
0 0 2,073
PetrKraus
NXP Employee
NXP Employee

If you need to create of modify YML files describing SDK release and included SW components, you can get detailed information about a format of those YML files here:

https://bitbucket.sw.nxp.com/projects/MCUCORE/repos/mcu-sdk-generator/browse/doc/Yml%20data%20record...

詳細を読む...

件数が多いもの
2 0 2,262
Kathleen
NXP Employee
NXP Employee

As a marketer, I never like to use the suffix “less” as it usually has a negative connotation.  “Less” means not having; without; free from something. Words like hopeless, motionless, and helpless come to mind.  So, when a system architect recently spoke to me about the products in the i.MX RT series and referred to them as being flashless, I cringed a little.

But, is being flashless such a bad thing?  Yes, it means it has no flash memory on-chip, but that is actually giving customers more - More opportunity for differentiated on-chip peripherals.  More options for selecting the perfect memory.  And more opportunity to create cost competitive solutions.

詳細を読む...

件数が多いもの
0 0 1,953
tomaslestyan
NXP Employee
NXP Employee

ENG

TODO

 

CZ-SK

Vytvorenie témy

Dokument je možné vytvoriť na internej komunite dostupnej výhradne NXP zamestnancom. Po tom čo zadanie splní všetky potrebné náležitosti, bude presunuté na verejne dostupnú komunitu.

Vzor pre vytvorenie témy*.

詳細を読む...

件数が多いもの
1 0 1,609
nxf47831
NXP Employee
NXP Employee

New features update:

  •  SDKGEN-865Support IAR compiler optimization strategy flag for library projects

        Compiler Optimization flags are supported for IAR application and library projects:

        1. -On / -Ol / -Om / -Oh / -Oh -Ssize / -Oh -Sspeed / -Oh -Sbalance / --no_size_contraints

詳細を読む...

件数が多いもの
1 0 2,055