RDDRONE-BMS772 Development Board Accessories RDDRONE-BMS772开发板配件 I want to purchase the RDDRONE-BMS772 development board for battery-related experiments. I need to measure and record the voltage, current, and temperature data of the experimental battery. Besides the accessories included with the development board on the official website, what other accessories do I need to purchase, such as the battery itself and a compatible battery charger? In other words, I need to conduct battery experiments and measure and record the battery's voltage, current, and temperature data. In addition to the accessories included in the development board packaging, what other related accessories do I need for this experiment? Could you please provide a detailed list of accessories, preferably including the compatible models of these accessories? I need to purchase them all at once for the experiments. Thank you very much.
我现在想要购买RDDRONE-BMS772这个型号的开发板进行电池的相关实验需要测量记录实验电池的电压、电流和温度数据,现在除了官网上开发板包含的配件之外,我还需要购买哪些配件,比如电池、和电池匹配的电池充电器这些其他需要的相关配件;就是说我现在需要进行电池实验,需要测量记录电池的电压、电流和温度数据,在这个实验的基础上,除了开发板包装里的配件之外我还需要哪些相关的其他配件,你能不能帮我列个详细的配件清单,最好能把适配开发板的这些配件型号也帮我列一下,我需要一次性购买来进行实验,万分感谢。 Re: RDDRONE-BMS772 Development Board Accessories RDDRONE-BMS772开发板配件 Dear Fan007,
for battery state estimation research, the RDDRONE-BMS772 requires a real 3S to 6S Li-ion battery pack with a balance connector and a matching charger. The documentation does not specify a particular battery or charger model. You just need to make sure that the parameters are within specified limits.
JozefKozon_1-1783586246113.png JozefKozon_2-1783586292642.png
For firmware development and debugging, an external debugger is recommended, such as:
SEGGER J-Link Mini
PEMicro Universal Multilink
Other compatible JTAG debuggers
The board provides JTAG (J2) and DCD-LZ (J19) debug interfaces. There is no direct USB programming/debugging from a PC, so an external debugger is necessary.
Minimum recommended setup:
RDDRONE-BMS772 board
3S Li-ion battery pack with balance connector
Compatible 3S charger
J-Link or PEMicro debugger
Windows PC with S32 Design Studio
This setup allows measurement of cell voltages, pack voltage, current (coulomb counting), temperature, and cell balancing, making it suitable for SOC/SOH algorithm development.
With Best Regards,
Jozef
Re: RDDRONE-BMS772 Development Board Accessories RDDRONE-BMS772开发板配件 I apologize, you didn't understand me. My current research is about battery state estimation, which requires measuring the voltage, current, and temperature data of a real battery. Therefore, I don't need a battery simulator; I need a real battery. So, I need a battery compatible with my development board and a specific model of the corresponding battery charger. Also, are the PEMicro adapter and SEGGER J-Link Mini debugger mentioned in the link necessary hardware for debugging or programming algorithms on the development board? Can't the development board be directly connected to a computer for debugging and programming? Are these adapters and debuggers available on the market? Furthermore, besides the hardware you mentioned, are there any other necessary hardware components for the development board? Please answer these questions in detail. Thank you very much.
抱歉,你没理解我的意思,我目前的研究是关于电池状态估计的,需要测量真实电池的电压电流和温度数据,所以我不需要电池模拟器,我需要的是真实的电池,所以我需要适配开发板的电池和对应电池充电器的具体型号;并且那个链接里提到的PEMicro适配器以及SEGGER J-Link Mini调试器是开发板调试或者烧录算法必须的硬件吗?开发板不能直接连接到电脑上进行调试和烧录程序吗?这些适配器和调试器在市面上可以买到吗?还有,开发板除了你提到的这几个硬件之外还有别的必须硬件吗?请您详细解答一下这些疑问,万分感谢。 Re: RDDRONE-BMS772 Development Board Accessories RDDRONE-BMS772开发板配件 I apologize, you didn't understand me. My current research is about battery state estimation, which requires measuring the voltage, current, and temperature data of a real battery. Therefore, I don't need a battery simulator; I need a real battery. So, I need a battery compatible with my development board and a specific model of the corresponding battery charger. Also, are the PEMicro adapter and SEGGER J-Link Mini debugger mentioned in the link necessary hardware for debugging or programming the development board? Can't the development board be directly connected to a computer for debugging and programming? Are these adapters and debuggers available on the market? Furthermore, besides the hardware you mentioned, are there any other necessary hardware components for the development board? Please answer these questions in detail. Thank you very much.
抱歉,你没理解我的意思,我目前的研究是关于电池状态估计的,需要测量真实电池的电压电流和温度数据,所以我不需要电池模拟器,我需要的是真实的电池,所以我需要适配开发板的电池和对应电池充电器的具体型号;并且那个链接里提到的PEMicro适配器以及SEGGER J-Link Mini调试器是开发板调试或者烧录算法必须的硬件吗?开发板不能直接连接到电脑上进行调试和烧录程序吗?这些适配器和调试器在市面上可以买到吗?还有,开发板除了你提到的这几个硬件之外还有别的必须硬件吗?请您详细解答一下这些疑问,万分感谢。 Re: RDDRONE-BMS772 Development Board Accessories RDDRONE-BMS772开发板配件 Dear Fan007,
for the additional HW needed with the RDDRONE-BMS772 please refer to this link.
JozefKozon_0-1783575667159.png
For the battery pack, we can offer you a BATT-6EMULATOR and BATT-14EXTENDER. The battery emulator can be used instead of the battery pack, but because there are different connectors, the battery extender should be in between.
With Best Regards,
Jozef
View full article