Hello:
Here's an example of an S32K358 running on a dual-core EB29.0 system, preferably with RTD4.0; however, if RTD4.0 isn't available, other versions are also acceptable.
Hello:
I'd like to provide an example of an S32K358 system based on a dual-core EB29.0 processor, preferably with RTD4.0; however, if RTD4.0 is unavailable, other versions are also acceptable.
Hello,
There are multiple examples for multicore.
For example directly in the:
https://community.nxp.com/t5/S32K/S32K324-Multi-Core-Example-Project-based-on-Whiteboard/m-p/1547771
or:
There are demos directly in the S32DS package.
Since EB tresos is not NXP tool, I am not aware of direct multicre demo here. You will probably need to do porting from the S32DS demos. RTD Drivers contain EB tresos based examples, but I did not find a full multicore project.
petervlna_0-1783669665552.png
You can also check attached presentation.
best regards,
Peter
https://community.nxp.com/t5/S32K/S32K324-Multi-Core-Example-Project-based-on-Whiteboard/mp/1547771I opened this link and found an example (s32k324_dualcore_demo), which is based on S32K3_RTD_1_0_0_D2110_ASR_REL_4_4_REV_0000_20211007, with an RTD of 1.0. I am currently using S32. I'm having trouble opening the example code with DS v3.5 and RTD 4.0. I can't find this version of RTD on the official website. Could you please send it to me? Also, I'm using S32 DS v3.5. Does RTD 1.0 support this? Do I need to install v3.4? Can I install both v3.4 and v3.5 at the same time?