Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Grow a Garden 2 Movement Guide: How to Walk Faster Instantly If you have spent any decent amount of time grinding in Roblox Grow a Garden 2, you already know the pain of moving at a snail's pace. When a rare mutation event triggers and you need to secure those seeds before anyone else, or when a greenhouse thief is trying to swipe your hard work, every second counts. Navigating those massive plots can feel like a massive chore if you are stuck at base speed. Fortunately, you do not have to settle for the default walk cycle. Whether you want a permanent passive buff, a quick consumable sprint, or a hilarious physics glitch to launch yourself across the map, here is exactly how to maximize your movement speed instantly. Permanent Speed Boosts: The Bunny Stack Strategy If you want a reliable, permanent upgrade to your baseline speed, you need to dive into the game’s pet system. The undisputed kings of passive speed are Bunny pets. Each active Bunny pet you equip gives you a flat +5 Walk Speed bonus. When you first start out, the game allows you to equip up to three pets simultaneously. By stacking a full squad of three Bunnies right off the bat, you instantly gain a +15 speed bonus, completely changing how fast you cover ground. Getting your hands on these little speed demons comes down to two main methods: Keep an eye on the map. Bunnies randomly spawn in the world, and you can buy them outright for 20,000 Sheckles. Try your luck at the gacha. You can hatch them from a Common Egg, which features a pretty generous 30% hatch rate. Once you have your squad assembled, you can push your passive movement caps even higher by applying Pet Toys to your equipped Bunnies, which further enhances their baseline stats. Temporary Speed Boosts: Mushrooms and Teleportation Sometimes you do not need permanent speed; you just need an immediate, aggressive burst of velocity to chase down an intruder or sprint to the shop before a timer runs out. That is where gear and consumables come into play. Speed Mushrooms: For a quick fix, head over to the Gear Store and pick up some Speed Mushrooms for 1,500 Sheckles. Consuming one gives you a massive velocity boost for a short duration, perfect for clutch situations. Teleporter Wrench: If you have some cash to burn, save up 18,000 Sheckles for the Teleporter Wrench at the Gear Store. This legendary item lets you completely bypass the act of walking altogether by letting you instantly blink a short distance forward. The Fun Alternative: The Celestberry Physics Glitch If you are low on Sheckles but still want to move at hyper-speed, you can exploit a structural physics glitch carried over from the original game. It takes a little bit of setup, but the results are ridiculous. First, you need to grow a massive plant. A Celestberry works perfectly for this, though any high-tier, heavy plant like Bamboo will do. To super-size it, group multiple Basic and Advanced Sprinklers closely around the plant until it grows to a massive weight, ideally around 12 to 14 kg. Once your mega-plant is fully grown, harvest it and equip it directly into your hand. To trigger the launch, switch your camera view into first-person. Face completely away from your intended destination, hold down your backward movement key, turn on Shift Lock, and continuously tap your jump key. Because of the bizarre collision geometry of the giant fruit interacting with your character model, the game physics will break, violently flinging you backward across the map at insane speeds. Whether you choose to build a dedicated Bunny army, stock up on mushrooms, or fling yourself across the zone with a giant berry, there is no reason to suffer through slow walk speeds anymore. Pick the method that fits your budget and start zooming around your plot.
View full article
《种植花园2》运动指南:如何立即提高步行速度 如果你在 Roblox Grow a Garden 2 中花费了相当多的时间,你肯定已经体会过那种蜗牛般缓慢前进的痛苦。当罕见的变异事件触发信号,你需要抢在其他人之前获得这些种子,或者当温室窃贼试图偷走你的劳动成果时,每一秒都至关重要。如果速度被限制在基础速度,那么探索这些庞大的地图会感觉像是一项艰巨的任务。 幸运的是,你不必局限于默认的行走循环。无论你是想要永久被动增益、快速消耗冲刺,还是利用搞笑的物理漏洞把自己弹射到地图的另一端,这里都详细介绍了如何立即最大化你的移动速度。 永久加速:兔子堆叠策略 如果你想可靠、永久地提升你的基础速度,你需要深入了解游戏中的宠物系统。被动速度之王当属兔子宠物。 每装备一只活跃的兔子宠物,即可获得 +5 行走速度加成。游戏初期,玩家最多可以同时装备三只宠物。一开始就组建一支由三只兔子组成的完整队伍,你就能立即获得 +15 的速度加成,彻底改变你行进的速度。 想要入手这些速度小恶魔主要有两种方法: 密切关注地图。兔子会在世界各地随机出现,你可以花 20,000 谢克尔直接购买它们。 试试扭蛋的运气吧。你可以从普通蛋中孵化它们,普通蛋的孵化率相当高,为 30%。 组建好队伍后,你可以给装备了宠物玩具的兔子佩戴,进一步提升它们的被动移动上限,从而增强它们的基础属性。 临时加速手段:蘑菇和传送 有时你不需要持续的速度;你只需要立即爆发出惊人的速度去追赶入侵者,或者在计时器归零前冲到商店。这就需要用到装备和消耗品了。 速度蘑菇:想要快速提升速度,可以前往装备商店,花费 1,500 谢克尔购买一些速度蘑菇。服用一粒即可在短时间内大幅提升速度,非常适合关键时刻使用。 传送扳手:如果你钱多得没处花,那就攒够 18,000 谢克尔去装备商店购买传送扳手吧。这件传奇物品可以让你完全跳过行走这一行动,瞬间向前闪现一小段距离。 有趣的替代方案:Celestberry 物理故障 如果你谢克尔币不多,但仍然想以超高速移动,你可以利用从原版游戏中继承下来的结构物理漏洞。虽然需要一些前期准备工作,但结果令人难以置信。 首先,你需要种植一株巨大的植物。虽然任何高级、重型植物(如竹子)都可以,但用天青树做植物就非常合适。为了让它长得更大,可以在植物周围紧密地放置多个基础型和高级型喷水器,直到它长到非常重,理想情况下达到 12 到 14 公斤左右。 当你的巨型植物完全成熟后,收获它并直接装备到你的手中。 要触发信号,用上市,请将相机视角切换到第一人称视角。完全背对目的地,按住后退键,打开 Shift Lock,然后连续 TAP 跳跃键。由于巨型水果与你的角色模型相互作用时产生了奇异的碰撞几何形状,游戏物理引擎将会崩溃,将你以疯狂的速度猛烈地向后抛出地图的另一端。 无论你是选择组建一支专用的兔子军队,囤积蘑菇,还是用一颗巨大的浆果把自己弹射到地图的另一端,你都不必再忍受缓慢的行走速度了。选择适合您预算的方法,然后开始在您的地块上快速行驶。
View full article
i.MX 93 CAN1 多工化ドキュメントの不一致 こんにちは、NXPコミュニティの皆さん、 技術的な質問をしているうちに、現行版の i.MX 93リファレンスマニュアルと旧版の間にMUXモードの不一致があることに気づきました。 問題のCPUパッドはPDM_STREAM0(ピンJ17)で、現在のリファレンスマニュアル(Rev.7、2026-02-10)では、MUXモードオプション6をCAN1_TXと説明しています。 voipacHW_0-1781789044248.png 一方、古いリファレンスマニュアル(2023年版)や現在のConfig Tools for i.MX(バージョン26.03)では、代わりにCAN1_RX機能が表示されています: voipacHW_3-1781789377931.png voipacHW_2-1781789238035.png この不一致についてご説明いただけますか? ありがとう、 マーティン Re: i.MX 93 CAN1 Muxing Documentation Mismatch こんにちは、 @voipacHW さん。 文書の変更点を確認しましたが、そのページには変更内容に関連するコメントは見当たりませんでした。現時点では、これはタイプミスであると思われます。 現在、社内チームからの確認を待っているところですが、入手可能な情報に基づくと、単なるタイプミスである可能性が高いです。 よろしくお願いします、 チャビラ Re: i.MX 93 CAN1 Muxing Documentation Mismatch こんにちは、 @Chavira さん。 お返事ありがとうございます。 はい、同僚からの確認が取れ次第、お知らせください。 もし誤字が確認できれば、現在のリファレンスマニュアルで修正することをお勧めします。 ありがとう、 マーティン Re: i.MX 93 CAN1 Muxing Documentation Mismatch こんにちは、 @voipacHW さん。 社内チームは、これが確かにタイプミスであることを確認しました。 ご指摘いただき、またご意見をいただきありがとうございます。感謝しています フィードバックをいただくと、次回のリファレンスマニュアル改訂で問題が修正されます。 よろしくお願いします、 チャビラ
View full article
ADC用パッド/マルチプレクサ制御 こんにちは。現在、カスタムi.MX8Xキャリアボード用のファームウェアを開発中です。ADC_IN0~ADC_IN5については、特にsw_configフィールドに関して、パッド/マルチプレクサの制御設定をどうすべきか、現時点では不明です。 フィールド値を「デフォルト」に設定すると、パッドに設定されているmuxモードに自動的に設定されますか(つまり、自動的にADCに調整されるのと、GPIOに変更した場合とを比較するとどうでしょうか? ADCピンの設定を「デフォルト」にするのは良い選択でしょうか、それとももっと適切なフィールド選択方法がありますか? i.MX 8ファミリ | i.MX 8QuadMax (8QM) | 8QuadPlus Re: Pad/Mux Control for ADC こんにちは、 「デフォルト」は多重化モードに対応しておらず、ADCにも対応していません。 i.MX8XのADCピンについては、パッド制御を明示的に設定して、すべてのプル/キーパーを無効にし、デジタルの影響を最小限に抑えてください。 よろしくお願いいたします。 アルド。
View full article
S32K311チップのUARTを設定する際、単純な送信機能であっても、正しく送信するためには、制御基板の電源を毎回オフにしてから再度オンにする必要があります。 S32K311チップのUARTを設定する際、単純な送信機能では、データを正しく送信するために、制御基板の電源を毎回オン/オフする必要があります。データ送信には、Lpuart_Uart_Ip_AsyncSend関数を使用することをお勧めします。 Re: S32K311芯片 在配置uart时,简单的发送函数,每次都需要给控制板断电重新上电才能正常发送 こんにちは、フィンクさん プロジェクトの詳細を教えていただければ、私が確認いたします。 使用しているハードウェアを教えてください。公式のEVBでない場合は、外部水晶発振器の周波数を教えてください。 Re: S32K311芯片 在配置uart时,简单的发送函数,每次都需要给控制板断电重新上电才能正常发送 ソフトウェアバージョン S32DS 3.6.0RTD 6.0.0、外部水晶発振器 20MHz Finnc_1-1782090062838.png Re: S32K311芯片 在配置uart时,简单的发送函数,每次都需要给控制板断电重新上电才能正常发送 こんにちは、フィンクさん ご提供いただいたプロジェクトを確認し、テストしてみました。私の環境では問題なく動作しました。
View full article
NXP releases (MCAL, SDK, NBU) Hello, As we discussed in the call, please see below the list of NXP KW45 releases: NXP_KW45_MCAL_4.3_RTM_1.0.8 - NBU Release - 1.9.23.4, cdd_ble_component rtm_1_0_9   https://community.nxp.com/t5/Marquardt-KW3x/NBU-CDD-library-release-NBU-version-1-9-23-4-cdd-ble-component/ta-p/2383134  NBU Version 1.9.23.4 (kw45b41_nbu_ble_1.9.23.4_20260605) SDK release 25.06.00 NXP_KW45_MCAL_4.3_RTM_1.0.8 - NBU Release - 1.9.23.2   https://community.nxp.com/t5/Marquardt-KW3x/NBU-release-NXP-KW45-MCAL-4-3-RTM-1-0-8-NBU-Release-1-9-23-2/ta-p/2326071  NBU Version 1.9.23.2 (kw45b41_nbu_ble_1.9.23.2_20260127) SDK release 25.06.00 NXP_KW45_MCAL_4.3_RTM_1.0.8 - NBU Release - 1.9.23.0   https://community.nxp.com/t5/Marquardt-KW3x/MCAL-Release-NXP-KW45-MCAL-4-3-RTM-1-0-8/ta-p/2171146  NBU Version 1.9.23.0 (kw45b41_nbu_ble_1.9.23.0_20250627) KW45 Early Access - Home (sharepoint.com)  SDK release 25.06.00 NXP_KW45_MCAL_4.3_RTM_1.0.7 - NBU Release - 1.9.14.4 MCAL release Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-RTM-1-0-7-NBU-Release-NBU-version-1-9-14-4/ta-p/2017789 NBU Version 1.9.14.4 (kw45b41_nbu_ble_1.9.14.4_20241220) KW45 Early Access - Home (sharepoint.com)  SDK release 2.16.100 NXP_KW45_MCAL_4.3_RTM_1.0.7 - NBU Release - 1.9.14.1 MCAL release Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-Release-NXP-KW45-MCAL-4-3-RTM-1-0-7-NBU-1-9-14-1/ta-p/1974166  NBU Version 1.9.14.1 (kw45b41_nbu_ble_1.9.14.1_20241030) KW45 Early Access - Home (sharepoint.com)  SDK release 2.16.100 NXP_KW45_MCAL_4.3_RTM_1.0.6 - NBU Release - 1.9.14.0 MCAL release Community link: https://community.nxp.com/t5/Marquardt-KW3x/NBU-Release-NBU-version-1-9-12-7-for-RTM1-04-and-RTM1-0-5/ta-p/1871915  NBU Version 1.9.14.0 (kw45b41_nbu_ble_1.9.14.0_20240712) KW45 Early Access - Home (sharepoint.com)  SDK release 2.16.000 NXP_KW45_MCAL_4.3_RTM_1.0.4/1.0.5 - NBU Release - 1.9.12.13 + BLE host libraries (1.8.17.5) MCAL release Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-RTM-1-0-4-NBU-amp-Host-Libraries-Release-NBU-version-1-9-12/ta-p/2015139  NBU Version 1.9.12.13 (kw45b41_nbu_ble_1.9.12.13_20241216) KW45 Early Access - Home (sharepoint.com)  SDK release 2.12.7 NXP_KW45_MCAL_4.3_RTM_1.0.4/1.0.5 - NBU Release - 1.9.12.9 + BLE host libraries (1.8.17.3) MCAL release Community link: https://community.nxp.com/t5/Marquardt-KW3x/NBU-Release-amp-BLE-Host-Libraries-NBU-version-1-9-12-9-for-RTM1/ta-p/1891371  NBU Version 1.9.12.9 (kw45b41_nbu_ble_1.9.12.9_20240607) KW45 Early Access - Home (sharepoint.com)  SDK release 2.12.7 NXP_KW45_MCAL_4.3_RTM_1.0.4/1.0.5 - NBU Release - 1.9.12.7 MCAL release Community link: https://community.nxp.com/t5/Marquardt-KW3x/NBU-Release-NBU-version-1-9-12-7-for-RTM1-04-and-RTM1-0-5/ta-p/1871915  NBU Version 1.9.12.7 (kw45b41_nbu_ble_1.9.12.7_20240523) KW45 Early Access - Home (sharepoint.com)  SDK release 2.12.7 NXP_KW45_MCAL_4.3_RTM_1.0.5 - NBU Release - 1.9.12.3 MCAL release Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-Release-NXP-KW45-MCAL-4-3-RTM-1-0-5/ta-p/1867995  NBU Version 1.9.12.3 (kw45b41_nbu_ble_1.9.12.3_20240205) KW45 Early Access - Home (sharepoint.com)  SDK release 2.12.7 NXP_KW45_MCAL_4.3_RTM_1.0.4 - NBU Release - 1.9.12.3 MCAL release Community link: [MCAL Release] NXP_KW45_MCAL_4.3_RTM_1.0.4 - NXP Community NBU Version 1.9.12.3 (kw45b41_nbu_ble_1.9.12.3_20240205) KW45 Early Access - Home (sharepoint.com)  SDK release 2.12.7 NXP_KW45_MCAL_4.3_RTM_1.0.3 - NBU Release - 1.9.11.1 MCAL release Community link: [MCAL Release] NXP_KW45_MCAL_4.3_RTM_1.0.3 - NXP Community NBU Version 1.9.11.1 (kw45b41_nbu_ble_1.9.10.0_20230721) KW45 Early Access - Home (sharepoint.com)  NXP_KW45_MCAL_4.3_RTM_1.0.2 - NBU Release - 1.9.10.8 MCAL release Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-4-3-RTM1-0-2-NBU-Release-kw45b41-nbu-ble-1-9-10-8/ta-p/1779168  NBU Version 1.9.10.8 (kw45b41_nbu_ble_1.9.10.8_20231221.zip) KW45 Early Access - Home (sharepoint.com)  SDK release - NXP_KW45_MCAL_4.3_RTM_1.0.2 - NBU Release - 1.9.10.7 MCAL release Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-4-3-RTM1-0-2-NBU-Release-kw45b41-nbu-ble-1-9-10-7/ta-p/1771606  NBU Version 1.9.10.7 (kw45b41_nbu_ble_1.9.10.7_20231208.zip) KW45 Early Access - Home (sharepoint.com)  SDK release - NXP_KW45_MCAL_4.3_RTM_1.0.2 - NBU Release - 1.9.10.5 MCAL release Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-4-3-RTM1-0-2-NBU-release-kw45b41-nbu-ble-1-9-10-5/ta-p/1732042  NBU Version 1.9.10.5 SDK release SDK 2.12.5. Equivalent to NXP_KW45_MCAL_4.3_RTM_1.0.2 https://mcuxpresso.nxp.com/  NXP_KW45_MCAL_4.3_RTM_1.0.2 MCAL release Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-Release-NXP-KW45-MCAL-4-3-RTM-1-0-2/ta-p/1694174  NBU Version 1.9.10 SDK release SDK 2.12.5. Equivalent to NXP_KW45_MCAL_4.3_RTM_1.0.2 https://mcuxpresso.nxp.com/ Internal Name MR2 NXP_KW45_MCAL_4.3_RTM_1.0.1 MCAL release Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-Release-NXP-KW45-MCAL-4-3-RTM-1-0-1/ta-p/1663509 NBU Version 1.9.5  SDK release SDK 2.12.4. Equivalent to NXP_KW45_MCAL_4.3_RTM_1.0.1 https://mcuxpresso.nxp.com/ Internal Name MR1 QP1 XP_KW45_MCAL_4.3_RTM_1.0.0 - NBU Release - 1.9.9.4 MCAL release Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-4-3-RTM1-0-0-NBU-release-kw45b41-nbu-ble-1-9-9-4/ta-p/1737586  NBU Version 1.9.9.4 SDK release SDK 2.12.2. Equivalent to NXP_KW45_MCAL_4.3_RTM_1.0.0 https://mcuxpresso.nxp.com/    KW45_MCAL4.3_RTM_1.0.0_QPATCH_3 MCAL release Community link: [MCAL RFP NBU Qualified Patch 3] KW45_MCAL4.3_RFP_... - NXP Community NBU Version 1.9.3 NEW SDK release SDK 2.12.2. Equivalent to KW45_MCAL4.3_RFP. https://mcuxpresso.nxp.com/ Internal Name RFP QP3 KW45_MCAL4.3_RTM_1.0.0_QPATCH_2 MCAL release Community link: [MCAL RFP NBU Qualified Patch 2] KW45_MCAL4.3_RFP_... - NXP Community NBU Version 1.9.4 NEW SDK release SDK 2.12.2. Equivalent to KW45_MCAL4.3_RFP. https://mcuxpresso.nxp.com/ Internal Name RFP QP2 MCAL4.3_PRC_0.6.1_QPATCH MCAL release MCAL4.3_PRC_0.6.1 : Same as PRC 0.6.1 Community link: [MCAL PRC 0.6.1 NBU Qualified Patch] KW45_MCAL4.3_... - NXP Community cdd_ble_component library: Same as PRC 0.6.1 NBU Version 1.8.13    (KW45 Early access Sharepoint - kw45b41_nbu_ble_hosted_1.8.13_20230317.zip) SDK release Same as PRC 0.6.1 Internal Name kw45b41_nbu_ble_hosted_1.8.13 KW45_MCAL4.3_RTM_1.0.0_QPATCH MCAL release Community link: [MCAL RFP Qualified Patch] KW45_MCAL4.3_RFP_QPATCH - NXP Community NBU Version 1.9.1 KW45 Early Access - Home (sharepoint.com)  kw45b41_nbu_ble_hosted_1.9.1_20230210.zip SDK release SDK 2.12.2. Equivalent to KW45_MCAL4.3_RFP. https://mcuxpresso.nxp.com/ Internal Name RFP QP1 KW45_MCAL4.3_RTM_1.0.0 MCAL release KW45_MCAL4.3_RTM1.0.0 https://mcuxpresso.nxp.com/download/c53c540c7b9a02f188b47f10332e345b Community link: [MCAL Release] KW45_MCAL4.3_RFP - NXP Community cdd_ble_component_library: https://mcuxpresso.nxp.com/download/0558d76f71d8f7890ae4f613ada9e8c3 NBU Version 1.9.0 KW45 Early Access - Home (sharepoint.com)  kw45b41_nbu_ble_hosted_1.9.0_20221216.zip SDK release SDK 2.12.2. Equivalent to KW45_MCAL4.3_RFP. https://mcuxpresso.nxp.com/ Internal Name RFP MCAL4.3_PRC_0.6.2 MCAL release MCAL4.3_PRC_0.6.2 https://mcuxpresso.nxp.com/download/c53c540c7b9a02f188b47f10332e345b Community link: [MCAL Release] KW45_MCAL4.3_PRC_0.6.2 - NXP Community cdd_ble_component_library: https://mcuxpresso.nxp.com/download/fa0096a6d7d27d931ed31efd31143934 NBU Version 1.8.12  KW45 Early Access - Home (sharepoint.com) (kw45b41_nbu_ble_hosted_1.8.12_20221110.zip) SDK release SDK 2.12.0. Same as MCAL4.3_PRC_0.6.0. https://mcuxpresso.nxp.com/ Internal Name PRC 3.2     MCAL4.3_PRC_0.6.1 MCAL release MCAL4.3_PRC_0.6.1 https://mcuxpresso.nxp.com/download/050648acde1353ae305f9d6be3cb8ecd Community link: [MCAL Release] KW45_MCAL4.3_PRC_0.6.1 - NXP Community cdd_ble_component library: https://mcuxpresso.nxp.com/download/f7414559019c10c1f0e5ed0f14d0e368 NBU Version 1.8.11. Same as MCAL4.3_PRC_0.6.0. (KW45 Early access Sharepoint - kw45b41_nbu_ble_hosted_1.8.11_20220916.zip) SDK release SDK 2.12.0. Same as MCAL4.3_PRC_0.6.0. https://mcuxpresso.nxp.com/ Internal Name PRC 3.1   ---------------------------------------------------------------------------------------------------------------------------------  MCAL4.3_PRC_0.6.0 MCAL release MCAL4.3_PRC_0.6.0 https://mcuxpresso.nxp.com/download/b8be34921fac89be30ac2f270d0b2572 Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-Release-KW45-MCAL4-3-PRC-0-6-0/ta-p/1524004  NBU Version 1.8.11 (KW45 Early access Sharepoint - kw45b41_nbu_ble_hosted_1.8.11_20220916.zip) SDK release SDK 2.12.0 https://mcuxpresso.nxp.com/ Internal Name PRC 3.0   --------------------------------------------------------------------------------------------------------------------------------- MCAL4.3_PRC_0.5.1 MCAL release MCAL4.3_PRC_0.5.1 https://mcuxpresso.nxp.com/download/fa05fa1903a9459667d03950e4543440 Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-Release-KW45-MCAL4-3-PRC-0-5-1/ta-p/1491059  NBU Version 1.8.10 (KW45 Early access Sharepoint - kw45b41_nbu_ble_hosted_1.8.10_20220711) SDK release Not applicable - only updated the MCAL release  SDK 2.11.4 https://mcuxpresso.nxp.com/ Internal Name PRC 2.1   --------------------------------------------------------------------------------------------------------------------------------- MCAL4.3_PRC_0.5.0 MCAL release MCAL4.3_PRC_0.5.0 https://mcuxpresso.nxp.com/download/ac7f55a6cd1e2f54becf20bed09adda0  Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-Release-KW45-MCAL4-3-PRC-0-5-0/ta-p/1487460 NBU Version 1.8.10 (KW45 Early access Sharepoint - kw45b41_nbu_ble_hosted_1.8.10_20220711) SDK release SDK 2.11.4 https://mcuxpresso.nxp.com/ Internal Name PRC 2.0   --------------------------------------------------------------------------------------------------------------------------------- MCAL_4.3_PRC_0_4_1 MCAL release MCAL_4.3_PRC_0_4_1 https://mcuxpresso.nxp.com/download/8fd26a41a95246d1e301b418e27bf93b Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-Release-NXP-KW45B41Z-MCAL-4-3-PRC-0-4-1/m-p/1459050 NBU Version 1.8.7 (KW45 Early access Sharepoint - kw45b41_nbu_ble_hosted_1.8.7_20220429) SDK release SDK 2.11.2 https://mcuxpresso.nxp.com/ Internal Name PRC 1.1 --------------------------------------------------------------------------------------------------------------------------------- MCAL_4.3_PRC_0_4_0 MCAL release MCAL_4.3_PRC_0_4_0 https://mcuxpresso.nxp.com/download/cf051d7abecbf716a946a58fabd9913f NBU Version 1.8.7 (KW45 Early access Sharepoint - kw45b41_nbu_ble_hosted_1.8.7_20220429) SDK release SDK 2.11.1 https://mcuxpresso.nxp.com/ Internal Name PRC 1.0 --------------------------------------------------------------------------------------------------------------------------------- MCAL_4.3_PRC_0_3_1 MCAL release MCAL_4_3_EAR_0_3_1 Community link: https://community.nxp.com/t5/Marquardt-KW3x/MCAL-Release-NXP-KW45B41Z-MCAL-4-3-EAR-0-3-1/ta-p/1428523 NBU Version 1.8.6 (KW45 Early access Sharepoint - kw45b41_nbu_ble_hosted_1.8.6_20220310.zip) SDK release SDK 2.10.4 https://mcuxpresso.nxp.com/ Internal Name EAR3.0
View full article
LPC5504: SPI via FLEXCOMM2/5 Hello, we would like to use SPI via FLEXCOMM5, but we have found conflicting information between the datasheet, reference manual, configurator, and community posts. From the documentation, SPI appears to be supported in some places: The datasheet lists SPI functionality on the FLEXCOMM5 pins: mme255_0-1781790955442.png The datasheet also refers to FLEXCOMM0–FLEXCOMM7 under SPI: mme255_1-1781791008935.png The reference manual states that SPI is available on all FLEXCOMM interfaces: mme255_4-1781791319751.png However, other sources suggest that SPI may not be supported on FLEXCOMM5: The configurator does not allow an SPI peripheral to be assigned to FLEXCOMM5: mme255_3-1781791035223.png The relevant table in the reference manual does not explicitly list SPI support for FLEXCOMM5: mme255_5-1781791439888.png I also found this NXP Community post, which says SPI is not available on FLEXCOMM5 due to missing SSEL pins: Support of SPI in FlexComm5 in LPC55S06 - NXP Community Could you clarify whether SPI can actually be used on FLEXCOMM5? Specifically, if we manually control the slave-select signal using a GPIO instead of a hardware SSEL pin, is it possible to use FLEXCOMM5 as an SPI interface at the hardware level? If it is possible from a hardware perspective, what SDK changes would be required to enable this? Also, are there any plans to officially support SPI on FLEXCOMM5 through the SDK in a future release? Thank you. LPC55xx Peripherals Re: LPC5504: SPI via FLEXCOMM2/5 Hi @mme255, Thank you for your post! The FlexComm 2 and FlexComm 5 instances on the LPC550x family do not support SPI. These FlexComm can still be used with other communication interfaces without any issues. Apologize the inconvenience this may cause. Re: LPC5504: SPI via FLEXCOMM2/5 Hi Carlos, thank you for the clarification and quick response. Best regards
View full article
LPC5504: FLEXCOMM2/5経由のSPI こんにちは、 FLEXCOMM5を通じてSPIを利用したいのですが、データシート、リファレンスマニュアル、コンフィギュレーター、コミュニティ投稿の間で情報が矛盾していることが判明しました。 ドキュメントによると、SPIは一部の場所でサポートされているようです: データシートには、 FLEXCOMM5のピンにおけるSPI機能が記載されています。 mme255_0-1781790955442.png データシートでは、 SPI の項目でFLEXCOMM0 ~ FLEXCOMM7についても言及されています。 mme255_1-1781791008935.png リファレンス・マニュアルには、SPIがすべてのFLEXCOMMインターフェースで利用可能であると記載されています。 mme255_4-1781791319751.png しかし、他の情報源によると、FLEXCOMM5ではSPIがサポートされていない可能性があるとのことです。 構成器はFLEXCOMM5にSPIペリフェラルを割り当てることを許可していません: mme255_3-1781791035223.png リファレンス・マニュアルの該当表には、FLEXCOMM5のSPIサポートが明示的に記載されていません。 mme255_5-1781791439888.png また、NXPコミュニティの投稿を見つけました。そこにはSSELピンが欠けているため、SPIはFLEXCOMM5で利用できないと書かれています: LPC55S06年のFlexComm5におけるSPIのサポート - NXPコミュニティ SPIが実際にFLEXCOMM5に使えるのか、詳しく教えていただけますか? 具体的には、ハードウェアSSELピンの代わりにGPIOを使ってスレーブセレクト信号を手動で制御した場合、ハードウェアレベルでFLEXCOMM5をSPIインターフェースとして使うことは可能でしょうか? もしハードウェアの観点から可能なら、これを有効にするためにはどのようなSDKsの変更が必要でしょうか?また、FUTUREにSDKsを通じてFLEXCOMM5上でSPIを正式にサポートする計画はありますか? よろしくお願いします。 LPC55xx ペリフェラル Re: LPC5504: SPI via FLEXCOMM2/5 こんにちは、 @mme255 さん。 投稿ありがとうございます! LPC550xファミリのFlexComm 2およびFlexComm 5インスタンスはSPIをサポートしていません。これらのFlexCommは他の通信インターフェースでも問題なく使用できます。 ご迷惑をおかけして申し訳ございません。 Re: LPC5504: SPI via FLEXCOMM2/5 こんにちは、カルロスさん。 ご説明と迅速なご対応、ありがとうございました。 よろしくお願いいたします。
View full article
LPC5504:通过FLEXCOM2/5接口进行SPI通信 你好, 我们想通过FLEXCOMM5使用 SPI ,但我们发现数据手册、参考手册、配置器和社区帖子之间存在相互矛盾的信息。 从文档来看,SPI 似乎在某些地方受支持: 数据手册列出了FLEXCOMM5引脚上的SPI功能: mme255_0-1781790955442.png 数据手册中还提到了SPI 下的FLEXCOMM0–FLEXCOMM7 : mme255_1-1781791008935.png 参考手册指出,所有FLEXCOMM接口均支持SPI: mme255_4-1781791319751.png 然而,其他消息来源表明,FLEXCOMM5 可能不支持 SPI: 配置器不允许将 SPI 外设分配给FLEXCOMM5 : mme255_3-1781791035223.png 参考手册中的相关表格并未明确列出FLEXCOMM5对SPI的支持情况: mme255_5-1781791439888.png 我还找到了这篇 NXP 社区帖子,其中提到由于缺少 SSEL 引脚,FLEXCOMM5 不支持 SPI: LPC55S06 中 FlexComm5 对 SPI 的支持 - NXP 社区 请问SPI是否真的可以在FLEXCOMM5上使用? 具体来说,如果我们使用 GPIO 而不是硬件 SSEL 引脚手动控制从机选择信号,是否可以将 FLEXCOMM5 用作硬件级别的 SPI 接口? 如果从硬件角度来看可行,需要对 SDK 进行哪些更改才能实现这一点?另外,未来版本中是否有计划通过 SDK 正式支持 FLEXCOMM5 上的 SPI? 谢谢! LPC55xx 外设 Re: LPC5504: SPI via FLEXCOMM2/5 嗨@mme255 , 感谢您的帖子! LPC550x 系列的 FlexComm 2 和 FlexComm 5 实例不支持 SPI。这些 FlexComm 仍然可以与其他通信接口一起使用,不会出现任何问题。 由此造成的不便,我们深表歉意。 Re: LPC5504: SPI via FLEXCOMM2/5 嗨,卡洛斯, 感谢您的澄清和快速回复。 顺祝商祺!
View full article
外部供給クロック信号の電圧仕様(MCX A185 VLH) 最大値が見つかりません。データシート上のMCXA185VLH MCUのEXTAL48Mピンで許容される電圧。 LPCxxxファミリのマイクロコントローラでは、発振器入力がこの振幅(0.85Vppなど)に非常に厳格であることを知っています。 外部から生成された3.3Vの発振クロック信号を直接EXTAL48Mピンに送ることはできますか? クロック|タイマー MCXA Re: Voltage specification for externally provided clock signal (MCX A185 VLH) 投稿ありがとうございます。 はい、データシートには最大 Vec (外部から提供される入力クロック振幅) が指定されています。電圧はVIHとして表されます。しかし、VIHは0.7xVDDなので、VDD=3.3Vの場合、最大ベクトル。電圧は2.31Vのみになります。 つまり、このデータシートの仕様が間違っているか、VDD=3.3Vの場合、Vecの最大値は実際には2.31Vなのでしょうか? Re: Voltage specification for externally provided clock signal (MCX A185 VLH) こんにちは、 @wyss-11 投稿ありがとうございます! MCXA18にはEXTAL48M入力電圧の定義がありますが、それは独立した固定のEXTAL48M電圧値としてではなく、VDDに対する標準入力しきい値VIH/VILを介して間接的に指定されます。 データシートには、発振のピークツーピーク振幅が標準値として0.6Vと記載されているだけです。 VDDが3.3 Vの場合EXTAL48M、クロックがVIH/VILの閾値を満たし、かつVDD + 0.3 Vの入力制限を超えない限り、3.3 Vの外部発振器で駆動可能です。 Re: Voltage specification for externally provided clock signal (MCX A185 VLH) こんにちは、 @wyss-11 VEC仕様とは、外部発振器入力が有効な低状態および高状態を認識するために必要な最小電圧レベルを指します。 VDD = 3.3 Vの場合、2.31 Vは有効なハイレベルとして検出される最小電圧です。
View full article
MC33774 无响应 MC33774 无响应 MC33665+MC33774 的当前 DEMO 例程实现了 665 初始化、774 初始化以及电压和温度采集功能。实验台的布置如图所示。1. JozefKozon_0-1781765038190.png 当 S32K314 主控单元使用 JLINK 连接到 SWD 调试端口进行调试和仿真时,33774 和 33665 都能正常响应,返回回复帧并获取正确的单元电压和 GPIO 端口数据。台式上电顺序为“采样从板上电 -> MC33665A 上电 -> MCU 主板上电”。通信初始化请求读取寄存器消息显示为 MC33774_FIRST(其中 CAN 类型消息为 MC33665 回复帧)。2. 当仿真器断开连接且整个平台断电一段时间后,按“采样从板上电 -> MC33665A 上电 -> MCU 主板上电”的顺序再次上电时,MC33774 没有响应,只有 MC33665A 可以返回响应帧。通过开关机重新初始化MCU主板没有效果;只有在使用J-Link进行调试时才能与MC33774正常通信。消息如 MC33774_SECOND 所示。我想知道在排查故障时可以采取哪些步骤。 当前MC33665+MC33774的DEMO例程实现665初始化、774初始化以及电压温度采集功能,台架构成如图: Embedded_novice_0-1781746636464.png 1.当S32K314主控部分使用JLINK链接SWD调试口进行调试仿真时,33774和33665均能正常响应返回应答帧并采集正确的适配器电压和GPIO端口数据。台架上电顺序为“采样从主板上电->MC33665A上电->MCU模块上电”。通讯初始化至请求读取读取报文如MC33774_FIRST所示(其中CAN报文类型为MC33665回复帧) 2.当断开仿真器并且将台架全部下电后等待一段时间,重新按照“采样从主板上电->MC33665A上电->MCU主板上电”顺序上电后,MC33774无响应,则MC33665A能返回响应帧。重新将MCU主板上下电进行初始化也无效,只有用JLINK调试时才正常与MC33774通讯。报文如MC33774_SECOND所示。 我想知道排查的方向有哪些? Re: MC33774 is unresponsive MC33774无响应 亲爱的嵌入式新手: MC33665 包含内部通信管理功能,不具备透明桥接功能。 当 MC33665 RESET 而 MC33774 仍保持通电状态时,TPL 链路将失去同步,导致设备处于 SPI 通信工作但 TPL 转发未启用的状态。 执行两次初始化可以有效地清除内部状态并重新建立链路同步,这就是它解决问题的原因。 建议的解决方案是确保正确重新初始化 TPL 或同步 RESET 两个设备。 最诚挚的问候, 约瑟夫 Re: MC33774 is unresponsive MC33774无响应 通过实验,我发现问题是由 MC33665 断电引起的。当我的 MC33774 保持通电状态,而 MC33665 断电重启,MCU 也断电重启时,尽管软件逻辑重新初始化了 MC33665,但它似乎处于无法转发 TPL 数据的状态。这是因为我的消息表明 MC33665 可以发送回复帧。因此,MC33665 一定处于某种状态,导致它无法转换 TPL 信号并将其发送到 33774。目前,我可以通过在软件逻辑中执行两次相同的 MC33665 初始化来避免这种现象。但是,我不清楚为什么 MC33665 会出现这种行为。你有什么想法吗? 我通过实验发现是由于MC33665下电导致的,当我的MC33774保持上电,MC33665下电重启,因为MCU也下电重启后,虽然软件逻辑上到MC33665重新初始化,但是此时MC33665似乎无法转发TPL数据的状态,我的报文中可以看出MC33665能够发出状态回复帧,所以MC33665应该有某种原因导致无法转换TPL信号不断出现33774。我当前在软件逻辑中进行两次相同的MC33665初始化就能够避免这种现象。但是我并并MC33665为什么会这样。请问您有什么办法吗? Re: MC33774 is unresponsive MC33774无响应 亲爱的嵌入式新手: 这个问题很可能是由启动时序依赖性引起的。当使用 J-Link 调试系统时,MCU 执行会被延迟,从而给 MC33774 足够的时间完成其内部初始化。在正常上电情况下,MCU 会立即启动并在 MC33774 准备就绪之前发送通信请求,导致没有响应。 建议在第一次通信之前引入延迟(例如 50-200 毫秒),实施重试机制,并确保 MC33665 在寻址 MC33774 之前正确初始化并唤醒 TPL 通信链。此外,还应验证 MC33774 的 RESET 和电源斜坡条件。 最诚挚的问候, 约瑟夫
View full article
imx93 lpddr4x の JSL4BAG16 設定が不安定です こんにちは、専門家の皆様: JSL4BAG16 の lpddr4x 設定に関して問題があります。設定後、「機能」テストはパスしますが、「最適化->CA 最適化の Vref」で失敗することがあります。常に失敗するわけではなく、時々失敗します。 「vTSA -> CA eye」のテストを実行すると、合格と表示されますが、同時に「エラーログ」も表示されます。 「Vref DQ config」と「Vref CA config」の調整方法について質問があります。JSL4BAG16のVref値は「EVKで使用されているミクロン値」と異なりますが、範囲0または範囲1を設定する必要がありますか? 私の知る限り、Vref DQは「アイダイアグラム」テストの結果に基づいて設定されますが、「読み取りダイアグラム」と「書き込みダイアグラム」のどちらを使用すればよいのでしょうか? JSL4BAGのデータシートと、「CA eye」テストログおよびmexファイルを添付しました。     よろしくお願いします。 Re: imx93 lpddr4x config for JSL4BAG16 unstable こんにちは、 LPDDR4Xは、 https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-93-Memory-Compatibility-Guide/ta-p/1725656の一部です。 Vref DQ チューニングには、JSL4BAG16 のレンジ 1 (デフォルト) を使用し、読み取りではなく書き込みアイ ダイアグラムを使用してください。   Micron/EVKの設定を再利用しないでください。必ずJSL4BAG16に合わせてVrefを再調整してください。 Re: imx93 lpddr4x config for JSL4BAG16 unstable こんにちは、オズワラグさん。 ご返信ありがとうございます。私は「i.MX config tool」でテストに合格し、「最適化」テスト結果でDQとCAの「Vref」を使用しました。 しかし、まだ2つの問題があります。 1.あるボードでは「CA Charts」が表示されず、「CA Eye」テストには誤差がありますが、合格と表示されます 2.lpddr4x_timing.cを更新した後すべての合格ボードで「i.MX config tool」によって生成されたものをシステムで「memtest」を実行すると、「Stuck Address」で失敗します。常にではありませんが、時々発生します。 よろしくお願いします。 Re: imx93 lpddr4x config for JSL4BAG16 unstable 私のFRDM-IMX93ボードにも同じチップが搭載されていますが、市販のイメージファイルでは正常に起動しません。どうすれば解決できますか? Re: imx93 lpddr4x config for JSL4BAG16 unstable いいえ、していません。弊社では、flex-installerが提供する市販のイメージファイルを使用して、市販のfrdm-imx93ボードを使用しています。 入門マニュアルには「i.Mx設定ツール」についての記載はありません。 手順はどうなりますか?マニュアルはありますか?また、使い始めるにあたって、どのような手順で部品を交換する必要がありますか? これはまた、すべてのFRDM-IMX93ボードに対して1つの標準イメージを使うことはできず、各ボードを確認するか、搭載DDRによって2〜3つのイメージバージョンを持つ必要があるということですか? ご注意ください。私たちは(共有の)お客様に対して既製の動作を期待しています。 Re: imx93 lpddr4x config for JSL4BAG16 unstable こんにちは、SynchronicITさん。 「i.MX config tool」を使用してDDRテストに合格しましたか?まずそれを通過させてから、lpddr4x_timging.c を使用する必要があります。「i.MX設定ツール」によって生成されました。 Re: imx93 lpddr4x config for JSL4BAG16 unstable こんにちは: NXP公式の「FRDM i.MX 93開発ボード」と公式リリースを使っているようですね。大丈夫でしょう。「DDRテスト」を行う必要はありません。私は「FRDMボード」を持っていません。NXPのボードの使い方に関するドキュメントを参照できるかもしれません。
View full article
A sentence in readme file Hi, Several example readme files for imx95lpd5evk19 board have this sentence: "Please note this application can't support running with Linux BSP!" Could you please explain why these Cortex M7 example apps cannot run simultaneously with Linux in Cortex A55? me@myhost:~/mcuxpresso/mcuxsdk/mcuxsdk/examples((HEAD detached at refs/heads/manifest-rev))> grep url .git/config url = https://github.com/nxp-mcuxpresso/mcuxsdk-examples me@myhost:~/mcuxpresso/mcuxsdk/mcuxsdk/examples((HEAD detached at refs/heads/manifest-rev))> git log --decorate |head -3 commit 55092a561762d34b1b0fa6dba52d1944b2710e65 (HEAD, test, manifest-rev) Author: Fikret Eren Date: Fri May 8 07:25:09 2026 +0200 me@myhost:~/mcuxpresso/mcuxsdk/mcuxsdk/examples((HEAD detached at refs/heads/manifest-rev))> find _boards/imx95lpd5evk19/*examples/*/ |grep -i readme |xargs grep "support running" _boards/imx95lpd5evk19/cmsis_driver_examples/lpi2c/int_b2b_transfer/slave/example_board_readme.md:**Please note this application can't support running with Linux BSP!** _boards/imx95lpd5evk19/cmsis_driver_examples/lpi2c/int_b2b_transfer/master/example_board_readme.md:**Please note this application can't support running with Linux BSP!** _boards/imx95lpd5evk19/cmsis_driver_examples/lpi2c/edma_b2b_transfer/slave/example_board_readme.md:**Please note this application can't support running with Linux BSP!** _boards/imx95lpd5evk19/cmsis_driver_examples/lpi2c/edma_b2b_transfer/master/example_board_readme.md:**Please note this application can't support running with Linux BSP!** _boards/imx95lpd5evk19/cmsis_driver_examples/lpuart/edma_transfer/example_board_readme.md:**Please note this application can't support running with Linux BSP!** _boards/imx95lpd5evk19/cmsis_driver_examples/lpuart/interrupt_transfer/example_board_readme.md:**Please note this application can't support running with Linux BSP!** _boards/imx95lpd5evk19/driver_examples/flexio/i2c/read_accel_value_transfer/board.readme:#### Please note this application can't support running with Linux BSP! #### _boards/imx95lpd5evk19/driver_examples/flexio/i2c/interrupt_lpi2c_transfer/example_board_readme.md:**Please note this application can't support running with Linux BSP!** ... Re: A sentence in readme file Hello @jukka1  Hope you are doing very well. The warning does not mean the Cortex-M7 cannot run simultaneously with Linux on the i.MX95. The i.MX95 supports heterogeneous operation with Linux on Cortex-A55 and firmware on Cortex-M7. However, these SDK examples were developed as standalone demonstrations and assume exclusive ownership of peripherals, clocks, pins, and DMA resources. When Linux is running, the same resources may already be assigned to Linux drivers, which can lead to conflicts. Therefore the examples are not validated for concurrent execution with the Linux BSP unless the system is properly configured in the System Manager. Best regards, Salas. Re: A sentence in readme file Hello Salas, Thanks, I am doing very well. I hope that you are too. OK, then do you have such M7 examples, which have the proper configuration for the System Manager, and are validated for concurrent execution with the Linux BSP? I am especially interested in examples for lpi2c/interrupt_b2b_transfer and lpspi/interrupt_b2b_transfer. BR, jukka
View full article
ガーデニング入門2:より早く成長するためのトップ10の秘訣 もしあなたが『Roblox Grow a Garden 2』で何百万シェケルも稼ぎ、急速に進めたいなら、その作業がどれほど厳しくなるかはすでにご存知でしょう。続編では、新しい円形の庭園区画、完全に刷新された突然変異システム、オフラインでの成長、そしてかなり激しい夜間の襲撃メカニズムなど、多くの点が変更された。 競争相手を圧倒的に凌駕するには、単一収穫作物、積み重ねられた装備ブースト、そしてサーバーの仕組みを最適な組み合わせで活用し、作物の収穫量を最大化する必要があります。ここでは、小さな初期区画を巨大で収益性の高い農業帝国へと変貌させるための、プレイヤーにとって役立つトップ10の秘訣を実践的に解説します。 1. 「壊れた」竹の戦略を悪用する 一度収穫できる作物は、このゲームで序盤に富を築く最も速い方法だが、竹は現状完全にバランスが崩れている。種子は約700シェケルかかりますが、よく強化された竹の子は簡単に5,500シェケル以上売れます――しかも希少な突然変異を考慮していないのです。自分のためにも、ありふれた作物をすべて取り除き、土地の隅々まで竹で埋め尽くしましょう。そうすれば利益が飛躍的に伸びます。 2. 異なるスプリンクラーを重ねて設置する 最高級のスプリンクラーだけを購入して、それ以外は捨ててしまうという間違いを犯さないでください。異なるバリエーションを組み合わせたい場合は、コモン、アンコモン、レア、レジェンダリーのスプリンクラーを全く同じ場所に設置すると、それらの成長倍率と幸運倍率が実際に合算されます。この便利なテクニックを使えば、作物を大幅に大きく育てることができ、極端なサイズ増加(例えば15kgを超えるような巨大な品種)をはるかに速く引き起こすことができます。 3. 鹿のペットで構成されたチームを編成する ペットは全体的な効率性を高める上で不可欠ですが、純粋な成長速度を求めるなら、鹿のペットが最高です。装備した鹿のペット1匹につき、植物の成長速度が10%向上します。ペットの卵にいくらかお金を費やして、鹿の群れで装備スロットを最大まで満たせば、農業作業の待ち時間を劇的に短縮できます。 4. 販売店の割引オプションを利用する 大量の在庫を処分する際は、決して何も考えずに「売却」ボタンをクリックしてはいけません。販売商人とのやり取りの際は、必ずゲーム内の「値引き交渉」オプションを使用してください。高級果物や高品質の竹をうまく交渉することで、収穫ごとの配当を大幅に増やし、同じ肉体労働に対して総収入を倍増させることができます。 5. 7人の友達とプレイして、大きなブーストを得よう Grow a Garden 2は、サーバー倍率を大幅に高めることで、協力プレイを非常に有利にしています。サーバーにいる友達一人一人につき、成長率と幸運度が段階的に上昇します。7人の友達でファーミングすると、総資産と成長率が70%という驚異的な倍率が得られ、公開やグループでの周回はソロ飛行よりもはるかに優れています。 6. ゴールデンフルーツとレインボーフルーツを植え続ける 運良くレジェンダリー+やミシカルの変異種(レインボーやミダスタッチなど)に遭遇した場合は、すぐに収穫しないでください。これらの極めて希少な品種は、庭にそのままの状態で残しておきましょう。それらを植えたままにしておくことで、他の高レベルプレイヤーと安全に取引して希少な種子パックを入手したり、ゲーム終盤での最大の利益率を得るために保存したりすることができます。 7. 夜の泥棒になる(または夜の泥棒から身を守る) このゲームにおける進歩は、必ずしも完全に平和的なものである必要はない。ゲーム内の時計が夜に切り替わると、他のプレイヤーの庭に直接飛び込み、高価値作物を盗むことができます。失うものが何もない初心者なら、裕福な庭園を襲撃するのは、数百万ドルを稼ぐ近道だ。逆に、もしあなたが標的にされたのなら、柵で囲まれた庭に閉じこもるか、シャベルで侵入者を叩き潰して盗まれた物を取り戻しましょう。 8. ギルド報酬を稼ぐ できるだけ早くギルドに参加するか、ゲーム内ギルドを結成しましょう。ギルドは、集団での作業によってポイントを獲得できる、特別なギルド報酬システムを導入しています。これらのポイントは、限定の変異シード、強力な装備のアップグレード、通常のショップでは入手できない週間報酬パックと直接交換できます。 9. オフライン成長メカニズムをマスターする あなたが完全にオフラインの状態でも、あなたの庭は文字通り成長し続けます。その日の作業を終える前に、ドラゴンフルーツやゴーストペッパーなど、成熟に時間がかかり価値の高い種を密植し、散水器を戦略的に配置することで、区画の利用効率を最大限に高めていることを確認してください。次回ログイン時には、膨大な支払い履歴が表示されます。 10. 有効なプロモーションコードを引き換える 無料のリソースは決して見逃してはならない。開発者は定期的に、無料の種、化粧品、卵アイテムなどがもらえるプロモーションコードを配布しています。RDCAwardやBEANORLEAVE10などの最新の有効なコードを確認し、ゲームメニューからすぐに引き換えて、無料で有利なスタートを切りましょう。
View full article
ラズベリーパイカメラ V1.0i.MX93 CSI-2インターフェースで動作しない チームの皆さん、こんにちは。 弊社ではNXP社のi.MX93ボードを使用しています。NXP MIPI CSI-2(2レーン)カメラは正常に動作しています。 また、CSI-2の2レーンインターフェースを使用するRaspberry PiカメラモジュールV1.0も接続してみました。対応するカメラドライバーはLinuxにインストールされていますが、カメラは動作せずアクセスできません。 根本原因を特定する手助けをしていただけますか?i.MX93でRaspberry Piカメラをサポートするために、追加のデバイスツリー設定、ドライバの変更、またはMIPI CSI-2互換性の要件はありますか? ログやデバッグ情報が必要な場合はお知らせください。 ありがとうございます。 Re: Raspberry Pi Camera V1.0 Not Working on i.MX93 CSI-2 Interface 確認すべき事項(実用的なデバッグチェックリスト) ステップ1:I2Cの基本通信を確認する i2cdetect -y dmesg | grep imx219 / ov5647 重要な質問: 検出されたがプローブが失敗 → クロック/リセットの問題 検出されません → ハードウェア/ピン/電源の問題 ステップ2:クロック出力を確認する 確認する: CLKピンは実際に波形を出力する 周波数補正済み(24/25 MHz) ステップ3:リセット/電源オフGPIOの検証 DTSに以下が含まれていることを確認してください。 reset-gpios = <...>; pwdn-gpios = <...>; テスト: 手動で切り替える(デバッグ出力またはGPIOシステムファイルシステム) ステップ4:動作中のNXPカメラDTSと比較する 使用: BSP製のOV5640またはAP1302 DTS 比較する: エンドポイント ポート レーン設定 ステップ5:メディアグラフを確認する media-ctl -p パイプラインが完了したことを確認します。 ステップ6:レーン構成を確認する 不一致の例: データレーン数 = <1 2>; 時計レーン = <0>; 設定が間違っています → ストリームが再生されません 推奨事項: オプションA(プロジェクトに推奨): NXP検証済みのカメラモジュールを使用 → 立ち上げに数週間かかるのを回避 オプションB(Raspberry Piカメラを使用する必要がある場合): 必要がある: フルポートセンサードライバーのチューニング: クロック周波数 リンク周波数 MIPIタイミング 慎重に位置合わせしてください: 電源シーケンス リセットタイミング DTS + パイプラインの調整 相当な努力が必要になることを覚悟してください。
View full article
寻求有关人工智能驱动的半导体供应链平台的行业洞察 您好,先生, 我是 Shaileshwar,目前是 NIT Warangal 电子与通信工程专业的大四本科生。 我的团队正在探索构建“半导体供应链 2.0”平台的想法——这是一个面向半导体公司的 AI 驱动的智能和协调系统。我们的愿景是提供整个生态系统的端到端可视性,将晶圆厂、OSAT(外包半导体组装测试)厂商、供应商、组装和测试合作伙伴以及物流供应商聚集在一个统一的平台上。 我们正在考虑的一些功能包括: • 人工智能驱动的全球风险情报(地缘政治事件、自然灾害、贸易限制、供应商中断) • 实时查看存货和生产状态 • 需求预测和产能规划 • 供应商风险评分和替代采购建议 • 瓶颈和延误的预测分析 • 半导体运营团队的决策支持仪表板 我们非常希望您能就以下问题提供一些见解:这些是否是行业中真正存在的痛点,以及哪些领域具有最高的创新价值。 感谢您抽出时间,期待您的指导。 问候, 沙伊莱什瓦尔 电子与通信工程学士学位 瓦朗加尔国立理工学院 机器学习
View full article
MC33774 is unresponsive MC33774无响应 The current DEMO routine for MC33665+MC33774 implements 665 initialization, 774 initialization, and voltage and temperature acquisition functions. The bench setup is shown in the figure. 1. JozefKozon_0-1781765038190.png When the S32K314 main control unit uses JLINK to connect to the SWD debug port for debugging and simulation, both 33774 and 33665 can respond normally, returning reply frames and acquiring the correct unit voltage and GPIO port data. The bench power-on sequence is "sampling slave board power-on -> MC33665A power-on -> MCU main board power-on". The communication initialization to request read register message is shown as MC33774_FIRST (where the CAN type message is the MC33665 reply frame). 2. When the emulator is disconnected and the entire bench is powered down, wait for a period of time, and then power on again in the sequence of "sampling slave board power-on -> MC33665A power-on -> MCU main board power-on", the MC33774 does not respond, and only the MC33665A can return a response frame. Re-initializing the MCU motherboard by powering it on and off didn't work; it only communicates normally with the MC33774 when debugging with J-Link. The message is as shown in MC33774_SECOND. I'd like to know what directions I can take for troubleshooting. 当前MC33665+MC33774的DEMO例程实现665初始化、774初始化以及电压温度采集功能,台架构成如图: Embedded_novice_0-1781746636464.png 1.当S32K314主控部分使用JLINK链接SWD调试口进行调试仿真时,33774和33665均能正常响应返回回复帧并且采集正确的单体电压和GPIO端口数据。台架上电顺序为“采样从板上电->MC33665A上电->MCU主板上电”。通讯初始化至请求读取寄存器报文如MC33774_FIRST所示(其中CAN 类型的报文为MC33665回复帧) 2.当断开仿真器并且将台架全部下电后等待一段时间,重新按照“采样从板上电->MC33665A上电->MCU主板上电”顺序上电后,MC33774无响应,仅有MC33665A能返回响应帧。重新将MCU主板上下电进行初始化也无效,只有用JLINK调试时又能正常与MC33774通讯。报文如MC33774_SECOND所示。 我想知道有什么排查的方向吗? Re: MC33774 is unresponsive MC33774无响应 Dear Embedded Novice, The MC33665 includes internal communication management and does not behave as a transparent bridge. When the MC33665 is reset while the MC33774 remains powered, the TPL link becomes unsynchronized, leaving the device in a state where SPI communication works but TPL forwarding is not enabled. Executing initialization twice effectively clears the internal state and re-establishes link synchronization, which is why it resolves the issue. The recommended solution is to ensure proper TPL re-initialization or synchronized reset of both devices. With Best Regards, Jozef Re: MC33774 is unresponsive MC33774无响应 Through experimentation, I discovered that the issue is caused by the MC33665 being powered off. When my MC33774 remains powered on, and the MC33665 powers off and restarts, and the MCU also powers off and restarts, although the software logic reinitializes the MC33665, it seems to be in a state where it cannot forward TPL data. This is because my messages show that the MC33665 can send reply frames. Therefore, the MC33665 must be in some state that prevents it from converting the TPL signal and sending it to the 33774. Currently, I can avoid this phenomenon by performing the same MC33665 initialization twice in the software logic. However, I am unclear why the MC33665 behaves this way. Do you have any ideas? 我通过实验发现是由于MC33665下电导致的,当我的MC33774保持上电,MC33665下电重启,MCU也下电重启后,虽然软件逻辑上会对MC33665重新初始化,但是此时MC33665似乎处于无法转发TPL数据的状态,因为我的报文中可以看出MC33665能够发出回复帧,所以MC33665应该处于某种状态导致无法转换TPL信号并发送给33774。我当前是在软件逻辑中进行两次相同的MC33665初始化就能够避免这种现象。但是我并不清楚MC33665为什么会这样。请问您有什么思路吗? Re: MC33774 is unresponsive MC33774无响应 Dear Embedded Novice, The issue is most likely caused by a startup timing dependency. When the system is debugged with J‑Link, the MCU execution is delayed, giving sufficient time for the MC33774 to complete its internal initialization. In a normal power-up scenario, the MCU starts immediately and sends communication requests before the MC33774 is ready, resulting in no response. It is recommended to introduce a delay (e.g., 50–200 ms) before the first communication, implement a retry mechanism, and ensure that the MC33665 correctly initializes and wakes up the TPL communication chain before addressing the MC33774. Additionally, the reset and power ramp conditions of the MC33774 should be verified. With Best Regards, Jozef
View full article
readmeファイル内の一文 こんにちは、 imx95lpd5evk19ボード用のいくつかのサンプルreadmeファイルには、次の文が含まれています。 「このアプリケーションはLinux BSPでの動作をサポートできませんのでご注意ください!」 なぜCortex M7の例アプリがCortex A55でLinuxと同時に動作できないのか説明していただけますか? me@myhost:~/mcuxpresso/mcuxsdk/mcuxsdk/examples((HEAD detached at refs/heads/manifest-rev))> grep url .git/config URL = https://github.com/nxp-mcuxpresso/mcuxsdk-examples me@myhost:~/mcuxpresso/mcuxsdk/mcuxsdk/examples((HEAD detached at refs/heads/manifest-rev))> git log --decorate |head -3 コミット 55092a561762d34b1b0fa6dba52d1944b2710e65 (HEAD、test、manifest-rev) 著者: フィクレット エレン 日付: 2026年5月8日(金) 07:25:09 +0200 me@myhost:~/mcuxpresso/mcuxsdk/mcuxsdk/examples((HEAD detached at refs/heads/manifest-rev))> find _boards/imx95lpd5evk19/*examples/*/ |grep -i readme |xargs grep "サポート running" _boards/imx95lpd5evk19/cmsis_driver_examples/lpi2c/int_b2b_transfer/slave/example_board_readme.md:**お願いしますこのアプリケーションはLinux BSPでの動作をサポートしません!** _boards/imx95lpd5evk19/cmsis_driver_examples/lpi2c/int_b2b_transfer/master/example_board_readme.md:**このアプリケーションはLinux BSPでの動作をサポートしません!** _boards/imx95lpd5evk19/cmsis_driver_examples/lpi2c/edma_b2b_transfer/slave/example_board_readme.md:**このアプリケーションはLinux BSPでの動作をサポートしません!** _boards/imx95lpd5evk19/cmsis_driver_examples/lpi2c/edma_b2b_transfer/master/example_board_readme.md:**このアプリケーションはLinux BSPでの動作をサポートしません!** _boards/imx95lpd5evk19/cmsis_driver_examples/lpuart/edma_transfer/example_board_readme.md:**このアプリケーションはLinux BSPでの動作をサポートしません!** _boards/imx95lpd5evk19/cmsis_driver_examples/lpuart/interrupt_transfer/example_board_readme.md:**このアプリケーションはLinux BSPでの動作をサポートしません!** _boards/IMX95lpd5evk19/driver_examples/flexio/i2c/read_accel_value_transfer/board.readme:#### Please note this application can't support running with Linux BSP! #### _boards/imx95lpd5evk19/driver_examples/flexio/i2c/interrupt_lpi2c_transfer/example_board_readme.md:**お願いしますこのアプリケーションはLinux BSPでの動作をサポートしません!** ... Re: A sentence in readme file こんにちは、@jukka1さん お元気でお過ごしのことと思います。 この警告は、Cortex-M7がi.MX95上でLinuxと同時に動作できないという意味ではありません。 i.MX95は、Cortex-A55上のLinuxとCortex-M7のファームウェアで異種動作をサポートします。 しかし、これらのSDK例は単独のデモンストレーションとして開発されており、ペリフェラル、クロック、ピン、DMAリソース の独占所有権を想定しています。 Linuxが動作している場合、同じリソースがすでにLinuxドライバに割り当てられている可能性があり、競合を引き起こすことがあります。したがって、システムマネージャで適切に設定されていない限り、Linux BSPとの同時実行が検証されません。 よろしくお願いいたします。 サラス。 Re: A sentence in readme file こんにちは、サラスさん。 ありがとうございます。おかげさまで元気です。あなたもそうであってほしいと願っています。 では、System マネージャに適した設定が正しく、Linux BSPと同時実行が検証されているM7の例はありますか? 特にlpi2c/interrupt_b2b_transferとlpspi/interrupt_b2b_transferの例に興味があります。 BR、 ユッカ
View full article
树莓派摄像头 V1.0i.MX93 CSI-2 接口无法正常工作 大家好, 我们使用的是NXP i.MX93板。NXP MIPI CSI-2(2 通道)摄像头工作正常。 我们还尝试连接了 Raspberry Pi Camera Module V1.0,它使用 CSI-2 2 通道接口。Linux 系统中已安装了相应的相机驱动程序,但相机无法工作,也无法访问。 请问您能否帮我们找出根本原因?要在 i.MX93 上支持 Raspberry Pi 摄像头,是否需要额外的设备树配置、驱动程序修改或 MIPI CSI-2 兼容性要求? 如有需要,请与我们联系是否需要任何日志或调试信息。 谢谢。 Re: Raspberry Pi Camera V1.0 Not Working on i.MX93 CSI-2 Interface 你应该检查哪些内容(实用调试清单) 步骤 1:验证 I2C 基本通信 i2cdetect -y dmesg | grep imx219 / ov5647 关键问题: 检测到问题但探测失败 → 时钟/RESET问题 未检测到 → 硬件/引脚/电源问题 步骤 2:检查时钟输出 确认: CLK引脚实际上输出波形 频率校正(24/25 MHz) 步骤 3:验证 RESET/掉电 GPIO 确保DTS包含以下内容: RESET GPIOS = <...>; pwdn-gpios = <...>; 测试: 手动切换(调试打印或 GPIO sysfs) 步骤 4:与 NXP 摄像机 DTS 进行比较 使用: 来自电路板支持包的 OV5640 或 AP1302 DTS 比较: 端点 端口 车道配置 步骤五:检查媒体图表 media-ctl -p 确认管道已完成。 步骤 6:确认车道配置 不匹配示例: 数据通道 = <1 2>; 时钟通道 = <0>; 配置错误 → 无流 推荐: 方案A(项目推荐方案): 使用NXP 认证的摄像头模块→ 可节省数周的启动时间 方案 B(如果必须使用树莓派摄像头): 你需要: 完全端口传感器驱动器调校: 时钟频率 链路频率 MIPI 时序 仔细对齐: 电源序列 复位时序 调整 DTS + 管道 预计需要付出相当大的努力。
View full article
Raspberry Pi Camera V1.0 Not Working on i.MX93 CSI-2 Interface Hi Team, We are using an NXP i.MX93 board. The NXP MIPI CSI-2 (2-lane) camera is working correctly. We also tried connecting a Raspberry Pi Camera Module V1.0, which uses a CSI-2 2-lane interface. The corresponding camera driver has been installed in Linux, but the camera is not working and cannot be accessed. Could you please help us identify the root cause? Is there any additional device tree configuration, driver modification, or MIPI CSI-2 compatibility requirement needed to support the Raspberry Pi camera on i.MX93? Please let us know if any logs or debug information are required. Thanks. Re: Raspberry Pi Camera V1.0 Not Working on i.MX93 CSI-2 Interface What you should check (practical debug checklist) Step 1: Verify I2C basic communication i2cdetect -y dmesg | grep imx219 / ov5647 Key question: detected but probe fails → clock/reset issue not detected → HW / pin / power issue Step 2: Check clock output Confirm: CLK pin actually outputs waveform frequency correct (24/25 MHz) Step 3: Validate reset / power-down GPIO Ensure DTS includes: reset-gpios = <...>; pwdn-gpios = <...>; Test: toggle manually (debug prints or GPIO sysfs) Step 4: Compare with working NXP camera DTS Use: OV5640 or AP1302 DTS from BSP Compare: endpoint port lane config Step 5: Check media graph media-ctl -p Verify pipeline is complete. Step 6: Confirm lane configuration Mismatch examples: data-lanes = <1 2>; clock-lane = <0>; Wrong config → no stream Recommendation: Option A (recommended for project): Use NXP-validated camera module → saves weeks of bring-up Option B (if must use RPi camera): You need to: Fully port sensor driver tuning: clock frequency link frequency MIPI timing Carefully align: power sequence reset timing Adjust DTS + pipeline Expect non-trivial effort
View full article