Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
SPSDK v3.13.0 now available We are excited to announce the release of Secure Provisioning SDK (SPSDK) 3.13.0 🆕 New device support MCXC353, MCXC352 MCXN526T MIMXRT1183, MIMXRT118D ✨ Key new features nxpdebugmbox: new tool execute command, Debug Authentication Response export, improved debug connection diagnostics, and probe discovery without a mandatory family filter. Debug probes: ARM ADIv6 (CoreSight 600 / DPv3) support with automatic ADI-version detection and MEM-AP/debug-mailbox discovery. nxpimage: DevHSM SRK-set support plus secondary-image tables and parallel AHAB verification for MIMXRT266x devices. nxpele: new forward-boot-crypto command, HSE core reset/status support, and second Cortex-M7 core support for MCXE327 and MCXE32B. nxpcrypto: new --fuse-script option for rot calculate-hash to generate device-specific RoT fuse scripts where supported. Migration checks: new SPSDK_DEPRECATED_STRICT environment variable to report deprecated register aliases and schema properties as errors. For more details: Release Notes Supported Devices Github PyPi Documentation SPSDK Plugins: Github (Plugins) PyPi (Plugins) Note: nxp-codecheck was moved to separated repository bellow: SPSDK Codecheck: GitHub: https://github.com/nxp-mcuxpresso/nxp-codecheck PyPi: https://pypi.org/project/nxp-codecheck/ announcement
View full article
ICEを使用したPROFINET上の周期的および非周期的通信 こんにちは、 私はFRDM i.MX RT1186ボード用のPROFINET入出力デバイスを開発しています。ICCツールでアプリケーションを作成し、ICEツールを使って動作を確認しました。 これまでにサイクリック通信をテストしましたが、wiresharkでコントローラが定期的にパケットを送受信していることがわかります。非巡回通信をテストすることは可能でしょうか?例えば、コントローラからIOデバイスを設定するための通信です。 goal_appl.c のappl_pnioCbWriteRecord 関数とappl_pnioCbReadRecord 関数は、私がやりたいことに関連しているようですが、ICE を介して非巡回通信をどのように実装すればよいのかわかりません。   よろしくお願いします!
View full article
Cyclic and acyclic communications on PROFINET with ICE Hi,  I'm working on a PROFINET I/O device for the FRDM i.MX RT1186 board. I have managed to create the application with the ICC tool and have used the ICE tool to verify that the application works. So far I have tested cyclic communications, and I can see on wireshark that the controller sends/receives packets periodically. I was wondering if it's possible to test acyclic communications. For example, communications intended to configure the IO device from the controller.   The functions appl_pnioCbWriteRecord, and appl_pnioCbReadRecord in goal_appl.c seem relevant for what I want to do, but I'm not sure how to implement the acyclic communications through ICE.   Thanks!
View full article
在PROFINET上使用ICE进行循环和非循环通信 你好, 我正在为 FRDM i.MX RT1186 板开发 PROFINET I/O 设备。我已经使用 ICC 工具创建了应用程序,并使用 ICE 工具验证了该应用程序是否有效。 到目前为止,我已经测试了循环通信,并且我可以在 Wireshark 中看到控制器周期性地发送/接收数据包。我想知道是否可以测试非循环通信。例如,用于从控制器配置 I/O 设备的通信。 goal_appl.c 中的appl_pnioCbWriteRecord 和 appl_pnioCbReadRecord 函数似乎与我想要做的事情相关,但我不知道如何通过 ICE 实现无循环通信。   谢谢您!
View full article
LPC43S57 USB1 Host Configuration issue Hi     We are trying to use USB1 peripheral of LPC43S57 controller as USB host to connect a device in customer board. We are using KEIL MDK to configure the USB stack and USB driver.   When we call USBH_Initialize(1) function it returns an error indicating "Controller does not exist". We tried to search on the internet regarding the USB1 Hardware connections, and we observed that in many places it is mentioned that USB1 peripheral will not work without external PHY. However, the datasheet indicates that it supports on chip full speed PHY.    Can you clarify for us if the USB1 does have on chip full speed PHY?   The USB1_VBUS pin is not used since it is a Host and the device we are connecting is a self powered device.   Also please find below the snapshot of the USB1 connection we have done as Host   Regards Sabarish Kumar Re: LPC43S57 USB1 Host Configuration issue Okay, let's unpack this USB conundrum! Is it the internal PHY or some hardware quirk messing things up? That controller error is always a headache. Finding the right USB configuration can feel like navigating a maze. Once, I was wrestling with a stubborn Arduino setup, trying to get it to communicate with a sensor for a project. Spent hours tracing wires and debugging code only to realize a simple power supply issue was the root cause, completely sidelining my @geometry dash -filled afternoon. Sometimes, the obvious escapes us, right? Re: LPC43S57 USB1 Host Configuration issue That's a tricky issue with the USBH_Initialize function! I remember facing similar hardware connection problems before. Sometimes, even seemingly minor details in the setup can cause headaches. While I can't offer specific hardware debugging advice here, have you considered checking out the Geometry Dash forums? The community there is surprisingly knowledgeable about all sorts of technical challenges, and someone might have encountered a similar problem with USB device initialization. Re: LPC43S57 USB1 Host Configuration issue It sounds like you're facing a tricky hardware configuration issue! I've definitely been there with USB setups. Regarding the on-chip PHY, double-checking the specific silicon revision and errata sheet for your chip might provide clarity. While you're troubleshooting, testing your reaction time and mouse skills on a CPS test website could be a fun distraction. It helps sharpen focus! Hope you resolve your USB issue soon! Re: LPC43S57 USB1 Host Configuration issue Hi @Unblocked Games Thanks for sharing the schematic snapshot. Besides the PHY question, it would be helpful to know whether USB0 works correctly on the same board, as that could help isolate whether the issue is hardware- or software-related. Re: LPC43S57 USB1 Host Configuration issue It's interesting that you're running into issues with the USB1 peripheral on the LPC43S57, especially since the datasheet suggests it has an on-chip full-speed PHY. That "Controller does not exist" error is definitely frustrating. I'd be curious to know if anyone else has successfully used USB1 as a host on this chip, maybe for something like pokerogue . Good luck figuring this out! Re: LPC43S57 USB1 Host Configuration issue That “Controller does not exist” message sounds frustrating. I’d probably start by checking the USB1 clock configuration, pin assignments, and whether the USB1 host initialization matches the selected full-speed configuration. The distinction between the on-chip full-speed PHY and the external PHY requirement is especially important here. It’s always useful to test each part of the setup separately before changing several settings at once. After spending too much time troubleshooting hardware, I usually take a short break with a quick game such as Geometry Dash Game before coming back to the problem with a fresh mind. Re: LPC43S57 USB1 Host Configuration issue This sounds like a tricky hardware/software interaction! I've definitely been there, pulling my hair out over documentation that seems to contradict real-world behavior. It's especially frustrating when you're dealing with low-level peripheral details like on-chip PHYs. When I hit these kinds of roadblocks, I find it incredibly helpful to bounce ideas off other developers who might have faced similar issues. You might find some good insights on the Bad Parenting platform – sometimes a fresh pair of eyes or a different perspective is all it takes to spot the solution.
View full article
将外部 32K 振荡器定义为 FLL 源时存在问题 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我配置32K作为时钟源时遇到问题……配置代码附在后面。 MCG_C2 = 0; //new MCG_C2 = MCG_C2_HGO_MASK | MCG_C2_EREFS_MASK; //new MCG_C1 = 0; //new /* Wait for crystal to initialize */ while (!(MCG_S & MCG_S_OSCINIT_MASK)) {}; /* Wait for Reference Clock Status bit to clear */ while (MCG_S & MCG_S_IREFST_MASK) {}; /* Wait for clock status bits to show clock source * is external reference clock */ //while (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) != 0x2) {}; //new while (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) != 0x0) {}; //new FEE MCG_C4 |= MCG_C4_DMX32_MASK | MCG_C4_DRST_DRS(3); /* Now in FBE * Configure PLL Reference Divider, PLLCLKEN = 0, PLLSTEN = 0, PRDIV = 0x18 * The crystal frequency is used to select the PRDIV value. * Only even frequency crystals are supported * that will produce a 2MHz reference clock to the PLL. */ //MCG_C5 = MCG_C5_PRDIV(BSP_REF_CLOCK_DIV - 1); /* Ensure MCG_C6 is at the reset default of 0. LOLIE disabled, * PLL disabled, clock monitor disabled, PLL VCO divider is clear */ MCG_C6 = 0; /* Calculate mask for System Clock Divider Register 1 SIM_CLKDIV1 */ SIM_CLKDIV1_COPY = SIM_CLKDIV1_OUTDIV1(BSP_CORE_DIV - 1) | SIM_CLKDIV1_OUTDIV2(BSP_BUS_DIV - 1) | SIM_CLKDIV1_OUTDIV3(BSP_FLEXBUS_DIV - 1) | SIM_CLKDIV1_OUTDIV4(BSP_FLASH_DIV - 1); Re: Problem with defining external 32K oscillator as FLL source 感到孤独吗?打破沉默,瞬间与世界连接!试试Omegle 聊天,结识来自世界各地的新朋友,随时随地开启即兴对话。 Re: Problem with defining external 32K oscillator as FLL source 感到孤独吗?打破沉默,瞬间与世界连接!试试 Omegle 聊天,结识来自世界各地的新朋友,随时随地开启即兴对话。https://omeglechat.love/ Re: Problem with defining external 32K oscillator as FLL source <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 在 SIM 模块中有一个寄存器;SIM_SOPT2,其中包含字段;MCGCLKSEL,允许您将 RTS 振荡器(EXTAL32 和 XTAL32 输入)映射到 FLL。您已将此字段设置为 1。 从那里,您可以使用 FEE 模式来产生更高的 FLL 时钟频率。 Re: Problem with defining external 32K oscillator as FLL source <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 那就是罪魁祸首。我可以将实时时钟 (RTC) 配置为系统时钟吗? Re: Problem with defining external 32K oscillator as FLL source <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 1. 您的外部 32K 振荡器是连接到 EXTAL 还是 EXTAL32 / XTAL32(RTC 振荡器)?
View full article
S32K328 HyperRAM read write errors at low temperatures Hello NXP Community, we are using an NXP S32K328 with an Infineon S27KL0642DPBHB023 64-Mbit HyperRAM connected through the QuadSPI interface. The interface operates with the following basic configuration:   HyperRAM voltage = 3.3 V   QuadSPI clock = 120 MHz   Interface mode = Octal DDR   Clock mode = Single-ended CK   Read-data strobe = External RWDS   Latency mode = Fixed latency   Normal memory access = Memory-mapped AHB At room temperature, the HyperRAM interface appears to work correctly. At low temperatures, down to −40 °C, we observe read/write comparison errors. The problem appears to be related mainly to the temperature of the S32K328. Cooling the S32K328 can reproduce the errors, while cooling the HyperRAM alone has a much smaller effect. The relevant S32K328 QuadSPI settings are: DDR_EN = 1   DQS_EN = 1   External DQS/RWDS = selected   DQS_OUT_EN = 1   VAR_LAT_EN = 0   FLSHCR.TCSS = 4   FLSHCR.TCSH = 7   FLSHCR.TDH = 1 The current DLL configuration is:   SLV_DLL_BYPASS = 0   SLAVE_AUTO_UPDT = 1   SLV_EN = 1   SLV_DLY_COARSE = 0   FREQEN = 1   DLL_CDL8 = 0   DLLRES = 8   DLL_REFCNTR = 2   SMPR.FSPHS = 0   SMPR.FSDLY = 0   SMPR.DLLFSMPFA = 0 We tested all available combinations of:   SLV_DLY_OFFSET = 0 to 7   SLV_FINE_OFFSET = 0 to 15 At low temperatures, failures occur across all tested DLL configurations. The sweep shows differences between the configurations, but it does not provide a completely error-free operating range or a clearly optimal DLL parameter set. Therefore, we are currently not sure whether the problem is caused by the DLL configuration itself or by another temperature-dependent part of the S32K328 QuadSPI interface. Could you please help us with the following questions? Is the S32K328 QuadSPI configuration shown above suitable for HyperRAM operation at 120 MHz? Are the selected DLL parameters correct for this frequency and the full temperature range? Which values should be used for FREQEN, DLL_CDL8, DLLRES and DLL_REFCNTR at 120 MHz? Which DLL status flags should be monitored to verify correct operation? Should both DLLA_LOCK and SLVA_LOCK be checked before accessing the HyperRAM? How should DLLA_RANGE_ERR or FINE_UNDERFLOW be handled? Could the QuadSPI DLL or external-DQS path operate outside its valid range at low temperatures? Does the DLL configuration affect only read-data sampling, or can it also affect write timing? Are FLSHCR.TCSS = 4, FLSHCR.TCSH = 7 and FLSHCR.TDH = 1 suitable for 120 MHz HyperRAM operation? Which pad settings are recommended for CK, CS#, DQ[7:0] and RWDS at 120 MHz Octal DDR? Are there any known S32K328 errata or RTD issues related to QuadSPI, external DQS or operation at low temperatures? Is there a validated S32K328 HyperRAM initialization example or register configuration for 120 MHz operation? Any guidance on additional S32K328 registers or status information that should be checked would be very helpful. Thank you. Re: S32K328 HyperRAM read write errors at low temperatures 1) The operating mode is supported, but the current configuration does not fully match the required 120 MHz DDR external-DQS settings in Table 66. FREQEN should be 0, SMPR.DLLFSMPFA should be 4, FLSHCR.TCSS should be 2, FLSHCR.TCSH should be 5, and both delay offsets should initially be 0. The remaining listed settings match Table 66. The configuration should be corrected before further low-temperature testing. 2) The operating mode is supported, but the current configuration does not fully match the required 120 MHz DDR external-DQS settings in Table 66. FREQEN should be 0, SMPR.DLLFSMPFA should be 4, FLSHCR.TCSS should be 2, FLSHCR.TCSH should be 5, and both delay offsets should initially be 0. The remaining listed settings match Table 66. The configuration should be corrected before further low-temperature testing. 3) According to Table 66: FREQEN = 0 DLL_CDL8 = 0 DLLRES = 8 DLL_REFCNTR = 2 The DLL programming sequence described in the “DLL and delay chain usage” chapter must also be followed. 4) Monitor these DLLSR flags: DLLA_LOCK = 1: DLL reference chain is locked. SLVA_LOCK = 1: Slave delay chain is locked. DLLA_RANGE_ERR = 0: DLL master delay chain is within its valid range. DLLA_FINE_UNDERFLOW = 0: No fine-delay-chain underflow occurred. 5) Yes. When the DLL and slave delay line are enabled, both DLLA_LOCK and SLVA_LOCK should indicate lock before starting HyperRAM accesses. 6) These flags indicate that the configured delay cannot be generated correctly. HyperRAM operation should not be considered reliable while either error is present. Recheck the Table 66 configuration and the required DLL initialization sequence. If the error remains, reduce the QuadSPI frequency for further testing. 7) Please retest with the documented settings first. 😎 The external DQS and slave-DLL settings primarily control read-data sampling. Write timing is mainly determined by CK, CS#, data-output timing, pad configuration and the FLSHCR timing fields. Separate read-only and write/read-back tests can help identify which path is failing. 9) They do not match Table 66. For the characterized 120 MHz DDR configuration, use: FLSHCR.TCSS = 2 FLSHCR.TCSH = 5 FLSHCR.TDH = 1 10) The data-sheet characteristics use DSE = 1 and SRE = 0. They assume a maximum output load of 25 pF, an input transition time of 1 ns and QuadSPI traces no longer than 2 inches. These conditions and the actual CK/RWDS signal quality should be verified on the board. 11) I have not identified a published S32K328 erratum specifically describing external-DQS failures at low temperature. The applicable errata and the release notes for the exact RTD version should nevertheless be checked. 12) No validated HyperRAM initialization example is currently available. Please use the configuration specified in Table 66 of the S32K3xx Data Sheet as the reference for the QuadSPI settings. Re: S32K328 HyperRAM read write errors at low temperatures Hello NXP Community, we are continuing our investigation of temperature-dependent HyperRAM errors on an S32K328 connected to an Infineon S27KL0642DPBHB023, 8 MiB, 3.3 V. The interface operates at 120 MHz in Octal DDR mode using external edge-aligned RWDS/DQS. Normal memory access uses the QuadSPI AHB memory-mapped window:     0x68000000 to 0x687FFFFF Current relevant configuration ------------------------------     QuadSPI SCK             = 120 MHz     DDR_EN                  = 1     DQS_EN                  = 1     DQS_FA_SEL              = 3     DQS_OUT_EN              = 1     FLSHCR.TCSS             = 2     FLSHCR.TCSH             = 5     FLSHCR.TDH              = 1     SMPR.DLLFSMPFA          = 4     SMPR.FSDLY              = 0     SMPR.FSPHS              = 0     DLL FREQEN              = 0     DLL_CDL8                = 0     DLL_REFCNTR             = 2     DLLRES                  = 8     SLV_DLY_OFFSET          = 0     SLV_FINE_OFFSET         = 8     SLAVE_AUTO_UPDT         = 1     SLV_EN                  = 1     SLV_DLL_BYPASS          = 0 The fine offset of 8 was selected empirically from temperature tests. It is not taken from the zero-offset reference configuration in Data Sheet Rev. 14.  Our current initialization contains this sequence:     Configure QuadSPI and LUT     Configure DLL using auto-update     Perform one dummy AHB read     Perform QuadSPI software reset     Configure DLL again     Read HyperRAM registers using IP commands     Start normal AHB accesses The dummy read currently performs a volatile 32-bit read first and invalidates the corresponding Cortex-M7 cache line afterwards. Difference from Data Sheet Rev. 14 ---------------------------------- In S32K3xx Data Sheet Rev. 14, Table 66 appears to specify the following for the S32K328 120 MHz DDR, External DQS, Edge Aligned configuration:     FLSHCR.TCSS             = 3     FLSHCR.TCSH             = 3     FREQEN                  = 0     DLL_REFCNTR             = 2     DLLRES                  = 8     SLV_DLY_OFFSET          = 0     SLV_FINE_OFFSET         = 0     SLAVE_AUTO_UPDT         = 0     SLV_UPD                 = 1, according to the RM programming sequence     DLLFSMPFA               = 4     FSDLY                   = 0 This differs from our current TCSS/TCSH = 2/5, fine offset 8 and auto-update mode. Failure signature ----------------- Temperature testing still shows occasional memory-test failures even with settings near the center of the measured sampling window. The reported failures have a repeatable signature: - A complete 32-byte block is affected. - When reading address A, the returned block appears to match the expected pattern for address A + 0xFFE0. - The same signature was reported with several DLL offset/fine settings. The initialization-time DLL status indicated:     DLLA_LOCK              = 1     SLVA_LOCK              = 1     DLLA_RANGE_ERR         = 0     FINE_UNDERFLOW         = 0 We have not yet confirmed that these status values remain unchanged at the exact instant of every memory failure. The 0xFFE0 displacement is notable because it equals 0x10000 - 0x20, but we do not assume that this proves a 64-KiB wrap or AHB addressing issue. Questions --------- 1. For the S32K328 at 120 MHz DDR with external edge-aligned DQS, should we use the complete configuration from Data Sheet Rev. 14 Table 66, including:        TCSS/TCSH             = 3/3        SLAVE_AUTO_UPDT       = 0        SLV_DLY_OFFSET        = 0        SLV_FINE_OFFSET       = 0 2. Could you confirm the correct FLSHCR.TDH value for this exact Table 66 column? 3. If SLAVE_AUTO_UPDT = 0 is required, what is the exact sequence for:        SLV_EN        SLV_UPD        DLLEN        DLLA_LOCK        SLVA_LOCK        SLV_UPD clear 4. Is the following initialization sequence valid?        DLL configuration        dummy AHB read        QuadSPI software reset        second DLL configuration        first IP access        first AHB memory-mapped access    Or should software reset occur before the only DLL initialization? 5. After clearing SLV_UPD, which DLL lock indications remain valid and should be checked before the first HyperRAM access? 6. Which QuadSPI AHB buffers, FIFOs and sequence pointers must be cleared after software reset, DLL reconfiguration or IP-command access? 7. For the dummy AHB read, should the CPU cache line be invalidated and a DSB executed before the volatile read? 8. Is there any known S32K328 QuadSPI behavior that could return a complete 32-byte block associated with another address, particularly with an apparent displacement of 0xFFE0? 9. Which measurements or register traces would NXP recommend to distinguish between:        read-address generation error        write-address error        stale AHB buffer data        CPU cache coherency        HyperBus address wrapping        external-DQS sampling error We can provide the complete LUT contents, initialization source and register dumps as attachments. Thank you.
View full article
S32K328 HyperRAM 在低温下出现读写错误 NXP社区的各位朋友,大家好! 我们使用NXP S32K328 ,并通过 QuadSPI 接口连接Infineon S27KL0642DPBHB023 64-Mbit HyperRAM 。 该接口采用以下基本配置运行:   HyperRAM 电压 = 3.3 V   QuadSPI 时钟频率 = 120 MHz   接口模式 = 八进制 DDR   时钟模式 = 单端 CK   读取数据选通 = 外部 RWDS   延迟模式 = 固定延迟   普通内存访问 = 内存映射 AHB 在室温下,HyperRAM 接口似乎工作正常。 在低至-40 °C 的温度下,我们观察到读/写比较错误。问题似乎主要与 S32K328 的温度有关。冷却 S32K328 可以重现这些错误,而单独冷却 HyperRAM 的效果则小得多。 S32K328 QuadSPI 的相关设置如下: DDR_EN = 1   DQS_EN = 1   外部 DQS/RWDS = 已选择   DQS_OUT_EN = 1   VAR_LAT_EN = 0   FLSHCR.TCSS = 4   FLSHCR.TCSH = 7   FLSHCR.TDH = 1 当前 DLL 配置为:   SLV_DLL_BYPASS = 0   SLAVE_AUTO_UPDT = 1   SLV_EN = 1   SLV_DLY_COARSE = 0   频率 = 1   DLL_CDL8 = 0   DLLRES = 8   DLL_REFCNTR = 2   SMPR.FSPHS = 0   SMPR.FSDLY = 0   SMPR.DLLFSMPFA = 0 我们测试了所有可能的组合:   SLV_DLY_OFFSET = 0 到 7   SLV_FINE_OFFSET = 0 到 15 在低温下,所有测试的 DLL 配置都会出现故障。扫描结果显示了不同配置之间的差异,但并未提供完全无错误的运行范围或明显最优的 DLL 参数集。 因此,我们目前还不确定该问题是由 DLL 配置本身引起的,还是由 S32K328 QuadSPI 接口中其他与温度相关的部分引起的。 请问您能否协助我们解答以下问题? 上述 S32K328 QuadSPI 配置是否适合 120 MHz 的 HyperRAM 运行? 所选的 DLL 参数是否适用于此频率和整个温度范围? 在 120 MHz 时,FREQEN、DLL_CDL8、DLLRES 和 DLL_REFCNTR 应该使用哪些值? 应该监测哪些 DLL 状态标志来验证其运行是否正确? 访问 HyperRAM 之前是否应该同时检查 DLLA_LOCK 和 SLVA_LOCK? 应该如何处理 DLLA_RANGE_ERR 或 FINE_UNDERFLOW 错误? QuadSPI DLL 或外部 DQS 路径在低温下是否会在其有效范围之外运行? DLL 配置是否仅影响读取数据采样,还是也会影响写入时序? FLSHCR.TCSS = 4、FLSHCR.TCSH = 7 和 FLSHCR.TDH = 1 是否适用于 120 MHz HyperRAM 运行? 对于 120 MHz 八进制 DDR,CK、CS#、DQ[7:0] 和 RWDS 的推荐焊盘设置是什么? 是否存在与 QuadSPI、外部 DQS 或低温运行相关的已知 S32K328 勘误或 RTD 问题? 是否有经过验证的适用于 120 MHz 运行的 S32K328 HyperRAM 初始化示例或寄存器配置? 任何关于需要检查的其他 S32K328 寄存器或状态信息的指导都将非常有帮助。 谢谢! Re: S32K328 HyperRAM read write errors at low temperatures 1) 支持该操作模式,但当前配置与表 66 中要求的 120 MHz DDR 外部 DQS 设置不完全匹配。FREQEN 应为 0,SMPR.DLLFSMPFA 应为 4,FLSHCR.TCSS 应为 2,FLSHCR.TCSH 应为 5,两个延迟偏移量最初应为 0。其余列出的设置与表 66 相符。在进行进一步的低温测试之前,应先修正配置。 2) 支持该操作模式,但当前配置与表 66 中要求的 120 MHz DDR 外部 DQS 设置不完全匹配。FREQEN 应为 0,SMPR.DLLFSMPFA 应为 4,FLSHCR.TCSS 应为 2,FLSHCR.TCSH 应为 5,两个延迟偏移量最初应为 0。其余列出的设置与表 66 相符。在进行进一步的低温测试之前,应先修正配置。 3)根据表66: 频率 = 0 DLL_CDL8 = 0 DLLRES = 8 DLL_REFCNTR = 2 还必须遵循“DLL 和延迟链使用”章节中描述的 DLL 编程顺序。 4) 监测以下 DLLSR 标志: DLLA_LOCK = 1:DLL 引用链已锁定。SLVA_LOCK = 1:从设备延迟链已锁定。DLLA_RANGE_ERR = 0: DLL 主延迟链在其有效范围内。DLLA_FINE_UNDERFLOW = 0:未发生精细延迟链下溢。 5)是的。当 DLL 和从属延迟线启用时,DLLA_LOCK 和 SLVA_LOCK 都应在开始 HyperRAM 访问之前指示锁定。 6) 这些标志表明无法正确生成配置的延迟。当出现上述任一错误时,HyperRAM 的运行都不能被视为可靠。重新检查表 66 配置和所需的 DLL 初始化顺序。如果错误仍然存在,请降低 QuadSPI 频率进行进一步测试。 7)请先按照文档中记录的设置重新测试。 😎 外部 DQS 和从属 DLL 设置主要控制读取数据采样。写入时序主要由 CK、CS#、数据输出时序、焊盘配置和 FLSHCR 时序字段决定。分别进行只读测试和写/读回测试可以帮助确定哪条路径出现故障。 9)它们与表 66 不符。对于典型的 120 MHz DDR 配置,请使用: FLSHCR.TCSS = 2 FLSHCR.TCSH = 5 FLSHCR.TDH = 1 10) 数据表特性采用 DSE = 1 和 SRE = 0。他们假设最大输出负载为 25 pF,输入转换时间为 1 ns,QuadSPI 走线长度不超过 2 英寸。这些条件和实际的CK/RWDS信号质量需要在板上进行验证。 11) 我尚未找到已发布的 S32K328 勘误表,专门描述低温下的外部 DQS 故障。不过,仍应查看适用的勘误表和确切 RTD 版本的发行说明。 12) 目前没有经过验证的 HyperRAM 初始化示例。请以 S32K3xx 数据手册表 66 中指定的配置作为 QuadSPI 设置的参考。 Re: S32K328 HyperRAM read write errors at low temperatures NXP社区的各位朋友,大家好! 我们正在继续研究连接到英飞凌 S27KL0642DPBHB023、8 MiB、3.3 V 的 S32K328 上与温度相关的 HyperRAM 错误。 该接口在八进制 DDR 模式下以 120 MHz 的频率运行,采用外部边缘对齐的 RWDS/DQS。正常的内存访问使用 QuadSPI AHB 内存映射窗口:     0x68000000 至 0x687FFFFF 当前相关配置 ------------------------------     QuadSPI SCK = 120 MHz     DDR_EN = 1     DQS_EN = 1     DQS_FA_SEL = 3     DQS_OUT_EN = 1 FLSHCR.TCSS = 2 FLSHCR.TCSH = 5     FLSHCR.TDH = 1     SMPR.DLLFSMPFA = 4 SMPR.FSDLY = 0     SMPR.FSPHS = 0     DLL 频率 = 0     DLL_CDL8 = 0     DLL_REFCNTR = 2 DLLRES = 8 SLV_DLY_OFFSET = 0 SLV_FINE_OFFSET = 8     SLAVE_AUTO_UPDT = 1     SLV_EN = 1 SLV_DLL_BYPASS = 0 精细偏移量 8 是通过温度测试经验性地选定的。它并非取自数据手册第14版中的零偏移参考配置。 我们当前的初始化包含以下序列: 配置 QuadSPI 和 LUT 使用自动更新配置 DLL 执行一次虚拟 AHB 读取 执行 QuadSPI 软件 RESET 再次配置 DLL 使用 IP 命令读取 HyperRAM 寄存器 开始正常AHB访问 目前,虚拟读取操作首先执行易失性 32 位读取,然后使相应的 Cortex-M7 缓存行失效。 与数据手册第 14 版的差异 ---------------------------------- 在 S32K3xx 数据手册 Rev. 14 中,表 66 似乎对 S32K328 120 MHz DDR、外部 DQS、边缘对齐配置规定了以下内容: FLSHCR.TCSS = 3 FLSHCR.TCSH = 3     频率 = 0     DLL_REFCNTR = 2 DLLRES = 8 SLV_DLY_OFFSET = 0 SLV_FINE_OFFSET = 0     SLAVE_AUTO_UPDT = 0 根据 RM 编程序列,SLV_UPD = 1 DLLFSMPFA = 4 FSDLY = 0 这与我们目前的 TCSS/TCSH = 2/5、精细偏移 8 和自动更新模式不同。 故障特征 ----------------- 即使将设置调整到接近测量采样窗口中心的位置,温度测试仍然偶尔会出现内存测试失败的情况。 所报告的故障具有可重复的特征: 一个完整的 32 字节块受到影响。 -读取地址 A 时,返回的块似乎与地址 A + 0xFFE0 的预期模式相匹配。 -报告称,在多个 DLL 偏移/精细设置下,都出现了相同的签名。 初始化时 DLL 状态指示如下: DLLA_LOCK = 1     SLVA_LOCK = 1 DLLA_RANGE_ERR = 0     FINE_UNDERFLOW         = 0 我们尚未确认这些状态值在每次内存故障发生的瞬间是否保持不变。 0xFFE0 位移值得注意,因为它等于 0x10000 - 0x20,但我们并不认为这证明了 64-KiB 的循环或 AHB 地址问题。 问题 --------- 1.对于采用外部边沿对齐 DQS 的 120 MHz DDR 内存的 S32K328,我们是否应该使用数据手册 Rev. 14 表 66 中的完整配置,包括: TCSS/TCSH = 3/3        SLAVE_AUTO_UPDT = 0 SLV_DLY_OFFSET = 0 SLV_FINE_OFFSET = 0 2.您能否确认一下表 66 列中 FLSHCR.TDH 的正确值? 3.如果需要将 SLAVE_AUTO_UPDT 设置为 0,那么具体的操作顺序是什么? SLV_EN        SLV_UPD        DLLEN DLLA_LOCK SLVA_LOCK        SLV_UPD 清除 4.以下初始化序列是否有效? DLL 配置 虚拟 AHB 读取 QuadSPI 软件RESET 第二个 DLL 配置 首次 IP 访问 首次 AHB 内存映射访问 或者,软件 RESET 应该在唯一的 DLL 初始化之前进行吗? 5.清除 SLV_UPD 后,哪些 DLL 锁定指示仍然有效,在首次访问 HyperRAM 之前应该检查哪些? 6.软件 RESET、DLL 重新配置或 IP 命令访问后,必须清除哪些 QuadSPI AHB 缓冲区、FIFO 和序列指针? 7.对于虚拟 AHB 读取,是否应该在易失性读取之前使 CPU 缓存行失效并执行 DSB? 8.是否有已知的 S32K328 QuadSPI 行为可以返回与另一个地址关联的完整 32 字节块,特别是当位移明显为 0xFFE0 时? 9. NXP建议使用哪些测量值或寄存器轨迹来区分: 读取地址生成错误 写入地址错误        过时的 AHB 缓冲区数据 CPU缓存一致性 HyperBus地址包装 外部DQS采样误差 我们可以提供完整的 LUT 内容、初始化源代码和寄存器转储作为附件。 谢谢!
View full article
外部32K発振器をFLLソースとして定義する際の問題 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 32Kをクロックソースとして設定する際に問題が発生しています。設定コードを添付します。 MCG_C2 = 0; //new MCG_C2 = MCG_C2_HGO_MASK | MCG_C2_EREFS_MASK; //new MCG_C1 = 0; //new /* Wait for crystal to initialize */ while (!(MCG_S & MCG_S_OSCINIT_MASK)) {}; /* Wait for Reference Clock Status bit to clear */ while (MCG_S & MCG_S_IREFST_MASK) {}; /* Wait for clock status bits to show clock source * is external reference clock */ //while (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) != 0x2) {}; //new while (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) != 0x0) {}; //new FEE MCG_C4 |= MCG_C4_DMX32_MASK | MCG_C4_DRST_DRS(3); /* Now in FBE * Configure PLL Reference Divider, PLLCLKEN = 0, PLLSTEN = 0, PRDIV = 0x18 * The crystal frequency is used to select the PRDIV value. * Only even frequency crystals are supported * that will produce a 2MHz reference clock to the PLL. */ //MCG_C5 = MCG_C5_PRDIV(BSP_REF_CLOCK_DIV - 1); /* Ensure MCG_C6 is at the reset default of 0. LOLIE disabled, * PLL disabled, clock monitor disabled, PLL VCO divider is clear */ MCG_C6 = 0; /* Calculate mask for System Clock Divider Register 1 SIM_CLKDIV1 */ SIM_CLKDIV1_COPY = SIM_CLKDIV1_OUTDIV1(BSP_CORE_DIV - 1) | SIM_CLKDIV1_OUTDIV2(BSP_BUS_DIV - 1) | SIM_CLKDIV1_OUTDIV3(BSP_FLEXBUS_DIV - 1) | SIM_CLKDIV1_OUTDIV4(BSP_FLASH_DIV - 1); Re: Problem with defining external 32K oscillator as FLL source 寂しさを感じていますか?沈黙を破り、世界と瞬時に繋がろう!Omegleチャットを試して、世界中の新しい興味深い人々と出会い、いつでも気軽に会話を始めてみましょう。 Re: Problem with defining external 32K oscillator as FLL source 寂しさを感じていますか?沈黙を破り、世界と瞬時に繋がろう!Omegleチャットを試して、世界中の新しい興味深い人々と出会い、いつでも気軽に会話を始めてみましょう。https://omeglechat.love/ Re: Problem with defining external 32K oscillator as FLL source <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> SIMモジュールには、レジスタSIM_SOPT2があり、その中にMCGCLKSELフィールドが含まれています。このフィールドを使用すると、RTS発振器(EXTAL32およびXTAL32入力)をFLLにマッピングできます。このフィールドを1に設定します。 そこからFEEモードを使ってFLLからより高いクロックレートを生成できます。 Re: Problem with defining external 32K oscillator as FLL source <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> それが原因だった。RTCクロックをシステムクロックとして設定できますか? Re: Problem with defining external 32K oscillator as FLL source <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 1. 外部の32KオシレーターはEXTALにコネクテッドされていますか、それともRTCオシレーター EXTAL32 / XTAL32に接続されていますか?
View full article
LPC43S57 USB1 主机配置问题 HI 我们正在尝试使用 LPC43S57 控制器的 USB1 外围设备作为 USB 主机来连接客户主板中的设备。我们使用 KEIL MDK 配置 USB 栈和 USB 驱动程序。   当我们调用 USBH_Initialize(1)函数时,它会返回一个错误,表明"Controller 不存在" 。我们尝试在互联网上搜索有关 USB1 硬件连接的信息,发现很多地方都提到,如果没有外部 PHY,USB1 外围设备将无法工作。不过,数据表显示它支持片上全速 PHY。   能否向我们说明 USB1 是否具有全速 PHY 芯片?   不使用 USB1_VBUS 引脚,因为它是主机,而我们连接的设备是自供电设备。   下面是我们作为主机连接 USB1 的快照   此致 萨巴里什-库马尔 Re: LPC43S57 USB1 Host Configuration issue 你好@HeatherUlrich 您是否将 USB1 从主机模式更改为设备模式并开发了 device_cdc 项目? 如果是,你可以先在板上运行 LPCopen 下的 CDC 演示版进行测试。 这将有助于确认硬件是否存在任何问题。 谢谢。 BR 爱丽丝 Re: LPC43S57 USB1 Host Configuration issue @Slope Game总之,说到令人震惊的崩溃,我曾经花了一整个周末的时间来处理一个无法正确枚举的微控制器。结果发现,一个错误配置的时钟速度是罪魁祸首,由此引发了一连串意想不到的错误,真是 调试。这真是令人难以置信的沮丧。 Re: LPC43S57 USB1 Host Configuration issue 你好@Alice_Yang 我已经将 CLK_USB1 配置为为 60MHZ 的 USB1 接口生成时钟。我已将 USB1 配置为设备(全速模式)并连接到 PC。在 LPC43S57 USB 控制器中,我可以在 USB 状态寄存器中看到 USB 是作为设备连接的,但在 PC 中我看不到任何 COM 端口或任何其他 USB 设备已连接。我已将 USB0 配置为设备并连接到 PC,它被检测为 COM 端口,不适用于 USB 1 配置。 我附上了 USB1 设备配置图片供你参考 此致 萨巴里什-库马尔 Re: LPC43S57 USB1 Host Configuration issue 你好@Sabarish 在 USB 全速模式下,使用 CLK_USB1 为 USB1 接口产生时钟,无需外部 PHY。在高速模式下,外部 PHY 为 USB1 接口产生时钟,必须通过系统配置块中各自的引脚配置寄存器在引脚 PC_0 或 P8_8 上启用 USB1_ULPI_CLK。 请检查 USB1_DP 和 USB1_DM 信号是否正确连接到设备。此外,请确保正确安装软件配置。作为参考,您可以参考 LPCopen 库中提供的USB主机演示。 Alice_Yang_0-1757931704656.pngAlice_Yang_0-1757931704656.png BR 爱丽丝 Re: LPC43S57 USB1 Host Configuration issue 好吧,让我们来解开这个 USB 的难题!是内部 PHY 还是某些硬件怪癖在捣乱?控制器出错总是让人头疼。寻找合适的 USB 配置就像在迷宫中穿行。有一次,我正在与一个顽固的 Arduino 设置搏斗,试图让它与一个项目中的传感器通信。花了几个小时追踪电线和调试代码,最后才发现一个简单的电源问题就是根本原因,这让我这个充满 @geometrydash的下午彻底泡汤了。有时,显而易见的事情会被我们忽略,不是吗? Re: LPC43S57 USB1 Host Configuration issue 这是 USBH_Initialize 函数的一个棘手问题!我记得以前也遇到过类似的硬件连接问题。有时,即使是设置中看似微小的细节也会让人头疼。虽然我无法在此提供具体的硬件调试建议,但您是否考虑过查看 Geometry Dash论坛?那里的社区出人意料地了解各种技术挑战,可能有人在USB设备初始化时遇到了类似的问题。 Re: LPC43S57 USB1 Host Configuration issue 听起来你遇到了棘手的硬件配置问题!我肯定用过 USB 设置。关于片上 PHY,仔细检查芯片的具体硅修订版和勘误表可能会有所帮助。在您排除故障的同时,还可以在 CPS 测试中测试您的反应时间和鼠标技能。 CPS 测试网站上测试您的反应时间和鼠标技能,这可以分散您的注意力。它有助于突出重点!希望你能尽快解决 USB 问题! Re: LPC43S57 USB1 Host Configuration issue 您好 @UnblockedGames感谢您分享示意图快照。除了 PHY 问题外,了解 USB0 在同一块主板上能否正常工作会很有帮助,因为这可以帮助确定问题是与硬件还是软件有关。 Re: LPC43S57 USB1 Host Configuration issue 您在使用 LPC43S57 的 USB1 外设时遇到了问题,这很有意思,尤其是考虑到数据手册表明它具有片上全速 PHY。“控制器不存在”错误确实令人沮丧。我很想知道是否有人成功地将 USB1 用作该芯片上的主机,比如用于Pokerogue之类的程序。祝你好运,希望你能弄明白! Re: LPC43S57 USB1 Host Configuration issue “控制器不存在”这条消息听起来很令人沮丧。我可能会先检查 USB1 时钟配置、引脚分配,以及 USB1 主机初始化是否与选定的全速配置匹配。这里,片上全速 PHY 和外部 PHY 要求之间的区别尤为重要。在一次性更改多个设置之前,最好先分别测试设置的每个部分。在花费太多时间排查硬件故障后,我通常会玩一会儿像《几何冲刺》这样的小游戏休息一下,然后再以全新的思维方式重新解决问题。 Re: LPC43S57 USB1 Host Configuration issue 这听起来像是棘手的硬件/软件交互问题!我绝对有过这样的经历,因为文件似乎与现实世界的行为相矛盾而抓狂。当处理片上 PHY 等底层外围细节时,这种情况尤其令人沮丧。当我遇到这类难题时,我发现与其他可能遇到过类似问题的开发者交流想法非常有帮助。你或许能在“糟糕的育儿方式”平台上找到一些有用的见解——有时候,只需要一双全新的眼睛或一个不同的视角就能找到解决办法。
View full article
S32K328 HyperRAMの低温時の読み書きエラー こんにちは、NXPコミュニティの皆さん、 私たちは、QuadSPIインターフェースを通じてコネクテッドされた64Mbit HyperRAMを搭載したNXP S32K328 S27KL0642DPBHB023を使用しています。 インターフェースは以下の基本構成で動作します:   HyperRAMの電圧 = 3.3V   QuadSPIクロック = 120MHz   インターフェースモード = オクタルDDR   クロックモード = シングルエンドCK   読み取りデータストローブ = 外部RWDS   レイテンシモード = 固定レイテンシ   通常メモリアクセス = メモリマッピングされたAHB 室温ではHyperRAMインターフェースは正常に動作しているようです。 低温、具体的には-40℃までの温度では、読み書き比較エラーが発生することが確認されました。この問題は主にS32K328の温度に関連しているようです。S32K328を冷却すれば誤りを再現できますが、HyperRAMを冷却するだけでは効果ははるかに小さいです。 S32K328 QuadSPIの関連設定は以下のとおりです。 DDR_EN = 1   DQS_EN = 1   外部DQS/RWDS = 選択済み   DQS_OUT_EN = 1   VAR_LAT_EN = 0   FLSHCR.TCSS = 4   FLSHCR.TCSH = 7   FLSHCR.TDH = 1 現在のDLL構成は以下のとおりです。   SLV_DLL_BYPASS = 0   SLAVE_AUTO_UPDT = 1   SLV_EN = 1   SLV_DLY_COARSE = 0   頻度 = 1   DLL_CDL8 = 0   DLLRES = 8   DLL_REFCNTR = 2   SMPR.FSPHS = 0   SMPR.FSDLY = 0   SMPR.DLLFSMPFA = 0 以下のすべての組み合わせをテストしました。   SLV_DLY_OFFSET = 0~7   SLV_FINE_OFFSET = 0~15 低温環境では、テストしたすべてのDLL構成において不具合が発生する。このスイープテストでは、構成間の違いは明らかになるものの、完全にエラーのない動作範囲や、明確に最適なDLLパラメータセットが得られるわけではない。 したがって、この問題がDLL構成自体によるものなのか、それともS32K328 QuadSPIインターフェースの温度依存の別の部分によるものかは現時点では確信が持てません。 以下の質問にご協力いただけますか? 上記に示したS32K328 QuadSPI構成は、120MHzでのHyperRAM動作に適していますか? 選択されたDLLパラメータは、この周波数および全温度範囲に対して適切ですか? 120 MHz の場合、FREQEN、DLL_CDL8、DLLRES、DLL_REFCNTR にはどの値を使用すべきですか? DLLの動作が正しいことを確認するために、どのステータスフラグを監視すべきでしょうか? HyperRAMにアクセスする前にDLLA_LOCKとSLVA_LOCKの両方を確認するべきでしょうか? DLLA_RANGE_ERRまたはFINE_UNDERFLOWはどのように処理すべきですか? QuadSPI DLLや外部DQS経路は低温時に有効範囲外で動作可能でしょうか? DLLの設定は読み取りデータサンプリングのみに影響を与えるのでしょうか、それとも書き込みタイミングにも影響しますか? FLSHCR.TCSS = 4、FLSHCR.TCSH = 7、FLSHCR.TDH = 1 は、120 MHz HyperRAM の動作に適していますか? 120MHzオクタルDDRにおいて、CK、CS#、DQ[7:0]、RWDSに推奨されるパッド設定はどれですか? S32K328に関して、QuadSPI、外部DQS、または低温動作に関連する既知の不具合やRTDの問題はありますか? 120MHz動作に対応した、検証済みのS32K328 HyperRAM初期化例またはレジスタ構成はありますか? S32K328のレジスタやステータス情報の中で、他に確認すべき項目があれば、ご教示いただけると大変助かります。 よろしくお願いします。 Re: S32K328 HyperRAM read write errors at low temperatures 1) 動作モードはサポートされていますが、現在の構成は表66の必要な120MHz DDR外部DQS設定と完全に一致していません。FREQENは0、SMPR.DLLFSMPFAは4、FLSHCR.TCSSは2、FLSHCR.TCSHは5に設定し、両方の遅延オフセットは初期値として0に設定してください。残りの設定値は表66に一致します。低温試験をさらに進める前に、設定を修正する必要があります。 2) 動作モードはサポートされていますが、現在の構成は表66の必要な120MHz DDR外部DQS設定と完全に一致していません。FREQENは0、SMPR.DLLFSMPFAは4、FLSHCR.TCSSは2、FLSHCR.TCSHは5に設定し、両方の遅延オフセットは初期値として0に設定してください。残りの設定値は表66に一致します。低温試験をさらに進める前に、設定を修正する必要があります。 3) 表66によると: FREQEN = 0 DLL_CDL8 = 0 DLLRES = 8 DLL_REFCNTR = 2 「DLLと遅延チェーンの使用」の章で説明されているDLLプログラミングの手順にも従う必要があります。 4) これらのDLLSRフラグを監視します。 DLLA_LOCK = 1: DLL参照チェーンがロックされています。SLVA_LOCK = 1: スレーブ遅延チェーンがロックされています。DLLA_RANGE_ERR = 0: DLLマスター遅延チェーンは有効範囲内です。DLLA_FINE_UNDERFLOW = 0: 細遅延チェーンのアンダーフローは発生しませんでした。 5)はい。DLLとスレーブ遅延線が有効の場合、HyperRAMアクセスを開始する前にDLLA_LOCKとSLVA_LOCKの両方がロックを示すはずです。 6) これらのフラグは、設定された遅延が正しく生成できないことを示します。いずれかのエラーが発生している間は、HyperRAMの動作は信頼できるとはみなすべきではありません。表66の構成と必要なDLL初期化シーケンスを再確認してください。エラーが解消されない場合は、QuadSPIの周波数を下げてさらにテストしてください。 7) まずは、記載されている設定で再テストしてください。 😎 外部DQSおよびスレーブDLLの設定は、主に読み取りデータのサンプリングを制御します。書き込みタイミングは主に、CK、CS#、データ出力タイミング、パッド構成、およびFLSHCRタイミングフィールドによって決定されます。読み取り専用と書き込み/読み戻りの別々のテストを行うことで、どのパスが失敗しているかを特定するのに役立ちます。 9) これらは表66と一致しません。特性評価済みの120MHz DDR構成の場合は、以下を使用してください。 FLSHCR.TCSS = 2 FLSHCR.TCSH = 5 FLSHCR.TDH = 1 10) データシートの特性では、DSE = 1、SRE = 0 を使用しています。これらは、最大出力負荷25pF、入力遷移時間1ns、およびQuadSPIトレースの長さが2インチ以下であることを前提としています。これらの条件と実際のCK/RWDS信号品質はボード上で確認されるべきです。 11) 低温における外部DQSの故障を具体的に記述したS32K328の正誤表は確認できていません。ただし、該当する正誤表と、該当するRTDバージョンのリリースノートを確認する必要があります。 12) 現在、検証済みのHyperRAM初期化例は提供されていません。QuadSPIの設定については、S32K3xxデータシートの表66に記載されている構成を参考にしてください。 Re: S32K328 HyperRAM read write errors at low temperatures こんにちは、NXPコミュニティの皆さん、 インフィニオンS27KL0642DPBHB023にコネクテッドされたS32K328の温度依存的なHyperRAMエラーの調査を継続しています。8 MiB、3.3 Vです。 インターフェースは外部エッジアライメントされたRWDS/DQSを用いたオクタルDDRモードで120MHzで動作します。通常のメモリアクセスでは、QuadSPI AHBメモリマップウィンドウを使用します: 0x68000000~0x687FFFFF 現在の関連構成 ------------------------------     QuadSPI SCK = 120 MHz     DDR_EN = 1     DQS_EN = 1     DQS_FA_SEL = 3     DQS_OUT_EN = 1     FLSHCR.TCSS             = 2     FLSHCR.TCSH             = 5     FLSHCR.TDH = 1     SMPR.DLLFSMPFA = 4     SMPR.FSDLY              = 0     SMPR.FSPHS = 0     DLL 頻度 = 0     DLL_CDL8 = 0     DLL_REFCNTR = 2     DLLRES                  = 8     SLV_DLY_OFFSET          = 0     SLV_FINE_OFFSET         = 8     SLAVE_AUTO_UPDT = 1     SLV_EN = 1     SLV_DLL_BYPASS          = 0 微調整値8は、温度試験の結果に基づいて経験的に選択された。これは、データシート改訂版14に記載されているゼロオフセット基準構成から取得したものではありません。 現在の初期化処理には、以下のシーケンスが含まれています。 QuadSPIとLUTの設定 自動更新でDLLを設定 ダミーAHB読み取りを1回実行します QuadSPIソフトウェアリセットを実行する DLLを再度構成します IPコマンドを使用してHyperRAMレジスタを読み取る 通常のAHBアクセスを開始します ダミー読み取りは現在、まず揮発性の32ビット読み取りを行い、その後対応するCortex-M7キャッシュラインを無効化します。 データシート改訂版14との違い ---------------------------------- S32K3xxデータシートRev.14の表66には、S32K328 120MHz DDR、外部DQS、エッジアライン構成について、以下の仕様が記載されているようです。     FLSHCR.TCSS             = 3     FLSHCR.TCSH             = 3     頻度 = 0     DLL_REFCNTR = 2     DLLRES                  = 8     SLV_DLY_OFFSET          = 0     SLV_FINE_OFFSET         = 0     SLAVE_AUTO_UPDT = 0     SLV_UPD                 = 1、RMプログラミングシーケンスによる     DLLFSMPFA               = 4     FSDLY                   = 0 これは現在のTCSS/TCSH = 2/5、ファインオフセット8、自動更新モードとは異なります。 失敗の署名 ----------------- 温度テストでは、測定サンプリングウィンドウの中央付近の設定であっても、メモリテストで時折失敗することが依然として確認されている。 報告された不具合には、再現性のある特徴が見られる。 - 32バイトのブロック全体が影響を受けます。 -アドレス A を読み取ると、返されたブロックはアドレス A + 0xFFE0 の期待されるパターンと一致しているように見えます。 -複数のDLLオフセット/ファイン設定で同じ署名が報告されました。 初期化時のDLLステータスが示した内容:     DLLA_LOCK              = 1     SLVA_LOCK = 1     DLLA_RANGE_ERR         = 0     FINE_UNDERFLOW         = 0 これらのステータス値が、メモリ障害発生のまさにその瞬間に変化しないことを、我々はまだ確認できていません。 0xFFE0の変位は、0x10000 - 0x20に等しいため注目に値しますが、これが64KiBのラップまたはAHBアドレッシングの問題を証明するとは考えていません。 質問 --------- 1.外部エッジアラインDQSを備えた120MHz DDRのS32K328の場合、データシートRev.14の表66に記載されている構成全体を使用する必要がありますか? TCSS/TCSH = 3/3        SLAVE_AUTO_UPDT = 0        SLV_DLY_OFFSET        = 0        SLV_FINE_OFFSET       = 0 2. この正確な表66列のFLSHCRを確認できますか?TDH値ですか? 3. SLAVE_AUTO_UPDT = 0 が必要な場合、以下の手順を正確に実行してください。        SLV_EN        SLV_UPD DLLEN        DLLA_LOCK SLVA_LOCK SLV_UPD クリア 4.次の初期化シーケンスは有効ですか? DLL構成 ダミーAHB読み取り QuadSPIソフトウェアリセット        2番目のDLL構成 最初のIPアクセス 最初のAHBメモリマップアクセス それとも、ソフトウェアのリセットは唯一のDLL初期化の前に行うべきでしょうか? 5. SLV_UPDをクリアした後、どのDLLロック表示が有効であり、最初のHyperRAMアクセス前に確認すべきか? 6. ソフトウェアリセット、DLL再設定、IPコマンドアクセス後にクリアしなければならないQuadSPI AHBバッファ、FIFO、シーケンスポインタは? 7.ダミーAHB読み出しの場合、揮発性読み出しの前にCPUキャッシュラインを無効化し、DSBを実行する必要がありますか? 8. 0xFFE0の明らかな変位がある場合、他のアドレスに関連付けられた完全な32バイトブロックを返すことができるS32K328 QuadSPIの既知の挙動はありますか? 9. NXPは、以下の2つの違いを区別するために、どの測定値またはレジスタトレースを推奨しますか? 読み取りアドレス生成エラー 書き込みアドレスエラー        古い AHB バッファ データ CPUキャッシュのコヒーレンシ HyperBusアドレスラッピング 外部DQSサンプリング誤差 LUTの完全な内容、初期化ソース、レジスタダンプを添付ファイルとして提供できます。 よろしくお願いします。
View full article
Problem with defining external 32K oscillator as FLL source I have a problem with configuring 32K as clock soure.. Attached is the configuration code. MCG_C2 = 0; //new MCG_C2 = MCG_C2_HGO_MASK | MCG_C2_EREFS_MASK; //new MCG_C1 = 0; //new /* Wait for crystal to initialize */ while (!(MCG_S & MCG_S_OSCINIT_MASK)) {}; /* Wait for Reference Clock Status bit to clear */ while (MCG_S & MCG_S_IREFST_MASK) {}; /* Wait for clock status bits to show clock source * is external reference clock */ //while (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) != 0x2) {}; //new while (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) != 0x0) {}; //new FEE MCG_C4 |= MCG_C4_DMX32_MASK | MCG_C4_DRST_DRS(3); /* Now in FBE * Configure PLL Reference Divider, PLLCLKEN = 0, PLLSTEN = 0, PRDIV = 0x18 * The crystal frequency is used to select the PRDIV value. * Only even frequency crystals are supported * that will produce a 2MHz reference clock to the PLL. */ //MCG_C5 = MCG_C5_PRDIV(BSP_REF_CLOCK_DIV - 1); /* Ensure MCG_C6 is at the reset default of 0. LOLIE disabled, * PLL disabled, clock monitor disabled, PLL VCO divider is clear */ MCG_C6 = 0; /* Calculate mask for System Clock Divider Register 1 SIM_CLKDIV1 */ SIM_CLKDIV1_COPY = SIM_CLKDIV1_OUTDIV1(BSP_CORE_DIV - 1) | SIM_CLKDIV1_OUTDIV2(BSP_BUS_DIV - 1) | SIM_CLKDIV1_OUTDIV3(BSP_FLEXBUS_DIV - 1) | SIM_CLKDIV1_OUTDIV4(BSP_FLASH_DIV - 1); Re: Problem with defining external 32K oscillator as FLL source Feeling lonely? Break the silence and connect with the world instantly! Try Omegle chat to meet new, interesting people from across the globe and spark spontaneous conversations anytime. Re: Problem with defining external 32K oscillator as FLL source Feeling lonely? Break the silence and connect with the world instantly! Try Omegle chat to meet new, interesting people from across the globe and spark spontaneous conversations anytime. https://omeglechat.love/ Re: Problem with defining external 32K oscillator as FLL source In the SIM module there is a register; SIM_SOPT2 that contains the field; MCGCLKSEL that allows you to map the RTS oscillator (EXTAL32 and XTAL32 inputs) to the FLL. You set this field = 1. From there you can use FEE mode to generate higher clock rates out of the FLL. Re: Problem with defining external 32K oscillator as FLL source That was the fault. can I configure the RTC clock as the system clock? Re: Problem with defining external 32K oscillator as FLL source 1. Is your external 32 K oscillator connected to EXTAL  or  EXTAL32 / XTAL32 (the RTC oscillator) ?
View full article
LPC43S57 USB1ホスト構成の問題 ハイ LPC43S57 コントローラの USB1 ペリフェラルを USB ホストとして使用して、お客様のボード内のデバイスを接続しようとしています。USB スタックと USB ドライバを構成するために KEIL MDK を使用しています。   USBH_Initialize(1)関数を呼び出すと、「コントローラが存在しません」というエラーが返されます。USB1 ハードウェア接続に関してインターネットで検索してみたところ、多くの場所で USB1 ペリフェラルは外部 PHY がないと動作しないと記載されていることがわかりました。ただし、データシートには、オンチップフルスピード PHY をサポートしていることが示されています。   USB1 にオンチップのフルスピード PHY が搭載されているかどうかを明確にしていただけますか?   USB1_VBUS ピンはホストであり、接続しているデバイスは自己電源デバイスであるため使用されません。   また、ホストとして行ったUSB1接続のスナップショットを以下に示します。   よろしくお願いします。 サバリッシュ・クマール Re: LPC43S57 USB1 Host Configuration issue こんにちは@HeatherUlrich USB1 をホスト モードからデバイス モードに変更して、 device_cdc プロジェクトを開発しましたか? はい、そうであれば、まずボード上で LPCOpen の CDC デモを実行してテストすることができます。 これにより、ハードウェアに問題があるかどうかを確認できます。 ありがとう。 BR アリス Re: LPC43S57 USB1 Host Configuration issue @Slope Gameところで、派手にクラッシュする話ですが、以前、正しくエニュメレーションを行なわない怪しいマイクロコントローラと格闘して週末を丸々過ごしたことがあります。結局、クロック速度の設定ミスが一つだけ原因で、それが次々と予期せぬエラーを引き起こし、デバッグの現実味を帯びてきました。本当にイライラさせられました。 Re: LPC43S57 USB1 Host Configuration issue こんにちは@Alice_Yang CLK_USB1をUSB1インターフェースの60MHzクロック生成用に設定済みです。USB1をデバイス(フルスピードモード)として設定し、PCに接続しました。LPC43S57 USBコントローラーのUSBステータスレジスタでは、USBがデバイスAとして接続されていることが確認できますが、PC側ではCOMポートや他のUSBデバイスが接続されていることが確認できません。USB0をデバイスとして設定し、PCに接続したところ、COMポートとして検出され、USB1の設定では動作しません。 参考までにUSB1デバイスの構成画像を添付しました。 よろしくお願いします。 サバリッシュ・クマール Re: LPC43S57 USB1 Host Configuration issue こんにちは@Sabarish USB フルスピード モードでは、CLK_USB1 を使用して USB1 インターフェース のクロックを生成します。外部 PHY は必要ありません。高速モードでは、外部 PHY が USB1 インターフェースのクロックを生成するため、システム構成ブロック内のそれぞれのピン構成レジスタを介してピン PC_0 または P8_8 で USB1_ULPI_CLK を有効にする必要があります。 USB1_DP​​およびUSB1_DM​​信号がデバイスに正しくコネクテッドされていることを確認してください。さらに、ソフトウェア構成が適切に設定されていることを確認してください。参考までに、LPCopen ライブラリで提供されている USB ホスト デモを参照CANます。 Alice_Yang_0-1757931704656.pngAlice_Yang_0-1757931704656.png BR アリス Re: LPC43S57 USB1 Host Configuration issue さて、この USB の難問を解明してみましょう。これは内部 PHY の問題でしょうか、それともハードウェアの不具合が原因でしょうか?そのコントローラエラーはいつも頭痛の種です。適切な USB 構成を見つけるのは、迷路を進むような感じになります。かつて私は、あるプロジェクトのためにセンサと通信させようと、頑固な Arduino セットアップに格闘していました。何時間も配線をトレースし、コードをデバッグした結果、単純な電源の問題が根本原因であることがわかり、@ geometry dashでいっぱいの午後は完全に無駄になってしまいました。時々、明白なことが私たちには分からないことがありますよね? Re: LPC43S57 USB1 Host Configuration issue これは、USBH_Initialize 関数に関する難しい問題です。以前にも同様のハードウェア接続の問題に直面したことを覚えています。場合によっては、セットアップにおける些細な詳細でも頭痛の種になることがあります。ここでは具体的なハードウェア デバッグのアドバイスを提供することはできませんが、 Geometry Dashフォーラムをチェックすることを検討しましたか?そこのコミュニティはあらゆる種類の技術的な課題について驚くほど知識が豊富で、USB デバイスの初期化で同様の問題に遭遇した人がいるかもしれません。 Re: LPC43S57 USB1 Host Configuration issue 難しいハードウェア構成の問題に直面しているようです。USB セットアップでは確かに同じ状況になりました。オンチップ PHY に関しては、チップの特定のシリコン リビジョンとエラッタ シートを再確認すると、明確になる場合があります。トラブルシューティング中に、 CPS テストWeb サイトで反応時間やマウス スキルをテストしてみると、楽しい気晴らしになるかもしれません。集中力を高めるのに役立ちます!USBの問題がすぐに解決されることを願っています! Re: LPC43S57 USB1 Host Configuration issue こんにちは、@ Unblocked Gamesさん。設計図のスナップショットを共有していただきありがとうございます。PHYに関する質問に加えて、同じボード上でUSB0が正しく動作するかどうかを知ることも役立ちます。そうすることで、問題がハードウェア関連なのかソフトウェア関連なのかを特定するのに役立つからです。 Re: LPC43S57 USB1 Host Configuration issue LPC43S57のUSB1ペリフェラルで問題が発生しているのは興味深いですね。特にデータシートにはオンチップのフルスピードPHYが搭載されていると書かれているのに。「コントローラは存在しません」というエラーは本当にイライラします。このチップ上でUSB1をホストとして正常に使用した人がいるかどうか、例えばpokerogueのようなゲームで使用したことがある人がいるかどうか知りたいです。これを解明するのは大変でしょう! Re: LPC43S57 USB1 Host Configuration issue 「コントローラは存在しません」というメッセージはイライラします。まずはUSB1のクロック設定、ピン割り当て、そしてUSB1ホストの初期化が選択されたフルスピード設定と一致しているかどうかを確認することから始めるでしょう。ここでは、オンチップのフルスピードPHYと外部PHYの要件との区別が特に重要となる。複数の設定を一度に変更する前に、セットアップの各部分を個別にテストすることは常に有効です。ハードウェアのトラブルシューティングに時間をかけすぎた後は、 Geometry Dashのような手軽なゲームで少し休憩を取り、気分転換してから問題に取り組むようにしています。 Re: LPC43S57 USB1 Host Configuration issue これはハードウェアとソフトウェアの複雑な相互作用のようですね!私も確かに、現実の行動と矛盾しているように見えるドキュメントに頭を抱えたことがあります。特にオンチップのPHYのような低レベルの周辺ディテールを扱うとイライラします。こうした壁にぶつかったとき、同じような問題に直面した他の開発者とアイデアを交換することが非常に役立っています。Bad Parentingプラットフォームで有益な洞察が得られるかもしれません。時には、新しい視点や異なる視点があれば解決策を見つけられます。
View full article
SPI Communication on "s32k31XEVB-Q100 Evaluation Board" Hello, I have a s32k31XEVB-Q100 Evaluation Board and try to implement a SPI communication between the S32 and the FS23. My Pin-Configuration: PTB0 -> lpspi0_pcs0 PTC8 -> lpxpi0_sck PTC9 ->lpxpi0_sin PTB1 -> lpxpi0_sout In Peripherals I added Lpspi /* SPI */ /* Time to transfer all frame data */ #define BCC_MSG_SIZE 4U #define RX_BUFFER_SIZE 4U #define TIMEOUT ((uint32)1000000UL) #define NUMBER_OF_BYTES (10) uint16 numberOfBytes = BCC_MSG_SIZE; static void handleSPI(void) { static int counterSPI = 0; __attribute__(( aligned(32) )) uint8_t rxBuffer[BCC_MSG_SIZE] = {0x00};// = {0,0,0,0,0,0,0,0,0,0,0,0}; /* Buffer for receiving. */ __attribute__(( aligned(32) )) uint8_t txBuffer[BCC_MSG_SIZE] = {0x00}; /* Transmission buffer. */ /* M_DEV_PROG_ID * */ txBuffer[0] = 0x01 << 1; // General status flags ( Register address / Read/Write) txBuffer[1] = 0x00; // Read Data txBuffer[2] = 0x00; // Read Data txBuffer[3] = 0x00; // CRC if (counterSPI++ >= 5000000) { counterSPI = 0; lpspi_status = Lpspi_Ip_SyncTransmit(&MASTER_EXTERNAL_DEVICE, &txBuffer[0], &rxBuffer[0], numberOfBytes, 100000); } } int main(void) { /* Write your code here */ Clock_Ip_StatusType clockStatus; clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); if (CLOCK_IP_SUCCESS != clockStatus) { exit_code = -1; } /* Initial Pins */ Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals, g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals); /* Initial ISR */ IntCtrl_Ip_Init(&IntCtrlConfig_0); IntCtrl_Ip_EnableIrq(FlexCAN0_0_IRQn); /* already enabled in IntCtrl_Ip - Interrupt Controller */ //IntCtrl_Ip_EnableIrq(FlexCAN0_1_IRQn); //IntCtrl_Ip_EnableIrq(FlexCAN0_2_IRQn); //IntCtrl_Ip_EnableIrq(FlexCAN0_2_IRQn); FlexCAN_Ip_Init(INST_FLEXCAN_0, &FlexCAN_State0, &FlexCAN_Config0); FlexCAN_Ip_SetRxIndividualMask(INST_FLEXCAN_0,RX_MB_IDX,0xFFFFFFFF); FlexCAN_Ip_ConfigRxMb(INST_FLEXCAN_0, RX_MB_IDX, &rx_info, Rx_MSG_ID); FlexCAN_Ip_SetStartMode(INST_FLEXCAN_0); //FlexCAN_Ip_Receive(INST_FLEXCAN_0,RX_MB_IDX,&rxData,false); lpspi_status = Lpspi_Ip_Init(&Lpspi_Ip_PhyUnitConfig_SpiPhyUnit_0_Instance_0); /* update Transfer Mode */ //Lpspi_Ip_UpdateTransferMode(MASTER_EXTERNAL_DEVICE.Instance, LPSPI_IP_INTERRUPT); for(;;) { handleSPI(); handleCAN(); handleLED(); if(exit_code != 0) { break; } } return exit_code; } Now I connected my Logic-Analyzer to J39 on the Board. The result of this code is: Now I have some questions: 1) Do I send the values in the right order? 2) Do I have to send the CRC when I just want to read some Data? 3) Which register of the FS23 on this board returns fixed data? Or data which I could know to verify the answer? 4) in the CLK I see sometimes that the clk is longer than normal. Do you have some hints to get the SPI-Communication working for me? Re: SPI Communication on "s32k31XEVB-Q100 Evaluation Board" Hi John Please see comment below: Here I only support FS23 not the S32K so I will reply to you from the view point of FS23. Now I have some questions: 1) Do I send the values in the right order? [gw]Please see answer2 for more detail format about read and write operations. Please also read AN12149 page16--5 MCU communication for getting more info about READ/WRITE/CRC 2) Do I have to send the CRC when I just want to read some Data? [gw]Yes,The SPI communication frame format is as follows: CRC is present by default and cannot be disabled. During read and write operations, the MSB is transmitted first and the LSB last. When SPI is idle, i.e., when the CSB pin is high, MISO is in a high-impedance state. In the AN14129 Page11 page16 introduce the INIT CRC and normal CRC calculation methods. They are different. 3) Which register of the FS23 on this board returns fixed data? Or data which I could know to verify the answer? [gw] M_DEV_PROG_ID  address is  0x01 4) in the CLK I see sometimes that the clk is longer than normal. [gw]You test waveform when CS change to low the CLCK is high but in our timing diagram it's low.
View full article
Request for archived S32K3 FreeRTOS 2.0.0 package for MR-CANHUBK344 Hello, I am using the NXP MR-CANHUBK344 evaluation board and I need the archived FreeRTOS package required by the original NXP example project. Required file: SW32K3_FreeRTOS_10_4_6_UOS_2_0_0_DS_updatesite_D2204.zip My environment: Board: MR-CANHUBK344 MCU: S32K344 S32 Design Studio: 3.4 S32K3 Development Package: 3.4.3 S32K3 RTD AUTOSAR 4.4: 2.0.0 I have already downloaded the required S32DS, S32K3 Development Package and RTD versions, but FreeRTOS 2.0.0 is no longer available in the download portal. Could you please provide access to this archived FreeRTOS 2.0.0 package or enable it for my NXP account? Thank you. Re: Request for archived S32K3 FreeRTOS 2.0.0 package for MR-CANHUBK344 Hi @lxndrkurus  You cannot see the product because it is archived. It means there can be bugs in it, that will not be fixed. We usually recommend that customers use the newer version. However, if you insist on testing the older version, then please wait while I contact the internal team to have them add the software to your account. Best Regards, Robin Re: Request for archived S32K3 FreeRTOS 2.0.0 package for MR-CANHUBK344 @lxndrkurus  Go to: Automotive SW - S32K3 Standard Software -> Automotive SW - S32K3 - FreeRTOS ->  Previous: SW32K3_FreeRTOS_10.4.6_2.0.0_D2204 Re: Request for archived S32K3 FreeRTOS 2.0.0 package for MR-CANHUBK344 Hi @lxndrkurus  It should have been added to your account by now. Please note that the product you are requesting—SW32K3_FreeRTOS_10.4.6_2.0.0_D2204—has been archived, which means that any existing bugs may not be fixed. Please download it by click S32K3 Reference Software -> Automotive SW - S32K3 - FreeRTOS -> Previous -> 2.0.0 SW32K3_FreeRTOS_10.4.6_2.0.0_D2204 Best Regards, Robin
View full article
PF09:KITPF09FRDMPGMとKL25Zなしで、別のI²C MCUボード(例:STM3 こんにちは、NXPチームの皆様、 PF09の場合、KITPF09FRDMPGMとKL25Zを使わず、STM32ボードのようなI²Cインターフェースを持つ別のMCUボードを使ってOTPエミュレーションやプログラミングを行うことは可能でしょうか? これに関する規定や文書的なサポートはありますか?可能であれば、それについて説明している文書を教えてください。 ありがとう、 マヘシュ i.MX用PMIC Re: PF09: Can OTP be programmed without KITPF09FRDMPGM and KL25Z, using another I²C MCU board (e.g. こんにちは、マヘシュタンカラ そのようなOTPプログラムはサポートしていませんが申し訳ありません。
View full article
S32K312 ICU SAIC DMA Hi NXP Team: 关于K3的ICU模块,有一个问题如下: 配置一个ICU输入通道测量PWM,SAIC模式,采用DMA搬运数据。首先是SAIC DMA模式RTD代码里会强制改为双边沿触发,然后在双边沿触发的情况下,如果输入的PWM信号线中途断开后再重新接上,当接上信号那一瞬间如果PWM波形处于高电平时刻,则下一个触发的边沿为下降沿,导致后续测量的占空比均是反的,例如PWM波形是20%占空比,ICU的测量结果就是80% 一个完整的PWM波形为: 上升沿——>高电平——>下降沿——>低电平 双边沿触发模式下有可能从下降沿开始采样,将前一个波形的低电平区和后一个波形的高电平区重新组成为一个波形。 请问是否有遇到过类似问题以及有什么好的解决方案吗? 谢谢! Re: S32K312 ICU SAIC DMA 我将按照上述步骤进行调试。非常感谢您的回复! Re: S32K312 ICU SAIC DMA 您好, 您所描述的行为可能发生在 SAIC 与双边沿触发一起使用,并且软件仅根据捕获的时间戳顺序确定 PWM 高/低时间时。输入信号中断后,下一个捕获的边沿可能是下降沿,这可能导致测量极性反转。 但是,eMIOS SAIC 提供了一个边缘捕获功能,特别适用于这种情况。启用 IcuSaicEdgeCapturing 后,AS2 位 31 包含与捕获的时间戳关联的输入信号电平。即使使用双边沿触发,软件也能区分上升沿和下降沿,从而在信号重新连接后恢复正确的 PWM 边沿序列。 请考虑启用此功能,并在处理 DMA 采样时使用捕获的信号电平信息。应检查具体的 DMA 数据处理,以确保 AS2 信号电平位得到传输和保留。 或者,如果符合应用/通道配置,可以考虑使用专用的 eMIOS IPW/IPWM 测量模式,因为这些模式是专门为脉冲宽度/PWM 测量而设计的。 BR,彼得
View full article
RFIDDiscover hello i need to use RFIDdiscover Lite with pegoda CLRD730, can you provide me with link to download it. also i found that the full version of the RFIDdiscover needs a NDA agreement, so can any one tell me whats the steps i need to do (the process of the NDA) so i can complete the NDA and have access to the tool. thanks RF
View full article
FS26 standby Hi, NXP expert, I have encountered a problem related to FS26: Testing revealed that the FS26 cannot enter standby mode. Single-step execution continues, but the FS26 fails to enter standby mode. A reset occurs whenever the Sbc_fs26_SetOperatingMode() interface is run at full speed. The hardware wake signal has been removed, and no other signals are connected to the reset pin. Small Engine Driver Re: FS26 standby Hi Chenxu From which state did you switch to standby state? Could you please provide the command you issued? Re: FS26 standby Hi, thank you for your help, the problem is solved. Testing revealed that when the wake-up time is less than 5ms, reading the M_WIO_FLG register returns 0, indicating that the wake-up source cannot be read. Could you please help answer this question? Thank you. Re: FS26 standby HI CHENXU Please submit a new ticket for the new topic! https://support.nxp.com/s/?language=en_US
View full article
Interface hiding issue in guiguider 2.0.1 In GuiGuider 2.0.1, sometimes adding the "hidden" flag to the properties on the right side of an interface can cause other interfaces to also become invisible, and this cannot be fixed without restarting the software. 回复: 界面隐藏问题guiguider2.0.1 Hi @ZYQ  Thanks for your information. I can reproduce this issue. And i have reported it to our GUIGUIDER team. BR Harry
View full article