Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
AEC-Q100 MFS2613HMDA2AD 是否符合 AEC-Q100 标准?所有 FS26 零件编号都符合 AEC-Q100 标准吗? 谢谢, 恩里科 Re: AEC-Q100 你好 ESof 再会! 是的,整个 FS26 系列产品均符合 AEC-Q100 标准。证明这一点的文件属于机密文件,因此如果您需要该文件,我建议您直接与我们联系,看看我们能做些什么并开始签署保密协议的流程。 希望这些信息对您有所帮助,如果您还需要其他帮助,请告诉我。 由此给您带来的不便,我们深表歉意。 祝你今天过得愉快,一切顺利。
View full article
LX2160ARDB Default boot images Hi, Can anyone please suggest a way to get the default boot images been used in LX2160A-RDB-B board. Evaluation Board Re: LX2160ARDB Default boot images You could use the latest Layerscape Yocto BSP v26.06 The following precompiled images are hosted on https://www.nxp.com/lgfiles/llsdk/walnascar/ > 14 firmware_lx2160ardb-rev2_uboot_emmcboot.img BSP firmware image for LX2160ARDB eMMC boot 15 firmware_lx2160ardb-rev2_uboot_sdboot.img BSP firmware image for LX2160ARDB SD boot 16 firmware_lx2160ardb-rev2_uboot_xspiboot.img BSP firmware image for LX2160ARDB xSPI boot 23 fsl-image-networking-lx2160ardb-rev2.rootfs.tar.gz Layerscape rootfs supports basic networking functionality on LX2160ARDB 24 fsl-image-networking-full-lx2160ardbrev2.rootfs.tar.gz Layerscape rootfs supports full networking functionality on LX2160ARDB 25 flex-installer Deploy tools 4 boot_lx2160ardb-rev2_lts_6.12.tgz Bootpartition image for LX2160ARDB Layerscape Software Development Kit User Guide for Yocto: UG10374.pdf Layerscape Linux SDK User Guide: UG10381.pdf
View full article
PN7642 SPI controller interface SPI controller interface is mentioned in the PN7642 documents and PN7642.h, as well as on OM27642EVK (as SPIM) but that's all. I can't find an example or driver for that SPI controller (I don't mean Host SPI). AI search says that there are specific SPI function calls ,phhalSpi.h ,phhalSpi.c. , but I can't find anything even similar. Does it exist and how can I find it? Thanks for the help. Re: PN7642 SPI controller interface Hello, thank you for your interest in our products. PN7642 does have a set of SDK examples. I'm not sure if you have already imported some of them.     Fabian_R_1-1784755580455.png   As you are able to see, you can just import the examples from the Quick Start panel -> Import SDK examples and search for the SPI as shown in the image. Please keep in mind that OM27642EVK has Follower Pins and Leader Pins. Please also mind section 7 of the Quick Start Guide documentation.
View full article
AEC-Q100 MFS2613HMDA2ADはAEC-Q100規格に適合していますか?FS26のすべての部品番号はAEC-Q100規格に適合していますか? ありがとう、 エンリコ Re: AEC-Q100 こんにちはESof 良い一日! はい、FS26ファミリ全体がAEC-Q100の資格を持っています。これを証明するドキュメントは機密扱いなので、必要なら直接私たちにケースを開いて、何ができるか確認し、NDAの手続きを開始することをお勧めします。 この情報がお役に立てば幸いです。他に何かご不明な点がありましたら、お気軽にお問い合わせください。 ご迷惑をおかけして申し訳ございません。 良い一日をお過ごしください。幸運を祈ります。
View full article
S32K358 + FreeRTOS: Random HardFault during PendSV_Handler Hi Team, I am facing a random HardFault issue on an S32K358 running FreeRTOS. The application runs normally for a long duration and then suddenly hangs. After the system stops executing, the Software Watchdog (SWT) is not serviced and eventually resets the controller. The failure is not immediate—it occurs after approximately 1 to 2 hours of continuous execution When halted after the failure, the call stack shows: PendSV_Handler() ↓ HardFault_Handler() Register values: LR = 0xA5A5A5A5 PC = 0x00407BD9 LR = 0xA5A5A5A5 looks like a memory initialization pattern rather than a valid return address. Other registers: R0 = 0x204011A8 R3 = 0x2040012C R12 = 0x20400010 Any suggestions or debugging recommendations would be greatly appreciated. Re: S32K358 + FreeRTOS: Random HardFault during PendSV_Handler Hi @nirmal_masilamani, It looks like the task context saved during the FreeRTOS context switch has been corrupted. PendSV is used by FreeRTOS for context switching, therefore, if the HardFault occurs inside PendSV_Handler(), it often means the scheduler is attempting to restore an invalid task context. One possible root cause is a task stack overflow. I would recommend increasing the stack size of the tasks and enabling FreeRTOS stack overflow detection: configCHECK_FOR_STACK_OVERFLOW Implement: vApplicationStackOverflowHook(). Additionally, you can periodically monitor the remaining stack space of each task using uxTaskGetStackHighWaterMark(). This can help identify tasks that are running close to their stack limits before the fault occurs. Regards, Daniel Re: S32K358 + FreeRTOS: Random HardFault during PendSV_Handler Hello @danielmartynek , Thank you for response, I already tried increased stack size, enabled stack overflow hook. Added debug CAN msg in overflow hook, I am not receiving that message when fault occur. Also monitoring uxTaskGetStackHighWaterMark(), when fault occur Task 1 : 1977 × 4 ≈ 7908 bytes free Task 2: 1971 × 4 ≈ 7884 bytes free Task 3: 3988 × 4 ≈ 15952 bytes free Re: S32K358 + FreeRTOS: Random HardFault during PendSV_Handler Hi @nirmal_masilamani, So we can probably exclude a stack overflow as the root cause. However, the task context is still getting corrupted. The processor is restoring LR = 0xA5A5A5A5, which results in a UsageFault. 0xA5A5A5A5 is the pattern generated from tskSTACK_FILL_BYTE (0xA5U) and is used by FreeRTOS to fill task stacks when they are created. danielmartynek_0-1784709240297.png Therefore, if LR becomes 0xA5A5A5A5, the context is restored from a location that still contains the original stack fill pattern rather than a valid register value. This could happen if the SP gets corrupted. In that case, PendSV_Handler() would restore the task context from a wrong location in RAM. You should be able to identify the SRAM region from the stack pointer address.  I would recommend that you properly protect the region by MPUs and XRDC.  Also, are any interrupts calling FreeRTOS APIs? If so, are they using the FromISR() variants, and are their priorities configured correctly with respect to configMAX_SYSCALL_INTERRUPT_PRIORITY? Regards, Daniel
View full article
S32K358 + FreeRTOS:PendSV_Handler 期间出现随机硬故障 大家好, 我在运行 FreeRTOS 的S32K358上遇到了随机硬故障问题。 应用程序长时间正常运行后突然卡死。系统停止运行后,软件看门狗(SWT)得不到服务,最终导致控制器重置。 故障并非立即发生,而是在连续执行约1 至 2 小时后出现。 故障停止后,调用堆栈显示: PendSV_Handler() ↓ HardFault_Handler() 寄存器值: LR = 0xA5A5A5A5 PC = 0x00407BD9 LR = 0xA5A5A5A5看起来像是内存初始化模式,而不是有效的返回地址。 其他登记簿: R0 = 0x204011A8 R3 = 0x2040012C R12 = 0x20400010 任何建议或调试技巧都将不胜感激。 Re: S32K358 + FreeRTOS: Random HardFault during PendSV_Handler 你好@nirmal_masilamani , 看起来在 FreeRTOS 上下文切换期间保存的任务上下文已损坏。 PendSV 被 FreeRTOS 用于上下文切换,因此,如果在 PendSV_Handler() 内部发生 HardFault,通常意味着调度程序正在尝试恢复无效的任务上下文。 一个可能的根本原因是任务堆栈溢出。我建议增加任务的堆栈大小并启用 FreeRTOS 堆栈溢出检测: configCHECK_FOR_STACK_OVERFLOW 实现: vApplicationStackOverflowHook()。 此外,您可以使用 uxTaskGetStackHighWaterMark() 定期监测每个任务的剩余堆栈空间。这有助于在故障发生之前识别出接近堆栈限制运行的任务。 此致, 丹尼尔 Re: S32K358 + FreeRTOS: Random HardFault during PendSV_Handler 你好@danielmartynek , 感谢您的回复。 我已经尝试过增加堆栈大小,启用堆栈溢出钩子。 我在溢出钩子中添加了调试 CAN 消息,但发生故障时没有收到该消息。 同时监控uxTaskGetStackHighWaterMark(),当发生故障时 任务 1:1977 × 4 ≈ 7908 字节可用空间 任务 2:1971 × 4 ≈ 7884 字节可用空间 任务 3:3988 × 4 ≈ 15952 字节可用空间 Re: S32K358 + FreeRTOS: Random HardFault during PendSV_Handler 你好@nirmal_masilamani , 因此,我们大概可以排除堆栈溢出是根本原因的可能性。 然而,任务上下文仍然会遭到破坏。处理器正在恢复 LR = 0xA5A5A5A5,这导致了 UsageFault。0xA5A5A5A5 是由 tskSTACK_FILL_BYTE (0xA5U) 生成的模式,FreeRTOS 使用该模式在创建任务堆栈时填充任务堆栈。 danielmartynek_0-1784709240297.png 因此,如果 LR 变为 0xA5A5A5A5,则上下文将从仍然包含原始堆栈填充模式的位置恢复,而不是从有效的寄存器值恢复。 如果存储过程损坏,就可能发生这种情况。在这种情况下,PendSV_Handler() 会从 RAM 中的错误位置恢复任务上下文。 你应该能够根据堆栈指针地址识别出 SRAM 区域。 我建议您使用 MPU 和 XRDC 对该区域进行适当保护。 另外,是否有任何中断调用 FreeRTOS API?如果是这样,他们是否使用了 FromISR() 变体,并且他们的优先级是否根据 configMAX_SYSCALL_INTERRUPT_PRIORITY 正确配置? 此致, 丹尼尔
View full article
Zone Node Logic Control (Main model overview) 1 Table of Contents • Introduction • Black-Box Overview • Simulink Model Overview • Inputs • Algorithm • Outputs • References • Conclusion 2 Introduction This article explains the internal behavior of the Zone Node by opening the component "black box" and describing how information flows through the application. The objective is to provide a functional understanding of the model, starting from the incoming inputs, continuing through the internal processing logic, and concluding with the generated outputs. The Zone Node acts as an intermediary between the Central Controller and the Edge Nodes located within a vehicle zone. While previous articles introduced the component and the development environment, this article focuses on the application's behavior and the responsibilities performed by the embedded software. This article focuses on the functional behavior of the Zone Node and explains how information flows through the component. Detailed aspects such as CAN routing implementation, LIN scheduling mechanisms, peripheral configuration, and communication stack integration will be covered in dedicated articles later in the series. 3 Black-Box Overview From a system perspective, the Zone Node behaves as a communication gateway and data aggregation component. It receives information from different communication networks, processes that information according to predefined routing rules, and forwards the resulting data to other parts of the system. At a high level, the component can be represented as: dragostoma_1-1784789757571.png Figure 1. Black-Box Overview The Zone Node does not implement vehicle-level control strategies. Functions such as braking decisions, steering calculations, or vehicle state management remain the responsibility of higher-level controllers. Instead, the Zone Node focuses on: Receiving messages from the Central Controller Receiving messages from Edge Nodes Acquiring data from local LIN-connected devices Routing information between networks Aggregating and forwarding data Providing monitoring and diagnostic information The result is a reusable communication component that can be deployed in different vehicle zones while maintaining the same overall behavior. 4 Simulink Model Overview The Zone Node functionality is implemented as a Simulink model organized around communication, routing, scheduling, and diagnostic subsystems. From a model perspective, the application can be divided into four logical areas: Input handling Routing and processing Communication scheduling Outputs and diagnostics dragostoma_6-1784790002961.png Figure 2. Main Simulink Application The input layer receives information from CAN and LIN communication interfaces and makes it available to the application logic. The processing layer evaluates incoming messages and determines how they should be handled. The scheduling layer manages periodic communication activities, while the output layer is responsible for forwarding messages and generating diagnostic information. This separation helps keep the model modular and makes it easier to extend the application with additional communication paths or Edge nodes without changing the core routing behavior. 5 Inputs The Zone Node receives information from three main categories of inputs. 5.1 CAN Network Inputs CAN communication represents the primary source of information processed by the Zone Node. Messages can originate from: Central Controller Lighting modules Steering modules Motor control modules Other Edge Nodes within the zone Typical examples include: Vehicle commands Status reports Diagnostic information Fault indications Actuation requests The exact set of messages depends on the specific Edge Nodes connected to the zone. 5.2 LIN Device Inputs The Zone Node also acquires information from LIN-connected devices. In the reference implementation, LIN communication is used to retrieve parking sensor information. The Zone Node periodically requests data from the LIN device and receives measurement values in response. Examples include: Front parking distances Rear parking distances Other LIN-based sensor information From the perspective of the Zone Node, LIN data behaves similarly to any other external input source. 5.3 Configuration Inputs Before normal operation begins, the Zone Node initializes its communication interfaces and loads the required configuration information. Examples include: CAN interface configuration LIN interface configuration Communication schedules Routing rules These parameters define how the application interacts with the surrounding networks. 6 Algorithm Internally, the Zone Node performs three main processing activities. 6.1 Message Reception The first step consists of collecting incoming communication data. Whenever a message arrives, the application captures: Communication source Message identifier Data payload Message length This information becomes available to the routing and aggregation logic. dragostoma_0-1784789836990.png Figure 3. CAN Reception Pipeline 6.1.1 Model Representation of Message Reception Within the Simulink model, message reception is implemented using communication interface blocks and dedicated processing subsystems that capture incoming network events and make the received information available to the rest of the application. dragostoma_7-1784790035889.png Figure 4. CAN Reception Main Flow dragostoma_8-1784790056735.png Figure 5. CAN Reception Subsystem At a high level, the reception subsystem performs three actions: Detects incoming communication events Stores the received information Makes the information available to the routing logic This allows the routing algorithm to operate independently from the physical communication interface. 6.2 Message Routing Message routing represents the primary responsibility of the Zone Node. The routing logic determines the origin of each incoming message and forwards it to the appropriate communication interface. The behavior can be simplified as: dragostoma_1-1784789857331.png Figure 6. Bidirectional CAN Routing Messages received from the Central Controller are forwarded toward the Edge Nodes, while messages originating from Edge Nodes are routed back toward the Central Controller. The routing mechanism remains independent of the actual application payload, allowing the same software architecture to support different message sets and vehicle functions. 6.2.1 Model Representation of Routing Logic The routing functionality is implemented as a dedicated subsystem responsible for deciding where each received message should be forwarded. dragostoma_9-1784790120286.png Figure 7. Message Routing Main Flow dragostoma_10-1784790141963.png Figure 8. Message Routing Subsystem The routing subsystem evaluates the origin of the received message and selects the appropriate destination interface. At this level, the application does not interpret individual signal meanings; it simply ensures that information reaches the correct communication network. This approach keeps the routing layer independent from application-specific functionality and allows the same architecture to be reused across different deployments. 6.3 LIN Scheduling and Data Acquisition In parallel with CAN routing, the Zone Node periodically acquires data from LIN-connected devices. The sequence follows a simple request-response model: dragostoma_2-1784789896373.png Figure 9. LIN Parking Acquisition Cycle This mechanism allows information originating on a LIN network to become available to the rest of the vehicle through CAN communication. 6.3.1 Model Representation of LIN Scheduling Periodic LIN communication is implemented using a dedicated scheduling subsystem. dragostoma_11-1784790193540.png Figure 10. LIN Scheduling Main Flow The scheduler periodically requests data from LIN-connected devices, waits for a response, and updates the application data used by the rest of the system. Depending on the communication requirements, the scheduler may manage one or more request-response sequences while maintaining a deterministic execution pattern. 6.4 High-Level Data Flow The internal data flow implemented by the Zone Node can be summarized as follows: dragostoma_3-1784789923452.png Figure 11. Zone Node Data Flow 7 Outputs The Zone Node produces several categories of outputs that are consumed by different parts of the vehicle architecture and by development tools used during validation and debugging. 7.1 Routed CAN Messages The primary outputs of the Zone Node are CAN messages forwarded between communication networks. Examples include: Commands sent from the Central Controller to Edge Nodes Status information returned from Edge Nodes Diagnostic messages Fault reports Configuration updates By routing these messages between communication domains, the Zone Node maintains communication between the central controller and the devices located within its assigned vehicle zone. 7.2 Aggregated Device Data In addition to forwarding CAN traffic, the Zone Node generates CAN messages containing information acquired from locally connected devices. One example is parking sensor data collected through a LIN interface and republished on CAN. This allows the Central Controller to access the information without requiring direct interaction with the LIN-connected device. The process can be summarized as: dragostoma_4-1784789955066.png Figure 12. LIN-to-CAN Data Path This approach creates a unified communication interface while hiding the complexity of the underlying network topology. 7.3 Diagnostic Outputs The Zone Node generates diagnostic information that is useful during development, system integration, and troubleshooting activities. Examples include: Communication counters Status variables Network activity indicators Communication statistics Device data used for monitoring purposes These outputs provide insight into the current behavior of the application and can be accessed through development tools such as FreeMASTER. 7.4 Visual Indicators In addition to communication outputs, the Zone Node drives visual indicators available on the evaluation hardware. The on-board LEDs provide immediate feedback regarding: Message reception activity Message transmission activity LIN communication activity Application execution status Although these indicators are not used by the vehicle itself, they simplify application bring-up and validation by providing a quick visual confirmation that the software is operating correctly. 7.5 Output Destinations The outputs generated by the Zone Node are consumed by several different system components. Central Controller Receives: Status information from Edge Nodes Aggregated sensor data Diagnostic information generated within the zone Edge Nodes Receive: Commands originating from the Central Controller Configuration and control messages forwarded through the Zone Node Local Devices Receive: Periodic requests issued by the Zone Node Communication messages required to acquire local measurements Development Tools Receive: Monitoring variables Communication statistics Diagnostic information used for debugging and validation 7.6 High-Level Output Flow dragostoma_5-1784789974523.png Figure 13. System Topology This output structure allows the Zone Node to act as a communication intermediary while simultaneously providing visibility into the behavior of the system during development and validation. 8 References NXP Model-Based Design Toolbox (MBDT) S32K3 Microcontroller Documentation S32K344-WB Evaluation Board Documentation 9 Conclusion This article described the internal behavior of the Zone Node by examining its inputs, processing logic, and outputs. By presenting the component as a functional black box, it explained how information is received, routed, aggregated, and distributed throughout the system without focusing on implementation-specific details. The next articles in the series will build upon this foundation by examining individual communication paths in more detail, including CAN-to-CAN routing, LIN-to-CAN routing, and the techniques used to validate and troubleshoot communication behavior.
View full article
Creating virtual vehicle with MathWorks - SW & HW Environment 1 Table of Contents • Introduction • Software Environment • Hardware Environment • References • Conclusion 2 Introduction Turning a vehicle concept into an interactive Virtual Vehicle requires more than a standalone simulation model. It requires a connected software and hardware environment that can define the vehicle architecture, simulate the powertrain and vehicle dynamics, place the vehicle in realistic driving scenarios, visualize the behavior in 3D, and allow user interaction through driver-in-the-loop inputs. This article continues the Virtual Vehicle system series by moving from the system-level overview to the enablement layer behind the application. It highlights the MathWorks tools and host-side hardware resources that make the virtual vehicle demonstrator possible. At the core of the workflow is Model-Based Design. MathWorks tools are used to configure the vehicle architecture with Virtual Vehicle Composer, model the powertrain and vehicle dynamics, define and execute driving scenarios, create 3D road environments, exchange CAN-based signals, and analyze simulation results. The same environment also supports interactive execution, where driver inputs from a steering wheel and pedals can influence the virtual vehicle behavior during scenario playback. 3 Software Environment The software environment provides the modeling, simulation, scenario definition, visualization, communication, and analysis capabilities required by the Virtual Vehicle system. Each MathWorks tool contributes a specific part of the workflow, from vehicle architecture definition and plant modeling to 3D scenario execution and CAN-based interaction with external systems. 3.1 MATLAB and Simulink R2025b MATLAB and Simulink form the central engineering environment for the Virtual Vehicle. MATLAB.pngFigure 1. MATLAB MATLAB provides the scripting, data management, parameterization, and analysis capabilities required to configure simulations, process logged signals, and evaluate test results. Simulink.pngFigure 2. Simulink Simulink provides the model-based design environment in which the virtual vehicle, control logic, communication interfaces, and test harnesses are assembled. The system-level model can connect plant models, vehicle dynamics, driver inputs, scenario interfaces, and network communication blocks into a single executable simulation. 3.2 Virtual Vehicle Composer Virtual Vehicle Composer.pngFigure 3. Virtual Vehicle Composer Virtual Vehicle Composer is the configuration and assembly environment used to create the Virtual Vehicle model. It allows the user to define the vehicle class, select the powertrain architecture, choose the vehicle dynamics fidelity, configure components, specify test scenarios, select logged signals, build the vehicle model, run the configured tests, and analyze the results. In this Virtual Vehicle system, Virtual Vehicle Composer acts as the entry point for building a consistent vehicle model. It assembles the selected architecture from predefined and customizable components and prepares the model for closed-loop simulation in Simulink. The app also supports repeatable test execution. The same virtual vehicle can be operated across selected scenarios, while relevant signals are logged for review. This makes it suitable for early design studies, component comparison, control validation, and system-level behavior analysis before moving to hardware integration. 3.3 Powertrain Blockset Powertrain Blockset.pngFigure 4. Powertrain Blockset Powertrain Blockset provides the vehicle powertrain modeling foundation for the Virtual Vehicle model. It includes reference applications and component libraries for conventional, hybrid, and battery-electric propulsion systems. In this system, Powertrain Blockset supports the definition of the propulsion architecture, energy storage, electric motors, drivetrain elements, tires, driver models, and supervisory control behavior. It also provides workflows that help configure, resize, calibrate, and analyze the selected powertrain components. The generated vehicle model can be used for performance analysis, energy management studies, range evaluation, component sizing, control parameter optimization, and hardware-in-the-loop preparation. Because the models are open, project-specific subsystems can be integrated into the generated architecture when needed. 3.4 Vehicle Dynamics Blockset Vehicle Dynamics Blockset.pngFigure 5. Vehicle Dynamics Blockset Vehicle Dynamics Blockset provides the vehicle motion and handling foundation for the Virtual Vehicle. It includes reference applications and component libraries for propulsion, steering, suspension, vehicle body, brakes, tires, driver models, and supervisory controllers. For the Virtual Vehicle system, the blockset enables different levels of vehicle dynamics fidelity depending on the simulation objective. Longitudinal dynamics can be used for drive-cycle and energy studies, while combined longitudinal, lateral, and vertical dynamics can be used for handling, chassis behavior, and more complex driving scenarios. The blockset also supports 3D visualization workflows, allowing the virtual vehicle behavior to be observed in a realistic environment. This helps connect numerical simulation results with intuitive visual feedback during ride, handling, ADAS, and driver-in-the-loop demonstrations. 3.5 Automated Driving Toolbox Automated Driving Toolbox.pngFigure 6. Automated Driving Toolbox Automated Driving Toolbox supports the definition, simulation, and analysis of driving scenarios used to exercise the Virtual Vehicle. It provides capabilities for creating road layouts, actors, trajectories, sensor-related contexts, and repeatable test cases. In this setup, the toolbox is used to create controlled and repeatable traffic situations around the ego vehicle. These scenarios can be used to evaluate how the virtual vehicle behaves in predefined maneuvers, traffic interactions, lane-following conditions, or other driving situations relevant to the demonstration. By combining scenario definition with the vehicle model, the Virtual Vehicle can be validated in a structured way. Instead of testing only isolated model behavior, the complete system can be exercised against realistic road and traffic conditions. 3.6 Vehicle Network Toolbox Vehicle_Network_Toolbox.pngFigure 7. Vehicle Network Toolbox Library Vehicle Network Toolbox brings vehicle network communication into the model-based workflow. It provides MATLAB functions and Simulink blocks for sending, receiving, encoding, and decoding messages over in-vehicle network protocols such as CAN, CAN FD, J1939, and XCP. In the Virtual Vehicle, the toolbox is used to exchange selected vehicle signals with external systems or hardware components. CAN messages can be packed and unpacked using database-driven definitions, allowing the model to follow the same signal structure expected by the vehicle-level architecture. This makes communication behavior visible and testable during simulation. Commands, feedback, status information, and selected virtual vehicle signals can be validated before deployment or integration with physical controllers, reducing late-stage integration risk. 3.7 RoadRunner RoadRunner.pngFigure 8. RoadRunner RoadRunner provides the 3D scene creation environment used by the Virtual Vehicle system. It enables the design of detailed road networks, intersections, lane markings, traffic signs, buildings, terrain, and other environmental assets required for realistic driving simulation. In this workflow, RoadRunner supplies the visual and spatial context in which the virtual vehicle operates. The generated scenes can represent controlled proving-ground layouts, urban intersections, highway segments, or demonstration environments used for scenario execution. When combined with Simulink and the vehicle model, RoadRunner helps transform the simulation from a signal-level model into an interactive visual experience. This is especially useful for driver-in-the-loop demonstrations, ADAS workflows, and stakeholder-facing presentations. 3.8 Simulink 3D Animation Simulink 3D Animation.pngFigure 9. Simulink 3D Animation Library Simulink 3D Animation connects Simulink models and MATLAB algorithms to a 3D simulation environment, enabling dynamic systems to be visualized in photorealistic scenes. In the Virtual Vehicle system, it provides the visualization and interaction layer used to observe vehicle behavior in a 3D environment during simulation. The toolbox can use prebuilt scenes or imported scenes created in RoadRunner, and it allows vehicles, objects, lighting, weather effects, and sensor-related elements to be controlled during simulation. This makes it suitable for connecting the Virtual Vehicle model to visually rich driving environments. For driver-in-the-loop operation, Simulink 3D Animation also supports interactive navigation and manual control through hardware devices. This allows steering wheel and pedal inputs to influence the simulated vehicle while the resulting motion is visualized in the 3D scene. 3.9 Stateflow Stateflow.pngFigure 10. Stateflow Library Stateflow provides the graphical environment for modeling state machines, decision logic, and event-driven behavior inside the Virtual Vehicle system. It is used when vehicle behavior must depend on operating modes, transitions, conditions, timers, or fault states. Within the Virtual Vehicle model, Stateflow can support supervisory control, mode management, scenario state handling, driver input interpretation, startup and shutdown sequencing, or fallback behavior. This helps separate discrete decision logic from continuous plant and controller behavior. Using Stateflow keeps the system behavior easier to understand, review, and validate. Complex conditions can be represented explicitly as states and transitions, which improves traceability during simulation and debugging. 4 Hardware Environment The hardware environment provides the execution platform, user input interface, and visualization resources required to operate the Virtual Vehicle system interactively. The main components are the GPU-accelerated PC and the Xbox-compatible steering wheel and pedal controller. 4.1 PC with GPU Acceleration The PC is the main host platform for the Virtual Vehicle system. It runs MATLAB, Simulink, Virtual Vehicle Composer, RoadRunner-related workflows, and the supporting toolboxes used to model, simulate, visualize, and analyze the vehicle behavior. GPU acceleration is important because the system includes visually rich 3D scenes and interactive simulation workflows. The graphics hardware helps render the driving environment smoothly, maintain responsive visualization, and support a more realistic driver-in-the-loop experience. In this setup, the PC also acts as the integration point between the simulation model, the 3D environment, the input devices, and any external communication interfaces. This makes it the central execution and orchestration node of the Virtual Vehicle demonstration. 4.2 Xbox-Compatible Wheel Controller Xbox-Compatible Wheel Controller The Xbox-compatible wheel controller provides the physical driver input interface for the Virtual Vehicle system. It allows the user to control steering, acceleration, and braking through a steering wheel and pedal set instead of using keyboard-based commands. This input device makes the simulation suitable for driver-in-the-loop demonstrations. User actions can be mapped into the Simulink model and used to influence the virtual vehicle response during scenario execution. The wheel controller improves the realism and accessibility of the demonstration. It allows engineers and stakeholders to experience the virtual vehicle behavior interactively, making it easier to evaluate the relationship between driver input, vehicle response, and 3D scene feedback. 5 References The following resources provide useful background for the technologies referenced in this article: MathWorks MATLAB and Simulink documentation MathWorks Virtual Vehicle Composer documentation MathWorks Powertrain Blockset documentation MathWorks Vehicle Dynamics Blockset documentation MathWorks Automated Driving Toolbox documentation MathWorks Vehicle Network Toolbox documentation MathWorks RoadRunner documentation MathWorks Simulink 3D Animation documentation MathWorks Stateflow documentation 6 Conclusion This section described the software and hardware enablement required for the Virtual Vehicle system. The software environment combines MATLAB and Simulink with Virtual Vehicle Composer, Powertrain Blockset, Vehicle Dynamics Blockset, Automated Driving Toolbox, Vehicle Network Toolbox, RoadRunner, Simulink 3D Animation, and Stateflow to support vehicle configuration, system-level modeling, scenario execution, 3D visualization, communication, and analysis. The hardware environment combines a GPU-accelerated PC with a steering wheel and pedal controller to support interactive driver-in-the-loop execution. Together, these elements provide the foundation for building, operating, visualizing, and validating the virtual vehicle before integration with physical controllers or target hardware.
View full article
Streams and Transcode Video with Gstreamer This article shows how to use the i.MX6DL/Q to transcode and stream videos on 1080i/p @ 24fps and 720p @ 30fps. For this test, we used one i.MX6DL as server and an i.MX6DL and i.MX6Q as clients. The video is streamed by the server, playing the sound at the same time, while the clients show the video in the HDMI output, as the image below: Bio_TICFSL_0-1784751985670.jpeg This test depends on some GStreamer plugins. To check that the right GStreamer plugins are installed type the following commands: $ gst-inspect-1.0 | grep h264 To return all the H.264 related plugins, or: $ gst-inspect-1.0 decodebin To check directly the command. To connect more than one board to the minicom, open it with the command: $ sudo minicom –s This way, you open the configuration menu. Enter in the “Serial port setup” option and press “A” to set or change the PORTNUMBER, in “ttyUSB$PORTNUMBER”. To set the HDMI output, run the commands below from the U-Boot prompt: => setenv mmcargs 'setenv bootargs console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 consoleblank=0' => saveenv Be sure that the IPs are correctly setted: SERVER: => ifconfig eth0 $SERVERIP CLIENTS: => ifconfig eth0 $CLIENTSIP Streaming transcoded video only SERVER: => gst-launch-1.0 filesrc location=/home/root/bbb_720p.mp4 ! decodebin ! queue max-size-buffers=0 ! vpuenc_h264 gop-size=2 bitrate=20000 ! queue max-size-buffers=0 ! rtph264pay config-interval=2 ! queue max-size-buffers=0 ! gdppay ! tcpserversink blocksize=512000 host=$SERVERIP$ port=8554 CLIENTS: => gst-launch-1.0 tcpclientsrc host=$SERVERIP$ port=8554 ! gdpdepay ! queue max-size-buffers=0 ! 'application/x-rtp, media=(string)video, clock10-rate=(int)90000, payload=(int)96' ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! autovideosink sync=false Streaming transcoded video + audio SERVER: => gst-launch-1.0 filesrc location=/home/root/bbb_720p.mp4 ! decodebin name=demux demux. ! queue max-size-buffers=0 ! vpuenc_h264 gop-size=2 bitrate=20000 ! queue max-size-buffers=0 ! rtph264pay config-interval=2 ! queue max-size-buffers=0 ! gdppay ! tcpserversink blocksize=512000 host=$SERVERIP$ port=8554 demux. ! alsasink CLIENTS: => gst-launch-1.0 tcpclientsrc host=$SERVERIP$ port=8554 ! gdpdepay ! queue max-size-buffers=0 ! 'application/x-rtp, media=(string)video, clock10-rate=(int)90000, encoding-name=(string)H264' ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! autovideosink sync=false You can check the results with the 1080p@24fps.
View full article
MCXN547: 利用可能な拡張Flex PWMインスタンスはいくつありますか? リファレンス・マニュアルには、PWMモジュールの2つのインスタンス(PWM0とPWM1)がMCXN547で提供されていると記載されています。しかし、ヘッダーファイル(MCXN547_cm33_core0_COMMON.h)では、PWM0のベースアドレスは含まれていますが、PWM1のベースアドレスは含まれていません。 私はMCXN547VKLTという部品を使用しており、PWM出力にはピン17(ポート2_3)を使用する予定です。データシートMCXN547、ポート2_3はALT5 - PWM1_B2機能として設定可能とされています。しかし、MCUXpresso IDEのピン設定ツールを使うと、ALT5 - PWM1_B2機能のためにPin17(ポート2_3)を選択するオプションがありません。 そこで、MCXN547VKLTが2つのEnhanced Flex PWMインスタンスをサポートしているかどうかを確認したいです。 クロック|タイマー MCX N Re: MCXN547: How many Enhanced Flex PWM instances are available? こんにちは、 @JawaharA さん。 投稿ありがとうございます。 MCXN547VKLT FlexPWMモジュールは1つ(FlexPWM0)しか持っていないことは確認できます。 リファレンス・マニュアルとピンマックステーブルは、いくつかのMCX Nシリーズデバイス(N94/N54/N53/N52/N24)に共通しているため、すべてのデバイスバリアントに存在しないペリフェラルに関連する信号が含まれている場合があります。 デバイス固有の機能の利用可否については、データシートの表4(機能比較)を参照してください。この表に基づくと、FlexPWM1はMCXN547VKLTでは利用できません。 Celeste_Liu_0-1784629787830.png したがって、P2_3は共通ピンマルチプレクサテーブルではPWM1_B2として記載されていますが、MCXN547VKLTではこの機能はサポートされていないため、MCUXpresso Config Toolsでは利用できません。 お役に立てば幸いです。他に質問がありましたら、お気軽にお知らせください。 BR セレステ
View full article
Simulinkに統合されるNXP MBDTツールボックスを使用してOSを開発することは実現可能でしょうか? こんにちは、チームのみなさん。 私の目的は、MATLAB/Simulink、Embedded Coder、NXP MBDTを用いて、NXP S32G3向けの完全なベアメタルオペレーティングシステム/ソフトウェアプラットフォームを開発する実現可能性を評価することです。 目標は、Simulinkで完全なソフトウェアスタックを開発し、Embedded Coderを使ってCコードを生成し、生成されたコードを外部オペレーティングシステムやRTOS、AUTOSAR BSWに依存せずに直接S32G3 Gold Boxにデプロイすることです。 特に、NXP MBDTを用いて、Cortex-AコアとCortex-Mコアの両方をS32G3上で実装し、生成されたソフトウェアがシステムの初期化、スケジューリング、割り込み管理、メモリ管理、ハードウェア抽象化、周辺機器初期化、IPCメカニズム、その他オペレーティングシステムで通常提供されるサービスとして技術的に実装できるかどうかを理解したいです。 Boot ROMはハードウェア上に常駐しており、アプリケーションより先に実行されると理解しています。私の意図としては、ハードウェアの起動プロセス以降のすべての処理を、可能な限りNXP MBDTワークフローを通じてSimulinkで生成されたコードを使用して実装することです。 したがって、私の主な質問は次のとおりです。 1. NXP Model-Based Design ToolboxとMATLAB/Simulink、Embedded Coderを組み合わせて、Cortex-AおよびCortex-Mの両方を対象としたS32G3向けのベアメタルソフトウェアプラットフォーム(OS風フレームワーク)を開発することは技術的に実現可能か?MBDTのワークフローに制限がある場合、どの部分が手書きのCやアセンブリを必要とするのかを明確に教えていただけますか? MBDTはNXPによって開発されたものだと理解しています。しかし、もしこの質問にNXP MBDTチームがより適切に回答できる場合は、適切な連絡先やサポートチャネルをご案内していただけるとありがたいです。 ご指導ありがとうございました。 Re: Is it feasible for developing the OS using NXP MBDT toolbox which will be integrated to simulink こんにちは、 @charan032001 投稿ありがとうございます。 別のスレッドで言及され、返信もあったのに気づきました。 NXPの製品にご関心いただきありがとうございます。 BR チェイン
View full article
Is it feasible for developing the OS using NXP MBDT toolbox which will be integrated to simulink? Hi team, My objective is to evaluate the feasibility of developing a complete bare-metal operating system/software platform for the NXP S32G3 using MATLAB/Simulink, Embedded Coder, and the NXP MBDT. The goal is to develop the complete software stack in Simulink, generate C code using Embedded Coder, and deploy the generated code directly onto the S32G3 Gold Box without relying on an external operating system, RTOS, or AUTOSAR BSW. In particular, I would like to understand whether, using the NXP MBDT, it is technically feasible to implement software for both the Cortex-A cores and the Cortex-M core on the S32G3, with the generated software handling system initialization, scheduling, interrupt management, memory management, hardware abstraction, peripheral initialization, IPC mechanisms, and other services typically provided by an operating system. I understand that the Boot ROM is hardware-resident and executes before the application. My intention is for everything after the hardware boot process to be implemented, as much as possible, using Simulink-generated code through the NXP MBDT workflow. Therefore, my primary question is: 1. Is it technically feasible, using the NXP Model-Based Design Toolbox together with MATLAB/Simulink and Embedded Coder, to develop an entire bare-metal software platform (OS-like framework) for the S32G3 targeting both the Cortex-A and Cortex-M cores? If there are any limitations within the MBDT workflow, could you please clarify what portions would still require handwritten C or assembly? I understand that MBDT is developed by NXP. However, if this question is better addressed by the NXP MBDT team, I would appreciate it if you could kindly direct me to the appropriate contact or support channel. Thank you for your guidance. Re: Is it feasible for developing the OS using NXP MBDT toolbox which will be integrated to simulink Hello, @charan032001  Thanks for your post. I noticed it is mentioned via another thread and it had been replied. Thanks for your interest on NXP's product. BR Chenyin
View full article
使用NXP MBDT工具箱开发操作系统并将其集成到Simulink中是否可行? 大家好, 我的目标是评估使用 MATLAB/Simulink、Embedded Coder 和 NXP MBDT 为 NXP S32G3 开发完整的裸机操作系统/软件平台的可行性。 目标是在 Simulink 中开发完整的软件栈,使用 Embedded Coder 生成 C 代码,并将生成的代码直接部署到 S32G3 Gold Box 上,而无需依赖外部操作系统、RTOS 或 AUTOSAR BSW。 具体来说,我想了解使用 NXP MBDT 在技术上是否可行,能否在 S32G3 上为 Cortex-A 内核和 Cortex-M 内核实现软件,生成的软件能够处理系统初始化、调度、中断管理、内存管理、硬件抽象、外设初始化、IPC 机制以及操作系统通常提供的其他服务。 我了解到启动 ROM 是硬件驻留的,并且在应用程序之前执行。我的目标是尽可能地使用 NXP MBDT 工作流程,通过 Simulink 生成的代码来实现硬件启动过程之后的所有操作。 因此,我的主要问题是: 1. 使用 NXP 基于模型的设计工具箱以及 MATLAB/Simulink 和 Embedded Coder,为 S32G3 开发一个完整的裸机软件平台(类似操作系统的框架),同时面向 Cortex-A 和 Cortex-M 内核,在技术上是否可行?如果 MBDT 工作流程存在任何限制,能否请您说明哪些部分仍然需要手写 C 代码或汇编代码? 据我了解,MBDT是由NXP公司开发的。但是,如果这个问题更适合由 NXP MBDT 团队解答,请您指点我到合适的联系方式或支持渠道。 感谢您的指导。 Re: Is it feasible for developing the OS using NXP MBDT toolbox which will be integrated to simulink 你好, @charan032001 感谢你的帖子。 我注意到另一个帖子也提到了这件事,而且已经有人回复了。 感谢您对恩智浦产品的关注。 BR 陈银
View full article
MCXN547: How many Enhanced Flex PWM instances are available? The reference manual mentions 2 instances of PWM modules (PWM0 and PWM1) are available in MCXN547. However, in the header files (MCXN547_cm33_core0_COMMON.h), base addresses for PWM0 is included and not for PWM1.  I am using MCXN547VKLT part and I was planning to use Pin 17 (Port 2_3) for PWM output. MCXN547 datasheet indicates Port 2_3 can be configured as ALT5 - PWM1_B2 function. However, if I use the Pin config tool in MCUXpresso IDE, there is no option to select Pin17 (Port 2_3) for ALT5 - PWM1_B2 function.  Hence, I would like to get confirmation, whether MCXN547VKLT supports 2 instances of Enhanced Flex PWMs.  Clock|Timers MCXN Re: MCXN547: How many Enhanced Flex PWM instances are available? Hello @JawaharA , Thanks for your post. I can confirm that MCXN547VKLT only has one FlexPWM module (FlexPWM0). The Reference Manual and pinmux tables are common to several MCX N series devices (N94/N54/N53/N52/N24), so they may contain signals associated with peripherals that are not present on every device variant. For device-specific feature availability, please refer to Table 4 (Feature Comparison) in the Data Sheet. Based on this table, FlexPWM1 is not available on MCXN547VKLT. Celeste_Liu_0-1784629787830.png Therefore, although P2_3 is listed as PWM1_B2 in the common pinmux table, the function is not supported on MCXN547VKLT, which is why it is not available in MCUXpresso Config Tools. Hope it helps. Please let me know if you have any further questions. BR Celeste
View full article
MCXN547:有多少个增强型 Flex PWM 实例可用? 参考手册提到 MCXN547 中有 2 个 PWM 模块实例(PWM0 和 PWM1)。然而,在头文件(MCXN547_cm33_core0_COMMON.h)中,PWM0 的基地址已包含在内,但 PWM1 的基地址未包含在内。 我正在使用 MCXN547VKLT 器件,并计划使用引脚 17(端口 2_3)作为 PWM 输出。MCXN547 数据手册表明端口 2_3 可以配置为 ALT5 - PWM1_B2 功能。但是,如果我使用 MCUXpresso IDE 中的引脚配置工具,则没有选项可以选择引脚 17(端口 2_3)作为 ALT5 - PWM1_B2 功能。 因此,我想确认一下,MCXN547VKLT 是否支持 2 个增强型 Flex PWM 实例。 时钟|计时器 MCX N Re: MCXN547: How many Enhanced Flex PWM instances are available? 你好@JawaharA , 感谢你的帖子。 我可以确认 MCXN547VKLT 只有一个 FlexPWM 模块 (FlexPWM0)。 参考手册和引脚复用表是几个 MCX N 系列设备(N94/N54/N53/N52/N24)通用的,因此它们可能包含与某些设备变体上不存在的外围设备相关的信号。 有关设备特定功能的可用性,请参阅数据表中的表 4(功能比较)。根据此表可知,MCXN547VKLT 上没有 FlexPWM1。 Celeste_Liu_0-1784629787830.png 因此,尽管 P2_3 在通用引脚复用表中被列为 PWM1_B2,但 MCXN547VKLT 不支持该功能,因此 MCUXpresso 配置工具中没有该功能。 希望对您有所帮助。如果您还有其他问题,请告诉我。 BR 塞莱斯特
View full article
内部 DCDC DCDC_ANA_SENSE 和 VOUT_DCDC_1V8/DCDC_ANA 存在问题 尊敬的NXP支持团队: 在使用 MX RT1172 定制板时,在捕获DCDC_ANA_SENSE波形时,我们发现初始上升到 1.9V,然后稳定在 1.51V。 请问这是什么原因造成的?我附上了波形图和原理图供您参考。 deeporbit_0-1784609948051.png deeporbit_1-1784609973813.jpeg 期待您的回音。 此致, 深的 Re: Issue with internal DCDC DCDC_ANA_SENSE and VOUT_DCDC_1V8/DCDC_ANA 嗨@deeporbit , 非常感谢您对我们产品的关注以及对我们社区的使用。 根据提供的波形,VOUT_DCDC_1V8(DCDC_ANA_SENSE)的稳态电压约为1.51V,这与预期行为不符。在 MIMXRT1170-EVKB 上,我进行了测试,发现 DCDC_1V8_OUT 电源轨稳定在约 1.8 V。 我建议您检查以下内容: 1:确认 DCDC_ANA_SENSE 已正确连接到 VOUT_DCDC_1V8,并检查 0Ω 反馈电阻 R166 是否已正确安装和焊接。 2:检查是否有任何外部 1.8V 稳压器、外设、电平转换器或其他功率域连接到 VDD_1V8 / VOUT_DCDC_1V8 电源轨,并且可能对该电源轨进行拉动或反向驱动。 3:检查连接到 DCDC_ANA / VOUT_DCDC_1V8 的总负载。DCDC_ANA 的负载不得超过其规定的输出能力 150 mA。 mayliu1_1-1784626389774.png 4:如果可能,隔离下游 1.8 V 负载,再次测量 VOUT_DCDC_1V8。如果隔离后电源轨电压恢复到 1.8 V 左右,则问题可能与负载过大或外部电路连接到 1.8 V 电源轨有关。 此致, 5月
View full article
Issue with internal DCDC DCDC_ANA_SENSE and VOUT_DCDC_1V8/DCDC_ANA Dear NXP support team, While working with custom board with MX RT1172, while capturing waveforms of DCDC_ANA_SENSE, we found initial ramp to 1.9V then it stabilises at 1.51V. Could you tell why this is happening, I have attached waveforms and schematic for your reference. deeporbit_0-1784609948051.png deeporbit_1-1784609973813.jpeg Looking forward to hearing from you. Regards, Deep Re: Issue with internal DCDC DCDC_ANA_SENSE and VOUT_DCDC_1V8/DCDC_ANA Hi @deeporbit , Thank you so much for your interest in our products and for using our community. Based on the waveform provided, the steady-state voltage of VOUT_DCDC_1V8 ( DCDC_ANA_SENSE) is approximately 1.51 V, which does not match the expected behavior. On the MIMXRT1170-EVKB, I test and found the DCDC_1V8_OUT rail regulates at approximately 1.8 V. I would recommend checking the following: 1: Confirm that DCDC_ANA_SENSE is correctly connected to VOUT_DCDC_1V8 , and check whether the 0-Ω feedback resistor R166 is properly populated and soldered. 2: Check whether any external 1.8 V regulator, peripheral, level shifter, or other power domain is connected to the VDD_1V8 / VOUT_DCDC_1V8 rail and may be pulling or back-driving the rail. 3: Check the total load connected to DCDC_ANA / VOUT_DCDC_1V8 . The load on DCDC_ANA must not exceed its specified output capability of 150 mA. mayliu1_1-1784626389774.png 4: If possible, isolate the downstream 1.8 V loads and measure VOUT_DCDC_1V8 again. If the rail returns to around 1.8 V after isolation, the issue is likely related to excessive load or an external circuit connected to the 1.8 V rail.  Best regards, May
View full article
内部DCDC DCDC_ANA_SENSEおよびVOUT_DCDC_1V8/DCDC_ANAに関する問題 親愛なるNXPサポートチームの皆様、 MX RT1172を搭載したカスタムボードで作業中に、 DCDC_ANA_SENSEの波形をキャプチャしたところ、最初に1.9Vまで上昇し、その後1.51Vで安定することがわかりました。 なぜこうなるのか教えてもらえますか?参考のために波形と回路図を添付しました。 deeporbit_0-1784609948051.png deeporbit_1-1784609973813.jpeg あなたからの返信を楽しみにしています。 よろしくお願いいたします。 深い Re: Issue with internal DCDC DCDC_ANA_SENSE and VOUT_DCDC_1V8/DCDC_ANA こんにちは、 @deeporbit さん。 私たちの製品にご関心を寄せ、コミュニティをご利用いただき、本当にありがとうございます。 提供された波形に基づくと、VOUT_DCDC_1V8 (DCDC_ANA_SENSE) の定常状態電圧は約 1.51 V であり、これは期待される動作と一致しません。MIMXRT1170-EVKBでテストしたところ、DCDC_1V8_OUTレールは約1.8Vに安定化することが分かりました。 以下の点を確認することをお勧めします。 1: DCDC_ANA_SENSEが正しくVOUT_DCDC_1V8に接続されているか確認し、0 Ωフィードバック抵抗R166が正しく埋め込まれてはんだ付けされているか確認してください。 2: 外部の1.8Vレギュレーター、ペリフェラル、レベルシフター、その他の電源領域がVDD_1V8/VOUT_DCDC_1V8レールに接続されていて、レールを引き寄せたり逆動させたりしている可能性があるか確認してください。 3: DCDC_ANA / VOUT_DCDC_1V8に接続された総負荷を確認してください。DCDC_ANAにかかる負荷は、規定の出力能力である150mAを超えてはならない。 mayliu1_1-1784626389774.png 4: 可能であれば、下流の 1.8 V 負荷を分離し、VOUT_DCDC_1V8 を再度測定します。レールが絶縁後に約1.8Vに戻る場合、問題は過剰な負荷か1.8Vレールに接続された外部回路に関連している可能性が高いです。 よろしくお願いします、 5月
View full article
From Simulation to Vehicle Control: Real-Time Decision Making on the S32N55 1 Table of Contents • Introduction • Overview • Context • References • Conclusion 2 Introduction Modern vehicle development increasingly relies on digital validation before physical prototypes are available. Simulation enables rapid testing and iteration, but engineering teams also need to demonstrate how virtual behavior maps to real hardware. In the Hello World demonstrator, this connection is handled by the Main Node application running on the NXP S32N55. The Main Node acts as the central execution point of the demonstrator, transforming vehicle information generated inside MATLAB ® and Simulink ® into decisions and actions that can be observed on physical hardware. By combining Model-Based Design, CAN communication, and centralized decision making, the system creates a bidirectional link between the virtual vehicle and the physical demonstrator. This article explains how the Main Node converts simulation inputs into coordinated vehicle behavior while maintaining synchronization between the digital and physical domains. 3 Overview As introduced in the previous article, the S32N55 functions as the communication hub of the demonstrator, aggregating information from distributed modules and distributing commands throughout the system. Beyond communication, however, the Main Node also serves as the decision-making layer responsible for interpreting vehicle state and translating it into actionable control signals. Developed using the NXP Model-Based Design Toolbox (MBDT), the application is entirely modeled in Simulink and deployed directly onto the target hardware. This workflow enables engineers to focus on vehicle functionality and system behavior while leveraging automated code generation and integrated CAN communication support. The Main Node receives data from simulated and physical sources, maintains a coherent vehicle-state view, runs vehicle-level control logic, and sends commands to the actuator nodes that make up the demonstrator. This centralized architecture reflects the direction of modern software-defined vehicle platforms, where coordination moves from isolated ECUs toward higher-level compute nodes. figure_1_main_node_vehicle_brain_no_header.png Figure 1. Main Node overview showing how the S32N55 coordinates simulation inputs, vehicle-state processing, and commands to distributed hardware modules. 4 Context The Main Node is positioned between the virtual vehicle environment and the physical hardware modules that form the demonstrator. Driver inputs generated through the Driver-in-the-Loop simulation environment are transmitted over CAN and received by the S32N55, where they are processed alongside feedback arriving from multiple distributed nodes. Commands such as vehicle speed, steering angle, gear selection, braking requests, and lighting controls enter the Main Node from the simulation environment. These inputs are then evaluated by the application and translated into CAN messages that drive the corresponding hardware modules. This architecture enables the physical demonstrator to mirror the behavior of the virtual vehicle. When the simulated vehicle accelerates, the speed command is interpreted by the Main Node and forwarded to the motor control subsystem. Steering-wheel movements are translated into steering-angle commands for the steering module, while lighting commands activate headlights, fog lights, hazard lights, and turn indicators on the physical hardware. figure_2_virtual_physical_synchronization_no_header.png Figure 2. System context illustrating the Main Node as the bridge between the virtual vehicle environment and the physical demonstrator hardware. The Main Node can be driven either by the Driver-in-the-Loop simulation or by the External Control model. In both cases, the command source publishes the same DBC-defined CAN frames, so the S32N55 receives speed, steering, brake, gear, and lighting commands through the same interface. This allows the same deployed application to be exercised from two sources without changing the Main Node software. This approach is especially useful during integration, demonstrations, and incremental validation. Engineers can exercise the Main Node and the downstream actuator modules even when the complete virtual environment is not active, while still preserving the exact communication contract used by the full system. As a result, the application can be validated against two different input sources without changing the deployed software on the board. Rather than acting as a simple gateway, the Main Node continuously evaluates received information and executes vehicle-level decisions. One example is the processing of motor feedback data, where information from multiple motors is combined to derive a representative vehicle speed used throughout the system. Centralizing this functionality simplifies system coordination while ensuring consistency across all connected modules. Gear selection is handled as part of this centralized decision layer. The incoming gear command is interpreted as a driving mode that affects how the requested speed is applied: Park and Neutral block motion commands, Reverse changes the sign of the velocity reference, and Drive or Sport propagate the requested speed as a forward-driving command. This keeps speed-control behavior aligned with the selected driving mode while preserving the same driver-input signal set. The target-speed command is computed from the requested speed reference, the selected gear mode, the reported vehicle speed, and the effective brake command. Motor feedback is fused into a representative reported speed, which provides the actual-speed reference used during braking decisions. Under normal driving conditions, the requested target speed passes through the gearbox-aware logic and is converted into the motor-speed command sent over CAN. When braking is active, the Main Node bases the outgoing command on the detected speed and brake value, reducing the command until the vehicle is considered stopped. The Main Node also hosts the demonstrator's automated emergency braking functionality. Parking sensor nodes continuously report obstacle distances over CAN. The application evaluates these measurements and determines whether an object has entered a predefined safety zone. When this condition is met, the braking command issued by the driver can be overridden and replaced with an emergency braking request generated by the system. Picture1.png Figure 3. Parking sensors in action detecting nearby obstacles and providing distance feedback used by the Main Node to support emergency braking decisions. An important aspect of this implementation is that the braking behavior is reflected across both domains. The physical hardware responds to the braking request, while the simulation environment can receive corresponding vehicle-state updates through the same CAN-based loop. This closed-loop behavior demonstrates bidirectional interaction between simulation and embedded execution, allowing safety-related functionality to be validated in a realistic environment before a full vehicle prototype is available. figure_4_aeb_closed_loop_no_header.png Figure 4. Closed-loop emergency braking flow showing how parking sensor feedback can trigger an automated braking request across both the physical and simulated domains. CAN communication is the key enabler of this architecture. Every subsystem communicates through DBC-defined interfaces, allowing functionality to be distributed across multiple independent nodes while preserving a consistent and scalable communication framework. The shared DBC approach ensures that signal definitions remain synchronized across all parts of the demonstrator. To support this workflow, MathWorks Vehicle Network Toolbox ™ provides direct integration between MATLAB ® , Simulink ® , and CAN communication interfaces. DBC files can be used directly throughout the development process, simplifying signal management and ensuring consistency across the virtual vehicle, the Main Node, and all peripheral modules. As the demonstrator grows to include additional functionality, the same network definition can be reused across all participating systems, reducing integration effort and helping accelerate development. Note: The combination of NXP Model-Based Design Toolbox and MathWorks Vehicle Network Toolbox creates a workflow in which vehicle behavior, communication interfaces, and deployed software remain aligned from modeling through system integration. figure_5_shared_dbc_workflow_no_header.png Figure 5. CAN and DBC workflow showing how shared signal definitions keep the virtual vehicle, Main Node, and distributed hardware modules synchronized. 5 References NXP Model-Based Design Toolbox (MBDT) NXP S32N Vehicle Super-Integration Processors Vehicle Network Toolbox ™ NXP Model-Based Design Toolbox Community 6 Conclusion The Main Node demonstrates how a centralized compute platform can act as more than a communication gateway. Running on the NXP S32N55, it combines signal aggregation, decision making, and command distribution into a single application that coordinates the entire demonstrator. By transforming simulation-generated inputs into physical vehicle behavior and feeding real-world information back into the virtual environment, the Main Node creates a practical closed-loop development platform. Together, NXP Model-Based Design Toolbox, MathWorks Vehicle Network Toolbox, and CAN-based communication enable rapid iteration, simplified integration, and efficient validation of vehicle functionality across simulated and physical domains.
View full article
MCXW72のデバッグ認証応答 MCXW72のデバッグポートのロックを解除しようとしています。MCUXpressoのSecure Provisioning Toolでロック解除は正常に動作しますが、Debug Credential(DC)、DCK秘密鍵、デバイスから受け取ったDACに基づいて自分のアプリケーションを使ってポートのロック解除を試みています。 この分野のドキュメントは非常に不明瞭で(場合によっては誤りもあります)。 私の理解では、DARは以下の要素で構成されています。 DAR = DC + AB + UUID (DACより) + 署名 (リファレンス・マニュアルの図50ではUUIDとABフィールドの順序が誤っています。) OpenSSLを使って署名を計算したいのですが、どのデータを署名すべきか正確には判断できません。 a) DC + CV(DACから) b) DC + AB + CV (DACから) c) DC + AB + UUID (DACから) + CV (DACから) それとも全く別の何か? ドキュメントには署名がDARをチャレンジベクトル(CV)に結合すると記載されていますが、ハッシュ化と署名すべき正確なバイトシーケンスは明確に指定されていません。DAR署名を生成するために使われる正確なデータを教えていただけますか? MCXA セキュリティ(EdgeLock | セキュアブート | OTP) Re: Debug authentication Response for MCXW72 こんにちは、 @Surdej Secure Provisioning ToolはSecure Provisioning SDKの上に構築されています。詳細は https://spsdk.readthedocs.io/en/latest/ これはオープンソースなので、そこで答えが見つかります。
View full article