2397114_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2397114_en-US

2397114_en-US

MCXN547: How many Enhanced Flex PWM instances are available?

The reference manual mentions 2 instances of PWM modules (PWM0 and PWM1) are available in MCXN547. However, in the header files (MCXN547_cm33_core0_COMMON.h), base addresses for PWM0 is included and not for PWM1. 

I am using MCXN547VKLT part and I was planning to use Pin 17 (Port 2_3) for PWM output. MCXN547 datasheet indicates Port 2_3 can be configured as ALT5 - PWM1_B2 function. However, if I use the Pin config tool in MCUXpresso IDE, there is no option to select Pin17 (Port 2_3) for ALT5 - PWM1_B2 function. 

Hence, I would like to get confirmation, whether MCXN547VKLT supports 2 instances of Enhanced Flex PWMs. 

Clock|TimersMCXNRe: MCXN547: How many Enhanced Flex PWM instances are available?

Hello @JawaharA ,

Thanks for your post.

I can confirm that MCXN547VKLT only has one FlexPWM module (FlexPWM0).

The Reference Manual and pinmux tables are common to several MCX N series devices (N94/N54/N53/N52/N24), so they may contain signals associated with peripherals that are not present on every device variant.
For device-specific feature availability, please refer to Table 4 (Feature Comparison) in the Data Sheet. Based on this table, FlexPWM1 is not available on MCXN547VKLT.

Celeste_Liu_0-1784629787830.png

Therefore, although P2_3 is listed as PWM1_B2 in the common pinmux table, the function is not supported on MCXN547VKLT, which is why it is not available in MCUXpresso Config Tools.

Hope it helps. Please let me know if you have any further questions.

BR

Celeste

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-22-2026 04:31 AM
更新者: