2397010_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2397010_en-US

2397010_en-US

Issue with internal DCDC DCDC_ANA_SENSE and VOUT_DCDC_1V8/DCDC_ANA

Dear NXP support team,


While working with custom board with MX RT1172, while capturing waveforms of DCDC_ANA_SENSE, we found initial ramp to 1.9V then it stabilises at 1.51V.

Could you tell why this is happening, I have attached waveforms and schematic for your reference.

deeporbit_0-1784609948051.pngdeeporbit_1-1784609973813.jpeg

Looking forward to hearing from you.

Regards,

Deep

Re: Issue with internal DCDC DCDC_ANA_SENSE and VOUT_DCDC_1V8/DCDC_ANA

Hi @deeporbit ,

Thank you so much for your interest in our products and for using our community.

Based on the waveform provided, the steady-state voltage of VOUT_DCDC_1V8 ( DCDC_ANA_SENSE) is approximately 1.51 V, which does not match the expected behavior. On the MIMXRT1170-EVKB, I test and found the DCDC_1V8_OUT rail regulates at approximately 1.8 V.

I would recommend checking the following:

1: Confirm that DCDC_ANA_SENSE is correctly connected to VOUT_DCDC_1V8 , and check whether the 0-Ω feedback resistor R166 is properly populated and soldered.

2: Check whether any external 1.8 V regulator, peripheral, level shifter, or other power domain is connected to the VDD_1V8 / VOUT_DCDC_1V8 rail and may be pulling or back-driving the rail.

3: Check the total load connected to DCDC_ANA / VOUT_DCDC_1V8 . The load on DCDC_ANA must not exceed its specified output capability of 150 mA.

mayliu1_1-1784626389774.png

4: If possible, isolate the downstream 1.8 V loads and measure VOUT_DCDC_1V8 again. If the rail returns to around 1.8 V after isolation, the issue is likely related to excessive load or an external circuit connected to the 1.8 V rail.


 Best regards,

May

タグ(1)
評価なし
バージョン履歴
最終更新日:
4 週間前
更新者: