コネクト - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

ディスカッション

ソート順:
Every Linux distribution provides features useful in product development - each SoC provides features necessary to a product's success. If you can't take advantage of the distribution of your choice or the SoC of your choice - product development is hampered or stopped altogether. NXP provides technology easing the adoption of SoC specific components into the distribution of your choice. Learn more about this technology, and practical tips and tricks on how to build and use selected components from LSDK at the component isolated level. Topics include building and deploying PPA and boot loaders, building and booting the Linux kernel, and building and deploying select user space components. Emphasis is on native building because it's easier. This will be a two hour session to leave time for Q&A.
記事全体を表示
This session will cover serial reprogramming capability (download, execute, etc.). Show the boot process from the ARM® Cortex®-M4 core including controlling A53 boot. Procedure for building and running baremetal code on Cortex-M4 and A53 using a debugger. Will discuss and demonstrate runtime communication between A53 and Cortex-M4 cores - with a discussion of options and examples.
記事全体を表示
Today, wireless charging is not only used for mobile devices but also expanding to many industrial applications. This session will provide the in-depth technical detail and guidance of the design of wireless charging transmitter and receiver. Also a review of NFC/RFID cards protection that cover both low-power and medium-power applications.
記事全体を表示
Sensors are key to differentiate your products in the market and add context awareness, tamper detection, a robust user interface and intelligent wake-up. This class will step through all the leading applications in the IoT and IMM markets and provide a demonstration of the Sensor Toolbox tools for your product.
記事全体を表示
Introduction to the MCU Alexa Voice solution describing the features, architecture, and presenting the cost and ease of use benefits. We will be also showing the Out-of-Box Experience of on-boarding Alexa using Wi-Fi as well as interacting with Alexa by using a cost effective far-field Implementation.  
記事全体を表示
Extend your logistics track and trace with condition insights. NTAG SmartSensor enables sensing and logging with NFC readout. NTAG SmartSensor enables your IoT application for smart logistics, smart healthcare, drug delivery and smart packaging.
記事全体を表示
With a number of vehicles being connected to the internet, the need to have a secure environment inside the vehicle is increasing. This session will present secure use cases for edge nodes microcontroller in the vehicle and how the S32K can achieve them. Topics including what is security, NXP 4 layer of automotive security, and S32K CSEc.
記事全体を表示
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.
記事全体を表示
Smart Amp software enhancement integrated with smart amplifier to provide optimal end-to-end solution such as voice experience, audio capture and speech assist for mobile and IoT applications.
記事全体を表示
NXP is a recognized automotive market leader in Motion Sensors, Pressure Sensors, and Magneto-Resistive Sensors with an ever growing base of products and solutions. Join this training session to learn about the latest evolutions of the sensor product roadmaps and targeted applications.
記事全体を表示
Smart Amp software enhancement integrated with smart amplifier to provide optimal end-to-end solution such as voice experience, audio capture and speech assist for mobile and IoT applications.
記事全体を表示
Enhancing the performance of Cobra 55.
記事全体を表示
People today face way too many options, especially when it comes to so called smart devices which can easily contain 50+ functional settings. With most people only using a few preferred settings, this session shows product managers, UI designers, and engineers how to leverage NXP’s out of the box Face Rec based Friction Free Interface production grade platform to rapidly add a truly seamless interface to devices such as appliances, home comfort systems, and alarm/safety/security panels, as well as many types of industrial equipment. By recognizing who you are and what you prefer based on past usage, today’s smart machines can tailor their interface to meet end consumer needs person by person (including controlling access) significantly improving customer satisfaction. Wi-Fi and/or connection to the cloud is NOT required to move your interface design to the next level!
記事全体を表示
Introduction into secure element and use case overview secure element complementing secure µCs inside a car security infrastructure. Overview on tool chain including applet and secure gateway demonstrator.
記事全体を表示
This hands-on session will dive deep into the advanced debugging capabilities of the MCUXpresso IDE, including trace, profiling, coverage, watch points and more.
記事全体を表示
Introduction to the ISO26262/EC61508 standard - with emphasis on how to apply it, cross BL designing for advanced functional safety requirements- ASIL B/C/D.
記事全体を表示
Review of NXP’s current CAN portfolio and CAN functions, our support for CAN FD and an overview of the breakthrough products keeping CAN highly relevant for the new generation of vehicles.
記事全体を表示
This class will introduce/update on Android Things, the new version of Android designed for the IoT market. The when, what and how of Android Things will be explained and how NXP has worked with Google to enable certified boards based on NXP silicon and why IoT product developers should consider using Android Things for their next IoT project. Finally the relationship between Android Things, Google Voice Assistant and Chromecast built in will be explained and what NXP parts are most appropriate for optimal performance.
記事全体を表示
The System Controller Firmware is an essential part of the i.MX 8 architecture. In this session you will learn what the System Controller Firmware is and how to use its API on your application.
記事全体を表示