i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
I've been asked to help to upload the doc in MPU support space. The doc describes some ideas about how to support a customer to enable a mipi-csi2 sensor connected with i.MX6DQ/6DL. Hope this may be helpful.
查看全文
http://freescale.eefocus.com/bbs/article_175_179914.html Freescale i.mx53 i.mx6x series solution to speed up the progress of your product 深圳市优创科技有限公司 Josephwang 王伟 深圳市南山区高新技术产业园南区创维大厦C15 Tel:0755-26017990  13128865181        Mail:[email protected]        QQ:[email protected]
查看全文
Qt Creator can be a very good IDE in order to develop great QT applications. This IDE does not only helps with syntax highlighting, access to examples and tutorials, but also helps you to configure different toolchains Qt binary versions and target options. First download the binary installer from: For 32 bits: $ wget http://releases.qt-project.org/qtcreator/2.6.2/qt-creator-linux-x86-opensource-2.6.2.bin For 64 bits: $ wget http://releases.qt-project.org/qtcreator/2.6.2/qt-creator-linux-x86_64-opensource-2.6.2.bin execute the binary $ ./qt-creator-linux-x86_64-opensource-2.6.2.bin Follow the Installer GUI and choose a location. Default options should be OK. in my case the installation was done here: $ /home/b35153/qtcreator-2.6.2/bin Open Qt Creator (in my case from command line, use "&" to regain control of the terminal) $./qtcreator & Open Tools -> Options Choose Build & Run  on the menu of the left. and Select the Compilers Tab Here you can add the toolchain GCC compiler of your convenience. It will appear in the "Manual"  section. Now click on Qt Version Tab.  Here you can add the Qmake that you had created with your Qt installation; for example, the Qt5 installation described here: Building QT for i.MX6 It will appear in the Manual section. In my case I have Qmake for PC and Qmake for i.MX6. Now click on Kits Tab Here you can create combinations of Compilers and Qmake, and also specify where do you want the executables to go. In my case here I combined the i.MX6 toolchain and the Qmake for I.MX6 i had created. I did not set up device configuration since the sysroot is already shared to my device via NFS, but you can configure it so the files are sent via ssh to your device. And that's It! Next time you load a project you can choose which Kit you want to work on, and it will be compiled just as you need.
查看全文
In order to run the QT5 demos on i.MX6 you should follow the instructions on this link: Building QT for i.MX6 Some of the demos on the release such as  /examples/opengl/hellogl_es2,  consist of a group of multiple widgets appearing on the screen. Normally these demos should work OK in a windowed environment such as Wayland or X11. In the case of Linux only environment, the plugin that draws to the screen is called EGLFS. This plugin has the restriction that it only supports one single widget at a time on the screen surface. Then demos such as hellogl_es2 are *not intended* to work along with this plugin, and it will never work. The errors found when using EGLFS consist on: These issues can be seen in the Qt OpenGL examples.  "hellogl_es2" and "2dpaint" seem to display one rendered frame and then break --   "hellogl_es2" shows the QT word and bubbles, and the GUI is hidden, while  "2dpaint" just shows the openGL version without label. It seems that when including  a QGLWidget on a form, the QGLWidget would work OK, but the rest of the form would not appear. I couldn't click any buttons or do anything.   Along with these problems I would also see one or more of these error messages in the output:   * This plugin does not support setParent!   * This plugin does not support propagateSizeHints()   * QOpenGLContext::swapBuffers() called with non-opengl surface However other demos such as hellowindow work well with EGLFS because they are single widget.  Also all demos created with qtquick will work OK since all visual QML items are rendered as a single widget using the scene graph, a low-level, high-performance rendering stack, closely tied to OpenGL. This is better explained here: Qt5 QPainter vs. QML & Scene Graph.
查看全文
Dear All,       Our board is designed based on both EVK and HEG (Adeneo Embedded Home Energy Gateway), the ENET_FEC_RESET_B on EVK is replaced by LCD_D11 as it on HEG. We have re-config all pins based on i.mx28 BSP and successfully built by ltib. However, eth0 is not working due to "PHY is not found"! and we are still trying to figure it out.       The changes we apply on the BSP are(in mx28evk_pins.c): in static struct pin_desc mx28evk_fixed_pins[]:       the definition of LCD_D11 change to { .name = "LCD_D11", .id = PINID_LCD_D11, /* PHY reset pin*/ .fun = PIN_GPIO,      .voltage    = PAD_3_3V,      .strength = PAD_8MA,      .output     = 0, },      and replace all "PINID_ENET0_RX_CLK" in mx28evk_pins.c by "PINID_LCD_D11"      To prevent any possible interrupt, we also disable all LCD pins in both mx28_pins.h and mx28evk_pins.c since we don't have LCD.      Any comment/suggestion is highly appreciate! BR, TF
查看全文
The i.MX 6 D/Q L3.035_1.0.2 patch release is now available on the www.freescale.com ·         Files available # Name Description 1 L3.0.35_1.0.2_LDO_PATCH This patch release is based on the i.MX 6Dual/6Quad Linux   12.09.01 release. The purpose of this patch release is to manage the LDO and   PMIC ramp-up time correctly.
查看全文
       Overview The purpose of this document is to describe how to enable Bluetooth on i.MX 6Dual/Quad SabreSD board (RevC) for Android software. Hardware Changes i.MX 6Dual/Quad SabreSD board doesn't enable Bluetooth connection by default. To support bluetooth, the hardware rework is required. The above diagram shows the reserved connections for Bluetooth in SabreSD RevC board (All connections are marked as "DNP"). This Bluetooth cable connector is designed specifically for the WiFi/BT combo card SX-SDCAN-2830BT which is developed and sold by Silex Technology. Note that pin 1 (BT_DISABLE) of the cable connector on i.MX 6Dual/Quad SabreSD RevC is opposite Pin 20 of the WiFi/BT module. Note: when connecting Silex module and J13, the connection is reverted (For example, PIN 1 in J13 connects to PIN 20 in Silex module). To use the J13 connector, the following reworks are required:   R209-R211, R214-R215 need to be populated.           Where is them, you can refer to the below chart.   SPI nor flash U14 need to be depopulated. No other AUX boards should be connected.. Exchange UART5_RXD and UART5_TXD. Orange PAD connects to Orange PAD. Green PAD connects to Green PAD.      After hardware rework, the Bluetooth connection will like the following:   Pin on Silex Module Sabresd Board Mux Pad Pin-2  BT_UART_RTS  (output) UART5.RTS   (input) MX6Q_PAD_KEY_COL4__UART5_RTS Pin-3  BT_UART_TXD   (output) UART5.RXD   (input) MX6Q_PAD_KEY_ROW1__UART5_RXD Pin-4  BT_UART_CTS   (input) UART5.CTS   (output) MX6Q_PAD_KEY_ROW4__UART5_CTS Pin-5  BT_UART_RXD   (input) UART5.TXD   (output) MX6Q_PAD_KEY_COL1__UART5_TXD Pin-14  BT_PWD_L       (input) GPIO_2         (output) MX6Q_PAD_GPIO_2__GPIO_1_2   Software Information For earlier android version before Jelly Bean4.2 Take ICS as an example, for we didn't do this work when our last ICS version R13.4.1 released. So our formal release had no support on BT. Here will give out patches based on R13.4.1. Enable Bluetooth with the following setting (e.g. device/fsl/imx6/sabresd/init.rc)      # No bluetooth hardware present -    setprop hw.bluetooth 0 +    setprop hw.bluetooth 1 Ensure BOARD_HAVE_BLUETOOTH := true in device/fsl/imx6/sabresd/SabreSDBoardConfigComm.mk. Add BT feature support in device/fsl/imx6/sabresd/required_hardware.xml: <permissions>      <feature name="android.hardware.camera" /> +    <feature name="android.hardware.bluetooth" />   Add UART5 support in kernel: In this step you can refer to the attached (kernel patch for UART5 based on ICS.zip) to change PinMux PAD configuration for UART5.   Add AR3002 BT firmware support: Update external/linux-firmware with the attached patch(0001-ENGR00270791-BT-add-AR3002-firmware-support.patch) to add AR3002 BT firmware support for Silex's BT is AR3002.   Then you can manually run the command “hciattach -n -s 115200 /dev/ttymxc4 ath3k 115200 flow nosleep” in console to see whether bluetooth can attach HCI successfully.   At last, you need add rfkill for BT reset in kernel, here also give a patch for reference: 0001-ENGR00270791-BT-add-rfkill-for-bt-reset.patch   BT is not enable in kernel default. You can control whether to enable it in bootargs like the following  in device/fsl/sabresd_6dq/BoardConfig.mk. BOARD_KERNEL_CMDLINE := console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale  bluetooth For android version since Jelly Bean4.2 From Jelly Bean4.2, Bluez is no longer used.Android provides a default Bluetooth stack, BlueDroid, that is divided into two layers: The Bluetooth Embedded System (BTE), which implements the core Bluetooth functionality and the Bluetooth Application Layer (BTA), which communicates with Android framework applications. A Bluetooth system service communicates with the Bluetooth stack through JNI and with applications through Binder IPC. The system service provides developers access to various Bluetooth profiles. The following diagram shows the general structure of the Bluetooth stack: For bluedroid, we have supported it in our formal release including Android4.3. You can get it from our website. Or just get HAL code from attached(libbt-ath3k.zip). Known issue For  KEY_COL4 is both used by uart5 and pcie,  if you enable BT, 3G  mobile will not work. For its power disable pin is conflict with uart5's UART_RTS. This is also why we didn't enable BT in formal release. Supported and tested profile workable profile not tested profile Hid Handset & Handfree(not support for hardware restrict) A2DP Pbap Opp Pan
查看全文
With Qt5  you will find the addition of new technologies that will make your development much easier. Qtquick2 SceneGraph Qml Qt5 is backwards compatible,  that means you can run your Qt 4.8 applications, But that doesn't mean they will have the best performance, sometimes it is better to do a porting to use the newest features. Qt5, has two options to paint components into the screen. Painting in Qt 5 is primarily done either with: The imperative QPainter API Qt’s declarative UI language, QML, and its scene graph back-end. QPainter As this document mentions  Qt5GraphicsOverview | Qt Wiki | Qt Project  The Qpainter engine uses software to paint, and is used when drawing Qimages or Qwidgets. Its  advantage over OpenGL is the high quality when antialiasing is enabled, and a complete feature set. The Qpainter can use an OpenGL engine, but as the document mentions it is more suceptible to state changes. And has to be used carefully. QML & Scene Graph. All visual QML items are rendered using the scene graph, a low-level, high-performance rendering stack, closely tied to OpenGL. Qt Quick 2 makes use of a dedicated scene graph based on OpenGL ES 2.0 or OpenGL 2.0 for its rendering. Using a scene graph for graphics rather than the traditional imperative painting systems (QPainter and similar), means the scene to be rendered can be retained between frames and the complete set of primitives to render is known before rendering starts. This opens up for a number of optimizations, such as batch rendering to minimize state changes and discarding obscured primitives. The QML scene graph is a new back-end for QML in Qt 5, and is based on OpenGL. It generally improves the performance of QML significantly over the QPainter-based back-end used in Qt 4. It achieves better performance in a number of ways: The scene graph uses OpenGL directly instead of going though a QPainter which could be using either the raster or OpenGL paint engine. This means that all the resources, like geometry, textures and shaders can be stored in a format suitable for OpenGL rather than using classes such as QPainterPath, QPixmap, QBrush, or QPen, which the QPainter would need to translate into OpenGL primitives and possibly cache. QML, being a declarative language, defines how the end result should look like, but it doesn’t define how and in which order each individual element is drawn. The drawing can therefore be reordered to reduce the number of state changes, or merged to reduce the number of draw calls. The scene graph uses a separate render thread, and synchronizes the animations with the vertical retrace on platforms where this can be supported. The render thread allows the preparation of the next frame to be done at the same time the current frame is being rendered. This has a positive effect also on single-core systems, since the render thread might block on OpenGL commands. The synchronization with the vertical retrace improves the perceived smoothness of the animations. We have tested on i.MX6 Both options, having the best results using QML Qtquick2 elements. When we tried using QtPainter via Widgets we face the problem that if not using a windowing system like X11 or Wayland the painter wont work well and will only show the QtGLWidget. With QML scene graph we are able to have an OpenGL element and a Qt element on the same environment, and there is an easy way to communicate one with the other and share variables.  Please look at the example results here: I.MX6 scene graph Qt5 - YouTube And the great advantage, the sceneGraph is all accelerated via OpenGL.
查看全文
The i.MX 6 Android 13.4.1.03 patch release is now available on www.freescale.com IMX6_R13.4103_ANDROID_LDO_PATCH This patch release is based on the i.MX6 Android R13.4.1 release. The purpose of this patch release is to manage the LDO and PMIC ramp-up time correctly.
查看全文
i.MX25 for Industrial and General Embedded The i.MX25 family of multimedia applications processors extends the Freescale ARM9™ portfolio and makes the industrial and general embedded market a key focus of i.MX with the integration of many new features. Speed up to 400 MHz, low power consumption and multiple connectivity options support the growing needs of industrial and general embedded products, while allowing customers to reduce their overall system bill of materials cost. The i.MX258 processor provides additional security features making it the ideal solution for payment terminal (POS), or any other type of product needing secure system boot and tamper detection. i.MX25 for Automotive Today's drivers expect more connectivity in more places from more things—phones, media players and, increasingly, cars. Bluetooth™ connectivity is becoming the norm as more people keep their hands on the wheel instead of on the phone. Connectivity and compatibility with media players is becoming a requirement as consumers' media investment goes digital. The challenge: how can designers support high-end features such as connectivity and media playback without charging high-end prices? The i.MX25 family of processors offers integration that tailors itself to the connectivity requirements of today's automobile but eliminates expensive parts not needed for a cost-conscious infotainment system. The i.MX25 applications processor is a Freescale Energy-Efficient Solutions product. Product Information on Freescale.com i.MX257: Multimedia Applications Processor i.MX251: Multimedia Applications Processor i.MX253: Multimedia Applications Processor i.MX255: Multimedia Applications Processor i.MX258: Multimedia Applications Processor Additional Resources i.MX25 PDK Board I.MX25 PDK Board Get Started i.MX25 PDK Board Flashing NAND i.MX25 PDK Board Flashing SPI NOR i.MX25 PDK Board Flashing SD Card i.MX25 PDK Board Running Linux I.MX25 PDK U-boot SplashScreen I.MX25 PDK U-boot SDCard I.MX25 PDK Using FEC i.MX25: When using 120MHz UPLL as clock source, GPT counter returns unexpected results Limitations of the i.MX SIM Controller to Pass the EMV Certification
查看全文
Summary of the Issue: We have had customers reporting failure to run MC and SC production parts at 1GHz or higher frequencies. The signature of the fail is that the system will hang once it tries to ramp from the boot frequency of 800MHz to 1GHz or higher. The root cause was tracked to the setting of the LDO_VOLT_CHANGE_EN fuse in production parts. The LDO_VOLT_CHANGE_EN fuse sets the LDO boot voltage to either 1.15V (indicated by a fuse setting of “1”) or 1.1V  (indicated by a fuse setting of “0”). In production parts the fuse is set to “1”, i.e. 1.15V, since this is the optimal setting based on characterization data. On pre-production units the LDO voltage was set to the lower setting of 1.1V (i.e. fuse set to “0”). The reason this is a problem with MC/SC parts is because the fuse is read by the ROM during boot and overwrites the LDO ramp rate bits in the PMU_MISC2 register based on the setting of the fuse. When the LDO_VOLT_CHANG_EN fuse is set to “1” then the LDO ramp up time to spec voltage is set (in PMU_MISC2) to 500uS instead of the 50uS assumed by the CPUFreq driver. This will cause the system to hang when transitioning from the boot frequency to a higher frequency/voltage point since the required voltage to support the higher frequency is not yet present. In real terms, customers who have production i.MX 6Quad/6Dual/6DualLite and 6 Solo parts have seen failures to ramp their products to 1GHz or higher frequencies. This is completely fixed by a software patch that corrects the LDO ramp setting in the PMU_MISC_2 register by setting it back to the fastest ramp time. Note that the LDO_VOLT_CHANGE_EN fuse is not in the reference manual since it is not a customer visible fuse. It is programmed and locked at final test. This is a mandatory fix for all customers. Affected Parts: i.MX 6Quad – all SC and MC parts, consumer and automotive. Industrial MC parts not yet shipping. i.MX 6Dual – all SC and MC parts, consumer and automotive. Industrial MC parts not yet shipping. i.MX 6DualLite – all MC parts consumer parts. Automotive and industrial MC parts not yet shipping. i.MX 6Solo – all MC consumer parts. Automotive and industrial MC parts not yet shipping. Patch Availability and Location: Patches exist for both Linux and Android. They are available on freescale.com. See below for more details. i.MX 6Quad – www.freescale.com/imx6q i.MX 6Dual – www.freescale.com/imx6d i.MX 6DualLite – www.freescale.com/imx6dl  i.MX 6Solo – www.freescale.com/imx6s Select the “Software and Tools” tab and then expand the section “Updates and Patches”.  The relevant patches are: Linux – L3.0.35_1.1.1_LDO_PATCH (i.MX 6Quad/6Dual) Linux – L3.0.35_3.0.3_LDO_PATCH (i.MX 6DualLite/6Solo) Android – IMX6_R13.4103_ANDROID_LDO_PATCH (i.MX 6Quad/6Dual/6DualLite/6Solo) Communication Roll-out: i.MX FAE’s: done (via maillist). Will post copy of this email to i.MX support space by end of day 1 st March. i.MX DFAE’s: 8 th March. Customer notification: 8 th March. i.MX community: 8 th March (to coincide with customer notification). We are also working on an engineering bulletin that describes the change for customers who are not using our provided Linux and Android BSP’s. Target date: TBD. But goal is to make this available on/around mid-March. Best regards, Amanda and Kyle This document was generated from the following discussion: i.MX 6 Series LDO Ramp Issue: Linux and Android Patches Now Available
查看全文
In an earlier topic (Linux fast boot on i.MX6 Sabresd board.) about Linux fast boot on i.MX6 SabreSD board, the demo showed an application startup procedure including u-boot boot, Linux kernel boot, rootfs mount, demo application load and run. Additionally, this demo shows a live video on a LVDS screen from board CSI camera. Its total boot up time is about 1.x seconds. Now, based on Linux fast boot, we integrate it with another demo application: surround view, this demo shows 4 different live videos on LVDS screen from 4 UDP data sockets. In this demo video is drawn by GPU to screen, that means the frame buffers decode by video decoder directly pass to GPU, which is not same as previous demo. The encode video format is also MJPEG in this demo. This demo creates 4 different threads every thread handle one UDP socket, receive buffer, push this buffer to video decoder, get frame buffer from video decoder, pass this buffer to GPU, start GPU render, command GPU draw the render buffer to the screen; this thread needs to occupy one ARM processor to show every video smoothly. So we need a i.MX 6DQ board in this demo. Hardware: i.MX 6DQ SabreSD board Software: 12.09 GA BSP Difference with previous fast boot demo: U-boot difference with previous fast boot demo. 1: Add logo show. (For remove CSI2, V4L2, Capture modules ) Kernel different with previous fast boot demo. 1: Add SMP support. 2: Add Network support. (IPV4, PHY, network driver(FEC)) 3: Remove CSI2, V4L2, Capture. (Remove this need in U-boot procedure Freescale logo show on the screen! ) 4: Add GPU support in kernel. Rootfs difference with previous fast boot demo: 1: Keep rc.s firstly run, while in previous fast boot demo, demo is the firstly running program on rootfs. 2: Get rid of almost all service in rc.conf just keep “mount /proc and /sys” service. Network performance on this demo Software : The default network receive buffer is about 128KB. This default size is too small for this demo; the demo application can't fetch receive buffer in time while kernel network stack will discard some UDP packets if we don't enlarge it. We enlarge this receive buffer through command in inittab before demo running. Hardware: i.MX6 DQ TOI less than 1.2 version has some Ethernet mac layer issue, this issue will also cause some UDP packets lost. So please ensure the SabreSD board i.MX6 DQ chip TOI version is equal 1.2 or more. Attached are some files for your reference. Below patches assume this SabreSD board boot from SD3 and default display port is LVDS1. 1: U-boot and kernel patches based on 12.09. 2: Demo application based on 12.09 vpu test program and vpu test program running configure file. 3: Rootfs startup scripts.
查看全文
These questions and answers are about interrupt generation at a dedicated (configurable) video output port. The i.MX6D manual (Rev. 0) Image Processing Unit (IPU) chapter mentions: Every DI has 10 timing generator counters. The IPU Interrupt Generator has 10 DI0 counters (1...10) and just 2 DI1 counters (3 & 😎 as interrupt sources. The Interrupt Control Register lists 11 DI0 counters (0...10) Q1. Are the DI timing-generator counters linked to the counters in the interrupt controller, or are they different counters? A1. Yes, the DI timing generator counters are linked to the counters in the interrupt controller. Q2. Why are there 11 counters listed in the interrupt controller, but just 10 counters in the timing generator? A2. There is disp_clk_en_pre in the interrupt controller. Thus the 11 counters: 10 timing generator counters and 1 disp clock generator counter. Q3. Is configurable timing feasible for DI0 by using the timing generator counters? A3. Yes, using the 10 internal timing counters you can generate various timing relationships. In addition, you can detect any of the interrupt counters. For example, if you use counter 8, then you can detect the interrupt associated with counter 8. Q4. Explain the impact of the DI1 counter access of only channels 3 and 8. A4. DI1 also has 10 timing generator counters and 1 disp clock generator counter, which you can use to generate desired waveforms. This is similar to DI0. The difference is only 2 of the 10 counters (plus another disp_clk) are connected to the interrupt controller for DI1. Therefore, there is a restriction for detection. If you use counter 7, read out the counter 7 interrupt of DI1 is not possible. However, 2 channels should be sufficient. These interrupts are usually used to indicate a frame start or a frame end. We usually use counter 3 to represent Vsync. So normally we only use counter 3 interrupt. DI1 has only 3 accesses because this covers the anticipated use case and the desire was to restrict register size. The extra counters facilitate flexible DI1 timing generation.
查看全文
Product Family Features Freescale's i.MX family of applications processors has demonstrated leadership in the portable handheld market. The i.MX21 multimedia applications processor is the latest addition to this family and builds on its low-power, high-performance heritage. Freescale has shipped more than 60 million chips of our industry-founding applications processors. That means you can start smart by picking products with a technology pedigree to handle all the creativity you can pump into them. The i.MX21 features the advanced and power-efficient ARM926EJ-S core operating at speeds starting at 266 MHz and is part of a growing family of Smart Speed products that offer high performance processing optimized for lowest power consumption. ARM926EJ-S™ core (16 KB I-Cache, 16 KB D-Cache) Smart Speed Switch 16/18-bit color LCD controller up to SVGA USB On-The-Go (two-host port) MPEG-4 and H.263 encode/decode acceleration up to CIF 30 fps Additional Resources IMX21-ADS I.MX21 ADS Board Flashing IMX21-and-iMXL-Lite-Kit
查看全文
Linphone is an internet phone or Voice Over IP phone (VoIP). With Linphone you can communicate freely with people over the internet, with voice, video, and text instant messaging. Linphone makes use of the SIP protocol, an open standard for internet telephony. You can use Linphone with any SIP VoIP operator, including our free SIP audio/video service. Linphone is free software (or open-source), you can download and redistribute it freely. Linphone is available for desktop computers: Linux, Windows, Mac OSX, and for mobile phones: Android, iPhone, Blackberry. Linphone-android is a good example to show the integration of Java code based on Android SDK with native CODEC, network protocols. Not like XBMC-Android that is almost total c++/c project. Perform the following steps to build a linphone-android project: 1. git clone git://git.linphone.org/linphone-android.git --recursive 2. sudo apt-get install autoconf automake libtool pkg-config 3. "cd" to the root of "git clone" : cd /home/user/linphne-android // wherver git'ed linphone-android is 4. export PATH=/home/user/android-ndk:$PATH //wherever your android-ndk, android-sdk tools, and platform-tools, and ANT are stored in.             For example on my PC.      export PATH=/home/alanz/android-ndk-r8d:/home/alanz/android-sdk-linux/tools:/home/alanz/android-sdk-linux/platform-     tools:/home/alanz/bin/apache-ant-1.8.4/bin:$PATH             Note: PATH contains the ndk, sdk, and ant. 5. Make sure the network is working, then execute "./prepare_sources.sh" at the linphone-android root 6. Then, execute "/home/alanz/android-ndk-r8d/ndk-build", it will take a while to be finished 7. Modify Makefile as following example, modify it accordingly.      NDK_PATH=/home/alanz/android-ndk-r8d      SDK_PATH=/home/alanz/android-sdk-linux/tools      SDK_PLATFORM_TOOLS_PATH=/home/alanz/android-sdk-linux/platform-tools      .....................      generate-libs:           $(NDK_PATH)/ndk-build ....... (remove -j$(NUMCPUS) by the end of this command line) 8. execute "make", after finish, the apk file can be found under bin/ subdirectory.
查看全文
Documents Imx53-fastboot-example i.MX53 Multimedia Applications Processors I.MX53 QSB Board Get Started IMX53 QSB enable WIFI android I.MX53 QSB Ubuntu Dual Display i.MX53 Quick Start Board IMX53 SABRE AI i.MX53 Start-R Lab Exercise - Prof. Massimo Violante Politecnico of Torino i.MX53 Start-R Lab Exercise - Developing a loadable kernel module to manage GPIOs in i.MX53QSB ConnectCore® i.MX53 / Wi-i.MX53 by Digi International NOVPEK i.MX53 by NovTech
查看全文
The SNVS LDO output (VDD_SNVS_CAP) requires an external capacitor. Freescale's updated recommendation is that this should be a single 0.22 uF capacitor. Freescale is working to get documents in alignment. As of Feb 2013, some documents (such as schematics or user guides) show a single 0.22 uF capacitor, others do not.
查看全文
Make boot SD Card for imx-android-r13.4-20121128 1. Extract imx-android-r13.4-20121128 2. Check mount device  @Disk Util     My case SD Card : /dev/sdb 3. Insert the uSD Card    Use 16GByte SD Card Cat10 4. Android/imx-android-r13.4-20121128$./device/boundary/mksdcard.sh /dev/sdb 5. Wait about 5 minutes. Finish!
查看全文
The new i.MX 6 Platform SDK 1.1 release is now available on the http://www.freescale.com/ site. NOTICE: The Platform SDK is no longer available and is unsupported. Please contact your Sales team for assistance. ·      Files available i.MX 6Series Platform SDK Bare-metal SDK for the i.MX 6 series, including reusable drivers and tests for many peripherals, and much example code. Also includes register definition headers files, and register definitions for debuggers. BSD open source license. New features and fixes - Fixed EIM test failure on sabre_ai board. - Added obds application. - Improved FAT filesystem cache. - Improved uSDHC API to allow access to entire 4GB card. - Added stream benchmark application. - Moved filesystem read/write performance test to be a new app. - New cpu_workpoint API in sdk/drivers/cpu_utility. - Improved menu API in sdk/utility/menu.h. - Fixed bug in D-cache invalidate and clean routines. - If an application returns from main(), _sys_exit() will now be called automatically. - Fixed a DDR region overflow linker error when using version 4.5.2 of the toolchain. - Removed smbus driver, as no i.MX6 boards have compatible devices and thus was untested. - Improved GIC driver by making it easier to init with new gic_init() API. - Implemented support for CSI test mode. - Converted SATA driver to use standard register definition macros. - Improvements to PWM driver. - Completely removed use of hw_module_t struct throughout SDK. Driver APIs that previously used this struct have been updated to take the relevant parameters, such as the peripheral instance, directly. Affected drivers: i2c, epit, uart, snvs, gpt, timer, flexcan. - The SDK build system now supports parallel builds. - Added jump_to_sdp() API in system_util.h to enter ROM Serial Download Protocol mode. - Static initialization of C++ objects now works as expected. - Fixed BCH ECC encoded reads and writes in GPMI driver. - Updated DCDs and debugger init scripts to the most recent versions. - Added GpioPin class in gpio driver. See sdk/drivers/gpio/gpio_pin.h. - Added classes for I2C and SPI devices. See sdk/drivers/i2c/i2c_device.h and sdk/drivers/spi/spi_device.h. - Added class to provide a software I2C port. See sdk/drivers/i2c/software_i2c_port.h. - Added gpio_set_gpio() API to gpio driver which configures the pin mux for a GPIO pin. - Added lwIP open source TCP/IP stack to the SDK. - Added two demo applications for lwIP: ping and httpd. - Implemented some minor improvements to ENET and FEC driver APIs. - Changed ENET driver so that it no longer puts the PHY into external loopback mode. A new API is added to enable loopback for the ENET unit test. - Added set_card_access_mode() API to uSDHC driver to replace some global variables that were used to configure DMA and interrupt mode. - Added read_input_string() and read_int() APIs to system_util.h. - Fixed ESAI driver so that it no longer always outputs each sample 3 times. - New arm_set_interrupt_state() API in cortex_a9.h. - Versions of all debugger init scripts are now provided for ARM DS-5. - Fixed a compiler warning generated by gcc 4.7.2 in the gpmi driver. - New version 3.4.0.4 of the IOMux Tool. - New driver for the MMA8451 accelerometer. - Added a full-featured USB Device stack under sdk/common/usb_stack. - Normalized line ending style to Unix (LF) for a few source files. - Created new APIs to manage starting up and shutting down secondary CPU cores. See cpu_start_secondary() and cpu_disable() in sdk/drivers/cpu_utility/cpu_utility.h. - Converted the multicore_demo application to a unit test under sdk/drivers/cpu_utility/test. - Added smp_primes multicore example application. - Improved spinlock API to work correctly in SMP situations. - Many small changes and improvements. - The startup code leaves interrupts disabled, and platform_init() now explicitly enables them. - Added readme files for all applications. - Changed how the makefiles archive objects in .a libraries. The timestamps of objects are compared with their copies in the archive, rather than being compared with the timestamps of the archive itself. This is to work around certain older Linux systems that do not save fractions of a second in file timestamps. One side effect of this is that the ar tool is invoked once per object that needs updating, where previously it was invoked to update a number of files at once. To reduce build log clutter, the archive messages are no longer shown.
查看全文
Boundary Devices has a tool to load directly a U-boot binary file, all using the USB OTG port. Assuming that you have connected your i.MX board to your Linux Host through an USB cable, board is power-on  with dip switches configure to 'Serial Download Mode' (this configuration depends on the board you are booting),  clone the imx_usb_loader repo, generate the tool then boot as indicate below: $ git clone https://github.com/boundarydevices/imx_usb_loader.git $ cd imx_usb_loader $ make $ ./ imx_usb   ../ tmp/deploy/images/ u-boot.imx On the console terminal, you should see the booting kernel logs and at the end reaching the login prompt. Useful Links: [1] Unbricking a Nitrogen6X or Sabre Lite i.MX6 board [2] Boundary Devices Repos [3] Boundary Devices Main page
查看全文