i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
The new i.MX OTP Tools release is now available on http://www.freescale.com/, under this link. Change details: Fixes an issue with the rom-plugin device firmware that is used by BitBurner and otp_burner tools to program fuses. These tools are part of IMX_OTP_TOOLS package.    The plugin was failing to check the status whether the data packets have been received or not.    As such, at times before receiving data from host the firmware was processing the usb buffer    with previously sent or received data resulting in incorrect values being programmed. To fix    this issue we modified the firmware to make sure we receive the data before processing the usb buffer.                 Here is the sequence of usb transfers (protocol):                 1.            Cmd-phase: Host send cmd to write to otp register with cmd type, register index and number of registers to write                 2.            Data-phase: Host send data for values to write to otp register.                 3.            Status-phase: Device sends status to host                 4.            Cmd-phase: Host send cmd to read otp register to verify data written was correct                 5.            Data-phase: Device send data from otp registers                 6.            Status-phase: Device sends status to host   The problem was at #2 wherein device would process usb buffer before confirming whether data has received or not.
記事全体を表示
Dear IMX community, We usingiMX6 Quad processor and run Android 13.4, After below log file and android handup, We also run DDR stress test without problems found, Can anyone give a suggestions on this issue Best Regards, Jim ================================ U-Boot 2009.08-00008-g5f5b708-dirty (Mar 18 2013 - 17:23:58) CPU: Freescale i.MX6 family TO1.2 at 792 MHz Temperature:   52 C, calibration data 0x5b051d69 mx6q pll1: 792MHz mx6q pll2: 528MHz mx6q pll3: 480MHz mx6q pll8: 50MHz ipg clock     : 66000000Hz ipg per clock : 66000000Hz uart clock    : 80000000Hz cspi clock    : 60000000Hz ahb clock     : 132000000Hz axi clock   : 264000000Hz emi_slow clock: 29333333Hz ddr clock     : 528000000Hz usdhc1 clock  : 198000000Hz usdhc2 clock  : 198000000Hz usdhc3 clock  : 198000000Hz usdhc4 clock  : 198000000Hz nfc clock     : 24000000Hz Board: MX6Q-SABRELITE:[ POR] Boot Device: I2C I2C:   ready DRAM:   1 GB MMC:   FSL_USDHC: 0,FSL_USDHC: 1 JEDEC ID: 0x20:0x20:0x16 *** Warning - bad CRC, using default environment In:    serial Out:   serial Err:   serial Net:   got MAC address from IIM: 00:00:00:00:00:00 FEC0 [PRIME] Hit any key to stop autoboot:  0 mmc0(part 0) is current device reading /6q_bootscript 353 bytes read ## Executing script at 10008000 reading uimage 4016476 bytes read reading uramdisk.img 212592 bytes read ## Booting kernel from Legacy Image at 10800000 ...    Image Name:   Linux-3.0.35    Image Type:   ARM Linux Kernel Image (uncompressed)    Data Size:    4016412 Bytes =  3.8 MB    Load Address: 10008000    Entry Point:  10008000    Verifying Checksum ... OK ## Loading init Ramdisk from Legacy Image at 12800000 ...    Image Name:   Android Root Filesystem    Image Type:   ARM Linux RAMDisk Image (uncompressed)    Data Size:    212528 Bytes = 207.5 kB    Load Address: 12800000    Entry Point:  12800000    Verifying Checksum ... OK    Loading Kernel Image ... OK OK Starting kernel ... Initializing cgroup subsys cpuset Initializing cgroup subsys cpu Linux version 3.0.35 (leo@pluto) (gcc version 4.6.2 20120613 (release) [ARM/embedded-4_6-bra                                 nch revision 188521] (GNU Tools for ARM Embedded Processors) ) #10 SMP PREEMPT Tue Mar 19 11                                 :34:02 CST 2013 CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine: Freescale i.MX 6Quad Sabre-Lite Board Memory policy: ECC disabled, Data cache writealloc CPU identified as i.MX6Q, silicon rev 1.2 PERCPU: Embedded 7 pages/cpu @c1119000 s5760 r8192 d14720 u32768 Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 210944 Kernel command line: arm_freq=1000 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 video=mxcfb1                                 :off console=ttymxc0,115200 init=/init rw no_console_suspend androidboot.console=ttymxc0 vma                                 lloc=400M PID hash table entries: 2048 (order: 1, 8192 bytes) Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) Memory: 576MB 256MB = 832MB total Memory: 833728k/833728k available, 214848k reserved, 442368K highmem Virtual kernel memory layout:     vector  : 0xffff0000 - 0xffff1000   (   4 kB)     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)     DMA     : 0xfbe00000 - 0xffe00000   (  64 MB)     vmalloc : 0xd9800000 - 0xf2000000   ( 392 MB)     lowmem  : 0xc0000000 - 0xd9000000   ( 400 MB)     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)     modules : 0xbf000000 - 0xbfe00000   (  14 MB)       .init : 0xc0008000 - 0xc0041000   ( 228 kB)       .text : 0xc0041000 - 0xc0770fb0   (7360 kB)       .data : 0xc0772000 - 0xc07e0da0   ( 444 kB)        .bss : 0xc07e0dc4 - 0xc090f7d0   (1211 kB) Preemptible hierarchical RCU implementation. NR_IRQS:496 MXC GPIO hardware sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms MXC_Early serial console at MMIO 0x2020000 (options '115200') bootconsole [ttymxc0] enabled Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 512 Initializing cgroup subsys cpuacct CPU: Testing write buffer coherency: ok hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available CPU1: Booted secondary processor CPU2: Booted secondary processor CPU3: Booted secondary processor Brought up 4 CPUs SMP: Total of 4 processors activated (6324.22 BogoMIPS). print_constraints: dummy: NET: Registered protocol family 16 print_constraints: vddpu: 725 <--> 1300 mV at 1150 mV fast normal print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal print_constraints: vdd3p0: 2800 <--> 3150 mV at 3000 mV fast normal ------------ Board type Sabre Lite Flexcan NXP tja1040 hw-breakpoint: found 6 breakpoint and 1 watchpoint registers. hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step. hw-breakpoint: maximum watchpoint size is 4 bytes. L310 cache controller enabled l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B IMX usb wakeup probe bio: create slab <bio-0> at 0 print_constraints: VDDA: 2500 mV print_constraints: VDDIO: 3300 mV machine_constraints_voltage: VDDD: unsupportable voltage constraints reg-fixed-voltage reg-fixed-voltage.2: Failed to register regulator: -22 reg-fixed-voltage: probe of reg-fixed-voltage.2 failed with error -22 print_constraints: vmmc: 3300 mV SCSI subsystem initialized spi_imx imx6q-ecspi.0: probed usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb Freescale USB OTG Driver loaded, $Revision: 1.55 $ add wake up source irq 75 i2c i2c-0: Invalid 7-bit I2C address 0x00 i2c i2c-0: Can't create device at 0x00 imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7) imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7) mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a MIPI CSI2 driver module loaded Advanced Linux Sound Architecture Driver Version 1.0.24. Bluetooth: Core ver 2.16 NET: Registered protocol family 31 Bluetooth: HCI device and connection manager initialized Bluetooth: HCI socket layer initialized Bluetooth: L2CAP socket layer initialized Bluetooth: SCO socket layer initialized i2c-core: driver [max17135] using legacy suspend method i2c-core: driver [max17135] using legacy resume method Switching to clocksource mxc_timer1 NET: Registered protocol family 2 IP route cache hash table entries: 16384 (order: 4, 65536 bytes) TCP established hash table entries: 65536 (order: 7, 524288 bytes) TCP bind hash table entries: 65536 (order: 7, 786432 bytes) TCP: Hash tables configured (established 65536 bind 65536) TCP reno registered UDP hash table entries: 256 (order: 1, 8192 bytes) UDP-Lite hash table entries: 256 (order: 1, 8192 bytes) NET: Registered protocol family 1 RPC: Registered named UNIX socket transport module. RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. Unpacking initramfs... Freeing initrd memory: 204K Static Power Management for Freescale i.MX6 wait mode is enabled for i.MX6 cpaddr = d9880000 suspend_iram_base=d98fc000 PM driver module loaded IMX usb wakeup probe i.MXC CPU frequency driver highmem bounce pool size: 64 pages ashmem: initialized JFFS2 version 2.2. (NAND) ? 2001-2006 Red Hat, Inc. msgmni has been set to 764 io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) MIPI DSI driver module loaded mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver hdmi mxc_hdmi mxc_hdmi: Detected HDMI controller 0x13:0xa:0xa0:0xc1 fbcvt: 1920x1080@60: CVT Name - 2.073M9 imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7) mxc_sdc_fb mxc_sdc_fb.1: Can't get fb option for mxcfb1! mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver ldb _regulator_get: get() with no identifier mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 0(VIC 16): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 1(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 2(VIC 1): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 3(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 4(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 5(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 6(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 7(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 8(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 9(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 10(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 11(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 12(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 13(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 14(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 15(VIC 0): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 16(VIC 16): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 18(VIC 1): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 19(VIC 2): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 20(VIC 3): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 21(VIC 4): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 22(VIC 31): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 23(VIC 19): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 24(VIC 17): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 25(VIC 18): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 29(VIC 16): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 30(VIC 3): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 31(VIC 4): mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 32(VIC 18): fbcvt: 1920x1080@60: CVT Name - 2.073M9 imx-sdma imx-sdma: loaded firmware 1.1 imx-sdma imx-sdma: initialized Serial: IMX driver imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX console [ttymxc0] enabled, bootconsole disabled console [ttymxc0] enabled, bootconsole disabled imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX loop: module loaded m25p80 spi0.0: m25p32 (4096 Kbytes) Creating 3 MTD partitions on "m25p80": 0x000000000000-0x0000000c0000 : "bootloader" 0x0000000c0000-0x0000000c2000 : "ubparams" mtd: partition "ubparams" doesn't end on an erase block -- force read-only 0x0000000c2000-0x000000400000 : "unused" mtd: partition "unused" doesn't start on an erase block boundary -- force read-only vcan: Virtual CAN interface driver CAN device driver interface flexcan netdevice driver flexcan imx6q-flexcan.0: device registered (reg_base=d9970000, irq=142) FEC Ethernet Driver fec_enet_mii_bus: probed PPP generic driver version 2.4.2 PPP Deflate Compression module registered PPP BSD Compression module registered PPP MPPE Compression module registered NET: Registered protocol family 24 PPTP driver version 0.8.5 tun: Universal TUN/TAP device driver, 1.6 tun: (C) 1999-2004 Max Krasnyansky <[email protected]> ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1 fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000 fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected add wake up source irq 72 fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2 fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200 fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00 hub 2-0:1.0: USB hub found hub 2-0:1.0: 1 port detected usbcore: registered new interface driver cdc_acm cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters Initializing USB Mass Storage driver... usbcore: registered new interface driver usb-storage USB Mass Storage support registered. usbcore: registered new interface driver usbserial usbserial: USB Serial Driver core USB Serial support registered for GSM modem (1-port) usbcore: registered new interface driver option option: v0.7.2:USB Driver for GSM modems USB Serial support registered for Qualcomm USB modem usbcore: registered new interface driver qcserial ARC USBOTG Device Controller driver (1 August 2005) android_usb gadget: Mass Storage Function, version: 2009/09/11 android_usb gadget: Number of LUNs=1 lun0: LUN: removable file: (no medium) Gadget Android: controller 'fsl-usb2-udc' not recognized android_usb gadget: android_usb ready Suspend udc for OTG auto detect fsl-usb2-udc: bind to driver android_usb mousedev: PS/2 mouse device common for all mice input: gpio-keys as /devices/platform/gpio-keys/input/input0 egalax_ts 2-0004: egalax_ts: failed to read firmware version egalax_ts: probe of 2-0004 failed with error -5 input: ak4183ts as /devices/platform/imx-i2c.1/i2c-1/1-0048/input/input1 i2c-core: driver [isl29023] using legacy suspend method i2c-core: driver [isl29023] using legacy resume method using rtc device, snvs_rtc, for alarms snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0 i2c /dev entries driver Linux video capture interface: v2.00 ov5640_read_reg:write reg error:reg=300a ov5640_probe:cannot find camera mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16 mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17 mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18 mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19 mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20 usbcore: registered new interface driver uvcvideo USB Video Class driver (v1.1.0) i2c-core: driver [mag3110] using legacy suspend method i2c-core: driver [mag3110] using legacy resume method usb 2-1: new high speed USB device number 2 using fsl-ehci imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1) device-mapper: uevent: version 1.0.3 device-mapper: ioctl: 4.20.0-ioctl (2011-02-02) initialised: [email protected] Bluetooth: Virtual HCI driver ver 1.3 Bluetooth: HCI UART driver ver 2.2 Bluetooth: HCIATH3K protocol initialized Bluetooth: Generic Bluetooth USB driver ver 0.6 usbcore: registered new interface driver btusb sdhci: Secure Digital Host Controller Interface driver sdhci: Copyright(c) Pierre Ossman mmc0: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA sdhci sdhci-esdhc-imx.3: no write-protect pin available! mmc1: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed VPU initialized mxc_asrc registered revserved_memory_account:viv_gpu registerd Thermal calibration data is 0x5b051d69 anatop_thermal_counting_ratio: raw25c=1456 raw_hot=1309 hot_temp=105 Anatop Thermal registered as thermal_zone0 anatop_thermal_probe: default cooling device is cpufreq! usbcore: registered new interface driver usbhid usbhid: USB HID core driver logger: created 256K log 'log_main' logger: created 256K log 'log_events' hub 2-1:1.0: USB hub found logger: created 256K log 'log_radio' logger: created 256K log 'log_system' usbcore: registered new interface driver snd-usb-audio mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio Cirrus Logic CS42888 ALSA SoC Codec Driver i2c-core: driver [cs42888] using legacy suspend method i2c-core: driver [cs42888] using legacy resume method hub 2-1:1.0: 4 ports detected mmc0: new high speed MMC card at address 0001 mmcblk0: mmc0:0001 eMMC   3.71 GiB mmcblk0boot0: mmc0:0001 eMMC   partition 1 2.00 MiB mmcblk0boot1: mmc0:0001 eMMC   partition 2 2.00 MiB mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4 mmcblk0boot1: unknown partition table mmcblk0boot0: unknown partition table asoc: sgtl5000 <-> imx-ssi.1 mapping ok imx_3stack asoc driver asoc: mxc-hdmi-soc <-> imx-hdmi-soc-dai.0 mapping ok ALSA device list:   #0: sgtl5000-audio   #1: imx-hdmi-soc Netfilter messages via NETLINK v0.30. nf_conntrack version 0.5.0 (13030 buckets, 52120 max) ctnetlink v0.93: registering with nfnetlink. NF_TPROXY: Transparent proxy support initialized, version 4.1.0 NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd. xt_time: kernel timezone is -0000 IPv4 over IPv4 tunneling driver GRE over IPv4 demultiplexor driver ip_tables: (C) 2000-2006 Netfilter Core Team arp_tables: (C) 2002 David S. Miller TCP cubic registered NET: Registered protocol family 10 ip6_tables: (C) 2000-2006 Netfilter Core Team IPv6 over IPv4 tunneling driver NET: Registered protocol family 17 NET: Registered protocol family 15 can: controller area network core (rev 20090105 abi 😎 NET: Registered protocol family 29 can: raw protocol (rev 20090105) can: broadcast manager protocol (rev 20090105 t) Bluetooth: RFCOMM TTY layer initialized Bluetooth: RFCOMM socket layer initialized Bluetooth: RFCOMM ver 1.11 Bluetooth: BNEP (Ethernet Emulation) ver 1.3 Bluetooth: BNEP filters: protocol multicast Bluetooth: HIDP (Human Interface Emulation) ver 1.2 L2TP core driver, V2.0 PPPoL2TP kernel driver, V2.0 L2TP IP encapsulation support (L2TPv3) L2TP netlink interface L2TP ethernet pseudowire support (L2TPv3) lib80211: common routines for IEEE802.11 drivers VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4 Bus freq driver module loaded Bus freq driver Enabled mxc_dvfs_core_probe DVFS driver module loaded regulator_init_complete: VDDIO: incomplete constraints, leaving on regulator_init_complete: VDDA: incomplete constraints, leaving on regulator_init_complete: vddpu: incomplete constraints, leaving on snvs_rtc snvs_rtc.0: setting system clock to 1970-01-02 00:04:27 UTC (86667) Freeing init memory: 228K usb 2-1.4: new low speed USB device number 3 using fsl-ehci init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead. input: HID 04d9:0499 as /devices/platform/fsl-ehci.1/usb2/2-1/2-1.4/2-1.4:1.0/input/input2 generic-usb 0003:04D9:0499.0001: input,hidraw0: USB HID v1.10 Mouse [HID 04d9:0499] on usb-f                                 sl-ehci.1-1.4/input0 EXT4-fs (mmcblk0p5): recovery complete EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: (null) EXT4-fs (mmcblk0p7): recovery complete EXT4-fs (mmcblk0p7): mounted filesystem with ordered data mode. Opts: noauto_da_alloc,errors                                 =panic EXT4-fs (mmcblk0p6): warning: mounting unchecked fs, running e2fsck is recommended EXT4-fs (mmcblk0p6): mounted filesystem without journal. Opts: (null) init: cannot find '/system/bin/gpu_init.sh', disabling 'gpu_init' init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery' android_usb: already disabled adb_open mtp_bind_config adb_bind_config warning: `rild' uses 32-bit capabilities (legacy support in use) root@android:/ # ERROR: v4l2 capture: slave not found! ERROR: v4l2 capture: slave not found! request_suspend_state: wakeup (3->0) at 20324699670 (1970-01-02 00:04:45.205101336 UTC) eth0: Freescale FEC PHY driver [Micrel KSZ9021 Gigabit PHY] (mii_bus:phy_addr=1:07, irq=284) ADDRCONF(NETDEV_UP): eth0: link is not ready acc_open acc_release PHY: 1:07 - Link is Up - 100/Full ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready CPU3: shutdown CPU2: shutdown Unable to handle kernel paging request at virtual address f40c4010 pgd = d3e04000 [f40c4010] *pgd=02011452(bad) Internal error: Oops: 2d [#1] PREEMPT SMP Modules linked in: CPU: 0    Not tainted  (3.0.35 #10) PC is at _clk_arm_get_rate+0xc/0x28 LR is at clk_get_rate+0x40/0x50 pc : [<c005ac7c>]    lr : [<c006650c>]    psr: a0000193 sp : d3e51db0  ip : c004c6b0  fp : d3ceae00 r10: 00100100  r9 : c111a588  r8 : 00200200 r7 : 010da000  r6 : 00000001  r5 : d6f15e8c  r4 : c07e1040 r3 : f40c4000  r2 : d3e51dd8  r1 : 00000000  r0 : c0790430 Flags: NzCv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment user Control: 10c53c7d  Table: 23e0404a  DAC: 00000015 PC: 0xc005abfc: abfc  1affffdc eaffffee c078f07c c07e1654 c078f0d0 e92d4010 e59f304c e5900028 ac1c  e1500003 0a000007 e59f3040 e1500003 13a04001 0a000003 eb002e24 e1a01004 ac3c  eb076b36 e8bd8010 e3a03901 e34f340c e5934014 eb002e1d e7e24dd4 e2844001 ac5c  e1a01004 eb076b2d e8bd8010 c078f124 c078e260 e3a03901 e34f240c e92d4010 ac7c  e5934010 e5900028 eb002e10 e2041007 e2811001 eb076b21 e8bd8010 e92d4038 ac9c  e1a05001 e5900028 eb002e08 e1a01005 e1a04000 eb076b19 e2501000 03a01001 acbc  0a000001 e3510040 23a01040 e1a00004 eb076b12 e8bd8038 e92d40f8 e1a05001 acdc  e5900028 eb002df9 e1a01005 e1a07000 eb076b0a e2504000 01a06004 03a04001 LR: 0xc006648c: 648c  c07e1684 c0574908 c06a6f80 e59f3010 e3500000 e593000c 1a000000 ea000167 64ac  ea000189 c07e15fc e3500000 012fff1e e3700a01 91d003d0 83a00000 e12fff1e 64cc  e3500000 e92d4008 08bd8008 e3700a01 83a00000 9a000005 e8bd8008 e5900028 64ec  e3500000 0a000006 e3700a01 8a000005 e590303c e3530000 0afffff7 e12fff33 650c  e8bd8008 e8bd8008 e3a00000 e8bd8008 e92d4008 e2503000 01a00003 08bd8008 652c  e3730a01 83a00000 88bd8008 e5933044 e3530000 0a000001 e12fff33 e8bd8008 654c  e1a00003 e8bd8008 e3500000 012fff1e e3700a01 95900028 83a00000 e12fff1e 656c  e3500000 e92d4010 e1a04001 1a000003 ea00000d e5900028 e3500000 0a00000a SP: 0xd3e51d30: 1d30  c111a040 c1119040 00000006 00000003 00000006 c1119040 00000000 393f7476 1d50  00000006 0000040f 0000000d 00000001 010da000 c00469d0 c0790430 00000000 1d70  d3e51dd8 f40c4000 c07e1040 d6f15e8c 00000001 010da000 00200200 c111a588 1d90  00100100 d3ceae00 c004c6b0 d3e51db0 c006650c c005ac7c a0000193 ffffffff 1db0  c07e1040 c006650c c0059e84 c0059e90 c0059e84 c006650c c004c6d8 c004c6ec 1dd0  d3e51dd8 c00a799c d3e51dd8 d3e51dd8 c0783cd0 d3e50000 c003fc18 00000000 1df0  00000000 d3e51e20 d6085a00 c00412c0 ffffffff f2a00100 00000405 00000001 1e10  00000000 d3e50000 d6085a00 c0046a4c 00000000 010da000 00000000 d3e50000 IP: 0xc004c630: c630  e59f3018 e1a0000c e5933004 e12fff33 e28dd014 e8bd8000 c078b1c8 c004c16c c650  c0783a2c e3510003 e1a0c00d e3cc2d7f 93a03000 83a03001 e3510001 03833001 c670  e3c2203f e3530000 e5922014 1a000009 e3520003 ca000007 e2822008 e7d0c002 c690  e20cc0fc e18c1001 e6ef1071 e7c01002 e1a00003 e12fff1e e3e03015 eafffffb c6b0  e3013040 e34c307e e1a01000 e3a00000 e5933000 e5932008 e5831004 e3822001 c6d0  e5832008 e12fff1e e92d4010 e3014040 e34c407e e5940004 eb006777 e1a0300d c6f0  e3c3cd7f e3032cd0 e3ccc03f e34c2078 e594300c e59cc014 e792210c e1a01000 c710  e5840008 e7930002 e8bd4010 ea015288 e59f304c e593000c e3500000 012fff1e FP: 0xd3cead80: ad80  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 ada0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 adc0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 ade0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 ae00  c10d5580 00000001 00000000 00000000 00000000 00000000 c10d5580 00000001 ae20  00000000 00000000 00000000 00000000 c10d5580 00000001 00000000 00000000 ae40  00000000 00000000 c10d5580 00000001 00000000 00000000 00000000 00000000 ae60  c10d5580 00000001 00000000 00000000 00000000 00000000 c10d5580 00000001 R0: 0xc07903b0: 03b0  c06a7998 c078f9ac c07903cc c07903a4 c06a79a4 c06a9e14 c0791738 c07903e0 03d0  c07903b8 c06a79b4 c06a9e14 c079178c c07903f4 c07903cc c06a79c4 c06a9e14 03f0  c07917e0 c0790408 c07903e0 00000000 c06a79d4 c07906d0 c079041c c07903f4 0410  00000000 c06a79e0 c078f568 c07cd698 c0790408 00000000 c06a79ec c078f5bc 0430  5f757063 006b6c63 00000000 00000000 00000000 00000000 00000000 00000000 0450  d40a0228 00000000 c078f4c0 00000000 00000001 00000000 00000000 c005ac70 0470  c005bc28 00000000 00000000 00000000 00000000 61746173 6b6c635f 00000000 0490  00000000 00000000 00000000 00000000 00000000 d4044aa8 00000000 c078f370 R2: 0xd3e51d58: 1d58  0000000d 00000001 010da000 c00469d0 c0790430 00000000 d3e51dd8 f40c4000 1d78  c07e1040 d6f15e8c 00000001 010da000 00200200 c111a588 00100100 d3ceae00 1d98  c004c6b0 d3e51db0 c006650c c005ac7c a0000193 ffffffff c07e1040 c006650c 1db8  c0059e84 c0059e90 c0059e84 c006650c c004c6d8 c004c6ec d3e51dd8 c00a799c 1dd8  d3e51dd8 d3e51dd8 c0783cd0 d3e50000 c003fc18 00000000 00000000 d3e51e20 1df8  d6085a00 c00412c0 ffffffff f2a00100 00000405 00000001 00000000 d3e50000 1e18  d6085a00 c0046a4c 00000000 010da000 00000000 d3e50000 d67c9c60 0000002a 1e38  00000001 00000001 c10d5580 00000000 d6085a00 d3ceae00 00000000 d3e51e68 R3: 0xf40c3f80: 3f80  ******** ******** ******** ******** ******** ******** ******** ******** 3fa0  ******** ******** ******** ******** ******** ******** ******** ******** 3fc0  ******** ******** ******** ******** ******** ******** ******** ******** 3fe0  ******** ******** ******** ******** ******** ******** ******** ******** 4000  ******** ******** ******** ******** ******** ******** ******** ******** 4020  ******** ******** ******** ******** ******** ******** ******** ******** 4040  ******** ******** ******** ******** ******** ******** ******** ******** 4060  ******** ******** ******** ******** ******** ******** ******** ******** R4: 0xc07e0fc0: 0fc0  412fc09a 00000000 00000000 00000000 00000000 00000000 00000000 00000000 0fe0  c07a0b20 c07ccc64 00000000 00000000 00000000 c0798518 00000001 00000000 1000  00000001 00000000 00000000 d8fff000 00000000 c0067230 c00542e0 00000000 1020  10004000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 1040  d9800600 c0790874 0bcd3d80 c0043028 00000000 00000000 00030000 00000005 1060  00000001 00000001 00000004 00000000 00000000 c078c518 00000000 00000000 1080  00000000 00000000 00000000 d60e8000 d60e9000 d60ea000 d60eb000 d60ec000 10a0  d60ed000 d60ee000 d60ef000 d60f0000 d60f1000 d60f2000 d60f3000 d60f4000 R5: 0xd6f15e0c: 5e0c  00000002 00000001 c0046a4c c0574e78 00000005 f2a01000 00000001 d6f15e8c 5e2c  c111a580 00000000 c111a580 010da000 c111a588 00000001 c0574f04 00000000 5e4c  d6f15e60 c004bbac c00a708c 20000113 ffffffff d6f14000 00000000 c004c6d8 5e6c  00000001 c0574f00 c0783cd0 d6f15f3c c00a71c0 c0041eb0 d6134600 80002001 5e8c  00100100 00200200 c004c6d8 00000000 00000001 00018d00 ffffffff c07ccdcc 5eac  00000000 d6f15f3c 00000001 d6f15f3c c004c850 c004c808 c0098c2c c07ff7fc 5ecc  c07ff7e4 00000000 00000001 ffffffff c0098d80 00000000 001312d0 00000000 5eec  d6f15f3c d63128e0 00000000 c0783ac4 00000004 c0783b00 c0098db4 00000000 R9: 0xc111a508: a508  00008288 00000000 2b85e900 00000006 00000000 00000000 0008f4da 00000000 a528  ffff968e ffffffe5 d6f93800 00000000 00000000 00000000 00000000 00000000 a548  00000000 00000000 00000000 00000000 00000000 00000000 c07740e0 00200200 a568  c00972ac 00000000 00000000 00000000 00000000 00000000 c111a580 c111a580 a588  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 a5a8  00000000 00000000 00000000 00000000 00000000 00000000 00000000 c111a5c0 a5c8  c111a5c8 c111a5c8 00000000 c111a5d4 c111a5d4 00000000 00000000 00000000 a5e8  00000084 00000000 00000000 00000000 00000000 00000000 00000000 00000000 Process WindowManagerPo (pid: 2301, stack limit = 0xd3e502f0) Stack: (0xd3e51db0 to 0xd3e52000) 1da0:                                     c07e1040 c006650c c0059e84 c0059e90 1dc0: c0059e84 c006650c c004c6d8 c004c6ec d3e51dd8 c00a799c d3e51dd8 d3e51dd8 1de0: c0783cd0 d3e50000 c003fc18 00000000 00000000 d3e51e20 d6085a00 c00412c0 1e00: ffffffff f2a00100 00000405 00000001 00000000 d3e50000 d6085a00 c0046a4c 1e20: 00000000 010da000 00000000 d3e50000 d67c9c60 0000002a 00000001 00000001 1e40: c10d5580 00000000 d6085a00 d3ceae00 00000000 d3e51e68 c0103478 c0114ba8 1e60: 60000013 ffffffff c0103478 c0114b38 60000013 c0103478 00000000 00000001 1e80: d3e51f40 00000001 00000001 0000000e d3e50000 d4288e7c ffffffff fffffdee 1ea0: d6085a00 00000000 00000000 d3e51f80 d3e50000 00000000 5c66e6f4 c00fb338 1ec0: 00000000 00000000 d61e0f8c 00000000 00000000 00000001 ffffffff d6085a00 1ee0: 00000000 00000000 00000000 00000000 d6f93be0 c0047184 00000000 00000000 1f00: 00000000 00000000 d3e51f08 d3e51f08 00000001 d3e50000 00000001 d624ea48 1f20: d6ee11a0 00000001 00000001 00000000 00000000 00000000 5eacafff d624ea48 1f40: 4007a0e4 00000000 d6085a00 00000001 4007a0e3 d3e51f80 00000001 c00fba3c 1f60: 00000000 c00fd050 d6085a00 4007a0e3 00000000 00000000 00000001 c00fbcac 1f80: 00000000 00000000 006ae0fc 00000001 4007a0e3 006ae0e8 00000000 00000004 1fa0: c0047184 c0047000 4007a0e3 006ae0e8 0000005d 4007a0e3 00000001 5bc63d90 1fc0: 4007a0e3 006ae0e8 00000000 00000004 5c66e6e0 5bc63d38 00000000 5c66e6f4 1fe0: 4007d058 5c66e6b8 40075d1b 400c5474 20000010 0000005d 00000000 00000000 [<c005ac7c>] (_clk_arm_get_rate+0xc/0x28) from [<c006650c>] (clk_get_rate+0x40/0x50) [<c006650c>] (clk_get_rate+0x40/0x50) from [<c0059e90>] (_clk_twd_get_rate+0xc/0x14) [<c0059e90>] (_clk_twd_get_rate+0xc/0x14) from [<c006650c>] (clk_get_rate+0x40/0x50) [<c006650c>] (clk_get_rate+0x40/0x50) from [<c004c6ec>] (twd_update_frequency+0x14/0x48) [<c004c6ec>] (twd_update_frequency+0x14/0x48) from [<c00a799c>] (generic_smp_call_function_s                                 ingle_interrupt+0xd0/0x130) [<c00a799c>] (generic_smp_call_function_single_interrupt+0xd0/0x130) from [<c00412c0>] (do_I                                 PI+0xec/0x208) [<c00412c0>] (do_IPI+0xec/0x208) from [<c0046a4c>] (__irq_svc+0x4c/0xe8) Exception stack(0xd3e51e20 to 0xd3e51e68) 1e20: 00000000 010da000 00000000 d3e50000 d67c9c60 0000002a 00000001 00000001 1e40: c10d5580 00000000 d6085a00 d3ceae00 00000000 d3e51e68 c0103478 c0114ba8 1e60: 60000013 ffffffff [<c0046a4c>] (__irq_svc+0x4c/0xe8) from [<c0114ba8>] (mnt_drop_write+0x70/0xa4) [<c0114ba8>] (mnt_drop_write+0x70/0xa4) from [<c0103478>] (pipe_write+0x26c/0x510) [<c0103478>] (pipe_write+0x26c/0x510) from [<c00fb338>] (do_sync_write+0xa4/0xe4) [<c00fb338>] (do_sync_write+0xa4/0xe4) from [<c00fba3c>] (vfs_write+0xa8/0x138) [<c00fba3c>] (vfs_write+0xa8/0x138) from [<c00fbcac>] (sys_write+0x40/0x6c) [<c00fbcac>] (sys_write+0x40/0x6c) from [<c0047000>] (ret_fast_syscall+0x0/0x30) Code: c078e260 e3a03901 e34f240c e92d4010 (e5934010) ---[ end trace dcbcbc34e4f8c36f ]--- Kernel panic - not syncing: Fatal exception in interrupt [<c004cdb0>] (unwind_backtrace+0x0/0xf8) from [<c056c398>] (panic+0x74/0x18c) [<c056c398>] (panic+0x74/0x18c) from [<c004aad4>] (die+0x220/0x284) [<c004aad4>] (die+0x220/0x284) from [<c056c1a8>] (__do_kernel_fault.part.3+0x54/0x74) [<c056c1a8>] (__do_kernel_fault.part.3+0x54/0x74) from [<c0050ae0>] (do_translation_fault+0x                                 0/0xa0) [<c0050ae0>] (do_translation_fault+0x0/0xa0) from [<f40c4010>] (0xf40c4010) CPU1: stopping [<c004cdb0>] (unwind_backtrace+0x0/0xf8) from [<c00413a8>] (do_IPI+0x1d4/0x208) [<c00413a8>] (do_IPI+0x1d4/0x208) from [<c0046a4c>] (__irq_svc+0x4c/0xe8) Exception stack(0xd6f15e18 to 0xd6f15e60) 5e00:                                                       c0574e78 00000005 5e20: f2a01000 00000001 d6f15e8c c111a580 00000000 c111a580 010da000 c111a588 5e40: 00000001 c0574f04 00000000 d6f15e60 c004bbac c00a7088 20000113 ffffffff [<c0046a4c>] (__irq_svc+0x4c/0xe8) from [<c00a7088>] (generic_exec_single+0x70/0x90) [<c00a7088>] (generic_exec_single+0x70/0x90) from [<c00a71c0>] (smp_call_function_single+0x1                                 18/0x1d0) [<c00a71c0>] (smp_call_function_single+0x118/0x1d0) from [<c004c850>] (twd_cpufreq_transitio                                 n+0x48/0x58) [<c004c850>] (twd_cpufreq_transition+0x48/0x58) from [<c0098c2c>] (notifier_call_chain+0x44/                                 0x84) [<c0098c2c>] (notifier_call_chain+0x44/0x84) from [<c0098d80>] (__srcu_notifier_call_chain+0                                 x44/0x60) [<c0098d80>] (__srcu_notifier_call_chain+0x44/0x60) from [<c0098db4>] (srcu_notifier_call_ch                                 ain+0x18/0x20) [<c0098db4>] (srcu_notifier_call_chain+0x18/0x20) from [<c037e508>] (cpufreq_notify_transiti                                 on+0xa0/0xe0) [<c037e508>] (cpufreq_notify_transition+0xa0/0xe0) from [<c006959c>] (mxc_set_target+0x194/0                                 x220) [<c006959c>] (mxc_set_target+0x194/0x220) from [<c037dcc4>] (__cpufreq_driver_target+0x50/0x                                 64) [<c037dcc4>] (__cpufreq_driver_target+0x50/0x64) from [<c0382aa8>] (cpufreq_interactive_up_t                                 ask+0x168/0x1b4) [<c0382aa8>] (cpufreq_interactive_up_task+0x168/0x1b4) from [<c00939b0>] (kthread+0x80/0x88) [<c00939b0>] (kthread+0x80/0x88) from [<c0047ae4>] (kernel_thread_exit+0x0/0x8)
記事全体を表示
This is the prototype demo to enable surround view demo on SabreSD.   The attached Files are HW&SW guides and demo video. Updating Notes: Add miniPCIE Surround View_Rev A design file (include schematic and layout) as attachement. Add Gerber file   i.MX6Q Surround view patch https://community.freescale.com/docs/DOC-95143 Original Attachment has been moved to: Gerber-file.zip Original Attachment has been moved to: miniPCIe-Surround-View_Rev-A.zip
記事全体を表示
Author:Fourier Email:[email protected] AMP:(Asymmetric Multiple Processing) Scenario:cpu core 0 run Linux, cpu core 1 run uC/OS-II RTOS. HDMI display panel link to Linux, LCD display panel link to uC/OS-II RTOS. Platform: Mars Board(freesclae i.mx6 dual Coretex-A9 core, 1GB 64bit DDR3) Panda Board(TIOMAP4460 dual Cortex-A9 core, 1GB 32bit DDR3) Altera SoC EVMBoard(dual Cortex-A9 core, (512MB+256MB ECC) DDR3 on HPS, 512MB on FPGA) Video Demo On Mars Board: Youtube: http://youtu.be/yb6KC6Cf8i4 http://youtu.be/1uzrX-YZBnQ Youku: http://v.youku.com/v_show/id_XNTMyNTAzNjky.html AMP Port: Linux SMP boot procedure is not mention here, For detail about the Linux SMP boot procedure please refer to the document here,http://www.linux-arm.org/LinuxBootLoader/SMPBoot.I just move the boot secondary procedure from Linux to U-boot as figure 1 in the AMP implementation, and figure2 describe the GIC relationship between two core and physical memory layout between Linux and uC/OS-II. Figure 1 Figure 2 Display Subsystem Block on Mars Board and Panda Board: Figure 3 imx6 display subsystem(Mars Board) Figure 4 omap4460 display subsystem on panda board
記事全体を表示
Overview The purpose of this document is to provide GPU P11.1 upgraded kernel patches and binaries for ICS R13.4-GA or R13.4.1 release. This GPU upgrade fixed some issues and improve the performance, for example chrome browser mess display issue, GUI miss alignment issue, YV12 CTS verifier fail, improve Antutu benchmark performance, improve HTML5 performance, etc. Software and HW platform Software: R13.4-GA or R13.4.1 Android releases Hardware: MX6Dual/Quad SabreSD board or MX6DualLite SabreSD board. Patches You can get the patches from attached zip. For R13.4-GA, please apply the kernel patch and gpu binaries in r13.4-ga-p11.1-gpu-upgrade folder, find them in attach. For R13.4.1, please apply the kernel patch and gpu binaries in 13.4.1-p11.1-gpu-upgrade folder, find them in attach.
記事全体を表示
According to EHSET_v1.01.pdf description (http://testusb.com/EHHS.html), the USB physical certification test are from 2 sides. One test case is PC running USB-IF HSET utility as being USB host to test the target board being USB device; the other case is target board acting as USB host to initate test signals to a test fixture. The principle of test modes supported are based on Vid/Pid pair  during enumration by host whoever takes. Apply the attached patch (I use r13.4.1 kernel_imx tree), then enable "FSL_USB_TEST_MODE" in kernel config, rebuild uImage to get the test modes support kernel.
記事全体を表示
According to iMX6DQRM chapter 46 (On-Chip OTP Controller), the UID field is located at offsets 0x410 and 0x420 from the base address of the OCOTP.  That is: OTP Bank0 Word1 - contains the first word of the UID OTP Bank0 Word2 - contains the second word of the UID. md.l 21bc410 021bc410: d72d7372 d72d7372 d72d7372 d72d7372    rs-.rs-.rs-.rs-. 021bc420: 906709d4 906709d4 906709d4 906709d4 ..g...g...g...g. Comparing to the read information under Linux shell: cat /proc/cpuinfo ......... Serial : 906709d4d72d7372 The value is identical from uboot and linux kernel reading back.
記事全体を表示
This work is the result of my daughter's idea, she finished it with my guidance. Cradle-1 Palmsize mini-HPC World's first full function heterogeneous mini-HPC, this is what it looks like: 1 Architecture         Overall:  CPU+GPU heterogeneous, 4 nodes, connected by a 100M Ethernet switcher;         Nodes: FreeScale I.MX6 Quad core mini-pc, with 4 ARM Cortex-A9 cores and 1 Vivante GC2000 GPU 2  Software         OS:   Ubuntu 11.10 linaro         OpenCL driver: Vivante GC2000 OpenCL driver         Compiler:  C/C++: gcc 4.6.1, Fortan90/95:  gfortran 4.6.1,         MPI Parallel Computing: MPICH2 1.4-1         NFS network file system: nfs-kernel-server 1.2.4         SSH security:   openssh   1:5.8 3 Hardware         The hardware of all nodes are the same, only the software configurations are slightly different. One of them was assigned as the master node, the others are slave nodes. They were TV sticks originally, with android 4.0 installed. The node's hardware specification is:         CPU: 4 1.2G Cortex-A9 cores         GPU: 1 Vivante GC2000 GPU         RAM: 1G DDR         ROM: 8G SD         NIC:   usb2.0 100M Ethernet Adapter (this NIC is not the TV stick's component, we added it)         WIFI: 150M         Display Interface:  HDMI         Network Switcher: 5 port 100M Ethernet Switcher 4  Network         Each node has one USB2.0 NIC and one WIFI interface, the WIFI is used as the backup connection for NIC connection. Network configurations are:         IP Address assignment:  (baby1 - baby4 are the four computing nodes)         baby1: 100M NIC 192.168.10.1 WIFI 192.168.0.111         baby2: 100M NIC 192.168.10.2 WIFI 192.168.0.112         baby3: 100M NIC 192.168.10.3 WIFI 192.168.0.113         baby4: 100M NIC 192.168.10.4 WIFI 192.168.0.114 5  Performance         Cradle-1 has 16 1.2G ARM Cortex-A9 cores and 4 Vivante GC2000 GPU cores, the total computing power of these 20 computing devices is more than 100GFLOPS,   more powerful than an ordinary desktop. The whole machine is only a little bigger than a palm, and the total power consumption is less than 15 watts.          The overall architecture of Cradle-1 is almost the same as Chinese Tianhe-1A or the Titan in the oak ridge lab. they used the same set of software, LINUX+OPENCL+OPENMPI. Cradle-1 supports C/C++, Fortran90/95. And almost all kinds of parallel computing algorithms can run on it, the only difference is the scale.         We coded a MPI parallel computing program for large matrix multiplication with 4 processes, each process had 5 threads, four threads for the four CPU cores, and one thread for GPU computing. 6 Appearance Front Back Top Left Right One node, it has three interfaces, the right is HDMI interface, upper-left is the wireless adapter for keyboard and mouse, down-left is the power connection. One node is running Ubuntu 11.10. Coded a simple OpenCL program to display OpenCL driver information On a notebook, using remote desktop access function to obtan the node baby1's desktop. This is the sign in desktop of baby1 node. Baby 1 has X11VNC server installed. sign in baby1, open a terminal Ran a MPI testing program, ensuring that all babies (baby1 - baby4) were working     Any comments? please mail to [email protected]
記事全体を表示
Host : Ubuntu 11.10 Part 1. Installation of QNX 6.50 and QNX 6.50 SP1        1.1 Create an account and activate the created account that will be assigned an 30-days evaluation serial numberin then on www.qnx.com, and download qnxsdp-6.5.0-201007091524-linux.bin, qnxsdp-6.5.0SP1-201206271006-linux.bin;        1.2 Execute "sudo apt-get install ia32-libs"        1.3 Execute "sudo -E /your/path/qnxsdp-6.5.0-201007091524-linux.bin", follow the guides as prompted, enter the received evaluation serial number, then the installation of QNX 6.50 will be done;        1.4 Logout, and re-login, so far typing "qconfig" will return the following messages:         --------------------------------------------------------------------------------------------------------------------- alanz@alanz-VirtualBox:~$ qconfig QNX Installations   Installation Name: QNX Software Development Platform 6.5.0             Version: 6.5.0      Base Directory: /opt/qnx650            QNX_HOST: /opt/qnx650/host/linux/x86          QNX_TARGET: /opt/qnx650/target/qnx6         ---------------------------------------------------------------------------------------------------------------------        1.5 Execute "sudo chmod a+rw /etc/qnx/license/licenses"        1.6 Execute "sudo -E /your/path/qnxsdp-6.5.0SP1-201206271006-linux.bin"        1.7 Logout, and re-login, so far typing "qconfig" will return the following messages:         --------------------------------------------------------------------------------------------------------------------- alanz@alanz-VirtualBox:~$ qconfig QNX Installations   Installation Name: QNX Software Development Platform 6.5.0             Version: 6.5.0      Base Directory: /opt/qnx650            QNX_HOST: /opt/qnx650/host/linux/x86          QNX_TARGET: /opt/qnx650/target/qnx6 Additional Packages    Package Name: QNX Software Development Platform         Version: 6.5.0SP1            Base: QNX SDP 6.5.0    Installation Path: /opt/qnx650         ---------------------------------------------------------------------------------------------------------------------        1.8 Download bsp-nto650-freescale-mx6q-sabrelite-trunk-201301161142.zip, and unzip it; Part 2. Build i.MX6Q SabreLite QNX BSP        2.1 Edit a envsetup.sh as following:         --------------------------------------------------------------------------------------------------------------------- #!/bin/bash export QNX_HOST=/opt/qnx650/host/linux/x86 export QNX_JAVAHOME=/opt/qnx650/_jvm export QNX_TARGET=/opt/qnx650/target/qnx6 export QNX_CONFIGURATION=/etc/qnx export ARCH=arm export CPULIST=arm export VARIANTLIST=v7 export MAKEFLAGS=-I/opt/qnx650/target/qnx6/usr/include export PATH=$PATH:/opt/qnx650/host/linux/x86/usr/bin export QCONFIG=/opt/qnx650/target/qnx6/usr/include/qconfig.mk export BSP_ROOT_DIR=/home/alanz/Downloads/QNX_Software/i.MX6Q_SabreLite4QNX         ---------------------------------------------------------------------------------------------------------------------        Note: BSP_ROOT_DIR is the BSP unzip directory.        2.2 Execute "make clean", then "make". The generated file will be under images/ifs-mx6q-sabrelite.raw Part 3. Running i.MX6Q SabreLite QNX BSP        3.1 Copy images/ifs-mx6q-sabrelite.raw to SD;        3.2 Modify u-boot environment as following:         --------------------------------------------------------------------------------------------------------------------- setenv loadaddr '0x10800000' setenv bootcmd_sd 'mmc dev 0; fatload mmc 0:1 ${loadaddr} ifs-mx6q-sabrelite.raw; go ${loadaddr}' setenv bootcmd 'run bootcmd_sd' saveenv boot         ---------------------------------------------------------------------------------------------------------------------        3.3 Connect i.MX6Q SabreLite w/ serial and ethernet, turn on, type "qconn" and "ifconfig" in the serial shell. Part 4. Debug w/ QNX Momentics IDE        4.1 Type "qde" to activate Momentics IDE        4.2 On the top-right corner, there exist several icons named in "xxx perspective" to switch the main window according to current selected "perspective" context. Click "QNX System Information Perspective" to create a target to conect and debug as following depicted.        4.3 Switch to "C/C++ perspective" to create QNX C/C++ project as following depicted.        4.4 Switch to "Debug perspective" to perform "Debug Configuration" as following depicted.        Then it can debug program on target i.MX6Q SabreLite board.
記事全体を表示
This is the prototype solution to enable second display showing different things on JB4.2.2 SabreSD. Make use of Class Presentation provided by android to be embedded into Status bar. When unlock the screen, the Presentation will show on second display. Now, the solution requires one .mp4 video placed in root sdcard. Of course, you may change it to show anything. The attached Files are a layout xml file, a patch and a recorded video. The layout file should be put into android/frameworks/base/packages/SystemUI/res/layout/ folder. The patch should be applied to frameworks/base.git. The recorded video shows the dual display demo as a reference.
記事全体を表示
i.MX28 GPIO pins only support the following IRQ types: IRQ_TYPE_EDGE_RISING, IRQ_TYPE_EDGE_FALLING, IRQ_TYPE_LEVEL_HIGH and IRQ_TYPE_LEVEL_LOW. IRQ_TYPE_EDGE_BOTH is not supported. It application requires interrupt on both rising and falling edges, software can set the IRQ type to level trigger and set the polarity in reverse to the current GPIO input level. Below is the example. value = gpio_get_value(pdata->id_gpio) ? 1 : 0; if (value)     set_irq_type(gpio_to_irq(pdata->id_gpio), IRQ_TYPE_LEVEL_LOW); else     set_irq_type(gpio_to_irq(pdata->id_gpio), IRQ_TYPE_LEVEL_HIGH); ... When GPIO input value is low, set the IRQ type to IRQ_TYPE_LEVEL_HIGH. When the GPIO input value is high, set the IRQ type to IRQ_TYPE_LEVEL_LOW. Do the same checking in the GPIO IRQ handler. In this way, interrupts on both edges can be captured. This document was generated from the following discussion: i.MX28: GPIO interrupt on both rising and falling edges
記事全体を表示
I've been asked to help to upload the doc in MPU support space. The doc describes some ideas about how to support a customer to enable a mipi-csi2 sensor connected with i.MX6DQ/6DL. Hope this may be helpful.
記事全体を表示
http://freescale.eefocus.com/bbs/article_175_179914.html Freescale i.mx53 i.mx6x series solution to speed up the progress of your product 深圳市优创科技有限公司 Josephwang 王伟 深圳市南山区高新技术产业园南区创维大厦C15 Tel:0755-26017990  13128865181        Mail:[email protected]        QQ:[email protected]
記事全体を表示
Qt Creator can be a very good IDE in order to develop great QT applications. This IDE does not only helps with syntax highlighting, access to examples and tutorials, but also helps you to configure different toolchains Qt binary versions and target options. First download the binary installer from: For 32 bits: $ wget http://releases.qt-project.org/qtcreator/2.6.2/qt-creator-linux-x86-opensource-2.6.2.bin For 64 bits: $ wget http://releases.qt-project.org/qtcreator/2.6.2/qt-creator-linux-x86_64-opensource-2.6.2.bin execute the binary $ ./qt-creator-linux-x86_64-opensource-2.6.2.bin Follow the Installer GUI and choose a location. Default options should be OK. in my case the installation was done here: $ /home/b35153/qtcreator-2.6.2/bin Open Qt Creator (in my case from command line, use "&" to regain control of the terminal) $./qtcreator & Open Tools -> Options Choose Build & Run  on the menu of the left. and Select the Compilers Tab Here you can add the toolchain GCC compiler of your convenience. It will appear in the "Manual"  section. Now click on Qt Version Tab.  Here you can add the Qmake that you had created with your Qt installation; for example, the Qt5 installation described here: Building QT for i.MX6 It will appear in the Manual section. In my case I have Qmake for PC and Qmake for i.MX6. Now click on Kits Tab Here you can create combinations of Compilers and Qmake, and also specify where do you want the executables to go. In my case here I combined the i.MX6 toolchain and the Qmake for I.MX6 i had created. I did not set up device configuration since the sysroot is already shared to my device via NFS, but you can configure it so the files are sent via ssh to your device. And that's It! Next time you load a project you can choose which Kit you want to work on, and it will be compiled just as you need.
記事全体を表示
In order to run the QT5 demos on i.MX6 you should follow the instructions on this link: Building QT for i.MX6 Some of the demos on the release such as  /examples/opengl/hellogl_es2,  consist of a group of multiple widgets appearing on the screen. Normally these demos should work OK in a windowed environment such as Wayland or X11. In the case of Linux only environment, the plugin that draws to the screen is called EGLFS. This plugin has the restriction that it only supports one single widget at a time on the screen surface. Then demos such as hellogl_es2 are *not intended* to work along with this plugin, and it will never work. The errors found when using EGLFS consist on: These issues can be seen in the Qt OpenGL examples.  "hellogl_es2" and "2dpaint" seem to display one rendered frame and then break --   "hellogl_es2" shows the QT word and bubbles, and the GUI is hidden, while  "2dpaint" just shows the openGL version without label. It seems that when including  a QGLWidget on a form, the QGLWidget would work OK, but the rest of the form would not appear. I couldn't click any buttons or do anything.   Along with these problems I would also see one or more of these error messages in the output:   * This plugin does not support setParent!   * This plugin does not support propagateSizeHints()   * QOpenGLContext::swapBuffers() called with non-opengl surface However other demos such as hellowindow work well with EGLFS because they are single widget.  Also all demos created with qtquick will work OK since all visual QML items are rendered as a single widget using the scene graph, a low-level, high-performance rendering stack, closely tied to OpenGL. This is better explained here: Qt5 QPainter vs. QML &amp; Scene Graph.
記事全体を表示
Dear All,       Our board is designed based on both EVK and HEG (Adeneo Embedded Home Energy Gateway), the ENET_FEC_RESET_B on EVK is replaced by LCD_D11 as it on HEG. We have re-config all pins based on i.mx28 BSP and successfully built by ltib. However, eth0 is not working due to "PHY is not found"! and we are still trying to figure it out.       The changes we apply on the BSP are(in mx28evk_pins.c): in static struct pin_desc mx28evk_fixed_pins[]:       the definition of LCD_D11 change to { .name = "LCD_D11", .id = PINID_LCD_D11, /* PHY reset pin*/ .fun = PIN_GPIO,      .voltage    = PAD_3_3V,      .strength = PAD_8MA,      .output     = 0, },      and replace all "PINID_ENET0_RX_CLK" in mx28evk_pins.c by "PINID_LCD_D11"      To prevent any possible interrupt, we also disable all LCD pins in both mx28_pins.h and mx28evk_pins.c since we don't have LCD.      Any comment/suggestion is highly appreciate! BR, TF
記事全体を表示
The i.MX 6 D/Q L3.035_1.0.2 patch release is now available on the www.freescale.com ·         Files available # Name Description 1 L3.0.35_1.0.2_LDO_PATCH This patch release is based on the i.MX 6Dual/6Quad Linux   12.09.01 release. The purpose of this patch release is to manage the LDO and   PMIC ramp-up time correctly.
記事全体を表示
       Overview The purpose of this document is to describe how to enable Bluetooth on i.MX 6Dual/Quad SabreSD board (RevC) for Android software. Hardware Changes i.MX 6Dual/Quad SabreSD board doesn't enable Bluetooth connection by default. To support bluetooth, the hardware rework is required. The above diagram shows the reserved connections for Bluetooth in SabreSD RevC board (All connections are marked as "DNP"). This Bluetooth cable connector is designed specifically for the WiFi/BT combo card SX-SDCAN-2830BT which is developed and sold by Silex Technology. Note that pin 1 (BT_DISABLE) of the cable connector on i.MX 6Dual/Quad SabreSD RevC is opposite Pin 20 of the WiFi/BT module. Note: when connecting Silex module and J13, the connection is reverted (For example, PIN 1 in J13 connects to PIN 20 in Silex module). To use the J13 connector, the following reworks are required:   R209-R211, R214-R215 need to be populated.           Where is them, you can refer to the below chart.   SPI nor flash U14 need to be depopulated. No other AUX boards should be connected.. Exchange UART5_RXD and UART5_TXD. Orange PAD connects to Orange PAD. Green PAD connects to Green PAD.      After hardware rework, the Bluetooth connection will like the following:   Pin on Silex Module Sabresd Board Mux Pad Pin-2  BT_UART_RTS  (output) UART5.RTS   (input) MX6Q_PAD_KEY_COL4__UART5_RTS Pin-3  BT_UART_TXD   (output) UART5.RXD   (input) MX6Q_PAD_KEY_ROW1__UART5_RXD Pin-4  BT_UART_CTS   (input) UART5.CTS   (output) MX6Q_PAD_KEY_ROW4__UART5_CTS Pin-5  BT_UART_RXD   (input) UART5.TXD   (output) MX6Q_PAD_KEY_COL1__UART5_TXD Pin-14  BT_PWD_L       (input) GPIO_2         (output) MX6Q_PAD_GPIO_2__GPIO_1_2   Software Information For earlier android version before Jelly Bean4.2 Take ICS as an example, for we didn't do this work when our last ICS version R13.4.1 released. So our formal release had no support on BT. Here will give out patches based on R13.4.1. Enable Bluetooth with the following setting (e.g. device/fsl/imx6/sabresd/init.rc)      # No bluetooth hardware present -    setprop hw.bluetooth 0 +    setprop hw.bluetooth 1 Ensure BOARD_HAVE_BLUETOOTH := true in device/fsl/imx6/sabresd/SabreSDBoardConfigComm.mk. Add BT feature support in device/fsl/imx6/sabresd/required_hardware.xml: <permissions>      <feature name="android.hardware.camera" /> +    <feature name="android.hardware.bluetooth" />   Add UART5 support in kernel: In this step you can refer to the attached (kernel patch for UART5 based on ICS.zip) to change PinMux PAD configuration for UART5.   Add AR3002 BT firmware support: Update external/linux-firmware with the attached patch(0001-ENGR00270791-BT-add-AR3002-firmware-support.patch) to add AR3002 BT firmware support for Silex's BT is AR3002.   Then you can manually run the command “hciattach -n -s 115200 /dev/ttymxc4 ath3k 115200 flow nosleep” in console to see whether bluetooth can attach HCI successfully.   At last, you need add rfkill for BT reset in kernel, here also give a patch for reference: 0001-ENGR00270791-BT-add-rfkill-for-bt-reset.patch   BT is not enable in kernel default. You can control whether to enable it in bootargs like the following  in device/fsl/sabresd_6dq/BoardConfig.mk. BOARD_KERNEL_CMDLINE := console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale  bluetooth For android version since Jelly Bean4.2 From Jelly Bean4.2, Bluez is no longer used.Android provides a default Bluetooth stack, BlueDroid, that is divided into two layers: The Bluetooth Embedded System (BTE), which implements the core Bluetooth functionality and the Bluetooth Application Layer (BTA), which communicates with Android framework applications. A Bluetooth system service communicates with the Bluetooth stack through JNI and with applications through Binder IPC. The system service provides developers access to various Bluetooth profiles. The following diagram shows the general structure of the Bluetooth stack: For bluedroid, we have supported it in our formal release including Android4.3. You can get it from our website. Or just get HAL code from attached(libbt-ath3k.zip). Known issue For  KEY_COL4 is both used by uart5 and pcie,  if you enable BT, 3G  mobile will not work. For its power disable pin is conflict with uart5's UART_RTS. This is also why we didn't enable BT in formal release. Supported and tested profile workable profile not tested profile Hid Handset & Handfree(not support for hardware restrict) A2DP Pbap Opp Pan
記事全体を表示
With Qt5  you will find the addition of new technologies that will make your development much easier. Qtquick2 SceneGraph Qml Qt5 is backwards compatible,  that means you can run your Qt 4.8 applications, But that doesn't mean they will have the best performance, sometimes it is better to do a porting to use the newest features. Qt5, has two options to paint components into the screen. Painting in Qt 5 is primarily done either with: The imperative QPainter API Qt’s declarative UI language, QML, and its scene graph back-end. QPainter As this document mentions  Qt5GraphicsOverview | Qt Wiki | Qt Project  The Qpainter engine uses software to paint, and is used when drawing Qimages or Qwidgets. Its  advantage over OpenGL is the high quality when antialiasing is enabled, and a complete feature set. The Qpainter can use an OpenGL engine, but as the document mentions it is more suceptible to state changes. And has to be used carefully. QML & Scene Graph. All visual QML items are rendered using the scene graph, a low-level, high-performance rendering stack, closely tied to OpenGL. Qt Quick 2 makes use of a dedicated scene graph based on OpenGL ES 2.0 or OpenGL 2.0 for its rendering. Using a scene graph for graphics rather than the traditional imperative painting systems (QPainter and similar), means the scene to be rendered can be retained between frames and the complete set of primitives to render is known before rendering starts. This opens up for a number of optimizations, such as batch rendering to minimize state changes and discarding obscured primitives. The QML scene graph is a new back-end for QML in Qt 5, and is based on OpenGL. It generally improves the performance of QML significantly over the QPainter-based back-end used in Qt 4. It achieves better performance in a number of ways: The scene graph uses OpenGL directly instead of going though a QPainter which could be using either the raster or OpenGL paint engine. This means that all the resources, like geometry, textures and shaders can be stored in a format suitable for OpenGL rather than using classes such as QPainterPath, QPixmap, QBrush, or QPen, which the QPainter would need to translate into OpenGL primitives and possibly cache. QML, being a declarative language, defines how the end result should look like, but it doesn’t define how and in which order each individual element is drawn. The drawing can therefore be reordered to reduce the number of state changes, or merged to reduce the number of draw calls. The scene graph uses a separate render thread, and synchronizes the animations with the vertical retrace on platforms where this can be supported. The render thread allows the preparation of the next frame to be done at the same time the current frame is being rendered. This has a positive effect also on single-core systems, since the render thread might block on OpenGL commands. The synchronization with the vertical retrace improves the perceived smoothness of the animations. We have tested on i.MX6 Both options, having the best results using QML Qtquick2 elements. When we tried using QtPainter via Widgets we face the problem that if not using a windowing system like X11 or Wayland the painter wont work well and will only show the QtGLWidget. With QML scene graph we are able to have an OpenGL element and a Qt element on the same environment, and there is an easy way to communicate one with the other and share variables.  Please look at the example results here: I.MX6 scene graph Qt5 - YouTube And the great advantage, the sceneGraph is all accelerated via OpenGL.
記事全体を表示
The i.MX 6 Android 13.4.1.03 patch release is now available on www.freescale.com IMX6_R13.4103_ANDROID_LDO_PATCH This patch release is based on the i.MX6 Android R13.4.1 release. The purpose of this patch release is to manage the LDO and PMIC ramp-up time correctly.
記事全体を表示