i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
It's the demo for hibernation for Android. Restore Android and UI can operate about 6 sec.
View full article
Added two functions in DDR_Stress_Tester V1.0.2, find the attachment for the details. 1. Check the actual boot mode settings in H/W target board 2. Add test option for bit flip and bit spread walking test
View full article
For long I looked for a working tutorial to build Qt5 with YOCTO (Yocto Training - HOME) both the libraries for the board image and also a toolchain to build Qt5 applications for the board. See the full tutorial here: Building Qt5 using yocto on Wandboard - Wandboard Wiki The Tutorial is written for the Wandboard that also uses an i.MX6 CPU but you can adapt the tutorial for most of the boards of the i.MX6 family I think - in my case it worked with the i.MX6 SABRE AI without problems. You only have to adjust the sysroot and maybe also the toolchain-path because the wiki entry is a little bit older Ask your questions for this topic - maybe I can help.
View full article
This is a HW design checklist for customer's reference. Please read and fill it in carefully before requesting a schematic/design review.
View full article
Here is a quick summary at building a bootloader, a kernel and a root filesystem for the i.MX 6 sabre sd platform, using buildroot. This assumes you have a "working" Linux development environment at hand (e.g. Debian). Buildroot is a fine build system, which makes deploying Linux on embedded platforms really easy. It is comparable to Yocto in spirit, but much simpler. Thanks to my colleague gillestalis, buildroot now has builtin support for the i.MX6 sabre sd platform. Get buildroot sources We will use git to fetch buildroot sources: $ git clone git://git.busybox.net/buildroot This should create a buildroot directory with all the latest sources (after a while). Note that for more stability you might want to checkout a release instead of the latest version; to do so, list the available release tags with e.g. git tag -l '201*', and git checkout <the-desired-tag>. Compile The beauty of buildroot is that it will take care of everything for you, including preparing a cross compiler. You can download and build everything by doing: $ cd buildroot $ make freescale_imx6sabresd_defconfig $ make This should download and build everything, so it will take a while. buildroot detects the number of CPUs you have in your machine and builds with parallel jobs automatically; no need to specify any -j argument to make here. All build results fall under the output/images folder: output/images/ +- rootfs.ext2 +- rootfs.tar +- u-boot.bin `- uImage Format the SD card As for Debian, we need to format the SD card with two partitions; one small FAT partition to contain the Linux kernel, and one large ext4 partition, which will contain the root filesystem with the buildroot generated userspace. Also, we need to make sure we leave some space for u-boot starting from offset 1024B. Here is an example SD card layout: +-----+------+--------+-----+---------------+----------------- | MBR |  ... | u-boot | ... | FAT partition | Linux partition ... +-----+------+--------+-----+---------------+----------------- 0     512    1024           1M              ~257M (offsets in bytes) Here is an example SD card layout, as displayed by fdisk: Device    Boot      Start         End      Blocks   Id  System /dev/sdc1            2048      526335      262144    c  W95 FAT32 (LBA) /dev/sdc2          526336     8054783     3764224   83  Linux (units: 512B sectors) You can format the FAT boot partition with: # mkfs.vfat /dev/<your-sd-card-first-partition> Your SD card first partition is typically something in /dev/sd<X>1 or/dev/mmcblk<X>p1. You can format the Linux partition with: # mkfs.ext4 /dev/<your-sd-card-second-partition> Your SD card second partition is typically something in /dev/sd<X>2 or/dev/mmcblk<X>p2. Put on SD As explained here, u-boot should reside at offset 1024B of your SD card. Also, as buildroot generates an u-boot.bin (and not an u-boot.imx) we should skip its first KB, too. In summary, to put u-boot on your SD, do:   # dd if=output/images/u-boot.bin of=/dev/<your-sd-card> bs=1k seek=1 skip=1   # sync Your SD card device is typically something in /dev/sd<X> or /dev/mmcblk<X>. Note that you need write permissions on the SD card for the command to succeed, so you might need to su - as root, or use sudo, or do a chmod a+w as root on the SD card device node to grant permissions to users. Similarly to what this post describes, you can copy the kernel to the FAT boot partition with: # mount /dev/<your-sd-card-second-partition> /mnt # cp output/images/uImage /mnt/ # umount /mnt Your SD card first partition is typically something in /dev/sd<X>1 or/dev/mmcblk<X>p1. And not unlike what is done in this post, You can install your generated root filesystem to the Linux partition with: # mount /dev/<your-sd-card-second-partition> /mnt # tar -C /mnt -xvf output/images/rootfs.tar # umount /mnt Your SD card second partition is typically something in /dev/sd<X>2 or/dev/mmcblk<X>p2. Boot! Your SD card is ready for booting. Insert it in the SD card slot of your i.MX6 sabre sd platform, connect to the USB to UART port with a serial terminal set to 115200 baud, no parity, 8bit data and power up the platform. Like with Debian, u-boot default settings will not allow it to boot from the SD card, so we need to interrupt it by pressing enter at u-boot prompt for the first boot and setup u-boot environment to fix this: MX6Q SABRESD U-Boot > setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p2 rootwait' MX6Q SABRESD U-Boot > setenv bootcmd_mmc 'run bootargs_base bootargs_mmc; mmc dev 2; fatload mmc 2:1 ${loadaddr} ${kernel}; bootm' MX6Q SABRESD U-Boot > setenv bootcmd 'run bootcmd_mmc' MX6Q SABRESD U-Boot > saveenv Saving Environment to MMC... Writing to MMC(2)... done As this is saved in the SD card it need only to be done once at first boot. You can reboot your board or type boot; your buildroot system should boot to a prompt: (...) Welcome to Buildroot buildroot login: From there you may login as root. Enjoy! Tweak buildroot uses Linux kernel kconfig to handle its configuration. So, as for the Linux kernel, changes to the configuration can be done with e.g.: $ make menuconfig Most of the options can be tuned from there, including (most importantly) which packages get installed into the generated root filesystem. This is configuration section 'Filesystem images'. Further details are documented in buildroot manual. Tips ccache is natively supported by buildroot and can be easily enabled with configuration option BR2_CCACHE. If you only use the generated rootfs.tar as described in this post and do not care about the rootfs.ext2, you might as well save a few seconds of build by disabling its generation. This is done with configuration option BR2_TARGET_ROOTFS_EXT2. It is recommended to install an ssh server inside the target for further development. This is conveniently done with configuration option BR2_PACKAGE_OPENSSH. See also... Other root filesystems may make more sense for you; see this post for a Debian root filesystem, and this post for a minimal busybox filesystem. Freescale Yocto Project main page
View full article
Currently, we meet an issue that some jpeg pictures can't be displayed on  imx53 platform by command "gst-launch filesrc location=JPEGFILE ! jpegdec ! freeze ! mfw_isink", the system will meet application crash. So we did investigation on this, found imx6 aslo has such issue.   We found that the issue happen on specific jpeg pictures, the width & height is not 8 pixels alignment.   After track the code ,  found that the jpeg decoder send the width and height to isink plugin, also it send a outsize calculate by the width and height with algorithm that will do 2 pixels,4 pixles,8pixles alignment(I420_SIZE (width, height)). The isink use a different algorithm to calculate the decoder buffer, this size is always smaller than the size pass down by the jpeg decoder , in later memory copy, the code copy a large memory to smaller memory, it's out of boundery, corrupt the memoryand cause the application fail.   So we make a little change, to malloc the larger size to avoid the out of boundry. Original Attachment has been moved to: fix-8pixels-unalignment-jpeg-display-crash.patch.zip
View full article
Hi All, The new Android JB4.3_1.1.0-GA release is now available on www.freescale.com ·         Files available           Name Description IMX6_JB43_110_ANDROID_DOCS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Android   jb4.3_1.1.0 BSP Documentation. Includes Release Notes, User's Guide, QSG and   FAQ Sheet. IMX6_JB43_110_ANDROID_SOURCE_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Android   jb4.3_1.1.0 BSP, Documentation and Source Code for BSP and Codecs. IMX6_JB43_110_ANDROID_DEMO_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Android   jb4.3_1.1.0  BSP Binary Demo Files IMX6_JB43_110_AACP_CODEC_CODA AAC   Plus Codec for i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX   6Sololite Android jb4.3_1.1.0 ·         Target HW boards o   i.MX6DL  SABRE SD board o   i.MX6Q  SABRE SD board o   i.MX6DQ SABRE AI board o   i.MX6DL SABRE AI board o   i.MX6SL EVK board ·         Release Description i.MX Android jb4.3_1.1.0 release includes all necessary codes, documents and tools to assist users in building and running Android 4.3 on the i.MX 6Quad, i.MX 6DualLite and i.MX6SoloLite hardware board from the scratch. The prebuilt images are also included for a quick trial on Freescale i.MX 6Quad and i.MX 6DualLite SABRE-SD Board and Platform, i.MX 6Quad and i.MX 6DualLite SABRE-AI Board and Platforms and i.MX6SoloLite EVK Board and Platforms. This release includes all Freescale porting and enhancements based on Android open source code. Most of deliveries in this release are provided in source code with the exception of some proprietary modules/libraries from third parties. ·         What's in this release         Android Source Code Patch All   Freescale i.MX specific patches (apply to Google Android repo)   to enable Android on i.MX based boards. For example Hardware   Abstraction Layer implementation, hardware codec acceleration,   etc. Packed in   android_jb4.3_1.1.0-ga_source.tar.gz Documents The   following documents are included in android_jb4.3_1.1.0-ga_docs.tar.gz: ●   i.MX Android jb4.3_1.1.0-ga Quick Start: A   manual explains how to run android on i.MX board by using prebuilt images. ●   i.MX Android jb4.3_1.1.0-ga User Guide: A   detailed manual for this release package. ●   i.MX Android jb4.3_1.1.0-ga FAQ: A document lists   “Frequently Asked Questions”. ●   i.MX Android Codec Release Notes: A   document to describes the Freescale Codec Package ●   i.MX Android Wi-FI Display Sink API Introduction A   document to describes how to use i.MX Android Wi-Fi Display Sink API ●   i.MX6 G2D API User Guide document to introduce how to use i.MX6 G2D API for   2D BLT usage ●   i.MX Android jb4.3_1.1.0-ga Release Note A   document to introduce the key updates and known issues in this release. Tools Tools   in android_jb4.3_1.1.0-ga_tools.tar.gz ●  MFGTool. Manufacturing tools for i.MX platform ●  USB tethering windows .inf driver configure file.tool/tetherxp.inf Prebuilt Images You   can test Android on i.MX with prebuilt image on i.MX board before building   any code. ● android_jb4.3_1.1.0-ga_image_6qsabresd.tar.gz: Prebuilt   images for the SABRE-SD board. ●  android_jb4.3_1.1.0-ga_image_6qsabreauto.tar.gz: Prebuilt   images for the SABRE-AI board. ●  android_jb4.3_1.1.0-ga_image_6slevk.tar.gz: Prebuilt images for the 6SL   SABRE-AI board. All   prebuilt images are in another package. See "i.MX Android jb4.3_1.1.0-ga   Quick Start" and "i.MX Android jb4.3_1.1.0-ga User Guide" to   understand which image should be used in which case. ·         Known issues For known issues and limitations please consult the release notes
View full article
Q: The i.MX 6Dual/6Quad Applications Processor Reference Manual Rev. D says that i.MX6 supports eMMC 4.5.  But does the current BSP(L3.0.35_12.08.00) support eMMC 4.5?  If not, does Freescale have it in their release plan? A: i.MX 6Dual/6Quad RM and Datasheet declare that the uSDHC module is "fully compliant with the MMC command/response sets and Physical Layer as defined in the Multimedia Card System Specification, v4.2/4.3/4.4/4.41, including high-capacity (> 2 GB) HC MMC cards."  Therefore, if your eMMC4.5 card is backward-compatible with eMMC4.4, you can use it in eMMC4.4 mode to enable eMMC4.4 functionality and performance on the i.MX6 platform. For example, the current i.MX6 Linux BSP (L3.0.35_4.1.0) has added code to interface with an eMMC4.5 card to operate as an eMMC4.4 card. See the following code in drivers/mmc/core/mmc.c:         card->ext_csd.rev = ext_csd[EXT_CSD_REV];         /* workaround: support emmc 4.5 cards to work at emmc 4.4 mode */         if (card->ext_csd.rev > 6) {                 printk(KERN_ERR "%s: unrecognised EXT_CSD revision %d\n",                         mmc_hostname(card->host), card->ext_csd.rev);                 err = -EINVAL;                 goto out;         }
View full article
To get the FSL amrdecoder building and running on imx53 in 11.09 BSP: TIP: During debug for creation of these patches -> On the target, I had to make sure I had all the amr decoder libraries present, or it just wouldn't work. I narrowed those down by deleting "rm /root/.gstreamer-0.10/registry.arm.bin" and rerunning gst-inspect to rescan the plugins. With GST_DEBUG=3 I could see what libraries were missing and copied them over. But once everything was in place, it just worked. gst-launch playbin2 uri=file:////media/sd/media_file_with_amr_audio_encoding.3gp Attached are the new .spec files and patch files to get this to work. Regards, Randy
View full article
This is the procedure and patch to set up Ubuntu 13.10 64bit Linux Host PC and building i.MX6x L3.0.35_4.1.0. It has been tested to build GNOME profile and with FSL Standard MM Codec for i.MX6Q SDB board. A) Basic Requirement: Set up the Linux Host PC using ubuntu-13.10-desktop-amd64.iso Make sure the previous LTIB installation and the /opt/freescale have been removed B) Installed the needed packages to the Linux Host PC $ sudo apt-get update $ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev $ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool $ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool $ sudo apt-get install uuid-dev liblzo2-dev $ sudo apt-get install tcl dpkg $ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev $ sudo apt-get install texlive texinfo $ sudo apt-get install lib32z1 lib32ncurses5 lib32bz2-1.0 $ sudo apt-get install libc6-dev-i386 $ sudo apt-get install u-boot-tools $ sudo apt-get install scrollkeeper $ sudo apt-get install gparted $ sudo apt-get install nfs-common nfs-kernel-server $ sudo apt-get install git-core git-doc git-email git-gui gitk $ sudo apt-get install meld atftpd $ sudo ln -s /usr/lib/x86_64-linux-gnu/librt.so   /usr/lib/librt.so C) Unpack and install the LTIB source package and assume done on the home directory: $ cd ~ $ tar -zxvf L3.0.35_4.1.0_130816_source. tar.gz $ ./L3.0.35_4.1.0_130816_source/install      After that, you will find ~/ltib directory created D) Apply the patch to make L3.0.35_4.1.0 could be installed and compiled on Ubuntu 13.10 64bit OS $ cd ~/ltib $ git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_13.10_64bit_OS.patch What the patch is doing: a) The patch modifies the following files:    dist/lfs-5.1/base_libs/base_libs.spec    dist/lfs-5.1/m4/m4.spec    dist/lfs-5.1/ncurses/ncurses.spec b) Add the following files to the pkgs directory:    pkgs/m4-1.4.16-1383761043.patch    pkgs/m4-1.4.16-1383761043.patch.md5 E) Then, it is ready to proceed the rest of the LTIB env setup process: $ cd ~/ltib $ ./ltib -m config $ ./ltib Reference: L3.0.35_4.1.0_130816_docs/doc/mx6/Setting_Up_LTIB_host.pdf https://community.freescale.com/message/332385#332385 https://community.freescale.com/thread/271675 https://community.freescale.com/message/360556#360556 m4 compilation issue: 1. https://github.com/hashdist/hashstack/commit/f6be2a58de62327d05e052d89c9aa931d4c926b3 2. https://github.com/hashdist/hashstack/issues/81 rpm-fs package failed to build issue: https://community.freescale.com/message/355771#355771 scrollkeeper is for the gnome-desktop compilation NOTE: When compiling gstreamer, this warning was pop up.  Just ignore it seems okay.
View full article
This is the procedure and patch to set up Ubuntu 13.10 64bit Linux Host PC and building i.MX28 L2.6.35_1.1.0_130130. It has been tested to build GNOME profile and with FSL Standard MM codec. A) Basic Requirement: Set up the Linux Host PC using ubuntu-13.10-desktop-amd64.iso Make sure the previous LTIB installation and the /opt/freescale have been removed B) Installed the needed packages to the Linux Host PC $ sudo apt-get update $ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev $ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool $ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool $ sudo apt-get install uuid-dev liblzo2-dev $ sudo apt-get install tcl dpkg $ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev $ sudo apt-get install texlive texinfo $ sudo apt-get install lib32z1 lib32ncurses5 lib32bz2-1.0 $ sudo apt-get install libc6-dev-i386 $ sudo apt-get install u-boot-tools $ sudo apt-get install scrollkeeper $ sudo apt-get install gparted $ sudo apt-get install nfs-common nfs-kernel-server $ sudo apt-get install git-core git-doc git-email git-gui gitk $ sudo apt-get install meld atftpd $ sudo ln -s /usr/lib/x86_64-linux-gnu/librt.so   /usr/lib/librt.so C) Unpack and install the LTIB source package and assume done on the home directory: $ cd ~ $ tar -zxvf L2.6.35_1.1.0_130130_source.tar.gz $ ./L2.6.35_1.1.0_130130_source/install After that, you will find ~/ltib directory created D) Apply the patch to make L2.6.35_1.1.0_130130 could be installed and compiled on Ubuntu 13.10 64bit OS $ cd ~/ltib $ git apply 0001_make_L2.6.35_1.1.0_130130_compile_on_ubuntu_13.10_64bit_OS.patch What the patch is doing: a) The patch modifies the following files: dist/lfs-5.1/base_libs/base_libs.spec dist/lfs-5.1/elftosb/elftosb.spec dist/lfs-5.1/lkc/lkc.spec dist/lfs-5.1/mux_server/mux_server.spec dist/lfs-5.1/ncurses/ncurses.spec b) Add the following files to the pkgs directory: pkgs/elftosb-2.6.35.3-1385779630.patch pkgs/elftosb-2.6.35.3-1385779630.patch.md5 pkgs/lkc-1.4-lib.patch pkgs/lkc-1.4-lib.patch.md5 E) Then, it is ready to proceed the rest of the LTIB env setup process: $ cd ~/ltib $ ./ltib -m config $ ./ltib Reference: L2.6.35_1.1.0_130130_docs/doc/mx28/Setting_Up_LTIB_Host_on_Ubuntu_9_04.pdf https://community.freescale.com/docs/DOC-93394 https://community.freescale.com/message/332385#332385 https://community.freescale.com/thread/271675 https://community.freescale.com/message/360556#360556 scrollkeeper is for the gnome-desktop compilation elftosb compilation issue fixed by added -lm to LIBS in the elftosb-2.6.35.3-1.1.0/makefile.rules NOTE: When compiling gstreamer, this warning was pop up.  Just ignore it seems okay.
View full article
This is the procedure and patch to set up Ubuntu 12.04 64bit Linux Host PC and building i.MX28 L2.6.35_1.1.0_130130.  It has been tested to build GNOME profile and with FSL Standard MM codec. A) Basic Requirement: Set up the Linux Host PC using ubuntu-12.04.3-desktop-amd64.iso Make sure the previous LTIB installation and the /opt/freescale have been removed B) Installed the needed packages to the Linux Host PC $ sudo apt-get update $ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev $ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool $ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool $ sudo apt-get install uuid-dev liblzo2-dev $ sudo apt-get install tcl dpkg $ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev $ sudo apt-get install texlive texinfo $ sudo apt-get install ia32-libs libc6-dev-i386 lib32z1 $ sudo apt-get install uboot-mkimage $ sudo apt-get install scrollkeeper $ sudo apt-get install gparted $ sudo apt-get install nfs-common nfs-kernel-server $ sudo apt-get install git-core git-doc git-email git-gui gitk $ sudo apt-get install meld atftpd C) Unpack and install the LTIB source package and assume done on the home directory: $ cd ~ $ tar -zxvf L2.6.35_1.1.0_130130_source.tar.gz $ ./L2.6.35_1.1.0_130130_source/install After that, you will find ~/ltib directory created D) Apply the patch to make L2.6.35_1.1.0 could be installed and compiled on Ubuntu 12.04 64bit OS $ cd ~/ltib $ git apply 0001_make_L2.6.35_1.1.0_130130_compile_on_ubuntu_12.04_64bit_OS.patch a) The patch modifies the following files:    dist/lfs-5.1/base_libs/base_libs.spec    dist/lfs-5.1/lkc/lkc.spec    dist/lfs-5.1/mux_server/mux_server.spec    dist/lfs-5.1/ncurses/ncurses.spec b) Add the following files to the pkgs directory:    pkgs/lkc-1.4-lib.patch    pkgs/lkc-1.4-lib.patch.md5 E) Then, it is ready to proceed the rest of the LTIB env setup process: $ cd ~/ltib $ ./ltib -m config $ ./ltib Reference: L2.6.35_1.1.0_130130_docs/doc/mx28/Setting_Up_LTIB_Host_on_Ubuntu_9_04.pdf https://community.freescale.com/docs/DOC-93394 https://community.freescale.com/message/332385#332385 https://community.freescale.com/thread/271675 https://community.freescale.com/message/360556#360556 scrollkeeper is for the gnome-desktop compilation NOTE: When compiling gstreamer, this warning was pop up.  Just ignore it seems okay.
View full article
This is the procedure and patch to set up Ubuntu 12.04 64bit Linux Host PC and building i.MX6x L3.0.35_4.1.0.  It has been tested to build GNOME profile and with FSL Standard MM Codec for i.MX6Q SDB board. A) Basic Requirement: Set up the Linux Host PC using ubuntu-12.04.3-desktop-amd64.iso Make sure the previous LTIB installation and the /opt/freescale have been removed B) Installed the needed packages to the Linux Host PC $ sudo apt-get update $ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev $ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool $ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool $ sudo apt-get install uuid-dev liblzo2-dev $ sudo apt-get install tcl dpkg $ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev $ sudo apt-get install texlive texinfo $ sudo apt-get install ia32-libs libc6-dev-i386 lib32z1 $ sudo apt-get install uboot-mkimage $ sudo apt-get install scrollkeeper $ sudo apt-get install gparted $ sudo apt-get install nfs-common nfs-kernel-server $ sudo apt-get install git-core git-doc git-email git-gui gitk $ sudo apt-get install meld atftpd C) Unpack and install the LTIB source package and assume done on the home directory: $ cd ~ $ tar -zxvf L3.0.35_4.1.0_130816_source.tar.gz $ ./L3.0.35_4.1.0_130816_source/install After that, you will find ~/ltib directory created D) Apply the patch to make L3.0.35_4.1.0 could be installed and compiled on Ubuntu 12.04 64bit OS $ cd ~/ltib $ git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_12.04_64bit_OS.patch The patch modifies the following files: dist/lfs-5.1/base_libs/base_libs.spec dist/lfs-5.1/ncurses/ncurses.spec E) Then, it is ready to proceed the rest of the LTIB env setup process: $ cd ~/ltib $ ./ltib -m config $ ./ltib Reference: L3.0.35_4.1.0_130816_docs/doc/mx6/Setting_Up_LTIB_host.pdf https://community.freescale.com/message/332385#332385 https://community.freescale.com/thread/271675 https://community.freescale.com/message/360556#360556 scrollkeeper is for the gnome-desktop compilation NOTE: When compiling gstreamer, this warning was pop up.  Just ignore it seems okay.
View full article
This is a hardware design checklist for i.MX28. Please go through this checklist and check your design before requesting a schematics review. Arthur
View full article
Tel Aviv, December 2013   Variscite announces the support of Yocto over its iMX6 System-on-Modules   Variscite, a leading manufacturer of embedded solutions and System-on-Modules and Freescale’s Connected Partner, is pleased to announce the support of Yocto v4.1 Dora release over all Variscite’s iMX6 embedded products. Variscite develops, produces and manufactures a powerful range of System-on-Modules (SoM) and Single-Board-Computers (SBC), consistently setting market benchmarks in terms of speed and innovation. Today Variscite’s cost sensitive high performance portfolio serves over a thousand c ustomers in over 50 countries worldwide. The Yocto project was announced in 2010 to enable the creation of Linux distributions for embedded software that are independent of the underlying architecture of the embedded software itself. Variscite’s support of Yocto over its iMX6 solutions aligns with the company’s strategy to provide its customers with a complete set of leading embedded software and hardware solution, reducing development risk, cost and time-to-market. Variscite’s Yocto v4.1 Dora release supports iMX6 Solo, Dual Lite, Dual and Quad processors with a variety of speed grades, memory sizes and interfaces. More information can be found in: http://www.variwiki.com/index.php?title=Yocto_V4.1_Dora#Supported_hardware_and_features   About Variscite:   In less than a decade Variscite has taken a leading position in the System-on-Modules (SoM) design and manufacturing market. A trusted provider of development and consulting services for a variety of embedded platforms, Variscite transforms clients’ visions into successful products. Learn more about Variscite by visiting: www.variscite.com or contacting: Variscite Sales, [email protected] , +972-9-9562910
View full article
The attached patches slow-down the DDR's clock (from 528000000Hz to 396000000Hz) on i.MX6Q Sabre SDB-P boards. These were tested on Android JB4.2.2_1.0.0 and Linux L3.0.35_4.1.0. To verify patches were correctly applied, one the serial console one should see the following TWO bold lines Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ] Boot Device: MMC I2C:   ready DRAM:   1 GB MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3 *** Warning - bad CRC or MMC, using default environment mx6q pll1: 792MHz mx6q pll2: 528MHz mx6q pll3: 480MHz mx6q pll8: 50MHz ipg clock     : 49500000Hz ipg per clock : 49500000Hz uart clock    : 80000000Hz cspi clock    : 60000000Hz ahb clock     : 99000000Hz axi clock   : 198000000Hz emi_slow clock: 99000000Hz ddr clock     : 396000000Hz usdhc1 clock  : 198000000Hz usdhc2 clock  : 198000000Hz usdhc3 clock  : 198000000Hz usdhc4 clock  : 198000000Hz nfc clock     : 24000000Hz In:    serial Out:   serial Err:   serial Found PFUZE100! deviceid=10,revid=10 Net:   got MAC address from IIM: 00:04:9f:02:67:46 FEC0 [PRIME] Hit any key to stop autoboot:  0 kernel   @ 10808000 (4709060) ramdisk  @ 11800000 (183100) kernel cmdline:     use boot.img command line:     console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale Starting kernel ... Uncompressing Linux... done, booting the kernel. . . . sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms Set periph_clk's parent to pll2_pfd_400! arm_max_freq=1.2GHz . . .
View full article
Question: What is the correct path for the buffer generated by the GPU and sent to the display? When referring to Linux Manual Chapter 5 "Image Processing Unit (IPU) Drivers" and sect.37.5.68 "Current Buffer Register 0". i.MX6DQ Reference Manual (rev.1  4/2013) and further on text and associated with buffer events interrupts. A lot of printouts in the mxc_ipuv3_fb.c file have been added and in other files located in the drivers/video/mxc/ directory and still unable to capture the interrupt generated by the IPU. An open GL buffer (using the GLES and EGL) is generated with the frame buffer mechanism to a monitor connected to the HDMI output on the evaluation board. Direct it to /dev/fb0. The following functions are used to create EGL context fbGetDisplayByIndex(0) fbCreateWindow(…); Everything works and openGL on the monitor can be seen. To measure how long it takes for the data to be sent to the display/monitor after the buffer is ready in the GPU, can it be done in the IPU if where it is performed is known? Where is the exact location where the interrupt can be captured. The ltib on the Ubuntu 12.04 OS (the alsa-utils package was also installed using some patch)) is installed. Answer: GPU EGL swapbuffer is asyncronous. It means when you call swapbuffer it will not be displayed immediately. If will just flush the command buffer and when the GPU completes the frame, it will be displayed to the scree, To make sure the frame is complete, use glFinish after eglswapbuffer. Also please try with simple program rather using GPU driver to measure time to display on the screen. Swapbufferinterval will work when FB_MULTI_BUFFER = 2. By default it will be 1.
View full article
To build Android version earlier than Lollipop from source code, you need the Sun's 1.6 SDK to be installed for ubuntu as the link Initializing a Build Environment | Android Developers. You may still cannot get the Sun's JDK  with below instruction: $ sudo add-apt-repository "deb http://archive.canonical.com/ lucid partner" $ sudo apt-get update $ sudo apt-get install sun-java6-jdk    There are below options to help install the Sun's JDK  if you cannot find a valid source through apt-get commands: $ wget --no-cookies --header "Cookie: gpw_e24=http%3A%2F%2Fwww.oracle.com%2F" http://download.oracle.com/otn-pub/java/jdk/6u45-b06/jdk-6u45-linux-x64.bin $ chmod u+x jdk-6u45-linux-x64.bin $ ./jdk-6u45-linux-x64.bin $ sudo mv jdk1.6.0_45 /opt $ sudo update-alternatives --install /usr/bin/java java /opt/java/64/jdk1.6.0_45/bin/java 1 $ sudo update-alternatives --install /usr/bin/javac javac /opt/java/64/jdk1.6.0_45/bin/javac 1 $ sudo update-alternatives --install /usr/bin/jar jar /opt/java/64/jdk1.6.0_45/bin/jar 1 # if you have already install some other version of JDK, please export the JAVA_HOME env before your android build every time $ export JAVA_HOME=/opt/jdk1.6.0_45/ #or you can directly link the java binary to the sdk version you need as below: sudo ln -s /opt/java/64/jdk1.6.0_45/bin/jar /bin/jar sudo ln -s/opt/java/64/jdk1.6.0_45/java /bin/java sudo ln -s/opt/java/64/jdk1.6.0_45/javac /bin/javac sudo ln -s/opt/java/64/jdk1.6.0_45/javah /bin/javah sudo ln -s/opt/java/64/jdk1.6.0_45/javadoc /bin/javadoc sudo ln -s/opt/java/64/jdk1.6.0_45/javaws /bin/javaws    To built the Android version Lollipop and Marshmallow from source code, you need the OpenJDK 7 to be installed for ubuntu as the link Initializing a Build Environment | Android Developers. $ sudo apt-get update $ sudo apt-get install openjdk-7-jdk You may have both openjdk7 and SUN JDK 1.6 intalled in your ubuntu to build different Android version. If you have default java SDK to be Sun's JDK 1.6, you can just use below commands to make android build system use the openjdk7 for Lollipop built $ export JAVA_HOME=/usr/lib/jvm/java-7-openjdk-amd64/ $ cd myandroid $ . ./build/envsetup.sh           //be sure to resetup the envsetup, and pick the platform to be built $ lunch
View full article
Question: The code signing tool(CST) of i.MX6 with "CST -h" command just for viewing help message took about 22 minutes. On other system, it was shorter but still took about 2 minutes. CST version is BLN_CST_MAIN_02.00.00. More test results: 1. Print help message => 4 min. dnlk@bauer-mm2014:~/secureboot/bBLN_CST_MAIN_02.00.00/linux$ date && ./cst --help && date Fri Oct 18 14:10:52 KST 2013 Fri Oct 18 14:15:01 KST 2013 2. Signing 512MB file => 11 min. dnlk@bauer-mm2014:~/secureboot/bBLN_CST_MAIN_02.00.00/linux$ date && ./cst --output "out_system.csf" < "example_system.csf" && date Fri Oct 18 14:15:01 KST 2013 CSF Processed successfully and signed data available in out_system.csf Fri Oct 18 14:25:47 KST 2013 3. Signing 3MB file => 17 min. dnlk@bauer-mm2014:~/secureboot/bBLN_CST_MAIN_02.00.00/linux$ date && ./cst --output "out_kernel.csf" < "example_kernel.csf" && date Fri Oct 18 14:25:47 KST 2013 CSF Processed successfully and signed data available in out_kernel.csf Fri Oct 18 14:42:39 KST 2013 4. Signing 160KB file => 2 min. dnlk@bauer-mm2014:~/secureboot/bBLN_CST_MAIN_02.00.00/linux$ date && ./cst --output "out_uboot.csf" < "example_uboot.csf" && date Fri Oct 18 14:42:39 KST 2013 CSF Processed successfully and signed data available in out_uboot.csf Fri Oct 18 14:45:05 KST 2013 Answer: The slow performance is caused by lack of entropy source and it takes long time to initialize random number generator. Check amount of entropy  "cat /proc/sys/kernel/random/entropy_avail" Tried to install package rng-tools. 1. $sudo apt-get install rng-tools 2. add the following settings in /etc/default/rng-tools HRNGDEVICE=/dev/urandom RNGDOPTIONS=”-W 90% -t 1? 3. sudo /etc/init.d/rng-tools restart 4. cat /proc/sys/kernel/random/entropy_avail After rng-tools starts, entropy increases from less than 100 to more than 1000, then command ./cst -h can run very smoothly.
View full article
This is a copy of the currently posted i.MX25 reference manual to be used to enter community comments.  Please feel free to add inline comments in this reference manual. You can point out where more information is needed or where existing information is incorrect.  You can also enter information in your comment that expands on existing information in the document, based on your experience with the device.  If you are pointing out that more information is needed in a paragraph or a section, please be very specific, not “needs more information”.  Your comments in this manual may help other members and will drive improvements in this and future documentation. Note: The doc viewer does not support going directly to a specified page.  Instead of manually paging through one page at a time, you can do a search on a string on a page such as "types of resets", or you can go to chapter links listed in the inline comments.  To do this, page down to the comments below the doc view, select "Inline Comments", sort the comments by "page", and then select the chapter you want to view.
View full article