i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
MX7D_DDR3_压力测试应用手册_V1_201611108.doc
View full article
MX6UL_DDR3_调校_应用手册_V3_20160511.doc
View full article
MX6X_DDR3_调校_应用手册_V4_20150730.doc
View full article
MX6X_eMMC_turning_2014.11.11_V2.doc
View full article
MX6X_Uboot_V1-20130910.doc: 3.0.35: 3.0.35
View full article
i.MX6X_内核驱动代码与定制_V2-20150518.doc: 3.0.35
View full article
MX6X_3.14.28_Uboot_V1-20150917.doc
View full article
i.MX6X_3.14.28_内核驱动代码与定制_devicetree_V1-20150918.doc
View full article
Issue: kernel panic when repeating plug/unplug USB device(e.g. USB flash disk) in Linux 4.1.15 The issue is in kernel BLOCK DEVICE, this is not a hardware related issue(happens to all devices running L4.1.15 or L4.4.x), please refer to following link on kernel.org for more details and fixes: blockdev kernel regression (bugzilla 173031) - Patchwork 
View full article
The Linux L4.1.15_2.0.3 Patch for i.MX 6ULL@900MHz Release is now available on www.nxp.com. BSP Updates and Releases -> Linux -> Linux 4.1.15_2.0.3 Patch.   Files available: # Name Description 1 L4.1.15_2.0.3_6ULL_patch_images.tar.gz i.MX 6ULL-EVK@900MHz Linux Binary Demo Files   Information of release, see: README: http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/tree/README?h=imx-4.1-krogoth ChangeLog: http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/tree/ChangeLog?h=imx-4.1-krogoth
View full article
On L4.1.15 BSP, PWM output clock may be not stable, for example, it may switch between 200KHz and 50KHz. PWM clock source is perclk, in running mode, perclk is 24MHz, while in low power idle mode, perclk is reduced to 6MHz, so PWM output clock is reduced to 1/4. To keep PWM output stable clock, we should let perclk stay in 24MHz in low power idle mode. Attached is the patch for 6UL and 6ULL.
View full article
The i.MX Android N7.1.1_1.0.0 release is now available on Web Site (i.MX6 BSP Updates and Releases -> Android).   Files available: # Name Description 1 android_N7.1.1_1.0.0_docs.tar.gz i.MX Android N7.1.1_1.0.0 BSP Documentation 2 android_N7.1.1_1.0.0_source.tar.gz Source Code of Android N7.1.1_1.0.0 BSP (4.1 kernel) for i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo  i.MX 6Sololite, i.MX6SX and i.MX7D 3 android_N7.1.1_1.0.0_image_6dqpsabreauto.tar.gz Binary Demo Files of Android N7.1.1_1.0.0 BSP - SABRE for Automotive Infotainment based on i.MX 6QuadPlus, i.MX 6Quad, and i.MX 6DualLite 4 android_N7.1.1_1.0.0_image_6dqpsabresd.tar.gz Binary Demo Files of Android N7.1.1_1.0.0 BSP - SABRE Platform and SABRE Board based on i.MX 6QuadPlus, i.MX 6Quad and i.MX 6DualLite. 5 android_N7.1.1_1.0.0_image_6slevk.tar.gz Binary Demo Files of Android N7.1.1_1.0.0 BSP - i.MX 6Sololite evaluation kit. 6 android_N7.1.1_1.0.0_image_6sxsabresd.tar.gz Binary Demo Files of Android N7.1.1_1.0.0 BSP - SABRE Board based on i.MX 6SoloX 7 android_N7.1.1_1.0.0_image_6sxsabreauto.tar.gz Binary Demo Files of Android N7.1.1_1.0.0 BSP - SABRE for Automotive infotainment based on i.MX 6SoloX 8 android_N7.1.1_1.0.0_image_7dsabresd.tar.gz Binary Demo Files of Android N7.1.1_1.0.0 BSP - SABRE Board based on i.MX 7Dual 9 android_N7.1.1_1.0.0_tools.tar.gz Manufacturing Toolkit and VivanteVTK for N7.1.1_1.0.0   Supported Hardware SoC/Boards: MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-SD board and platform MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI board and platform MX 6SoloLite EVK platform MX 6SoloX SABRE-SD board and platforms MX 6SoloX SABRE-AI board and platforms MX 7Dual SABRE-SD board and platform   Changes: Compared to the M6.0.1_2.1.0 release, this release has the following major changes: Upgraded the Android platform version to Android 7.1. Upgraded the U-Boot and Linux Kernel Code base from the L4.1.15_1.0.0 release to the L4.1.15_1.2.0-ga release. Added support for the i.MX 7Dual SABRE-SD board. Upgraded the GPU driver from 5.0.11p8 to 6.2.0.p2.   Feature: For features please consult the release notes.   Known issues For known issues and more details please consult the Release Notes.
View full article
        The document will introduce how to setup cross‐compiling environment for android android7.1.1 BSP on Ubuntu 16.04.2 LTS, The purpose is to help i.MX customers create android BSP environment quickly, from this, save customer’s time and let them focus on the development of their product. Customer can compile android7.1.1 BSP according to the following steps: ‐‐Installing Ubuntu160.4.2 LTS 1. Running software updater to update system       Customer can download ubuntu‐16.04.2‐desktop‐amd64.iso from https://www.ubuntu.com/download/desktop Then install it to VMware workstation player v12 or PC, after finishing installation, use “Software Updater” to update system. 2. Installing necessary packages    Before compiling android7.1.1 source code, we need to install some neccesary software packages, see following, please! $ sudo apt-get install gnupg $ sudo apt-get install flex $ sudo apt-get install bison $ sudo apt-get install gperf $ sudo apt-get install build-essential $ sudo apt-get install zip $ sudo apt-get install zlib1g-dev $ sudo apt-get install libc6-dev $ sudo apt-get install lib32ncurses5-dev $ sudo apt-get install x11proto-core-dev $ sudo apt-get install libx11-dev $ sudo apt-get install lib32z1-dev $ sudo apt-get install libgl1-mesa-dev $ sudo apt-get install tofrodos $ sudo apt-get install python-markdown $ sudo apt-get install libxml2-utils $ sudo apt-get install xsltproc $ sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 $ sudo apt-get install gcc-multilib g++-multilib $ sudo apt-get install subversion $ sudo apt-get install openssh-server openssh-client $ sudo apt-get install uuid uuid-dev $ sudo apt-get install zlib1g-dev liblz-dev $ sudo apt-get install liblzo2-2 liblzo2-dev $ sudo apt-get install lzop $ sudo apt-get install git-core curl $ sudo apt-get install u-boot-tools $ sudo apt-get install mtd-utils $ sudo apt-get install android-tools-fsutils $ sudo apt-get install openjdk-8-jdk 3. Downloading android7.1.1 source code, u‐boot, linux kernel 3.1 Downloading android7.1.1 source code 3.1.1 Getting source code from google .    if users can access google site, she can get source code accroding to steps in "Android_User's_Guide.pdf" released by NXP 3.1.2 Getting source code from the server of tsinghua university( this is for customer in China ) Steps: (1) Getting repo # cd ~ # mkdir myandroid # mkdir bin # cd bin # git clone https://aosp.tuna.tsinghua.edu.cn/android/git-repo.git/ # cd git‐repo # cp ./repo ../ (2) Modifying repo File Open ~/bin/repo file with 'gedit' and Change google address From REPO_URL = 'https://gerrit.googlesource.com/git-repo' To REPO_URL = ' https://gerrit-google.tuna.tsinghua.edu.cn/git-repo (3) Setting email address # cd ~/myandroid # git config --global user.email "email address" # git config --global user.name "name" [ Email & Name should be yours] (4) Modifying manifest.xml # ~/bin/repo init -u https://aosp.tuna.tsinghua.edu.cn/android/platform/manifest -b android-7.1.1_r13 # cd ~/myandroid/.repo # gedit manifest.xml Then change the value of fetch to " https://aosp.tuna.tsinghua.edu.cn/android/ ", like following: <manifest> <remote name="aosp" fetch="https://aosp.tuna.tsinghua.edu.cn/android/" /> <default revision="refs/tags/android-5.1.1_r1" ...... (5) # ~/bin/repo sync [Note] During runing repo sync, maybe errors will occur like the following: ...... * [new tag] studio‐1.4 ‐> studio‐1.4 error: Exited sync due to fetch errors Then 'repo sync' exits. But don't worry about it, continue to run the command please ! " ~/bin/repo sync", downloading source code will be continous. 3.2 Getting uboot source code $ cd ~/myandroid/bootable $ mkdir bootloader $ cd bootloader $ git clone git://git.freescale.com/imx/uboot-imx.git uboot-imx $ cd uboot-imx $ git checkout n7.1.1_1.0.0-ga 3.3 Downloading linux kernel $ cd ~/myandroid $ git clone git://git.freescale.com/imx/linux-imx.git kernel_imx $ cd kernel_imx $ git checkout n7.1.1_1.0.0-ga 4. Downloading android7.1.1 BSP source code and patch it above source code 4.1 Android7.1.1 BSP can be downloaded from the link: Android OS for i.MX Applications Processors|NXP  ---Board Support Packages (66) After downloading it, copy it to /opt/ 4.2 Patch it to android source code $ cd ~/myandroid $ source /opt/android_N7.1.1_1.0.0_source/code/N7.1.1_1.0.0/and_patch.sh $ help $ c_patch /opt/android_N7.1.1_1.0.0_source/code/N7.1.1_1.0.0/ imx_N7.1.1_1.0.0 If everything is OK, "c_patch" generates the following output to indicate the successful patch: 5. Compiling android7.1.1 BSP source code for i.MX boards $ export ARCH=arm $ export CROSS_COMPILE=~/myandroid/prebuilts/gcc/linux-x86/arm/armlinux-androideabi-4.9/bin/arm-linux-androideabi- $ cd ~/myandroid $ source build/envsetup.sh $ lunch sabresd_6dq-user $ make –j2   (Using 2 CPU cores to compile) Probably, users will enconter this error during compiling: [Solve it like this:] $ export ANDROID_JACK_VM_ARGS="-Dfile.encoding=UTF-8 -XX:+TieredCompilation -Xmx4g" $  cd ~/myandroid $ ./prebuilts/sdk/tools/jack-admin kill-server then run "make " to continue compiling. After compiling, we can see images in output path: -------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------- Hope above items can help you! If customers have questions about the document, she can submit case to me by our saleforce system. the following is how to submit cases to us: ******************************************************************************************************************************************* In case a new customer is asking how to submit a technical case on nxp.com ,here is a template for your reference. 1) Please visit www.nxp.com and click on Support on the top of the webpage. 2) Select Sales and Support under Support Resources session. 3) Scroll down to the bottom ,click on “hardware & Software” . 4) Register by your business email to enter NXP Community 5) Get verification email and verify your account. 6) Select "contact support" on the top and click “submit a new case” to start the process. ******************************************************************************************** Then label : "please forward it to TIC Weidong Sun" in your content , I can get it. NXP TIC team Weidong.Sun 2017-03-16 in Shanghai China
View full article
Overview As more and more communication required between online and offline, the QR code is widely used in the mobile payment, mobile small apps, industry things identification and etc. The i.MX6UL/ULL has the IP of CSI and PXP for camera connection and image CSC/FLIP/ROTATION acceleration. A LCDIF IP is supporting the display, but no 3D IP support. This means this low power and low end AP is very suitable for the industry HMI segment, which does not require a cool 3D graphic display, but a simple and straightforward GUI for interaction. QR code scanner is one of the use cases in the industry segment, which more and more customer are focusing on. The i.MX6UL CPU freq of i.MX6UL is about 500Mhz, and it does not have GPU IP, so a lightweight GUI and window system is required. Here we recommend the QT with wayland backend (without X11), which would make the window system small and faster than traditional X11 UI. Why chose QT is because of it has open source version, rich components, platform independent, good performance for embedded system and strong development staffs like QtCreator for creating application. How to enable the QT development environment, check this: Enable QT developement for i.MX6UL (v2)  Here I made a QR code scanner demo based on QT5.6 + QZXing (QR/Bar code scan engine) running on the i.MX6UL EVK board with a UVC camera (at least 640x480 resolution is required) and 480x272px LCD. Source code is open here (License Apache2.0): https://github.com/muddog/QRScanner  Implementation To do camera preview and capture, you must think on the gstreamer first, which is easy use and has the acceleration pads which implemented by NXP for i.MX6UL. Yes, it's very easy for you to enable the preview in console like: $ gst-launch-1.0 v4l2src device=/dev/video1 ! video/x-raw,format=YUY2,width=640,height=320 ! imxvideoconvert_pxp ! video/x-raw,format=RGB16 ! waylandsink It works under the i.MX6UL EVK, with PXP IP to do color space convert from YUY2 -> RGB16 acceleration, also the potential scaling of the image. The CPU loading of this is about 20-30%, but if you use the component of "videoconvert" to replace the "imxvideoconvert_pxp", we do CSC and scale by CPU, then the loading would increase to 50-60%. The "/dev/video1" is the device node for UVC camera, it may different in your environment. So our target is clear, create such pipeline (with PXP acceleration) in the QT application, and use a appsink to get preview images, do simple "sink" to one QWidget by drawing this image on the widget surface for preview (say every 50ms for 20fps). Then in other thread, we fetch the preview buffer in a fixed frequency (like every 0.5s), then feed it into the ZXing engine to decode the strings inside this image. Here are the class created inside the source code: ScannerQWidgetSink It act as a gstreamer sink for preview rendering. Init the pipeline, create a timer with timeout every 50ms. In the timer handler, we use appsink to copy the camera buffer from gstreamer, and tell the ViewfinderWidget to do update (re-draw event). ViewfinderWidget This class inherit from the QWidget, which draw the preview buffer as a QImage onto it's own surface by using QPainter. The QImage is created at the very begining with the image buffer created by the ScannerQWidgetSink. Because QImage itself does not maintain the image buffer, so the buffer must be alive during it's usage. So we keep this buffer during the ScannerQWidgetSink life cycle, copy the appsink buffer from pipeline to it for preview. MainWindow Create main window, which does not have title bar and border. Start any animation for the red line scan bar. Create instance of DecoderThread and ScannerQWidgetSink. Setup and start them. DecoderThread A infinite loop, to wait for a available buffer released by the ScannerQWidgetSink every 0.5s. Copy the buffer data to it's own buffer (imgData) to avoid any change to the buffer by sink when doing decoding. Then feed this copy of buffer into ZXing engine to get decoder result. Then show on the QLabel. Screenshot under wayland (weston) desktop: Customize Camera instance Now I use the UVC camera which pluged in the USB host, which device node is /dev/video1. If you want to use CSI or other device, please change the construction parameters for ScannerQWidgetSink(): sink = new ScannerQWidgetSink(ui->widget, QString("v4l2src device=/dev/video1")); Image resolution captured and review Change the static member value of ScannerQWidgetSink class: uint ScannerQWidgetSink::CAPTURE_HEIGHT = 480; uint ScannerQWidgetSink::CAPTURE_WIDTH = 640; Preview fps and decoding frequency Find the "framerate=20/1" strings in the ScannerQWidgetSink::GstPipelineInit(), change to your fps. You also have to change the renderTimer start timeout value in the ::StartRender(). The decoding frequency is determined by renderCnt, which determine after how many preview frames showed to feed the decoder. Main window size It's fixed size of main window, you have to change the mainwindow.ui. It's easy to do in the QtCreate Designer. FAQ Why not use CSI camera in demo? Honestly, I do not have CSI camera module, it's also DNP when you buying the board on NXP.com. So a widely used UVC camera is preferred, it's also easy for you to scan QR code on your phone, your display panel etc. Why not use QCamera to do preview and capture? The QCamera class in the Qtmultimedia component uses the camerabin2 gstreamer plugin, which create a very long pipeline for different usage of viewfinder, image capture and video encoder. Camerabin2 would eat too much CPU and memory resource, take picture and recording are very very slow. The preview of 30fps would eat about 70-80% CPU loading even I hacked it using imxvideoconvert_pxp instread of software videoconvert. Finally I give up to implement the QRScanner based on QCamera. How to make sure only one instance of QT app is running? We can use QSharedMemory to create a share memory with a unique KEY. When second instance of app is started, it would check if the share memory with this KEY is created or not. If the shm is there, it means there's already one instance running, it has to exit(). But as the QT mentioned, the QSharedMemory can not be destroyed correctly when app crashed, this means we have to handle each terminate signal, and do delete by ourselves: static QSharedMemory *gShm = NULL; static void terminate(int signum) {    if (gShm) {       delete gShm;       gShm = NULL;    }    qDebug() << "Terminate with signal:" << signum;    exit(128 + signum); } int main(int argc, char *argv[]) {    QApplication a(argc, argv);    // Handle any further termination signals to ensure the    // QSharedMemory block is deleted even if the process crashes    signal(SIGHUP, terminate ); // 1    signal(SIGINT, terminate ); // 2    signal(SIGQUIT, terminate ); // 3    signal(SIGILL, terminate ); // 4    signal(SIGABRT, terminate ); // 6    signal(SIGFPE, terminate ); // 8    signal(SIGBUS, terminate ); // 10    signal(SIGSEGV, terminate ); // 11    signal(SIGSYS, terminate ); // 12    signal(SIGPIPE, terminate ); // 13    signal(SIGALRM, terminate ); // 14    signal(SIGTERM, terminate ); // 15    signal(SIGXCPU, terminate ); // 24    signal(SIGXFSZ, terminate ); // 25    gShm = new QSharedMemory("QRScannerNXP");    if (!gShm->create(4, QSharedMemory::ReadWrite)) {       delete gShm;       qDebug() << "Only allow one instance of QRScanner";       exit(0);    } .....
View full article
Following docs(English or Chinese version) are also can be referred as a hand on guide. Freescale i.MX6 DRAM Port Application Guide-DDR3  飞思卡尔i.MX6平台DRAM接口高阶应用指导-DDR3篇    Please find i.Mx6DQSDL LPDDR2 Script Aid through below link. i.Mx6DQSDL LPDDR2 Script Aid  Please find i.Mx6DQSDL DDR3 Script Aid through below link. i.MX6DQSDL DDR3 Script Aid  Please find i.MX6SX DDR3 Script Aid through below link. i.MX6SX DDR3 Script Aid  Please find i.MX6SL LPDDR2 Script Aid through below link. i.MX6SL LPDDR2 Script Aid  Please find i.MX6UL DDR3 Script Aid through below link.. https://community.nxp.com/docs/DOC-329899  Please find i.MX6UL LPDDR2 Script Aid through below link. i.MX6UL_LPDDR2_Script_Aid  Please find i.MX6ULL DDR3 Script Aid through below link. i.MX6ULL_DDR3_Script_Aid 
View full article
Following docs(English or Chinese version) are also can be referred as a hand on guide. Freescale i.MX6 DRAM Port Application Guide-DDR3 飞思卡尔i.MX6平台DRAM接口高阶应用指导-DDR3篇   Please find i.Mx6DQSDL LPDDR2 Script Aid through below link. i.Mx6DQSDL LPDDR2 Script Aid  Please find i.Mx6DQSDL DDR3 Script Aid through below link. i.MX6DQSDL DDR3 Script Aid  Please find i.MX6SX DDR3 Script Aid through below link. i.MX6SX DDR3 Script Aid  Please find i.MX6SL LPDDR2 Script Aid through below link.. i.MX6SL LPDDR2 Script Aid  Please find i.MX6UL DDR3 Script Aid through below link. I.MX6UL DDR3 Script Aid  Please find i.MX6UL LPDDR2 Script Aid through below link. i.MX6UL_LPDDR2_Script_Aid  Please find i.MX6ULL LPDDR2 Script Aid through below link. i.MX6ULL_LPDDR2_Script_Aid 
View full article
When configuring i.MX6 IPU IDMAC CPMEM parameters or debugging it, it's hard to find the value of a parameter inside the 160 bits word. This web tool separates the 160 bits words into parameters making it easier to check their values. Link: i.MX Tools 
View full article
Dear,   We want to start application program from bootloader, we have below questions: We we use I.MX6UL bootrom start BootLoader, we need use mkimage.sh, compile and generator bin file, then we convert to executable file. If we need use Bootloader run application program,whether application image also need convert by mkimage.sh?  The file which convert by mkimage.sh is compressed file. we do not know its format, how about its start address, how to realize the the address jump, do you have example? Thanks.  
View full article
I have a few questions about the various reference designs for the i.mx6UL. Please see the attachment for specifics.
View full article
i.MX 6 SoloX MCC MCC is a library for lightweight communication between cores Configured at compile time (mcc_config.h) Current version (2.0) is not backward compatible MCC works with shared memory area Communication is performed through ‘send’ and ‘receive’ functions Shared memory Cores communicate through shared memory Core structures of the MCC  MCC_ENDPOINT core Identifies a processor core, A9 is 0 and M4 is 1. node In Linux, each process using MCC has its own node number. MQX has only one node number. port Any number of ports per node is allowed. Value MCC_RESERVED_PORT_NUMBER is not allowed. The number of endpoints in system is defined during compile time by macro MCC_ATTR_MAX_RECEIVE_ENDPOINTS. MCC_BOOKEEPING_STRUCT Endpoint table I. MCC API  Functions Standard API −int mcc_initialize(MCC_NODE); −int mcc_destroy(MCC_NODE); −int mcc_create_endpoint(MCC_ENDPOINT*, MCC_PORT); −int mcc_destroy_endpoint(MCC_ENDPOINT*); −int mcc_send(MCC_ENDPOINT*, MCC_ENDPOINT*, void*, MCC_MEM_SIZE, unsigned int); −int mcc_recv(MCC_ENDPOINT*, MCC_ENDPOINT*, void*, MCC_MEM_SIZE, MCC_MEM_SIZE*, unsigned int); −int mcc_msgs_available(MCC_ENDPOINT*, unsigned int*); −int mcc_get_info(MCC_NODE, MCC_INFO_STRUCT*); MCC_SEND_RECV_NOCOPY_API_ENABLED −int mcc_get_buffer(void**, MCC_MEM_SIZE*, unsigned int); −int mcc_send_nocopy(MCC_ENDPOINT*, MCC_ENDPOINT*, void*, MCC_MEM_SIZE); −int mcc_recv_nocopy(MCC_ENDPOINT*, MCC_ENDPOINT*, void**, MCC_MEM_SIZE*, unsigned int); −int mcc_free_buffer(void*);
View full article