i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
A tutorial on 'Freescale Yocto Project'. Source code is located here NOTE: When doing 'repo init -u .... -b <LATEST_STABLE_BRANCH_NAME>', make sure you are using the latest stable branch (dora is the latest when writing this note)
查看全文
Flashing Kernel and Root File System using RedBoot Creating an image A kernel image and a root file system can be created using All Boards LTIB or compiling the kernel and setting the correct set of files. Create a root file system image from a set of files converting the files to a jffs2 file system. For this, install the package mtd-tools. In Ubuntu type apt-get install mtd-tools For making an root file system for flash, use the jffs2 file system like: mkfs.jffs2 -r rootfs -e 0x20000 -s 0x800 –n -o rootfs.jffs2 Where rootfs/ is the original set of file for the file system and rootfs.jffs2 is the output image file. Flashing Some connections errors can be avoided by Configuring RedBoot. The process below uses TFTP to copy the files between host and target. See All Boards TFTP for detail in configurations. Copy the kernel image and the root file system image to the TFTP dir. For example, in LTIB dir, type sudo cp ./rootfs/boot/zImage /tftpboot sudo cp rootfs.jffs2 /tftpboot/ Where /tftpboot is the dir configured for TFTP The next steps are performed in a Minicom session, and happens on the board. Formatting the flash: Format the flash redboot> fis init -f Make a Bad Block Table redboot> nand scan Flashing kernel Load kernel image (zImage) using the command below. Remember to modify the host IP address: redboot> load -r -b 0x100000 /tftpboot/zImage -h 10.29.244.99 The address 0x100000 is used as a temporary location Create the kernel at the right address (0x100000, for IMX27PDK) redboot> fis create -f 0x100000 kernel Flashing root file system Load root file system image (rootfs.jffs2) to the temporary address. Remember to modify the host IP address: redboot> load -r -b 0x100000 /tftpboot/rootfs.jffs2 -h 10.29.244.99 Create the root file system in the right address (0x600000, for IMX27PDK) redboot> fis create -f 0x600000 root Testing This step can be omitted! You can now load your kernel in the flash by typing: fis load kernel To know if the root file system written in the flash was correctly saved, execute the NFS file system and mount the flash. For load the the root file system by NFS, type: exec -c "noinitrd console=ttymxc0,115200 root=nfs nfsroot=<server_ip>:<root_path_on_server> ip=dhcp" Wait the system go up, then mount the flash at /mnt. Reminde that the flash has a jffs2 file system. mount -t jffs2 /dev/mtdblock4 /mnt ls /mnt List the /mnt contents. The output must be the right file system. For testing root file system on NAND, type exec -c "noinitrd console=ttymxc0,115200 root=/dev/mtdblock4 rw rootfstype=jffs2 ip=dhcp" Modifying the initial script Reset the board and press CTRL-C. Type fc to modify the configurations and insert the initialization script. RedBoot> fc Run script at boot: true Boot script: Enter script, terminate with empty line >> fis load kernel >> exec -c "noinitrd console=ttymxc0,115200 root=/dev/mtdblock4 rw rootfstype=jffs2 ip=dhcp" >> Boot script timeout (1000ms resolution): 1 Use BOOTP for network configuration: false Gateway IP address: 10.29.241.254 Local IP address: 10.29.241.6 Local IP address mask: 255.255.254.0 Default server IP address: 10.29.244.99 Board specifics: 0 Console baud rate: 115200 Set eth0 network hardware address [MAC]: false GDB connection port: 9000 Force console for special debug messages: false Network debug at boot time: false Update RedBoot non-volatile configuration - continue (y/n)? y ... Read from 0x07ee0000-0x07eff000 at 0x00080000: . ... Erase from 0x00080000-0x000a0000: . ... Program from 0x07ee0000-0x07f00000 at 0x00080000: . RedBoot> Remember to save the configuration in the flash by typing y Reset the system. To certify that the board is loading the system from flash, remove the ethernet cable.
查看全文
When to enable CONFIG_DEBUG_LL, choose the debug port and then CONFIG_EARLY_PRINTK on i.MX6, system will hang. There is no error information there as below, Uncompressing Linux... done, booting the kernel. Booting Linux on physical CPU 0x0 Initializing cgroup subsys cpu Initializing cgroup subsys cpuacct Linux version 4.1.15-00001-gd582989-dirty (jay@jay-ubuntu) (gcc version 4.9 20 150123 (prerelease) (GCC) ) #10 SMP PREEMPT Mon Jul 17 15:08:55 CST 2017 CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine model: Freescale i.MX6 Quad SABRE Smart Device Board bootconsole [earlycon0] enabled cma: Reserved 448 MiB at 0x2a000000 Memory policy: Data cache writealloc -------------- hang -----------------‍‍‍‍‍‍‍‍‍‍‍‍‍ The patch fix it on android n7.1.1_1.0.0, kernel: 4.1.15.
查看全文
About softISP Code : https://github.com/NXPmicro/gtec-demo-framework/tree/master/DemoApps/OpenCL/SoftISP/source Document : https://www.nxp.com/docs/en/application-note/AN12060.pdf demo is on path  /opt/imx-gpu-sdk/OpenCL/SoftISP of linux L4.19.35   About eIQ Community: https://community.nxp.com/community/eiq eIQ sample APPs : https://community.nxp.com/docs/DOC-343785 eIQ library source code : https://source.codeaurora.org/external/imx/meta-fsl-bsp-release/tree/imx/meta-ml/recipes-libraries?h=warrior-4.19.35-1.1.0
查看全文
Some i.MX25 customers reported an issue for the GPT timer, when using 120MHz (240MHz UPLL divided 2) clock source as the GPT per_clk, the timer will not be increased all the time in free-run mode. If using 66.5MHz IPG clock and 133MHz PER clock as the clock source, there are no such issue. There are 4 test cases in the attached test code. Case 0: in CCM_MCR, set bit 5 as 0 for 133MHz HCLK as the gpt_per_clk source;  in GPT_CR bit[8:6], set 0b001 ipg_clk (66.5MHz). There is no issue, the GPT counter is fixed at 4 between old_cnt and new_cnt. Case 1: in CCM_MCR, set bit 5 as 0 for 133MHz HCLK as the gpt_per_clk source;  in GPT_CR bit[8:6], set 0b010 ipg_clk_highfreq (133MHz). There is no issue, the GPT counter is fixed at 8 between old_cnt and new_cnt. Case 2: in CCM_MCR, set bit 5 as 1 for 240MHz UPLL divided by 2 as the gpt_per_clk source;  in GPT_CR bit[8:6], set 0b001 ipg_clk (60MHz). There is no issue, the GPT counter is fixed at 4 between old_cnt and new_cnt. Case 3: in CCM_MCR, set bit 5 as 0 for 240MHz UPLL divided by 2 as the gpt_per_clk source;  in GPT_CR bit[8:6], set 0b010 ipg_clk_highfreq (120MHz). There is issue, the GPT counter is not a fixed value between old_cnt and new_cnt, and sometimes it will be negative. Count 9874: 4 old_cnt: 0x188849dc new_cnt: 0x188849e0 Count 9877: 12 old_cnt: 0x18918400 new_cnt: 0x1891840c Count 9915: 4 old_cnt: 0x189aea90 new_cnt: 0x189aea94 Count 9937: -12 old_cnt: 0x18a42458 new_cnt: 0x18a4244c Count 9967: 4 old_cnt: 0x18adb17c new_cnt: 0x18adb180 In fact, it is not an issue, when using UPLL as the GPT clock source, the maxim frequency should be 60MHz. That's why all other three test case is OK and it only failed on this case.
查看全文
Some customer need to know how to add support RS485 mode half duplex? Here give some recommends. About i.MX6 UART to RS485 applications 1. Using RS485 mode of UART directly. On hardware, you should use UART_CTS_B to control RX & TX. On software, The link for you reference: Does UART in RS485 mode support only 9 Bit mode for i.MX6 ?  2. Sensing IO direction Automatically via hardware, don't need to tune software. For i.MX8QXP As the linux BSP for i.MX8QXP do not support RS 485 mode, so for the RS 485 using you can use the Sensing IO direction Automatically via hardware, don't need to tune software. As the above i.MX6 design.
查看全文
Copy redboot binary to /tftpboot. In this case: redboot.bin Load binary file to i.MX RAM memory: RedBoot> load -v -r -b 0x100000 /tftpboot/redboot.bin Run the loaded image RedBoot> run 0x100000 Enable NOR, NAND or MMC flash media for Redboot. In this case, NAND is beeing used. RedBoot> factive nand Update RedBoot in the flash with currently running image RedBoot> romupdate
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-345672 
查看全文
   Some of Chinese customer couldn’t normally download android source code from google site, here give a way to download android source from Mirror site of Tsinghua University. Customers in other areas can refer to the configurations of ubuntu 18.04 in the document. Updating software packages for ubuntu18.04 LTS 1、Using software updater to update software packages Press Install Now button to update software. Restart ubuntu18.04 2、Installing necessary software packages #sudo apt-get install flex # sudo apt-get install bison # sudo apt-get install gperf # sudo apt-get install build-essential # sudo apt-get install zlib1g-dev # sudo apt-get install lib32ncurses5-dev # sudo apt-get install x11proto-core-dev # sudo apt-get install libx11-dev # sudo apt-get install lib32z1-dev # sudo apt-get install libgl1-mesa-dev # sudo apt-get install tofrodos # sudo apt-get install python-markdown # sudo apt-get install libxml2-utils # sudo apt-get install xsltproc # sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 # sudo apt-get install gcc-multilib g++-multilib # sudo apt-get install subversion # sudo apt-get install openssh-server openssh-client # sudo apt-get install uuid uuid-dev # sudo apt-get install zlib1g-dev liblz-dev # sudo apt-get install liblzo2-2 liblzo2-dev # sudo apt-get install lzop # sudo apt-get install git-core curl # sudo apt-get install u-boot-tools # sudo apt-get install mtd-utils # sudo apt-get install android-tools-fsutils # sudo apt-get install openjdk-8-jdk # sudo apt-get install device-tree-compiler # sudo apt-get install aptitude # sudo aptitude install libcurl4-openssl-dev nss-updatedb 3、Downloading and unpacking Android release package https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applications-processors/android-os-for-i.mx-applications-processors:IMXANDROID?tab=Design_Tools_Tab --O8.1.0_1.3.0_ANDROID_SOURCE_8MQ_GA File name is imx-o8.1.0_1.3.0_8m.tar.gz # cd ~ # tar xzvf imx-o8.1.0_1.3.0_8m.tar.gz Downloading android8.1.0-1.3.0 source code Getting repo # cd ~ # mkdir bin # cd bin # curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo # chmod a+x ~/bin/repo # export PATH=${PATH}:~/bin   Modifying repo File Open ~/bin/repo file with 'gedit' and Change google address From REPO_URL = 'https://gerrit.googlesource.com/git-repo' To REPO_URL = 'https://mirrors.tuna.tsinghua.edu.cn/git/git-repo/' 3、Setting email address # git config --global user.email "[email protected]" # git config --global user.name "xxxx" [ Email & Name should be yours] 4、Modifying android setup script and Running it Open ~/ imx-o8.1.0_1.3.0_8m /imx_android_setup.sh and add a line like below: ...       if [ "$rc" != 0 ]; then          echo "---------------------------------------------------"          echo "-----Repo Init failure"          echo "---------------------------------------------------"          return 1       fi find -name 'aosp-O8.1.0-1.3.0.xml'| xargs perl -pi -e 's|https://android.googlesource.com/|https://aosp.tuna.tsinghua.edu.cn/|g' fi   # Don't Delete .repo directory and hidden files #rm -rf $android_builddir/.??* ... Then save it and exit. # cd ~/ # source ~/ imx-o8.1.0_1.3.0_8m/imx_android_setup.sh Then android_build directory is created at ~/ # export MY_ANDROID=~/android_build          48 hours later: Compiling android8.1.0-1.3.0 BSP # cd ~/android_build # gedit ./prebuilts/sdk/tools/jack-admin               And find “JACK_SERVER_COMMAND” ,change it to be: JACK_SERVER_COMMAND="java -XX:MaxJavaStackTraceDepth=-1 -Djava.io.tmpdir=$TMPDIR $JACK_SERVER_VM_ARGUMENTS -Xmx4096m -cp $LAUNCHER_JAR $LAUNCHER_NAME"          Save and exit. And run: # ./prebuilts/sdk/tools/jack-admin stop-server # ./prebuilts/sdk/tools/jack-admin start-server # export ARCH=arm64 # export CROSS_COMPILE=~/android_build/prebuilts/gcc/linux-x86/aarch64/aarch64-linuxandroid-4.9/bin/aarch64-linux-android- # export LC_ALL=C # source build/envsetup.sh # lunch evk_8mq-userdebug               Begin to build android BSP for i.MX8MQ # make –j4 NXP TIC weidong sun 2018-08-15
查看全文
In i.MX51 platfrom the PMIC 13892 also has a internal RTC. We can use this RTC instead of the i.mx51 SRTC. Attached was the implementation of it.
查看全文
Qt Creator can be a very good IDE in order to develop great QT applications. This IDE does not only helps with syntax highlighting, access to examples and tutorials, but also helps you to configure different toolchains Qt binary versions and target options. First download the binary installer from: For 32 bits: $ wget http://releases.qt-project.org/qtcreator/2.6.2/qt-creator-linux-x86-opensource-2.6.2.bin For 64 bits: $ wget http://releases.qt-project.org/qtcreator/2.6.2/qt-creator-linux-x86_64-opensource-2.6.2.bin execute the binary $ ./qt-creator-linux-x86_64-opensource-2.6.2.bin Follow the Installer GUI and choose a location. Default options should be OK. in my case the installation was done here: $ /home/b35153/qtcreator-2.6.2/bin Open Qt Creator (in my case from command line, use "&" to regain control of the terminal) $./qtcreator & Open Tools -> Options Choose Build & Run  on the menu of the left. and Select the Compilers Tab Here you can add the toolchain GCC compiler of your convenience. It will appear in the "Manual"  section. Now click on Qt Version Tab.  Here you can add the Qmake that you had created with your Qt installation; for example, the Qt5 installation described here: Building QT for i.MX6 It will appear in the Manual section. In my case I have Qmake for PC and Qmake for i.MX6. Now click on Kits Tab Here you can create combinations of Compilers and Qmake, and also specify where do you want the executables to go. In my case here I combined the i.MX6 toolchain and the Qmake for I.MX6 i had created. I did not set up device configuration since the sysroot is already shared to my device via NFS, but you can configure it so the files are sent via ssh to your device. And that's It! Next time you load a project you can choose which Kit you want to work on, and it will be compiled just as you need.
查看全文
Attached is a chunk of the filesystem for the Linux Image https://community.freescale.com/docs/DOC-93887
查看全文
ccache is a C compiler cache. ccache can save a large amount of compilation time on recurring builds and builds restarted from a clean repository after make clean or git clean. It is well suited for e.g. u-boot and Linux compilation. Caching the host compiler Caching "native" builds is easily done by adding in the beginning of your $PATH a special directory, which contains links to ccache to override the usual compiler. On e.g. Debian this directory is readily available as /usr/lib/ccache, So you can do:   $ export PATH="/usr/lib/ccache:$PATH" Typical links found in this folder are:   c++ -> ../../bin/ccache   cc -> ../../bin/ccache   g++ -> ../../bin/ccache   gcc -> ../../bin/ccache etc... Caching the cross compiler Caching cross-compiled builds can be done in the same way as native builds, provided you create links of the form e.g. arm-linux-gnueabihf-gcc pointing to ccache. But there is an even more convenient way for those projects, which rely on a $CROSS_COMPILE environment variable (as is the case for e.g. u-boot and Linux). You can prefix the cross compiler with ccache there in e.g. the following way:   $ export CROSS_COMPILE="ccache arm-linux-gnueabihf-" Monitoring efficiency Now that your builds are cached, you might want to see how much is "spared" with this technique. ccache -s will tell you all sorts of statistics, such as:   cache directory                     /home/vstehle/.ccache   cache hit (direct)                 10852   cache hit (preprocessed)            3225   cache miss                         19000   called for link                    33267   called for preprocessing            9463   compile failed                         3   preprocessor error                     1   couldn't find the compiler           117   unsupported source language          921   unsupported compiler option         2167   no input file                      31681   files in cache                     51694   cache size                           1.3 Gbytes   max cache size                       4.0 Gbytes Here you see a somewhat typical 50%/50% hit/miss ratio. Enjoy! See Also ccache is usually supported natively by build systems, such as Buildroot or Yocto.
查看全文
Q: how to do PCIe compliance measurement on the Sabre SDB? Phase Jitter on the PCIe reference clock had been see problem. Pin C7  "CLK1_N" and Pin D7 "CLK1_P"  were used like on the Sabre SD. During Compliance meassurments  margin of -80% and more.... was seen. Is there a known issue? Has someone done a similar compliance measurement on the Sabre SDB? A: The PCIe TX compliance tests on i.MX6 SD boards in TK's Open Lab.  Based on the internal PLL clock, i.MX6 SD boards pass the PCIe TX compliance tests. 1, please check the capacitor on NVCC_PLL_OUT, it should no less than 10uF, 22uF is better. 2, please check if the 24MHz input crystal is good enough. 50ppm is required. 3, please check the test step: 1.1     TX Test Configuration and Procedures Overview of Test Steps 1.      Integrate the patch for PCIE test to mainline, recompile the Kernel , and replace the old image of the board under test. ·         Make sure the following configuration has been set, when re-compiling the kernel image. # MX6 Options: # CONFIG_IMX_PCIE=y 2.      Correctly set up the test environment: ·         Connect the compliance load board (CLB x1/x16) revision 2.0 into the slot of DUT, and change the switch and jumpers to select x1 . ·         Connect the lane under test to oscilloscope via differential probe and matched coaxial , do remember that cable calibration should be done before test. ·         Connect the clock signal to the oscilloscope. The clock must have SSC enabled or disabled to be consistent with settings for the system during normal operation. ·         Power on the system. 3.      After I.MX6x enters Polling.Compliance , press the Toggle Button on CLB to select the output , make sure the data waveform is compliance pattern, 5.0GT/s for GEN2, 2.5GT/s for GEN1. 4.      Follow the Oscilloscope operation instruction, set it to the right mode. 5.      Capture and save at least 1 million * 200 ps of data and clock simultaneously at the sample rate of 50GS/s for GEN2, or 250,000 UI * 400 ps of data at the sample rate of 25GS/s for GEN1. 6.      Run free software Sigtest to analyze the PCIE TX signal. 7.      Customer could adjust the parameters of the PCIE_PHY by changing IOMUXC_GPR8 register settings to get the test past. a.       The default of this Register is configured as: imx_pcie_clrset(IOMUXC_GPR8_TX_DEEMPH_GEN1, 0 << 0, IOMUXC_GPR8); imx_pcie_clrset(IOMUXC_GPR8_TX_DEEMPH_GEN2_3P5DB, 0 << 6, IOMUXC_GPR8); imx_pcie_clrset(IOMUXC_GPR8_TX_DEEMPH_GEN2_6DB, 20 << 12, IOMUXC_GPR8); imx_pcie_clrset(IOMUXC_GPR8_TX_SWING_FULL, 127 << 18, IOMUXC_GPR8); imx_pcie_clrset(IOMUXC_GPR8_TX_SWING_LOW, 127 << 25, IOMUXC_GPR8); b.      write the Register, Address: 20E_0000h base + 20h offset = 20E_0020h; command: /unit_tests/memtool -32 0x020e0020= FFFD4000 This document was generated from the following discussion: i.Mx6 PCIe compliance
查看全文
1. Set up HDMI Set up your kernel to use HDMI adding the following code to bootargs on u-boot: video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 2. Test raw audio In order to test only raw audio, use the following command: aplay -D hw:1,0 Kaleidoscope.wav 3. Make HDMI audio the default output In order to configure audio output over HDMI, please, replace content of file ~/.asoundrc to the following one pcm.dmix_48000{      type dmix      ipc_key 5678293      ipc_key_add_uid yes      slave{           pcm "hw:1,0"           period_time 0           period_size 2048           buffer_size 24576           format S16_LE           rate 48000      } } pcm.!dsnoop_44100{      type dsnoop      ipc_key 5778293      ipc_key_add_uid yes      slave{           pcm "hw:0,0"           period_time 0           period_size 2048           buffer_size 24576           format S16_LE           rate 44100      } } pcm.!dsnoop_48000{      type dsnoop      ipc_key 5778293      ipc_key_add_uid yes      slave{           pcm "hw:1,0"           period_time 0           period_size 2048           buffer_size 24576           format S16_LE           rate 48000      } } pcm.asymed{      type asym      playback.pcm "dmix_48000"      capture.pcm "dsnoop_44100" } pcm.dsp0{      type plug      slave.pcm "asymed" } pcm.!default{      type plug      route_policy "average"      slave.pcm "asymed" } ctl.mixer0{      type hw      card 0 } This will configure alsa to use sound card hw:1,0. Please, pay attention to use the proper audio card name for your device. In order to see available sound cards on board: root@imx53qsb:~# aplay -l **** List of PLAYBACK Hardware Devices **** card 0: imx3stack [imx-3stack], device 0: SGTL5000 SGTL5000-0 []   Subdevices: 1/1   Subdevice #0: subdevice #0 card 1: imx3stackspdif [imx-3stack-spdif], device 0: IMX SPDIF mxc spdif-0 []   Subdevices: 1/1   Subdevice #0: subdevice #0 For detail on how to create asound.conf, please see alsa-lib configuration introduction. 4. Encoded audio For encoded (i.e. AC3, DTS) audio, you can use, for example, ac3dec, an utility provided by alsa-tools with the following command line: ac3dec -D hw:1,0 -C test.ac3 This would work for both HDMI audio and SPDIF audio. Double check your hardware and/or schematic in order to know which one to use.
查看全文
Author:Fourier Email:[email protected] AMP:(Asymmetric Multiple Processing) Scenario:cpu core 0 run Linux, cpu core 1 run uC/OS-II RTOS. HDMI display panel link to Linux, LCD display panel link to uC/OS-II RTOS. Platform: Mars Board(freesclae i.mx6 dual Coretex-A9 core, 1GB 64bit DDR3) Panda Board(TIOMAP4460 dual Cortex-A9 core, 1GB 32bit DDR3) Altera SoC EVMBoard(dual Cortex-A9 core, (512MB+256MB ECC) DDR3 on HPS, 512MB on FPGA) Video Demo On Mars Board: Youtube: http://youtu.be/yb6KC6Cf8i4 http://youtu.be/1uzrX-YZBnQ Youku: http://v.youku.com/v_show/id_XNTMyNTAzNjky.html AMP Port: Linux SMP boot procedure is not mention here, For detail about the Linux SMP boot procedure please refer to the document here,http://www.linux-arm.org/LinuxBootLoader/SMPBoot.I just move the boot secondary procedure from Linux to U-boot as figure 1 in the AMP implementation, and figure2 describe the GIC relationship between two core and physical memory layout between Linux and uC/OS-II. Figure 1 Figure 2 Display Subsystem Block on Mars Board and Panda Board: Figure 3 imx6 display subsystem(Mars Board) Figure 4 omap4460 display subsystem on panda board
查看全文
Multiple-Display means video playback on multiple screens. In case playback needs to be in a unique screen, the mfw_isink element must be used and some pipelines examples can be found on this link: GStreamer iMX6 Multi-Overlay. Number of Displays Display type Kernel parameters Pipelines # Set these shells variables before running the pipelines alias gl=gst-launch SINK_1="\"mfw_v4lsink device=/dev/video17\"" SINK_2="\"mfw_v4lsink device=/dev/video18\"" SINK_3="\"mfw_v4lsink device=/dev/video20\"" media1=file:///root/media1 media2=file:///root/media2 media3=file:///root/media3 2 hdmi + lvds video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 gl playbin2 uri=$media1 video-sink=$SINK_1 playbin2 uri=$media2 video-sink=$SINK_2 2 lvds + lvds video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 gl playbin2 uri=$media1 video-sink=$SINK_1 playbin2 uri=$media2 video-sink=$SINK_2 2 lcd + lvds video=mxcfb0:dev=lcd,800x480M@55,if=RGB565 video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 gl playbin2 uri=$media1 video-sink=$SINK_1 playbin2 uri=$media2 video-sink=$SINK_2 3 hdmi + lvds + lvds video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 video=mxcfb1:dev=ldb,LDB-XGA,if=RGB6 video=mxcfb2:dev=ldb,LDB-XGA,if=RGB666 gl playbin2 uri=$media1 video-sink=$SINK_1 playbin2 uri=$media2 video-sink=$SINK_2 playbin2 uri=$media3 video-sink=$SINK_3
查看全文
Update 2 Nov 2016: The work begun with this current sensor board has been superseded by this 4-channel solution. The ribbon cables used below, although easier to solder, were very stiff and tended to lift the sensors off the double sticky foam tape, which endangered the target application board. This post remains for historical purposes. This little board set was put together quickly to measure run current as well as sleep current. The sensor board is intended to be affixed with double sided tape to the board under test. A flat ribbon cable connects to the connection board where the power and current sensor connections may be made. The holes accommodate banana jacks. The current range is selected via the dip switch on the connection board. Below is an image of the schematic. The attached PDF contains the schematic, layout and partial Digikey parts lists along with embedded source files (look for the thumb-tacks).   The DMN1019USN FETs have a Vgs of 8V, which limits the maximum current which may be measured (currents above will starve the output of the current sensor amplifiers since the output cannot swing high enough). With a supply of ~7.5V, a maximum high current of ~3A is possible with the 2V/A gain (A4) version of the INA250. With a 2 Ohm shunt for the low current range, the maximum current with an INA212 (1000V/V gain) is ~3mA. Two FETs in parallel were used to decrease the series resistance when shorting the low current shunt. [NOTE: The voltage applied to the gates of the FETs assumes that the ground on the both board under test and the current sense board combo are in common.  An isolated supply could have been used but was not for simplicity.] The high current range is intended for normal operation, i.e., measuring run currents.The low current range should only be selected once the board is configured for a low power mode. Once in that mode, the low power mode may be selected.  To use an instrumented target board without having to have the connection board hooked up and powered, jump the two vias (spaced 0.1", labeled "Jump" by the current input connections). These vias short the 2 Ohm low current shunt resistor. The target board is connected via the 3-pin header. The outer two points are the negative input connection; the center is the positive. Two negative connections are provided to avoid having to cross the connection wires. These wires should be kept as short as possible. The series resistance at the input in the high range (dip switch off) was under 25mOhms, so the connections wires only add to that. The board set may be used as-is before snapping apart since connections between the boars runs through the row of snap-vias. A ribbon cable needs be used after snapping them apart. Finer pitch ribbon could have been used but it'd be much less friendly for hand soldering. Board sets in multiples of 3 may be ordered here. Here are some photos of the prototype board (some silk screen errors and the banana jack holes were drilled too small). Before snapping apart on the left and after with the ribbon cable and connectors added on the right. Here is a photo of the i.MX6SL on the EVK instrumented for low-power sleep-mode current measurement on VDD_HIGH_IN: SENSOR CALIBRATION CHECK: The calibration of three sensor boards was checked by forcing an accurate, known current with a Keysight B2902A Source Measure Unit (SMU). The average sensor output was measured for each forced current in the high and low range. The data was plotted and best fit lines were applied: The data for each sensor was very linear. The coefficients and offsets of all 6 best fit lines were very similar as can be seen above. The data can be perused in the attached Excel file (HiLo-sensors-1-3-calib.xlsx). The three sets of coefficients for the high range sensor (the INA250A4) were averaged. For each sensor's output, the current was calculated using these averaged coefficients and tabulated next to the forced current (the brown data). All of the calculated currents were within at most 20mA of the actual current forced by the SMU. TO DO: Two outputs are somewhat cumbersome; it'd be handier to just switch which sensor is outputting to the measurement device. It'd also be really handy to have a 4 channel distribution board and 4 sensor boards, which would allow the use of a 4 channel oscilloscope. Some LEDs on the distribution board indicating which measurement range is in use would also be nice... UPDATE 7 OCT 2016: Working now on a Kinetis-based, data-logging capable, 4-channel power profiler for run and sleep. The Kinetis ADCs will be used to measure the sensor outputs and power supply rail voltages, which should be fine given the level of accuracy that is required. Data is sent up the line in real time via a USB serial port, which opens the possibility of the target board profiling it's own power consumption, including low power modes (a wake-up line for the target board is provided for just that purpose). For more information on current measurements in general, see this tutorial series: A Current Sensing Tutorial--Part 1: Fundamentals | EE Times  A Current Sensing Tutorial-Part II: Devices | EE Times  A Current Sensing Tutorial--Part III: Accuracy | EE Times  A Current Sensing Tutorial-Part IV: Layout and Troubleshooting Guidelines | EE Times 
查看全文
ATK (Advanced Toolkit) ATK (Advanced Toolkit) is a Windows software for programming the flash memory of i.MX boards. It can be downloaded here. Using ATK This section will describe the procedure to erase the flash memory and program the bootloader. 1 - Connect a serial cable between PC and i.MX board. 2 - Some hardware configurations (switches) must be done to flash the board. Set red and cream switches as below: Switch SW5 -> 000000 Switch SW4 -> 1000000 {{Note|On SW5 and SW4, "1" means the keys selected towards the edge of the board.} 3 - Run ATK (1.6 or above) going to Start -> Programs -> AdvancedToolKit -> AdvancedToolKit Set the options: i.MX CPU -> i.MX35_TO2 Device memory -> DDR2; Custom Initial File -> (keep it unmarked) Communication Channel -> Serial Port (Usually COM1) If you are using TO1, Device Memory -> MDDR 4 - Click on Flash Tools to erase, program or dump the the flash memory and click GO NAND Flash Erasing 1- Configure the Dip Switch of Personality Board: Switch 1 2 3 4 5 6 7 8 SW1 OFF OFF OFF OFF N/A N/A N/A N/A SW2 ON OFF OFF ON ON OFF OFF OFF 2- Choose NAND model K9LAG08U8M 3- Continue the steps Remember to select the checkbutton BBT (Back Block Table)
查看全文
Introduction to Linux In 1989, a Finnish student called Linus Torvalds started an improvement work of Minix's Kernel, an operational system like Unix wrote by Andrew Tannenbaum, calling his own Kernel as Linux, a mix of Linus and Minix. The main idea about this new Kernel is that it's free. Anyone can develop to improve the Kernel, share the software, change it specific application and distribute without any fee or restriction. All the code is open. Finally, in 1991, Linus launched the first official Linux version, later joining Richard Stallman's GNU project in 1992 with the objective to produce the complete operational system that we know today. Linux had fast success on the x86 architecture and soon it had ported for various processor architectures and became very popular on embedded devices in many different applications like automotive, industrial, telecommunications, consumer and internet appliances. The use of Linux in embedded devices has many advantages: Supports many devices, file systems, networking protocols High portability, since it has been ported for many CPU architectures Large number of ready applications Mature source code with constant actualization Large community of programmers and users over the world testing and adding new features Which Linux distribution should I install on my PC? There are many distributions of Linux available for free. Below are a list of some of them: Ubuntu (IPA: [uːˈbuːntuː] in English,[3][ùbúntú] in Zulu) is an operating system for desktops, laptops, and servers. It has consistently been rated among the most popular of the many Linux distributions. Ubuntu's goals include providing an up-to-date yet stable Linux distribution for the average user and having a strong focus on usability and ease of installation. It is a derivative of Debian, another popular distribution. Ubuntu is sponsored by Canonical Ltd, owned by South African entrepreneur Mark Shuttleworth. The name of the distribution comes from the African concept of ubuntu which may be rendered roughly as "humanity toward others", "we are people because of other people", or "I am who I am because of who we all are", though other meanings have been suggested. This Linux distribution is named as such to bring the spirit of the philosophy to the software world. Ubuntu is free software and can be shared by any number of users. Kubuntu and Xubuntu are official subprojects of the Ubuntu project, aiming to bring the KDE and Xfce desktop environments, respectively, to the Ubuntu core (by default Ubuntu uses GNOME for its desktop environment). Edubuntu is an official subproject designed for school environments, and should be equally suitable for children to use at home. Gobuntu is an official subproject that is aimed at adhering strictly to the Free Software Foundation's Four Freedoms. The newest official subproject is JeOS. Ubuntu JeOS (pronounced "Juice") is a concept for what an operating system should look like in the context of a virtual appliance. Ubuntu releases new versions every six months, and supports those releases for 18 months with daily security fixes and patches to critical bugs. LTS (Long Term Support) releases, which occur every two years, are supported for 3 years for desktops and 5 years for servers. The most recent LTS version, Ubuntu 10.04 LTS (Lucid Lynx), was released on 29 April 2010. The current non-LTS version is 10.10 (Maverick Meerkat) released on 10/10/10 (10 October 2010). Click here for official site Mandriva Linux (formerly Mandrakelinux or Mandrake Linux) is a Linux distribution created by Mandriva (formerly Mandrakesoft). It uses the RPM Package Manager. The product lifetime of Mandriva Linux releases is 18 months for base updates and 12 months for desktop updates. Click here for official site openSUSE, (pronounced /ˌoʊpɛnˈsuːzə/), is a community project, sponsored by Novell and AMD, to develop and maintain a general purpose Linux distribution. After acquiring SUSE Linux in January 2004, Novell decided to release the SUSE Linux Professional product as a 100% open source project, involving the community in the development process. The initial release was a beta version of SUSE Linux 10.0, and as of October 2007 the current stable release is openSUSE 10.3. Beyond the distribution, openSUSE provides a web portal for community involvement. The community assists in developing openSUSE collaboratively with representatives from Novell by contributing code through the open Build Service, writing documentation, designing artwork, fostering discussion on open mailing lists and in Internet Relay Chat channels, and improving the openSUSE site through its wiki interface. Novell markets openSUSE as the best, easiest distribution for all users. Like most distributions it includes both a default graphical user interface (GUI) and a command line interface option; it allows the user (during installation) to select which GUI they are comfortable with (either KDE, GNOME or XFCE), and supports thousands of software packages across the full range of open source development. Click here for official site Fedora is an RPM-based, general purpose Linux distribution, developed by the community-supported Fedora Project and sponsored by Red Hat. Fedora's mission statement is: "Fedora is about the rapid progress of Free and Open Source software." One of Fedora's main objectives is not only to contain free and open source software, but also to be on the leading edge of such technologies. Also, developers in Fedora prefer to make upstream changes instead of applying fixes specifically for Fedora – this ensures that updates are available to all Linux distributions. Click here for official site Debian (pronounced [ˈdɛbiən]) is a computer operating system (OS) composed entirely of software which is both free and open source (FOSS). Its primary form, Debian GNU/Linux, is a popular and influential Linux distribution. It is a multipurpose OS; it can be used as a desktop or server operating system. Debian is known for strict adherence to the Unix and free software philosophies. Debian is also known for its abundance of options — the current release includes over twenty-six thousand software packages for eleven computer architectures. These architectures range from the Intel/AMD 32-bit/64-bit architectures commonly found in personal computers to the ARM architecture commonly found in embedded systems and the IBM eServer zSeries mainframes. Throughout Debian's lifetime, other distributions have taken it as a basis to develop their own, including: Ubuntu, MEPIS, Dreamlinux, Damn Small Linux, Xandros, Knoppix, Linspire, sidux, Kanotix, and LinEx among others. A university's study concluded that Debian's 283 million source code lines would cost 10 billion USA Dollars to develop by proprietary means. Prominent features of Debian are its APT package management system, its strict policies regarding its packages and the quality of its releases. These practices afford easy upgrades between releases and easy automated installation and removal of packages. Debian uses an open development and testing process. It is developed by volunteers from around the world and supported by donations through SPI, a non-profit umbrella organization for various free software projects. The default install provides popular programs such as: OpenOffice, Iceweasel (a rebranding of Firefox), Evolution mail, CD/DVD writing programs, music and video players, image viewers and editors, and PDF viewers. Only the first CD/DVD is necessary for the default install; the remaining discs contain all 26,000+ extra programs and packages currently available. If a user does not wish to download the CDs/DVDs, these extras can be downloaded and installed separately using the package manager. Debian can also be configured to download and install updates automatically. Click here for official site Slackware is a Linux distribution created by Patrick Volkerding of Slackware Linux, Inc. Slackware was one of the earliest distributions, and is the oldest currently being maintained. Slackware aims for design stability and simplicity, and to be the most Unix-like GNU/Linux distribution. Click here for official site
查看全文