i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Q: What is the Min LPDDR2 clock frequency allowed by the i.MX6? The Jedec Spec for LPDDR2 allows for a min tck period of 100ns. Are there any required relashionship between the DDR clock frequency and other clocks in the i.MX6? A: The JEDEC maximum period for the MX6 is 100nS as per the LPDDR2 specification.  There is a minimum period during boot, before everything is configured and fully up to speed of 18nS. Are you saying the imx6 memory controller can operatate down to the min frequecies specified in the LPDDR2 JEDEC spec? Given that there is no limit specified in the data sheet, it should operate that slowly, provided the clocking can be set for it to operate so slowly. I would imagine that the core will need to be running slowly as well, since it does not make sense to slow the memory bus without slowing the core down as well.
查看全文
JTAG Hardware and Software There are many opened and proprietary JTAG solutions. Here are some of them: Proprietary IAR Systems In-Circuit Debugging Probes Macraigor usb2Demon Segger - Jlink Free and Open Source Software GDB OpenOCD Open Hardware Turtelizer
查看全文
We have validated Toshiba Smart NAND in our i.MX6SX platform, and boot successfully. The results are as below: 1. chip part number: THGBR2G5D1JTA00,  page_size: 16k+64  pages_per_block: 256 2. test platform: i.MX6SX Some information to take care of: 1. The pin assignment of smart nand is different from common raw nand, that is, Nand pin1 must connect to Vcc, pin2 connects to Vss, pin23 connects to VssQ, pin24 connects to VccQ, pin38 connects to VccQ 2. The ECC layout of FCB page itself must be set according to the i.MX6SX RM, otherwise FCB can't be read correctly. 3. EccBlock0EccType and EccBlockNEccType in FCB must be set as 0, and raw data can be put in DBBT and firmware without any ECC check codes.
查看全文
This document is describe the control method of USB Power based on I.MX6ULL-EVK.   1. Hardware Design USB OTG can be working as device mode, host mode, or switching between both device mode and host mode. (a) USB OTG Device mode When USB OTG is working as device mode, the USB OTG ID pin should be pulled up by a resistor. And the 5V power comes from the VBUS pin of MicroUSB which is the 5V from the external USB HOST. From the above schematic :- When the USB OTG1 ID is pulled to high, the G/S of the NMOSFET Q2SK3018 is turned on. The ENA pin of U1101 is low, and then no 5V output from OUTA. If USB OTG1 is connected to the external USB HOST, a 5V power source will enter the board and supply to the USB OTG1 VBUS pin. (b) Switch between Device and Host mode This is also called USB OTG’s Dual Role. When we plug in MicroUSB with USB TYPE-AB to USB TYPE-A-F cable, USB OTG1 will switch from USB device to Host mode. At this time, the USB OTG1 ID pin will be pulled down to low, the G / S of the NMOSFET will be turned off, the ENA pin of U1101 will be pulled low, and OUTA will output 5V voltage to the VBUS pin of MicroUSB. (c) USB OTG Host mode When USB OTG is working as host mode,  USB OTG1 ID pin connect an external resistor to pull it down or use internal resistor to pull it down. If using external resistor, 2.2K/3.3K ohm resistor is recommended. The USB_OTG1_PWR should output High to enable ENA of U1101, then OUTA will output 5V to USB OTG1 VBUS. On i.MX6ULL-EVK, USB OTG2 port is designed to be Host mode. It can be a design reference. When the USB_OTG2_PWR pulled to high, the U1101 supplies 5V to the outside. 2. Software modification The GPIO1_IO04 can be used to control USB OTG1 power.
查看全文
Add the above line to conf/local.conf file: PREFERRED_PROVIDER_virtual/kernel = "linux-fslc" Check this page to see what the mainline Linux kernel supports for a particular Freescale board.
查看全文
    Xenomai is real-time framework, which can run seamlessly side-by-side Linux as a co-kernel system, or natively over mainline Linux kernels (with or without PREEMPT-RT patch). The dual kernel nicknamed Cobalt, is a significant rework of the Xenomai 2.x system. Cobalt implements the RTDM specification for interfacing with real-time device drivers. The native linux version, an enhanced implementation of the experimental Xenomai/SOLO work, is called Mercury. In this environment, only a standalone implementation of the RTDM specification in a kernel module is required, for interfacing the RTDM-compliant device drivers with the native kernel. You can get more detailed information from Home · Wiki · xenomai / xenomai · GitLab       I have ported xenomai 3.1 to i.MX Yocto 4.19.35-1.1.0, and currently support ARMv7 and tested on imx6ulevk/imx6ull14x14evk/imx6qpsabresd/imx6dlsabresd/imx6sxsabresdimx6slevk boards. I also did stress test by tool stress-ng on some boards.      You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm.git, and git checkout Linux-4.19.35-1.1.0. (which inlcudes all patches and bb file) and add the following variable in conf/local.conf before build xenomai by command bitake xenomai.  XENOMAI_KERNEL_MODE = "cobalt"  PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" DISTRO_FEATURES_remove = "optee" or XENOMAI_KERNEL_MODE = "mercury" PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" DISTRO_FEATURES_remove = "optee" If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch. The following is test result by the command (/usr/xenomai/demo/cyclictest -p 50 -t 5 -m -n -i 1000 😞 //Mecury on 6ULL with stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 128M --metrics-brief policy: fifo: loadavg: 6.08 2.17 0.81 8/101 534 T: 0 (  530) P:99 I:1000 C:  74474 Min:     23 Act:  235 Avg:   77 Max:    8278 T: 1 (  531) P:99 I:1500 C:  49482 Min:     24 Act:   32 Avg:   56 Max:    8277 T: 2 (  532) P:99 I:2000 C:  36805 Min:     24 Act:   38 Avg:   79 Max:    8170 T: 3 (  533) P:99 I:2500 C:  29333 Min:     25 Act:   41 Avg:   54 Max:    7069 T: 4 (  534) P:99 I:3000 C:  24344 Min:     24 Act:   51 Avg:   60 Max:    7193   //Cobalt on 6ULL with stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 128M --metrics-brief policy: fifo: loadavg: 7.02 6.50 4.01 8/100 660 T: 0 (  652) P:50 I:1000 C: 560348 Min:      1 Act:   10 Avg:   15 Max:      71 T: 1 (  653) P:50 I:1500 C: 373556 Min:      1 Act:    9 Avg:   17 Max:      78 T: 2 (  654) P:50 I:2000 C: 280157 Min:      2 Act:   14 Avg:   20 Max:      64 T: 3 (  655) P:50 I:2500 C: 224120 Min:      1 Act:   12 Avg:   15 Max:      57 T: 4 (  656) P:50 I:3000 C: 186765 Min:      1 Act:   31 Avg:   19 Max:      53   //Cobalt on 6qp with stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 512M --metrics-brief policy: fifo: loadavg: 8.11 7.44 4.45 8/156 1057 T: 0 (  917) P:50 I:1000 C: 686106 Min:      0 Act:    3 Avg:    5 Max:      53 T: 1 (  918) P:50 I:1500 C: 457395 Min:      0 Act:    3 Avg:    5 Max:      49 T: 2 (  919) P:50 I:2000 C: 342866 Min:      0 Act:    2 Avg:    4 Max:      43 T: 3 (  920) P:50 I:2500 C: 274425 Min:      0 Act:    3 Avg:    5 Max:      58 T: 4 (  921) P:50 I:3000 C: 228682 Min:      0 Act:    2 Avg:    6 Max:      46   //Cobalt on 6dl with stress-ng --cpu 2 --io 2 --vm 1 --vm-bytes 256M --metrics-brief policy: fifo: loadavg: 3.35 4.15 2.47 1/122 850 T: 0 (  729) P:50 I:1000 C: 608088 Min:      0 Act:    1 Avg:    3 Max:      34 T: 1 (  730) P:50 I:1500 C: 405389 Min:      0 Act:    0 Avg:    4 Max:      38 T: 2 (  731) P:50 I:2000 C: 304039 Min:      0 Act:    1 Avg:    4 Max:      45 T: 3 (  732) P:50 I:2500 C: 243225 Min:      0 Act:    0 Avg:    4 Max:      49 T: 4 (  733) P:50 I:3000 C: 202683 Min:      0 Act:    0 Avg:    5 Max:      38   //Cobalt on 6SX stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 512M  --metrics-brief policy: fifo: loadavg: 7.51 7.19 6.66 8/123 670 T: 0 (  598) P:50 I:1000 C:2314339 Min:      0 Act:    3 Avg:    8 Max:      60 T: 1 (  599) P:50 I:1500 C:1542873 Min:      0 Act:   15 Avg:    8 Max:      72 T: 2 (  600) P:50 I:2000 C:1157152 Min:      0 Act:    4 Avg:    9 Max:      55 T: 3 (  601) P:50 I:2500 C: 925721 Min:      0 Act:    5 Avg:    9 Max:      57 T: 4 (  602) P:50 I:3000 C: 771434 Min:      0 Act:    6 Avg:    6 Max:      41   //Cobalt on 6Solo lite stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 512M  --metrics-brief policy: fifo: loadavg: 7.01 7.04 6.93 8/104 598 T: 0 (  571) P:50 I:1000 C:3639967 Min:      0 Act:    9 Avg:    7 Max:      60 T: 1 (  572) P:50 I:1500 C:2426642 Min:      0 Act:    9 Avg:   11 Max:      66 T: 2 (  573) P:50 I:2000 C:1819980 Min:      0 Act:   11 Avg:   10 Max:      57 T: 3 (  574) P:50 I:2500 C:1455983 Min:      0 Act:   12 Avg:   10 Max:      56 T: 4 (  575) P:50 I:3000 C:1213316 Min:      0 Act:    7 Avg:    9 Max:      43   //Cobalt on 7d with stress-ng --cpu 2 --io 2 --vm 1 --vm-bytes 256M --metrics-brief policy: fifo: loadavg: 5.03 5.11 5.15 6/107 683 T: 0 (  626) P:50 I:1000 C:6842938 Min:      0 Act:    1 Avg:    2 Max:      63 T: 1 (  627) P:50 I:1500 C:4561953 Min:      0 Act:    4 Avg:    2 Max:      66 T: 2 (  628) P:50 I:2000 C:3421461 Min:      0 Act:    0 Avg:    2 Max:      69 T: 3 (  629) P:50 I:2500 C:2737166 Min:      0 Act:    3 Avg:    2 Max:      71 T: 4 (  630) P:50 I:3000 C:2280969 Min:      0 Act:    2 Avg:    1 Max:      33   //////////////////////////////////////// Update for Yocto L5.10.52 2.1.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.10.52 2.1.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm and git checkout xenomai-5.10.52-2.1.0. Updating: 1, Upgrade Xenomai to v3.2 2, Enable Dovetail instead of ipipe. Copy xenomai-arm to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL_append += " xenomai" Notice: If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch. //////////////////////////////////////// Update for Yocto L5.15.71 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.15.71 2.2.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm and git checkout xenomai-5.15.71-2.2.0. Updating: 1, Upgrade Xenomai to v3.2.2 Copy xenomai-arm to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL:append += " xenomai" Notice: If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch.   ///////// Later update for Later Yocto release, please refer to the following community post //////////// 移植实时Linux方案Xenomai到i.MX ARM64平台 (Enable real-time Linux Xenomai on i.MX ARM64 Platform)   
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343102 
查看全文
Copy Redboot binary to /tftpboot. In this case: redboot.bin Load binary file to i.MX ram memory: RedBoot> load -v -r -b 0x100000 /tftpboot/redboot.bin Run the loaded image RedBoot> run 0x100000 Enable NOR, NAND or MMC flash media for Redboot. In this case, NAND is beeing used. RedBoot> factive nand Update Redboot in the flash with currently running image RedBoot> romupdate Copy redboot binary to /tftpboot. In this case: redboot.bin Load binary file to i.MX ram memory: RedBoot> load -v -r -b 0x100000 /tftpboot/redboot.bin Run the loaded image RedBoot> run 0x100000 Enable NOR, NAND, or MMC flash media for Redboot. In this case, NAND is being used. RedBoot> factive nand Update Redboot in the flash with currently running image RedBoot> romupdate
查看全文
Features Additional Information Features The i.MX31 PDK, with Smart Speed™ technology, is a completely integrated hardware and software solution that simplifies product development so you can focus on your critical differentiation needed for market success. Reduce development time, and design products that have power to spare, even when running multiple applications simultaneously. Receive stellar image and graphic performance in a system design that dramatically reduces power consumption. The i.MX31 PDK provides: Modular hardware enabling multiple connectivity technologies Optimized development software for Linux®, Windows® CE 5.0 and Windows Embedded CE 6.0 operating systems Out-of-box experience, complete with demonstration software and performance data Maximum performance and power savings Complete "Design. Debug. Demo." capability as simple as 1,2,3 i.MX31 Applications Processor Module i.MX31 Applications Processor - ARM11™ 128 MB DDR SDRAM 256 MB NAND FLASH Power Management (PMIC MC13783) + Power Circuitry Audio HS USB PHY Touch Controller Connector Debug Module (Software Development) Debug Ethernet Port Debug Serial Port JTAG Reset, Interrupt, Boot Switches Debug LEDs CodeTest Interface Power Source Current/Power Monitoring Personality Module (Demo-ready) Acceleromater MMA7450L (Freescale) User I/O Connectivity (FM, 802.11, Bluetooth, USB OTG, USB HS) Button 2.7"TFT Display 2MP Camera Module SDcard, ATA HDD External Connectors (dock, headphones, TV out, GPS) Microphone Speaker Additional Information i.MX31 PDK Contents If you are new to i.MX31PDK development we suggest checking out:Not authorized to view the specified document 1673 To flash BootLoader: i.MX31 PDK Board Flashing Miscellaneous Tutorials Blink i.MX 31PDK LEDs Using U-Boot i.MX31 Testing RNGA I.MX31 Testing TvOut I.MX31 Using CLKO
查看全文
This is ov5645 driver and tested with i.MX6 L3.0.35 BSP .  It is modified based on ov5640.c. P.S. The power down function for OV5645 is different from the OV5640. So modify the function in your_board.c like this: static void mx6q_mipi_powerdown(int powerdown) {     if (!powerdown)         gpio_set_value(MIPI_PWDN, 1);     else         gpio_set_value(MIPI_PWDN, 0);     msleep(5); }
查看全文
For Fedora Users: Open a terminal as root Edit tftp file -> #gedit /etc/xinetd.d/tftp Add these lines: service tftp     {   socket_type = dgram   protocol = udp   wait = yes   user = root   server = /usr/sbin/in.tftpd   server_args = /tftpboot   disable = no   per_source = 100 2   flags = IPv4 } Restart the service: # /etc/init.d/xinetd restart OR # service xinetd restart
查看全文
Q: What is latency figures for the VPU to decode Device: i.MX6Q OS: Linux Resolution:                         1920x1080(HD) Frame rate:                        30 FPS Function:                             Overlay messages. Input/Output:                   8 bit / YUV 4:2:0 / NAL stream Profile level:                      4.1. Constrained Baseline. I and P frames support. A: It depend on the syntax in H.264, includes num_reorder_frames,max_dec_frame_buffering,num_ref_frames,MaxDpbSize,etc. for start latency: it cover vpu driver loading, allocate buffers, init, decoding the first frame less than 100ms on iMX6/Linux. This document was generated from the following discussion: VPU Latency i.MX6
查看全文
Currently the default i.MX51 wince release doesn't support high capacity MMC card. Attached was the patch of how to enable high capacity MMC card in i.mx51. Original Attachment has been moved to: High-capacity-MMC-support.zip
查看全文
In new iMX8QM and iMX8QXP BSP, it had implemented hardware partition to split the resource and memory regions. The default Android Auto BSP had given example for shared memory between M4 and A core, it is used for RPMSG. Here is an example to add a new shared memory for iMX8QXP MEK board with Android Auto P9.0.0_GA2.1.0 BSP, which can be accessed in both M4, Uboot and Linux Kernel. The new shared memory region is from 0xF6000000 to 0xFDFFFFFF, total 128MB, it covers the RPMSG region too. RPMSG shared memory is moved to 0xF6000000 ~ 0xF6BFFFFF, total 12MB. vendor_nxp_fsl-proprietary_uboot-firmware.patch SCFW patch for board file to change the old shared memory region (0x90000000~0x90BFFFFF) to new shared memory region (0xF6000000~0xFDFFFFFF). This patch is applied to android_build/vendor/nxp/fsl-proprietary/uboot-firmware/imx8q_car/board-imx8qxp.c, after patched, copy this file to SCFW porting kit and build out a new SCFW image, put it to "android_build/vendor/nxp/fsl-proprietary/uboot-firmware/imx8q_car/mx8qx-scfw-tcm.bin". vendor_nxp-opensource_uboot-imx.patch This is the Uboot patch to map the shared memory region, if Uboot doesn't need access these memory, this patch is not needed. vendor_nxp-opensource_kernel_imx.patch This is the kernel patch to map the shared memory region. Note: VPU reserved memory address shouldn't be changed, otherwise it will impact the VPU function. So the new reserved memory region had been moved to 0xF600000~0xFDFFFFFF. vendor_nxp_mcu-sdk-auto_SDK_MEK-MIMX8QX.patch M4 patch for RPMSG address changed from 0x90000000 to 0xF6000000. Note: 1. In this example, we put the two shared memory regions together, then it will not split the memory region used in Linux. Another reason for such modification is the limitation of memory region counts in SCFW. 2. Since the RPMSG shared memory had been moved from 0x90000000 to 0xF6000000, the M4 code who used shared memory should also be changed. 2019-07-29 Update: When "#define PHYS_SDRAM_2_SIZE  0x0" in Uboot, it will create a 0 size memory region, this will impact the Uboot shared memory patch. Added the "uboot_imx8_cpu.patch" to avoid such issue.
查看全文
This is a series of documents that intend to help you grasp he concept of the System Controller Unit (SCU) / System Controller Firmware (SCFW).    Getting started Power management service  Resource management service Pad configuration service Timer service Miscellaneous service   Other Useful resources: https://community.nxp.com/docs/DOC-344684 (2019) i.MX 8 System Controller Unit and System Controller Firmware Overview (2018) Clusters & Infotainment: Introduction to the i.MX 8 System Controller Unit (2017 Slightly outdated, for correct boot sequence go to Chapter 5 System Boot of the Reference Manual) System Controller Firmware command line utility for QNX and Linux You can get the latest System Controller Firmware Porting kit from the i.MX Software and development webpage: The porting kit contains documentation and allows you to build the SCFW from source and do modifications to the board dependent parts: The API documents explain the System Controller Firmware API syntax and it has a section for introduction and general overview of the system. The port document contains information on what each board component function does and the overall process of porting the SCFW.
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343344 
查看全文
This document shows the steps for the creation of Archlinux and kernel 4.18.5 on the UDOO board. Required material: UDOO board, Ubuntu 16.04 and SD card. Firts we need u-boot (universal bootloader), for that reason we need update the host. $ sudo apt-get update Then we need the file *.img and SPL for the file system $ wget http://os.archlinuxarm.org/os/imx6/boot/udoo/SPL $ wget http://os.archlinuxarm.org/os/imx6/boot/udoo/u-boot.img Kernel 4.18.5 and file system: $ sudo mkdir archlinux $ wget http://os.archlinuxarm.org/os/ArchLinuxARM-armv7-latest.tar.gz $ sudo tar -xzvf  ArchLinuxARM-armv7-latest.tar.gz $ sudo rm -rf *.tar.gz You must have the following files Now  We are going to burn the memory, we need a 16Gb of space: We need to make sure it is empty Then partitions: $ sudo fdisk /dev/sdc O, P, N, P, 1 space, 8192 default, W At the end the sdc is partition, then create the filesystem partition $ sudo mkfs.ext4 /dev/sdc1 The working directory $ sudo mkdir mnt mount the partition 1 $ sudo mount /devsdc1 mtn/ Now we where the kernel and filesystem are and copy all the file in mnt: $ sudo cp -vr * ~/mnt/ Once it finish we execute $ sync then unmount the partition of sdc1: $ sudo umount mnt/ Now is moment to load the SPL and u-boot: and $ sync we retire the sd and turn on the board. Now you are on ArchLinux. user: alarm                  root: Root Pass: alarm                 pass: root Now the firts thing we must do it is upgrade the keys: $ pacman -key --init $ pacman -key --populate archlinuxarm $ pacman -Syyuu We can add another user: $ useradd - m -g user  -s /bin/bash user_name $ passwd user_name $ paman -S sudo $ visudo Root ALL= (ALL) ALL user_name ALL=(ALL) ALL $ exit For the graphic we are going to install the xorg: $ sudo pacman -S xorg-server $ sudo pacman -S xorg-apps Now we can execute startx and observe the windows of xorg $ startx To have a windows gestor: $ sudo pacman -S sddm $ sudo pacman -S plasma kde-applications $ sudo systemctl enable sddm Reboot and you are ArchLinux graphics windows
查看全文
This document explains the pad implementation and its relationship with the System Controller Firmware pad configuration service. There are two components to pad configuration in the SCFW, there are the modules that generate the signals that will ultimately appear on the physical pad, let's say GPIO/Ethernet/I2C/UART etc... and then there is the part that configures the muxing of the pad (what signal is going to be outputted through the specific pad), the drive strength of the pad, pull selection, etc, this is the part that the SCFW pad service configures. Introduction‌ The i.MX8 has three types of I/Os: 1.8V only I/Os 3.3V only I/Os 1.8V / 3.3V I/Os Dual Voltage I/Os Note: USB High Speed Inter-Chip (HSIC) and Ethernet interfaces have specific integration schemes with dedicated features. They are a modified versions of the above I/O types. HSIC are a special kind of I/O modified to sustain 480Mbps data rates ENET I/Os are modified versions of Dual Voltage I/Os to support 2.5V operations All of these I/Os have "common features" and "technology specific features" which depend on the type of I/O and the chip manufacturing process (FDSOI in the i.MX8QM case) I/O common features Muxing capability of up to 4 signals Each Pad can have up to 4 signals, only one signal can be present in the pad. To select the signal that will output on the pad simply look at the Pinmux spreadsheet and use the desired alternative, for instance in the following image SCU_GPIO0_00 has 3 options, SCU_GPIO (ALT0 - GPIO controlled directly by the SCU), SCU_UART0_RX (ALT1 - SCU UART receiver) or LSIO_GPIO0_IO28 (ALT3 - Low speed I/O GPIO).   Pads without GPIO functionality (i.e. without the GPIO option in the pinmux spreadsheet) are implemented for one purpose only, these pins are connected directly to the module that drives them and they feature their own physical interface. Examples are XTAL pins, DDR pins and SCU PMIC interface (shown above). Mode of operation All GPIO types support four modes of operation: Normal mode Data is being driven directly to the pad (an internal signal of 1 shows in the pad as a 1 and vice-versa) and the pad works either as an output or as an input but not both at the same time. The output buffer while on this mode looks like this: Open drain Data is being driven through an open drain configuration, the output on the pad switches between 0 and high-z. The pad works either as an output or as an input but not both at the same time, e.g. if the Output Buffer is enabled the Input Buffer is disabled. This is how the output buffer looks like on Open drain mode: Open drain and input Output buffer acts as in open drain mode but with the input buffer enabled regardless of the output buffer state (enabled/disabled), this allows to simultaneously read the signal at the pad while driving it. Output and input Output buffer acts as in normal mode but with the input buffer enabled regardless of the output buffer state (enabled/disabled), this allows to read the signal at the pad while driving it. Wake-up capability Each I/O can be configured to wake-up the device, the following configuration options are available: OFF I/O cannot wake-up the system Low detect Generate wake-up event when the pad remains in low-level High detect Generate wake-up event when the pad remains in high-level Rising edge Generate wake-up event on rising edge detection Falling edge Generate wake-up event on falling edge detection Technology specific features Some of the available features for each pad depend on two factors: Chip manufacturing process (FDSOI or LPP) I/O type (1.8V, 3.3V or Dual Voltage) The i.MX8QM is manufactured using FDSOI technology and it features all of the three available I/O types. Drive strength Drive strength options vary within I/O types and chip manufacturing options. The available options for a FDSOI chip are: 1.8V Drive strength options 3.3V Drive strength options Dual Voltage drive strength options Drive strength of 1mA Drive strength of 2mA Low drive strength (50 ohms) Drive strength of 2mA Drive strength of 4mA High drive strength (33 ohms) Drive strength of 4mA Drive strength of 8mA Drive strength of 6mA Drive strength of 12mA Drive strength of 8mA Drive strength of 10mA Drive strength of 12mA High-speed drive strength Pull Select The pull select available options are almost the same for all I/O types (1.8V being the exception) and they also depend on chip manufacturing process. The available options for a FDSOI chip are: Pull select options for FDSOI Bus-keeper (only available for 1.8V) Pull-up Pull-down No Pull (Disabled) A bus-keeper or bus-holder is used to keep the last state on the bus. In normal operation it makes no difference, but once the bus is tri-stated it keeps the last logic level in the bus to prevent the bus from floating. Compensation The compensation feature is only available on Dual Voltage I/Os. Dual Voltage I/Os have a different implementation, they require: Voltage reference generator - which provides a voltage reference to the supply detector and compensation cell Supply detector - detects automatically whether the I/O is being supplied with 1.8V or 3.3V and broadcasts this information to compensation cell and I/O  Compensation cell - adjusts drive strength of dual voltage I/Os depending on Process Voltage and Temperature (PVT) conditions. The default configuration takes care of adjusting this parameters and no further modifications are required. Pad configuration service SCFW API Mux selection The very first function that needs to be called to configure a pad is: sc_err_t sc_pad_set_mux(sc_ipc_t ipc, sc_pad_t pad, uint8_t mux, sc_pad_config_t config, sc_pad_iso_t iso);‍‍‍‍‍‍‍‍‍‍‍‍‍‍ This function takes care of configuring the muxing alternative and setting the common features, its parameters are: ipc - The Inter Processor Communication (IPC) channel that you will use to communicate with the SCU. You need to call sc_ipc_open to obtain it. pad - The pad you want to configure, the different pad definitions are in imx8qm_pads.h, this is basically the same list that is included in the scfw_api_qm.pdf document (page 27 Chapter 5 Pad List) and it also mimics the Pinmux excel sheet. mux - The mux setting that you require, basically Alt0 -> 0, Alt1 -> 1, Alt2 -> 2 and Alt3-> 3, the pinmux spreadsheet contains the required information (take a look at I/O common features above). config - Used to select the desired mode of operation (take a look at I/O common features above), the available options are declared under sc_pad_config_t Normal mode - SC_PAD_CONFIG_NORMAL Open Drain mode - SC_PAD_CONFIG_OD Open Drain and input - SC_PAD_CONFIG_OD_IN Output and input - SC_PAD_CONFIG_OUT_IN iso - This is the low-power isolation configuration (take a look at I/O common features above). The available options are declared under sc_pad_iso_t ISO_OFF - SC_PAD_ISO_OFF ISO_EARLY - SC_PAD_ISO_EARLY ISO_LATE - SC_PAD_ISO_LATE ISO_ON - SC_PAD_ISO_ON For instance to configure M40_I2C0_SCL with its UART alternative in normal mode with low-power isolation off, the call would look like this: sc_pad_set_mux(ipc, SC_P_M40_I2C0_SCL, 1, SC_PAD_CONFIG_NORMAL, SC_PAD_ISO_OFF);‍‍‍‍‍‍‍‍‍‍ Pad configuration To configure drive strength and pull select options the technology specific functions need to be used (FDSOI for i.MX8QM): sc_pad_set_gp is being used by our Linux team because it admits the passing of the configuration parameters as a single value and this eases the handling on the device tree, but you should aim to use the technology specific functions. sc_err_t sc_pad_set_gp_28fdsoi(sc_ipc_t ipc, sc_pad_t pad, sc_pad_28fdsoi_dse_t dse, sc_pad_28fdsoi_ps_t ps);‍‍‍‍‍‍‍‍‍‍‍ This function takes care of configuring the drive strength (DSE) and pull select settings (PS) for the specified pad, here is a break down of the parameters it uses: ipc - The Inter Processor Communication (IPC) channel that you will use to communicate with the SCU. You need to call sc_ipc_open to obtain it. pad - The pad you want to configure, the different pad definitions are in imx8qm_pads.h, this is basically the same list that is included in the scfw_api_qm.pdf document (page 27 Chapter 5 Pad List) and it also mimics the Pinmux excel sheet. dse - The desired drive strength configuration (see Technology specific features above). DSE settings depend on the I/O type being used, the available options for each I/O type are defined under sc_pad_28fdsoi_dse_t: ENET pads capable of operating at 2.5V are a subset of dual voltage I/Os, the dse options available for these pads are the same as normal dual voltage I/Os. i.e. High drive and low drive. ps - The desired pull select configuration (see Technology specific features above). The available options are defined under sc_pad_28fdsoi_ps_t: To determine whether a GPIO pad is 1.8V, 3.3V or Dual Voltage one can look at the pinmux spread sheet, the supply for the pad will indicate what implementation of the GPIO is used. For instance: pads under VDD_SIM_1P8_3P3 are Dual voltage I/Os pads under VDD_SCU_1P8 are 1.8V I/Os pads under VDD_ADC_3P3 are 3.3V I/Os taking the same example as above we could configure the M40_I2C0_SCL as follows: sc_pad_set_gp_28fdsoi(ipc, SC_P_M40_I2C0_SCL, SC_PAD_28FDSOI_DSE_DV_LOW, SC_PAD_28FDSOI_PS_NONE);‍‍‍‍‍‍‍‍‍‍‍‍‍ Configuration under Linux Linux configures pads through the device tree, the full documentation of the binding is under Documentation/devicetree/bindings/pinctrl/fsl,imx8qxp-pinctrl.txt. but here is an extract: * Freescale i.MX8QXP IOMUX Controller Required properties: - compatible: "fsl,imx8qxp-iomuxc" - fsl,pins: each entry consists of 2 integers. Its format is <pin_id pin_config>. pin_config definition: - i.MX8QXP have different pad types, please refer to below pad register definitions, the pinctrl driver will just write the pin_config into the hardware register.‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The driver uses the following API: sc_err_t sc_pad_set_gp (sc_ipc_t ipc, sc_pad_t pad, uint32_t ctrl) ‍‍‍ Instead of configuring each parameter individually as done with sc_pad_set_gp_28fdsoi it configures the pad as if writing to a register, the bitfield format is under the binding documentation but it is as follows: struct _hw_pad_iomux_bitfields0 { uint32_t GP : 19; /*!< [18:0] GP controls. */ uint32_t WAKEUP : 3; /*!< [21:19] Wakeup controls. */ uint32_t WAKEUP_ENB : 1; /*!< [22] Wakeup write enable. */ uint32_t LPCONFIG : 2; /*!< [24:23] Low-power config. */ uint32_t CONFIG : 2; /*!< [26:25] Config. */ uint32_t IFMUX : 3; /*!< [29:27] Mux. */ uint32_t GP_ENB : 1; /*!< [30] GP write enable. */ uint32_t IFMUX_ENB : 1; /*!< [31] Mux write enable. */ } B; ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ All the configurations mentioned above can be configured, but they are done in a single pass, e.g. Muxing, Configuration (Norma, Open Drive, etc...), Wakeup control, and GP controls are for Pull Select Drive Strenght etc... Check the Reference Manual Chapter for IOMUXD for the register definition for each pad. References For more details refer to the sc_fw_api.pdf document: Chapter 1.3.3 Pad Configuration Service Chapter 6 Pad List Chapter 9.3 (SVC) Pad Service System Controller Firmware 101 
查看全文
gst-inspect is a tool to to get documentation about GStreamer elements. Pipeline Check installed GST elements gst-inspect | tail -1 Check installed FSL GST elements gst-inspect | grep imx Element documentation gst-inspect <gst element>
查看全文
UUU is an evolution of MFGTools. The introduction of UUU detail you can see the uuu.pdf file.. Please download uuu.exe and follow the UUU introduction. Here are some running examples. If you are not familiar with uuu, you can refer to them firstly. Under Windows (should be as admin): • For SD card:  Linux:  .\uuu -b sd_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard • For EMMC:  Linux:  .\uuu -b emmc_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard  or  .\uuu.exe uuu.auto  Android:  .\uuu_imx_android_flash.bat -f imx8mm -u trusty Under Linux: • For EMMC  Linux:  sudo .\uuu uuu.auto If you download BSP release from nxp.com, you could find a file uuu.auto in the package. This is a preset script that can be executed directly (default for EMMC). You could change the script based on your requirement. Copy the uuu.exe under the release package, then execute the instructions. For UUU tool the prebuilt image and document are here: • https://github.com/NXPmicro/mfgtools/releases • UUU.pdf is snapshot of wiki   Environment PC: Window 10 64bit Board: i.MX8MMLPDDR4 EVK BSP: Q10.0.0_2.0.0 Demo images Screen: MX8-DSI-OLED1 Downloading android images to i.MX 8M Mini EVK LPDDR4 via UUU Tool 1\Hardware Preparations (1) Make the board enter serial download mode. For Rev. B boards, change the first two bits of board's sw1101 to 10 (from 1-2 bit) to enter serial download mode. For Rev. C boards, change the first four bits of board's sw1101 to 1010 (from 1-4 bit) to enter serial download mode. (2) Connecting J901to PC USB by a USB OTG cable. (3) Connecting J301(usb type c) to PC USB. (4) Plugging adapter into Power Jack (J302) (5) Power on i.MX 8M Mini EVK LPDDR4 board via SW101 Switch When first connect the board to PC, windows 10 64bit can’t automatically install FT2232D  driver from official website of manufacture, you need to Install the usb to uart driver manually: https://www.ftdichip.com/Drivers/D2XX.htm Download the setup executable and then install it. When installed success you can see the usb serial port can be used. 2\Downloading UUU Tool For the UUU binary file, download it from github: uuu release page on github. For the Q10.0.0_2.0.0 version use the UUU 1.3.124 version. For Linux OS, download the file named "uuu". For Windows OS, download the file named "uuu.exe". Here I use win10 system, so I download the uuu.exe file.   3\Download the Q10.0.0_2.0.0 Demo images for i.MX8MM   Now all the android os for i.MX products are here: Android OS for i.MX Applications Processors. Decompress release_package/android-10.0.0_2.0.0_image_8mmevk.tar.gz for LPDDR4 board. The package contains the image files and uuu_imx_android_flash tool. Copy uuu.exe to the directory of Q10.0.0_2.0.0 Demo images. 4\ Execute the uuu_imx_android_flash to flash image Power on the board. Open the serial port terminal and setting as following: Open a command line window. For the use and the Options for uuu_imx_android_flash tool details can see the Table 2 in the Android_Quick_Start_Guide. Here I use the OLED screen, to test MIPI panel output, need execute the tool with "-d mipi-panel". So here I use the .\uuu_imx_android_flash.bat -f imx8mm -e -d mipi-panel . When I use the download I meet the follow question: C:\Work\Products\Android BSP\New folder\Q10.0.0_2.0.0 Demo images\android-10.0.0_2.0.0_image_8mmevk>.\uuu_imx_android_flash.bat -f imx8mm -e -d mipi-panel This script is validated with uuu 1.3.124 version, it is recommended to align with this version. dtbo is supported dual slot is supported dynamic partition is supported You do not have sufficient privilege to perform this operation.   So here can change to use the Windows PowerShell, it works well and finished download.   Power off the board. 5\Boot up the board from emmc Set boot mode For Rev. C boards: Change sw1101 to 0110110010 and change sw1102 to 0001101000 if you want to boot from SD card. Change sw1101 to 0110110001 and change sw1102 to 0001010100 if you want to boot from eMMC. Set the U-Boot environment variables for the MIPI panel display U-Boot > setenv bootargs console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200 init=/init androidboot.console=ttymxc1 androidboot.hardware=freescale cma=800M@0x400M-0xb80M androidboot.primary_display=imx-drm firmware_class.path=/vendor/firmware transparent_hugepage=never androidboot.wificountrycode=CN androidboot.lcd_density=240 U-Boot > saveenv Then use the boot to boot up and then display on OLED screen.   Hope this can do help for some users. Best Regards Rita
查看全文