i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
This article is to show how to use CLK2 for PCIe ref clock for i.MX8MQ. Test Environment  i.MX8MQ + BSP L5.10.52 Background In order to cost down, some customers used CLK2 as PCIe reference clock as below while no external OSC installed, which is different with i.MX8MQ EVK design, so no clock output for PCIe.  CLK2 for PCIE clock.png Checked L4.14.98_2.3.0 and found it added internal PLL for PCIe clock support. internal PLL of PCIe REF_CLK.JPG Solution The attached patch based on 4.14.98 can’t be used directly on 5.10.52, the following is the main modification for PLLOUT of PCIe clock. PLLOUT Monitor Configuration Register contains bits to control the clock that will be generated on the CCM clock mapped to CLK2_P/N. internal PLL clock.png        
查看全文