i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
This article is to show how to use CLK2 for PCIe ref clock for i.MX8MQ. Test Environment  i.MX8MQ + BSP L5.10.52 Background In order to cost down, some customers used CLK2 as PCIe reference clock as below while no external OSC installed, which is different with i.MX8MQ EVK design, so no clock output for PCIe.  CLK2 for PCIE clock.png Checked L4.14.98_2.3.0 and found it added internal PLL for PCIe clock support. internal PLL of PCIe REF_CLK.JPG Solution The attached patch based on 4.14.98 can’t be used directly on 5.10.52, the following is the main modification for PLLOUT of PCIe clock. PLLOUT Monitor Configuration Register contains bits to control the clock that will be generated on the CCM clock mapped to CLK2_P/N. internal PLL clock.png        
記事全体を表示