Host TFTP and NFS Configuration    Now configure the Trivial File Transfer Protocol (TFTP) server and Networked File System (NFS) server. U-Boot will download the Linux kernel and dtb file using tftp and then the kernel will mount (via NFS) its root file system on the computer hard drive.    1. TFTP Setup     1.1.1 Prepare the TFTP Service     Get the required software if not already set up. On host for TFTP:       Install TFTP on Host      $ sudo apt-get install tftpd-hpa        (Note: There are a number of examples in various forums, etc, of how to automatically start the TFTP service - but not all are successful on all Linux distro's it seems! The following may work for you.)        Start the tftpd-hpa service automatically by adding a command to /etc/rc.local.      $ vi /etc/rc.local             Now, just before the exit 0 line edit below command then Save and Exit.      $ service tftpd-hpa start             Now, To control the TFTP service from the command line use:      $ service tftpd-hpa restart              To check the status of the TFTP service from the command line use:      $ service tftpd-hpa status          1.1.1 Setup the TFTP Directories        Now, we have to create the directory which will contain the kernel image and the device tree blob file.       $ mkdir -p /imx-boot/imx6q-sabre/tftp             Then, copy the kernel image and the device tree blob file in this directory.       $ cp {YOCTO_BUILD_DIR}/tmp/deploy/images/{TARGET}/zImage /imx-boot/imx6q-sabre/tftp $ cp {YOCTO_BUILD_DIR}/tmp/deploy/images/{TARGET}/<dtb file> /imx-boot/imx6q-sabre/tftp           OR       we can use the default directory created by yocto {YOCTO_BUILD_DIR}/tmp/deploy/images/{TARGET}/           The tftpd-hpa service looks for requested files under /imx-boot/imx6q-sabre/tftp  The default tftpd-hpa directory may vary with distribution/release, but it is specified in the configuration file: /etc/default/tfptd-hpa. We have to change this default directory with our directory        Edit default tftp directory      $ vi /etc/default/tftpd-hpa        Now, change the directory defined as TFTP_DIRECTORY with your host system directory which contains kernel and device tree blob file.       Using created directory      TFTP_DIRECTORY=”/imx-boot/imx6q-sabre/tftp”       OR       Using Yocto directory path      TFTP_DIRECTORY=”{YOCTO_BUILD_DIR}/tmp/deploy/images/{TARGET}”          Restart the TFTP service if required      $ service tftpd-hpa restart        1.2 NFS Setup    1.2.1 Prepare the NFS Service    Get the required software if not already set up. On host for NFS:       Install NFS on Host      $ sudo apt-get install nfs-kernel-server          The NFS service starts automatically. To control NFS services :      $ service nfs-kernel-server restart          To check the status of the NFS service from the command line :      $ service nfs-kernel-server status           1.2.2 Setup the NFS Directories       Now, we have to create the directory which will contain the root file system.      $ mkdir -p /imx-boot/imx6q-sabre/nfs           Then, copy the rootfs in this directory.      $ cp -R {YOCTO_BUILD_DIR}/tmp/work/{TARGET}-poky-linux-gnueabi/{IMAGE}/1.0-r0/rootfs/* /imx-boot/imx6q-sabre/nfs        OR       we can use the default directory created by yocto.      $ {YOCTO_BUILD_DIR}/tmp/work/{TARGET}-poky-linux-gnueabi/{IMAGE}/1.0-r0/rootfs       1.2.3 Update NFS Export File       The NFS server requires /etc/exports to be configured correctly to access NFS filesystem directory to specific hosts.      $ vi /etc/exports            Then, edit below line into the opened file.       <”YOUR NFS DIRECTORY”> <YOUR BOARD IP>(rw,sync,no_root_squash,no_subtree_check)    Ex.  If you created custom directory for NFS then,  /imx-boot/imx6q-sabre/nfs <YOUR BOARD IP>(rw,sync,no_root_squash,no_subtree_check)  Ex: /imx-boot/imx6q-sabre/nfs 192.168.*.*(rw,sync,no_root_squash,no_subtree_check)    OR    /{YOCTO_BUILD_DIR}/tmp/work/{TARGET}-poky-linux-gnueabi/{IMAGE}/1.0-r0/rootfs <YOUR BOARD IP>(rw,sync,no_root_squash,no_subtree_check)              Now, we need to restart the NFS service.      $ service nfs-kernel-server restart        2 Target Setup     We need to set up the network IP address of our target.       Power On the board and hit a key to stop the U-Boot from continuing. Set the below parameters,       setenv serverip 192.168.0.206       //This must be your Host IP address             The path where the rootfs is placed in our host has to be indicated in the U-Boot,       Ex.  // if you choose default folder created by YOCTO   setenv nfsroot /{YOCTO_BUILD_DIR}/tmp/work/{TARGET}-poky-linux-gnueabi/{IMAGE}/1.0-r0/rootfs     OR    // if you create custom directory for NFS  setenv nfsroot /imx-boot/imx6q-sabre/nfs             Now, we have to set kernel image name and device tree blob file name in the u-boot,       setenv image < zImage name >  setenv fdt_file <dtb file name on host>             Now, set the bootargs for the kernel boot,      setenv netargs 'setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp'          Use printenv command and check loadaddr and fdt_addr environment variables variables for I.MX6Q SABRE,       loadaddr=0x12000000  fdt_addr=0x18000000            Also, check netboot environment variable. It should be like below,      netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;          Now, set environment variable bootcmd to boot every time from the network,      setenv bootcmd run netboot          Now finally save those variable in u-boot:      saveenv          Reset your board; it should now boot from the network:       U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+ga57b13b (Apr 17 2018 - 17:13:43 +0530)    (..)   Net:   FEC [PRIME]  Normal Boot  Hit any key to stop autoboot:  0      Booting from net ...  Using FEC device  TFTP from server 192.168.0.206; our IP address is 192.168.3.101  Filename 'zImage'.  Load address: 0x12000000  Loading: #################################################################           #################################################################           #################################################################           #################################################################           #################################################################           #################################################################           ###########################################################           2.1 MiB/s  done  Bytes transferred = 6578216 (646028 hex)  Using FEC device  TFTP from server 192.168.0.206; our IP address is 192.168.3.101  Filename 'imx6q-sabresd.dtb'.  Load address: 0x18000000  Loading: ####           1.8 MiB/s  done  Bytes transferred = 45893 (b345 hex)  Kernel image @ 0x12000000 [ 0x000000 - 0x646028 ]  ## Flattened Device Tree blob at 18000000     Booting using the fdt blob at 0x18000000     Using Device Tree in place at 18000000, end 1800e344  switch to ldo_bypass mode!     Starting kernel ...       
        
        查看全文