无线连接知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wireless Connectivity Knowledge Base

讨论

排序依据:
1.    Introduction   1.1 Document Purpose This post entry provides a detailed description of how to integrate the NFC Reader Library to a KW3x Bluetooth Low Energy application.   1.2 Audience The goal of this post is to serve as a guide for software developers who want to use, adapt and integrate the NFC Reader Library to an SDK wireless connectivity example.   1.3 References and Resources - NFC Reader Library:  nxp.com/pages/:NFC-READER-LIBRARY - NCF3320: nxp.com/products/:NCx3320  - CLRC663 plus: nxp.com/products/:CLRC66303HN - FRDM-KW36 board: nxp.com/demoboard/FRDM-KW36 - KW35/KW36 SDK: https://mcuxpresso.nxp.com/en/select - MCUXpresso IDE: nxp.com/products/: MCUXpresso-IDE   2. NFC Reader Library Overview   The NXP NFC Reader Library is a modular software library written in C language, which provides an API that enables customers to create their own software stack and applications for the NXP contactless reader ICs: - PN512; - CLRC633 family; - PN7462 family; - PN5180; This API facilitates the most common operations required in NFC applications such as: - reading or writing data into contactless cards or tags; - exchanging data with other NFC-enabled devices; - allowing NFC reader ICs to emulate cards. The NFC Reader Library is designed in a way to be easily portable to many different microcontrollers with a multi-layered architecture:   As main blocks, we have: - Application Layer (AL) - implements the command sets to interact with MIFARE cards and NFC tags. - NFC activity - implements a configurable Discovery loop for the detection of contactless cards, NFC tags or other NFC devices. - HCE and P2P components, for the emulation of Type 4 tags and P2P data exchange respectively. - Protocol abstraction layer (PAL) - contains the RF protocol implementation of the ISO14443, Felica, vicinity and NFC standards. - Hardware abstraction layer (HAL) - implements the drivers for controlling the NFC frontends RF interface and capabilities. - Driver Abstraction Layer (DAL) - implements the GPIO pinning, the timer configuration and the physical interface (BAL) between the host MCU and the reader IC. - OSAL module, in charge of abstracting the OS or RTOS specifics (tasks events, semaphores, and threads)   3. The KW3x Wireless Microcontroller Overview The KW3x wireless microcontrollers (MCU are highly integrated single-chip devices that enable Bluetooth Low Energy (Bluetooth LE) and Generic FSK connectivity for automotive, industrial and medical/healthcare embedded systems.   The KW36/35 Wireless MCU integrates an Arm® Cortex®-M0+ CPU with up to 512 KB flash and 64 KB SRAM and a 2.4 GHz radio that supports Bluetooth LE 5.0 and Generic FSK modulations. The Bluetooth LE radio supports up to 8 simultaneous connections in any master/slave combination. The KW36A/36Z includes an integrated FlexCAN module enabling seamless integration into an automotive or industrial CAN communication network, enabling communication with external control and sensor monitoring devices over Bluetooth LE.   For more details please refer to the NXP website information: https://www.nxp.com/products/wireless/bluetooth-low-energy:BLUETOOTH-LOW-ENERGY-BLE.   4. NFC Reader Library – integration with FRDM-KW36 The current NFC Reader Library v5.21.01 is not containing support for Kinetis KW3x MCU. We will use a reference the K82 NFC Reader Library package: www.nxp.com/pages/:NFC-READER-LIBRARY. The steps required to integrate the library are: - Hardware preparation (the connection between FRDM-KW36 and NFC reader board); - Setting up the development environment (SDK download, workspace); - Preparing adaptation files for FRDM-KW3x board; - Integrating NFC application to Wireless_UART Bluetooth LE example; - Running the demo;   4.1 Hardware preparation Hardware required: - NCF3320 Antenna v1.0 board as an NFC transceiver; - FRDM-KW36 board as host MCU, used to load and run the Bluetooth Low Energy Stack and NFC application logic;   The communication between the boards will be via the SPI communication using the following pin configuration: ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ Master board (FRDM-KW36)         Connects to            Slave board (NCF3320 Antenna v1.0)           ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ PTB0  (J2-pin10)                                      -                    IRQ PTB1  (J2-pin9)                                         -                    Reset PTA16 (J2-pin1 - SPI1_Sout)                   -                    MOSI PTA17 (J1-pin5 - SPI1_Sin)                     -                    MISO PTA18 (J1-pin7 - SPI1_SCK)                   -                    SCK PTA19 (J2-pin3 - SPI1_CS)                     -                    CS GND   (J3-pin7)                                        -                    GND ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~   4.2 Setting up the development environment   Install MCUXpresso IDE (for this example we are using v10.2.0 build 759)   - Go to MCUXpresso-IDE webpage and download the latest version of IDE: www.nxp.com/products/: MCUXpresso-IDE. - Install the IDE;     Get the latest NFC Reader Library release (for this example we are using v5.21.00) - Go to NXP NFC Reader Library webpage (www.nxp.com/pages/:NFC-READER-LIBRARY) - Go to the Downloads tab and click on the download button - Download the NFC Reader Library for Kinetis K82F package:     Generate a downloadable SDK package for FRDM-KW36 board (SDK_2.2.1_FRDM-KW36) - Navigate to https://mcuxpresso.nxp.com/en/select and select FRDM-KW36 board; - Select Build MCUXpresso SDK. - As toolchain, please make sure that the MCUXpresso IDE is selected. - Use Download SDK button to start downloading SDK package:   Create MCUXpresso workspace - Open MCUXpresso IDE and create a workspace; - Drag and drop the SDK_2.2.1_FRDM-KW36 into the installed SDKs tab of the MCUXpresso IDE;   - Import Wireless_Uart Example to the current workspace:     4.3 Preparing adaptation files for FRDM-KW3x board This chapter describes the Driver Abstraction Layer (DAL) changes required for FRDM-KW36: - unzip the NFC Reader Library and navigate to boards folder:   - Create an equivalent file for FRDM-KW36 (Board_FRDM_KW36FRc663.h) by setting the right configuration for GPIOs and handlers; - Below are the differences required for FRDM-KW36 board in comparation with a FRDM-K82F board:   - Add the FRMD-KW36 to …DAL\cfg\BoardSelection.h file:   #ifdef PHDRIVER_FRDM_KW36FRC663_BOARD #include <Board_FRDM_KW36FRc663.h> #endif   - In KinetisSDK folder, update the following dependencies: o PIT Driver IRQ name:   o Open drain and pin lock configuration: - phDriver_KinetisSDK.c:   - phbalReg_KinetisSpi.c:   - add PHDRIVER_FRDM_KW36FRC663_BOARD define to …\NxpNfcRdLib\types\ph_NxpBuild_Platform.h file to enable the right NFC transceiver:     4.4  Integrating NFC application to Wireless_UART Bluetooth LE example In this chapter we will integrate the BasicDiscoveryLoop NFC example to Wireless_UART Bluetooth LE application. For this, the following steps are required: - On the wireless_uart project location create an “nfc” folder:   - Copy from modified NFC Reader Library the DAL, NxpNfcRdLib and phOsal folders:   - On the wireless_uart project location, “source” folder create a new “nfc” subfolder to integrate the BasicDiscovery loop files:   - Some changes will be required on the BasicDiscoveryLoop files: o Main function renamed to NFC_BasicDiscoveryLoop_Start; o Removed drivers/OS initialization; (all the changes can be observed in the attachment) - Update MCUXpresso workspace by pressing F5 to see the latest changes:   - Update the linker information (Project Properties -> C/C++ Build -> Settings) and preprocessor defines (Project Properties -> C/C++ Build -> Preprocessor):     - Add dependencies: o PIT module/ PIT module initialization; o Update LED, SW configuration; o Increase heap size (gTotalHeapSize_c); o Add functionality for NFC in wireless_uart.c application; (all the changes can be observed in the attachment);   Considering the attached ZIP archive, we can be easily dragged and drop, frdmkw36_w_uart_ncf3320_basic_discovery.zip file, to the MCUXpresso workspace:       4.5 Running the demo - Create hardware connection based on chapter 4.1; - Open a serial terminal on the corresponding COM port for FRDM-KW36 board. The BaudRate used is 115200. - Press SW2 on FRDM-KW36 to start advertising. - Open Mobile APP - IOT toolbox - Wirreless UART.  The FDRM-KW36 board will be listed as NXP_WU:   - Create Bluetooth LE connection. The serial log will contain the log for Bluetooth LE operations:     - Use NFC Cards close to NCF3320 Antenna v1.0 board to initiate discovery demo. - Once the card is detected, an event is sent to the mobile application including technology and UUID of the card: (https://www.youtube.com/watch?v=wCCz5zDIwHE&feature=youtu.be)     Attached is the source code for this example application (frdmkw36_w_uart_ncf3320_basic_discovery).
查看全文
The radio certification has been performed on JN5189, QN9090 and K32W products. The certificates or declaration of conformity are available in attached files.   And click here to know more on the best way to build a PCB the first time right with K32W061, QN9090 or JN5189 ! 
查看全文
In the process of practical application, customers often need the combination of ble + NFC. At present, our IOT-DK006 is the only development board with NFC module. But the NFC example is not perfect. So we porting the library of NFC reader- PN7150, to support KW series microcomputer so that KW series can handle the demand of ble + NFC function. Now I will introduce you how to port the NFC lib to KW. 1 PN7150 Introduction PN7150 is the high-performance version of PN7120, the plug’n play NFC solution for easy integration into any OS environment, reducing Bill of Material (BOM) size and cost. PN71xx controllers are ideal for home-automation applications such as gateways and work seamlessly with NFC connected tags. 2 Tools hardware:FRDM-KW36,PN7150 , some wire software:mcuxpresso11.3 package:NXP-NCI MCUXpresso example Project This package contains the nfc library and example that we need. We will refer the ‘NXPNCI-K64F_example’ firstly. Sdk version: 2.2.8, Example: frdmkw36_rtos_examples_freertos_i2c  3 Steps Hardware part:We need connect the PN7150 to KW36 like the picture. Although we can connect the PN7150 to board through the ardunio connector, the pin’s voltage is not enough to drive the PN7150. So we need a wire connected to U1 to get 3.3V.   PN7150 FRDM-KW36 VBAT/PVDD 3.3V VANT 5V GND GND IRQ PTA16 VEN PTC15 SCL PTB0,I2C0 SDA PTB1,I2C0 Software part:We should add the nfc library and directory into our project. You can check the following picture to know what file is necessary. If you want to know how to add directory into our project, you can refer this link. The red line shows what file we need. Please notice that when we add file path into the mcuxpresso configuration, we also need add the path into ‘Path and Symbols’ .   We need add some macro into ‘Preprocessor’.   We copy the NXPNCI-K64F_example’s main file content into our ‘freertos_i2c.c’. Next, we need modify the file pin_mux.c, tml.c and board.h   In file board.h,add the following macro. Don't forget to enable the pin clock. /* NXPNCI NFC related declaration */ #define BOARD_NXPNCI_I2C_INSTANCE I2C0 #define BOARD_NXPNCI_I2C_BAUDRATE (100000) #define BOARD_NXPNCI_I2C_ADDR       (0x28) #define BOARD_NXPNCI_IRQ_PORTIRQn PORTA_IRQn #define BOARD_NXPNCI_IRQ_GPIO     (GPIOA) #define BOARD_NXPNCI_IRQ_PORT     (PORTA) #define BOARD_NXPNCI_IRQ_PIN      (16U) #define BOARD_NXPNCI_VEN_GPIO     (GPIOC) #define BOARD_NXPNCI_VEN_PORT     (PORTC) #define NXPNCI_VEN_PIN            (5U)     In file pin_mux.c, add head file ‘board.h’. Add the following code in function ’ BOARD_InitPins’. The step is to configure the VEN, IRQ and I2C0. This example contains the I2C1’s code, you can comment them.     /* Initialize NXPNCI GPIO pins below */   /* IRQ and VEN PIN_MUX Configuration */   PORT_SetPinMux(BOARD_NXPNCI_IRQ_PORT, BOARD_NXPNCI_IRQ_PIN, kPORT_MuxAsGpio);   PORT_SetPinMux(BOARD_NXPNCI_VEN_PORT, NXPNCI_VEN_PIN, kPORT_MuxAsGpio);   /* IRQ interrupt Configuration */   NVIC_SetPriority(BOARD_NXPNCI_IRQ_PORTIRQn, 6);   EnableIRQ(BOARD_NXPNCI_IRQ_PORTIRQn);   PORT_SetPinInterruptConfig(BOARD_NXPNCI_IRQ_PORT, BOARD_NXPNCI_IRQ_PIN, kPORT_InterruptRisingEdge);   Finally, in file tml.c, modify PORTC_IRQHandler as PORTA_IRQHandler We finished all steps. 4 Results We use ntag to test the reading and writing operation.   When the tag is closed to the PN7150, we will get the following message.   The text recording is ‘VER=03’. Next, we will modify the text recording We need add the new macro to preprocessor.   We can modify the variable NDEF_MESSAGE in function task_nfc_reader to modify the text recording.   Then we download the program again. We will see the original text ‘VER=03’ and the text has been modified. Then we read the tag again. We will see the new text.   If we want to send the larger text, what should we do? We need modify the macro ‘ADD’. When only 4 characters are sent, ‘ADD’ is 0. And every additional character is added, the ‘ADD’ will add. We modify the tag as ‘Ver=03’, and we have two more characters. So ‘ADD’ needs to be defined as 2   It firstly shows the text ‘Test’. Then it will show the new text ‘Ver=03’. Other tags’ reading and writing operation can be enabled by defining some macro.      
查看全文
This document provides the calculation of the Bluetooth Low Power consumption linked to the setting of the Kinetis.   The Power Profile Calculator is build to provide the power consumption of your application. It's a mix between real measurements in voltage and temperature. The process is not taken into account which may create some variation.   DISCLAIMER: This excel workbook is provided as an estimation tool for NXP customers and is based on power profile measurements done on a set of randomly selected parts. A specific part may exhibit deviation from the nominal measurements used on this tool.   This document is the summary of all the information available in the AN12180 Power Consumption Analysis - FRDM-KW36 available in the NXP web page.   Several parameters could be fill-in: Buck or bypass mode (DCDC) Supply Voltage (2.4V to 3.6V) Temperature (-40°C to +105°C) Processor configuration (20MHz, 32MHz or 48MHz) 2 different deep sleep modes (LLS3 or VLLS2) Different Tx output power (0dBm, +3.5dBm or +5dBm) Possibility to set the Advertising interval, connection interval, scan interval and active scan windows duration Fix the Bluetooth Packet sizes in Advertising and Connection  Tx/Rx payload.   One optional information is to provide an idea of the duration life time on typical batteries.
查看全文
The High Power board design files can be found on the JN5189 product webpage, in the JN-RD-6054-JN5189 Design Files. More precisely, the reference manual and the design files are attached to this article (OM15072-2_MOD_EXT_AMP_QFN40_PCB2467-2.0.zip and JN-RM-2078-JN5189-Module-Development_1V4.pdf) Some guidance is available here. The RF performances are presented in the attached test report (powerpoint file). The FCC/IC Certificates or Declarations of conformity are in the article "Certificates/Declarations of conformity (nxp community)".  
查看全文
简介: 当 OTAP 客户端(接收软件更新的设备,通常为 Bluetooth LE 外围设备)从 OTAP 服务器 (发送软件更新的设备,通常为 Bluetooth LE Central)请求软件更新时,您可能希望保留一 些数据,例如绑定信息,系统振荡器的匹配值或您的应用程序的 FlexNVM 非易失数据。 本 文档指导您在执行 OTAP 更新时, 如何保留您感兴趣的闪存数据内容。 本文档适用于熟悉 OTAP 定制 Bluetooth LE 服务的开发人员,有关更多基础信息,您可以阅读以下文章: 使用 OTAP 客户端软件对 KW36 设备进行重新编程。 OTAP 标头和子元素 OTAP 协议为软件更新实现了一种格式,该格式由标题和定义数量的子元素组成。 OTAP 标 头描述了有关软件更新的一般信息,并且其定义的格式如下图所示。 有关标题字段的更多 信息,请转至 SDK 中的<SDK_2.2.X_FRDM-KW36_Download_Path> \ docs \ wireless \ Bluetooth 中的《 Bluetooth Low Energy Application Developer's Guide》文档的 11.4.1 Bluetooth Low Energy OTAP 标头一章。   每个子元素都包含用于特定目的的信息。 您可以为您的应用程序实现专有字段(有关子元 素字段的更多信息, 请转至 SDK 中的<SDK_2.2.X_FRDM-KW36_Download_Path> \ docs \ wireless \ Bluetooth 中的《 Bluetooth Low Energy Application Developer's Guide》文档的 11.4.1 Bluetooth Low Energy OTAP 标头一章。 OTAP 包含以下子元素: 镜像文件子元素 值字段长度(字节) 描述 升级镜像 变化 该子元素包含实际的二进制可执行镜像,该镜像将被复制到 OTAP 客户端设备的闪存中。 该子元素的最 大大小取决于目标硬件。 扇区位图 32 该子元素包含目标设备闪存的扇区位图,该位图告诉引导加载程序哪些扇区应被覆盖,哪些扇区保持完 整。 该字段的格式是每个字节的最低有效位在前,最低有效字节和位代表闪存的最低存储部分。 镜像文件CRC 2 是在镜像文件的所有元素(此字段本身除外)上计算的 16 位 CRC。 该元素必须是通过空中发送的镜像文件中的最后一个子元素。   OTAP 扇区位图子元素 KW36 闪存分为: 一个 256 KB 程序闪存( P-Flash)阵列, 最小单元为 2 KB 扇区,闪存地址范围为 0x0000_0000 至 0x0003_FFFF。 一个 256 KB FlexNVM 阵列, 最小单元为 2 KB 扇区,闪存地址范围为 0x1000_0000 至 0x1003_FFFF, 同时它也会被映射到地址范围为 0x0004_0000 至 0x0007_FFFF 的空间。 位图子元素的长度为 256 位,就 KW36 闪存而言,每个位代表 2KB 扇区,覆盖从 0x0- 0x0007_FFFF 的地址范围(P-Flash 到 FlexNVM 映射地址范围),其中 1 表示该扇区应 被擦 除, 0 表示应保留该扇区。 OTAP 引导加载程序使用位图字段来获取在使用软件更新对 KW36 进行编程之前应擦除的地址范围,因此必须在发送软件更新之前对其进行配置,以使包含您 的数据的内存的地址范围保持不变。仅擦除将被软件更新覆盖的地址范围。 例如:假设开发人员想要保留 0x7D800-0x7FFFF 之间的地址范围和 0x0-0x1FFF 之间的地址 范围,并且必须擦除剩余的存储器。 0x7D800-0x7FFFF 之间的地址范围对应于前 5 个闪存 扇区, 0x0-0x1FFF 之间的地址范围是最低的 4 个扇区。 因此,这意味着应将 256 和 252 之间的位(256、 255、 254、 253 和 252)以及 4 和 1 之间 的位(4、 3、 2 和 1)设置为 0,这样本示例的 OTAP 位图为 : 0x07FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF0 使用 NXP 测试工具配置 OTAP 位图以保护地址范围 在恩智浦网站上下载并安装用于连接产品的测试工具   在 PC 上打开 NXP Test Tool 12 软件。 转到“ OTA 更新-> OTAP 蓝牙 LE”,然后单击“浏 览...”按钮加载用于软件更新的映像文件(NXP 测试工具仅接受.bin 和.srec 文件)。 您 可以配置 OTAP 位图,选择“覆盖扇区位图”复选框,并通过新的位图值更改默认值。 配 置位图后,选择“保存...”。   然后,将显示一个窗口,用于选择保存.bleota 文件的目的地,保存文件可以自行取名。 您可以将此文件与 Android 和 iOS 的 IoT Toolbox App 一起使用,以使用 OTAP 更新软 件。 这个新的.bleota 文件包含位图,该位图告诉 OTAP 引导加载程序哪些扇区将被擦 除,哪些扇区将被保留。    
查看全文
URL : https://community.nxp.com/docs/DOC-343990 版本:3 最后更新:09-14-2020 更新:EdgarLomeli 介绍 本文档介绍了如何通过无线编程引导加载程序将新的软件镜像加载到KW41 设备中。此外, 还将详细说明如何设置客户端软件以更改镜像文件的存储方式。 软件要求 1. IAR 嵌入式集成开发环境或MCUXpresso IDE 2. 下载两个软件包,SDK FRDM-KW41Z 和SDK USB-KW41Z。 硬件要求 1. FRDM-KW41Z 板 更新过程中的OTAP 内存管理 KW41 具有512KB 程序闪存,其闪存地址范围为0x0000_0000 至0x0007_FFFF。 1. OTAP 应用程序将闪存分为两个独立的部分,即OTAP 引导加载程序(Bootloader)和 OTAP 客户端。OTAP Bootloader 会验证OTAP 客户端上是否有可用的新镜像文件要对 设备进行重新编程。OTAP 客户端软件提供了将OTAP 客户端设备与包含新镜像文件 的OTAP 服务器进行通信所需的Bluetooth LE 自定义服务(OTAP 服务器设备可以是连 接到安装有测试工具的PC 或安装有IoT 工具箱应用的智能手机的另一个FRDM-KW41Z 板)。因此,需要对OTAP 客户端设备进行两次编程,首先编程OTAP Bootloader,然后 编程支持OTAP 客户端的Bluetooth LE 应用程序。为使两个不同的软件共存于同一设备 而使用的方法是将每个软件存储在不同的存储区域中。此功能由链接器文件实现。在 KW41 设备中,引导加载程序已从0x0000_0000 到0x0003_FFF 保留了16 KB 的内存区 域,因此OTAP Client 演示程序保留了其余的内存空间。 2. 要为客户端设备创建新的镜像文件,开发人员需要在链接文件中指定将以16 KB 的偏移 量放置代码,因为必须把最前面的地址空间预留给OTAP Bootloader。 3. 在连接状态下,OTAP 服务器通过蓝牙LE 将镜像数据包(称为块)发送到OTAP 客户 端设备。OTAP 客户端设备可以首先将这些块存储在外部SPI 闪存或片上闪存中。在 OTAP 客户端软件中可以选择代码存储的目的地。 4. 当连接完成,并将所有块都从OTAP 服务器发送到OTAP 客户端设备后,OTAP 客户端 软件会将信息,比如镜像更新的来源(外部闪存或内部闪存)写入称为Bootloader 标 志的内存部分中并复位MCU 以执行OTAP Bootloader 代码。OTAP 引导加载程序 (Bootloader)会读取引导加载程序(Bootloader)标志以获取对设备进行编程所需的信 息,并触发编程以使用新应用程序对MCU 进行重新编程。由于新应用程序的偏移地 址为16 KB,因此OTAP Bootloader 从0x0000_4000 地址开始对设备进行编程,并且 OTAP 客户端应用程序将被新镜像文件所覆盖,因此,通过该方法对设备重新编程后, 将无法二次以同样的方法对设备再次编程。最后,OTAP 引导加载程序(Bootloader) 会触发命令以自动开始执行新代码。 使用IAR 嵌入式开发工具准备软件以测试KW41Z 设备的OTAP 客户端 ⚫ 加载OTAP Bootloader 到FRDM-KW41Z 上。可以通过以下路径从SDK FRDM-KW41Z 中包含的项目中编程OTAP Bootloader 软件,也可以从以下路径中拖放已编译好的二进 制文件。 ⚫ OTAP Bootloader 项目: <SDK_2.2.0_FRDM-KW41Z_download_path>\boards\frdmkw41z\wireless_examples\framework\bootloader_otap\bm\iar\bootloader_otap_bm.eww OTAP Bootloader 已编译好的二进制文件: <SDK_2.2.0_FRDM-KW41Z_download_path>\tools\wireless\binaries\bootloader_otap_frdmkw41z.bin ⚫ 打开位于以下路径的SDK FRDM-KW41Z 中包含的OTAP Client 项目。 <SDK_2.2.0_FRDM-KW41Z_download_path>\boards\frdmkw41z\wireless_examples\bluetooth\otap_client_att\freertos\iar\otap_client_att_freertos.eww ⚫ 自定义OTAP 客户端软件以选择存储方式。在工作区的源文件夹中找到 app_preinclude.h 头文件。 1. 要选择外部闪存存储方式,请将“gEepromType_d”定义为 “gEepromDevice_AT45DB041E_c” 2. 要选择内部闪存存储方式,请将“gEepromType_d”定义为 “gEepromDevice_InternalFlash_c” ⚫ 配置链接标志。打开项目选项窗口(Alt + F7)。在“Linker->Config”窗口中,找到 “Configuration file symbol definitions”窗格。 1. 要选择外部闪存存储方式,请删除“gUseInternalStorageLink_d = 1”链接标志 2. 要选择内部闪存存储方式,请添加“gUseInternalStorageLink_d = 1”链接标志 ⚫ 加载OTAP 客户端软件到FRDM-KW41Z 板上(Ctrl + D).停止调试会话(Ctrl + Shift + D). 项目默认的链接器配置会把OTAP 客户端应用程序存储到相应的内存偏移位置上。 使用MCUXpresso IDE准备软件以测试KW41Z 设备的OTAP 客户端 ⚫ 加载OTAP Bootloader 到FRDM-KW41Z 上。可以通过以下路径从SDK FRDM-KW41Z 中包含的项目中编程OTAP Bootloader 软件,也可以从以下路径中拖放已编译好的二进 制文件。 OTAP Bootloader项目: wireless_examples->framework->bootloader_otap->bm OTAP Bootloader 已编译好的二进制文件 <SDK_2.2.0_FRDM-KW41Z_download_path>\tools\wireless\binaries\bootloader_otap_frdmkw41z.bin • 单击"Quickstart Panel"视窗中的"Import SDK examples(s)"选项 • 双击frdmkw41z 图标 • 打开位于下列路径中包含在SDK FRDM-KW41Z 中的OTAP 客户端项目 wireless_examples->bluetooth->otap_client_att->freertos • 自定义OTAP 客户端软件以选择存储方式。在工作区的源文件夹中找到 app_preinclude.h 头文件。 1. 要选择外部闪存存储方式,请将“gEepromType_d”定义为 “gEepromDevice_AT45DB041E_c” 2. 要选择内部闪存存储方式,请将“gEepromType_d”定义为 “gEepromDevice_InternalFlash_c” • 配置链接文件 1. 若选择外部闪存存储方式,从此时起无需对项目中做任何修改,可跳过此步骤。 2. 若选择内部闪存存储方式,搜索位于下列路径中SDK USB-KW41Z 中的链接文件, 替换OTAP 客户端项目中源文件夹中的默认链接文件。你可以从SDK USB-KW41Z 复制(Ctrl+C ) 链接文件,并直接粘贴(Ctrl + V)在工作区中。这将显示一条警告消息,选择”Overwrite "。 SDK USB-KW41Z 上的链接文件: <SDK_2.2.0_USB-KW41Z_download_path>\boards\usbkw41z_kw41z\wireless_examples\bluetooth\otap_client_att\freertos\MKW41Z512xxx4_connectivity.ld • 保存项目中的更改。在“Quickstart Panel”中选择“Debug”。一旦项目已经加载到 设备上,请停止调试会话。 在IAR 嵌入式工作台中为FRDM-KW41Z OTAP 客户端创建S 记录镜像文件 • 从SDK FRDM-KW41Z 中打开要使用OTAP Bootloader 进行编程的一个无线连接的 项目。本示例是一个使用葡萄糖传感器的项目,该项目位于以下路径。 <SDK_2.2.0_FRDM-KW41Z_download_path>\boards\frdmkw41z\wireless_examples\bluetooth\glucose_sensor\freertos\iar\glucose_sensor_freertos.eww • 打开项目选项窗口(Alt + F7)。在“Linker->Config”窗口中,在“Configuration file symbol definitions”文本框中添加以下链接标志。 gUseBootloaderLink_d=1 • 转到“Output Converter”窗口。取消选择“Override default”复选框,展开“Output format”组合框,然后选择Motorola S-records 格式,然后单击“确定”按钮。 • 重编译项目。 • 在以下路径中搜索S-Record 文件(.srec)<SDK_2.2.0_FRDM-KW41Z_download_path>\boards\frdmkw41z\wireless_examples\bluetooth\glucose_sensor\freertos\iar\debug 在MCUXpresso IDE 中为FRDM-KW41Z OTAP 客户端创建S-Record 镜像文件 • 从MCUXpresso IDE 中打开要使用OTAP Bootloader 进行编程的一个无线连接的项 目。本示例是一个使用葡萄糖传感器的项目,该项目位于以下路径。 wireless_examples->bluetooth->glucose_sensor->freertos • 搜索位于以下路径的SDK FRDM-KW41Z 中的链接文件,并替换Glucose Sensor 项 目中源文件夹中的默认链接文件。你可以从SDK FRDM-KW41Z 复制(Ctrl + C) 链接文件,然后直接粘贴(Ctrl + V)到工作区中。这将显示一条警告消息,请选择“Overwrite”。 SDK FRDM-KW41Z 上的链接文件: <SDK_2.2.0_FRDM- KW41Z_download_path>\boards\frdmkw41z\wireless_examples\bluetooth\otap_client_att\freertos\MKW41Z512xxx4_connectivity.ld • 打开新的“MKW41Z512xxx4_connectivity.ld”链接文件。找到下图的段位置,并删除 “FILL”和“BYTE”语句。 • 编译项目。 在工作区中找到“Binaries”图标。在“.axf”文件上单击鼠标右键。选择“Binary Utilities/Create S-Record”选项。S-Record 文件将保存在工作区中带有“.s19”扩展名的 “Debug”文件夹中。 使用IoT Toolbox App 测试OTAP 客户端演示 1. 将通过上一节中的步骤创建的S-Record 文件保存在智能手机中的已知位置。 2. 打开IoT Toolbox App,然后选择OTAP 演示。按“SCAN”开始扫描合适的广告客户。 3. 按下FRDM-KW41Z 板上的“SW4”按钮开始广告。 4. 与找到的设备建立连接。 5. 按“Open”并搜索S-Record 文件 6. 按“Upload”开始传输。 7. 传输完成后,请等待几秒钟,直到引导加载程序(bootloader)完成对新镜像文件 的编程。新的应用程序将自动启动。 标签:KW KW41Z | 31Z | 21Z frdm-kw41
查看全文
从 MKW36Z512VHT4 到 MKW36A512VFT4 的软件移植指南 URL:https://community.nxp.com/docs/DOC-345487 由 Edgar Eduardo Lomeli Gonzalez 于 2020-09-14 创建的文档 引言 这篇文章将指导您如何从 MKW36Z512VHT4 移植到 MKW36A512VFT4 MCU。本示例将使用 “信标(beacon)” SDK 示例程序。 SDK 的下载和安装 1- 前往 MCUXpresso 网页:MCUXpresso 网页 2- 使用您的注册帐户登录。 3- 搜索“ KW36A”设备。单击建议的处理器型号,然后单击“Build MCUXpresso SDK”。 4- 点击后将显示另一页面。在“Toolchain / IDE”框中选择“All toolchains”,并提供名称以标 识软件包。然后点击“Download SDK”。   5- 接受许可协议。等待几分钟直到系统将软件包放入您的配置文件中。 单击“下载 SDK 存 档”(Download SDK Archive),下载 SDK,如下图所示。   6- 如果使用了 MCUXpresso IDE,请在“ Installed SDK’s”视图中拖放 KW36A SDK 压缩文件 夹来安装软件包。 至此,您已经下载并安装了 KW36A 芯片的 SDK 软件包。 MCUXpresso IDE 中的软件迁移 1- 在 MCUXpresso 工作区上导入“信标(beacon)”示例。单击“Import SDK examples(s)…” 选项,将出现一个新窗口。然后选择“ MKW36Z512xxx4”,单击 FRDM-KW36 图像。点击 “Next >”按钮。   2- 搜索信标例程并选择您的项目版本(裸机的 bm 或带 freertos 操作系统)。 3- 转到 Project/Properties。展开 C / C ++ Build / MCU 设置,然后选择 MKW36A512xxx4 MCU。单击“Apply and Close”按钮以保存配置。 4- 将 MKW36Z 文件夹重命名为 MKW36A,单击鼠标右键并选择“重命名”。这些是以下内容: framework/DCDC/Interface -> MKW36Z framework/DCDC/Source -> MKW36Z framework/LowPower/Interface -> MKW36Z framework/LowPower/Source -> MKW36Z framework/XCVR -> MKW36Z4 5- 在 MCUXpresso IDE 中打开“Project/Properties”窗口。 转到 C / C ++ Build / Settings,然 后在 Tool Settings 窗口中选择 MCU C Compiler / Includes 文件夹。在创建之前,根据 MKW35 文件夹,编辑与 MKW36 MCU 相关的所有路径。结果类似如下所示: ../framework/LowPower/Interface/MKW36A ../framework/LowPower/Source/MKW36A ../framework/DCDC/Interface/MKW36A ../framework/XCVR/MKW36A4  6- 在工具设置中选择 MCU Assembler/General 文件夹。 编辑与 MKW36 MCU 相关的路径。 结果类似如下所示: ../framework/LowPower/Interface/MKW36A ../framework/LowPower/Source/MKW36A ../framework/DCDC/Interface/MKW36A ../framework/XCVR/MKW36A4 7- 转到 Project/Properties。展开 MCU CCompiler/Preprocessor 窗口。编辑 “ CPU_MKW36Z512VHT4”和“ CPU_MKW36Z512VHT4_cm0plus”符号,分别将其重命名为 “ CPU_MKW36A512VFT4”和“ CPU_MKW36A512VFT4_cm0plus”。保存更改。 8- 转到工作区。删除位于 CMSIS 文件夹中的“ fsl_device_registers,MKW36Z4, MKW36Z4_features,system_MKW36Z4.h 和 system_MKW36Z4.c”文件。然后解压缩 MKW35Z SDK 软件包并在以下路径中搜索“ fsl_device_registers,MKW36A4,MKW36A4_features, system_MKW36A4.h 和 system_MKW36A4.c”文件到该文件夹中: <SDK_folder_root>/devices/MKW36A4/fsl_device_registers.h <SDK_folder_root>/devices/MKW36A4/MKW36A4.h <SDK_folder_root>/devices/MKW36A4/MKW36A4_features.h <SDK_folder_root>/devices/MKW36A4/system_MKW36A4.h <SDK_folder_root>/devices/MKW36A4/system_MKW36A4.c 9- 通过位于路径<SDK_folder_root> /devices/MKW36A4/mcuxpresso/startup_mkw36a4.c 中的“ startup_mkw36a4.c”覆盖“ startup_mkw36z4.c”(位于启动文件夹中)。 您只需拖放 启动文件夹,然后删除较旧的文件夹即可。 10- 在 CMSIS 文件夹中打开“ fsl_device_registers.h”文件。在以下代码(文件的第 18 行)中 添加“ defined(CPU_MKW36A512VFT4)”: 11- 在 bluetooth->host->config 文件夹中打开“ ble_config.h”文件。在以下代码中添加 “ defined(CPU_MKW36A512VFT4)”(文件的第 146 行): 12- 在 source-> common 文件夹中打开“ ble_controller_task.c”文件。在以下代码(文件的 第 272 行)中添加“ defined(CPU_MKW36A512VFT4)”: 13-生成项目。 至此,该项目已经在 MCUXpresso IDE 环境中移植完成。 IAR Embedded Workbench IDE 中的软件移植 1- 打开位于以下路径的信标项目: 2- 在工作区中选择项目,然后按 Alt + F7 打开项目选项。 3- 在 General Options/Target”窗口中,单击器件名称旁边的图标,再选择合适的器件 NXP / KinetisKW / KW3x / NXP MKW36A512xxx4,然后单击“确定”按钮。 4- 在以下路径中创建一个名为 MKW36A 的新文件夹: <SDK_root>/middleware/wireless/framework_5.4.6/DCDC/Interface <SDK_root>/middleware/wireless/framework_5.4.6/DCDC/Source <SDK_root>/middleware/wireless/framework_5.4.6/LowPower/Interface <SDK_root>/middleware/wireless/framework_5.4.6/LowPower/Source <SDK_root>/middleware/wireless/framework_5.4.6/XCVR   5- 复制位于上述路径的 MKW36Z 文件夹内的所有文件,然后粘贴到 MKW36A 文件夹中。   6- .在工作区中选择信标项目,然后按 Alt + F7 打开项目选项窗口。 在“ C/C++ Compiler/Preprocessor”窗口中,将所有路径里的 MKW36Z 文件夹重命名为 MKW36A 文件 夹。在已定义的符号文本框中,将 CPU_MKW36Z512VHT4 宏重命名为 CPU_MKW36A512VFT4。结果如下图所示:单击确定按钮。 7- 展开启动文件夹,选择所有文件,单击鼠标右键,然后选择“Remove”选项。在文件夹上 单击鼠标右键,然后选择““Add/Add files”。添加位于以下路径的 startup_MKW36A4.s: <SDK_root>/devices/MKW36A4/iar/startup_MKW36A4.s 另外,将 system_MKW36A4.c 和 system_MKW36A4.h 添加到启动文件夹中。 这两个文件都 位于如下的路径中: 8- 在 bluetooth->host->config 文件夹中打开“ ble_config.h”文件。在以下代码中添加 “ defined(CPU_MKW36A512VFT4)”: 9- 在 source-> common 文件夹中打开“ ble_controller_task.c”文件。在以下代码中添加 “ defined(CPU_MKW36A512VFT4)”: 10-生成项目。 至此,该项目已经在 IAR Embedded Workbench IDE 环境中移植完成。          
查看全文
Symptoms In the KW36 SDK, there is an API bleResult_t Controller_SetTxPowerLevel(uint8_t level, txChannelType_t channel) to set the Tx power, but the unit of param[in] level is not dBm. But how do we set a Tx power in dBm? Diagnosis By going through the source code, we found that two conversions are required between the actual dBm and the set value of the API. One is PA_POWER to Transmit Output Power conversion table:     Other is Level to PA_POWER  conversion table: .tx_power[0] = 0x0001, .tx_power[1] = 0x0002, .tx_power[2] = 0x0004, .tx_power[3] = 0x0006, .tx_power[4] = 0x0008, .tx_power[5] = 0x000a, .tx_power[6] = 0x000c, .tx_power[7] = 0x000e, .tx_power[8] = 0x0010, .tx_power[9] = 0x0012, .tx_power[10] = 0x0014, .tx_power[11] = 0x0016, .tx_power[12] = 0x0018, .tx_power[13] = 0x001a, .tx_power[14] = 0x001c, .tx_power[15] = 0x001e, .tx_power[16] = 0x0020, .tx_power[17] = 0x0022, .tx_power[18] = 0x0024, .tx_power[19] = 0x0026, .tx_power[20] = 0x0028, .tx_power[21] = 0x002a, .tx_power[22] = 0x002c, .tx_power[23] = 0x002e, .tx_power[24] = 0x0030, .tx_power[25] = 0x0032, .tx_power[26] = 0x0034, .tx_power[27] = 0x0036, .tx_power[28] = 0x0038, .tx_power[29] = 0x003a, .tx_power[30] = 0x003c, .tx_power[31] = 0x003e, The input parameter 'level' of the API is the subscript of this array. The array value is PA_POWER of first conversion table, then we can find the final Tx power. From another perspective, the parameter 'level' is the index of the first table.   Solution The following demonstrates a conversion process.  
查看全文
This document describes a simple process for enabling the user controls the radio through serial commands. Hardware requirements: • FRDM-KW41Z/QN902x board or a board programmed with HCI black box application. Software requirements: • Test Tool 12 application. It can be downloaded from the NXP web page. • HCI Black Box binary.   Running Demo 1. Load the board with hci_black_box example. 2. Open the Test Tool 12 software 3. Set up the correct Serial Configuration. If there were no changes in the application the default configuration will correspond to the one showed in the following figure. 4. Double click on the active device that you want to test, this will open the COM port in the command console. 5. Set the command set to the BLE_HCI.xml. This file has a list of the HCI commands that the user can send to the device, some of the commands have some options to be configured if necessary or some data to be filled. 6. To make easier the use of frequent commands, there is the option to add a shortcut to the command and the chosen behavior will be added to the panel. 7. Once you add the shortcut or choose the command or your preference, just double click over it and the tool will send the command to the device. In this case, we will send a reset on the board, this command does not receive any extra parameters, data or need any extra configuration.   8. If successful there will be a response or acknowledge of the behavior that will be shown in the right panel. Hope it helps. Regards, Mario
查看全文
The homologation requirements in China (MIIT [2002]353) obviously are planned (end of December 2022) to be sharpened (MIIT publication from 2021-01-27: “Notice on Matters Related to Radio Management in the 2400MHz, 5100MHz and 5800MHz Bands”).   A modification register is need on the KW38 and KW36 to pass the new Chinese  requirement with acceptable margin: PA_RAMP_SEL value must be set to 0x02h (2us) instead of 0x01h (1us default value) Modification SW: XCVR_TX_DIG_PA_CTRL_PA_RAMP_SEL(2) in the nxp_xcvr_common_config.c All the details are in the attached file.   Note: This SW modification is for China country only.
查看全文
This example of custom profile uses the Temperature Sensor and Temperature Collector examples as a base, so it can be easily modified. Both examples are in the SDK, so this document explains how to add the Humidity profile, and how to modify the code to get the Humidity Sensor and Collector working. Introduction Generic Attribute Profile (GATT) establishes in detail how to exchange all profile and user data over a BLE connection. GATT deals only with actual data transfer procedures and formats. All standard BLE profiles are based on GATT and must comply with it to operate correctly. This makes GATT a key section of the BLE specification, because every single item of data relevant to applications and users must be formatted, packed, and sent according to the rules. GATT defines two roles: Server and Client. The GATT server stores the data transported over the Attribute Protocol (ATT) and accepts Attribute Protocol requests, commands and confirmations from the GATT client. The GATT client accesses data on the remote GATT server via read, write, notify, or indicate operations. Notify and indicate operations are enabled by the client but initiated by the server, providing a way to push data to the client. Notifications are unacknowledged, while indications are acknowledged. Notifications are therefore faster, but less reliable.  GATT Database establishes a hierarchy to organize attributes. These are the Profile, Service, Characteristic and Descriptor. Profiles are high level definitions that define how services can be used to enable an application and Services are collections of characteristics. Descriptors defined attributes that describe a characteristic value.    To define a GATT Database several macros are provided by the GATT_DB API in the Freescale BLE Stack, which is part KW38 SDK. Server (Sensor)  First, we need to use the Temperature Sensor project as a base, to create our Humidity Custom Profile Server (Sensor). BLE SIG profiles To know if the Profile or service is already defined in the specification, you have to look for in Bluetooth SIG profiles and check in the ble_sig_defines.h file (${workspace_loc:/${ProjName}/bluetooth/host/interface) if this is already declared in the code. In our case, the service is not declared, but the characteristic of the humidity is declared in the specification. Then, we need to check if the characteristic is already included in ble_sig_defines.h. Since, the characteristic is not included, we need to define it as shown next:   /*! Humidity Charactristic UUID */ #define gBleSig_Humidity_d 0x2A6F   GATT Database The Humidity Sensor is going to have the GATT Server, because is going to be the device that has all the information for the GATT Client. On the Temperature Sensor demo have the Battery Service and Device Information, so you only have to change the Temperature Service to Humidity Service    In order to create the demo we need to define or develop a service that has to be the same as in the GATT Client, this is declared in the gatt_uuid128.h.If the new service is not the same, they will never be able to communicate each other. All macros, function or structure in SDK have a common template which helps the application to act accordingly. Hence, we need to define this service in the gatt_uuid128.h as shown next:    /* Humidity */ UUID128(uuid_service_humidity, 0xfe ,0x34 ,0x9b ,0x5f ,0x80 ,0x00 ,0x00 ,0x80 ,0x00 ,0x10 ,0x00 ,0x02 ,0x00 ,0xfa ,0x10 ,0x10)   All the Service and Characteristics is declared in gattdb.h. Descriptors are declared after the Characteristic Value declaration but before the next Characteristic declaration. In this case the permission is the CharPresFormatDescriptor that have specific description by the standard. The Units of the Humidity Characteristic is on Percentage that is 0x27AD. Client Characteristic Configuration Descriptor (CCCD) is a descriptor where clients write some of the bits to activate Server notifications and/or indications.   PRIMARY_SERVICE_UUID128(service_humidity, uuid_service_humidity) CHARACTERISTIC(char_humidity, gBleSig_Humidity_d, (gGattCharPropNotify_c)) VALUE(value_humidity, gBleSig_Humidity_d, (gPermissionNone_c), 2, 0x00, 0x25) DESCRIPTOR(desc_humidity, gBleSig_CharPresFormatDescriptor_d, (gPermissionFlagReadable_c), 7, 0x0E, 0x00, 0xAD, 0x27, 0x00, 0x00, 0x00) CCCD(cccd_humidity)   After that, create a folder humidity in the next path ${workspace_loc:/${ProjName}/bluetooth/profiles. Found the temperature folder, copy the temperature_service.c and paste inside of the humidity folder with another name (humidity_service.c). Then go back and look for the interface folder, copy temperature_interface.h and change the name (humidity_interface.h) in the same path. You need to include the path of the created folder. Project properties>C/C+ Build>Settings>Tool Settings>MCU C Compiler>Includes: Humidity Interface The humidity_interface.h file should have the following code. The Service structure has the service handle, and the initialization value.   /*! Humidity Service - Configuration */ typedef struct humsConfig_tag { uint16_t serviceHandle; int16_t initialHumidity; } humsConfig_t; /*! Humidity Client - Configuration */ typedef struct humcConfig_tag { uint16_t hService; uint16_t hHumidity; uint16_t hHumCccd; uint16_t hHumDesc; gattDbCharPresFormat_t humFormat; } humcConfig_t;   Humidity Service At minimum on humidity_service.c file, should have the following code. The service stores the device identification for the connected client. This value is changed on subscription and non-subscription events.   /*! Humidity Service - Subscribed Client*/ static deviceId_t mHums_SubscribedClientId;   The initialization of the service is made by calling the start procedure. This function is usually called when the application is initialized. In this case is on the BleApp_Config().   bleResult_t Hums_Start(humsConfig_t *pServiceConfig) { mHums_SubscribedClientId = gInvalidDeviceId_c; /* Set the initial value of the humidity characteristic */ return Hums_RecordHumidityMeasurement(pServiceConfig->serviceHandle, pServiceConfig->initialHumidity); }   On stop function, the unsubscribe function is called.   bleResult_t Hums_Stop(humsConfig_t *pServiceConfig) { /* Stop functionality by unsubscribing */ return Hums_Unsubscribe(); } bleResult_t Hums_Unsubscribe(void) { /* Unsubscribe by invalidating the client ID */ mHums_SubscribedClientId = gInvalidDeviceId_c; return gBleSuccess_c; }   The subscribe function will be used in the main file, to subscribe the GATT client to the Humidity service.   bleResult_t Hums_Subscribe(deviceId_t clientDeviceId) { /* Subscribe by saving the client ID */ mHums_SubscribedClientId = clientDeviceId; return gBleSuccess_c; }   Depending on the complexity of the service, the API will implement additional functions. For the Humidity Sensor only have a one characteristic. The measurement will be saving on the GATT database and send the notification to the client. This function will need the service handle and the new value as input parameters.   bleResult_t Hums_RecordHumidityMeasurement(uint16_t serviceHandle, int16_t humidity) { uint16_t handle; bleResult_t result; bleUuid_t uuid = Uuid16(gBleSig_Humidity_d); /* Get handle of Humidity characteristic */ result = GattDb_FindCharValueHandleInService(serviceHandle, gBleUuidType16_c, &uuid, &handle); if (result != gBleSuccess_c) return result; /* Update characteristic value */ result = GattDb_WriteAttribute(handle, sizeof(uint16_t), (uint8_t*) &humidity); if (result != gBleSuccess_c) return result; Hts_SendHumidityMeasurementNotification(handle); return gBleSuccess_c; }   After save the measurement on the GATT database with GattDb_WriteAttribute function we send the notification. To send the notification, first have to get the CCCD and after check if the notification is active, if is active send the notification.   static void Hts_SendHumidityMeasurementNotification ( uint16_t handle ) { uint16_t hCccd; bool_t isNotificationActive; /* Get handle of CCCD */ if (GattDb_FindCccdHandleForCharValueHandle(handle, &hCccd) != gBleSuccess_c) return; if (gBleSuccess_c == Gap_CheckNotificationStatus (mHums_SubscribedClientId, hCccd, &isNotificationActive) && TRUE == isNotificationActive) { GattServer_SendNotification(mHums_SubscribedClientId, handle); } }   Humidity Sensor Main file There are some modifications that have to be done, to use the new Humidity profile in our sensor example. First, we need to declare the humidity service:   static humsConfig_t humsServiceConfig = {(uint16_t)service_humidity, 0};   Then, we need to add or modify the following functions: BleApp_Start You need to modify this line:   /* Device is connected, send humidity value */ BleApp_SendHumidity();   BleApp_Config You need to start the Humidity Service, and to modify the PrintString line:   humsServiceConfig.initialHumidity = 0; (void)Hums_Start(&humsServiceConfig);     AppPrintString("\r\nHumidity sensor -> Press switch to start advertising.\r\n");   BleApp_ConnectionCallback There are some modifications required in two Connection Events. gConnEvtConnected_c   (void)Hums_Subscribe(peerDeviceId); gConnEvtDisconnected_c   gConnEvtDisconnected_c   (void)Hums_Unsubscribe();   BleApp_GattServerCallback   /* Notify the humidity value when CCCD is written */ BleApp_SendHumidity()   BleApp_SendHumidity And, we need to add this function:   static void BleApp_SendHumidity(void) { (void)TMR_StopTimer(appTimerId); /* Update with initial humidity */ (void)Hums_RecordHumidityMeasurement((uint16_t)service_humidity, (int16_t)(BOARD_GetTemperature())); #if defined(cPWR_UsePowerDownMode) && (cPWR_UsePowerDownMode) /* Start Sleep After Data timer */ (void)TMR_StartLowPowerTimer(appTimerId, gTmrLowPowerSecondTimer_c, TmrSeconds(gGoToSleepAfterDataTime_c), DisconnectTimerCallback, NULL); #endif }   In this example, the Record Humidity uses the BOARD_GetTemperature, to use the example without any external sensor and to be able to see a change in the collector, but, in this section would be a GetHumidity function. Client (Collector)  First, we need to use the Temperature Collector project as a base, to create our Humidity Custom Profile Client (Collector). BLE SIG profiles The same applies for the Client. To know if the Profile or service is already defined in the specification, you have to look for in Bluetooth SIG profiles and check in the ble_sig_defines.h file (${workspace_loc:/${ProjName}/bluetooth/host/interface) if this is already declared in the code. In our case, the service is not declared, but the characteristic of the humidity is declared in the specification. Then, we need to check if the characteristic is already included in ble_sig_defines.h. Since, the characteristic is not included, we need to define it as shown next:   /*! Humidity Charactristic UUID */ #define gBleSig_Humidity_d 0x2A6F   GATT Database The Humidity Collector is going to have the GATT client; this is the device that will receive all information from  the GATT server. Demo provided in this post works like the Temperature Collector. When the Collector enables the notifications from the sensor, received notifications will be printed in the serial terminal. In order to create the demo we need to define or develop a service that has to be the same as in the GATT Server, this is declared in the gatt_uuid128.h.If the new service is not the same, they will never be able to communicate each other. All macros, function or structure in SDK have a common template which helps the application to act accordingly. Hence, we need to define this service in the gatt_uuid128.h as shown next:   /* Humidity */ UUID128(uuid_service_humidity, 0xfe ,0x34 ,0x9b ,0x5f ,0x80 ,0x00 ,0x00 ,0x80 ,0x00 ,0x10 ,0x00 ,0x02 ,0x00 ,0xfa ,0x10 ,0x10)   After that, copy the humidity profile folder from the Sensor project, to the Collector project ${workspace_loc:/${ProjName}/bluetooth/profiles. And also for this project, include the path of the new folder. Project properties>C/C+ Build>Settings>Tool Settings>MCU C Compiler>Includes: Humidity Collector Main file In the Collector source file, we need to do also some modifications, to use the Humidity Profile. First, we need to modify the Custom Information of the Peer device:   humcConfig_t humsClientConfig;   BleApp_StoreServiceHandles   static void BleApp_StoreServiceHandles ( gattService_t *pService ) { uint8_t i,j; if ((pService->uuidType == gBleUuidType128_c) && FLib_MemCmp(pService->uuid.uuid128, uuid_service_humidity, 16)) { /* Found Humidity Service */ mPeerInformation.customInfo.humsClientConfig.hService = pService->startHandle; for (i = 0; i < pService->cNumCharacteristics; i++) { if ((pService->aCharacteristics[i].value.uuidType == gBleUuidType16_c) && (pService->aCharacteristics[i].value.uuid.uuid16 == gBleSig_Humidity_d)) { /* Found Humudity Char */ mPeerInformation.customInfo.humsClientConfig.hHumidity = pService->aCharacteristics[i].value.handle; for (j = 0; j < pService->aCharacteristics[i].cNumDescriptors; j++) { if (pService->aCharacteristics[i].aDescriptors[j].uuidType == gBleUuidType16_c) { switch (pService->aCharacteristics[i].aDescriptors[j].uuid.uuid16) { /* Found Humidity Char Presentation Format Descriptor */ case gBleSig_CharPresFormatDescriptor_d: { mPeerInformation.customInfo.humsClientConfig.hHumDesc = pService->aCharacteristics[i].aDescriptors[j].handle; break; } /* Found Humidity Char CCCD */ case gBleSig_CCCD_d: { mPeerInformation.customInfo.humsClientConfig.hHumCccd = pService->aCharacteristics[i].aDescriptors[j].handle; break; } default: ; /* No action required */ break; } } } } } } }   BleApp_StoreDescValues   if (pDesc->handle == mPeerInformation.customInfo.humsClientConfig.hHumDesc) { /* Store Humidity format*/ FLib_MemCpy(&mPeerInformation.customInfo.humsClientConfig.humFormat, pDesc->paValue, pDesc->valueLength); }   BleApp_PrintHumidity   /*www.bluetooth.com/specifications/assigned-numbers/units */ if (mPeerInformation.customInfo.humsClientConfig.humFormat.unitUuid16 == 0x27ADU) { AppPrintString(" %\r\n"); } else { AppPrintString("\r\n"); }   BleApp_GattNotificationCallback   if (characteristicValueHandle == mPeerInformation.customInfo.humsClientConfig.hHumidity) { BleApp_PrintHumidity(Utils_ExtractTwoByteValue(aValue)); }    CheckScanEvent   foundMatch = MatchDataInAdvElementList(&adElement, &uuid_service_humidity, 16);   BleApp_StateMachineHandler mAppIdle_c   if (mPeerInformation.customInfo.humsClientConfig.hHumidity != gGattDbInvalidHandle_d)   mAppServiceDisc_c   if (mPeerInformation.customInfo.humsClientConfig.hHumDesc != 0U) mpCharProcBuffer->handle = mPeerInformation.customInfo.humsClientConfig.hHumDesc;   mAppReadDescriptor_c   if (mPeerInformation.customInfo.humsClientConfig.hHumCccd != 0U)   BleApp_ConfigureNotifications   mpCharProcBuffer->handle = mPeerInformation.customInfo.humsClientConfig.hHumCccd;   Demonstration Now, after connection, every time that you press the SW3 on KW38 Humidity Sensor is going to send the value to KW38 Humidity Collector.  
查看全文
1 Introduction Two development boards transmit control information through ble. One development board connects to paj7620 and provides gesture information through IIC bus. The other development board uses ble and USB HID. Ble is used to receive data, and USB HID is used to simulate keyboard input and control ppt                  Figure  1 2 Preparation We need two development boards qn908x and gesture control device paj7620. We use IAR as development enviroment.The example we use is temperature_sensor, and temperature_ colloctor. The SDK version is 2.2.3   3 Code 3.1  temperature_sensor code We want to implement IIC to read gesture information from paj7620 and send data. The pins used by IIC are PA6 and PA7 Simply encapsulate the IIC reading and writing code in the code to create i2c_ operation.c and i2c_ operation.h. Realize IIC initialization and reading / writing register function in it                        Figure  2                        Figure  3   3.1.1 After having these functions, we begin to write gesture recognition code. First, we add two blank files paj7620.c and paj7620.h into our project.   Select bank register area                               Figure 4   Wake up paj7620 to read device state                    Figure 5   Initialize device                    Figure 6   Gesture test function                                   Figure 7   3.1.2 When you are ready to read the device information, You should initialize IIC and paj7620 in BleApp_Init function                                Figure 8 In principle, we need to create a custom service for the PAJ device, but we replace the temperature data as our gesture control data. If you want to create a custom service, refer to this link custom profile   3.1.3 Create a timer that sends gesture data regularly. In file temerature_sensor.c Define a timer,static tmrTimerID_t dataTimerId; Allocate a timer, dataTimerId = TMR_AllocateTimer(); Define the callback function of this timer                                           Figure 9 Start timer                                    Figure 10 Close the low power mode. #define cPWR_UsePowerDownMode 0 3.2 temperature_collector code The most important thing here is to port USB HID into our project. The USB  example we use is the USB keyboard and mouse. 3.2.1 Add the OSA and USB folder under the example to the project directory, and copy the file to the corresponding folder according to the file structure of the original example.                      Figure 11 3.2.2 Add header file directory after completion                                           Figure 12 At the same time, in this tab, add two macro definitions USB_STACK_FREERTOS_HEAP_SIZE=16384 USB_STACK_FREERTOS   3.2.3 Next, we need to modify the main function in usb example . Open composite.c file.                      Figure 13 It calls the APP_task. So this function also need to be modified.                                   Figure 14 3.2.4Find hid_mouse.c,Comment function USB_DeviceHidMouseAction Find hid_keyboard.h. Define the gesture information.                                  Figure 15 Find hid_keyboard.c. We need to modify the function USB_DeviceHidKeyboardAction as following figure.                                                  Figure 16   Among them, we also need to implement the following function. When the up hand gesture is detected, the previous ppt will be played. The down hand gesture will be the next PPT, the left hand gesture will exit PPT, and the forward hand gesture will play ppt                                                  Figure 17 It also refers to an external variable gesture_from_server. The variable definition is in file temperature_ collocation.c,.     3.2.5 After that, let's go to BleApp_Statemachinehandler function in temperature_colloctor.c. In case mApppRunning_c, we will call usb_main to initialize USB HID                                                  Figure 18 3.2.6 In BleApp_PrintTemperature, we will save the gesture data to gesture_from_server                                                         Figure 19 We finished the all steps.        
查看全文
Where can I find the KW20-30-40 radio certification documents?     FRDM-KW40 platforms have passed the CE RED & FCC radio certification (BLE & 15.4).  Find below for information the certification documents and test reports.  For further information on the FRDM board and the product please refer to the corresponding KW40 Product Summary page and FRDM-KW40.
查看全文
KW39_38_37 radio certification information 
查看全文
This guide describes the hardware for the KW38 minimum BoM development board. The KW38 Minimum BoM development board is configurable, low-power, and cost-effective evaluation and development board for application prototyping and demonstration of the KW39A/38A/37A/39Z/38Z family of devices. The KW38 is an ultra-low-power, highly integrated single-chip device that enables Bluetooth Low Energy (Bluetooth LE) or Generic FSK (at 250, 500 and 1000 kbps) for portable, extremely low-power embedded systems. The KW38 integrates a radio transceiver operating in the 2.36 GHz to 2.48 GHz range supporting a range of GFSK, an ARM Cortex-M0+ CPU, up to 512 KB Flash and up to 64 KB SRAM, Bluetooth LE Link Layer hardware and peripherals optimized to meet the requirements of the target applications. MKW38 device is also available on the FRDM-KW38 Freedom Development Board. For more information about the FRDM-KW38 Freedom Development Board, see the FRDM-KW38 Freedom Development Board User's Guide (document FRDMKW38ZUG available in the NXP Connectivity website also).
查看全文
This guide will show a way to set up and enable an I2C Serial Interface to send a string of data instances using one of the Wireless Bluetooth SDK examples and the Serial Manager API.
查看全文
Introduction   This post explains how to create a BLE GATT database using FSCI commands sent to the BLE Server device. Additionally, this document explains how to set up the fields of each FSCI command used to create the BLE GATT database for the BLE Server.   Main FSCI commands to create the BLE GATT DB in the BLE Server device   The following, are the main commands to create, write and read the GATT DB from the BLE Server perspective. The purpose of this post is to serve as a reference and summary of the most important commands. The full list of commands FSCI commands can be found in the Framework Serial Connectivity Interface (FSCI) for Bluetooth Low Energy Host Stack documentation within your SDK package. GATT-InitRequest This command is used to initialize the GATT database at runtime, and it must be sent before any other command to declare a database in your BLE Server device. GATTServer-RegisterCallback.Request This command installs an application callback for the GATT Server module, enabling the device to respond to the FSCI request from the CPU application through an FSCI indication. GATTDBDynamic-AddPrimaryServiceDeclaration.Request It adds a primary service to the database. It has 3 parameters that should be configured, the desired handle, the UUID type (16 bits, 32 bits, 128 bits), and the UUID value. Usually, the desired handle should be set to zero and the stack will assign the handle of the primary service automatically.   If the GATT application callback was installed through the GATTServer-RegisterCallback.Request command, the GATT Server responds to the GATTDBDynamic-AddPrimaryServiceDeclaration.Request command with a GATTDBDynamic-AddPrimaryServiceDeclaration.Indication that contains the handle assigned to the primary service. The following example shows how to prepare this command to define the battery service in the database. GATTDBDynamic-AddCharacteristicDeclarationAndValue.Request It adds a characteristic and its value to the database. It has 7 parameters that should be configured, the UUID type (16 bits, 32 bits, 128 bits), the UUID value, characteristic properties, the maximum length of the value (only for variable-length values), the initial length of the value, the initial value of the characteristic and value access permissions. The characteristic declared using this command, belongs to the last primary service declared in the database. For values with a fixed length, the maximum length parameter should be set to 0, and the length is obtained from the initial length of the value parameter.   If the GATT application callback was installed, the response of this command is indicated by the GATTDBDynamic-AddCharacteristicDeclarationAndValue.Indication command. The following example shows how to prepare this command to define the battery level characteristic in the database with a fixed length of 1 byte and an initial value of 90%. GATTDBDynamic-AddCharacteristicDescriptor.Request It adds a characteristic descriptor to the database. It has 5 parameters that should be configured, the UUID type (16 bits, 32 bits, 128 bits), UUID value, length of the descriptor value, descriptor’s value, and descriptor access permissions. The descriptor declared using this command, belongs to the last characteristic declared in the database.   If the GATT application callback was installed, the response of this command is indicated by the GATTDBDynamic-AddCharacteristicDescriptor.Indication command. The following example shows how to prepare this command to add the characteristic presentation format descriptor of the battery level characteristic in the database.   GATTDBDynamic-AddCccd.Request It adds a CCDD into the database. This command does not have parameters. The CCCD declared using this command, belongs to the last characteristic declared in the database. The response of this command is indicated by GATTDBDynamic-AddCccd.Indication.   GATTDB-FindServiceHandle.Request This command is used to find the handle of a service previously declared in the database. It has 3 parameters that should be configured, the handle to start the search (should be 1 on the first call), the UUID type of the service to find (16 bits, 32 bits, 128 bits), and the UUID value of the service that you are searching.   If the GATT application callback was installed, the response of this command is indicated by the GATTDB-FindServiceHandle.Indication command, which contains the handle of the found service. The following example shows how to prepare this command to find the handle of the battery service declared in the previous examples. Notice that the result of the search corresponds to the handle returned by the GATTDBDynamic-AddPrimaryServiceDeclaration.Indication as expected.   GATTDB-FindCharValueHandleInService It finds the characteristic´s handle of a given service previously declared in the database. It has 3 parameters that should be configured, the handle of the service that contains the characteristic, the UUID type of the characteristic to find (16 bits, 32 bits, 128 bits), and the UUID value of the characteristic that you are searching for.   If the GATT application callback was installed, the response of this command is indicated by the GATTDB-FindCharValueHandleInService.Indication command, which contains the handle of the found characteristic’s value. The following example shows how to prepare this command to find the handle of the battery level value. Notice that the result of the search corresponds to the handle returned by the GATTDBDynamic-AddCharacteristicDeclarationAndValue.Indication plus one, because the AddCharacteristicDeclarationAndValueIndication command returns the handle of the characteristic and, on the other hand, FindCharValueHandleInService returns the handle of the characteristic’s value. GATTDB-FindDescriptorHandleForcharValueHandle.Request It finds the descriptor´s handle of a given characteristic previously declared in the database. It has 3 parameters that should be configured, the handle of the characteristic’s value that contains the descriptor, the UUID type of the descriptor to find (16 bits, 32 bits, 128 bits), and the UUID value of the descriptor that you are searching.   If the GATT application callback was installed, the response of this command is indicated by the GATTDB-FindDescriptorHandleForCharValueHandle.Indication command, which contains the handle of the found descriptor. The following example shows how to prepare this command to find the handle of the characteristic presentation format descriptor. The result corresponds to the handle returned by the GATTDBDynamic-AddCharacteristicDescriptor.Indication   GATTDB-FindCccdHandleForCharValueHandle.Request It finds the CCCD’s handle of a given characteristic previously declared in the database. It has only one parameter, the handle of the characteristic’s value that contains the CCCD.   If the GATT application callback was installed, the response of this command is indicated by the GATTDB-FindCccdHandleForCharValueHandle.Indication command, which contains the handle of the found CCCD. The following example shows how to prepare this command to find the handle of CCCD. The result corresponds to the handle returned by the GATTDBDynamic-AddCccd.Indication.   GATTDB-WriteAttribute.Request It writes the value of a given attribute from the application level. It has 3 parameters that should be configured, the handle of the attribute that you want to write, the length of the value in bytes, and the new value.   In the following example, we will modify the battery level characteristic’s value from 90% to 80%.   GATTDB-ReadAttribute.Request   It reads the value of a given attribute from the application level. It has 2 parameters that should be configured, the handle of the attribute that you want to read, and the maximum bytes that you want to read. The GATT application callback must be installed, since the response of this command indicated by the GATTDB-ReadAttribute.Indication command contains the value read from the database. In the following example, we will read the battery level characteristic’s value, the result is 80%.      
查看全文
Introduction This document is a quick start guide to load a new software image in a KW36 device through FSCI (Freescale Serial Communication Interface) bootloader software. Also, it contains all the steps needed to install the software required in a Windows host to handle the FSCI communication protocol. Software Requirements IAR Embedded Workbench IDE or MCUXpresso IDE. FRDM-KW36 SDK. Hardware Requirements FRDM-KW36 board. Downloading the SDK When downloading the SDK, select your specific IDE or simply choose all toolchains as shown below. In the option "Add software component", ensure to select all middleware components as depicted below. Installing FSCI Host in Windows OS The host software for the Windows OS was designed to work in a Python environment. The following steps are to download and install the software needed to use FSCI in a Windows OS. Visit the Python web site and download the latest Python 2.7.x MSI installer package for Windows OS. Open the MSI installer package. When customizing the installation options, check "Add python.exe to Path" as shown below Complete the rest of the steps for the Python installation process. Unzip the FRDM-KW36 SDK. Depending on your Python environment architecture, copy the HSDK.dll from <SDK_root>\tools\wireless\host_sdk\sdk-python\lib\<x86_or_x64> to <Python_directory>\DLLs (default in C:\Python27\DLLs). Download and install Visual C++ Redistributable Packages for Microsoft Visual Studio 2013 depending on the Windows architecture (vcredist_x86.exe or vcredist_x64.exe) from the Microsoft web site. Download and install the Microsoft Visual C++ Compiler for Python 2.7 from the following web site. To run Python scripts from the Command Prompt of Windows, we must create a system variable named PYTHONPATH. Search “System” in the Windows browser. Go to Advanced system settings -> Environment Variables… -> System variables. Click on the “New…” button and create the PYTHONPATH variable with the following value: <SDK_root>\tools\wireless\host_sdk\hsdk-python\src. Programming the FSCI bootloader on FRDM-KW36 board Attach the FRDM-KW36 board to your PC. Drag and drop the “bootloader_fsci_frdmkw36.bin” from the previously unzipped SDK file, you can find this file in: <SDK_root>\tools\wireless\binaries to your board. Like a common USB device. Creating a binary image to reprogram the device   IAR Embedded Workbench Open the connectivity project that you want to program through the FSCI bootloader from your SDK. This example will make use of the heart rate sensor project, located at the following path: <SDK_root>\boards\frdmkw36\wireless_examples\bluetooth\hrs\freertos\iar\hrs_freertos.eww. Open the project options window (Alt+F7). In Linker -> Config window, edit the “Configuration file symbol definitions” add the “gUseBootloaderLink_d=1” linker flag as shown below. Go to the “Output Converter” window and ensure that the output file is in binary format (.bin), otherwise, deselect the “Override default” checkbox, expand the “Output format” combo box and select “Raw binary. Click the OK button. Rebuild the project. The binary will be saved at: <SDK_root>\boards\frdmkw36\wireless_examples\bluetooth\hrs\freertos\iar\debug   MCUXpresso IDE Import your FRDM-KW36 SDK to MCUXpresso. Drag and drop your SDK on the "installed SDK's" toolbar. (In this step, it is not necessary to unzip the package). Open any connectivity project that you want to program through the FSCI bootloader from your SDK. This example will make use of the heart rate sensor project. Go to Project -> Properties, a new window will appear. Then, open the C/C++ Build -> Settings -> Linker -> Miscellaneous. Press the icon below, a new window will be deployed. Add “--defsym=gUseBootloaderLink_d=1”. Click on “Apply and Close”. Build the project. Deploy the “Binaries” icon in the workspace. Click the right mouse button on the “.axf” file. Select “Binary Utilities -> Create binary” option. The binary file will be saved at “Debug” folder in the workspace with “.bin” extension. Reprogramming an FRDM-KW36 board using the FSCI bootloader The following steps are to test the FSCI bootloader in a Windows OS. Search "Command Prompt" in the Windows browser. Run the "fsci_bootloader.py" Python script. Type the “python.exe” path in the console (default C:\Python27\python.exe). Drag and drop the “fsci_bootloader.py” from: <SDK_root>\tools\wireless\host_sdk\hsdk-python\src\com\nxp\wireless_connectivity\test\bootloader on the command prompt screen. Search the COM Port of your FRDM-KW36 board and type in the console. You can find it typing ‘Device manager’ from windows home and then search it in Ports (COM & LPT) toolbar. As you can see in this example the port may change depending on each case. Search the binary image file (created in the last section). Drag and drop on the screen. Press “Enter” to start the firmware update trough FSCI bootloader. Automatically the KW36 device will trigger to run the new software. To see all your process running, you can download the ‘IoT Toolbox’ from the app store to your smartphone and connect your device with the board to verify the random data that the heart rate sensor example generates.
查看全文
This post covers the below details. Introduction to Framework Serial Communication Interface (FSCI). BLE Server. Useful Commands to create a GATT database. Demonstrate the heart rate sensor profile using the FSCI black box application with Test Tool. Framework Serial Communication Interface The Framework Serial Communication Interface (FSCI) is a software module and a protocol that supports interfacing the Protocol Host Stack (i.e. BLE, Thread, and ZigBee) with a host or a PC tool (Test Tool for Connectivity Products) using a serial communication interface (e.g. UART, USB, SPI, and I2C). The below figure shows interaction between different layers.  Figure 1. System Overview The Host Processor (Application layer and control for Connectivity Stack) The Black Box application (APIs to interact with the Connectivity Stack) The below figure illustrates Interfacing between the host processor and black box application.  Figure 2. Protocol stack separation The Test Tool software for the connectivity products is an example of a host processor that can communicate with FSCI black boxes at various layers. The figure below shows FSCI based application structure.  Figure 3. FSCI based Application Structure The FSCI module executes in the context of the Serial Manager task. For more details regarding FSCI and Serial Manager module refer to the ‘Connectivity Framework Reference Manual.pdf’ document available inside SDK Documentation at location <SDK_Documentation\docs\wireless\Common>. The detailed description of the Bluetooth Low Energy Host Stack serial commands, communication packet structure, and usage of the Framework Serial Communication Interface is provided inside the ‘Bluetooth Low Energy Host Stack FSCI Reference Manual.pdf’ document available inside SDK Documentation at location <SDK_Documentation\docs\wireless\Bluetooth>. The detail about FSCI Host is described here. An example of FSCI based BLE temperature sensor application is described in AN12896. Bluetooth Low Energy Server Bluetooth Low Energy allows exchange of information using the Generic Attribute Profile (GATT), GATT defines below two roles: Server: Device that stores the information. Client: Device that request for information from the server. Going forward, this post describes how to implement a BLE Server using the FSCI black box application with Test Tool. The server device can implement the GATT Database using below two methods. Static database: MACROs are used to add services, characteristics, etc. Dynamic database: APIs are used to add services, characteristics, etc. It is useful when runtime database update is required. This is the approach used by FSCI for the management of GATT databases. The below figure shows an example of database hierarchy.  Figure 4. GATT Database Service: It is a set of information. i.e., sensor location, sensor read value, etc. Bluetooth SIG has defined universally unique identifier (UUID) for various services and characteristics. This UUID will be useful to add services and characteristics to the database. Heart Rate, Battery Information, Device Information are examples of the service. Characteristic and value: It is the actual entity where information and its value are stored when the characteristic and value are added into the database. i.e., Device information service can have characteristics like manufacturer name, model string, Hardware version, etc. Descriptor: It is used to provide additional information regarding the characteristic and its value, e.g. format, scale, unit, etc. Client Characteristic Configuration Descriptor (CCCD): It is a descriptor used by the client device to enable or disable the notifications or indications. When the specific component is added using GATT_DB APIs, the stack will assign a handle to that component to index it in the database. Useful commands to create GATT database FSCI provides a set of commands for the management of the GATT Database. The most used ones are described below. Table 1 Some of the Basic GATT_DB Command Command Description No. of Handle assigned GATTDBDynamic-AddPrimaryServiceDeclaration.Request To add the primary service. 1 GATTDBDynamic-AddCharacteristicDeclarationAndValue.Request To add the characteristic and its value. It will be added as part of previously added service. 2 GATTDBDynamic-AddCharacteristicDescriptor.Request To add the descriptor for the previously added characteristic. 1 GATTDBDynamic-AddCccd.Request To add the CCCD for the previously added characteristic. 1 The attached Test Tool macro file demonstrates steps and setup required to implement a Heart Rate Sensor profile. The steps to execute it are described in the attached lab guide.
查看全文