Technology Days - Training Material

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

Discussions

Sort by:
Review of NXP’s current CAN portfolio and CAN functions, our support for CAN FD and an overview of the breakthrough products keeping CAN highly relevant for the new generation of vehicles.
View full article
The NXP® eIQ™ machine learning software development environment enables the use of ML algorithms on NXP microcontrollers and microprocessors. eIQ software includes inference engines, neural network compilers and optimized libraries. This software not only leverages open-source technologies, it is fully integrated into our MCUXpresso SDK and Yocto development environments, allowing you to develop complete system-level applications with ease.
View full article
The presenter explains the key principles for localizing objects and gives a description of the silicon IP that is included in the KW devices and supports localization. Algorithms such as RSSI, Time-of-Flight and AoA/AoD are clearly described and examples of implementation are provided through the delivery of test results obtained on devices such as the KW35 and KW36. Partnership with external companies is also mentioned so that support can be obtained companies having a long experience in his technical domain.
View full article
At NXP, our broad portfolio of analog, interface and NFC solutions means that we are able to offer complete solutions around the core. With a range of options that attach to any core, our product expertise in areas such as NFC, power management, networking and interfaces is deep-rooted.
View full article
LX2160A is NXP’s highest performance multicore device with 16 Arm-v8 64-bit A72 cores at up to 2.2 GHz. It also has 24 SerDes lanes running at 25 GHz supporting dual 100GE interfaces and up to 24 lanes of PCIe Express. It has security acceleration to 50 Gbps and data compression/decompression to 100 Gbps. This session will explain LX2160A’s suitability for the main target applications (5G, industrial, ADAS, storage, NIC, and edge routing), benchmarking results (CoreMark, Dhrystone, DPDK, SpecInt, …), software and reference board enablement, 3rd-party board solutions, and how it stacks up against the Xeon-D family of devices.
View full article
Understand the value, benefits and features  of Arm's latest Cortex-M33 core through a LPC5500-based product training and hand-on session.
View full article
This class will provide an overview of NXP's broad and scalable MCU portfolio and give details on which product families are available for different markets and use cases. It will also give an overview of the unified tools, software and solutions that enable the portfolio as well as a demo presentation across the MCU portfolio.
View full article
This session will reacquaint the audience with the NXP MEMS sensor portfolio, highlighting the latest products, development tools, and algorithms aimed at Industrial and Medical IoT market segments.
View full article
From media & graphics-focused applications to networking & communications-focused applications, and all the edge-processing applications in between, you are sure to find a processor & ecosystem to optimize your design within NXP’s scalable portfolio of Arm® devices. Presenters: Marcel Baessler, Arrow Franck Roux, Products and Solutions Marketing Manager, NXP
View full article
Solutions from NXP provide the right hardware, modular software, certifications, partners and documentation to accelerate time-to-market for our customers. Join this class to experience a deep dive on what is delivered from the newly launched SLN-POS-RDR Card Reader Solution.
View full article
In this section, NXP (SIP) will introduce the key products surround the USB Type-C connectors. The section will covers Power Delivery Controller, Power Delivery PHY, CC logic controller, high speed switch and high speed redriver. We will go over NXP Type-C hardware architecture, differentiation and product advantage.
View full article
With the secure CAN transceiver, NXP offers a very efficient hardware based security solution for CAN Networks, complementing the overall NXP 4+1 layered security approach. This sessions clarifies, the different use cases and how STINGER helps on system level for a highly efficient solution.
View full article
Extending the scalable range of the i.MX product line, the i.MX 8 series establishes an unmatched range of cost-performance scaling with pin-compatible options and the highest level of software reuse. Built with a high-level integration to support graphics, video, image processing, vision, audio and voice functions, the i.MX 8 series transforms your everyday interactions. Preview the next generation i.MX 8 series applications processors for Automotive, Consumer and Industrial applications.
View full article
Near-field-communication (NFC) is the better, safer way to protect brands while ensuring ease of use for accessories and consumables. With NFC, the device itself can verify the authenticity and can configure operating modes or change settings based on the type of accessory or consumable. With a standard NFC phone, a user can check the originality or trigger a reorder through a simple tap. In this presentation we will show which options exist on NFC tag and reader side, and how to implement a solution in a practical example.
View full article
Introduction to the new i.MX 8 and 8X automotive applications processor product families and associated target applications, development tools, and software ecosystem.
View full article
Getting started with MCUXpresso SDK, IDE, and Config tools.
View full article
Machine learning can performed on a wide range of device categories - from MCUs with Arm® Cortex®-M4 and M7 cores to complex SoCs with high-end A-class cores, GPUs, DSPs, and dedicated machine learning accelerators. The first step is learning how to utilize proper training techniques for model development, but beyond that how to generate optimized inference engines that can be used to perform classifications, anomaly detection, predictions, and other types of decisions. This presentation highlights some basic training techniques, such as data augmentation, but the primary focus will be on various ways to deploy neural network frameworks and classical machine learning algorithms, and most importantly, utilizing a variety of open source tools and techniques. We will show how these techniques fit in with some real use cases such as object recognition and anomaly detection.
View full article
No other company has the breadth and diversity of embedded solutions for addressing the challenge of IoT security. From secure element ICs to advanced multimedia and networking microprocessors, NXP delivers the technology needed for securing the entire Lifecycle of the end or edge node. In addition, with Edgescale Cloud services software, devices can be maintained from deployment until decomissioning. Join this class for an overview of NXP's security solution.
View full article
Sensors are key to differentiate your products in the market and add context awareness, tamper detection, a robust user interface and accurate media compatibility. This class will step through some of key the leading applications in the Medical and Industrial markets that have found usage of motion and pressure sensors as well as some up and coming applications. 
View full article