テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
Extend your logistics track and trace with condition insights. NTAG SmartSensor enables sensing and logging with NFC readout. NTAG SmartSensor enables your IOT application for smart logistics, smart healthcare, drug delivery and smart packaging.
記事全体を表示
Combustion and motor control is moving to more computation-intensive techniques.  Hear about how the S32 Automotive platform will support this trend with Arm® NEON and math acceleration.
記事全体を表示
AWS Greengrass - Labs 3-4
記事全体を表示
This class will explain several software solutions offered for the i.MX 8. SafeAssure software allows for a system partitioning that takes full advantage of the ability of some of the safety features of the i.MX 8. Fast Path software allows to route/bridge data between 2 network interfaces in order to maximize data routing performance with minimum CPU load requirements to the main processor. Trusted Environment allows for fully leveraging the Arm® Trustzone capability.
記事全体を表示
Learn about the powerful, easy to use replacement for MfgTool Command-line driven (no GUI). The session will touch on the following topics: Single command image download, fully scriptable; Supports all flash types (eMMC, NAND, QSPI, SD…); Fully open-sourced, on Github today with full documentation.
記事全体を表示
Lab 2 - Getting Started with MCUXpresso
記事全体を表示
This class will teach you how to spin a BLDC, PMSM or ACIM motor with i.MX RT. You do not need prior motor control experience.
記事全体を表示
Overview of Safety and Power Management portfolio of products focusing on system solutions for the target markets.
記事全体を表示
Start using UUU and the Pins Tool for i.MX family. First, overview of the new firmware download tool called Univeral Update Utility. Then learn about exciting updates to the Pins Tool for streamlining hardware development.
記事全体を表示
You need to get a lot of things right to build a truly secure system. Join this session to learn how the EdgeLock™ secure enclave that’s built into our i.MX 8ULP applications processors protects the entire system against attacks. Best of all, it simplifies complex implementations so you’re less likely to make errors when you configure security. With the secure enclave, you can achieve security goals with less security expertise, freeing you to focus on new ways to differentiate your application. Presenter: Lawrence Case, Systems Engineer and Security Architect, NXP
記事全体を表示
TensorFlow® Lite, ArmNN, and GLOW are popular open-source machine learning inference frameworks for mobile and IoT devices. In this session, you’ll learn how to use TensorFlow Lite, and ArmNN on NXP i.MX 8 MPU-class devices in Linux, and how to take advantage of not only Arm® Cortex®-A CPU cores, but also dedicated on-chip GPU and NPU accelerators. For NXP i.MX RT MCU-class devices we will introduce two approaches: 1)TensorFlow Lite for Microcontrollers with CMSIS-NN kernel implementation optimized for Cortex-M cores, and 2) GLOW, a neural network compiler, which generates code “Ahead of Time” for Cortex-M cores and DSP. Presenter: Robert Kalmar, Machine Learning SW Engineer, NXP
記事全体を表示
Experience design freedom through our advanced analog technologies, motor and load drivers, power management, in-vehicle networking, etc.
記事全体を表示
Low-power wearable/IoT applications are becoming more and more popular. In this session, we will go over some of the key aspects when considering the system-level power management solution for these application, pros and cons when choosing different topologies (for example, DC/DC regulator vs. LDO), overall system level power optimization, and key components selection consideration, etc.
記事全体を表示
Learn how to solve your I2C system challenges by deploying I3C. Our experts will provide a comprehensive introduction into the new MIPI I3C interface and its advantages compared to the well-known, I2C interface. This session gives an overview of how to develop I3C-based systems as well as provide a view of NXP’s MIPI I3C slave RTL, which is the first verified, freely available RTL source code available for download.
記事全体を表示
Solutions Around the Core – Interfaces and Power Solutions
記事全体を表示
Unlocking the full capability of NXPs next-generation multi-media processors require a dedicated power management solution that is fully aligned with the processor's power management needs. Presenting a full overview of PF8100 PMIC attach power management and functional safety solution.
記事全体を表示
Bluetooth speakers and headsets, printers, cameras, projectors, set-top-boxes, TVs, Wi-Fi routers and a variety of home appliances like fridges, washing machines, air purifiers, coffee machines, blenders all have one thing in common: Near Field Communication (NFC) allows new features and easier handling. Just bringing two NFC-enabled devices close together is all it takes to create a connection. Accessories and consumables can be authenticated and configured without any user interaction, and without power supply. And commissioning an IOT node into a wireless network has never been as easy as it is now with NFC. We will share the latest status of NFC support in iOS and present the brand new NFC Tandem module.
記事全体を表示
i.MX 8 product family introduces advanced security subsystem providing state-of-the-art safety of sensitive information and secure software execution. Hardware architecture has evolved over the years to adapt to the extra sense of security required these days and how it is utilized to protect chip secrets. This session will involve going through the security subsystem and overview of the underlying concepts. Both hardware and software aspects of security implementation will be discussed.
記事全体を表示
Whether you are looking for an easy and cost-efficient parametrization solution or want to use a smartphone for ad-hoc diagnosis of a device - Near-field-communication (NFC) makes this possible now. Or you might want to communicate with a fully sealed, batteryless device? Learn in this session about many new use cases, in which NFC simplifies handling, saves cost or enables features which were not possible before in industrial or healthcare applications. With iPhones now also enabled for NFC reading there are more possibilities than you would have imagined!
記事全体を表示
With the push for EV and HEV vehicles and the push for cordless connections in everyday products, there is a growing need for battery cell controllers and battery management systems. In this class, we will discuss the automotive battery management system trends and requirements and we'll go through typical battery management applications. We will examine NXP’s product portfolio and solutions and highlight key product and system features. Finally, we will explore NXP’s tools that make developing battery management systems with NXP.
記事全体を表示