NXP Tech Blog

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Tech Blog

shinjihontani-b
NXP Employee
NXP Employee

本記事では、i.MX 93内蔵のEdgeLock® Secure Enclave(ELE)の暗号アクセラレータおよび鍵管理の機能をPKCS#11経由で使用する方法について解説いたします。
PKCS#11は暗号処理において広く使用されているAPIであり、同じく広く使用されているライブラリであるOpenSSLとの統合も可能です。そのためPKCS#11やOpenSSLを使用した認証処理を行うアプリケーション全て(例: Eclipse Mosquitto™ etc.)に対して、アプリケーション側の改造無しで保護機能の適用も可能です。
暗号アクセラレータおよび鍵管理の機能を提供するという点は別記事で紹介しているSE050などのセキュアエレメントとも共通します。
暗号アクセラレータおよび鍵管理の概要、セキュアエレメントとの大まかな比較や使い分けは以下の記事も参照ください。
作業時間: 約55分 (yoctoのビルド除く)
  1. pkcs11-tool経由でのELEの使用 : 10分
  2. openssl経由でのELEの使用 : 10分
  3. PKCS#11 URI PEMファイルの作成 : 5分
  4. Azure IoT Hubへのクラウド接続 : 30分
 
Read more...

More
1 0 65
pavelsvadbik
NXP Employee
NXP Employee

Building functionally safe motor control systems doesn’t have to mean sacrificing performance or redesigning your architecture. Discover how NXP combines AMMCLib and ASCLib to separate safety from motor control, reduce development effort, and accelerate certification—without compromising efficiency.
Read more...

More
2 0 236
weiping_liu
NXP Employee
NXP Employee

 

  There are many open-source low-light AI-ISP models. The table below is a comparison table provided by Copilot. 

 

Algorithm

GitHub

Type

i.MX95 NPU Suitability

 

MSR (Retinex)

jsrsinchana/.../MSR-algorithm

Non-AI (ISP)

Medium

 

Zero-DCE++

arnabroy734/low_light_enhancement

Lightweight CNN + Curve

Very High

 

RetinexNet

weichen582/RetinexNet

CNN (Retinex)

Medium

 

EnlightenGAN

VITA-Group/EnlightenGAN

GAN (CNN)

Very High (lite)

 

FLOL

cidautai/FLOL

Lightweight CNN

High

 

SNR-aware

JIA-Lab-research/SNR-Aware

Transformer + CNN

Low

 

KinD

zhangyhuaee/KinD

Retinex + CNN

Medium

 

RetinexNet-lite

Derived

Light CNN

Medium

 

EnlightenGAN-lite

Derived

Small CNN

Very High

 

Fast LLIE CNN

Various

Small CNN

High

 

 

Tested above open-source models with UVC to perform performance evaluation on the exip-os08a20 module with linear mode. Found that SCI(GitHub - vis-opt-group/SCI: [CVPR 2022] This is the official code for the paper "Toward Fast, Flexib...) computation is relatively small, low-light performance is good in subjective evaluations, and it can basically run on the IMX95. The testing method involves copying the tflite file and test script to the /root/ directory of the IMX95 and running the following command: `python3 test_sci_cvpr_illu_imx95_int8.py --model sci_tpami_illu_imx95_int8.tflite`. The comparison interface shown below is displayed.

weiping_liu_0-1784087656398.png

 

 

More
0 0 226
ZihengXu
NXP Employee
NXP Employee

A lightweight CPU utilization monitor built with eBPF + libbpf.  
It hooks into the kernel scheduler (sched_switch tracepoint) to measure per-CPU
active time with nanosecond precision — more accurate than polling-based tools like
top, and with lower overhead at high process counts.
Read more...

More
0 0 239
EsaHuang
NXP Employee
NXP Employee

Upgrading from LF6.12 to LF6.18 on i.MX943 brings a noticeable increase in S2R resume latency — from ~1420 ms up to ~3420 ms under default BSP configuration. This is not a regression to be fixed, but an intentional consequence of a critical suspend panic fix introduced in LF6.18. This article explains the root cause behind the PCIe FLR timing change, the secondary CRNG reseeding delay, and provides a confirmed workaround to reduce observable resume time.

Read more...

More
0 0 155
hiroshihiraga
NXP Employee
NXP Employee

Zephyr-series-4-title.png

Zephyrのソフトウェア再利用性を高めるための特徴であるデバイスツリーとKconfigの概要を説明します。そして、それらを実践で利用するためにステップを踏んで説明していきます。

このぜZephyrシリーズ第1回から今回の第4回までを読み終えると、Zephyr RTOSを利用してプログラムが書けるようになります。

Read more...

More
1 0 863
Kogiso
NXP Employee
NXP Employee

MCUXpresso Config Toolsの中から「Pins Tool」にフォーカスし、ピン設定の基本および設定方法を解説します。
VS Code環境での導入方法から、ピン設定の変更によるLED点滅デモまで紹介します。

(作業時間:10分 *MCUXpresso for VSC (Visual Studio Code), SDKをインストールしている前提)

Read more...

More
2 0 520
atsushihonda
NXP Employee
NXP Employee

i.MX95 でのセキュアブートに使用する署名付きのコンテナ・イメージを Secure Provisioning SDK (SPSDK) で作成し、起動する手順をハンズオン形式で学べる内容となっています。

楕円曲線デジタル署名暗号 (ECDSA)と、耐量子暗号 (PQC) ML-DSA 両方の署名認証を行うHybrid boot での実現例を紹介します。

(作業時間:半日 *一度i.MX 95向けの Linux BSP のビルドが完了している前提)

Read more...

More
1 0 663
akifumiokano
NXP Employee
NXP Employee

ZephyrのHTTPサーバーサンプルをFRDM-MCXN947で動かし,PCのブラウザからボード上のLEDをON/OFFする手順をステップ・バイ・ステップで解説します.ルーター経由での固定IP/DHCP接続に加え,PCとボードをLANケーブル1本で直結する構成にも対応しています.Zephyrのビルド環境がインストール済みであれば,設定ファイルの編集からビルド・書き込みまで,コマンド数本で動作を確認できます.
(作業時間:15分 *Zephyr開発環境インストール済,PCネットワークに慣れていれば)

スクリーンショット 2026-06-11 15.39.32.png

Read more...

More
1 0 506
ZHOU_XIAO
NXP Employee
NXP Employee

 産業機器における通信は、従来のフィールドバスからEthernetベースへと急速に移行しています。その中心となっているのが、産業用Ethernetプロトコルです。

 本記事では、広く利用されている以下の3つのプロトコルにフォーカスし、それぞれの技術構造設計思想の違いを分かりやすく解説します。

  1. EtherCAT
  2. PROFINET
  3. EtherNet/IP

(※評価・実装方法については別の記事で解説予定です)

 
産業用Ethernet主流のEtherCAT・PROFINET・EtherNet/IPの3大プロトコルを取り上げ、それぞれの技術構造と設計思想の違いを分かりやすく解説します。
 

(読了時間:15分)

Read more...

More
3 0 1,001
Keita_Nagashima
NXP Employee
NXP Employee

前回は、SPI通信の 前編としてFRDMボード2台用いて、SPI通信のサンプルアプリケーションを動かしてみました。

今回は、4つのSPIモードの設定を変えながら、実際に送受信されるSPI信号を確認してみようと思います。本稿では、以下の[前編]記事の作業が完了していることを前提に進めます。

[前編] SPI通信のサンプルアプリケーションを動かしてみる。

[後編] SPIのモードを変えながら、実際のSPI信号を観測して、変化を見てみる。

(作業時間:20分) ※前編の内容(MCUXpresso for VSC, SDKがインストールされていて、SPIのアプリケーション動作確認)が済んでいる前提。

Read more...

More
0 0 500
Keita_Nagashima
NXP Employee
NXP Employee

FRDMボードを2台用いて、SPI通信の動作と、実際に送信されるSPI信号を確認していきます。
2回に分けて説明をしていきますが、今回は前編で、先ずはSPIのプログラムを動かしてみたいと思います。

[前編] SPI通信のサンプルアプリケーションを動かしてみる。

[後編] 実際のSPI信号を観測し、SPIのモードを変えながら信号の変化を見てみる。

(作業時間:15分) ※MCUXpresso for VSC, SDKがインストールされている前提。SPI通信のサンプルアプリケーションを動作させるまで。

Read more...

More
0 0 563
Kogiso
NXP Employee
NXP Employee

MCUXpresso Config Toolsの中から「Clocks Tool」にフォーカスし、クロック設定の基本および設定方法を解説します。VS Code環境での導入方法から、CPUクロック変更によるLED点滅デモまで紹介します。
(作業時間:10分 *MCUXpresso for VSC (Visual Studio Code), SDKをインストールしている前提)

Read more...

More
0 0 612
EsaHuang
NXP Employee
NXP Employee

On i.MX95, OD, ND, and LD represent different system operating modes used to balance performance and power consumption. OD (OverDrive) mode targets the highest performance, allowing higher clock frequencies with a higher SoC supply voltage. ND (Nominal Drive) mode provides the standard operating point for normal performance and power efficiency. LD (Low Drive) mode is intended for lower-power operation, reducing voltage and limiting clock frequencies to save energy. In practice, switching between these modes involves coordinated changes of VDD_SOC, system clocks, and DDR operating frequency so that the device can move between high-performance and low-power states safely and efficiently.

 

Here is a table about the Maximum frequency of modules of different modes.

 

OverDrive Mode

Nominal Mode

LowDrive Mode

VDD_SOC (typical)

0.9 V

0.85 V

0.8 V

VDD_ARM (typical)

0.9 V

0.85 V

0.8 V

A55 frequency

1800 MHz

1400 MHz

900 MHz

NPU frequency

1000 MHz

800 MHz

500 MHz

ISI frequency

667 MHz

500 MHz

333 MHz

GPU frequency

500 MHz

500 MHz

500 MHz

Display frequency

800 MHz

666 MHz

400 MHz

VPU frequency

666 MHz

500 MHz

333 MHz

 

Read more...

More
2 0 641
araki
NXP Employee
NXP Employee

車載BMSの新しい技術として、近年、EIS(Electrochemical Impedance Spectroscopy:電気化学インピーダンス分光法)が注目されています。
EISが注目されている背景や採用するメリット、またNXPのソリューション(プレスリリース)を簡単に紹介します。
現状BMSを扱っているが、今後どのような方向性で精度や機能を改善していけばよいのか悩まれている方のヒントになれば幸いです。

(読了:15分)

Read more...

More
1 0 891
shigenobukatagi
NXP Employee
NXP Employee

今までにFRDM-IMX95を使ってネットワークカメラ、Yoloによる物体認識をそれぞれ紹介しました。

今回はこれらを組み合わせ、「AIネットワークカメラ」を実現してみます。

(作業時間:10分) *i.MX95ネットワークカメラカメラ+AIの最適化が完了している前提

Read more...

More
0 0 591
shigenobukatagi
NXP Employee
NXP Employee

i.MX 95にはカメラ入力ポートに加えて、ハードウェアのビデオコーデックも内部に実装されています。
今回は、これらの機能を活用し、ネットワークカメラを実際に動かしてみます。

  • FRDM-IMX95でカメラのライブ画像をH.265で圧縮してネットワーク経由で送信
  • Ubuntu PC側でカメラのライブ画像を受信→復号して、映像を表示

(作業時間:20分) *i.MX 95カメラアプリケーションの導入が完了している前提

Read more...

More
0 0 686
shigenobukatagi
NXP Employee
NXP Employee

前回、こちらの記事FRDM-IMX95を用いてYOLOを使った物体認識デモを紹介しました。
その記事の中では、12~15fps程度のフレームレートになっていましたが、本記事では最適化を行い、フレームレートの大幅な向上を図ってみます。

(作業時間:10分) *i.MX95カメラ+AI – YOLOv8mの例が完了している前提

Read more...

More
0 0 651
shigenobukatagi
NXP Employee
NXP Employee

AIでの物体認識として人気のYoloをFRDM-IMX95で動かしてみます。

使うモデルはYOLOv8mです。

(作業時間:30分) *LinuxイメージがFRDM-IMX95に書き込み、カメラの動作が確認できている前提

Read more...

More
0 0 1,164
shigenobukatagi
NXP Employee
NXP Employee

FRDM-IMX95ボードを使って、カメラ画像をAIで物体認識させてみます。
Linux BSPは6.18.2_1.0.0を使用しています。使うモデルはmobilenetです。

(作業時間:15分) *LinuxイメージがFRDM-IMX95に書き込めている前提、Neutron SDKダウンロード時間を除く

Read more...

More
0 0 868
shigenobukatagi
NXP Employee
NXP Employee

FRDM-IMX95ボードを使って、カメラを動かしてみます。
・Gstreamer
・Python/OpenCV
の2通りを実施します。
使用しているのはLinux BSPは6.18.2_1.0.0です。

(作業時間:10分) *LinuxイメージがFRDM-IMX95に書き込めている前提

Read more...

More
0 0 721
Keita_Nagashima
NXP Employee
NXP Employee

最近注目を集める比較的新しいRTOSがあります。それが「Zephyr® OS」です。読み方は、「ゼファー」です。

このZephyr OSは、世界の名だたる有名企業がこぞって開発協力やサポートを強化しているオープンソースのRTOSで、NXPはこのZephyr設立当初からのプラチナメンバーとして活動しています。

本ページでは、Zephyr OSを使うためのお役立ち情報をまとめていますので、是非ご活用ください。

Read more...

More
0 0 2,229
hiroshihiraga
NXP Employee
NXP Employee

 
 

tech_blog_LED_Blinky.png

 
Zephyrシリーズ第3回はLチカプログラムを通してZephyrによるソフトウェア再利用の手法を解説します。

Zephyr RTOSで簡単なLチカプログラムの作成を通し、ソースコードに加え、CMakeファイルやconfファイルなども一から作成し、更にはそのコードを他のHWでも動作する再利用性を考慮したZephyr流コーディング手法を説明します。

Read more...

More
2 0 1,177
Kogiso
NXP Employee
NXP Employee

昨年(2025年)に引き続きまして、徳島県の神山まるごと高専で jig.jp創業者・福野泰介氏が行う新入生向けの導入授業「ITブートキャンプ2026」に、ボランティアとして参加させていただきました。本ブログでは、授業や学内の様子、そして今年学生の皆さんに実施いただいた課題について紹介します。

(読了:10分)

Read more...

More
1 0 1,009
shinjihontani-b
NXP Employee
NXP Employee

以前の記事では、SE05x(セキュアエレメント)向けライブラリである「Plug and Trust Middleware」のRaspberry Pi上でのセットアップ方法を紹介しました。

本記事執筆時点のPlug and Trust Middleware 04.07.01は、標準ではi.MX 93のFRDM開発ボード(FRDM-IMX93)に対応の旨記載はありませんが、セットアップして動作させることができたため、その方法を紹介いたします。

セットアップ完了後はOpenSSL経由でSE05xを使用する方法Eclipse Mosquitto clientを使用したAzure IoT Hubへの接続も同様に動作させることができます。

(作業時間: 30分)

Read more...

More
0 0 876
ino
NXP Employee
NXP Employee

NXPのFRDMボード「FRDM-MCXA156」を使用して、モーター制御について分かりやすく解説していきます。基礎編と実践編に分かれていますので、興味のある内容から参考いただければ幸いです。

・基礎編①~⑦、実践編①~③

今回は基礎編④として、「ベクトル制御の仕組み」をご紹介します。

(読了:10分)

Read more...

More
0 0 2,067
akifumiokano
NXP Employee
NXP Employee

Zephyr公式のGetting Started Guideに従ってインストールしたZephyr SDK 1.0.0をMCUXpresso for VSCにインポートすると,デバッガ(GDB)の起動に失敗するという問題が2026年3月23日現在確認されています.原因はSDK 1.0.0でツールチェーンのディレクトリ構造が変更されたことにあり,MCUXpresso機能拡張が新しいパス構造に未対応であるためです.launch.jsonへの直接記述でも回避できないこの問題は,SDK 1.0.0ディレクトリのルートに旧来のパスへのシンボリックリンクを作成するという簡単な操作で解決できます.本記事では,Zephyr環境のインポート手順からシンボリックリンクによるワークアラウンドの適用まで,スクリーンショットを交えてステップごとに解説します.スクリーンショット 2026-03-23 8.33.46.png

Read more...

More
0 0 738
akifumiokano
NXP Employee
NXP Employee

NXPの汎用マイコン向けRTOS「Zephyr OS」で,タッチ対応液晶GUIを動かすまでの手順をステップ・バイ・ステップで解説します.

GUIの構築には,マイコン向け軽量GUIライブラリ「LVGL」と,そのコードをGUI操作で生成できるNXP製ツール「GUI Guider」を使用します.GUI GuiderのサンプルプロジェクトをZephyr用にエクスポートし,i.MX RT1060評価キット(MIMXRT1060-EVKC)と液晶パネル(RK043FN66HS-CTG)上で実際に動作させることがゴールです.

なお,このGUIサンプルのビルドには,現時点ではZephyr OS v4.0.0とZephyr SDK 0.17.0の特定の組み合わせが必要です.この記事では,最新のZephyr環境(v4.3.99)からv4.0.0へ一時的に切り替える方法,パッチの適用,ビルドと書き込み,そして作業後に元の環境へ戻す手順までを詳しく説明します.

DSC_2621 (1).jpeg

 

Read more...

More
0 0 1,391
shinjihontani-b
NXP Employee
NXP Employee

前回の記事でOpenSSL経由でSE05xを使用する方法を解説しました。

OpenSSLを使用した認証処理を行うアプリケーションの例として、実際にEclipse Mosquitto™ clientを使用したMicrosoft Azure IoT Hubへの接続例を紹介します。

(作業時間:30分 *前回記事までの内容がセットアップ済みの前提)

Read more...

More
0 0 1,055
shinjihontani-b
NXP Employee
NXP Employee

前回の記事では、SE05x(セキュアエレメント)向けライブラリである「Plug and Trust Middleware」のセットアップを、Raspberry PiとFRDM-IMX93(i.MX 93向け開発ボード) 向けに行う手順を紹介しました。

セキュアエレメントと「*Plug and Trust Middleware」を用いることで、OpenSSLを使用した認証処理を行うアプリケーション全て(例: Eclipse Mosquitto™ etc.)に対して、アプリケーション側の改造無しで保護機能を適用できます。

本記事では、SE05x と OpenSSL を連携させた実践的な使い方を解説します。

(作業時間:10分 *Plug and Trust Middlewareがセットアップ済みの前提)

*Plug and Trust Middlewareには、Linux上で広く使用されているOpenSSLとの統合も含まれています。

Read more...

More
0 0 995