I have built an application to interface an accelerometer with the new LPC845 Breakout board using the I2C SDK driver.
The accelerometer acts as an I2C slave device to the LPC845 master device. Colors on the on-board RGB LED change according to the accelerometer position.
The accelerometer is a slave device in this application with slave address: 0x1D. The position of the board is determined by the x,y,z-axis values obtained from this slave device. The change in these x,y,z values detects the movement of the LPC845 Breakout board. I have assigned various patterns to the RGB LEDs for each movement along the y-axis.
詳細を読む...