Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Example MPC5748G-FlexCAN_with_interrupts S32DS_1.0 ******************************************************************************** * Detailed Description: * This example shows, how to initialize FlexCAN modules for simple transmission * and reception using RX interrupt. Both modules are configured for 100kbit/s * bit rate. CAN_0 module transmits message using MB0. CAN_1 module receives * message using interrupt via MB0. * * * ------------------------------------------------------------------------------ * Test HW:         MPC5748G-324DS, MPC574XG - Motherboard * MCU:             PPC5748GMMN6A 1N81M * Fsys:            PLL0 160MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          internal_FLASH (debug mode, release mode) * EVB connection:  Connect jumpers J15 and J16 on motherboard *                    Connect P14 H to P15 H *                    Connect P14 L to P15 L * ******************************************************************************** ******************************************************************************** * Detailed Description: * This example shows, how to initialize FlexCAN modules for simple transmission * and reception using RX interrupt. Both modules are configured for 100kbit/s * bit rate. CAN_0 module transmits message using MB0. CAN_1 module receives * message using interrupt via MB0. * * * ------------------------------------------------------------------------------ * Test HW:         MPC5748G-324DS, MPC574XG - Motherboard * MCU:             PPC5748GMMN6A 1N81M * Fsys:            PLL0 160MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          internal_FLASH (debug mode, release mode) * EVB connection:  Connect jumpers J15 and J16 on motherboard *                    Connect P14 H to P15 H *                    Connect P14 L to P15 L * ******************************************************************************** General Re: Example MPC5748G-FlexCAN_with_interrupts S32DS_1.0 Thank you, It works Best regards Re: Example MPC5748G-FlexCAN_with_interrupts S32DS_1.0 Hello, if you want FlexCAN example based on SDK, this is directly included in S32 Design Studio. If you want to use this one. you can simply create new project and manually migrate source codes or you can try to use following tutorial https://community.nxp.com/docs/DOC-335361  Regards, Martin Re: Example MPC5748G-FlexCAN_with_interrupts S32DS_1.0 Hello martinkovar, Do you have any updated version of this example to work with the SDK or new version of compiler? If not, could you please tell me what should I do to get this example to work on R1.2017? Thank you so much Re: Example MPC5748G-FlexCAN_with_interrupts S32DS_1.0 Hello, Do you have the example with DMA enabled on FlexCAN? Thanks, Xiaofeng Re: Example MPC5748G-FlexCAN_with_interrupts S32DS_1.0 Hello, which version of S32DS you use? If you recompiled this in S32DS v1.2 or R1.2017, it would not work correct, because there are some significant changes in compiler. Regards, Martin Re: Example MPC5748G-FlexCAN_with_interrupts S32DS_1.0 Hi,I download your code,it can run,but i have some problems when debug it. when i debug it ,it would go to dummy interruption function。like below picture, then,i press the F5(step into),it will enter main() function.like below; I'm confused, why it's not the first to go into main () function. Thank you . Regards, YSl
View full article
低功耗模式,带 USB 唤醒 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Kinetis系列具有丰富的低功耗模式。客户可能会感到困惑,不知道如何从低功耗模式唤醒。 1) 在 VLPR、VLPW 中:NVIC 仍然对中断敏感,因此任何中断都会得到服务。 2)在停止、VLPS 状态下:设备只能通过USB唤醒中断唤醒。 3) 在LLS、VLLSx中:设备将无法从任何 USB 源 唤醒 。 4) LLWU 用于 唤醒 ,因此客户可以从任何可用的 LLWU 唤醒 源 唤醒 。 至于 USB模块,对于USB恢复事件有两种不同的中断。一个异步可以从低功耗模式 唤醒 ,由 USB 线路状态 的 变化触发。另一个是同步的,仅在检测到 K 状态(D+ = 0、D- = 1,表示全速)后 2.5 微秒触发。应用程序负责在需要时转换到低功耗模式,为此,它必须检查USB堆栈报告的设备状态。当在总线中检测到挂起条件时,将触发 SLEEP 中断并且堆栈将其状态更改为挂起;然后应用程序将转换到低功耗模式。当发生此 SLEEP 中断时,异步唤醒中断被启用,并在触发时被禁用(这是模块清除中断所必需的)。在正常情况下,同步恢复中断或复位中断将会随后被触发,导致堆栈状态转换为非挂起状态。然后应用程序就可以知道通信再次处于活动状态,并避免再次进入低功耗模式。
View full article
实践研讨会:使用全新 LPC54114 节能 MCU 为 Always-On 市场设计嵌入式解决方案 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本次会议将以 LPC54000 低功耗系列的最新版本 LPC54114 MCU 为特色,演示如何在始终在线的应用中利用双核架构。通过本次实践课程优化产品设计以延长电池寿命并快速将其推向市场。主题涵盖系统架构、软件设计和调试、功率优化、声音检测和语音触发。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本次会议将以 LPC54000 低功耗系列的最新版本 LPC54114 MCU 为特色,演示如何在始终在线的应用中利用双核架构。通过本次实践课程优化产品设计以延长电池寿命并快速将其推向市场。主题涵盖系统架构、软件设计和调试、功率优化、声音检测和语音触发。
View full article
S32K344 - Six-step commutation control S32K344 - Six-step commutation control These examples demonstrate a a 3-phase Brushless DC (BLDC) motor control drive using a Six-step commutation control with Hall position sensor and without any position sensor (sensorless). This design serves as an example of motor control design using NXP S32K3 automotive family. Examples were designed on S32K344 Brushless Direct Current and Permanent Magnet Synchronous Motor Control Development Kit.  C-project based examples are part of MCSPTE1AK344 Development Kit Application Software. An innovative drivers set, Real-Time Drivers (RTD),are used to configure and control the MCU. It complies with Automotive-SPICE, ISO 26262, ISO 9001 and IATF 16949. Production-ready Automotive Math and Motor Control Library set provides essential building blocks for algorithm. FreeMASTER is used as useful run-time debugging tool. Application software contains:  MCSPTE1AK344_BLDC_6Step_hall_ll-. Hall sensor-based example. Detailed description of the example can be found in attachment to this article MCSPTE1AK344 - 6-step hall.pdf. MCSPTE1AK344_BLDC_6Step_sensorless_ll – Sensorless based example. Detailed description of the example can be found in attachment to this article MCSPTE1AK344_- 6-step sensorless.pdf. MATLAB Simulink based project (Motor Control BLDC Example - s32k344_mc_bldc_ebt) is build using Model-Based Design Toolbox (MBDT) and can be downloaded from NXP Model-Based Design Toolbox for S32K3xx - version 1.4.0 or newer releases.
View full article
iMX8M Plus - SW1 電源オン/オフボタン こんにちは、 iMX8M Plus EVK の開発に取り組んでおり、SW1 を約 5 秒間押し続けると EVK の電源がオフになり、約 1 秒間押すと再び電源がオンになることを確認しました。この動作がハードウェアやPMICによって処理されるのか、それともソフトウェアによって処理されているのかを確認してください。 また、SW3をON位置に移動させると、SW1を押さずに自動的に電源が入ります。これがi.MX8M Plus EVKの想定されるデフォルト動作であるかどうかをご確認ください。 Re: iMX8M Plus - SW1 ON/OFF Button こんにちは、@Govind1807。 NXPサポートまでご連絡いただきありがとうございます。 この挙動はプロセッサ内に実装された内部FSMに関連しています。 より理解を深めていただくために、FSMの動作と状態遷移を示す対応するブロック図を添付しました。 よろしくお願いします、 チャビラ
View full article
S32K3X8EVB-Q289搭載デバッガを使ってカスタムS32K358ターゲットをプログラムする方法 現在はS32K3X8EVB-Q289評価ボードを使用しており、S32K358 MCUを基にカスタムハードウェア設計を開発しました。 もう少し詳しく教えていただけますか: EVBの搭載デバッガを使って外部S32K358ターゲットのプログラミングやデバッグは公式にサポートされていますか? サポートされている場合、EVB上でどのようなジャンパー設定またはハードウェアの変更が必要ですか? この目的にはどのデバッグコネクタを使用すべきですか? S32デバッグプローブを使用する場合と比較して、何か制限事項はありますか? この構成について説明したドキュメントやアプリケーションノートはありますか? ご支援ありがとうございます。 よろしくお願いいたします。 ヤシュ・グプタ Re: Using S32K3X8EVB-Q289 On-Board Debugger to Program a Custom S32K358 Target こんにちは、 @Yash2530 さん。 1. はい、S32K3X8EVB-Q289搭載デバッガを使って外部S32K358ターゲットのプログラミング/デバッグが可能です。実際、EVBの搭載OpenSDAデバッガはP&E Microが開発したブートローダー/デバッグアプリケーションを使用しています - https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1715877 2. この用途ではEVBのはんだ付けの再作業やジャンパー設定は不要です。 3. J55 USBホストコネクタ。 4. 実際には、標準的なフラッシュおよび外部S32K358ターゲットのソースレベルのデバッグには、EVBの搭載デバッガで十分であるべきです。あなたにとってどの機能が重要なのか分からないので、ご自身で機能を比較してみてください。 https://www.nxp.com/design/design-center/software/automotive-software-and-tools/s32-design-studio-ide/s32-debugger-for-s32-platform:S32DBG-S32PLATFORM https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320180&productTab=5045 5. はい、 https://www.nxp.com/webapp/Download? colCode=S32K3X8EVB-Q289HWUM よろしくお願いいたします。 パベル Re: Using S32K3X8EVB-Q289 On-Board Debugger to Program a Custom S32K358 Target @PavelL 、 外部コントローラをプログラムしようとしたときにこのエラーが出ました。 CMD>VC オブジェクトファイルのCRC-16をデバイス範囲と照合しています... ブロック 00400000-0042F4B7 ... 計算されたCRC-16がブロックと一致しません。(ファイル = $A9EE、デバイス = $EDEF) デバイスのフラッシュメモリの検証エラー Flashプログラミング中にエラーが発生しました。 情報: DAP IDCODE = 0x6BA02477 情報:DAPの電源投入に成功しました。DP CTRL/STAT = 0xF0000000 リセットスクリプトを開始します (C:\NXP\S32DS.3.6.7\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_6.1.8.202603121731\supportFiles_ARM\NXP\S32K3xx\S32K358.mac)... REM MC_MEモジュールで選択したコアのクロックを有効にする 200ミリ秒遅延します... 終わり。 REM RAMとDMAを初期化します。 REM DMA TCD の初期化: REM 使用する各コアに対して、有効な実行可能コードをRAMにコピーします。 REM MC_ME で必要なコアを有効にする: 20ミリ秒遅延します... 終わり。 20ミリ秒遅延します... 終わり。 リセットスクリプト (C:\NXP\S32DS.3.6.7\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_6.1.8.202603121731\supportFiles_ARM\NXP\S32K3xx\S32K358.mac)完了しました。 PEmicro GDB 起動失敗: フラッシュプログラミング中にエラーが発生しました。デバッグセッションを終了します。 PEエラー:デバイスへのダウンロード中にエラーが発生しました。デバッグセッションを終了します。 127.0.0.1 経由で「127.0.0.1」から切断されました。ポート「53100」による6224からの切断 PEエラー: エラー: 応答を送信しようとしましたが、接続が既に閉じられています。 127.0.0.1 経由で「127.0.0.1」から切断されました。ポート「53104」による7224からの切断 情報: DAP IDCODE = 0x6BA02477 ターゲットとの接続が切断されました。 Yash2530_0-1789183717483.jpegYash2530_0-1789183717483.jpegYash2530_0-1789183717483.jpegYash2530_0-1789183717483.jpegYash2530_0-1789183717483.jpegYash2530_0-1789183717483.jpeg これらの問題を解決するのを手伝ってください。 よろしくお願いいたします。 ヤシュ・グプタ Re: Using S32K3X8EVB-Q289 On-Board Debugger to Program a Custom S32K358 Target こんにちは、 @Yash2530 さん。 S32K3X8EVB-Q289とJ55経由で接続されたオンボードのPEmicroデバッガを使ってリファレンステストを行いました。 私のテストでは、最初のCRC認証でも既存のフラッシュコンテンツがダウンロード中のアプリケーションと異なるため、不一致が報告されました。しかし、その後、プログラミング処理はフラッシュメモリの消去とプログラミングへと続いた。したがって、最初のCRC不一致は必ずしも根本原因ではなく、それ自体ではセキュアデバッグが有効になっていることを確認するものではありません。 重要な違いは、あなたが提供したログでは、最初のVCコマンドの直後にデバッグセッションが終了している点です。フラッシュメモリの消去と書き込みを行うための、後続のEMコマンドとPMコマンドが見当たりません。 PEmicroのデバッグ起動設定を確認してください。特に、実行ファイルのダウンロードとフラッシュメモリへの書き込みが有効になっているかどうかを確認してください。セッション開始時からのPEmicroのログ全体もご提供ください。ログの冒頭には、CMコマンドと選択された.arpファイルが表示されるはずです。フラッシュアルゴリズム。 参考までに、HSE無効化デバイスでテストを成功させた際に使用したアルゴリズムは以下のとおりです。 PavelL_0-1789370094591.pngPavelL_0-1789370094591.pngPavelL_0-1789370094591.pngPavelL_0-1789370094591.pngPavelL_0-1789370094591.png 設定で選択したアルゴリズムが、S32K358デバイスの実際の状態(例えば、HSE無効またはHSE有効)に対応していることを確認してください。   ちなみに、次回は新しいThreadを作成してください。私たちは最後の回答からわずか7日後にコミュニティThreadを積極的に追跡していました。私は更新情報の購読メールしか受け取らず、それも時々見逃されることがあります。 よろしくお願いいたします。 パベル Re: Using S32K3X8EVB-Q289 On-Board Debugger to Program a Custom S32K358 Target こんにちは、@PavelL デバイスの問題はJTAGのリセットピンがオンボードMCUとTargetボードのMCUと競合していることだとプログラムしました。そこでリセットピンをJTAG RESETピンから分離し、プログラムは正常に動作しました。今はMCUを手動でリセットしなければならない唯一の問題です。 EVKボードのJTAG(J50およびJ55(USB))コネクタと併せて、カスタムターゲットも使用しましたか? よろしくお願いいたします。 ヤシュ・グプタ Re: Using S32K3X8EVB-Q289 On-Board Debugger to Program a Custom S32K358 Target こんにちは、 @Yash2530 さん。 はい、外部のPEmicroデバッガとLauterbach TRACE32の両方を使用したことがあります。 私のメモによると、EVBのジャンパーはすべてデフォルトの位置に保たれていましたが、J685とJ23は2〜3の位置に設定されていました。 参考までに、ジャンパーの設定は以下のとおりです。 J685: 2-3 J23: 2-3 J25: 1-2 J30: 1-2 J31:1-2 J691: 1-2 J37: 2-3 J746: 2-3 J13: 1-2 J16:1-2 J701: 1-2 この構成では、私の環境ではプログラミング、デバッグ、自動リセットが正しく動作しました。これらのジャンパー設定を、現在お使いのEVBの設定と比較してください。 よろしくお願いいたします。 パベル Re: Using S32K3X8EVB-Q289 On-Board Debugger to Program a Custom S32K358 Target こんにちは、 @Yash2530 さん。 「i2cとSPIの例コードを提供する」という新しいテーマです。Threadの明確さを保つために、新しい専用Threadを作成してください。 ご理解いただきありがとうございます。 よろしくお願いいたします。 パベル Re: Using S32K3X8EVB-Q289 On-Board Debugger to Program a Custom S32K358 Target @PavelL さん、 ご返信ありがとうございます。とても助かりました。RTDの例にはループバックの例が含まれているので、i2cやspiの例も共有してもらえますか?私はペリフェラルをSPIとi2Cでマスターのままにして初期化しようと試みましたが、mosiやmisoの両方でsk上のクロック信号が応答しません。もし共有していただけると大変助かります。 ありがとうございます ヤシュ・グプタ
View full article
LA9310 LLCP 外部接口信号描述和交流时序表 尝试将 ADRV9002 与 LA9310 连接。需要LA9310 LLCP外部接口信号描述和交流时序表, LA9310 材料提供的细节不足以绘制地图: LLCP车道数 精确的序列字格式 I/Q 位排序 ADC/DAC 采样是原始数据流还是封装的交易 或者 我们可以绕过或关闭ADC和DAC的电源吗? 或者 如何配置与 ADRV9002 兼容的 SSI LVDS 接口的 LA9310? Re: LA9310 LLCP external interface signal description and AC timing table, 你好, 不, 现有的 LA9310 文档 没有 提供 足够的 信息 , 无法 将 ADRV9002 SSI/LVDS 直接 映射 到 LA9310 LLCP 接口 。LA9310 文档 定义 了 LLCP 引脚、 链路 样式、 事务 类型 和 电气 /时序 特性 , 并且 还 表明 内部 ADC / DAC 可以 置于 低 电源 模式 。但 我 找不到 指定 LLCP 详细 信息 的 文档 , 满足 ADRV9002 互操作性 设计 所需 的 级别 , 每个 超过 单个 data+strobe 对 方向 通道数 、 I/Q 流 的 精确 端到端 串行 采样 字 格式 、 LLCP 引脚 上 明确的 I/Q 位 顺序 , 或者 任何 关于 LLCP 与 SSI 兼容的 声明。 此致 Re: LA9310 LLCP external interface signal description and AC timing table, 谢谢, 此外,如果您能推荐任何适用于 240 至 360MHz 频率的兼容零中频或近零中频射频集成电路 (RFIC),那就更好了。我正在研究 LMS7002,但如果没有 TSP,它的用途就大大减少了。或者,如果您建议不使用 TSP,那么我可以使用 LA9310 吗? 使用 LMS7002 内部 TSP 通常可以获得: 数字升频/降频 插值/抽取滤波 智商矫正 直流偏移校正 一些增益控制功能 数字频率偏移 数字波形整形 或 我发现,如果像上面提到的那样,其他功能也可以集成到 LA9310 中,那么 CMX998 可以实现 BPSK/QPSK/8PSK,适用于 5KHz 和 25KHz 等低带宽信道,收发数据速率仅为 2.4 KB/s 至 64KB/s。
View full article
我尝试在 FRDM-MCXN947 上运行 Zephyr HTTP 服务器(日本博客) 0. 这篇文章是关于什么的? 传统上,在使用嵌入式微控制器的网络功能时,首先要弄清楚“如何让它工作”。你需要找到目标微控制器供应商提供的SDK和示例代码,然后根据其API编写代码。由于每个微控制器的API都不同,每次想做类似的事情时,往往都得从头开始研究。网络功能涉及很多知识,例如初始化TCP协议栈和使用套接字API,我相信很多人都经历过还没来得及编写自己的应用程序就因为这些知识而感到力不从心的情况。 Zephyr OS 或许能解决这些问题。Zephyr 作为一款实时操作系统 (RTOS),提供了一套标准的 API,其主要优势在于,一旦掌握了使用方法,同一段代码就能在不同的开发板上运行。在众多可用的示例代码中,也包括我们将要讨论的HTTP 服务器示例,而且它的运行出乎意料地简单。 本文提供了在 NXP FRDM-MCXN947评估板上运行 HTTP 服务器示例的分步指南。示例运行后,您将能够通过 PC 的 Web 浏览器访问 FRDM-MCXN947,并使用页面上的按钮打开/关闭板上的 LED 灯。 目标: 通过浏览器访问 FRDM-MCXN947 上的 HTTP 服务器,并使用页面上的“LED 开”和“LED 关”按钮控制 LED。 在阅读本文之前 这假设 Zephyr 构建环境已经安装,并且您熟悉 west build 和 west flash 的基本操作。 如果您要从设置环境开始,可以参考 Zephyr 官方网站上的“入门指南”,或者观看指导视频,该视频可让您使用 MCUXpresso for VSC 轻松进行设置。 让我们开始吧!请参阅“MCUXpresso 与 VS Code 和 Zephyr OS”。 目录 0. 这篇文章是关于什么的? 1. 你需要准备什么 1.1 硬件 1.2 软件(必须安装) 2. 准备工作:激活环境变量 3. 配置 prj.conf(指定 IP 地址) 3.1 使用静态 IP 地址时 3.2 使用 DHCP(自动获取 IP 地址) 3.3 当PC与主板直接一对一连接时 4. 建造 4.1 对于静态 IP 地址 4.2 使用 DHCP 时 5. 写信给董事会 6. 运行检查 6.1 使用串口终端检查 IP 地址 6.2 通过浏览器访问 参考资料 1. 你需要准备什么 1.1 硬件 产品名称 备注 FRDM-MCXN947评估板 Zephyr 文档 USB 连接线(包含在上述 FRDM 板中) 这样就把主板上的 J17 连接器连接到了 PC。 LAN 线缆 这样就把主板上的以太网接口连接到了网络上。 1.2 软件(必须安装) 最新 Zephyr 开发环境(西部,Zephyr SDK)   2. 准备工作:激活环境变量 这次,我们将使用 macOS 终端屏幕上的命令进行操作。 打开终端后,首先执行以下两个命令。 首先,激活Python执行环境: source ~/zephyrproject/.venv/bin/activate 如果使用 MCUXpresso for VSC 安装 bin/activate 的位置与标准位置不同。 在 macOS 上,它位于 ~/.mcuxpressotools/.venv_3_14/ 中。 在 Windows 系统中,它位于 C:\Users\<ユーザ名>\.mcuxpressotools\.venv_3_12\Scripts 中。 *使用 Windows PowerShell 时,所使用的命令和文件名与 Linux 和 macOS 上的命令和文件名有所不同,因此请在继续操作之前参阅“入门指南”。 接下来,我们将设置构建 Zephyr 所需的环境变量。该命令允许您从任何文件夹构建 Zephyr: source ~/zephyrproject/zephyr/zephyr-env.sh 接下来,导航到示例文件夹: cd ~/zephyrproject/zephyr/samples/net/sockets/http_server   3. 配置 prj.conf(指定 IP 地址) 此文件夹中的 prj.conf 文件包含网络设置。请根据您的连接类型从以下三种方法中选择一种。 部分 连接类型 IP设置方法 第 3.1 节 通过路由器连接到局域网 手动配置静态IP地址。 第 3.2 节 通过路由器连接到局域网 通过 DHCP 自动获取资源(简单) 第 3.3 节 使用一根网线将电脑和主板直接连接起来。 为电脑和主板都设置静态IP地址。 参考:IP 地址:静态和 CHCP 3.1 使用静态 IP 地址(通过路由器) 此方法需要通过路由器连接到局域网,并为开发板分配一个固定的 IP 地址。请在文本编辑器中打开 prj.conf ,并根据您的网络环境修改以下两行代码。 更改前(默认): CONFIG_NET_CONFIG_MY_IPV4_ADDR="192.0.2.1" CONFIG_NET_CONFIG_MY_IPV4_GW="192.0.2.2" 更改后(例如): CONFIG_NET_CONFIG_MY_IPV4_ADDR="192.168.1.100" CONFIG_NET_CONFIG_MY_IPV4_GW="192.168.1.1" 设置项目 意义 CONFIG_NET_CONFIG_MY_IPV4_ADDR 要分配给电路板的 IP 地址(指定路由器子网内与其他设备不重叠的地址)。 CONFIG_NET_CONFIG_MY_IPV4_GW 网关(路由器)的 IP 地址。如果您仅从同一局域网内的电脑访问它,则并非绝对必要。 这里没有指定子网掩码,但在我测试的环境中,它被设置为 255.255.255.0 。 本文以“192.168.1.100”为例,请根据您的网络环境进行更改。 3.2 使用 DHCP(自动获取 IP 地址) 将 FRDM-MCXN947 连接到路由器(无线路由器)时,它可以自动从路由器获取 IP 地址。为此,请对 prj.conf 进行以下更改: CONFIG_NET_DHCPV4=y # 追加 CONFIG_NET_CONFIG_MY_IPV4_ADDR="" # 空文字列に変更 或者,您可以选择不编辑 prj.conf ,而是使用稍后描述的构建命令指定配置文件(参见第 4.2 节)。 3.3 当PC与主板直接一对一连接时 它还可以通过一根网线将PC和FRDM-MCXN947直接连接,无需路由器。在这种情况下,由于没有DHCP服务器,您需要在PC和开发板上手动设置静态IP地址。 关键点有以下两点: 在同一子网内,为PC和主板分配不同的IP地址。 由于它不会连接到互联网,因此不需要网关设置(或者任何值都可以接受)。 以下是一个设置示例: 主题 IP地址 子网掩码 PC(有线 LAN 适配器) 192.168.100.1 255.255.255.0 FRDM-MCXN947 192.168.100.2 255.255.255.0 (自动设置) 在电路板侧,按照 3.1 节中的方法编辑 prj.conf 。使用上表中的值时的示例设置: CONFIG_NET_CONFIG_MY_IPV4_ADDR="192.168.100.2" CONFIG_NET_CONFIG_MY_IPV4_GW="192.168.100.1" PC端有线LAN适配器的IP地址需要在操作系统设置界面手动设置: macOS:前往“系统偏好设置”→“网络”→选择您的有线 LAN 适配器→将“IP 设置”更改为“手动”,然后输入地址 192.168.100.1 和子网掩码 255.255.255.0 Windows:转到“控制面板”→“网络和共享中心”→“更改适配器设置”→右键单击有线 LAN 适配器→“属性”→“Internet 协议版本 4 (TCP/IPv4)”→选择“使用下面的 IP 地址”并输入相同的信息。 如果启用了 DHCP ,则连接路由器的标准配置(3.2 节)会更简单,因为它不需要更改电脑的 IP 设置。直接连接适用于在没有路由器的环境中进行测试,或者当您不想更改电脑的网络设置时。 4. 建造 设置完成后,继续进行构建(编译和链接)。 工作目录为“~/zephyrproject/zephyr/samples/net/sockets/http_server”。 4.1 如果您拥有静态 IP 地址,或者如果您已将系统配置为在 prj.conf 中使用 DHCP 使用以下命令构建它。 west build -p auto -b frdm_mcxn947/mcxn947/cpu0 4.2 使用 DHCP 时 prj.conf 要在不编辑文件的情况下启用 DHCP,请运行以下命令: west build -p auto -b frdm_mcxn947/mcxn947/cpu0 -- -DEXTRA_CONF_FILE="overlay-dhcpv4.conf" -DEXTRA_CONF_FILE="overlay-dhcpv4.conf" 这将导致在构建过程中将启用 DHCP 的配置文件添加到 prj.conf 中。 在此配置中,如果未启用 DHCP 服务器,则默认设置 prj.conf 中写入的静态 IP 地址。   5. 写信给董事会 构建完成后,将其写入电路板。 使用 USB 电缆将板载J17(USB)连接器(位于以太网连接器左侧)连接到您的 PC,并将LAN 电缆连接到以太网连接器。 运行以下命令: west flash 编写过程完成后,董事会将开始运作。   6. 运行检查 6.1 使用串口终端检查 IP 地址 打开串口终端(如 Tera Term、PuTTY 或 VS Code 的串口监视器),选择 FRDM-MCXN947 端口,并将波特率设置为115200 。 市面上有多种类型的串口终端,您可以根据自己的喜好选择使用哪一种。有关其安装和使用方法,请参阅相关文章。 uart:~$ 看到提示符后,输入以下命令: net iface 将显示网络设置列表。如果您指定了静态 IP 地址,则会显示该值;如果您使用了 DHCP,则会显示路由器分配的 IP 地址,请检查该地址。 如果错过了启动日志, 可以通过按下开发板上的 SW1(RESET) 按钮重启开发板。重启后,您也可以立即查看输出中的 IP 地址。 6.2 通过浏览器访问 在浏览器地址栏中输入已确认的 IP 地址并访问它(在本例中为 http://192.168.1.100 )。 如果工作正常,屏幕上将显示“ LED 开”和“ LED 关”按钮。按下这些按钮即可打开/关闭 FRDM-MCXN947 上的绿色 LED 指示灯。 参考资料 【Zephyr ®系列】第一部分:最近流行的 Zephyr OS 究竟是一款怎样的操作系统?(日语博客) 【Zephyr ®系列】第二部分:首次构建与测试(日语博客) Zephyr 项目入门指南 让我们开始吧!使用 MCUXpresso 和 VS Code 构建 Zephyr OS(视频教程) 试用 UI:Zephyr OS 上的 GUI Guider 示例代码(日本博客) 变更历史记录: 2026-06-16:第一版 ========================= 我们目前无法回复此帖子“评论”部分留下的评论。 由此给您带来的不便,我们深表歉意。如有任何疑问,请参考“NXP 技术问题 - 如何联系我们(日语博客)”。 (如果您已经是恩智浦的分销商或与恩智浦有业务关系,您可以直接咨询您的代表。) 本指南将逐步讲解如何在 FRDM-MCXN947 上运行 Zephyr HTTP 服务器示例,并通过 PC 浏览器控制板上的 LED 灯亮灭。它支持通过路由器建立固定 IP/DHCP 连接,也支持使用单根网线将 PC 与开发板直接连接。如果已安装 Zephyr 构建环境,您只需几条命令即可完成从编辑配置文件到构建和烧录固件的整个过程,从而验证其运行情况。 (预计时间:15 分钟 *假设已安装 Zephyr 开发环境并熟悉 PC 网络) 以太网 介绍 MCX 日本博客
View full article
Hose Hawk Pro 值得一试吗?2026 年回顾 Hose Hawk Pro 正迅速成为2026 年最受欢迎的花园水管管理解决方案之一,因为它能帮助业主保持户外空间整洁、有序、无忧无虑。该设备专为方便日常使用而设计,结合了耐用的结构、便于存放软管和实用的设计,有助于防止缠结、扭结和不必要的磨损。无论您是浇花、洗车还是处理日常户外杂务,Hose Hawk Pro 都能为您提供简单可靠的方法,让您的花园软管得到保护、随时可用,并在最需要的时候随时准备好。点击订购 Hose Hawk Pro 来自官方网站 Hose Hawk Pro脱颖而出的原因在于其简单易用的设计。这种创新的软管管理解决方案无需处理缠绕的软管、杂乱的院子或复杂的存储系统,只需将花园软管整理好、保护好,并方便取用即可。许多房主都很喜欢它的快速安装,可用于花园、车道、庭院或任何需要高效水管存储的室外区域。 2026 年,随着越来越多的人投入时间和精力来维护美丽的户外空间,寻找一种可靠的方法来管理花园设备变得越来越重要。Hose Hawk Pro完全符合这一日益增长的趋势,它提供了一个实用的解决方案,有助于减少软管损坏,提高组织能力,使日常户外工作更加方便。它的设计经久耐用,功能简单易用,让院子里的工作压力更小,乐趣更大。 Hose Hawk Pro 值得购买吗?对于那些正在寻找一种耐用、方便、节省空间的软管存储解决方案的人来说,答案似乎是肯定的。其价值在于使用方便、结构坚固,并能保持软管整洁,随时可供使用。不过,只有按预期安装和使用,才能达到最佳效果。它非常适合想要用简单的方法将户外空间打理得井井有条、高效无忧的房主和园艺爱好者。 单击此处了解有关 Hose Hawk Pro 的更多信息 Re: Is Hose Hawk Pro Worth Trying? A 2026 Review 亲爱的 aura elitsa、 感谢您联系恩智浦并对我们的产品感兴趣。 您能否告诉我们您的询问是否与任何特定的恩智浦产品或设备有关?如果需要,我们很乐意为您提供进一步的帮助。 请查看我们的 NXP 网站,查找您需要的部件: https://www.nxp.com/ 如果您的问题与恩智浦产品无关,我们恐怕只能提供有限的详细支持。我们衷心感谢你们的理解。 如果需要,请随时提供更多详细信息,我们很乐意提供力所能及的帮助。 祝您愉快
View full article
S32K148 FlexCAN2が動作しない こんにちは、 Eclipse OpenBSWプロジェクトを使用しながら、S32K148でFlexCAN2を有効にしようとしています。 FlexCAN0は正常に動作していますが、FlexCAN2は有効なフレームを送信しません。 構成: MCU: S32K148 CANインスタンス: FlexCAN2 ピン: PB12 → CAN2_RX (ALT4) PB13 → CAN2_TX (ALT4) 外部トランシーバ:MCP2551(5V電源) バス終端:合計約60Ω ビットレート:500 kbps(従来型CAN) 観察された行動: バス上ではエラーフレームのみが観測される ビットスタッフィングエラーが発生する ACKは受信されませんでした。 質問: MCP2551(5Vトランシーバ)は、S32K148 FlexCANのI/Oレベルと互換性がありますか? PB12/PB13のALT4はFlexCAN2の正しいピンですか? FlexCAN0とFlexCAN2の間には、考慮すべき特定のクロックまたは構成上の違いはありますか? どのようなご指導もいただければ幸いです。 よろしくお願いします。 Re: S32K148 FlexCAN2 not working こんにちは、 @sousou54 さん。 1.MCP2551との互換性に問題は見当たりません。 2. はい。 3. 追加の設定は不要です。CAN0/1/2は同じクロックで動作します。 ノードのテストを段階的に試してみてください... トランシーバを使わずにTX/RXピン同士を接続してメッセージを送信してみてください。ACKが欠落しているため、メッセージが繰り返し表示されるはずです。TXエラーカウンタは0x80で、モジュールはエラーパッシブ状態です。それ以外の表示が出た場合は、PIN設定が間違っています。 TX/RXピンをトランシーバに通常通り接続し、バスからは切り離してください。メッセージを送る。上記と同じ画面が表示されるはずです。そうでない場合、トランシーバが無効になっているか、または終了していない可能性があります。 MCP2551のデータシートを見ると、RsピンをVssに接続して高速モードを選択する必要があることがわかります。 トランシーバを他のノード(例:CANツール)、メッセージの送受信。エラーが検出された場合、おそらくCANビットのタイミングが正しくないと考えられます。すべてのノードが同じビットレートとサンプルポイントを使用していることを確認してください。 以下のツールを使用できます: MPC5xxx/S32Kxx/LPCxxxx: CAN / CAN FD ビットタイミング計算。 最後に、これはカスタムボードですか、それともS32K148EVBを使用していますか?カスタムボードの場合は、 AN5426「S32K1xxのハードウェア設計ガイドライン」に記載されている接続を確認してください。 よろしくお願いします、 ジュリアン
View full article
RDMMA845X issues with Win 7 Pro. As a retired electronics man (but total newbie with PC + dev. boards) I hope this isn't too much of a stupid question. I have bought the above board. It works great on a Win 8.1 PC, but not on the Win 7 Pro PC - which is a shame because that's the one in my hobby lab! Win 7 finds the USB device and the Demo Screen correctly identifies the chip in use, etc. But hitting any of the 'lit' buttons just generates an Exception Handler window and I can go no further than that. I don't know what Ex Handler means so am at a loss! Wisdom greatfully accepted. Tks. John Accelerometers Re: RDMMA845X issues with Win 7 Pro. As an addition to my original post I should say that the exception window calls this an "unhandled exception". After some internet research I updated the .net framework to the latest ver (4.6.2) in case that was the cause. But it is not! Tks. J 
View full article
在 MIMXRT685-EVK 上配置 8CH-DMIC 板、闪存和测试 您好, 我正在尝试使用 8-DMIC 阵列板在 EVK-MIMXRT685 上运行 dmic_multi_channel CM33 演示。 根据演示文档,在 J31 上启用 8-DMIC 板需要移动多个电阻器(例如R379、R380、R384、R389、R390、R391、R392 至 2-3)。执行此操作后,FlexSPI 八进制闪存 (U19) 变得无法访问: -LinkServer 闪存失败 -ROM ISP (blhost) 已连接,但是 FLEX-SPI-或非显示扇区大小 = 0 /页面大小 = 0-无法擦除/写入闪存 我的问题是: 该演示能否在不使用八进制闪存(仅使用内存的工作流程)的情况下运行? 更换电阻器后是否有官方的闪存/启动程序? 是否所有电阻器都需要更改,还是某些电阻器可以保持默认状态以保证 FlexSPI 闪存工作? 现在看来所需的DMIC硬件设置会阻止正常的闪存编程/启动。如何测试和运行演示程序? 感谢您的指导。 MIMXRT685-EVK 8通道-麦克风 i.MX RT600 Re: 8CH-DMIC board configuration, flashing and testing on MIMXRT685-EVK 你好@mlkezarev、 非常感谢您关注我们的产品并使用我们的社区。 问题 1:该演示能否在不使用八进制闪存(仅使用内存的工作流程)的情况下运行? A1: 是的。该演示设计为仅通过 SRAM 运行,不需要八进制闪存。 问题2:更换电阻器后是否有官方的闪烁/启动程序? A2: 电阻器更改后,外部闪存将被物理断开。 因此,此硬件配置不支持闪存刷新或从闪存启动。 问题 3:是否所有电阻器都需要更改,还是某些电阻器可以保持默认状态,以保证 FlexSPI 闪存工作? A3: 如果要启用 8 个 DMIC,则需要更改所有指定的电阻。 我已经发布了引脚配置屏幕截图供您参考。 问题 4:现在看来所需的DMIC硬件设置会阻止正常的闪存编程/启动。如何测试和运行演示程序? A4:您可以在 SRAM 上运行,就像 SDK 演示一样"evkimxrt685_dmic_multi_channel_cm33" 顺祝商祺! MayLiu
View full article
Do you know the status of PCA9698 ? I thought I might need something like this. What is its status ? Are there any newer similar products ? Randy Re: Do you know the status of PCA9698 ? Hello Randy, PCA9698 is still active in production, but the HVQFN56 version (PCA9698BS) is being discontinued. The TSSOP56 version (PCA9698DGG) remains fully active and supported and is the recommended choice for new designs. There is no newer NXP device that offers the same 40‑bit GPIO count and current capability in a single chip, so PCA9698DGG is still the most appropriate solution if that functionality is required. BRs, Tomas
View full article
[RTD600 IP] S32K3X4EVB-T172 GPIO 唤醒 本示例项目将向用户展示如何使用和配置 WKPU + SIUL2 (GPIO) 的基本功能。 ------------------------------------------------------------------------------ * 测试硬件:S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU:S32K344 * IDE:S32DS v3.5& S32DS v3.6.x * SDK 发布版本:RTD 6.0.0 * 调试器:PE Micro * 目标: internal_FLASH ------------------------------------------------------------------------------ 该示例例程将 WKPU 配置为 GPIO 中断唤醒。这是最简单的 WKPU 例子。引脚 PTB19(WKPU42)配置为唤醒。 例程等待按下SW5,然后关闭绿色 LED,并进入 Wkpu_EnterStandby() 函数: 将核心时钟切换到 FIRC。 初始化 WKPU 实例。 配置 WKPU42 (PTB19)。 进入待机(或快速待机)状态。 按下 SW6 后,MCU 将唤醒、RESET 并轮询以再次按下 S W5。 本示例按原样提供,不提供任何保证和支持。
View full article
S32N55: ストリームゲートを無効にするRTD API こんにちは、チームの皆さん S32N55 リファレンス マニュアルによると、1588 タイマーの TMROFF_H/L を変更する前に、ストリーム ゲート インスタンスを無効にする必要があります。 現在、RTD のストリーム ゲート機能を無効にする API があるかどうか教えてください。 BR、 ブリジット RTD Re: S32N55: RTD API to disable the Stream Gate こんにちは、 ユーザーマニュアルを再度確認して確認します Re: S32N55: RTD API to disable the Stream Gate こんにちは@Bridget S32N_RTD_R21-11_1.8.0_CD07 のユーザー マニュアルによると、ストリーム ゲートを有効/無効にするには、構成ツール (EB Tresos) で設定します。 EthCtrlConfigEnableStreamGating = FALSE 設定 Re: S32N55: RTD API to disable the Stream Gate こんにちは、クオンさん。 gPTP 同期中など、場合によっては、実行時に TMROFF_H/L の値を更新する必要がある場合があります。S32N55 リファレンス マニュアルによると、1588 タイマーの TMROFF_H/L を変更する前に、Stream Gate インスタンスを無効にする必要があります。 このような状況では、Stream Gate 機能を無効/有効にする API が必要であると考えます。あなたが言及した EB の構成では、このシナリオを処理できないようです。 現在、RTD にストリーム ゲート機能を無効/有効にする API があるかどうか教えてください。 BR、 ブリジット
View full article
S32G399A 自定义板在吹掉 BOOT_CFG1 和 FUSE_SEL 后被砖块砸了 你好 我有一块带有 QSPI NOR 闪存的自定义 S32G399A 板(标准连接,类似于 RDB3 原理图)。 我想强制从 QSPI NOR 启动,所以我按照 E VB 上 QSPI_BOOT_CFG 的 AN13456(S32G3 启动流程)所附的 Excel 表中的建议值和参考手册中的fuse map,将 Ocotp_Ip_Example_S32G399A_M7 (来自 RTD)改编为 熔断启动熔丝 。这篇文章附有代码片段和我参考的文档! 每次写入 BOOT_CFG 后,我都立即使用 Ocotp_Ip_ReadEFuse()验证是否成功,结果发现值被正确更新(0x2000000C 和 0x00000010)。 然而,现在 主板无法从 NOR 启动。 串行下载模式不再响应(" 无法在 S32 Flash Tool 上与目标设备建立通信 ")。 JTAG 调试器 (PE Micro) 报告"GDB 服务器无法与目标处理器建立连接" 。 您能帮忙找出根本原因吗? Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好@wael_b、 感谢您联系我们并详细描述了您的问题。就我所见,您打算配置以下内容: 在 BOOT_CFG1 中: 在 BOOT_CGF2 中,FUSE_SEL 位,因此 RCON 值取自熔丝,而不是从芯片外部的串行/并行值中获取。请告诉我是否正确理解了您的配置。 当您尝试以串行模式连接(用于闪存和调试)时,是否使用了这种配置?请注意,BOOT_MOD1 和 BOOT_MOD2 的值与 FUSE_SEL 为 0 时的效果不同。 请告诉我您使用的 BOOT_MOD 1 和 2 的值。 谢谢! Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好,感谢您的答复! 我确认使用了正确的 BootMod,FUSE_SEL = 1! 经过检查,我们发现 BOOT_CFG1 的位 15(这是 启动 excel 中的 " 不在乎 " 字段)正在配置 XOSC 模式(在配置熔丝后,我们丢失了 MCU 的 XTAL 和 EXTAL 引脚上的 XOSC 时钟信号) 因此,在我们当前的熔丝配置中,由于位 15 为零,我们处于显然不支持的 XOSC 差分旁路模式(查看随附的屏幕截图)) 你确认在我们的例子中 Bit 15 不 应该为零吗? 请支持我们进行第二次配置,因为我们还有一块没有配置熔丝的工作板! 谢谢。 Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好@wael_b、 问题在于,S32G_Bootconfigwords_EVB.xlsx 中显示的配置是针对 EVB/RDB 板的,而且,它本应在 RCON 位中进行配置,这些位是可重新配置的。正如你在 excel 表单底部看到的那样,对于不在乎的部分,最好查看参考手册: 例如,如果你检查 SD_BOOT_CFG,你会看到很多 " 不在乎 " 位,但是 " 不起作用 " 特别针对 EVB/RDB 板中的 SD 配置,并不是这些位本身没有任何影响。 关于 AN13456 中提到的不支持的配置,我需要内部检查以了解更多细节。 作为参考,我在内部文档中找到了以下内容: ” BOOT_CFG1 的 XOSC BYPASS MODE 位用于选择 FXOSC 模块的外部时钟源模式。FXOSC 模块可从三种时钟源模式中选择一种作为输入。三种时钟源模式分别是晶体(元器件)模式、(外部)差分(时钟源输入)模式和(外部单端时钟源)旁路模式。当客户使用无源晶体(工作于晶体模式)或有源差分时钟振荡器(工作于差分模式)作为 FXOSC 输入时,应将 XOSC BYPASS MODE 设置为 0。 在这种情况下,如果没有其他进一步设置,FXOSC 默认将输入视为工作于晶体模式。 否则,如果客户使用单端数字时钟源(在 BYPASS 模式下工作)作为 FXOSC 输入,则应设置 XOSC BYPASS MODE 1。 ” 因此,BOOT_CFG1:15 的值取决于设计的配置方式。例如,使用 0 需要像在 RDB3 板中一样使用外部振荡器: 对于你没有熔断 S32G3 熔丝的板,我建议使用 RCON 启动来测试适合你设计的配置,正如你从 fuse map 表中看到的那样,确切的配置将取决于 QSPI 内存的类型以及振荡器的配置方式。 如果您需要更多支持,请告诉我。 Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好 alejandro_e 我正在和 @wael_b 在同一个板上工作,它说的是 excel 文件吗: XOSC 旁路模式选择:如果 XOSC 配置熔丝未熔断,则选择 XOSC 模式。 0- 差分 1- 晶体或单旁路模式 因此,当 BOOT_CFG[15] =0 时,它处于差分模式、 但如果 =1,则要么是晶体模式,要么是单旁路模式 我想知道是哪份文件说 BOOT_CFG[15] =0 可以与晶体正常工作? 在板外我们有与 EVK 相同的晶体,在设置 BOOT_CFG [15] =0 之后,时钟源消失了,所以我相信 MCU 在等待这种差模晶体而不是驱动被动晶体。如果我说错了,请指正。 同样不可能使用 RCON,我们只能用熔丝启动它。所以我希望你能向我们建议如何使用熔丝启动我们的板(它基于 evk 同一个闪光灯的水晶)。 Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 您好@alejandro_e, 感谢您的支持!根据您建议的配置,我们有两种情况: 情况 1: BOOT_CFG1 -> 0x2000800C: 第 29、15、3、2 位 = 1,其余为 0。 BOOT_CFG2 -> 0x17: 位 4、2、1、0 = 1,其余为 0。 在这种情况下,JTAG 可以正常工作(使用推荐的串行配置,FUSE_SEL = 1),但是当我们尝试在 S32FT 中上传目标和算法时,出现了一个错误: " 错误:无法与目标设备建立通信。" 另外,XTAL 没有显示任何信号! 这种行为是否与 " XOSC_GM_SEL:相关 XOSC 模式 " Bits 8 到 11 中的 GM Sel值 BOOT_CFG2 有关? 案例 2: 我们使用 BOOT_CFG1 在第二块板上进行了配置-> 0x2000800C 还有 BOOT_CFG2-> 0x0 F: 位 0,1,2,3 = 1 因为我们没有断开 FUSE _SEL 熔丝你认为这个 案例可以恢复吗? Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你可以在这里查看参考手册中关于 GM_SEL 的屏幕截图! Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好,@haythemLtifi和@wael_b、 很抱歉这么晚才回复,我终于收到了内部团队的信息,他们与我分享了以下内容: ” S32G3 不支持差分模式。我们建议客户使用晶体模式。 配置 Crystal 模式有两种方法: 当XOSC 配置 无效时,将XOSC BYPASS MODE SELECTION(XOSC 旁路模式选择)设为1 - 晶体模式。 当XOSC 配置 有效时,将XOSC MODE设置为11 - 晶体模式。 我们建议使用第二种配置,因为它能提供更高的稳定性。 “ XOSC 配置的有效性由 BOOT_CFG2[0]决定。 我还需要确认你的主板是否可以恢复。 Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好@wael_b、 下面是我的回答: 案例 1.对于晶体模式,应根据以下公式配置 GM_SEL: , 其中: gm:最小跨导值 ESR:等效串联电阻 f:晶体频率 C0: 晶体的寄生电容 C1: 晶体的额定负载电容 您还可以查看 S32G3 数据表 Rev4 中表 26 的一些示例: 我还检查了我们提供的示例项目中的配置。在这些数据上,我们使用1100b - 0.631×。 鉴于跨导是时钟信号的一种放大,使用 0 会导致芯片无法工作是合理的。我没有亲自测试过,所以如果更改 GM_SEL 的值对您的设置有任何影响,请告诉我。 对于案例 2。我的理解是,这将取决于 BOOT_CFG_LOCK 的值,如 fuse map 的 MISC 表所示: 理论上,如果锁定位为 00 或 01,您应该可以覆盖这些值。不过,我没有亲自做过测试,因此对其效果并不完全了解。 对于案例 1,你提到从串行启动是有效的,我假设在那个设置中 FXOSC 确实有输出信号,对吗? 在 QSPI 启动时,您在应用程序中使用的是 RTD 吗?还是你在使用完全自定义的软件? 谢谢! Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 您好,@haythemLtifi、 关于测试,我可以做,但现在不行,我下周再做。 我会让你们知道我从振荡器上看到了什么。 谢谢  Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好,@haythemLtifi、 您可以使用 S32DS 中的时钟视图修改该值: 更新代码后,更改应在以下文件中生效: 如《SW 启用指南》所述,在以该结构为参数运行 Clock_Ip_Init() 时,该更改将生效。 如果有帮助,请告诉我 Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好 、 很显然,我们相差 7 个小时,所以我想问你几个问题,明天 Wael 会重新回答你的其他问题: - 您提到的代码中的 gm 值是 0b1100 ,如何更改?是在时钟启动功能中吗? 或者我可以使用图形界面进行更改?我想将其设置为 0b1111 ,如何操作? 现在,当我测量 exTal 引脚上的晶体时,我看到的直流电压几乎在 800mv 左右,不知道晶体是否无法正常工作或者因为我没有使用有源探头,你能否在 EVK 上使用普通探头测量波形然后告诉我开启板后会看到什么?运行代码时 对于串行运行的板,当我们使用启动模式 0 和 1 选择串行时,我们会看到 Extal 的直流电压为 800 mv 差不多(它不是真正的信号波,但会振荡) Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好 @alejandro_e, 回复这个问题:" 在 QSPI 启动时,在你的应用程序中,你在使用 RTD 吗?还是你在使用完全自定义的软件?" = > 是的,我使用的是 RTD 示例,而不是自定义软件。 我有一些问题! -你能帮我理解启动过程文档中的这一部分吗?(参见随附的屏幕截图) -另外,是否有专用的.bin 可以下载到 或非 Flash 或 SD 卡启动中? - 我从 IVT 生成的 Siul_Dio_ToggleLed 应用程序大小为 5.3Mb,这有问题吗? Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好,@haythemLtifi、 感谢您提供的信息。说白了,在这个问题上,你不需要我再提供任何支持了,对吗? Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好、 我们发现了或非的问题,默认 bootROM 时钟为 30Mhz,在超时(500 毫秒)之前下载 S32G339A 的内存是不够的,我们取消了添加 QSPI 配置以将 bootROM 时钟提高到 200Mh 的选项,这就解决了问题。 感谢你的支持 Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好@wael_b、 感谢您提供的信息,并对迟复表示歉意。关于时钟测试,我会尽快进行,并与大家分享测试结果。 关于你最后的问题,没有专用的二进制文件可以下载到闪存或 SD 卡中,请记住,对于闪存,你需要在 0x0000 中对 IVT bin 进行编程,而对于 SD 卡,你需要在 0x1000 中对其进行编程。 关于二进制文件的大小,我刚刚用 S32G3 的 dio 示例做了一个快速的 IVT bin,它是 530M,大小应该不是问题。 也许我没有正确理解您的问题,如果我没有回答您的问题,请告诉我。 要测试二进制文件是否正确加载并由 bootROM 对其进行解析,你可以做的一件事是添加一个能开启板上的 LED 的 DCD,例如,请查看 S32G3 HSE 演示应用程序,任何版本都应该可以运行,例如在 0.2.51.0 版本中,你可以查看附录 11 部分。S32 DS — 生成 DCD 映像以开启 VDD_EFUSE 和系统 RAM 初始化,对于您的问题,相关部分是 VDD_EFUSE 步骤。如果你不熟悉,DCD 是一组非常简单的寄存器指令,你可以在程序开始执行之前添加,因此,如果你在添加 DCD 后看到板上的 LED 亮起,你可以确定你的二进制已正确加载并由 bootRoM 解析。 Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好,@haythemLtifi、 太好了,谢谢你告诉我。 如果您今后遇到任何问题,请创建一个新的帖子,我们将很乐意为您提供帮助。 顺祝商祺! Re: S32G399A Custom Board Bricked After Blowing BOOT_CFG1 and FUSE_SEL 你好 , 是的,我们很好,谢谢。
View full article
SAF - ASIL Certification Hi Support, Customer is using S32K31 with SW32K3_SAF_1.0.5_D2503.  They are asking for our SAF ASIL certificates, or any document to show it is ASIL "ready/compliance". Regards, Marcus Safety_SW Re: SAF - ASIL Certification Hi Support, Any updates? Re: SAF - ASIL Certification Hi Marcus, for every premium SAF package there is possible to download Safety SW Assessment Summary report. For SAF 1.0.5 I can see that on Flexera available as well: S32K3_SAF_1.0.5_Safety_SW_Assessment_Summary.pdf Kind Regards, Radoslav Re: SAF - ASIL Certification Hi @marcuslim , It is now technically and legally restricted to share files with customers, only legal way is via sales force I think. Anyway, I wanted screenshot from nxp.com from SAF product page, same as I have shared, to see that is really missing. How does customer get the release? Safety Assessment should be there, everybody else can see that. I'm attaching here internally the report and let you find the way how to legally share the file with the customer. But please try to explain the customer proper way how to get it nxp.com=>Software accounts=>Automotive SW - S32K3 Premium Software=>Automotive SW - S32K3 - Safety Software Framework Kind Regards, Radoslav Re: SAF - ASIL Certification Thanks Radoslav! The customer has found the document.  We can close this thread. Regards, Marcus
View full article
无 PHY 的 IMX8MP RGMII 连接 您好, 我正试图在不使用物理层的情况下建立与交换机的以太网 RGMII 连接。根据其他帖子,我将我的设备树配置如下: &fec { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_fec>, <&pinctrl_fec_phy>; phy-mode = "rgmii"; status = "okay"; fixed-link { speed = <1000>; full-duplex; }; }; pinctrl_fec: fecgrp { fsl,pins = , , , , , , , , , , , , , ; }; pinctrl_fec_phy: fecphygrp { fsl,pins = , ; }; ethtool 显示检测到链接:是,ifconfig 显示已分配 IP 地址。但是我无法 ping 到板或从板上执行 ping 操作。您能确认针脚的设置是否正确吗?谢谢。 i.MX 8 系列 | i.MX 8QuadMax (8QM) | 8QuadPlus Re: IMX8MP RGMII Connection with No PHY 谢谢您的答复,我已经看过那份文件,它帮我走到了今天。不过,我仍然需要进一步的帮助,才能让事情顺利进行。 Re: IMX8MP RGMII Connection with No PHY 请参阅所附文件,该文件对您的情况非常有用 Re: IMX8MP RGMII Connection with No PHY 对于 RGMII,当前电路板支持包默认支持此功能,你可以参考 https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/arch/arm64/boot/dts/freescale/imx8mp-evk.dts#L390
View full article
S32K 入力キャプチャ こんにちは、チーム S32K146 マイクロコントローラを使用していますが、入力キャプチャピンとしていずれかの入力ピンが必要です。どのモジュールで構成すればよいか教えていただけますか? FTM を信号測定として使用した場合、入力キャプチャ機能を実現できますか?それともic_pal機能を使うべきでしょうか? サポートをお願いします ありがとう シュルティ C Re: S32K Input Capture こんにちは、ペトルさん。 INT_SYS_InstallHandler(FTM0_Ch0_Ch1_IRQn, PWM_InputCapture_IRQHandler, NULL);関数はデフォルトのハンドラーを取得しており、このハンドラーFTM0_Ch0_Ch1_IRQnを取得していないため、使用できません。 私の設定は /* flexTimer_ic_1 InitConfig のグローバル設定 */ ftm_user_config_t flexTimer_ic_1_InitConfig = {     {         true , /* ソフトウェアトリガー状態 */         false , /* ハードウェアトリガー1の状態 */         false , /* ハードウェアトリガー2の状態 */         false , /* ハードウェアトリガー3の状態 */         false , /* 最大積載ポイント状態 */         false , /* 最小積載ポイント状態 */ FTM_SYSTEM_CLOCK、 /* INVCTRLレジスタの更新モード */ FTM_SYSTEM_CLOCK、 /* SWOCTRLレジスタの更新モード */ FTM_SYSTEM_CLOCK, /* OUTMASKレジスタの更新モード */ FTM_SYSTEM_CLOCK, /* CNTINレジスタの更新モード */         false , /* トリガーの自動クリア */ FTM_UPDATE_NOW, /* 同期ポイント */ }, FTM_MODE_INPUT_CAPTURE, /* FTMの動作モード */ FTM_CLOCK_DIVID_BY_1, /* FTMクロックプリスケーラ */ FTM_CLOCK_SOURCE_SYSTEMCLK, /* FTMクロックソース */ FTM_BDM_MODE_11, /* FTMデバッグモード */         false , /* 割り込み状態 */         false /* 初期化トリガー */ }; /* flexTimer_ic_1 の入力キャプチャ設定 */ ftm_input_param_t flexTimer_ic_1_InputCaptureConfig = {     1U , /* チャネル構成の数 */     65535U , /* 最大カウント値 */     flexTimer_ic_1_InputCaptureChannelConfig /* チャンネル設定*/ }; /* flexTimer_ic_1 入力キャプチャのチャネル構成構造体 */ ftm_input_ch_param_t flexTimer_ic_1_InputCaptureChannelConfig [ 1 ] = {     {         0U , /* チャネルID */ FTM_SIGNAL_MEASUREMENT, /* 入力キャプチャ操作モード */ FTM_RISING_EDGE, /* エッジアライメントモード */ FTM_FALLING_EDGE_PERIOD_MEASUREMENT, /* 信号測定操作タイプ */         0U , /* フィルター値 */         false , /* フィルターの状態(有効/無効) */         true , /* 連続測定状態 */         NULL, /* チャネルイベント情報のコールバックパラメータのベクトル */         NULL /* チャネルイベント情報のコールバックのベクター */    } }; Re: S32K Input Capture こんにちは、 はい、それらの機能で十分なはずです。SDK ドライバは FTM チャネル割り込みを有効にするので、起動時から適切なハンドラーを割り当てる必要があると思います。正しくない場合、ハンドラーは FTM0_Ch0_Ch1_IRQHandler になります。 キャプチャされた値を取得するには、FTM_DRV_GetInputCaptureMeasurement が呼び出されます。 BR、ペトル Re: S32K Input Capture こんにちは、ペトルさん。   分かりやすく説明していただき、ありがとうございます。   これらの関数を使用してFTMピンを入力キャプチャとして初期化できますか? `FTM_DRV_Init()` `FTM_DRV_InitInputCapture()`   パルス発生を捕捉するためのIRQハンドラをインストールする `INT_SYS_InstallHandler(FTM0_Ch0_Ch1_IRQn, PWM_InputCapture_IRQHandler, NULL)`     サポートをお願いします   ありがとう シュルティ C Re: S32K Input Capture こんにちは、 最も一般的で効率的な方法は、FTM を入力キャプチャ モードで設定し、FTM 機能を持つピンを使用することです。各 FTM チャネルは入力キャプチャ モードに設定でき、入力信号のエッジ (立ち上がり、立ち下がり、またはその両方) でタイマー値をキャプチャします。これは通常、信号周期、パルス幅、周波数の測定に使用されます。 IC PAL ドライバを使用すると、入力信号を検出し、チャネル入力信号のパルス幅または周期を測定できます。FTM、eMIOS、FLEXPWM、ETIMER をサポートするすべてのプラットフォームと IP 間でポータブルになるように設計されています。 SO、完全な制御とパフォーマンスが必要な場合は、FTM を直接使用してください。よりシンプルなコードと移植性が必要な場合は、IC PAL を使用してください。 BR、ペトル Re: S32K Input Capture こんにちは、 直接参照できる SDKs の例があります (ftm_signal_measurement)。 または、問題を示す簡略化されたプロジェクトを共有します。 BR、ペトル Re: S32K Input Capture こんにちは、 SDK の例では、直接参照しました (ftm_signal_measurement)。 この例では割り込み方法は使用されず、ポーリング方法が使用され、その後FTM_DRV_GetInputCaptureMeasurementが呼び出されました。 割り込みによる FTM 信号測定を探しています。入力キャプチャが信号を認識すると、割り込みがトリガーされ、 ISR で FTM_DRV_GetInputCaptureMeasurement 関数が呼び出されます。 これのコードを提供してもらえますか ありがとう シュルティ C Re: S32K Input Capture こんにちは、 ハンドラーを再度インストールする必要がある場合は、 外部void FTM0_Ch0_Ch1_IRQHandler(void); INT_SYS_InstallHandler(FTM0_Ch0_Ch1_IRQn、FTM0_Ch0_Ch1_IRQHandler、NULL); BR、ペトル Re: S32K Input Capture こんにちは、 はい、その関数は定義されていますが、その後関数呼び出しは無限ループに入り、さらに実行されます。 システム全体が機能しなくなる、 ありがとう シュルティ C Re: S32K Input Capture こんにちは、 サポートありがとうございます。コードスニペットも確認させていただきます。 T&R、 シュルティ C Re: S32K Input Capture こんにちは、 割り込み対応FTMピンへの入力を入力キャプチャとして取得できますか? よろしくお願いします。 シュルティ C Re: S32K Input Capture こんにちは、 ドライバはキャプチャ イベント情報に割り込みを使用していますが、例では直接示されていません。 FTM IC 設定を変更して、ワンショット モードを使用し、ドライバ割り込みから呼び出されるコールバックを追加しました。 ftm_signal_measurement_s32k146 デモの変更された main.c については、添付ファイルを参照してください。 BR、ペトル
View full article
PN7642 RF Design-in Tips and Tricks Prerequities:  PN7642 design-in recommendations   1// Impedance tuning  PN76 family antenna design guide The target impedance is chosen based on the target application. If full power is required (e.g., POS terminals). The target impedance of 15-17 Ω is recommended. For lower power applications using ULPCD, the higher impedance is typically preferred, 30-50 Ω (symmetrical tuning).   2// Dynamic power control  PN7642 - Basic RF power limitation using DPC   3// H-Field check  There are given limits, especially for the maximum H-field radiated by the reader. Exceeding these limits might lead to destroying the NFC Card/NFC Tag.   The H-Field can be measured with the help of test equipment, as  ISO 10373-6 Test PICC EMVCo 3.0 Test PICC  For indication only, the customers can use "smart" Field Strength Probes as shown below :    Note: The most critical position occurs when the card is placed directly on the NFC antenna . In this case, if the H-field exceeds the maximum allowed level, the output power must be reduced using DPC settings. 4// HF Attenuator value  Turn on the RF Field with the DPC set and enabled from the previous step  Read the CLIF_RXCTRL_STATUS register and check the HF_ATT_VAL as shown below.  The value for the "unloaded" condition with full power shall be approximately 35-45dec.  If the value is out of this range, the customer is required to adjust the Rx resistors to reach this value.  5// Receiver settings  Check the "Power" range and Communication Range with the default settings provided by NXP.  Power Range -> The distance at which the NFC Tag can still generate its answer, but the NFC Reader does not see it  Communication Range -> The distance at which the NFC Tag can still communitate with the NFC Reader  Ideally, Power Range ≈ Communication Range Also, the NFC Reader should not generate any false communications as e.g., "HAL COLLISION ERROR".  The optimisation of the receiver can be done in the following way:  Enter DPC Calibration  Go to the "ARC" menu and "disable" the ARC algorithm This will force the IC to use the RX settings from the following Register/EEPROM SIGPRO_RM_TECH_REG DGRM_RSSI_REG   5.1// SIGPRO_RM_TECH_REG (RM_MF_GAIN parameter) This parameter basically defines the gain of the input amplifier.  Select SIGPRO_RM_TECH_REG  Switch "operation" to EEPROM and choose the required technology  Increase the RM_MF_GAIN to 0x02 (it depends on the setup).     5.2// DGRM_RSSI_REG (DGRM_SIGNAL_DETECT_TH_OVR_VAL parameter) This parameter defines a threshold from which the internal logic starts to decode the incoming signal.  If the threshold is too low or very close to the noise floor, the system can detect the noise as an NFC Communication.  It is therefore,  Threshold + margin > noise floor The best routine is to perform "Signal Detection Threshold" analysis. This can be done with the help of the NFC Cockpit (described in PN7642 design-in recommendations) As a result, the user can obtain the mean value of the "Noise," and suggested "DGRM_SIGNAL_DETECT_TH_OVR_VAL" threshold based on the inserted "Margin."  Maring (m) + Noise mean value (μ) = Threshold  6+16=23 Then this value shall be written in "DGRM_RSSI_REG" EEPROM as shown below.    6// ULPCD Settings  We recommend the following ULPCD Settings as a starting point.  ULPCD VDDPA should be chosen in such a way that the HF Attenuator value is not 0x00! The typical value for HF Attenuator in ULPCD is around 0x05-0x0B.   6.1// RSSI Threshold evaluation  For a proper RSSI Threshold selection, it is recommended to perform the ULPCD Calibration, e.g., 20 times, and check the "jitter" of the RSSI signal for your device.  If you see that the RSSI value is jittering, e.g., 1 unit as shown above. The absolute minimum threshold for this case is 2. However, it is always recommended to include adequate margin (To prevent false wake-ups).   Generally, the margin of 2 units is sufficient. So in this case, the optimum threshold will be 4. 
View full article