about the function limit of EB Tresos Studio 29.0 Hello, I am trying to use the AutoSAR example project for S32K344. When I am configuring the project in EB Tresos and run "im- and exporters", there is only one option in the dropdown list as below screenshot. Does anyone know if this software only provides this option or I miss anything in installing and using the software? The software is downloaded from here: Thanks! Crane Re: about the function limit of EB Tresos Studio 29.0 Got it. Thanks Julian! Regards, Crane Re: about the function limit of EB Tresos Studio 29.0 Hi @cranes,
Yes, that is correct. Re: about the function limit of EB Tresos Studio 29.0 Hi, So, it means the license from the activation code provided in the SDK doesn't support full version of im- &exporters, right? Thanks! Crane Re: about the function limit of EB Tresos Studio 29.0 Hi @cranes,
Unfortunately, this is a licensing limitation issue. I recommend contacting EB Tresos to get full version of im- and exporters.
Best regards, Julián
查看全文