Hi team,
Today, I found that the S32DS PA V2.1 installed on my computer wouldn't start properly, which will quit automatically just few seconds after launch, try to setup another workspace still same. So I uninstall it and try to reinstall again, but the installation program will roll back few seconds after I input the activation codes, I can install it on anther computer successfully, so I guess the activation code is ok.
Anyone know how to solve this?
Install log file show below errors:
.....
Summary
-------
Installation: Unsuccessful.
62 Successes
24 Warnings
1 NonFatalErrors
1 FatalErrors
.....
S32 Design Studio for Power Architecture Version 2.1(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)
.....
RepositoryManager: Trying fallback repository location...
#
# INSTALLING VM: d:\NXP\S32DS_Power_v2.1\jre
#
System's temporary directory = C:\Users\shinlitaike08\AppData\Local\Temp
==== License service installation log start: ====
==== License service installation log end. ====
==== License activation log start: ====
#
# A fatal error has been detected by the Java Runtime Environment:
#
# EXCEPTION_ACCESS_VIOLATION (0xc0000005) at pc=0x611a8c19, pid=3644, tid=0x00001db0
#
# JRE version: Java(TM) SE Runtime Environment (8.0_202-b08) (build 1.8.0_202-b08)
# Java VM: Java HotSpot(TM) Client VM (25.202-b08 mixed mode windows-x86 )
# Problematic frame:
# C [cll_app.dll+0x18c19]
#
# Failed to write core dump. Minidumps are not enabled by default on client versions of Windows
#
I have found the solution for me, and it was related to permissions on the installation folder. I give the proper permissions to the installation folder, and then I was able to install the program.
Yes, I did it.
Hi,
Can you make sure you run the installer as Administratior?
Stan
Hi I have the same issue,
I have attached the log I got.
Hi,
Could you possibly try to re-install S32 Design Studio for PA again.
Please use your existing activation code. We've extended the license.
If it still does not work please let us know.
Stan
Hello,
I've moved your post to correct box.
Best regards,
Peter