Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
在 i.MX8 QuadMax 上使用 AAOS 15 启用多用户功能,并设置多显示器 各位同事好, 我们 在 i.MX8 QuadMax 平台 上使用 Android Automotive OS( AAOS) 15 。 我们目前的硬件配置包括三个显示器: 主中央显示屏(驾驶员/中央显示屏) 乘客显示屏 仪表盘显示 我们 希望 在 该 平台 上 启用 和 验证 Android 多用户 功能 , 包括 支持 用户 切换、 访客 用户 和 用户特定的 应用 程序/设置 。 请问 您 能否 就 以下 问题 提供 指导 : 在 i.MX8QM 上 启用 AAOS 15 的 多 用户 支持 需要 哪些 配置 ? NXP 方面 是否 需要 对 电路板支持包 进行 任何 特定的 更改 ? 必须 启用 哪些 框架 覆盖层、 功能 标志 或 系统 属性 ? 任何指导或建议都将不胜感激。   谢谢! Re: Enabling Multi-User Functionality in AAOS 15 on i.MX8 QuadMax with Multi-Display Setup 嗨@harshi03 请参阅官方 Android Automotive 文档: Android Automotive 多用户支持 前台和后台用户系统处理 对于多个显示器上的并发用户,请参考 Android Automotive 多显示器和乘员区域架构: Android Automotive 15 功能 多显示器通信 API 此致, 志明
查看全文
How to generate a Standalone IAR toolchain project from MCUXSDK application example - KWX/MCWX To generate a hello world (suppose) example for KW47-EVK for IAR toolchain. We asume that IAR toolchain is already installed. Set IAR_DIR environment variable. In Windows, this can be done via Edit environment variables system option. Example: IAR_DIR=C:\iar\ewarm-9.60.1.    Note: IAR toolchain version may change. Type the following commands on your MCUXSDK workspace: cd mcuxsdk west build -b kw47evk ./examples/demos_apps/hello_world --toolchain=iar -t standalone_project -Dcore_id=cm33_core0 --pristine -d ./build/kw47evk/kw47evk_standalone_hello_world_iar​ IAR project should have been generated on  MCUXSDK_WS/mcuxsdk/build/kw47evk/kw47evk_standalone_hello_world_iar/iar directory. IAR project has .eww file extension.  neidys_vargas_0-1784665664365.png  Relevant links IDE Project Generation: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/develop/build_system/IDE_Project.html# Note: Ruby is required for this feature. Typically, this tool is installed via MCUXpresso Installer. However, if having issues with this tool refer to the next link: Ruby Environment Setup: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/develop/build_system/IDE_Project.html#ruby-environment-setup Suppose you want to generate a hello world example for KW47-EVK for IAR toolchain as the previous example, but this time LPTMR driver is required for low-power timer operating purposes. We asume that IAR toolchain is already installed and IAR_DIR variable is already set. The easiest way to accomplish this is to add the lptmr Kconfig symbols with ‘yes’ value at Board-Application level (Refer to Kconfig User Guide). In this case, the target prj.conf file is located on  MCUXSDK_WS/mcuxsdk/examples/_boards/kw47evk/demo_apps/hello_world.​ Edit this file and add the LPTMR required symbols:  CONFIG_MCUX_COMPONENT_driver.lptmr=y CONFIG_MCUX_COMPONENT_component.lptmr_adapter=y​ neidys_vargas_4-1784665984531.png neidys_vargas_1-1784665840673.png Type the following command on your MCUXSDK workspace:  west build -b kw47evk ./examples/demo_apps/hello_world --toolchain=iar -t standalone_project -Dcore_id=cm33_core0 --pristine -d ./build/kw47evk/kw47evk_standalone_hello_world_iar IAR project should have been generated on MCUXSDK_WS/mcuxsdk/build/kw47evk/kw47evk_standalone_hello_world_iar/iar directory. IAR project has .eww file extension. This time LPTMR drivers should be included in iar/drivers/lptmr   neidys_vargas_2-1784665938476.png  neidys_vargas_3-1784665959007.png neidys_vargas_5-1784666017506.png
查看全文
Front and Rear Lights – SW & HW Environment 1 Table of Contents • Introduction • Required Software • Required Hardware • References • Conclusion 2 Introduction This article belongs to the Front and Rear Lights series and describes the software and hardware environment used throughout the project. Before looking into signal routing, control logic, or integration aspects, it is important to first understand the tools and platforms that support the development and execution of the front and rear lights application. This article introduces the software components used to develop, configure, and deploy the application, together with the hardware platforms used to demonstrate the lighting functionality. This information provides the foundation needed for the remaining articles in the series. Model-Based Design sits at the center of the workflow. MathWorks tools handle the modeling of the front and rear lighting control logic, the definition of the CAN communication interfaces, and validation across simulation stages. NXP tools then deploy those models to the S32K3 target platform, wiring the generated application to real-time peripherals, LED driver hardware, and lighting feedback signals. 3 Required Software 3.1. Vehicle Network Toolbox Within this workflow, Vehicle Network Toolbox plays a central role in defining, simulating, and validating the CAN interfaces of the front and rear lights module. It brings DBC-driven message definitions directly into Simulink, allowing communication behavior to be tested alongside the control logic long before integration. Every command received from the central controller and every status message sent back to the network is modeled using the exact structure defined in the DBC files, keeping the application perfectly aligned with the vehicle-level specification. Vehicle Network Toolbox is available as an add-on in MATLAB/Simulink, adding support for CAN communication and DBC-based message definitions.   Roxana_Grigore01_0-1784635448020.png Figure 1 - Vehicle Network Toolbox 3.2. Stateflow Stateflow is used to model the control logic of both lighting modules, translating the CAN commands received from the central controller into concrete lighting actions. Each function is represented as a state machine, where transitions are triggered by incoming signals and internal conditions. This approach keeps the logic structured and readable: activation, deactivation, mode switching, and fault handling are all captured in the same diagram. Stateflow is available as an add-on that can be installed directly from within MATLAB/Simulink, extending the environment with state machine modeling capabilities. Roxana_Grigore01_1-1784635471606.png Figure 2 - Stateflow 3.3. NXP Model-Based Design Toolbox for S32K3 NXP Model-Based Design Toolbox for S32K3 is the link between the Simulink model and the S32K3 microcontroller. It takes care of generating the code, building it, and running it on the target, turning the lighting model into a real embedded application. Through its peripheral blocks, the model can directly use the resources needed by the front and rear lights modules, such as DIO, CAN, and UART without leaving the Simulink environment. It also connects to the NXP configuration tools and supports FreeMASTER for real-time monitoring, which makes it easy to check how the lighting logic actually behaves on the hardware. Roxana_Grigore01_2-1784635492503.png Figure 3 - Development flow diagram 4 Required Hardware 4.1. FRDM Automotive S32K312 Development Board (FRDM-A-S32K312) The front and rear lights application runs on the FRDM Automotive S32K312 Development Board, a development platform based on the NXP S32K312 microcontroller. The board provides access to the communication interfaces and processing capabilities of the target device while offering an integrated platform for software development, debugging, and validation activities. Within the scope of this project, the board is used to execute the lighting application and exchange messages with the central controller through the CAN network. Its communication interfaces, debugging connectivity, and expansion capabilities make it suitable for evaluating body electronics use cases and lighting control scenarios. Roxana_Grigore01_3-1784635516304.png Figure 4 - FRDM Automotive S32K312 Development Board 4.2. CAN analyzer Emulates the central controller when the node is not yet integrated with the full system. It injects the CAN commands defined in the DBC files (turn signals, headlight modes, hazard, brake indication, etc.) and captures the status messages sent back by the module, enabling the CAN interface and control logic to be validated in a controlled and repeatable way. 4.3. Addressable LED Strip The physical lighting output is represented by an addressable LED strip, in which each LED can be controlled individually. This makes it possible to reproduce all the relevant lighting functions on a single strip - turn signals, hazard lights, headlight modes, and brake indication - by assigning different LEDs or groups of LEDs to each function. The result is a clear visual representation of the module's behavior, making it easy to demonstrate how the control logic reacts to incoming CAN commands. 5 References Model-Based Design Toolbox (MBDT) MATLAB® and Simulink® Documentation S32K3 Microcontrollers FRDM Automotive S32K312 Development Board (FRDM-A-S32K312) 6 Conclusion This article described the software and hardware enablement required for the front and rear lights modules. The software environment combines MathWorks modeling and vehicle network capabilities with NXP target support, while the hardware environment brings together the FRDM Automotive S32K312 Development Board, a CAN analyzer, and an addressable LED strip. Together, these elements provide the foundation for modeling, simulation, communication, code generation, deployment, and validation of the lighting application. The next article will focus on the architecture and model description of the front and rear lights modules, including the control logic, CAN interfaces, and overall application structure.
查看全文
Using FreeMASTER block in Simulink 1 Table of Contents • Overview • Context • FreeMASTER Blocks • Generated ELF File • Application Example • References • Conclusion 2 Overview This article introduces the FreeMASTER blocks available in NXP Model-Based Design Toolbox (MBDT) and explains how they are used within a Simulink model to prepare an application for FreeMASTER integration. The primary focus is the FreeMASTER Config block, which enables the FreeMASTER Driver in the generated application and allows users to configure the communication interface and runtime parameters required by FreeMASTER. The article also introduces the FreeMASTER Recorder block, which can be used to add data-recording capabilities to the application. Why is this Important? Before FreeMASTER can communicate with an embedded application, the FreeMASTER Driver should be enabled and configured in the embedded application. The FreeMASTER blocks provided by MBDT simplify this integration process by allowing all required settings to be configured directly within the Simulink environment. This article is intended for: Simulink users working with NXP Model-Based Design Toolbox Developers integrating FreeMASTER into embedded applications Engineers interested in runtime monitoring and debugging Users preparing an application for future interaction with FreeMASTER By reading this article, you will understand how FreeMASTER support is enabled within a Simulink model and how the generated application is prepared for runtime communication and data access. You will also learn how the code-generation process produces an ELF file containing symbolic information corresponding to application variables, which is later used by FreeMASTER to access, monitor, and visualize application data. 3 Context Dedicated Simulink blocks integrate FreeMASTER into a Model-Based Design Toolbox project by automatically generating the software infrastructure required by the application. The overall workflow is illustrated below: dragostoma_0-1784636089488.png Figure 1. FreeMASTER workflow In this workflow, the FreeMASTER blocks serve as the interface between the Simulink model and the FreeMASTER Driver that will be included in the generated application. 4 FreeMASTER Blocks FreeMASTER blocks can be found in the MBDT library under: S32K3xx Core, System, Peripherals and Utilities → Utility Blocks dragostoma_1-1784636129421.png Figure 2. FreeMASTER Simulink Library Three blocks are available for FreeMASTER integration: FreeMASTER Config block FreeMASTER Poll block FreeMASTER Recorder block 4.1 FreeMASTER Config Block The FreeMASTER Config block is responsible for enabling and configuring the FreeMASTER Driver within the generated application. It inserts the software infrastructure required for communication between the embedded target and the FreeMASTER desktop tool and serves as the foundation for integrating FreeMASTER functionality into a Simulink model. dragostoma_2-1784636149271.png Figure 3. FreeMASTER Config block This block provides a configuration interface divided into two sections: communication settings and runtime settings. 4.1.1 General Tab The General tab contains communication-related parameters: Connection Type – selects the communication interface used by FreeMASTER. Instance – specifies the peripheral instance assigned to FreeMASTER communication. Baudrate – defines the communication speed. ISR Priority – sets the interrupt priority associated with FreeMASTER communication. dragostoma_3-1784636164202.png Figure 4. FreeMASTER General tab During configuration, a dedicated communication peripheral is assigned to the FreeMASTER Driver. In the example shown, communication is performed through LPUART6 operating at 115200 bps. Note: The peripheral assigned to FreeMASTER should not be reused simultaneously for other communication purposes. During initialization, the FreeMASTER Driver assumes control of the communication resources associated with the selected peripheral. 4.1.2 FreeMASTER Configuration Tab The FreeMASTER Configuration tab contains runtime-related settings: Mode – defines the FreeMASTER operating mode. Number of Scopes – specifies the number of available scope instances. Max Variables – defines the maximum number of variables handled by a scope. Automatic Buffer Size – automatically calculates communication buffer size. FIFO Receiver Queue Size – configures the receive queue used by the communication driver. dragostoma_4-1784636183944.png Figure 5. FreeMASTER Configuration tab Together, these settings determine how the FreeMASTER Driver operates within the generated application. 4.2 FreeMASTER Recorder Block In addition to the configuration block, MBDT provides a FreeMASTER Recorder block that enables support for FreeMASTER recording functionality. dragostoma_5-1784636199716.png Figure 6. FreeMASTER Recorder block Unlike the Config block, which is primarily focused on communication setup and driver integration, the Recorder block is designed for high-speed monitoring and visualization of application variables. It configures data acquisition resources that can be accessed later through the FreeMASTER desktop application, enabling detailed analysis of system behavior. The Recorder block is typically placed in application execution paths where rapidly changing signals need to be captured periodically. To support this, it uses an on-board memory buffer to store acquired samples, allowing high-frequency data to be recorded without requiring immediate transfer to the host PC. The buffered data can then be retrieved and displayed in FreeMASTER for waveform visualization, performance evaluation, and post-run analysis. The block provides the following configuration parameters: Id – unique identifier of the recorder instance. Name – user-defined recorder name. Buffer Size – amount of memory allocated for storing captured samples. Timebase – time reference used during recording operations. dragostoma_6-1784636215463.png Figure 7. FreeMASTER Recorder block parameters The Recorder block is optional and can be used whenever runtime data recording capabilities are required. 4.3 FreeMASTER Poll Block MBDT also provides a FreeMASTER Poll block, which allows the application to explicitly call the FreeMASTER polling function within the Simulink model. dragostoma_7-1784636229746.png Figure 8. FreeMASTER Poll block The Poll block does not require any configuration parameters. Its purpose is to provide a configurable location within the application where FreeMASTER communication handling and command processing can be executed. dragostoma_8-1784636242667.png Figure 9. FreeMASTER Poll block mask The role of the Poll block depends on the operating mode selected in the FreeMASTER Config block. When the FreeMASTER Driver is configured in Poll Mode, the Poll block is responsible for both communication handling and command processing. When the Driver operates in Short Interrupt Mode, communication is handled by interrupts, while command processing is performed through the Poll block. Note: For both Poll Mode and Short Interrupt Mode, the Poll block is required and should be placed in an execution path that runs periodically, such as the application's main step function, to ensure timely processing of FreeMASTER requests. When the FreeMASTER Driver is configured in Long Interrupt Mode, communication handling and command processing are performed entirely by the driver interrupt routines. In this configuration, the Poll block is not required, and its execution has no effect on FreeMASTER operation. The Poll block complements the FreeMASTER Config and FreeMASTER Recorder blocks by providing a configurable mechanism for communication processing when required by the selected FreeMASTER operating mode. 5 Generated ELF File Once the FreeMASTER blocks have been added and configured, the model can be built using the standard code-generation workflow provided by Embedded Coder and MBDT. In addition to the application code generated from the Simulink model, the build process also produces an ELF (Executable and Linkable Format) file. When debug information is enabled during the build process, the ELF file contains symbolic information about application variables, functions, and memory locations stored in the DWARF debug sections. Otherwise, this information may be removed, preventing the FreeMASTER desktop tool from extracting the symbols required for variable access and monitoring. The ELF file is later loaded by the FreeMASTER desktop tool, allowing variables to be identified automatically without requiring manual memory address entry. This enables features such as variable monitoring, runtime configuration, data visualization, and recording. Note: Generating a valid ELF file with debug information is an important preparation step before attempting to establish communication with the target application. 6 Application Example To showcase the concepts described above, we can create a simple Simulink model example that uses the FreeMASTER Config block together with two application variables: counter and increment . In this example, the counter variable is periodically incremented by the value of the increment variable. The increment variable can be modified at runtime by the user directly from the FreeMASTER desktop application, allowing the rate at which counter grows to be adjusted on the fly. dragostoma_0-1785932572908.png Figure 10. Application example Simulink model This simple model demonstrates the two fundamental capabilities enabled by FreeMASTER integration: Variable monitoring – observing the value of counter as it changes over time. Runtime variable modification – updating the value of increment from FreeMASTER and immediately observing its effect on counter . image.png Figure 11. FreeMASTER application of the counter example   Once the model is built and the resulting application is running on the target, both variables become accessible through FreeMASTER using the symbolic information contained in the generated ELF file. The user can watch counter update in real time and interactively change increment to influence the application's behavior without recompiling or reflashing the target. 7 References Introduction to FreeMASTER FreeMASTER Driver and Documentation Package – The FreeMASTER Driver and its accompanying documentation are delivered as part of the MBDT installation. After installing the toolbox, they can be found in the root installation directory: NXP_MBDToolbox_S32K3\FreeMASTER\ 8 Conclusion This article introduced the FreeMASTER Configuration blocks provided by NXP Model-Based Design Toolbox and explained their role in preparing a Simulink model for FreeMASTER integration. By configuring the block appropriately, developers can include the required FreeMASTER support in the generated application and produce an ELF file suitable for runtime access to application data. The next article in this series will demonstrate how to use the generated application and ELF file to establish a connection between the target device and the FreeMASTER desktop application.
查看全文
S32K3X8EVB-Q289 Power Supply Question I bought the S32K3X8EVB-Q289 board and need to purchase a power cable separately. Should I buy a power adapter with 12V 2A or higher? Or is there a product recommended by NXP? The FRDM-A-S32K358 uses a USB Type-C port, so it was sufficiently powered by a laptop's USB port, Re: S32K3X8EVB-Q289 Power Supply Question Hello @wj_kwak, Yes, as noted inside the S32K3X8 EVB HW UM, you can use any external power supply as long as it provides +12V/≥2A; Julin_AragnM_0-1784565662949.png Best regards, Julián
查看全文
s32k324 写入 Dflash 问题 我使用 S32DS3.5 + RTD2.0 开发了 S32K324。现在,我根据示例“Fee_Example_S32K344”中的配置和代码编写了 S32K324 的程序,并且编译成功了。但是程序运行时,一进入代码“Fls_Init(NULL_PTR);”就会报错。当我单步执行时,发现它无法跳过函数“Fls_IPW_Init();”。错误导致程序进入此函数“ static inline void DevAssert(volatile boolean x) { 如果(x) { } 否则 { for(;;) {ASM_KEYWORD(BREAKPOINT_INSTR);} } }" 所以我想如果RTD版本不支持S32K324来使用费用函数模型的话?或者能否给我一些其他通过 S32k324 的 eeprom 模式写入 Dflash 的示例? 谢谢。 Re: s32k324 write Dflash problem 由于所有项目工程都是基于 RTD2.0 创建的,因此迁移可能不太方便。如果RTD2.0能够修改和使用费用就最好了。您能帮我审核一下这个程序吗? Re: s32k324 write Dflash problem S32DS 生成的 Fls_IPW_Init() 函数是否会输出错误日志? Re: s32k324 write Dflash problem 嗨@mmyjh_123 , 能否分享一下项目文件,或者至少分享一下 .mex 文件?文件? 另外,你用的还是很老旧的RTD。 我建议升级到 RTD 7.0.1 版本。 谢谢! BR,丹尼尔 Re: s32k324 write Dflash problem 嗨@mmyjh_123 , 你有两个选择。 1. 要么将其更改为 VARIANT-PRE-COMPILE danielmartynek_0-1784639285437.png 就按你平时的方式称呼它吧: Fls_Init(NULL_PTR); 2. 或者选择 VARIANT-POST-BUILD 代替 并拨打电话: Fls_Init(&Fls_Config_BOARD_InitPeripherals); 此致, 丹尼尔 Re: s32k324 write Dflash problem 哦,我明白了,谢谢。
查看全文
V5705芯片 您好,我有一台适用于Clio 5汽车的收音机。它采用的是恩智浦V5707芯片。但我没有找到这款芯片的任何技术规格。这款芯片属于哪个TEF系列?(例如TEF6686、TEF6687、TEF6688、TEF6689等) 标记 = v5705 54 10 sSD1462
查看全文
FS26 LDO Off Issue Hello I am using the FS26 and S32K358. I am using the FS26's VLDO2 as the power supply for the MCU and the FS26's VLDO1 as the power supply for the CAN transceiver. When the MCU is left in a state of CAN communication, the FS26's VLDO turns OFF, cutting off the MCU's power. (This occurs randomly, approximately every 1 to 8 hours.) The VLDO is restored only after the FS26's power supply is cut off and then restored. This issue occurs on all boards, not just a single one, and does not occur when CAN communication is not in progress. The status when the issue occurs is as follows: Vpre 6V O VDIG 1.6V O VBOS 5V O VLDO2 X VLDO1 X VCORE X DFS is disabled via OTP. I would like to know the current state of the FS26 and what causes this to happen. Re: FS26 LDO Off Issue Hello kjy106906  Good day! Is the watchdog enabled? What are the values of: FS_STATES FS_GRL_FLAGS FS_OVUV_REG_STATUS M_REG_FLG M_STATUS immediately after failure? Have you checked if FS26 is not displaying any UV or OV flags? Also could you share your M_STATUS? I hope this information has helped you, please let me know if you need help with anything else. Have a great day and best of luck. Re: FS26 LDO Off Issue @RafaR  Thank you for the reply. Unfortunately, the MCU is receiving power from the SBC, but communication is not possible because the VLDO is OFF. You must cut off and resupplied the board power for the MCU to function. The watchdog window is infinite. Re: FS26 LDO Off Issue Hello kjy106906 Good day! Looks as if the FS26 analog front end is still powered, but the internal power-tree supplying the system has been disabled. One possible explanation is that a fault has been detected on one of the monitored regulators (VCORE, VLDO1, VLDO2), and the configured reaction disables the regulator outputs. FS26 documentation indicates that regulators can remain disabled after a fault depending on the configured fault-reaction settings. I hope this information has helped you, please let me know if you need help with anything else. Have a great day and best of luck. Re: FS26 LDO Off Issue db16122_0-1785211448726.png Please refer to PMIC initiailization process for debug. AN13431 NXP PMIC solution for TI TMS570 series MCU should be helpful Re: FS26 LDO Off Issue Thank you @RafaR  This is an important issue, so I would appreciate your response. I would like to check exactly what state FS26 is in and why it failed. When the issue occurred, I read the registers using an external tool. FS26 [FS_STATES:0x17]R:0x0009; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MIRRORCMD:0x1c]W:0x001d; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MIRRORDATA:0x1d]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [ID_VOTP:0x1D]R:0x00 FS26 [FS_WDW_DURATION:0x0b]W:0xd08b; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_NOT_WDW_DURATION:0x0c]W:0x2f74; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_FLG:0x07]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_MSK:0x08]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_FLG:0x05]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_MSK:0x06]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_FLG:0x03]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_MSK:0x04]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_FLG:0x09]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_MSK:0x0a]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_STATUS:0x02]R:0x5020; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_FLG:0x0b]R:0x0005; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_MSK:0x0c]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_OVUV_REG_STATUS:0x10]R:0x1544; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_INTB_MASK:0x16]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY1:0x14]R:0x03c3; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY2:0x15]R:0x0010; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_SAFE_IOS_1:0x12]R:0xf000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_STATES:0x17]R:0x0009; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_GRL_FLAGS:0x00]R:0x5000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_DEVICEID:0x00]R:0x65d8; CRC[MOSI:0x00; MISO:0x00] FS26 [M_PROGID:0x01]R:0x0105; CRC[MOSI:0x00; MISO:0x00] FS26 [M_STATUS:0x02]R:0x5020; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_FLG:0x03]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_MSK:0x04]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_FLG:0x05]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_MSK:0x06]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_FLG:0x07]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_MSK:0x08]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_FLG:0x09]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_MSK:0x0a]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_FLG:0x0b]R:0x0005; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_MSK:0x0c]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_SYS_CFG:0x0d]R:0x0001; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_CFG:0x0e]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_CFG:0x0f]R:0x0002; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_CFG:0x10]R:0x0202; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_CTRL1:0x11]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_AMUX_CTRL:0x13]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CFG1:0x14]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CFG2:0x15]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CFG3:0x16]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CTRL:0x17]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MEMORY0:0x18]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MEMORY1:0x19]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_GRL_FLAGS:0x00]R:0x5000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_WDW_DURATION:0x0b]R:0xd08b; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_NOT_WDW_DURATION:0x0c]R:0x2144; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_WD_TOKEN:0x0e]R:0x5ab2; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_ABIST_ON_DEMAND:0x0f]R:0x0040; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_OVUV_REG_STATUS:0x10]R:0x1544; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_SAFE_IOS_1:0x12]R:0xf000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_SAFE_IOS_2:0x13]R:0x035f; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY1:0x14]R:0x03c3; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY2:0x15]R:0x0010; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_INTB_MASK:0x16]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_STATES:0x17]R:0x0009; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_LP_REQ:0x18]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_LDT_LPSEL:0x19]R:0x0000; CRC[MOSI:0x00; MISO:0x00] I am attaching the waveform when an issue occurs. kjy106906_0-1785205262839.png Blue VSUP / Red VBOS / Green RSTB / Yellow VDIG kjy106906_1-1785205354126.png Blue VSUP / Red VPre / Green Vcore / Yellow RSTB
查看全文
请求:RAppID 初始化 v2.1.0支持 MPC5644A 设备的版本(或更高版本)——需要下载链接 你好, 我正在做一个基于 MPC5644A 的项目,我需要获取支持该设备的 RAppID Init 工具。 我有一个现有的 RAppID Init 项目文件 (.rsp),该文件最初是为我们的平台创建的。文件头显示以下内容: 工具版本:2.1.0(工具版本主版本号 2,工具版本次版本号 1,子版本号 0) 目标设备:MPC5644A 创建时间:2013年4月 因此,RAppID Init v2.1.0 中显然存在对 MPC5644A 的支持。但是,我在NXP官网上找不到匹配的下载链接: “RAppID 初始化 Power Architecture”页面 (RAPPID) 列出了 11 个公开下载,但没有一个涵盖 MPC564xA 系列(仅涵盖 MPC564xL、MPC560xB/xS、MPC563xM、MPC567xR/xK/xF、MPC5748G、MPC577xK/M)。 我在存档部分找到了“存档:MPC564xA 引脚向导”,但没有找到相应的“MPC564xA 初始化”软件包。引脚向导不包含系统/外设初始化,也无法打开我的 .rsp 文件。项目文件。 请问版主能否提供 RAppID Init v2.1.0 的下载链接?或者更高版本,支持 MPC5644A 设备,这样我就可以打开和修改我现有的 .rsp 文件了。项目? 提前感谢您的帮助。 Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed 你好, 是的,您说得对,确实存在 RAPPID-564XASW。 但恩智浦并未在其公共网页上提供该产品。 我会内部询问获取该文件的程序。 顺祝商祺! Peter Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed 请查看以下链接:RAppID 初始化(适用于 Power Architecture)| NXP 半导体  RAppID 引导加载程序实用程序初始化(适用于 MPC564xL) https://www.nxp.com/design/design-center/software/embedded-software/rappid-initialization-for-power-architecture:RAPPID 顺便问一下, MPC5644A 在您那里用于什么应用? Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed 我什么时候能收到回复? Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed 我已经看过那个页面了,但我的情况不同,因为我的是 MPC5644A。 另外,我的 MPC5644A 似乎是用于车辆控制的。 Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed https://www.nxp.com/webapp/Download?colCode=ETPUGCT&appType=license&location=null eTPU图形化配置工具怎么样?它看起来也相当实用。由于该产品是比较老旧的设备,因此可能会出现一些服务延迟。
查看全文
AUTOSAR MCAL for MPC5744P 大家好, 我正在使用 MPC5744P 和生成的 AUTOSAR MCAL 包。 我遇到了一个版本错误: 没有找到该文件或目录——指的是 Os_memmap.h在 MemMap.h 中: #ifndef AUTOSAR_OS_NOT_USED #include "Os_memmap.h" #endif 但是,生成的文件中没有 Os_memmap.h 文件。 我该如何找回这个丢失的文件? 另外,如何使用 EB tresos 配置和生成新的 MCAL 包(或重新生成缺失的部分)? 非常感谢您的帮助! 谢谢! Re: AUTOSAR MCAL for MPC5744P 您好@petervlna ,请问是否有免费的编译器选项可以用来构建适用于 MPC5744P 的 AUTOSAR MCAL 应用程序? Re: AUTOSAR MCAL for MPC5744P 你好, 您可以使用生成的代码,并将其编译为 GHS 或 DIAB。 请务必参考 RTD 和 OS 发行说明中列出的受支持的编译器。 petervlna_0-1747642736488.png 顺祝商祺! Peter Re: AUTOSAR MCAL for MPC5744P 嗨,彼得, 谢谢你的解释! 请问:是否可以使用 GCC 编译生成的代码(来自 Tresos + MCAL),还是必须使用 S32DS 或 GHS 等工具链? 此致, 伟大的 Re: AUTOSAR MCAL for MPC5744P 你好, 我该如何找回这个丢失的文件? 它不是 MCAL 生成的文件的一部分,而是来自 Tresos 操作系统配置。 我认为可能是操作系统配置出了问题。 另请参阅此处: https://community.nxp.com/t5/S32K/No-such-file-or-directory-include-quot-Os-memmap-h-quot/td-p/1818413 另外,如何使用 EB tresos 配置和生成新的 MCAL 包(或重新生成缺失的部分)? 嗯,我们为此提供 S32 设计工作室。如需了解 Tresos 的相关培训,请联系 Elektrobit。 其实应该很简单。安装 MCAL 后,您只需创建项目,添加所需的插件,然后从 Tresos 生成 c/h 文件。然后,您需要将项目整理到 S32DS、GHS 等项目管理软件中,以便进行编译。 顺祝商祺! Peter
查看全文
S32K3X8EVB-Q289 電源に関する質問 S32K3X8EVB-Q289ボードを購入しましたが、電源ケーブルは別途購入する必要があります。12V 2A以上の電源アダプターを購入すべきでしょうか?それともNXPが推奨する製品はありますか? FRDM-A-S32K358はUSB Type-Cポートを使用しているため、ノートPCのUSBポートで十分な電力を供給していました。 Re: S32K3X8EVB-Q289 Power Supply Question こんにちは、 @wj_kwak さん、 はい、S32K3X8 EVB HW UMの中に記載されている通り、+12V/≥2Aを供給する外部電源ならどんなものでも使えます。 Julin_AragnM_0-1784565662949.png よろしくお願いします、 ジュリアン
查看全文
s32k324 write Dflash problem I used S32DS3.5 + RTD2.0 to develop S32K324. Now I wrote the program for the S32K324 based on the configuration and code in the example "Fee_Example_S32K344" and it compiled. but when it ran, the program would report an error as soon as it enters this code" Fls_Init(NULL_PTR);", when I step into it , I found it could not Skip this function " Fls_IPW_Init();". And the err made the program enter this function " static inline void DevAssert(volatile boolean x) { if(x) { } else { for(;;) {ASM_KEYWORD(BREAKPOINT_INSTR);} } }" So I guess if the RTD version doesn't support S32K324 to use the fee function model ? Or could give me some other examples to write Dflash by eeprom mode of S32k324. Thanks. Re: s32k324 write Dflash problem Since all the project engineering was created based on RTD2.0, the migration might not be very convenient. It would be best if RTD2.0 could modify and use the Fee. Could you please help me review the program? Re: s32k324 write Dflash problem Does the Fls_IPW_Init() generated by S32DS and is there any error log can be printed out? Re: s32k324 write Dflash problem Hi @mmyjh_123, Can you share the project or at least the .mex file? Also, you use a very old RTD. I would recommended upgrading to RTD 7.0.1. Thank you, BR, Daniel Re: s32k324 write Dflash problem Hi @mmyjh_123, You have two options. 1. Either change it to VARIANT-PRE-COMPILE danielmartynek_0-1784639285437.png And call it as you do: Fls_Init(NULL_PTR); 2. Or select VARIANT-POST-BUILD instead and call: Fls_Init(&Fls_Config_BOARD_InitPeripherals); Regards, Daniel Re: s32k324 write Dflash problem Oh, I got it,thanks.
查看全文
FS26 LDO 発行終了 Hello 私はFS26とS32K358を使用しています。 私はFS26のVLDO2をMCUの電源として、FS26のVLDO1をCANトランシーバの電源として使っています。 MCUがCAN通信状態のままになると、FS26のVLDOはオフになり、MCUの電源が遮断されます。 (これはランダムに発生し、およそ1~8時間ごとに起こります。) VLDOは、FS26の電源が遮断され、その後復旧された後にのみ復旧します。 この問題はすべてのボードで発生し、単一のボードだけでなく、CAN通信が進行中でない場合は発生しません。 問題発生時の状況は以下のとおりです。 Vpre 6V O VDIG 1.6VO VBOS 5V O VLDO2 X VLDO1 X VCORE X OTPによるDFSは無効化されています。 FS26の現状と、この問題が発生する原因について知りたいです。 Re: FS26 LDO Off Issue こんにちは、 kjy106906さん 良い一日! ウォッチドッグは有効になっていますか? 以下の値は何ですか? FS_STATES FS_GRL_FLAGS FS_OVUV_REG_STATUS M_REG_FLG 障害発生直後にM_STATUSが表示されますか? FS26にUVフラグやOVフラグが表示されていないか確認しましたか? また、あなたのM_STATUSも教えてもらえますか? この情報がお役に立てば幸いです。他に何かご不明な点がありましたら、お気軽にお問い合わせください。 良い一日をお過ごしください。幸運を祈ります。 Re: FS26 LDO Off Issue @RafaR ご返信ありがとうございます。 残念ながら、MCUはSBCから電力を受け取っていますが、VLDOがオフであるため通信は不可能です。 MCUが動作するためには、基板の電源を切って再供給しなければなりません。 監視ウィンドウは無限です。 Re: FS26 LDO Off Issue こんにちは、kjy106906さん 良い一日! FS26のアナログフロントエンドはまだ電源が供給されているようですが、システムに電力を供給する内部電源ツリーは無効化されています。 考えられる説明の一つは、監視対象のレギュレータ(VCORE、VLDO1、VLDO2)のいずれかに障害が検出され、設定された反応によってレギュレータの出力が無効になったというものです。FS26のドキュメントによると、故障後も設定された故障反応設定によってレギュレータは無効化されたままになることがあります。 この情報がお役に立てば幸いです。他に何かご不明な点がありましたら、お気軽にお問い合わせください。 良い一日をお過ごしください。幸運を祈ります。 Re: FS26 LDO Off Issue よろしくお願い申し上げます。 @RafaR これは重要な問題なので、ご回答をいただけるとありがたいです。 FS26が現在どのような状態にあり、なぜ失敗したのかを正確に確認したいです。 問題が発生した際、外部ツールを使用してレジスタを読み取りました。 FS26 [FS_STATES:0x17]R:0x0009; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MIRRORCMD:0x1c]W:0x001d; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MIRRORDATA:0x1d]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [ID_VOTP:0x1D]R:0x00 FS26 [FS_WDW_DURATION:0x0b]W:0xd08b; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_NOT_WDW_DURATION:0x0c]W:0x2f74; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_FLG:0x07]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_MSK:0x08]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_FLG:0x05]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_MSK:0x06]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_FLG:0x03]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_MSK:0x04]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_FLG:0x09]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_MSK:0x0a]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_STATUS:0x02]R:0x5020; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_FLG:0x0b]R:0x0005; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_MSK:0x0c]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_OVUV_REG_STATUS:0x10]R:0x1544; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_INTB_MASK:0x16]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY1:0x14]R:0x03c3; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY2:0x15]R:0x0010; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_SAFE_IOS_1:0x12]R:0xf000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_STATES:0x17]R:0x0009; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_GRL_FLAGS:0x00]R:0x5000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_DEVICEID:0x00]R:0x65d8; CRC[MOSI:0x00; MISO:0x00] FS26 [M_PROGID:0x01]R:0x0105; CRC[MOSI:0x00; MISO:0x00] FS26 [M_STATUS:0x02]R:0x5020; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_FLG:0x03]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_MSK:0x04]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_FLG:0x05]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_MSK:0x06]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_FLG:0x07]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_MSK:0x08]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_FLG:0x09]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_MSK:0x0a]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_FLG:0x0b]R:0x0005; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_MSK:0x0c]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_SYS_CFG:0x0d]R:0x0001; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_CFG:0x0e]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_CFG:0x0f]R:0x0002; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_CFG:0x10]R:0x0202; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_CTRL1:0x11]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_AMUX_CTRL:0x13]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CFG1:0x14]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CFG2:0x15]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CFG3:0x16]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CTRL:0x17]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MEMORY0:0x18]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MEMORY1:0x19]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_GRL_FLAGS:0x00]R:0x5000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_WDW_DURATION:0x0b]R:0xd08b; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_NOT_WDW_DURATION:0x0c]R:0x2144; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_WD_TOKEN:0x0e]R:0x5ab2; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_ABIST_ON_DEMAND:0x0f]R:0x0040; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_OVUV_REG_STATUS:0x10]R:0x1544; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_SAFE_IOS_1:0x12]R:0xf000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_SAFE_IOS_2:0x13]R:0x035f; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY1:0x14]R:0x03c3; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY2:0x15]R:0x0010; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_INTB_MASK:0x16]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_STATES:0x17]R:0x0009; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_LP_REQ:0x18]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_LDT_LPSEL:0x19]R:0x0000; CRC[MOSI:0x00; MISO:0x00] 問題発生時の波形を添付します。 kjy106906_0-1785205262839.png 青:VSUP / 赤:VBOS / 緑:RSTB / 黄:VDIG kjy106906_1-1785205354126.png 青色 VSUP / 赤色 VPre / 緑色 Vcore / 黄色 RSTB Re: FS26 LDO Off Issue db16122_0-1785211448726.png デバッグについては、PMICの初期化プロセスを参照してください。AN13431 TI TMS570シリーズMCU向けのNXP PMICソリューションは役立つはずです
查看全文
s32k324 Dflash書き込みの問題 S32K324の開発には、S32DS3.5とRTD2.0を使用しました。今回、サンプル「Fee_Example_S32K344」の構成とコードに基づいてS32K324用のプログラムを作成し、コンパイルしました。しかし実行されると、このコードを入力した直後にエラーを報告しました」Fls_Init(NULL_PTR);「、入ったときにこの機能をスキップできないことがわかりました」 Fls_IPW_Init();".そしてerrはプログラムにこの関数を入力させました static inline void DevAssert(volatile boolean x) { if(x) { } else { for(;;){ASM_KEYWORD(BREAKPOINT_INSTR);}} }" つまり、RTD版がS32K324をサポートしていないなら、手数料機能モデルを使うということですか?あるいは、S32k324のeepromモードでDflashを書く他の例を教えてもらえますか? ありがとうございます。 Re: s32k324 write Dflash problem プロジェクトエンジニアリングはすべてRTD2.0に基づいて作成されているため、移行はあまり容易ではないかもしれません。RTD2.0が手数料を修正して利用できれば最善でしょう。プログラムのレビューを手伝ってもらえますか? Re: s32k324 write Dflash problem S32DSで生成されたFls_IPW_Init()やエラーログは印刷できますか? Re: s32k324 write Dflash problem こんにちは、 @mmyjh_123 さん。 プロジェクトか、せめて.mexファイルを共有してもらえますか?ファイル? また、非常に古いRTDを使用しています。 RTD 7.0.1へのアップグレードをお勧めします。 ありがとうございました。 BR、ダニエル Re: s32k324 write Dflash problem こんにちは、 @mmyjh_123 さん。 選択肢は2つあります。 1. VARIANT-PRE-COMPILE に変更してください。 danielmartynek_0-1784639285437.png そして、あなたがそう呼ぶように呼んでください。 Fls_Init(NULL_PTR); 2. または、代わりにVARIANT-POST-BUILDを選択してください。 そして電話してください: Fls_Init(&Fls_Config_BOARD_InitPeripherals); よろしくお願いいたします。 ダニエル Re: s32k324 write Dflash problem ああ、わかりました、ありがとうございます。
查看全文
V5705 Chip Hi, I have got radio for Clio 5 car. It's have V5707 nxp chip. But i didnt find any technical spec for this chip. Which tef series does this chip belong to? (tef6686, tef6687, tef6688, tef6689 etc) marked = v5705 54 10 sSD1462 
查看全文
S32G3 LLCE CANドライバーをfreeRTOSで動かす方法 こんにちは、みんな、 私はS32G-VNP-RDB3ボードを扱っており、このモジュールでLLCE CANを使おうとしています。NXPのウェブサイトを検索しましたが、S32G2のポーティング方法がS32DS3.4しか見つかりませんでした。S32DS3.5は搭載されていません。S32G3の移植方法。私のセットアップはS32DS3.5です。RTDは4.4.4です。EB Tresos StudioとLLCEの場合、どのバージョンを使ってコードをコンパイルCAN2CAN通過させるべきでしょうか?S32G-VNP-RDB3(S32G399A)のポーティング方法はどこで見つけられますか?以下は私のS32DS.3.5ですインストール手順。 Jimmybai_0-1784536137448.png ゴールドVIP Re: How to let S32G3 LLCE CAN driver run in freertos こんにちは、 @Jimmybai 投稿ありがとうございます。 よろしければ、お使いのシステム構成を教えていただけますか? 1. テストで使用したLLCEのバージョンは何ですか?使用したRTDのバージョンは何ですか?(RTD4.4.4は存在しないため) 2. では、RDB3上のFreeRTOS内にCAN2CANアプリケーションを実装したいのですか? BR チェイン Re: How to let S32G3 LLCE CAN driver run in freertos こんにちは、チェンインさん 実際、あなたのRTDバージョンが何を指しているのか分かりません。もしかしてLLCE RTDのことでしょうか?LLCE環境のセットアップ方法についてはほとんど知識がありません。私のセットアップはS32G399Aベンチで、S32G3 RTDは4.0.0です。セットアップとダウンロードの位置におすすめのLLCEとRTDのバージョンS32G399A教えてもらえますか?本当に、S32G3用のLLCE設定ガイドが必要なんです。ありがとう。 Re: How to let S32G3 LLCE CAN driver run in freertos こんにちは、 @Jimmybai ご返信ありがとうございます。 専用のバージョン依存関係がない場合は、まず AN13423 を参考にしてS32GプラットフォームでのCAN2CAN基本的な使い方を学ぶことをお勧めします BR チェイン
查看全文
S32K3X8EVB-Q289 电源问题 我购买了S32K3X8EVB-Q289主板,还需要单独购买电源线。我应该购买12V 2A或更高规格的电源适配器吗?或者恩智浦半导体有没有推荐的产品? FRDM-A-S32K358 使用 USB Type-C 接口,因此可以通过笔记本电脑的 USB 接口供电。 Re: S32K3X8EVB-Q289 Power Supply Question 你好@wj_kwak , 是的,正如 S32K3X8 EVB HW UM 中所述,只要外部电源提供 +12V/≥2A,您就可以使用它; Julin_AragnM_0-1784565662949.png 此致, 朱利安
查看全文
AUTOSAR MCAL for MPC5744P Hello everyone, I'm working with the MPC5744P and using the generated AUTOSAR MCAL packages. I'm encountering a build error: No such file or directory — referring to Os_memmap.h inside MemMap.h: #ifndef AUTOSAR_OS_NOT_USED       #include "Os_memmap.h" #endif However, Os_memmap.h is not present in the generated files. How can I get this missing file? Also, how can I use EB tresos to configure and generate a new MCAL package (or regenerate the missing parts)? Any help would be appreciated! Thank you. Re: AUTOSAR MCAL for MPC5744P Hello @petervlna , is there any free compiler option to build the AUTOSAR MCAL applications for MPC5744P? Re: AUTOSAR MCAL for MPC5744P Hello, You can use the generated code and compile it in GHS or DIAB. Always refer to supported compilators in release notes of the RTD and OS. petervlna_0-1747642736488.png Best regards, Peter Re: AUTOSAR MCAL for MPC5744P Hi Peter, Thank you for the clarification! Just a quick question: Is it possible to compile the generated code (from Tresos + MCAL) using GCC, or is it mandatory to use toolchains like S32DS or GHS? Best regards, El-Greatly Re: AUTOSAR MCAL for MPC5744P Hello, How can I get this missing file? It is not part of generated files of MCAL but from the Tresos OS configuration. In my opinion probably there was something wrong in OS configuration. Have a look also here: https://community.nxp.com/t5/S32K/No-such-file-or-directory-include-quot-Os-memmap-h-quot/td-p/1818413 Also, how can I use EB tresos to configure and generate a new MCAL package (or regenerate the missing parts)? Hmm, we offer S32 design studio for such. For trainings on Tresos please get in touch with Elektrobit. Actually it should be very simple. Once you install MCAL you will simply create project, add desired pluggins and generate the c/h files from tresos. Then you will put the project together in some project manager like S32DS, GHS, etc... to be able to compile it. Best regards, Peter
查看全文
ライセンス更新申請 – S32 Design Studio for Power Architecture 2017.R1(ライセンス期限切れ間もなく) 親愛なるNXPサポートチームへ、 現在、S32 Design Studio for Power Architecture バージョン 2017.R1(ビルドID: 171018)を使っています。私のライセンス(アクティベーションコード:[4C46-757C-2641-913E])は数日後に期限切れになります。ツールを中断せずに使い続けられるように、更新を手伝ってもらえますか? 既にNXPアカウントにログインし、ライセンスの状態を確認済みです。他に何か情報が必要な場合はお知らせください。 再開まで今しばらくお待ちください。 よろしくお願いします、 [zt] アクティベーションID: 4C46-757C-2641-913E Re: License Renewal Request – S32 Design Studio for Power Architecture 2017.R1 (License about to exp こんにちは、 お客様のS32DSライセンスが延長されました。以前使用していたコードを使って、S32DSを再度有効化してください。
查看全文
FS26 低压差线性稳压器(LDO) 关闭问题 Hello 我使用的是 FS26 和 S32K358。 我使用 FS26 的 VLDO2 作为 MCU 的电源,使用 FS26 的 VLDO1 作为 CAN 收发器的电源。 当 MCU 处于 CAN 通信状态时,FS26 的 VLDO 会关闭,从而切断 MCU 的电源。 (这种情况随机发生,大约每 1 至 8 小时发生一次。) 只有当 FS26 的电源被切断再恢复后,VLDO 才能恢复正常工作。 这个问题出现在所有电路板上,而不仅仅是单个电路板上,而且当 CAN 通信未进行时不会出现此问题。 问题发生时的状态如下: Vpre 6V O VDIG 1.6VO VBOS 5V O VLDO2 X VLDO1 X VCORE X DFS已通过OTP禁用。 我想了解 FS26 目前的状况以及导致这种情况发生的原因。 Re: FS26 LDO Off Issue 你好kjy106906 再会! 监视程序是否已启用? 以下各项的值是多少: FS_STATES FS_GRL_FLAGS FS_OVUV_REG_STATUS M_REG_FLG 故障发生后立即出现 M_STATUS 吗? 你检查过FS26是否显示任何UV或OV标志吗? 另外,能否分享一下您的 M_STATUS? 希望这些信息对您有所帮助,如果您还需要其他帮助,请告诉我。 祝你今天过得愉快,一切顺利。 Re: FS26 LDO Off Issue @RafaR 感谢您的回复。 遗憾的是,MCU 已从 SBC 获得电源,但由于 VLDO 已关闭,因此无法进行通信。 必须切断并重新接通电路板电源,MCU才能正常工作。 监视窗口是无限的。 Re: FS26 LDO Off Issue 你好 kjy106906 再会! 看起来 FS26 模拟前端仍然通电,但为系统供电的内部电源树已被禁用。 一种可能的解释是,在受监测的调节器(VCORE、VLDO1、VLDO2)中检测到了故障,并且配置的反应禁用了调节器输出。FS26 文档表明,根据配置的故障响应设置,调节器在发生故障后可以保持禁用状态。 希望这些信息对您有所帮助,如果您还需要其他帮助,请告诉我。 祝你今天过得愉快,一切顺利。 Re: FS26 LDO Off Issue db16122_0-1785211448726.png 请参考PMIC初始化过程进行调试。AN13431 NXP 针对 TI TMS570 系列 MCU 的 PMIC 解决方案应该会有所帮助。 Re: FS26 LDO Off Issue 谢谢 @RafaR 这是一个重要的问题,所以我希望您能回复。 我想确切地了解 FS26 的状态以及它失败的原因。 问题发生时,我使用外部工具读取了寄存器。 FS26 [FS_STATES:0x17]R:0x0009; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MIRRORCMD:0x1c]W:0x001d; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MIRRORDATA:0x1d]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [ID_VOTP:0x1D]R:0x00 FS26 [FS_WDW_DURATION:0x0b]W:0xd08b; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_NOT_WDW_DURATION:0x0c]W:0x2f74; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_FLG:0x07]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_MSK:0x08]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_FLG:0x05]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_MSK:0x06]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_FLG:0x03]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_MSK:0x04]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_FLG:0x09]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_MSK:0x0a]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_STATUS:0x02]R:0x5020; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_FLG:0x0b]R:0x0005; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_MSK:0x0c]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_OVUV_REG_STATUS:0x10]R:0x1544; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_INTB_MASK:0x16]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY1:0x14]R:0x03c3; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY2:0x15]R:0x0010; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_SAFE_IOS_1:0x12]R:0xf000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_STATES:0x17]R:0x0009; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_GRL_FLAGS:0x00]R:0x5000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_DEVICEID:0x00]R:0x65d8; CRC[MOSI:0x00; MISO:0x00] FS26 [M_PROGID:0x01]R:0x0105; CRC[MOSI:0x00; MISO:0x00] FS26 [M_STATUS:0x02]R:0x5020; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_FLG:0x03]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_MSK:0x04]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_FLG:0x05]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_MSK:0x06]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_FLG:0x07]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_MSK:0x08]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_FLG:0x09]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_MSK:0x0a]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_FLG:0x0b]R:0x0005; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_MSK:0x0c]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_SYS_CFG:0x0d]R:0x0001; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_CFG:0x0e]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_CFG:0x0f]R:0x0002; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_CFG:0x10]R:0x0202; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_CTRL1:0x11]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_AMUX_CTRL:0x13]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CFG1:0x14]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CFG2:0x15]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CFG3:0x16]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CTRL:0x17]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MEMORY0:0x18]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MEMORY1:0x19]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_GRL_FLAGS:0x00]R:0x5000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_WDW_DURATION:0x0b]R:0xd08b; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_NOT_WDW_DURATION:0x0c]R:0x2144; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_WD_TOKEN:0x0e]R:0x5ab2; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_ABIST_ON_DEMAND:0x0f]R:0x0040; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_OVUV_REG_STATUS:0x10]R:0x1544; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_SAFE_IOS_1:0x12]R:0xf000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_SAFE_IOS_2:0x13]R:0x035f; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY1:0x14]R:0x03c3; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY2:0x15]R:0x0010; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_INTB_MASK:0x16]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_STATES:0x17]R:0x0009; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_LP_REQ:0x18]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_LDT_LPSEL:0x19]R:0x0000; CRC[MOSI:0x00; MISO:0x00] 当出现问题时,我会附上波形图。 kjy106906_0-1785205262839.png 蓝色 VSUP / 红色 VBOS / 绿色 RSTB / 黄色 VDIG kjy106906_1-1785205354126.png 蓝色 VSUP / 红色 VPre / 绿色 Vcore / 黄色 RSTB
查看全文