2396708_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2396708_en-US

2396708_en-US

S32K3X8EVB-Q289 Power Supply Question

I bought the S32K3X8EVB-Q289 board and need to purchase a power cable separately. Should I buy a power adapter with 12V 2A or higher? Or is there a product recommended by NXP?

The FRDM-A-S32K358 uses a USB Type-C port, so it was sufficiently powered by a laptop's USB port,

Re: S32K3X8EVB-Q289 Power Supply Question

Hello @wj_kwak,

Yes, as noted inside the S32K3X8 EVB HW UM, you can use any external power supply as long as it provides +12V/≥2A;

Julin_AragnM_0-1784565662949.png

Best regards,
Julián

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-21-2026 04:32 AM
更新者: